Hello Martin
I have read the link: https://community.nxp.com/thread/382735
chip number is PPC5775KMMY3 2N76P CTEZR1622B
I tried both DEAD_DEED_FADE_BADE and FEED_FACE_CAFE_BEEF, it still appears.


Power cycle part:
I tried to turn the power supply off and on by POWER-SW (with DC supply) on the Motherboard, and it didn’t work.
There are something confusing.I only connect the JTAG debugger and it seems to power the board. Does it make the power cycle failed (when I use DC power supply on motherboard to doing the power cycle ) because it always power the board? Also, the red LED D9 is always on. Is there any problem with the board or debugger?

Regards
Hai