An error occurred when adding the S32K3 Real-Time Drivers Update Sites in S32 Design Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

An error occurred when adding the S32K3 Real-Time Drivers Update Sites in S32 Design Studio

5,739 Views
Panpan
Contributor I

Hi Team,

An error occurred when adding the S32K3 Real-Time Drivers Update Sites(SW32K3_RTD_4.4_2.0.3_DS_updatesite_D2302.zip) in S32 Design Studio(V3.5), as shown below:

Panpan_0-1679023820774.png

Looking forward to your replay.

Thanks.

0 Kudos
Reply
10 Replies

5,721 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Panpan 

S32K3 RTD v.2.0.3 is delivered as an Update Site for S32 Design Studio "S32 Design Studio IDE v3.4 Update 3".

 

B.R.

VaneB

0 Kudos
Reply

5,709 Views
Panpan
Contributor I

Hi VaneB,

Might I ask a question?

How to install S32K3 Real-Time Drivers for S32 Design Studio IDE v3.5?

 

Best Regards.

0 Kudos
Reply

5,693 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Panpan 

I suggest you download the S32DS v.3.4. If you still want to use v.3.5, take a look at the below community posts:

0 Kudos
Reply

5,684 Views
Panpan
Contributor I

Hi @VaneB 

 

Thank you for your help.

I have installed the S32DS v.3.4. 

An error occurred when building the S32K344_HSE_OTA(SW32K3_OTADEMO_0.8.0) project, it seems to be missing the StandardTypes.h/S32K344_MU.h/Compiler.h etc. file, where can I find these file? or do you know the solution?

Panpan_0-1679466882359.png

 

Looking forward to your reply.

Best Regards.

0 Kudos
Reply

5,661 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Panpan 

For the S32K344_HSE_OTA project, you must have installed the Real Time Drivers v1.0.0 in S32DS v.3.4 and the S32K344 with AB_SWAP HSE firmware.

To run the project:

  1. Import the project to your S32DS workspace (File -> Import... -> General -> Existing Projects into Workspace)
  2. Build the project (right-click on project name -> Build project)
  3. Go to Run/Debug and select the desired debug configuration, and click on Launch.
  4. The PRACTICE script will halt the code at main().
  5. Type Go and enter
  6. Code will halt at Random Number Generation Demo (Demo_RandomNumberGeneration())
  7. Type Go and enter (to execute demo)
  8. Code will halt at Key Provisioning Demo (Demo_KeyProvisioning())
  9. Type Go and enter (to execute demo)
  10. Code will halt at Authentication Demo (Demo_Authentication())
  11. Type Go and enter (to execute demo)
  12. Code will halt at Symmmetric Cipher Demo (Demo_SymmetricCipher())
  13. Type Go and enter (to execute demo)
  14. Code will halt at Hash Demo (Demo_Hash())
  15. Type Go and enter (to execute demo)
  16. Code will halt at OTA Update Demo (Demo_OtaUpdate())
  17. Type Go and enter (to execute demo)
  18. Type CONTINUE to execute the practice script.
  19. RESET is issued to the device, and the OTA Update application will execute.
0 Kudos
Reply

5,650 Views
Panpan
Contributor I

Hi @VaneB 

 

Sorry to bother you, I have anther question to ask you.

For the S32K344_HSE_OTA project, it indicates the HW requires the S32K3XXEVB-Q172 and P&E debug tool. Where and how the P&E debug tool can be bought?

And how the Trace32 and Multi GHS software can be downloaded?

 

Looking forward to your reply.

Best Regards.

0 Kudos
Reply

5,634 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Panpan 

If you are using an EVB, it includes two options for debugging. You can connect a debugger to the 20-pin Cortex Debug D ETM Connector with TRACE or the 10-pin Cortex Debug JTAG Connector (depending on your board) and the on-board S32K3 debugger (see the below image).

 

VaneB_1-1679614353779.png

Also, I attached some links to HOWTOS that will be useful for you.

0 Kudos
Reply

5,620 Views
Panpan
Contributor I

Hi @VaneB 

 

Thank you for your reply.

I am planning to buy the S32K3X4EVB-T172 evaluation board, I need to purchase the TRACE connector from the third party. Right?

And is there a soft simulation environment for S32K3X4?

 

Best Regards.

0 Kudos
Reply

5,610 Views
VaneB
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

5,653 Views
Panpan
Contributor I

Hi @VaneB 

 

Thank you for your help, I solved the problem.

 

Best Regards.

0 Kudos
Reply