S32 Design Studio知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio Knowledge Base

讨论

排序依据:
Function printf is C library function, which sends formatted output to stdout. Because microcontroller does not contain stdout, it it necessary to redirect it to a different type of output. One of the possible way is using UART. All MPC57xx has LinFlexD module, which supports UART mode.   For proper use the LinFlexD module, it is necessary to initialize it and also create simple functions for transmit and receive data. You can create your own file or use the file uart.c in the attachment. If you want to create your own file, please do not forget to implement the methods, which are called by MW MSL libraries to perform console IO (please look at the attached file uart.c).   In uart.h file, you will find correct function prototypes for functions used in uart.c and also some important enum data types.   Third important file is uart_console_io.c which you find in folder, where S32DS was installed. Open the folder and choose path: S32DS/e200_ewl2/EWL_C/src/sys. This file contains routines which implement low-level console IO routines.   Now, we have all basic files which help us to use printf function. So lets create new project and test printf. Example project is created for MPC5744P.   Create new project, choose EWL library and finish project wizard. Include stdio.h to the file, where you want to call printf function.   Now add uart.c and uart_console_io.c files to the project folder src. Add uart.h file to project folder include.   Initialize system clock and clock for peripherals (look at the attached project). In uart.c file, there are settings for GPIO pins, LinFlex initialization for UART mode and also baud rate calculation (please look at the uart.c file in the attachment).   Now it is possible to use printf function. Important point is, that \n character triggers the data sending. Also, if you do not use this \n character, you will get compile error, but I will explain this further in this tutorial.   Run some terminal emulation, for example Putty and use the following settings:   Now open terminal and  run the code in the microcontroller. This should be the result:   /*************************************************************************************************************************************************************************************/ /*************************************************************************************************************************************************************************************/ /*************************************************************************************************************************************************************************************/   This was the easiest way, how to use printf function. But printf also provides some format characters for printing decimals, floating points, etc. All options you can find in ewl_c_reference.pdf document which is place in S32DS installation folder S32DS/help/pdf.   When you want to use some of the characters mentioned above, you get the following compile error:   When you do not use any format characters in printf argument, function _EWL_CDECL puts(const char_t * s) from puts.c file is called on background. But when you use format characters in printf argument, function int_t _EWL_CDECL printf(const char_t * _EWL_RESTRICT format, ...) from printf.c file is called instead of puts.   Variable result saves value, which function __pformatter returns. But function __pformatter is not implemented. Instead of __pformatter, function __pformatterFP (placed in __printformat.c file) is implemented.   So there are two possible workarounds.   First workaround is place the following code to the Linker flags in project properties: -Xlinker --undefined=__pformatterFP -Xlinker --defsym=__pformatter=__pformatterFP   The code says that there is undefined symbol __pformatterFP (part -Xlinker --undefined=__pformatterFP) and define symbol alias __pformatter=__pformatterFP (-Xlinker --defsym=__pformatter=__pformatterFP ). So from my point of view, symbol __pformatter is replaced by __pformatterFP. Now the correct function is called and the project could be successfully built.     Second workaround is add the printf.c file from S32DS installation folder S32DS/e200_ewl2/EWL_C/src/stdio to the project src folder and exchange __pformatter for __pformaterFP. Clean project and recompile.       I hope this document helps you while implementing printf function in your projects.   Regards, Martin
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM 2018.R1  Update 1          What is new? This update adds device support for S32K116  and installs the S32 SDK 1.8.7 EAR (Early Access Release) supporting the S32K116 (see attached S32K116 SDK release notes for more details) S32K116 EAR SDK v1.8.7 Examples - "Create S32DS Project from Example" Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 8          What is new? S32 SDK for Power Architecture 1.8.0 EAR supporting MPC5777C, MPC5775B, MPC5775E, MPC5746R, MPC5745R, MPC5743R This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7 ). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
查看全文
To prepare an SD card for a Linux boot, it is necessary to connect the SD card to a machine with Linux OS. If a Linux OS machine is not available, then a virtual machine installed to a Windows OS machine may be used. If you have access to a Linux OS machine, skip to step 4. Procedure 1) Download and install a virtual machine VMware Workstation Player Virtual Box 2) Download Ubuntu. This tutorial uses the Ubuntu version 14.04.5.  The image will be ubuntu-14.04.5-desktop-amd64.iso. 3) Launch VMware or Virtual Box and create a new virtual machine Use downloaded Ubuntu image when requested for installer disc image file Hit Next and select Linux as the guest operating system and select Ubuntu for the version. Hit Next and name your virtual machine and specify where you want to store it. Increase the disk size to 40 GB Hit Finish and install VMware Tools for Linux, if asked 4) Within C:\NXP\S32DS_Vision_v2.0\S32DS\s32v234_sdk\os extract 'build_content.tar.gz', then extract 'build_content.tar' and navigate to the 'v234_linux_build' folder 5) Start virtual machine May need to manually connect USB-mounted SD card reader Log in to virtual machine 6) In files, go to 'Home' directory and create a folder "VSDK" 7) Within VSDK folder, copy the files image, u-boot.s32, s32v234-evb.dtb, and rootfs.tar from the 'v234_linux_build' folder.  Note: The file s32v234-evb.dtb and u-boot.s32 will have names with XXXXX-suffix for the schematic number printed on the evaluation board (EVB) you are using. Be sure to use the files which correspond to your EVB. 😎 Load the card into the reader. If you are using a virtual machine, it is recommended to use a USB adapter instead of a built-in reader in the PC. 9) Within the virtual machine, launch the terminal program 10) Within the terminal program, enter command 'cat /proc/partitions' to view the names of the partitions and identify the names of the partitions on your SD card. Perhaps it is named 'sdb'. 11) Delete all existing partitions.    a) Enter command 'sudo fdisk /dev/sdb'.    b) Enter command 'd' and then the number of the partition to delete. Repeat as necessary until all partitions have been deleted 12) Create new partitions    a) Enter command 'n' for new    b) Enter 'p' (or just hit <enter>, as this is the default) for primary    c) Enter '1' (or just hit <enter>, as this is the default) for partition number 1.    d) Press <enter> to select the default value for the First sector    e) Enter '+255M' to set the size    b) Enter command 'n' again, for partition number 2, however, press <enter> to select the default value for the 'Last sector' 13) Set the partition type    a) Enter command 't' for type    b) Enter '1' for partition number 1    c) Enter 'c' for partition type FAT32    d) Enter command 't' again, for partition number 2, however, enter '83' for partition type LINUX If you get error 16: Device or resource busy, as shown above, use commands 'umount /dev/sdb1' and 'umount /dev/sdb2' to free the pre-existing partitions. Then try again and should be ok now 14) Write the new configuration, enter 'w' 15) Try to setup the filesystems. Enter 'sudo mkfs.vfat -n boot /dev/sdb1'. If you get the error '/dev/sdb1 contains a mounted filesystem', you will need to unmount the partition first. To save time, unmount both /dev/sdb1 and /dev/sdb2. Enter 'umount /dev/sdb1' and then 'umount /dev/sdb2' Now try 'sudo mkfs.vfat -n boot /dev/sdb1' again 16) It worked, so now enter 'sudo mkfs.ext3 -L rootfs /dev/sdb2'. It will take a minute or two for this to complete. Wait until you get the command prompt again. 17) Now it's time to load the BSP content from the VSDK. But first, change the directory to the one we created earlier for the BSP files. Enter 'cd /home/user/VSDK' or 'cd VSDK'. Enter the following commands: sudo dd if=u-boot.s32 of=/dev/sdb bs=512 seek=8 conv=fsync sudo cp Image /media/user/boot sudo cp s32v234-evb.dtb /media/user/boot 18) Now we need to extract the root filesystem, change the directory to its location 19) Enter command 'sudo tar -xvf /home/user/VSDK/rootfs.tar' 20) Once the files are extracted, enter command 'sync'   Now the SD card is ready to be used in the S32V234-EVB.
查看全文
Installation & Activation HOWTO: Install Lauterbach TRACE32 debugger plug-in into S32 Design Studio HOWTO: Install IAR Eclipse plug-in into S32 Design Studio for ARM  HOWTO: Activate S32 Design Studio     Getting Started HOWTO: Create a New Project in S32 Design Studio for ARM  HOWTO: Create S32DS Project from Example 'Hello World' for S32K144 (w/o SDK)    Build tools & Standard libraries  HOWTO: Build a Project and Setup a Debug Configuration for debugging in S32 Design Studio  HOWTO: Add a static library file into S32 Design Studio GCC project HOWTO: Place custom data into flash memory  HOWTO: Link a binary file(s) into the application project using GNU build tools HOWTO: Execute a library function from RAM memory using GNU build tools  NEW!   Debug  & Flash Programming HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio  HOWTO: Update OpenSDA Firmware on EVB Using GDB Server Monitor Commands from Eclipse GDB Console  HOWTO: Debug multiple elf files in S32 Design Studio with GDB  HOWTO: Reset MCU in S32 Design Studio debugger (Pemicro/OpenSDA interface) Debugging the Startup Code with Eclipse and GDB | MCU on Eclipse   https://community.nxp.com/docs/DOC-345344  HOWTO: Program multiple memory types in single debug session NEW!   S32 SDK & Other SDKs HOWTO: Create FreeRTOS project in S32 Design Studio How to change package on S32DS Processor Expert  HOWTO: Create the Blinking LED example project using S32K144 SDK  HOWTO: Show FreeRTOS Threads in Eclipse Debug View with Segger J-link and NXP S32 Design Studio  Tutorial: FreeRTOS 10.0.1 with NXP S32 Design Studio 2018.R1  Using custom FreeRTOS with S32K SDK and OSIF for ARM | MCU on Eclipse  Implementing FreeRTOS Performance Counters on ARM Cortex-M | MCU on Eclipse  HOWTO: Change the CPU Derivative in an SDK-Based Application Project  HOWTO: Working with AMMCLib SDKs  HOWTO: Working with FreeMASTER SDKs  HOWTO: Add custom SDK into existing project   HOWTO: Use SDK based example code as standalone (usable for GIT, SVN...)  NEW!   General Usage HOWTO: S32 Design Studio Command Line Interface  HOWTO: Add user example into S32DS HOWTO: Generate S-Record/Intel HEX/Binary file  HOWTO: Update S32 Design Studio  HOWTO: Set project optimization level  HOWTO: Export S32DS Project to IAR EW (S32K14x/S32K11x)  NEW!   Troubleshooting Troubleshooting: PEmicro Debug Connection: Target Communication Speed  Troubleshooting: Indexer errors on header file  S32 Design Studio Offline activation issue hot fix  Troubleshooting: Installer rolls back immediately following activation code entry  Troubleshooting: Activation fails with error message FNP ERROR 0 
查看全文
This document explains how to change the package of a processor expert project, for example, from S32K144 100LQFP to S32K144 64LQFP.  It does NOT explain how to change processor derivatives (e.g. S32K144 to S32K142). 1. Assuming that the project is opened and active, go to Components Library View and click on Processors     2. Expand the repository folders and double click on your processor (e.g. S32K144) 3. Select new package (e.g.S32K144_64) and click on finish. Now the new variant will be added to your project 4. Go to PinSettings component and click on Switch Configuration. This action will change the pins configuration for new package and will discard the original pin configuration.
查看全文
The list of S32 Design Studio examples has been moved here: https://community.nxp.com/docs/DOC-329623  MPC5644A Example MPC5644A BookE PinToggle - S32DS Power 2017.R1 MPC5744P Example MPC5744P PinToggleStationery S32DS_1.0  Example MPC5744P LINFlex UART with DMA S32DS_1.0  Example MPC5744P ETimerCountMode S32DS_1.0  MPC5777M Example MPC5777M PinToggleStationery S32DS_1.0 Processor Expert RAppID Suite for MPC5777M and S32 Design Studio Integration Multicore Example  MPC5775K Example MPC5775K PinToggleStationery S32DS_1.0  Example MPC5775K-DMA_Transfer S32DS_1.0  Example MPC5775K UART_with_DMA S32DS_1.0  Example MPC5775K-UART_with_Interrupts S32DS_1.0  Example MPC5775K FlexCAN_with_interrupts_v1.1 S32DS_1.1  Example MPC5775K Semaphores S32DS_1.0  Example MPC5775K eTimer_PWM S32DS_1.0  Example MPC5775K ADC_example S32DS_1.0  Example MPC5775K IIC Communication with RTC PCA8565TS/1 S32DS_1.0  Example MPC5775K DSPI_with_interrupts S32DS_1.0  MPC5748G Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0  Example MPC5748G PretendedNetworkingCAN S32DS_1.0  MPC5746R Example MPC5746R FlexCAN_with_interrupts S32DS Example MPC5746R PinToggleStationery - S32DS Power 2017.R1 S32R274 Example S32R274 FlexCAN_with_Interrupts S32DS_1.1  Example S32R274 Watchdog_example S32DS_1.1  Example S32R274 multi-core shared memory - S32DS Power v1.2  MPC5777C Example MPC5777C Single ELF multi-core Pin Toggling - S32DS Power v1.2
查看全文
One of the many great features of the S32DS for Vision is the ability to access the Linux BSP file system on the SD card in the S32V234-EVB. Once connected, you can drag and drop files between your PC and the EVB. Once you have completed HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP and HOWTO: Setup A Remote Linux Connection, you are ready to setup the Remote Systems view to connect to the Linux files system to view and access the file system. 1) Go to 'Window -> Show View -> Other' 2) Expand 'Remote Systems', then select "Remote Systems' and click OK 3) Click 'Define a connection to remote system' button OR right-click in the Remote Systems window and select 'New -> Connection' from the list 4) Select 'SSH Only' 5) Enter the IP address noted from HOWTO: Setup A Remote Linux Connection for Host name and click Finish 6) Right-click on the connection name in the Remote Systems window and select 'Connect' OR expand the folders under the connection name until the login window appears: Connection_name -> Sftp Files -> Root (window appears) 7) Enter "root" for User ID 😎 Click OK 9) The Linux file system is now visible in the Remote Systems window. You can drag and drop files to and from here.
查看全文
Online update In standard situation update can be started by clicking on message box appeared after S32DS Launch: If you don't see such message - you can check for updates/update your S32DS Installation manually. On main menu bar click on Help -> S32DS Extensions and Updates  Select from available items, then click "Install/Update" button  Offline update   Download update package from Updated/Patches (for S32DS 3.x - S32 Design Studio | NXP , for ARM S32DS - S32 Design Studio IDE for Arm® based MCUs|NXP, for Power Architecture S32DS - S32 Design Studio IDE for Power Architecture based MCUs | NXP ). Click on Help -> S32DS Extensions and Updates and choose Go to Preferences.   Click Add... Click Archive... and locate the zip file you downloaded and click OK Select the packages and updates then start the installation with the Install/Update button. 
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 11          What is new? S32K1xx SDK RTM-SR 3.0.2: SBC driver now supports UJA1169 as well as both UJA1168 and UJA1168A SBC variants (S32 SDK release notes) AMMCLIB v.1.1.18 for S32K1xx, KEA and S32V234 (AMMCLIB release notes) This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7, Update 8, Update 9, Update 10  ) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
查看全文
Bare-metal project migration from an older version of S32DS into a newer one is typically pretty straightforward. Despite of that the migration into S32DS Power v1.2+ requires more attention due the fact it includes a new version of GCC compiler + GCC binutils (see the GCC release notes - here). This version of GCC is now fully EABI VLE compliant  (in contrast to previous versions of S32DS Power  v1.0 and v1.1) and it has several consequences for the project migration object code/libraries are not backward compatible - if you have an object code/library built by a previous version of S32DS Power v1.x you have to rebuild it in new S32DS v1.2+ compiler. default compiler setup has changed - bitfield access is not volatile anymore. This may have a impact on a peripheral registers access via standard header file bitfield structures. Such access may require a specific load/store instruction e.g. "stw" but if compiler is allowed to optimize the access (e.g. use "stb" instead of "stw") an exception may occur. Therefore it is recommended to add  -fstrict-volatile-bitfields  flag into your project GCC compiler settings: linker script file (*.ld) requires some additional linker sections - Linker script file in S32DS Power v1.2+ must contain the sections below: •  KEEP for .init and .fini sections • .ctors and .dtors sections • .preinit array .init array and .fini array sections If the linker script file is not updated and the linker warnings are ignored you may experience an exception at the runtime - typically when __init routine is executed. Missing .init section causes that an invalid instructions is fetched and causes the core IVOR exception. There is an easy way how to automatically fix the linker script file issue directly in IDE. If you import and build an older project in S32DS Power v1.2 the linker issues these linker script related warnings: Right click on the warning and select Quick Fix: Select "Add missed section in linker script"  + "Select All" and press "Finish". Repeat these steps until all the linker script warnings disappears. If you don't use IDE project you have to add the sections below into your linker script manually: .text_vle : { INPUT_SECTION_FLAGS (SHF_PPC_VLE) *(.text.startup) *(.text) *(.text.*) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(16); } > m_text /* that will force pick VLE .text sections */ .ctors : { __CTOR_LIST__ = .; /* gcc uses crtbegin.o to find the start of the constructors, so we make sure it is first. Because this is a wildcard, it doesn't matter if the user does not actually link against crtbegin.o; the linker won't look for a file to match a wildcard. The wildcard also means that it doesn't matter which directory crtbegin.o is in. */ KEEP (*crtbegin.o(.ctors)) KEEP (*crtbegin?.o(.ctors)) /* We don't want to include the .ctor section from from the crtend.o file until after the sorted ctors. The .ctor section from the crtend file contains the end of ctors marker and it must be last */ KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)) KEEP (*(SORT(.ctors.*))) KEEP (*(.ctors)) __CTOR_END__ = .; } > m_text .dtors : { __DTOR_LIST__ = .; KEEP (*crtbegin.o(.dtors)) KEEP (*crtbegin?.o(.dtors)) KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)) KEEP (*(SORT(.dtors.*))) KEEP (*(.dtors)) __DTOR_END__ = .; } > m_text .preinit_array : { PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); } > m_text .init_array : { PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); } > m_text .fini_array : { PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); } > m_text‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ This may help you to avoid time consuming debugging to figure out the root cause of the core exception. 
查看全文
This application shows how to  build and debug BOOKE based project. It contains BOOKE startup/ISR code and it is compiled to generate non-VLE BOOKE code. Note: Before running this project please make sure your startup script is configuring MMU to use BOOKE instructions. The script is typically located here: "c:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.3.201803261737\win32\gdi\P&E\s32e200_mpc564xa.mac" The plugin version folder may differ. The updated script is part of attached ZIP archive.
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 7          What is new? MPC574xx SDK BETA 1.9.0 S32R SDK BETA 1.9.0  Radar SDK for S32R274 & S32R372 RTM 1.1.1 AMMCLib 1.1.13 for MPC560xB, MPC560xP, MPC564xL, MPC567xF, MPC567xK, MPC574xC, MPC574xG, MPC574xP, MPC574xR, MPC577xC, MPC577xK,  MPC577xM This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power v1.2, Update 1 1            What is new? The S32 Software Development Kit (S32 SDK v0.8.0 EAR) which is an extensive suite of peripheral drivers, RTOS, stacks and middleware designed to simplify and accelerate application development on NXP Power MPC5748G and MPC5746C microcontrollers. Release notes are available here: http://www.nxp.com/docs/en/release-note/C55_SDK_EAR_0.8.0-RN.pdf  Installation instructions The update is available for online (Eclipse Updater) or offline (direct download link) installation.   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_2/com.freescale.s32power.updatesite  select all available items and click "Next" button offline installation: go to S32 Design Studio product page -> Downloads section or use the direct download link to download the "S32 Design Studio for Power v1.2 - Update 1" file.   Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 1 archive file: Select all available items and click "Next" button.
查看全文
The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the ability to access the flash programming and debugging of the S32 Debug Probe via GDB command line. This document provides only the necessary commands specific to launching a debug session on NXP devices. It does not cover general GDB command line operations, these are covered in detail in the GNU communities and other public websites which are not associated with NXP.   Preparation Setup the software tools Install S32 Design Studio for S32 Platform  Install the Development Package for the device you are debugging. In this case, the S32R45 development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for initialization of the cores.   Setup the hardware Confirm the setup of the S32R45 evaluation board.  Connect the power supply cable Setup the S32 Debug Probe. Refer to the S32 Debug Probe User Manual for installation instructions. Connect the S32 Debug Probe to the evaluation board via JTAG cable.   Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard.   Procedure As separate debug threads need to be started for each core to be debugged, and the method for launching a debug thread differs depending upon whether it is a primary core or secondary core and if the executable image will be loaded or if the executable is already running and the debugger just needs to be attached. These scenarios will be covered by the following 3 sections: Primary Core Load Image and Run: The application image will be loaded directly to memory by the debugger and then initialized and started. The primary core will launch any secondary cores used by the application. Secondary Cores: The primary core has launched a secondary core, it is now running and the debugger will connect through the attach method. Primary Core Image Already In Memory and Running: The primary core has already been initialized and launched by other means, such as via a Linux OS on the target, so the debugger will connect through the attach method without initializing or loading the image to memory.   Please proceed with the section which applies to the core for which you are starting a debug thread.   Primary Core Load Image and Run Prepare the initialization script for the core(s) to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r45\s32r45_generic_bareboard_all_cores.py Uncomment the following lines: # _JTAG_SPEED = 50 # _PROBE_IP = "10.81.18.242" # _GDB_SERVER_HOST = 'localhost' # _GDB_SERVER_PORT = 45000 # _CORE_NAME = 'A53_0' # _RESET_TYPE = "default" # _RESET_DELAY = 1 # _REMOTE_TIMEOUT = 100 # _IS_LOGGING_ENABLED = True This file is used by the S32 Debugger within the S32 Design Studio IDE where the settings are provided from the GUI, so these lines are commented out in order to allow the GUI settings to have control. The commented lines are provided so the script could more easily be run by the command line method. Update the IP address line (_PROBE_IP) to match the IP address of the S32 Debug Probe which is connected to your PC. See the user guide for the S32 Debug Probe for details on how to obtain the IP address. Update the core name (_CORE_NAME), if necessary. See s32r45_context.py for complete list of supported cores. Save the file with a new name to preserve the original. For example, s32r45_gen_bb_all_c_my_probe.py. This ensures the S32 Debugger will still function correctly. Launch GTA server. From command prompt or Windows File Explorer run the command: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe  Should see a window appear like this:   Ensure Environment Variable for Python is set. From command prompt, run the command:  set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages   Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32)  OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window:   From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r45\\s32r45_gen_bb_all_c_my_probe.py This specifies the script for initialization. py board_init() This initializes the board. It should only be called for the initial core. In a multicore debugging workflow, the debugger launch for additional cores would omit this step. py core_init() This initializes the core specified in the initialization script in step 1. Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\ New_S32R_Project_M7_0\\Debug_RAM\\ New_S32R_Project_M7_0.elf load   Secondary Cores After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. Some additional steps will need to be performed from within the primary core GDB session, enter the following commands: set *0x34100000 = 0x34200000  set *0x34100004 = 0x34100025 set *0x34100024 = 0xFFFEF7FF set *0x34200000 = 0x34300000 set *0x34200004 = 0x34200025 set *0x34200024 = 0xFFFEF7FF b main c These lines prepare the environment for launching debugging on secondary cores. This will allow for multicore debugging in the case of separate ELF files for each core. These can be found in the Run Commands field of the Startup tab on the Debug Configuration for the primary core within S32 Design Studio IDE, of any multicore project created from the New Application Project Wizard. Note: If there is just one ELF file for all cores, then these 'set *0x... = 0x...' commands should be skipped. In general, it will be correct to set the break-point at main, as shown, but this might need to be changed depending on when the secondary cores are started within the project. Prepare the initialization script for the secondary core to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r45\s32r45_attach.py This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running. Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core Uncomment the following lines: #_JTAG_SPEED = 14000 #_GDB_SERVER_PORT = "127.0.0.1:45000" #_RESET_TYPE = "default" #_PROBE_IP = "s32dbg:10.222.24.64" #_CORE_NAME = 'M7' #_RESET_DELAY = 1 #_CMD_TIMEOUT = 7200 Make the following changes to the lines: _JTAG_SPEED = 14000 ->  None _GDB_SERVER_PORT = "127.0.0.1:45000" -> 45000 _RESET_TYPE = "default" _PROBE_IP = "s32dbg:10.222.24.64" -> None _CORE_NAME = 'M7' -> 'M7_1' (this should be set to match the name of the core to be debugged, see s32r45_context.py for complete list) _RESET_DELAY = 1 -> _REMOTE_TIMEOUT = 60 (add this line) _CMD_TIMEOUT = 7200 -> _IS_LOGGING_ENABLED = True (add this line) Save the file with a new name to preserve the original. For example, s32r45_attach_my_probe_core1.py. This ensures the S32 Debugger will still function correctly. The existing GTA server is used, so do not launch a new one. Open an new command window and follow similar steps as done for the primary core. Setup the Python environment variable, if not done globally set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Start GDB {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) A (gdb) prompt should now be displayed in the command window: From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r45\\s32r45_attach_my_probe_core1.py This specifies the script for initialization. We will not execute the py board_init() as this was already done for the primary core. py core_init() This initializes the core specified in the initialization script in step 2. Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\S32R45_Multicore\\S32R45_Multicore_M7_1\\Debug_RAM\\S32R45_Multicore_M7_1.elf load Repeat 3-6 for each additional core.   Primary Core Image Already in Memory and Running The core is running and does not need to be initialized. Prepare the initialization script for the core to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r45\s32r45_attach.py This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running. Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core Uncomment the following lines: #_JTAG_SPEED = 14000 #_GDB_SERVER_PORT = "127.0.0.1:45000" #_RESET_TYPE = "default" #_PROBE_IP = "s32dbg:10.222.24.64" #_CORE_NAME = 'M7' #_RESET_DELAY = 1 #_CMD_TIMEOUT = 7200 Make the following changes to the lines: _JTAG_SPEED = 14000  _GDB_SERVER_PORT = "127.0.0.1:45000" -> 45000 _RESET_TYPE = "default" _PROBE_IP = "s32dbg:10.222.24.64" -> (enter the IP address of your probe) _CORE_NAME = 'M7' -> 'M7_0' (this should be set to match the name of the core to be debugged, see s32r45_context.py for complete list) _RESET_DELAY = 1 -> _REMOTE_TIMEOUT = 60 (add this line) _CMD_TIMEOUT = 7200 -> _IS_LOGGING_ENABLED = True (add this line) Save the file with a new name to preserve the original. For example, s32r45_attach_my_probe_core0.py. This ensures the S32 Debugger will still function correctly.   Launch GTA server. From command prompt or Windows File Explorer run the command: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe Should see a window appear like this:   Ensure Environment Variable for Python is set. From command prompt, run the command: set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages   Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window:   From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r45\\s32r45_attach_my_probe_core0.py This specifies the script for debugger initialization. Do not execute the py board_init() as this will initialize the board, and reset the currently executing application, which is not desired for this case. py core_init() This initializes the debugger connection to the core specified in the initialization script in step 1.   Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\S32R_Multicore\\S32R_Multicore_M7_0\\Debug_RAM\\S32R_Multicore_M7_0.elf load   After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. See section ‘Secondary Cores’ for each additional core to be debugged.
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 3.1  Update 2          What is new? S32 SDK for S32S247TV EAR 0.8.1 - be installed on top of the previous EAR 0.8.0 This is a cumulative update -  it includes all the content of previous updates (Update 190508 , Update 190708 ) This update is ONLY applicable to S32 Design Studio 3.1 (DO NOT APPLY IT TO S32 Design Studio 3.2 or later) Installation instructions The update is available only via offline installation (direct download link)  offline installation:   go to S32 Design Studio product page -> Downloads section or use direct link to download the update archive zip file Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates" Add a new "Add.." S32DS Software Site and browse to select the downloaded update archive .zip file you downloaded in the previous step          Select from available items and click "Install/Update" button. This will start the update installation process.
查看全文
Version of MPC5777C Bootloader .rbf file for BookE (non-VLE) applications  + Supported UART0/eSCI_0(J20 on DB): GPIO89-90 pins(Speed: 115200b/s) + Supported  MCAN0(J5 on MB):  GPIO83-84 pins(Speed: 500Kb/s) + BookE (Non-VLE) code 
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 3          What is new? S32 SDK 1.8.8 EAR (Early Access Release) for S32K118. This is a cumulative update - it includes all the content of previous updates ( Update 1, Update 2) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 5          What is new? Service Pack WCT101xS. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
查看全文
UART0 communication is supported in the latest version of MPC5746R Bootloader .rbf file (attached below) + Supported UART0/LINFlexD_0: PD13-PD14 pins(Speed: 115200b/s)   Tested on the dev boards:   Development Board MPC5746R-252DC MPC57xx-MOTHERBOARD Processor PPC5746RTMMT5 - 1N83M  
查看全文