S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
The document describes the steps that need to be done in order to place and execute a library function from a custom memory section - typically RAM using GNU Build tools. The instructions are applicable to any GNU tool-chain. It is demonstrated on a New S32DS Project created in S32 Design Studio for ARM. Lets assume that we'd like to execute memcpy() function from the standard library (NewLib). 1) The first step is to exclude specific library object file(s) from the input section (using EXCLUDE_FILE) so they will not be linked into the standard .text* flash section.  The input section associated with EXCLUDE_FILE shall not interfere with the same input section used later in section list (e.g. with *(.text*) input section deleted from the list below). EXCLUDE_FILE in behaves the same was as *.(text*) rule - it only exclude selected file(s) but places all the remaining (non-excluded) input data. /* The program code and other data goes into internal flash */ .text : { . = ALIGN(4); *(.text) /* .text sections (code) */ /* Exclude file(s) from NewLib libc.a from .text.* section */ *(EXCLUDE_FILE (*libc.a:lib_a-memcpy-stub.o) .text*) *(.rodata) /* .rodata sections (constants, strings, etc.) */ *(.rodata*) /* .rodata* sections (constants, strings, etc.) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(4); } > m_text‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 2) Now let's place the memcpy object into a code_ram section which is already defined in the project .ld file. This section is dedicated to a code that shall be executed from RAM (startup routine initializes this section). For more details see HOWTO: Run a routine from RAM in S32 Design Studio  . The following line places the code (.text* section) from the object file (lib_a-memcpy-stub.o) from the standard NewLib (libc.a)  *libc.a:lib_a-memcpy-stub.o (.text*)‍ into .code section: .code : AT(__CODE_ROM) { . = ALIGN(4); __CODE_RAM = .; __code_start__ = .; /* Create a global symbol at code start. */ __code_ram_start__ = .; *(.code_ram) /* Custom section for storing code in RAM */ *libc.a:lib_a-memcpy-stub.o (.text*) /* add memcpy from the NewLib library here*/ . = ALIGN(4); __code_end__ = .; /* Define a global symbol at code end. */ __code_ram_end__ = .; } > m_data‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ After building the project you can check the map file to confirm memcpy is indeed placed into .code section in RAM memory: .code 0x1fff881c 0x18 load address 0x00000d90 0x1fff881c . = ALIGN (0x4) 0x1fff881c __CODE_RAM = . 0x1fff881c __code_start__ = . 0x1fff881c __code_ram_start__ = . *(.code_ram) *libc.a:lib_a-memcpy-stub.o(.text*) .text.memcpy 0x1fff881c 0x16 C:/NXP/S32DS_ARM_v2018.R1/Cross_Tools/gcc-6.3-arm32-eabi/arm-none-eabi/newlib/lib/thumb/v7e-m\libc.a(lib_a-memcpy-stub.o) 0x1fff881c memcpy 0x1fff8834 . = ALIGN (0x4) *fill* 0x1fff8832 0x2 0x1fff8834 __code_end__ = . 0x1fff8834 __code_ram_end__ = . 0x00000da8 __CODE_END = (__CODE_ROM + (__code_end__ - __code_start__)) 0x00000da8 __CUSTOM_ROM = __CODE_END‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Note If you are placing a function into RAM always consider to add sub-functions called by that function (typically located in a different object file).
View full article
The attached file is an example project based on KEA128 for LED flashing by toggle GPIO signals. It was developed   on S32 Design Studio for ARM 1.0.
View full article
On reset, all module registers have default values. These settings are typically not ideal for achieving optimal system performance. Also, some peripherals must be configured before they can be used. DCD is the configuration information contained in the DCD image that BootROM uses to configure peripherals on the device. BootROM determines the location of the DCD table from the associated pointer in the IVT.   The main functionality of the DCD Tool is to generate the Device Configuration Data (DCD) image using the format and constraints as specified in the Boot ROM reference manual.   In the steps below, an example process for creating the DCD binary for initializing SRAM is shown. To initialize the SRAM, a logic '1' must be written to the INITREQ bit within the PRAMCR register of the SRAMC and SRAMC_1 peripherals.   Procedure With a project open in project explorer (C/C++ perspective), switch to DCD perspective. Click on the arrow next to the 'Open S32 Configuration' button and select 'Open DCD'. Check that correct project is selected  In DCD Commands panel, select Command Type 'Write', then click 'Set' Click 'Add Register', then set the following settings. Can start typing the names to filter the list for faster setting selection.   For Peripheral setting, select 'SRAMC'. You can search for it by typing the name. Register setting, select 'PRAMCR'. The list is short, so it is not necessary to type the name. In Bitfields, select 'INITREQ' Now click on the highlighted bit to set it. Again using 'New Command' box, repeat settings of steps 3 & 4, however, this time select Peripheral 'SRAMC_1'. If everything was done correctly, in the DCD Binary panel to the right, should appear as shown. If so, click 'Export'. The generated DCD file will be displayed. By default, C format is selected. Select Binary format and click OK. Select a location to save the file (such as the project folder in the workspace directory) and give it a meaningful name. Click Save. You are done! DCD image file is created in binary format and ready to be imported to IVT Tool.  
View full article
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using either the A53 or the TEST_A53 build options. 3) The project is now built and the ELF file is ready to be loaded to the EVB for execution. Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234). Start A53 Debug 4) Select the debug drop-down menu and click Debug Configurations     5) Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 4 is selected (points to the IP address of your EVB). Click Debug     6) The first time you connect to a new IP address (i.e. the first time you debug after creating a new workspace), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts. You may get an error message on the first try, this is normal. Just try it again and it will work. 7) Once the Linux GDB has started on A53 core and the initial breakpoint is reached in main(), we need to set a breakpoint at the function apu_hal_Enable().    This breakpoint has already been created for you, you just need to enable it! Locate the breakpoint in the Breakpoints view. Due to some known issues with Eclipse CDT, it is necessary to enable->disable->enable the breakpoint so it will work properly. The issue only affects this breakpoint, due to the way it is provided, and will not affect breakpoints which you set elsewhere in the code. 😎 Press Resume twice, so that the breakpoint which was set at apu_hal_enable() is reached for the 2nd time. 9) Open Debug Configurations. You will see a debug configuration within the 'S32 Debugger' group (FAST9COLOR as shown below). This is the debug configuration we will use, however, it will require some setup.     10) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.       11) Click Apply then Debug. It may take a few moments for the APEX core debug to launch.   12) It may take a moment or two before the APEX2 debug thread launch is complete, see the Thread listed within the <kernel_name>[S32 Debugger] in the Debug window. Also note, a new breakpoint is listed in the Breakpoints view. This breakpoint is set for you at the start of the APEX2 graph function. 13) The debugger context is still on the A53 thread. Press RESUME and then select the APEX2 thread to see that it has stopped on the graph function break point. Now you can step through the graph. 14) To step through a kernel, locate the call to the kernel function in the graph function and set a break point on the line. 15) Press RESUME to advance the program counter to the new break point 16) Press STEP INTO to advance the program counter into the kernel. It may take several steps as the optimizations performed by the compiler produce some synchronization inconsistencies. 17) You may need to help the IDE to locate the source files. Now you can see the kernel wrapper function... and the kernel! 18) Step through, monitor variables and registers and set breakpoints.
View full article
So you've just installed the S32DS and are using it for the first time and would like to see how it works. Here is a quick and simple project to get you started. Prerequisite Before following the steps in this HOWTO, ensure you have the S32V2xx development package installed to S32DS. 1. Launch S32DS for Vision 2. Select 'S32DS Application Project' 3. Enter a name for the project 4. Select the 'A53 Linux' processor option 5. Click Next 6. Click the '...' next to the SDKs field 7. Check the box next to 'VSDK_MODULE_WIN' for Windows OS or 'VSDK_MODULE_LINUX' for Linux OS and click OK. 8. Click Finish 9. Build the project for Debug 10. Project is now built, ELF file is ready to be loaded to EVB for execution. However, if we have not prepared the EVB, we must first complete HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP. 11. Once the EVB is properly prepared, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234)  12. With the project debug configuration and remote linux connection selected, select the debug dropdown menu and click Debug Configurations 13. Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 10 is selected (points to the IP address of your EVB). Click Debug 14. The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed. 15. The executable file is copied to Linux file system and gdbserver starts. 16. The Debug perspective is opened. You can now step through the code*     *Only debugging of the A53 code is supported by Linux GDB. For multicore debugging, including ISP and APEX2, additional debugger and probe(S32 Debugger with S32 Debug Probe, Lauterbach, etc) will be required.
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power v1.2, Update 2             What is new? AMMCLIB v1.1.9 support for MPC56xx (MPC560xB, MPC560xP, MPC5643L, MPC567xF, MPC567xK) and for MPC57xxx (MPC574xC, MPC5748G, MPC574xP, MPC574xR, MPC577xC, MPC577xK, MPC577xM) updated PEmicro Eclipse Plugin Update v1.6.9 which fixes HSM mass erase problem for MPC5748G (see e.g.MPC5748G can not attach JTAG )   Installation instructions The update is available for online (Eclipse Updater) or offline (direct download link) installation.   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_2/com.freescale.s32power.updatesite  select all available items and click "Next" button   offline installation: go to S32 Design Studio product page -> Downloads section or use the direct download link to download the "S32 Design Studio for Power v1.2 - Update 2" file.   Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 2 archive file: Select all available items and click "Next" button.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 4          What is new? Radar SDK RTM 1.0.0. This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
View full article
In this document, we show the steps to use the New Project Wizard to create a new application project for APEX2, ISP, or both.   1. Launch S32DS for Vision 2. Select File -> New -> S32DS Application Project 3. Enter a name for the project 4. Select the 'A53 APEX2/ISP Linux' processor option 5. Click Next 6. Select the APEX2/ISP options you need.       a. APEX2 programming - will add support to your project for an APEX2 application, you need this for any new APEX2 project       b. ISP programming - will add support to your project for an ISP application, you need this for any new ISP project       c. ISP visual modeling - will create a separate project for your ISP data flow diagram, you will not need this if you plan to use an existing graph diagram. This can also be created later. 7. Select the SDK(s) as appropriate for your setup. For example, 'VSDK_MODULE_WIN' for Windows OS or 'VSDK_MODULE_LINUX' for Linux OS, the one which corresponds to your OS is selected for you by default. 7. Click Finish 8. You now have a project or set of projects for development on the S32V234.
View full article
There are 2 methods to run; GUI, and terminal window. GUI Method 1) Make sure EVB is powered and connected to PC via USB (micro to USB) 2) Launch DDR Stress Test Tool, C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\DDR_Tester.exe 3) Load Image (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\bin\s32v234_ddr_test.bin) 4) Load Init Script (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\scripts\S32V234_LDDR2_MMDC0_2Gb.inc) 5) Select COM port 6) Press Download, then wait for it to complete. (may temporarily show 'not responding') 7) In 32bit Memory Read/Write section, enter address 80000000 in ADDR field. 😎 Change SIZE to 32 WORD 9) Click Read 10) See results 11) In DDR Stress Test section, enter 533 in both Start Freq and End Freq fields 12) Click Stress Test 13) See results 14) Results can be saved (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\log) Terminal window Method (JTAG) This checks what settings are already uploaded in MMDC module 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach AND via USB cable. 2) In S32DS, create a simple project a. File->New->S32DS Application Project b. Enter name 'test' c. Select S32V234 Cortex-A53 d. Next e. Uncheck boxes for cores 2-4 f. Finish 3) Setup debug configuration a. Run->Debug Configurations… b. Select test_A53_1_PNE c. Change C/C++ Application to C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\ddr-test-uboot-jtag-s32v234.elf d. Select Debugger tab e. Click Advanced Options f. Check box for Enable initialization script g. Browse to find C:\NXP\S32DS_Vision_v2.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.1.3.201709051622\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR.mac h. OK 4) Click Debug. You will see error message indicating the source file could not be found. This is expected. 5) Open terminal (such as PuTTY.exe) and connect a serial line using the USB port you have connected to the EVB, speed set to 115200, 8 data bits, 1 stop bit, and no parity or flow control. 6) Click Resume in S32DS Debugger. 7) In terminal window, you will see the test script has started. 😎 Select the MMDC channel (for example, enter 1 for MMDC1) 9) Select the DDR density (for example, enter 6 for 32MB) 10) Enter 'n' to decline the DDR Calibration 11) Enter 'y' to accept the DDR Stress Test 12) Enter Start and End frequencies (for example, enter 533, as was done in GUI method) 13) Enter 0 to run only once 14) See the results
View full article
This document describes how to generate an executable file that includes data flash content and how to program it into DFLASH using PEMicro GDB debugger. The default project generated by the project wizard builds an executable with code flash sections only.  Note: It is demonstrated on MPC5744P project but with some small adjustments it's applicable to any other MPC56xx/57xx derivative supported by S32 Design Studio for Power. Let's first explain how to build an executable that contains DFLASH section:  Check the memory map of the target device in the reference manual to figure out where DFLASH is mapped into. Add DFLASH memory segment/section into the linker file  (MPC57xx_flash.ld).   MEMORY {     flash_rchw : org = 0x00FA0000,   len = 0x4     cpu0_reset_vec : org = 0x00FA0004,   len = 0x4             m_text :        org = 0x1000000, len = 2048K        m_data :        org = 0x40000000,   len = 384K        int_dram  : org = 0x50800000,   len = 64K                m_dflash :  org = 0x800000, len = 96K    /* data flash memory segment */ }  SECTIONS {   …   .dflash : { KEEP (*(.dflash)) } > m_dflash  /* place .dflash section into dflsah memory*/   … }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Select the data you want to place into the DFLASH section in the source code and associate it with the memory section you created in previous step (".dflash"). __attribute__((section(".dflash"))) const unsigned int dflash_int = 0xFEEDCAFE; __attribute__((section(".dflash"))) const char dflash_char[]= "Hello World form DFLASH!";‍‍‍‍‍‍‍‍ Build the project and check the generated .map file.  The custom".dflash" section should contain the selected data objects. .dflash         0x00800000       0x1d  *(.dflash)  .dflash        0x00800000       0x1d ./src/main.o                 0x00800000                dflash_int                 0x00800004                dflash_char‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Let's now adjust the project debug configuration to be able to program DFLASH.  First  make sure you installed the latest version of PEMicro Eclipse Plugin. See the post below - it's about ARM version of S32DS but the update process for S32DS for Power is exactly the same. You just need is to select e200 component instead of ARM: error while dubbing: "ERROR loading to the device"  If you need to control DFLASH programming separately from code flash you would need a separate debug configuration for DFLASH. You can use "Duplicate" feature on an existing Debug configuration. This creates a new configuration with pre-populated fields so you don't have to enter them all manually. Change the debug configuration name and press "Apply" Switch to the Debugger tab -> Advanced Options and tick "Use Alternative Algorithm" option. Open Browse dialog and go to the folder below where all flash programming algorithms are located (*.pcp) and  select the appropriate DFLASH programming algorithm e.g. for this example: freescale_mpc5744p_1x32x20k_dflash_cut2.pcp          "<S32_Power_v1.x>\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.5.6.201703011834\win32\gdi\P&E"   Note: Folder name "com.pemicro.debug.gdbjtag.ppc_1.5.6.201703011834" may differ depending on the latest version of Pemicro GDB plugin version installed on your machine. It's recommended to enter the latest version folder if there are multiple plugin versions available.   If you want to program DFLASH and code flash at once you can just adjust the existing debug configuration. In this case you should select combined cflash+dflash flash algorithm such as e.g. freescale_mpc5744p_cflash_dflash_cut2.pcp  Click on debug button and as soon as the debug session is established check the DFLASH memory space in the Memory View
View full article
This example performs basic initialization, sets PLL to maximum allowed frequency 200MHz, sets clock for peripherals, GPIO pins, PIT timer and interrupt controller. After initialization it blinks LED2 in the main loop using timeout counter variable. PIT timer generates periodical interrupts and toggles LED1 with 1s period. Test HW: MPC5746R-252BGA, MPC57xxMB Motherboard MCU:  PPC5746R 1N83M Fsys: PLL0 266MHz       Z4 Core 200MHz Debugger: PeMicro USB-ML-PPCNEXUS IDE/Compiler: S32DS for Power 2017.R1 / GCC Target: internal_FLASH - debug, release              internal_SRAM - debug_ram EVB connection:   Default EVB jumper setup   Connect LED1 to P14.3 on motherboard   Connect LED2 to P14.4 on motherboard
View full article
Requirements: SD card with installed Linux image connected to EVB (HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK ) Configured network connection between EVB and PC machine (HOWTO: S32V234 EVB Linux - Static IP address configuration ) S32DS for Vision Procedure: Build your Linux project. On main menu bar click Run->Debug configurations. Select C/C++ Remote Application in debug window main tab. Create new connection by clicking on New... button.  Select SSH connection type and fill connection details - IP address and user  name.    When done - click to apply and start debug session. Your elf file will be upload to SD card and executed by gdbserver on target machine. 
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 1          What is new? S32 SDK for Power Architecture 0.8.2 EAR (Early Access Release) for MPC574x-B-C-G and MPC574xP derivatives (see attached release notes for more details) MPC5744B, MPC5745B, MPC5746B MPC5744C, MPC5745C, MPC5746C - 1N84S (Cut 2.1), MPC5747C, MPC5748C MPC5746G, MPC5747G, MPC5748G - 0N78S (Cut 3.0) MPC5741P, MPC5742P, MPC5743P, MPC5744P - 1N15P (Cut 2.2B) S32 SDK  Power Architecture v0.8.2 Examples - "Create S32DS Project from Example" Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio v3.1         Austin, Texas, USA April 4, 2019    The Automotive Microcontrollers and Processors' Embedded Tools Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio v3.1.  Here are some of its major features: NXP GCC toolchains for ARM32 and aarch64 bareboard and Linux targets (GCC version 6.3.1 20170509, build 1574 revision g924fb68) S32 Debug Probe support provided with S32 Debugger and S32 Trace tool for S32V234 S32 Trace tool is integrated to provide software analysis features (profiling, code coverage, and other) P&E Debugger support for S32V23x Lauterbach Trace32® support S32 Flash Tool is delivered to support Flash/SD/MMC memory programming for S32V234 S32 SDK for S32V23x 0.9.0 Beta is integrated. Release notes here. The S32DS Extensions and Updates S32 Configuration Tool framework (EAR7) with the Pin, Clock, Peripheral, DCD, IVT, and DDR Configuration tools S32 Design Studio Versions Versioning convention has changed. The version of this release identified in red box below: Complete S32 Design Studio v3.1 release notes are available here.   Installation To download the installer please visit the S32 Design Studio product page download section or click the direct here.     The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application package available is Vision S32V2xx  (Other packages are coming soon). The application packages are managed by S32DS Extensions and Updates. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
View full article
Requirements: PC machine with telnet client (for Windows you can use Putty - Download PuTTY - a free SSH and telnet client for Windows ) DHCP server running on your PC machine or network connection with DHCP server How to install DHCP server on Linux https://www.ostechnix.com/install-dhcp-server-in-ubuntu-16-04/  DHCP server for Windows - Open DHCP Server download | SourceForge.net      S32 debug probe connected to network (with DHCP server) and visible for your PC machine   separate network using static IP addresses (or direct connection between PC and S32 debug probe). The scenario is similar like on this picture:  Procedure:   Connect power to S32 debug probe with already connected ethernet cable and wait until green LED (RX/TX) starts blink.Connect to S32 debug probe by telnet client. You can use default domain name FSLXXYYZZ where XXYYZZ are last 6 digits from S32 debug probe MAC address or assigned IP address: Static IP address can be set by netparam static_ip_address ADDRESS:NETMASK command. Make sure that you are choosing IP address from range of your Embedded network. My network uses standard 192.168.1.xxx here is mt setings:  netparam static_ip_address 192.168.1.100:255.255.255.0 You also need to set boot config from DHCP to Static: netparam bootconfig static Turn OFF and ON again S32 debug probe and check the settings by telnet with static IP address - in my case 192.168.1.100: We are done. 
View full article
Example shows how can be expanded default 512kB flash memory by 64 kB using FlexNVM as a program/data flash. In FlexNVM are stored two ASCII images and function PrintImage. FlexNVM is divided into 32kB data section and 32kB code section in the linker file. Output is printed on terminal. As a output device you can use putty or any other serial terminal. Terminal settings: 9600, 8N1 - no flow control. In debugger settings you have to Enable partitioning device with code 0F0C. This value is written into FCCOB4 and FCCOB5 registers before flashing. Putty settings: Test HW: S32K144EVB, MCU: S32K144 Debugger: OpenSDA Target: internal_FLASH (debug mode and release mode)
View full article
The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the capability to access the flash programming capabilities of the S32 Debug Probe via GTA command line and the GDB. This instruction details the steps to perform flash programming of the S32G274A EVB via the JTAG interface with the S32 Debug Probe.   Note: currently only QSPI flashing is supported.   Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. In this case, the S32G2xx development package. This is important as the S32 Debugger support within it contains the device-specific Python scripts required for initialization of the cores.  DanielBarbu_0-1729750035306.png   Setup the hardware Confirm the setup of the S32G274A evaluation board.  Configure the JTAG. The S32G274A evaluation board supports both 10- and 20- pin JTAG connections. The default board configuration is set to 20-pin, change the position of the jumper J59 from 2-3(default)  to 1-2, if you are using the 10 Pin JTAG interface. Both are supported by the S32 Debugger and S32 Debug Probe. Connect the power supply cable Setup the S32 Debug Probe Connect the S32 Debug Probe to the evaluation board via JTAG cable. Refer to the S32 Debug Probe User Manual for installation instructions. Use the JTAG connection as was confirmed in the previous step. Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard. DanielBarbu_0-1727938649769.png   Procedure Launch GTA server. From command prompt or Windows File Explorer run the command:  {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe Should see a window appear like this: DanielBarbu_1-1727938699487.png   Ensure Environment Variable for Python is set. From command prompt, run the command:  set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages DanielBarbu_2-1727938783899.png   Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window. DanielBarbu_3-1727939439489.png   Configure the EVB's Boot Mode switches for Serial Boot. Issue the following commands, replacing the PROBE_IP address and FLASH_NAME, as appropriate: source {S32DS Install Path}/S32DS/tools/S32Debugger/Debugger/scripts/gdb_extensions/flash/s32flash.py py _FLASH_TYPE = "qspi" py _PROBE_IP="10.81.64.66" py _JTAG_SPEED=20000 py _GDB_SERVER_PORT=45000 py _GDB_TIMEOUT=7200 py _REMOTE_TIMEOUT=30 py _RESET_DELAY=1 py _RESET_TYPE="default" py _INIT_SCRIPT="{S32DS Install Path}/S32DS/tools/S32Debugger/Debugger/scripts/s32g2xx/s32g274a_generic_bareboard.py" py _FLASH_NAME="MX25UM51245G" py _IS_LOGGING_ENABLED=False py flash()   Note: Replace the {S32DS Install Path} in the commands above with the actual path to your installation of S32 Design Studio. Now flash commands may be used. fl_blankcheck -- blank check fl_close -- close command fl_current -- current device command fl_dump -- dump command fl_erase -- erase section of memory command, will erase whole sectors starting from 'offset' through 'size' contiguously, so to erase only one sector, ensure that the 'offset' address is within the desired sector and 'size' does not extend into the following sector fl_erase_all -- erase all memory command fl_info -- info command, shows list of registered devices fl_protect -- protect section of memory command fl_unprotect -- unprotect section of memory command fl_write -- write memory command, hex or binary are supported, options to erase first and verify after write fl_write_elf -- write elf file to memory command, options to erase first, verify after, and rearrange flash base Type 'help fl_<command>' to print the help info on the specified command Type 'help support' to print a list of the fl_ commands For example, you may wish to write a binary file: fl_write -e 0x0 C:\\Users\\<userid_folder>\\workspaceS32DS\\hello_world\\Debug_RAM\\hello_world_blob.bin Happy flashing with S32DS Flash Programmer!
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 3.1  Update 190508          What is new? S32 Design Studio Platform Package 3.1.1 S32 Design Studio Platform Tools Package 3.1.1 Updated S32 Debugger and S32 Flash tool to support S32S247TV S32S2xxTV Development Package 3.1.0 S32V2xx Development Package 3.1.0 Vision Extension Package for S32V2xx 1.0.0 This is a cumulative update - it is applicable to S32 Design Studio 3.1 Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  online installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select all available items and click "Install/Update" button   offline installation:   go to S32 Design Studio product page -> Downloads section or use direct link to download the update archive zip file Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates" Add a new "Add.." S32DS Software Site and browse to select the downloaded update archive .zip file you downloaded in the previous step          Select all available items and click "Install/Update" button.   This will start the update installation process.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 3.2  Update 191226          What is new? Vision Extension Package for S32V234 1.1.0 with VSDK 1.5.0 integrated.(VSDK Release Notes) This is a cumulative update (includes previous updates: Update 191219) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  online installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button   offline installation:   go to S32 Design Studio product page -> Downloads section or use direct link to download the update archive zip file Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates" Add a new "Add.." S32DS Software Site and browse to select the downloaded update archive .zip file you downloaded in the previous step         Select from available items and click "Install/Update" button. This will start the update installation process.
View full article
S32 Platform Download and Install S32 Design Studio for S32 Platform v3.6  S32 Design Studio 3.6 Main Features Download and Install S32 Design Studio for S32 Platform v3.4    S32K1 Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2 A demonstration of the use of the Migration wizard in S32 Design Studio 3.4 to migrate S32K1 projects from S32 Design Studio for Arm and S32 SDK 3.0.x to S32 Design Studio 3.4 and S32 SDK 4.0.2   S32G2 Getting Started: Pins Tool Getting Started: DCD Tool Getting Started: IVT Tool Getting Started: DDR Tool   S32R45 Install S32R45 Development Package Install S32R45 Radar Extension Package Creating And Building A Project on the S32R45 for A53, LAX and SPT Cores in S32 Design Studio   S32V2 Create From Example 1 | Create an ISP project from example  A demonstration of how to load an example ISP image processing application project featuring RGB, YUV, and GS8 image formats, in the S32 Design Studio. 2 | Create an APEX2 project from example  A demonstration of how to load an example ORB-based APEX2 image processing application project in the S32 Design Studio. Create New Project 3 | Create a new ISP application  A demonstration of how to create a new Debayer-based ISP image processing application project in the S32 Design Studio. 4 | Create a new APEX2 application  A demonstration of how to create a new APEX2 image processing application project featuring upscaling and downscaling in the S32 Design Studio. Debug 5 | ISP Debugging w/S32 Debug Probe   A demonstration of how to setup and debug an ISP application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 6 | APEX2 debugging w/S32 Debug Probe  A demonstration of how to setup and debug an APEX2 application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 7 | APEX2 debugging with Emulator  A demonstration of how to debug an emulated-APEX2 image processing application project in the S32 Design Studio. 8 | Debug a Linux A53 project  A demonstration of how to debug a Linux A53 application project in the S32 Design Studio for Vision version 2.0. The example shown also includes code for APEX, but currently GDB Remote Linux only supports debug of the A53 code.
View full article