MCUXpresso IDE v11.1.0 SDK Handling Hotfix

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso IDE v11.1.0 SDK Handling Hotfix

lpcxpresso_supp
NXP Employee
NXP Employee
0 0 3,186

An issue has been identified in MCUXpresso IDE v11.1.0 with SDK 2.7 that in certain circumstances can cause the IDE to issue one or more erroneous duplicate file error popups when importing SDK examples or creating new SDK-based projects. This in particular may occur when targeting i.MX RT10xx devices, with the error referring to the XIP component, for example :

The file 'xip/evkmimxrt1060_flexspi_nor_config.c' already exists in your project but is different from the SDK component file.

pastedImage_1.png

 

We have now issued a "hotfix" for MCUXpresso IDE v11.1.0 to resolve this issue.

 

Installation Instructions

From within MCUXpresso IDE v11.1.0, select  "Help -> Check for Updates" from the main menu bar.

This should find the updated version of the "MCUXpresso IDE SDK handling" feature (11.1.0.202001201653):
pastedImage_1.png

Select this, then click through the update wizard to install this. As a final step, you will then need to restart the IDE to complete installation.

 

Note: You may also find that other updates are available to install, in particular for the "PEMicro Interface Debugging Support" (used for debugging via P&E Micro debug probes). You can also choose to install such updates at the same time as the "MCUXpresso IDE SDK handling" update if you wish.