MCUXpresso Config Tools v10 Now Available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso Config Tools v10 Now Available

petrstruzka
NXP Employee
NXP Employee
0 0 3,491

We are pleased to announce that MCUXpresso Config Tools v10 are now available.

Downloads

Revision History

10.0

  • Product based on Eclipse 2020-12
  • Moved from Open JDK 8 to Open JDK 11
  • Project cloner
    • supported create new CodeWarrior project for device from DSC SDK
    • improved path updates in component cmake source files list, now are replaced individually on cloning example for ARM GCC
  • TEE tool
    • LPC55S3x family supported
    • improved support for XRDC2 (used for RT1160/1170 processors)
      • added instance enable/disable
      • added MDAC enable/disable
      • implemented APC support
      • implemented EAL support
    • a new configuration now defaults to the secure state
    • implemented ability to create and edit multiple functional groups
    • minor improvements and fixes
      • processor reset dialog offers 2 choices where available
      • Memory Attribution Map displays dash ('-') in cells representing inexistent access
      • Memory Attribution Map cells show full access rights
      • Domains Overview is hidden for MCUs without domain-based security
      • RDC memory regions are shown as absolute instead of relative
      • Address column renamed to Start Address
      • minimum grid column size is now based on content
    • By default enabled highest security settings for LPC55xx and RT5xx/6xx processors
  • Pins tool
    • added support of expansion board adapters - expansion boards that contains additional expansion headers
    • numbered suffix is added to function names and prefixes by default for expansion board functions
    • processor reset dialog offers 2 choices where available
  • Peripherals tool
    • Component use cases
      • Current configuration of component instance can be stored as a use case
      • Add component dialog supports component instance creation from use case
      • Component use cases can be managed (import, export, remove, update) in the use cases library
    • Integration with MCUXpresso IDE
      • Peripheral tool components that configure SDK component present in the SDK package of current toolchain project will inform user that the Peripherals tool component is the right one even when the project does not contain the SDK component yet
      • Add component dialog newly provides option to offer only the Peripheral tool components that configure SDK componetns present in the SDK package of current project
      • New button that opens SDK components manager was added to the Add component dialog
    • Minor improvements and fixes
      • Processor reset offers new possibility to reset to predefined configuration of the processor
      • Board reset dialog will inform user that Peripherals tool cannot be reset when such configuration is not available instead of empty selection in the dialog
      • Tabs now also supports copy and paste actions
      • Copy and paste now works with system clipboard. Pasting into another configuration or another running Config Tools is possible
      • Links to other settings now show their current state with description what is wrong
      • Settings that can be collapsed are remembered when user collapses or expands them and tool will restore the state when view of instance is reopened
      • When GUI of the instance's view is recreated then selection in arrays and tabs is restored to state where it was last time the view was open
      • Modes of component instance which does not configure any peripheral on current processor are not offered to avoid problems
    • New register init. components for KV11/KV31 processors: ADC, CMP, FTM, PDB, PIT peripherals are supported
    • New lwip and Motor control (PMSM) middleware components
    • New features in FreeMASTER including update of CAN and new USB communication interface
    • Support of mipi_csi2 in camera middleware component
    • New spifi, mipi_dsi_split SDK init. components
    • Support of SDK 2.10.0
  • Newly added NPIs
    • New KM14/KM33/KM34 processors
    • New i.MX8MN packages

Community

MCUXpresso Config Tools