LPC845-BRK Board Projects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC845-BRK Board Projects

BlackNight
NXP Employee
NXP Employee
3 1 8,174

The LPC845-BRK is a great tiny sub-$6 breakout board featuring the LPC845M301JBD4 MCU:

  • ARM Cortex-M0+
  • 30 MHz, 64 KByte FLASH, 16 KByte SRAM
  • On-board CMSIS-DAP debug interface, works out-of-the-box with NXP MCUXpresso IDE or other 3rd party IDEs
  • 3 push buttons (user, RESET, ISP)
  • RGB LED
  • Potentiometer

NXP LPC845-BRK Board

Reference Material

 

Community Projects and Articles

Below you can find a lists of community post, blog and articles around this great board:

 

 

Post a comment if you have found another article or project to be added to this list!

 

Enjoy!

Erich

1 Comment
miguel_mendoza
NXP Employee
NXP Employee

Hi Erich,

Thanks for this great contribution!!

Here are two more projects for the LPC845 Breakout Board:
GPS: GPS Application Example Using LPC845 Breakout Board

OLED: OLED Display Application Example using LPC845 Breakout Board and SPI

Regards,
Miguel Mendoza