How to Change i.MX8X MEK+Base Board Linux Debug UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to Change i.MX8X MEK+Base Board Linux Debug UART

BiyongSUN
NXP Employee
NXP Employee
0 0 6,745

The example is to change the i.MX8QXP MEK debug uart(lpuart0) to the base board(lpuart2).

The lpuart2 is J37 on base board.

 

uart2-linux-uart2_L5.4.70_2.3.0.diff, uart2-u-boot-method1_L5.4.70_2.3.0.diff and uart2-u-boot-method2_L5.4.70_2.3.0.diff are the patches. 

 

Untitled.png

标记 (1)