NXPモデルベース・デザイン・ツールナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Model-Based Design Tools Knowledge Base

ラベル

ディスカッション

ソート順:
This video shows how: Install the Support Package Add-On Use of Installer Wizard Toolbox package download & install License generation and setup
記事全体を表示
In this video we discuss about how to use Processor-in-the-Loop (PIL) approach to generate the C-code and to validate the algorithm on the real hardware.  PIL simulation main goals are: - to generate and execute the C-code on the real target/microprocessor; - to help with specific algorithm and control designs by offering the means to optimize your software; - to establish a testing framework for the production code; PIL simulation can also use some of peripherals from the real target for inputs or outputs, making the simulation environment more realistic and closed to the final SW design specifications.   We discuss about: - What is PIL, When to use it and What is recommended for;  - How to convert any Simulink generic algorithm to run with PIL support using the Model Based Design Toolbox; - PIL Reference models;  NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
This video shows: - motor control typical setup with S32K144 rev2.0 Evaluation Board; - Simulink model for a BLDC motor control; - how to setup Simulink to generate ANSI C code for S32K144 rev2.0 MCU; - quick tour of the Model Based Design Toolbox; - quick tour of the FreeMASTER data visualizer; - Motor Control example running with DevKit S32K144EVB and MotorGD shield;
記事全体を表示
This video shows how to program the ADC with Model Based Design Toolbox to obtain the speed reference for the BLDC speed closed loop control system. We discuss about: - How the ADC works - How to simulate the ADC operations - How to implement a simple program to read data from the ADC - How to use BAM to load the application into microprocessor memory - How to test in real time with FreeMaster - How to scale the Potentiometer voltage into a speed reference data that represents the rpm. - How to implement from scratch a Simulink model to cover the ADC functionality NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
This video explains the basics of the Permanent Magnet Synchronous Motors modes of operation with Field Oriented Control. It is not intended to replace a good engineering handbook and to go thru all the details of construction or mathematical models of the PMSM.  The topics highlighted in this video are chosen to provide specific details that represents the basics of PMSM motor control theory. The goal of this video is to refresh your knowledge about the motors and to explain some key aspects of the theory behind PMSM and Field Oriented Control that we are going to use in the next modules of the https://community.nxp.com/thread/464336 
記事全体を表示
In this video we discuss about control system theory and the mathematics behind the speed controller designing process. We are going to analyse the control system stability based on poles and zeros location and then we will compute the PI speed controller gains using the Root Locus allocation method. For the cases where the system transfer function is unknown we are discussing Ziegler Nichols method for finding the controller gains and we are going to verify the control system designing process by simulating a BLDC motor behavior and building a PI speed controller to handle the system response. We discuss about: - How to choose the controller type based on system transfer function; - How to analyze system stability starting from the characteristic polynomial; - What are the gain, zeros and poles of closed loop transfer function; - Root Locus allocation method based on second order ideal model with dumping factor and natural frequency; - Ziegler Nichols tuning methods; - Simulink models for BLDC motor and PI Speed Controller NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
This video shows the overall motor control application developed with Model Based Design Toolbox. We are going to assemble all the blocks developed throughout this course and we will have the motor running under Speed Controller supervision. We also discuss about the FreeMASTER and you can easily create nice control panels for the applications and how you can validate the Speed Controller and overall Motor Control application. We discuss about: - Speed Controller implementation in Simulink for real time systems; - Motor and Inverter protection for over-current, over- and under-voltage; - FreeMASTER control panel using HTML and Java Script; - Various tests on the MPC5744P DevKit and MotorGD DevKit;   NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
In this video we talk about  how hall sensors works, how the commutation sectors are defined based on hall transitions and how can we identify the hall patterns when no datasheet is available.   We discuss about: - Hall sensors - Commutation sectors  - Hall sensors alignment procedure - Hall sensors electronic circuit used on MotorGD and MPC5744P devkits NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
This video demonstrates how to: Wake up on time interrupt Read temperature via FlexIO interface Relay information to host PC via UART interface Go to sleep to preserve the power
記事全体を表示
In this video we discuss about power stage (DevKit MotorGD) configuration that involves the configuration and initialization of the MC34GD3000 FET pre-driver via SPI commands and the setup of the FlexPWM peripheral to generate PWM commands to the inverter MOSFETs via pre-driver MC34GD3000.   We discuss about: - Pre-driver MC34GD3000 initialization sequence; - Pre-driver MC34GD3000 programming via SPI; - How to configure and test the FlexPWM peripheral; - How to test and validate the SPI communication between MPC5744P and MC34GD3000; NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
This video shows how to program the GPIO with Model Based Design Toolbox to obtain the speed reference for the BLDC speed closed loop control system.   We discuss about: - How to implement a simple program to read data from the GPIO - How to test in real time with FreeMaster - How to transform GPI pulses into a speed reference data that represents the rpm. - How to implement from scratch a Simulink model to cover the GPIO functionality NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
This video presents the hardware and software setup used for Motor Control Class. It shows: - MPC5744P DevKit main hardware features - MotorGD DevKit main hardware features - How to install the Model Based Design Toolbox for MPC5744P revision 2.0.0 - How to generate a license - How to setup a compiler toolchain using S32 Design Studio for Power Architecture - How to add the Model Based Design Toolbox for MPC5744P into the Simulink Standard Libraries - How to validate the software installation by generation C code for the first time NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
This video shows: - how to download the Model Based Design Toolbox; - how to generate a license from your account; - how to setup the environment; - quick tour of the toolbox, supported functionalities and available examples;
記事全体を表示
This video discuss about how to mix together the ADC and GPIO models to obtain a common speed reference for the BLDC speed closed loop control system.   We discuss about: - How to use analog and digital inputs - How to create a variable that can be changed in real time via Freemaster - How to test the final application - Finalize the Speed Reference Block - Short Quiz NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
In this video we show how to build, simulate and test a speed estimator based on Hall Sensors for a BLDC motor. The estimator is first tested under Matlab Simulink environment and then ported into the Open Loop Control Simulink model and tested on the MPC5744P Development Kit with FreeMASTER over CAN interface.   We discuss about: - How to compute the speed; - How to build a speed estimator based on Hall sensors; - Step-by-step model building an enhancements; NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
In this video we implement Simulink models for reading the hall sensors directly via GPIO or based on Hall transitions interrupts via eTimer Capture.   We discuss about: - How to build simple hall reading application using the available MBD Toolbox GPIO blocks  - How to enhance this simple model by adding interrupt service routines capabilities to read the hall sensors only when there is a transitions - How to count the number of hall transitions - How to validate the applications with FreeMASTER NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
In this video we enhance a Simulink model to allow the reading of hall sensors after processor reset to get the initial position of the rotor.   We discuss about: - How to build a special initialization routine to read the halls once in the beginning - How to use StateFlow programming - How to mix the direct read of GPIOs with ISR based on hall transition readings NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
This video shows how to build a simple S32K application with NXP's Model-Based Design Toolbox that consists in: Read the SW2 push button state at each 0.1 seconds Switch on/off the Blue LED Record the value of the push button and display its state via serial communication in FreeMASTER
記事全体を表示
In this video we discuss about Open Loop Control strategy and for the first time in this course we will put together all the models we have created so far and build the Simulink model that will allow us to rotate the BLDC motor. We discuss about: - Open Loop Control diagram; - Step-by-step model building an enhancements; - Test the open loop control system on the BLDC motor;   NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
In this video we discuss about how to use Software-in-the-Loop (SIL) approach to generate the C-code for the first time and validate the algorithm at the concept level.   We discuss about: - What is SIL, When to use it and What is recommended for;  - How to convert any Simulink generic algorithm to run with SIL support using the Model Based Design Toolbox; - SIL Reference models;  NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示