Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
基于OpenIL Baremetal框架的核间通信应用开发 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本文档介绍了使用 NXP Layerscape 平台的 OpenIL Baremetal 框架架构,描述了如何运行示例裸机项目以及基于 OpenIL Baremetal 框架的核间通信应用程序开发。核间通信(ICC)应用程序在 Linux 核(主)和 Baremetal 核(从)上运行,通过 SGI 核间中断和共享内存块提供核之间的数据传输。 QorIQ Layerscape 平台的 Baremetal Framework 架构。 运行裸机二进制文件 基于裸机框架的核间通信(ICC)应用开发 运行 ICC 演示应用程序
查看全文
示例 MPC5748G SMPU 初始化 + 进程 ID 测试 GHS614 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ******************************************************************************** * 详细说明: *此示例初始化 SMPU_0 和 SMPU_1 以覆盖所有内存资源 * 所有大师。 * 本例进行简单测试:初始化后,SMPU_1 * 配置已更改为禁用对最后 4kB RAM 的写入访问 * 进程 ID 1。允许进程 ID 0 进行写访问。 * 如果在进程 ID 为 1 的情况下 CPU 写入该区域,则将引发异常 * 由于访问冲突而发生。 * ---------------------------------------------------------------------------------------------- * 测试硬件:MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * 微控制器: PPC5748GMMN6A 1N81M * 系统频率:160 MHz PLL * 调试器:Lauterbach Trace32 * 目标:internal_FLASH * ******************************************************************************** 概述
查看全文
How to Enable PCIe WiFi into i.MX6 Android Release? Overview The purpose of this doument is to introduce how to enable PCIe WiFi into i.MX6 Android release. Environment Setup Hardware: i.MX6 SABRE-SD board Software: Android Jelly Bean 4.2 Software Configurations The source codes of Intel PCIe WiFi have been integrated for i.MX6 SABRE-SD board into i.MX6 Android release. However it's disabled by default. To enable it for i.MX6 SABRE-SD board, you can do the following: Change BOARD_WLAN_VENDOR to INTEL in device/fsl board configuration files. For example, diff --git a/sabresd_6dq/BoardConfig.mk b/sabresd_6dq/BoardConfig.mk index 9c8a32d..912e752 100755 --- a/sabresd_6dq/BoardConfig.mk +++ b/sabresd_6dq/BoardConfig.mk @@ -11,7 +11,7 @@ TARGET_BOOTLOADER_BOARD_NAME := SABRESD PRODUCT_MODEL := SABRESD-MX6DQ # Wifi -BOARD_WLAN_VENDOR                       := ATHEROS +BOARD_WLAN_VENDOR                       := INTEL # for atheros vendor ifeq ($(BOARD_WLAN_VENDOR),ATHEROS) BOARD_WLAN_DEVICE                       := ar6003 @@ -30,6 +30,7 @@ WIFI_COMPAT_MODULE_ARG                         := "" endif #for intel vendor ifeq ($(BOARD_WLAN_VENDOR),INTEL) +BOARD_WLAN_DEVICE                       := INTEL BOARD_HOSTAPD_PRIVATE_LIB               ?= private_lib_driver_cmd BOARD_WPA_SUPPLICANT_PRIVATE_LIB        ?= private_lib_driver_cmd WPA_SUPPLICANT_VERSION                  := VER_0_8_X After changing BOARD_WLAN_VENDOR as "INTEL", the following files will be compiled for intel WiFi: device/fsl-proprietary/pcie-wifi/ external/wpa_supplicant_8 hardware/imx/wlan/intel/ hardware/libhardware_legacy/wifi/wifi_intel.c Enable PCIe WiFi driver in kernel_imx by running "make menuconfig" command: Select "System Type -> Freescale MXC Implementations -> PCI Express support" as "*" Select "Networking support -> Wireless ->  cfg80211 - wireless configuration API" as "*". Then select "Networking support -> Wireless -> Generic IEEE 802.11 Networking Stack (mac80211)" as "*" Select "Device Drivers ->  Network device support -> Wireless LAN -> Intel Wireless WiFi 4965AGN (iwl4965)" as "*" Then run "make" command to build kernel. The followings are the dependencies files to enable above configuration: Kernel configuration: * -> System Type -> Freescale MXC Implementations Select the PCI Express support. Then config intel WIFI driver: Generic IEEE 802.11 Networking Stack (mac80211) used by WIFI devices Symbol: MAC80211 [=y] Type : tristate Prompt: Generic IEEE 802.11 Networking Stack (mac80211) Defined at net/mac80211/Kconfig:1 Depends on: NET [=y] && WIRELESS [=y] && CFG80211 [=y] Location: -> Networking support (NET [=y]) -> Wireless (WIRELESS [=y]) Intel iwl4965 or iwl6300 card driver Symbol: IWL4965 [=y] Type : tristate Prompt: Intel Wireless WiFi 4965AGN (iwl4965) Defined at drivers/net/wireless/iwlegacy/Kconfig:65 Depends on: NETDEVICES [=y] && WLAN [=y] && PCI [=y] && MAC80211 [=y] Location: -> Device Drivers -> Network device support (NETDEVICES [=y]) Then you can follow up the instructions into Android User guide to build Android image. Known Limitation PCIe low power mode is not supported according to BSP release note. So when building in PCIe, the system suspend/resume should be disabled now. Android i.MX6DL i.MX6Dual i.MX6Quad Re: How to Enable PCIe WiFi into i.MX6 Android Release? Hi Sandesh      can you tell me the changes?thank Re: How to Enable PCIe WiFi into i.MX6 Android Release? HI Ross      can you upload the doc? thanks~ Re: How to Enable PCIe WiFi into i.MX6 Android Release? Dear Sir, I tried to load iwlagn.ko, and i got those log when WIFI ON: D/WifiService( 2578): setWifiEnabled: true pid=2831, uid=1000 W/WifiHW  ( 2578): is_wifi_driver_loaded W/WifiHW  ( 2578): got module patch /system/lib/modules/iwlagn.ko E/WifiStateMachine( 2578): Failed to reload STA firmware java.lang.IllegalArgumentException: command '12 softap fwreload wlan0 STA' failed with '501 12 SoftAP command has failed' W/CommandListener( 2209): Failed to retrieve HW addr for wlan0 (No such device) D/CommandListener( 2209): Setting iface cfg E/WifiStateMachine( 2578): Unable to change interface settings: java.lang.IllegalStateException: command '14 interface setcfg wlan0 0.0.0.0 0 down' failed with '400 14 Failed to set address (No such device)' D/WifiMonitor( 2578): startMonitoring(wlan0) with mConnected = false E/WifiHW  ( 2578): Unable to open connection to supplicant on "/data/misc/wifi/sockets/wlan0": No such file or directory D/BluetoothAdapter( 2831): 1102399976: getState() :  mService = null. Returning STATE_OFF D/Tethering( 2578): sendTetherStateChangedBroadcast 1, 0, 0 I/wpa_supplicant( 3398): Successfully initialized wpa_supplicant D/Tethering( 2578): InitialState.processMessage what=4 D/Tethering( 2578): sendTetherStateChangedBroadcast 0, 0, 0 E/WifiHW  ( 2578): Supplicant not running, cannot connect E/WifiHW  ( 2578): Supplicant not running, cannot connect E/WifiHW  ( 2578): Supplicant not running, cannot connect E/WifiHW  ( 2578): Supplicant not running, cannot connect E/WifiHW  ( 2578): Supplicant not running, cannot connect E/WifiMonitor( 2578): startMonitoring(wlan0) failed! E/WifiStateMachine( 2578): Failed to setup control channel, restart supplicant W/WifiHW  ( 2578): is_wifi_driver_loaded W/WifiHW  ( 2578): is_wifi_driver_loaded return 0 E/WifiStateMachine( 2578): Failed to reload STA firmware java.lang.IllegalArgumentException: command '17 softap fwreload wlan0 STA' failed with '501 17 SoftAP command has failed' D/CommandListener( 2209): Setting iface cfg D/CommandListener( 2209): Trying to bring down wlan0 E/WifiMonitor( 2578): startMonitor called with unknown iface=wlan0 D/BluetoothAdapter( 2831): 1102399976: getState() :  mService = null. Returning STATE_OFF I/wpa_supplicant( 3416): Successfully initialized wpa_supplicant But wifi still not work. Any suggestions for it ? Re: How to Enable PCIe WiFi into i.MX6 Android Release? Dear Sir, We are using i.MX6DL with Android 4.4.2 kitkat. WiFi module: Intel Wifi Link 5100  Model:512AN_HMW  When trying to turn on wifi , it shows: D/WifiService( 2625): setWifiEnabled: true pid=2943, uid=1000 W/WifiHW  ( 2625): got module patch /system/lib/modules/iwlagn.ko E/WifiStateMachine( 2625): Failed to load driver Any suggestions for it ? Re: How to Enable PCIe WiFi into i.MX6 Android Release? Dear Sir, Our customer would like to use WiFi module: Intel Wifi Link 5100  Model:512AN_HMW  on Android 4.4 system. Could you any suggestion for it? Re: How to Enable PCIe WiFi into i.MX6 Android Release? Everyone, It should be noted that this process will not work with the Intel 3160 due to its support of P2P (I have never tried using the Intel 4965, don't have that part on hand in any case). We also have had trouble with P2P with the Atheros 9k (AR9462 part), but finally got basic Wifi functionality working. In general, I have been very disappointed with Wifi support in the JellyBean 4.3 BSP. What would be nice to see is a patch released to upgrade  the wpa_supplicant to 2.1 stable (February 2014 release I think). Michael Robbeloth Re: How to Enable PCIe WiFi into i.MX6 Android Release? Sandesh, Thank you, yes I did. One of our engineers got our SX-PCEAN+ card (9280 based) working with the v3.0.35 Ubuntu BSP. Re: How to Enable PCIe WiFi into i.MX6 Android Release? Ross, Did you find solution to bringup wifi on Ath9K PCIe card? we modified the changes in hardware/imx/wlan/atheros/compat-wireless/Android.mk to bringup WiFi feature. Re: How to Enable PCIe WiFi into i.MX6 Android Release? Hi Xiaoli, Is there support for the Atheros AR9K family and what would the differences be in the above instructions to build JB for a AR9K PCIe card? I have two i.MX6 customers asking how to do this (one is Android JB and one is Linux). I plan on sharing your excellent document but wondered if you could share anything specific to the Atheros 9K family. Thanks..>Andy Re: How to Enable PCIe WiFi into i.MX6 Android Release? The attachment is some patches  to enable intel 4965 wifi card with android 4.2.2 on sabresd 6q.You can take it as a reference. Re: How to Enable PCIe WiFi into i.MX6 Android Release? Hi Xiaoli, I followed your instruction to build JB 4.2.2 with Intel mini-PCIe wifi support but got the error messages below. I was able to build ICS with the same configuration, strange. make: *** No rule to make target `out/target/product/sabresd_6dq/obj/STATIC_LIBRARIES/private_lib_driver_cmd_intermediates/export_includes', needed by `out/target/product/sabresd_6dq/obj/EXECUTABLES/hostapd_intermediates/import_includes'.  Stop.
查看全文
使用 i.MX28 添加对新型 NAND 的支持——NAND 分析 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本页介绍如何确定 NAND 驱动程序中使用的 NAND 时序参数。这与可能使用的任何操作系统无关。 分析NAND数据表 我们使用电子表格来捕获和分析 NAND 特性。该电子表格[附加到此 wiki 页面|使用 i.MX28 添加对新 NAND 的支持 - Nand 分析^nand_analysis_template.xls]。 我们分析一个 NAND,如下所述。 我们必须有 NAND 数据表才能进行分析。 将*分析电子表格*复制到一个新文件名,其中包含正在分析的 NAND 的确切零件编号。 填写分析电子表格的第 1 页(“封面”)。 接下来处理第 3 张表: 基本特征。 其他表。 如果 NAND 是数据表中列出的某个系列之一,则使用一个电子表格来分析整个系列。您可以使用“类似”行来查找家庭的其他成员。如果需要,添加更多行。 大多数 NAND 都有异步接口,因此不涉及简单的时钟频率。相反,存在各种设置时间、保持时间和输出延迟,这意味着 NAND 的 I/O 速率受到限制。电子表格比较了 NAND 的时序规格,以查看设置、保持和输出时间的总和是否短于最小读取周期或写入周期时间。该电子表格专门用于 STMP378x/i.MX233/i.mx28 中的 Nand 控制器芯片,因此电子表格执行时序计算,目的是得出这些 CPU 的时序参数 *TSU*、*TDS* 和 *TDH*。如果在计算完所有时间之后,TDS 和/或 TDH 量 {color:#ff0000} 变为红色{color},则计算出的 TDS 和/或 TDH 对于 NAND 的指定周期时间来说太短。在这种情况下: 您必须在软件中增加其中一个或两个。 在分析电子表格中的某处写下您选择的值的注释,但不要弄乱自动计算。 记录闪存如何表示工厂标记的坏块。(有些使用块的第一页,有些使用最后一页,等等)将其与此[当前坏块标记方法超集[ http://wiki.freescale.net/display/PSGSW/Storage+Media%2C+Flash+Bad+Block+Marks ]进行比较用于检测任何闪存工厂坏块。 实例分析 NAND 数据表和分析的示例可以在 [Hynix NAND 页面 | http://wiki.freescale.net/display/PSGSW/Hynix+NAND+Flash+Documents ] 上找到。 i.MX2x 回复:使用 i.MX28 添加对新 NAND 的支持–NAND 分析 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,谢谢你的信息。由于某些原因,链接不起作用。您能否提供分析电子表格的新链接?谢谢,马克
查看全文
i.MX25 PDK 板闪存 SPI NOR <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您可以按照以下步骤从 SPI NOR Flash 启动:      1——下载 ATK 版本 1.7。ATK 1.7 版本可以在这里下载。 2 - 将文件 iMX_AdvancedToolKit_R170.zip 解压缩到“C:\Program Files\freescale\AdvancedToolKit-STD\image\”。      3 - 打开文件“C:\Program Files\freescale\AdvancedToolKit-STD\config\ADSToolkit.cfg”并添加以下行: [MX25_TO11] MMC/SD::image\mx25_mmc.bin:0x(未知) NAND::image\mx25_nand.bin:0x(未知) SPI::image\mx25_spi.bin:0x(未知) [MX31] 4 - 在 MX25PDK 上设置 SPI 启动配置:   SW22:无影响 SW21[1-8]: 11110010 BT_MEM_CTL[0:1] = 11(扩展) BT_MEM_TYPE[0:1] = 11(通过 SPI 的串行 ROM) BT_PAGE_SIZE[0:1] = 无影响 BT_BUS_WIDTH[0:1] = 10(3 地址 SPI(24 位)注:BT_BUS_WIDTH[0]=1,BT_BUS_WIDTH[1]=0 在调试板上,红色开关: (SW5-SW10)= 000011(0=关闭) 个性板上的启动配置开关(SW21,SW22)没有影响。 5 - 连接主机 PC 和 PDK 之间的 USB 或串行电缆并执行 ATK 6 - 在 MX25PDK 上选择 USB/UART 串行启动并打开电路板电源 7-配置ATK如下: 设备 = i.MX25_TO1.1 设备内存初始=DDR2 通信通道:COMn(选择您PC上的COM端口) 或 通讯通道:USB 如果您选择 COM(串行 UART 连接),则必须断开 i.MX25 PDK 上 OTG 连接器上的 USB 电缆。 8-配置ATK“Flash工具”如下: 勾选“程序” 勾选“阅读回执” 闪存型号 = SPI 地址 = 0x0 图像 = mx25_3stack_redboot_TO1_1.bin(与 NAND 启动相同的文件)。 同样适用于 U-boot。 注意:SPI NOR Boot 需要内部启动模式。调试卡上的所有红色开关必须关闭 (SW5-SW10)= 000000(0=关闭)。 注意:如果从 SPI NOR 启动,Redboot 需要大约 2 秒钟才能在控制台上显示消息。 i.MX2x 回复:i.MX25 PDK 板闪存 SPI NOR <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 谢谢 Fabio! 这里的问题是 SD 卡启动在这个板上不起作用,我们正在调试以了解原因。 回复:i.MX25 PDK 板闪存 SPI NOR <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我发现该图像仅支持 CP(连续编程)模式,但是我的 spi flash 不支持它。并且源代码中有很多错误
查看全文
FreeMASTER 3.2 - 发布公告 NXP FreeMASTER 工具 3.2 版刚刚在线发布。 这是新 3.2.x 的第一个版本发布线。它向后兼容以前的 3.x 和 2.x 版本(请参阅以前的版本 公告)。最新版本带来了本文描述的新功能和错误修复。 更新后的安装程序以及文档和其他资源可在http://www.nxp.com/freemaster上获取。 发布说明 FreeMASTER是 NXP 开发和提供的一款强大的数据可视化工具,可帮助用户监视和控制在 NXP 目标上运行的嵌入式应用程序。它可与边缘处理和汽车业务线的几乎所有 NXP Arm ® Cortex ® -M 微控制器以及 DSC 和传统 Power Architecture、ColdFire 和 HCS12/Z 平台配合使用。请注意,许可条款和条件不允许将 FreeMASTER 与其他供应商的未经授权的系统一起使用。 3.2.0 版本是新 3.2.x 的第一个版本发布线。该安装程序不会取代系统中的旧安装,3.2 版本可能会与旧版本同时共存。 3.2 版完全向后兼容所有以前的版本,并添加了此处描述的新功能。传统上,它支持嵌入式应用程序的运行时监控,显示变量值、示波器实时图表、快速瞬态记录器图表,并支持与第三方应用程序的连接。此版本引入的主要新功能是支持 Microsoft Edge WebView2 浏览器组件,该组件可用于呈现在 FreeMASTER 主应用程序窗口中嵌入运行的仪表板和其他控制应用程序。 总的来说,现在有三种在 FreeMASTER 内部托管活动 HTML 内容的选项:版本 1.x 和 2.x 中引入的传统 Microsoft Internet Explorer 组件;版本 3.0 中引入的 Chromium CEF 组件和新的 Microsoft Edge WebView2 组件。 新的 Edge WebView2 也基于 Chromium 引擎,因此它与 FreeMASTER 的 JSON-RPC 客户端界面完全兼容。此外,Edge 还部分支持 COM+ 主机对象嵌入,从而可以访问“传统” FreeMASTER ActiveX 接口。这种多功能性使得最初为 Internet Explorer 创建的旧仪表板和控制页面能够顺利迁移到现代浏览器框架中。请注意,Microsoft 正在逐步淘汰 Internet Explorer 浏览器和相关技术,并且基于 IE 的应用程序在不久的将来可能无法再正常运行。 请在 FreeMASTER 欢迎页面上阅读 IE 迁移白皮书以了解更多信息。 FreeMASTER Lite服务是 FreeMASTER 安装包的一部分,为 Windows 和 Linux 系统提供通信核心。它可以通过 JSON-RPC 接口以类似 FreeMASTER 桌面应用程序的方式进行访问。FreeMASTER Lite 还嵌入了流行的Node-RED框架用于图形编程,并提供了许多使用 FreeMASTER 工具的示例。在专门的培训视频中查找与 Node-RED 相关的更多信息。 注意:安装 FreeMASTER Lite 将需要您输入激活码。在 许可证信息页面 的“许可证密钥” 选项卡上获取免费代码。 FreeMASTER Node.js 可安装模块支持在由“npm”包管理器管理的 Node.js 应用程序中方便地使用 FreeMASTER JSON-RPC 组件。 新增功能 关键的新功能是支持 Microsoft Edge WebView2 浏览器组件,该组件可用于将在 FreeMASTER 中运行的旧仪表板和其他 HTML 应用程序从 Internet Explorer 迁移到现代浏览器,而对 HTML 和 JScript 代码的更改却很少。 此外,ActiveX 和 JSON-RPC 接口已通过新方法进行了扩展,可以从脚本环境以编程方式访问项目内容和项目选项。 发布的目标受众群体 FreeMASTER 和 FreeMASTER Lite 主要针对希望在运行时监控和控制其应用程序的工业、物联网和汽车领域的 NXP 嵌入式应用程序的客户、工程师和开发人员。FreeMASTER 也是一个强大的框架,可用于创建交互式演示和用户界面,帮助更广泛的目标受众使用嵌入式应用程序。 前提条件 FreeMASTER 工具在主机上运行,并使用串行、CAN、以太网/WiFi 网络、JTAG、BDM 或其他物理接口与目标微控制器应用程序通信。微控制器通信驱动程序可作为 MCUXpresso SDK、S32 Design Studio 的一部分或独立安装包提供。在使用 FreeMASTER 工具之前,请熟悉通信协议和微控制器驱动程序 API。 许可条款和条件仅允许在基于NXP微处理器或微控制器系统的系统上使用FreeMASTER。 封装 包含 FreeMASTER 桌面应用程序和新 FreeMASTER Lite 服务的单个自解压安装包可用于 Windows 平台。带有 FreeMASTER Lite 服务的软件包也适用于 Linux。 访问 FreeMASTER 主页https://www.nxp.com/freemaster 上的安装和文档。
查看全文
使用 Kinetis 设备中的 DMA 模块 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 各位 Kinetis 爱好者,大家好, 微控制器编程是我们所有关注这个社区的人所热衷的事情,但有时,试图了解微控制器的外围设备并不是一件容易的事,特别是当我们第一次接触一个新模块或设备时。 在这篇文章中,您将找到一份详细解释 Kinetis 设备的 DMA 模块的文档,以及使用 DMA 和其他外设的 CodeWarrior 和 Kinetis Design Studio 的一些示例。 此处找到的文档是: 在 Kinetis 设备中使用 DMA 模块(完整):包含 DMA 模块说明的文档:使用 DMA 时需要了解的所有信息以及理解所含代码所需的信息(CW 的 K20_DMA 或 KDS 的 K20D72_DMA)。 在 Kinetis 设备中使用 DMA 模块(示例):包含理解所含代码所需信息的文档(用于 CW 的 K20_DMA 或用于 KDS 的 K20D72_DMA)。 附件是两个文件夹,名称如下: CW 的 DMA 示例:包括 CW 的 DMA 示例项目 KDS 的 DMA 示例:包括 KDS 的 DMA 示例项目。 每个文件夹包含 5 个示例: 请随意修改示例;我希望这对您有用。 非常感谢manuelrodriguez对开发和编辑这个项目提供的宝贵帮助。 :smileyinfo:对于 SPI 示例,有必要在 MOSI 和 MISO 引脚之间建立桥接(示例中使用主环路模式)。为此,使用了 TWR 电梯。 在附件中,您可以找到使用 SPI 和 DMA 时的一些额外信息。 顺祝商祺! 阿德里安·桑切斯·卡诺 技术支持工程师 Freedom开发平台 Kinetis K系列MCU Kinetis L系列MCU 回复:在Kinetis设备中使用DMA模块 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 使用 DMA-ADC-PIT 的示例可以在这里找到: FRDM-KL25z、FRDM-K64F、TWR-K60D100 和 TWR-K70 的 PIT-ADC-DMA 示例 此致, 阿德里安
查看全文
メンテナンスインターフェースとしてのNFC NXPのNTAG 5のような接続されたNFCタグを使用すると、NFC対応のスマートフォンをあらゆる種類のマシン、アプライアンス、またはコンポーネントの追加GUIとして使用できます。それらは、カジュアルな観察者に見えるようにすることができますが、その必要はありません。これにより、ユニットのデフォルトのユーザーインターフェースを、再構成やメンテナンススタッフが使用するセカンダリインターフェースから分離できます。この機能は、インダストリー4.0のコンテキストにおける説明責任とデータ保護の問題を解決するのに役立ちます。 NFCインターフェースがシステムにもたらすメリットについて疑問に思っている場合は、このセッションに参加してください。NFCが、通常の接続性がないシステムでもエッジコンピューティングのパワーを利用できるようにする方法をご覧ください。 プレゼンター: マリオ・ストルツ、コネクテッドタグ、プロダクトマネージャー、NXP Johannes Grüll氏、NXPスマート製品および認証グローバルマーケティングマネージャー 識別とセキュリティ NFCの|コントローラ&リーダIC
查看全文
第九届飞思卡尔杯智能赛车创意团队赛规则(1).pdf <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 附件最终规则适用于2014年飞思卡尔创新大赛规则 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 附件最终规则适用于2014年飞思卡尔创新大赛规则
查看全文
Varification of EMC Compliance for MYD-Y6ULX-CHMI The MYD-Y6ULX-CHMI Display Panel is an ultra-low cost Human Machine Interface (HMI) solution based on 528MHz NXPi.MX6UL/6ULL ARM Cortext-A7 processor. It is a Linux-ready device with ported QT, can be used in various applications including POS, Intelligent access control and more others. The panel provides a well-designed hardware with various peripherals and rich software resources to help users accelerate their time to the market. The MYD-Y6ULX-CHMI consists of an MYD-Y6ULX-HMI Development Board and a 7-inch capacitive LCD mounting on its top. The LCD offers 800x480 pixels display resolution. The MYD-Y6ULX-HMI Development Board provides peripherals and interfaces including RS232, RS485, Ethernet, USB Host/Device, LCD, Camera, TF card slot and etc. Considering wireless communication and dial-up functions, MYIR offers an optional IO board MYB-Y6ULX-HMI-4GEXP for the MYD-Y6ULX-CHMI Display Panel. The IO Board features on board AP6212 module for WiFi/Bluetooth and a Mini-PCIe interface for USB based 4G LTE module. Moreover, the IO Board has extended one more Ethernet interface and Audio in/out ports to further enhance the functionality of the panel, thus making a complete solution for HMI applications. The MYD-Y6ULX-CHMI has passed the verification of EMC Compliance.           MYD-Y6ULX-CHMI Display Panel                            MYD-Y6ULX-CHMI Display Panel + MYB-Y6ULX-HMI-4GEXP The MYD-Y6ULX-CHMI Display Panel is an ultra-low cost Human Machine Interface (HMI) solution based on 528MHz NXPi.MX6UL/6ULL ARM Cortext-A7 processor. It is a Linux-ready device with ported QT, can be used in various applications including POS, Intelligent access control and more others. The panel provides a well-designed hardware with various peripherals and rich software resources to help users accelerate their time to the market. The MYD-Y6ULX-CHMI consists of an MYD-Y6ULX-HMI Development Board and a 7-inch capacitive LCD mounting on its top. The LCD offers 800x480 pixels display resolution. The MYD-Y6ULX-HMI Development Board provides peripherals and interfaces including RS232, RS485, Ethernet, USB Host/Device, LCD, Camera, TF card slot and etc. Considering wireless communication and dial-up functions, MYIR offers an optional IO board MYB-Y6ULX-HMI-4GEXP for the MYD-Y6ULX-CHMI Display Panel. The IO Board features on board AP6212 module for WiFi/Bluetooth and a Mini-PCIe interface for USB based 4G LTE module. Moreover, the IO Board has extended one more Ethernet interface and Audio in/out ports to further enhance the functionality of the panel, thus making a complete solution for HMI applications. The MYD-Y6ULX-CHMI has passed the verification of EMC Compliance.           MYD-Y6ULX-CHMI Display Panel                            MYD-Y6ULX-CHMI Display Panel + MYB-Y6ULX-HMI-4GEXP
查看全文
面向采购/买家的汽车半导体 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 许多从事电子行业的人员需要具备半导体元件的基本知识,以便理解制造周期、半导体工厂整合和故障分析结果等问题。本次会议面向非技术受众,并对半导体器件及其制造方法进行了高层次的概述。讲座首先简要概述了半导体器件的工作原理。演示的大部分内容描述了半导体器件的通用制造流程,重点强调了所用设备/设施的复杂性和所需的处理时间。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 许多从事电子行业的人员需要具备半导体元件的基本知识,以便理解制造周期、半导体工厂整合和故障分析结果等问题。本次会议面向非技术受众,并对半导体器件及其制造方法进行了高层次的概述。讲座首先简要概述了半导体器件的工作原理。演示的大部分内容描述了半导体器件的通用制造流程,重点强调了所用设备/设施的复杂性和所需的处理时间。
查看全文
NFC 基本功能及更多! <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次会议将向参与者简要介绍 NFC 是什么、哪些产品属于产品组合的一部分以及如何在多个垂直领域的不同用例中使用它们。它还引导参与者快速了解可用于原型设计的开发套件和 SW 资源。简而言之,这是您开始使用 NFC 的最佳速成课程。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次会议将向参与者简要介绍 NFC 是什么、哪些产品属于产品组合的一部分以及如何在多个垂直领域的不同用例中使用它们。它还引导参与者快速了解可用于原型设计的开发套件和 SW 资源。简而言之,这是您开始使用 NFC 的最佳速成课程。 接口和连接 传感器
查看全文
PMIC PF3000/3001 Resources The PF3000 is a power management integrated circuit (PMIC) designed specifically for use with the NXP i.MX 7 and i.MX 6SL/SX/UL application processors. With up to four buck converters, six linear regulators, RTC supply, and coin-cell charger, the PF3000 can provide power for a complete system, including applications processors, memory, and system peripherals. This device is powered by SMARTMOS technology. The latest version datasheet :https://www.nxp.com/docs/en/data-sheet/PF3000.pdf  Application note:https://www.nxp.com/docs/en/application-note/AN5132.pdf                            https://www.nxp.com/docs/en/application-note/AN5161.pdf                           https://www.nxp.com/docs/en/application-note/AN5094.pdf                           https://www.nxp.com/docs/en/application-note/AN5113.pdf Evaluation board user's guide:https://www.nxp.com/docs/en/user-guide/KTPF3000FRDMEVMUG.pdf  GUI for PF Power Management Development Tools:https://www.nxp.com/downloads/en/device-drivers/PF3000-HID-GUI.zip EVM and Tools:https://www.nxp.com/webapp/sps/download/license.jsp?colCode=KITPF3000FRDMEVM  More information: https://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-application-processors/12-channel-configurable-pmic:PF3000 PF3000PF3001
查看全文
安全 CAN 通信——基于软件的方法和基于硬件的简单解决方案对系统的影响 借助安全的 CAN 收发器,恩智浦为 CAN 网络提供了非常高效的基于硬件的安全解决方案,补充了整体 恩智浦 4+1 分层安全方法。本课程阐明了不同的用例以及 TJA115x 安全 CAN 系列如何在系统级别上帮助实现高效的解决方案。 借助安全的 CAN 收发器,恩智浦为 CAN 网络提供了非常高效的基于硬件的安全解决方案,补充了整体 恩智浦 4+1 分层安全方法。本次会议阐明了不同的用例以及 STINGER 如何在系统层面上帮助提供高效的解决方案。
查看全文
MCUXpresso 软件和工具概述实验 1 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 开始使用 MCUXpresso SDK、IDE 和配置工具。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 开始使用 MCUXpresso SDK、IDE 和配置工具。 软件和工具
查看全文
Type-C端到端解决方案_Connect China <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> NXP 的 USB Type-C 端到端解决方案可轻松集成到客户设计中,包括用于电源的 AC/DC 转换器、PD PHY 和 CC 逻辑控制器、直接充电、信号转驱动器、信号开关、负载开关和身份验证。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> NXP 的 USB Type-C 端到端解决方案可轻松集成到客户设计中,包括用于电源的 AC/DC 转换器、PD PHY 和 CC 逻辑控制器、直接充电、信号转驱动器、信号开关、负载开关和身份验证。
查看全文
澳洲大学挂科怎么办 澳洲大学挂科怎么办联系QQ1252839746,考试挂科作弊、GPA低被开除退学、收到学术警告。澳洲大学2018 S1的Final成绩已经在陆续发放了,拿到成绩的时候,有些人难免会沮丧,复习了的内容没考,考的内容没复习,所以就有科目理所应当的挂科了…… 澳洲大学向来是宽!进!严!出!随着成绩的公布,小伙伴们都在问挂科了到底该怎么办?一起来了解一下不同情况的挂科该如何处理吧! 同一学期挂科科目挂科小于等于50% 什么叫挂科科目小于等于50%呢?各大学的课程设置都是一学期4门课,如果你在一学期中挂了1-2门,但是还没有出现double fail(一科已经连续fail两次以上),那么学校不会对你有任何行动,下学期一定要争取4门全部Pass来弥补! 同一学期挂科科目挂科大于等于50% 大于等于50%的意思就是如果在一学期中挂了2门以上课程,那一般学校就会采取第一次行动了,会对你发出一封警告信! 学校出勤率低于80% 和挂科无关,但非常重要。如果同学们在一学期中,因各种原因出勤率不满80%的,并且针对这过低的出勤率没有合理的理由,学校也会先对你做出警告需要解释,如果理由没有被学校接受,学校也有资格将你上报移民局,移民局可以会跟据情况取消签证。 努力学习却还是挂科 如果是平时十分努力却还是掌控不了挂科的同学门要及早正视自己的问题,对自己挂科的原因进行总结,可能是由于专业不适合,学习能力不够,学校和你的学习理念存在差异……而这类学生最重要的就是正视自己的情况考虑转学校或者是换专业。 警告信解释 当你不幸收到开除警告信后,书面解释的质量非常重要。 首先,解释列举的原因,一定是不可控的因素,由此导致的学习成绩差;接着表明自己坚信可以完成学业,并列举理由;最后认真的规划应该如何去克服困难,努力提高成绩。 如果以身体健康原因作为理由,必须准备辅助材料,如医生开具的证明等,一同上交。校方受理后会决定十分需要召开听证会,听证会后即会给出解释结果。 转校 这里需要提醒小伙伴们如果被公立大学开除,则无法转到其它公立大学继续学习,只能转到各种私立大学或学院,但可以在收到学校警告信后,马上开始准备转学事宜,在开除程序正式开始之前申请转学。 转学 若未读满6个月的课程就申请转学,首先需要获得想转学学校OFFER,然后向在读学校申请Release letter(放行信),在读学校会根据转学政策和程序审核申请,再决定是否发放Release letter; 如果已经在主课学校就读超过六个月,一般学校都会同意学生的转学申请。 在澳洲挂科除了昂贵的学费外,还有可能会面临强制退学和取消学生签证,并且3年都不得进入澳洲,所以要谨慎对待每次考试,澳洲大学挂科改成绩(Q1252839746)挂科GPA成绩修改,解决被退学开除等问题。 General
查看全文
示例 S12ZVL ADC0 由 TIM0 OC 触发更新 PWM 占空比 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ******************************************************************************** 详细描述: TIM0_Ch2 OC 每 50ms 触发 AN2(DEVKIT S12ZVL32,电位器)上的 ADC 测量。 ADC 中断更新 3 个相差 90° 的 PWM 信号的占空比 (0-100%)。 ADC 可以在触发或重启模式下工作。 PWM 信号被路由至 RGB LED(DEVKIT S12ZVL32)。 ---------------------------------------------------------------------------------------------- 测试硬件:DEVKIT-S12ZVL32 微控制器:S12ZVL32 调试器:CW11 目标:internal_FLASH ********************************************************************************
查看全文
LAT-DES-T2445 - PCB 布局技巧与窍门 – 稳健性之旅 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 加入我们,了解如何开发各种类型的 PCB 以及在恶劣环境下表现良好的复杂性。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 加入我们,了解如何开发各种类型的 PCB 以及在恶劣环境下表现良好的复杂性。
查看全文
DES-N1989 ハンズオンワークショップ:SCM-i.MX 6Dual6Quadクイックスタートボードのハンズオン <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> SCM-i.MX 6Dual/6Quadに内蔵されたSPI-NORフラッシュを効果的に使用する方法をご紹介します。取り上げるトピックには、16 MB の SPI-NOR に完全に収まる Linux イメージの特性や、SPI-NOR を eMMC などの外部ブート ソースと共に活用する方法の例が含まれます。また、参加者はクイックスタートボードを使用して複数のシナリオを試すことができます。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> SCM-i.MX 6Dual/6Quadに内蔵されたSPI-NORフラッシュを効果的に使用する方法をご紹介します。取り上げるトピックには、16 MB の SPI-NOR に完全に収まる Linux イメージの特性や、SPI-NOR を eMMC などの外部ブート ソースと共に活用する方法の例が含まれます。また、参加者はクイックスタートボードを使用して複数のシナリオを試すことができます。 デザイン |ソフトウェア&サービス
查看全文