Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
Arcturus Demo uCP1020 IoT Gateway Module and Mbarx IoT Middleware uCP1020 IoT Gateway Module hardware Mbarx IoT Gateway Middleware TLS secure remote site connectivity Data aggregation and proxy of remote IoT devices Seamless switching between local and remote IoT sites   Mbarx System Manager GUI IoT site management tool uCP1020 IoT Gateway System-On-Module Hardware This Demo Is Probably of Interest If You: Have various remote site locations that need to be centrally connected Require remote site data aggregation and secure connectivity, across public networks Need to implement a private cloud service architecture (e.g. develop your own device interactions/workflow) Require a versatile Linux platform to deploy various gateway services Are evaluating options for RYO or commercial IoT gateway hardware Differentiation This Demo Highlights Modular, off-the-shelf IoT gateway hardware Eco-system of Mbarx IoT solutions and tools Simple, GUI driven management of remote sites Complete system-level solution for private or public cloud IoT deployments   What this Demo is All About Video Link : 4542 uCP1020 IoT Gateway Demo - Using Mbarx IoT Gateway Middleware, End-points and System Manager Tool. Demo Diagram(s) IoT Physical Components Gateways SOC: QorIQ P1020 Dual-Core Communication Processor Boards/Modules: uCP1020 IoT Gateway Module hardware Software: Arcturus Mbarx IoT Gateway middleware Arcturus management middleware  Arcturus PBX/Communications software package Arcturus Mbarx-Operations Controller work-flow management middleware Open source Linux software (Kernel mainline branch) Edge Devices SOC:2x 10/100/1000BaseT networking supported natively by the P1020 processor and on board network PHYs Modules:Various PCIe and miniPCIe based connectivity options (see wireless below) Software:Linux Wireless Connectivity Modules:GSM/LTE/HSPA/UMTS/EVDO data (depending on providers, regions and certifications).  As tested using Telit HE910 family (HEPCHGPS204T701) Modules:Wi-Fi (depending on regions and certifications).  As tested using Atheros AR9390 family. Software:Linux Sensors SOC: Peripheral connectivity supported by SPI, I2C, UART, USB, SDHC, PCIe, miniPCIe Cloud Infrastructure/Services Software/Services: Arcturus Mbarx IoT Gateway middleware is fully compatible with Mbarx IoT end-nodes such as uCMK60 based on K60, K64. Mbarx IoT protocol supports TCP/IP sockets with TLS security and simple character driven protocol Mbarx IoT Gateway middleware supports remote-site aggregation, secure connectivity and device management proxy. Optional plugs-ins for MQTT, CoAP and other popular IoT/M2M protocols. Smart Devices/Apps Software: Mbarx-Operations Controller supports cross-platform work-flow driven, operational control using a responsive HTML5 architecture. Mbarx-System Manager site-wide IoT device/node management tool is available for PCs. IoT System Capabilities Device Management Secure remote site connectivity Remote site IoT node/device aggregation Bulk device firmware updates, bulk configuration, site wide-provisioning Secure IoT node/device management and configuration Cloud/App Communications/Interworking Wi-Fi Access Point (Host AP mode), cellular data Security SSL/TLS 1.1,1.2 server and client with X.509 IoT Development Capabilities Embedded Platforms Kinetis MCUs, QorIQ 32-bit Power Architecture processors Embedded Tools Linux - kernel, driver, middleware and user space application development U-boot development and customization MQX - KSDK Services Customization and system solutions available through direct engagement - contact Arcturus Hardware and software services available - contact Arcturus IoT Product Type Product/Component Vendor Research or Procure This Product/Component End User Hardware Laptop PC Win7, Win8, Win10 or Mac Commercial Laptop PC End User Software Arcturus Mbarx System Manager Tool Commercial Arcturus Mbarx IoT and M2M Solutions End User Smart Device Arcturus uCMK60 - VoIP / IoT Board/Modules Arcturus uCMK64 - IoT Board/Modules Commercial Arcturus uCMK60 - VoIP / IoT Boards/Modules End User Edge Device TP-Link TL-SF1008P 802.3af PoE Switch Commercial TP Link TL-SF1008P End User Edge Device Linksys EA6100 Dual Band Smart Wi-Fi Router Commercial Linksys EA6100 Dual Band Smart Wi-Fi Router Communications Infrastructure
查看全文
Porting Guideline for Zigbee 3.0 application from JN516x to KW41Z This Application Note provides guidance on migrating ZigBee 3.0 Base device application designed for the NXP JN516x wireless microcontrollers to the KW41Z with the help of attached PDF. JN KW41Z31Z21Z ZigBee Software
查看全文
教程:在 S32DS 3.1 上创建新的 ISP 项目 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 索引|上一页| 下一页 有关 S32DS 的更多视频、教程或信息,请访问: https://community.nxp.com/community/s32/s32ds (在 “我的视频” 中查看)
查看全文
Clusters & Infotainment: ハンズオンワークショップ: Qt プログラミング入門 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションは、Qt Frameworkでプログラミングをしたことがない方を対象としています。環境のセットアップから、電卓と温度計ディスプレイの2つの基本的なアプリケーションの開発まで、基本的な手順をご案内します。また、これらのデモと対話する機会もあります。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションは、Qt Frameworkでプログラミングをしたことがない方を対象としています。環境のセットアップから、電卓と温度計ディスプレイの2つの基本的なアプリケーションの開発まで、基本的な手順をご案内します。また、これらのデモと対話する機会もあります。
查看全文
How to move your CodeWarrior suite license Quick guide on how to generte a license with a new host information. ## codewarrior‌ #rehost‌ #codewarrior license‌
查看全文
The Next Wave of Industrial Networking with Time Sensitive Networking (TSN) Industrial OEMs have been hampered by the large array of networking protocols that they need to support in their devices. The new IEEE Time Sensitive Networking (TSN) standard offers to consolidate multiple proprietary protocols with a common IEEE based standard. Come learn what you can achieve with TSN. Industrial OEMs have been hampered by the large array of networking protocols that they need to support in their devices. The new IEEE Time Sensitive Networking (TSN) standard offers to consolidate multiple proprietary protocols with a common IEEE based standard. Come learn what you can achieve with TSN.
查看全文
ジェネレーターアップデート12.27 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 新機能のアップデート: SDKGEN-713 警告する全体的なロガーレベルを変更する ロガーのレベルを「ERROR」から「WARN」に変更しました。このようにして、警告が画面に表示されるため、警告を簡単に取得し、必要に応じて必要なコード変更を加えることができます。 以下はそのスナップショットです。   SDKGEN-683 ステージ1とステージ2で真のプロダクションを再実装 以前は、大量の yml レコードエラーに対応するために、stage1 と stage2 でプロダクションモードを無効にしていました。REL9を通じて、これらのエラーはほぼ修正されました。そのため、stage1 と stage2 のプロダクション モードが戻ってきました。 この製品版モードに詳しくない場合は、SDK Generator の概要と usage.md で詳細な説明をご覧ください。簡単に言うと、プロダクションモードが有効になっている場合、「エラー」が発生すると生成プロセスが中断されます。このモードは通常、正式なデプロイに使用されます。 リリース設定ymlから、"production: true"を設定してすべてのステージで有効にすることができますが、詳細については、設定方法を参照してくださいrelease_config file.md バッチから、ステージ1とステージ2で有効にするために「--production」を設定できますが、後のステージでは今のところバッチからプロダクションを取得できません usage.md
查看全文
从 MCU 到云端的机器学习 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 课程将概述物联网解决方案团队开发的“经典机器学习工具箱”,以及与 Microsoft Azure ML 集成的示例。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 课程将概述物联网解决方案团队开发的“经典机器学习工具箱”,以及与 Microsoft Azure ML 集成的示例。 i.MX 应用处理器
查看全文
Sensor Products for Medical and Industrial Markets Sensors are key to differentiate your products in the market and add context awareness, tamper detection, a robust user interface and accurate media compatibility. This class will step through some of key the leading applications in the Medical and Industrial markets that have found usage of motion and pressure sensors as well as some up and coming applications.  Sensors are key to differentiate your products in the market and add context awareness, tamper detection, a robust user interface and accurate media compatibility. This class will step through some of key the leading applications in the Medical and Industrial markets that have found usage of motion and pressure sensors as well as some up and coming applications. 
查看全文
ADAS & Driver Replacement: Automotive ADAS Update Covering Vision, Radar and Autonomous Systems ADAS roadmaps, value proposition, current and future plans for tools and reference designs. ADAS roadmaps, value proposition, current and future plans for tools and reference designs. Arm® Processors
查看全文
ADAS:スマートアクチュエーター—自動運転車の実現 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 未来の自動運転車は、安全性、信頼性、信頼性に関する新たな要件を打ち立てます。この講演では、将来の車両アーキテクチャに関する結果の要件と、スマートアクチュエータによってそれらがどのように実現されるかを確認します。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 未来の自動運転車は、安全性、信頼性、信頼性に関する新たな要件を打ち立てます。この講演では、将来の車両アーキテクチャに関する結果の要件と、スマートアクチュエータによってそれらがどのように実現されるかを確認します。
查看全文
恩智浦无线充电介绍 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次会议将概述恩智浦无线充电解决方案产品组合以及恩智浦采用 Qi 技术的原因。与会者将清楚地了解适用于汽车应用以及扩展到消费者和基础设施市场的发射器和接收器参考设计。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次会议将概述恩智浦无线充电解决方案产品组合以及恩智浦采用 Qi 技术的原因。与会者将清楚地了解适用于汽车应用以及扩展到消费者和基础设施市场的发射器和接收器参考设计。
查看全文
NXPワイヤレス充電のご紹介 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、NXPのワイヤレス充電ソリューションポートフォリオの概要と、NXPがQiテクノロジーを採用する理由について説明します。参加者は、車載アプリケーション向けのトランスミッタおよびレシーバのリファレンスデザインや、コンシューマ市場やインフラ市場への拡張について明確に理解することができます。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、NXPのワイヤレス充電ソリューションポートフォリオの概要と、NXPがQiテクノロジーを採用する理由について説明します。参加者は、車載アプリケーション向けのトランスミッタおよびレシーバのリファレンスデザインや、コンシューマ市場やインフラ市場への拡張について明確に理解することができます。
查看全文
Kinetis KW41Z入门指南 - BLE/802.15.4 IoT解决方案 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 了解如何开始设计基于 NXP 的 Kinetis KW41Z 多协议 BLE + 802.15.4 无线连接解决方案的蓝牙®低功耗或 Thread IoT 产品。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 了解如何开始设计基于 NXP 的 Kinetis KW41Z 多协议 BLE + 802.15.4 无线连接解决方案的蓝牙®低功耗或 Thread IoT 产品。
查看全文
利用基于 Arm ® Cortex ® -M33 的 LPC5500 MCU 系列实现端到端安全 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 参加本次会议,了解最近推出的 LPC5500 MCU 系列中集成的所有安全功能,并学习如何实现这些功能来设计具有强大安全性的低功耗系统。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 参加本次会议,了解最近推出的 LPC5500 MCU 系列中集成的所有安全功能,并学习如何实现这些功能来设计具有强大安全性的低功耗系统。 Kinetis Cortex ® -M 微控制器
查看全文
RS_Lang_Milestone_4 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> マイルストーン4(20ポイント、1週間):プロジェクトを完了する ビデオカメラからの情報(前方の車両、速度、距離)に基づいて、アプリケーションは、安全な距離と速度値をプリセットにできるだけ近づけるために、車の速度を更新する必要があります。 (マイビデオで視聴)
查看全文
i.MX 8 Fast-Packet Routing Software Presentation of the high-performance packet processing solutions being developed on i.MX processors and expected performance gains compared to a standard software stack. Presentation of the high-performance packet processing solutions being developed on i.MX processors and expected performance gains compared to a standard software stack.
查看全文
車載イーサネットPHY + ソフトウェア <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 車載イーサネットPHYは、必要な物理スループット電力を提供することで、将来の運転シナリオを可能にします。ソフトウェアは、セキュリティ、診断、エネルギー効率、安全性に付加価値をもたらします。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 車載イーサネットPHYは、必要な物理スループット電力を提供することで、将来の運転シナリオを可能にします。ソフトウェアは、セキュリティ、診断、エネルギー効率、安全性に付加価値をもたらします。
查看全文
采用恩智浦智能充电和谐振转换器进行设计 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 对于许多工程师来说,完成可投入生产的智能充电或谐振转换器设计可能是棘手、繁琐甚至具有挑战性的。1. 本次培训的目的是讨论智能充电的设计:介绍智能电源设计工具来解决设计挑战,从而提高转换率。2. 谐振转换器:重点介绍设计人员为了有效设计谐振转换器需要了解的关键要素。介绍了一种基于在线的谐振转换器设计工具,以进一步帮助谐振转换器设计。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 对于许多工程师来说,完成可投入生产的智能充电或谐振转换器设计可能是棘手、繁琐甚至具有挑战性的。1. 本次培训的目的是讨论智能充电的设计:介绍智能电源设计工具来解决设计挑战,从而提高转换率。2. 谐振转换器:重点介绍设计人员为了有效设计谐振转换器需要了解的关键要素。介绍了一种基于在线的谐振转换器设计工具,以进一步帮助谐振转换器设计。 电源管理
查看全文
在 Layerscape 上部署机器学习的五个简单步骤 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在本课程中,您将学习如何使用 Layerscape 系列处理器运用机器学习基础知识。课程内容包括:机器学习基础知识;用于训练的网络和不同模型;样本对象识别训练和推理用例;易于与 LS 平台一起使用进行机器学习。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在本课程中,您将学习如何使用 Layerscape 系列处理器运用机器学习基础知识。课程内容包括:机器学习基础知识;用于训练的网络和不同模型;样本对象识别训练和推理用例;易于与 LS 平台一起使用进行机器学习。 Layerscape 处理平台
查看全文