How to build memtool on i.MX 95 19mm x 19mm Evaluation Kit I am currently working on an i.MX95 platform running Android 16 with kernel version 6.12.52. Could someone guide me on the steps to build memtool? Re: How to build memtool on i.MX 95 19mm x 19mm Evaluation Kit
Hello,
Please check the attached guide. Re: How to build memtool on i.MX 95 19mm x 19mm Evaluation Kit Thanks for your reply. I use static link method mentioned in page4 to successfully build memtool and push into system. evk_95:/data/local/tmp # ./memtool 0x4acf0000 1 E Reading 0x1 count starting at address 0x4ACF0000 According to content from page5 to page12. I modify bsp as follow: (1)git diff arch/arm64/configs/imx95_gki.fragment +CONFIG_DEVMEM=y (2) kernel/configs$ git diff b/android-6.12/android-base-conditional.xml @@ -13,10 +13,10 @@ CONFIG_AEABI y - + CONFIG_OABI_COMPAT n @@ -97,10 +97,10 @@ y - + kernel/configs$ git diff c/android-6.12/android-base-conditional.xml @@ -13,10 +13,10 @@ CONFIG_AEABI y - + CONFIG_OABI_COMPAT n @@ -97,10 +97,10 @@ y - + (3) kernel/configs$ git diff b/android-6.12/android-base.config -# CONFIG_DEVMEM is not set kernel/configs$ git diff c/android-6.12/android-base.config -# CONFIG_DEVMEM is not set After applying three parts patches, I use following commans to rebuild the whole bsp successfully. source build/envsetup.sh lunch evk_95-nxp_stable-userdebug export TARGET_RELEASE=nxp_stable build_build_var_cache ./imx-make.sh -j4 2>&1 | tee build-log.txt The result checked under out folder. out/target/product/evk_95$ cat obj/KERNEL_OBJ/.config | grep "CONFIG_DEVMEM" CONFIG_DEVMEM=y Finally, I execute command to reproduce NXP kernel and produce boot.image: TARGET_IMX_KERNEL=true make bootimage I use SD card to flash image and not able to boot into homescreen. Error message as follow: [ 13.954824][ T1] init: Wait for partitions returned after 10010ms [ 13.961248][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<:string>): partition(s) not found after polling timeout: boot_a, dtbo_a, init_boot_a, metadata, super, vbmeta_a [ 13.979426][ T1] init: Failed to create devices required for first stage mount [ 13.987629][ T1] init: InitFatalReboot: signal 6 [ 13.993865][ T1] init: #00 pc 00000000003d4ed4 /init [ 13.995444][ T14] sdhci-esdhc-imx 42860000.mmc: Adding to iommu group 2 [ 13.999402][ T76] i2c 1-0074: deferred probe pending: pca953x: reg get err [ 14.006372][ T1] init: Reboot ending, jumping to kernel [ 14.007156][ T14] sdhci-esdhc-imx 42860000.mmc: Got CD GPIO [ 14.029979][ T1] kvm: exiting hardware virtualization [ 14.035397][ T1] reboot: Restarting system with command 'bootloader' Have I missed any steps or there are additional steps on imx95 bsp? Re: How to build memtool on i.MX 95 19mm x 19mm Evaluation Kit Please try to rebuild using the Android 16 flow, not the Android 12 PDF flow. Re: How to build memtool on i.MX 95 19mm x 19mm Evaluation Kit Sorry for not replying so long. I have already fix this problem by following steps provide by PDF on imx95 platform. Previous problem might be caused by not doing clean build. I add related change into patch file for anyone want to reference.
View full article