S32K Input Capture Hi Team, We are using S32K146 microcontroller, we need any one input pin as Input capture pin, can you please suggest me with which module should I configure? If I use FTM as signal measurement, am I able to achieve input capture function? Or shall I use ic_pal functionality? Please support Thanks Shruthi C Re: S32K Input Capture Hi Petr, Im unable to use INT_SYS_InstallHandler(FTM0_Ch0_Ch1_IRQn, PWM_InputCapture_IRQHandler, NULL); function as its taking default handler and not taking this handler FTM0_Ch0_Ch1_IRQn My configurations are /* Global configuration of flexTimer_ic_1 InitConfig */ ftm_user_config_t flexTimer_ic_1_InitConfig = { { true, /* Software trigger state */ false, /* Hardware trigger 1 state */ false, /* Hardware trigger 2 state */ false, /* Hardware trigger 3 state */ false, /* Max loading point state */ false, /* Min loading point state */ FTM_SYSTEM_CLOCK, /* Update mode for INVCTRL register */ FTM_SYSTEM_CLOCK, /* Update mode for SWOCTRL register */ FTM_SYSTEM_CLOCK, /* Update mode for OUTMASK register */ FTM_SYSTEM_CLOCK, /* Update mode for CNTIN register */ false, /* Automatic clear of the trigger */ FTM_UPDATE_NOW, /* Synchronization point */ }, FTM_MODE_INPUT_CAPTURE, /* Mode of operation for FTM */ FTM_CLOCK_DIVID_BY_1, /* FTM clock prescaler */ FTM_CLOCK_SOURCE_SYSTEMCLK, /* FTM clock source */ FTM_BDM_MODE_11, /* FTM debug mode */ false, /* Interrupt state */ false /* Initialization trigger */ }; /* Input capture configuration for flexTimer_ic_1 */ ftm_input_param_t flexTimer_ic_1_InputCaptureConfig = { 1U, /* Number of channel configurations */ 65535U, /* Maximum count value */ flexTimer_ic_1_InputCaptureChannelConfig /* Channels configuration*/ }; /* Channels configuration structure for flexTimer_ic_1 input capture */ ftm_input_ch_param_t flexTimer_ic_1_InputCaptureChannelConfig[1] = { { 0U, /* Channel id */ FTM_SIGNAL_MEASUREMENT, /* Input capture operation mode */ FTM_RISING_EDGE, /* Edge alignment mode */ FTM_FALLING_EDGE_PERIOD_MEASUREMENT, /* Signal measurement operation type */ 0U, /* Filter value */ false, /* Filter state (enabled/disabled) */ true, /* Continuous measurement state */ NULL, /* Vector of callbacks parameters for channels events */ NULL /* Vector of callbacks for channels events */ } }; Re: S32K Input Capture Hi,
yes, those functions should be enough. SDK driver enables FTM channel interrupt, right handler should be assigned from startup, I think. If not right handler is FTM0_Ch0_Ch1_IRQHandler.
The FTM_DRV_GetInputCaptureMeasurement is called to get captured value.
BR, Petr Re: S32K Input Capture Hi Petr, Thanks for your neat clarification. Can I use these functions to initialize FTM pin as input capture `FTM_DRV_Init()` `FTM_DRV_InitInputCapture()` And install an IRQ handler for capturing the pulse occurrence `INT_SYS_InstallHandler(FTM0_Ch0_Ch1_IRQn, PWM_InputCapture_IRQHandler, NULL)` Please support Thanks Shruthi C Re: S32K Input Capture Hi,
the most common and efficient way is to configure FTM in input capture mode and use pin which has FTM functionality. Each FTM channel can be configured for input capture mode, where it captures the timer value on an edge (rising, falling, or both) of the input signal. This is commonly used for measuring: signal period, pulse width, frequency.
The IC PAL driver allows to detect the input signal and measure pulse width or period of the channel input signal. It was designed to be portable across all platforms and IPs which support FTM , eMIOS, FLEXPWM and ETIMER.
So if you want full control and performance use FTM directly. If you want simpler code and portability use IC PAL.
BR, Petr
Re: S32K Input Capture Hi,
there is SDK example you can refer to directly (ftm_signal_measurement). Or share simplified project showing the issue.
BR, Petr Re: S32K Input Capture HI, In SDK example I referred to directly (ftm_signal_measurement). In this example they did not used Interrupt method they used polling method then they called FTM_DRV_GetInputCaptureMeasurement Im looking for FTM signal measurement with interrupt, once input capture recognizes the signal, I need interrupt to be triggered and call FTM_DRV_GetInputCaptureMeasurement function in ISR Can u pls provide code for this Thanks Shruthi C Re: S32K Input Capture Hi,
if you need to install handler again you should have
extern void FTM0_Ch0_Ch1_IRQHandler(void);
INT_SYS_InstallHandler(FTM0_Ch0_Ch1_IRQn, FTM0_Ch0_Ch1_IRQHandler, NULL);
BR, Petr Re: S32K Input Capture Hi, Yes I do have that function defined, but after that the function call goes to infinite loop, and it will run further Shruthi_C_0-1764752920959.png The whole system will not work, Thanks Shruthi C Re: S32K Input Capture Hi, Thanks for your support, and code snippet, I will check T&R, Shruthi C Re: S32K Input Capture Hi, Can I get any input for interrupt enabled FTM pin as input capture Thanks Shruthi C Re: S32K Input Capture Hi,
driver is using interrupt for capture event, only not shown in example directly. I modified FTM IC setting to use one shot mode and add Callback, which is called from driver interrupt.
PetrS_0-1764845224420.png
See attached for modified main.c of ftm_signal_measurement_s32k146 demo.
BR, Petr
記事全体を表示