JTAG on FRDM iMX95 Hi all, I just bought FRDM iMX95 recently, i am curious about how to use JTAG to debug this board As check in schematic it has JTAG exposed at 6 test point pin here At board layout it here How should i connect jtag to it, do i need any rework ? And does this JTAG support to debug all A55, M33, and M7 core ? Which device should i use here, it seem we have 6 pin needle but it 2x3 not 1x6 I would appreciate any guide or docment to set up JTAG Thank you !! Linux Re: JTAG on FRDM iMX95 Hello,
Your understanding is correct.
As you can see in schematic is needed to add the DNP resistors and a connector for the debugger.
Best regards. Re: JTAG on FRDM iMX95 Hello, Thank you for your confirmation @JorgeCas Summary : Please help with JTAG problem ""DAP: Could not power-up system power domain."" I have done the rework for 3 resistor and measure the pin, it successfully pull up. One note that to enable JTAG, i need to disable LPUART5 in device tree because it use the same pin (i follow the same modify as imx95-19x19-jtag.dtb ) or else TMS (Test point 49) will always LOW) diff --git a/arch/arm64/boot/dts/freescale/imx95-15x15-frdm.dts b/arch/arm64/boot/dts/freescale/imx95-15x15-frdm.dts
index c45f28efb568..598e16af0ebd 100644
--- a/arch/arm64/boot/dts/freescale/imx95-15x15-frdm.dts
+++ b/arch/arm64/boot/dts/freescale/imx95-15x15-frdm.dts
@@ -520,7 +520,7 @@ &lpuart5 {
/* BT */
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart5>;
- status = "okay";
+ status = "disabled";
bluetooth {
compatible = "nxp,88w8987-bt"; After this i need to find the connector with 1.27mm pin. It take me some time to find this pcb test by pogo pin, it has 6 pin, perfectly fit. Here is my current setup It seem a mess but the connection is not problem, i check the HWStatus and it look good J-Link>ShowHWStatus
VTref=3.324V
ITarget=0mA
TCK=1 TDI=1 TDO=0 TMS=0 TRES=1 TRST=1
Supported target interface speeds:
- 120 MHz/n, (n>=8). => 15000kHz, 13333kHz, 12000kHz, ...
- Adaptive clocking I try connect it by these 2 command for A55 and M33 but same issue show is "DAP: Could not power-up system power domain." zk47@ltu:~$ JLinkExe -device MIMX9516_M33 -if JTAG -speed 200
SEGGER J-Link Commander V9.42 (Compiled May 6 2026 12:36:02)
DLL version V9.42, compiled May 6 2026 12:35:00
zk47@ltu:~$ JLinkExe -device MIMX9516_A55 -if JTAG -speed 200 What could i do wrong here ? Maybe it fall to my JLink device is not good, can MCU-Link Pro replace it ? Can MCU-Link Pro debug both A55 and M core ? I would still prefer do the debug through JTAG because i already had it. Please help If you guy plan to add document guide for JTAG on FRDM iMX95, please update it soon like FRDM iMX93. Re: JTAG on FRDM iMX95 Dear @JorgeCas Any update ? Can i use MCU-Link Pro to debug all core A55, M33 and M7 core ? Re: JTAG on FRDM iMX95 Hello,
I apologize for the delay.
We suggest you any debugger from MACRAIGOR Systems, Wind River or any of ARM.
NXP team uses Lauterbach Trace32 as debugger tool for Cortex-A cores, J-link is for Cortex-M cores.
In the case of i.MX95, as prerequisite to use the CM7 or CA55 scripts the SM should be already running on the i.MX device. it has the CM33 for resource management and security reasons, it's open source, it's compliant to a HW resource management standard by ARM, and its code it's meant (between a lot of them) to partition hardware, assign resources to either Cortex-A or Cortex-M7.
You can use this document as reference.
Debugging Cortex-M with VS Code on i.MX 8M, i.MX 8ULP, and i.MX 9
If you still having issues after this considerations, please look for hardware issues in your adapter.
Best regards. Re: JTAG on FRDM iMX95 Dear @JorgeCas Thank you for your reply. Okay so the hardware could be the problem, but i am still wonder these thing Can i have a picture for your setup debug ? I am not sure what is the official way to connect to these test point. does we need to use kind of this 2. The docs only for Debug core M, not core A. Can you give me more guide for "Debug core A linux using Trace32 or JLink or MACRAIGOR " as you said ? 3. Not relate to this thread, but can i have the estimated release date for FRDM iMX95 Pro ? Re: JTAG on FRDM iMX95 Hello,
1. Our available boards for testing are not modified since if JTAG is needed, we use EVK instead FRDM boards. The recommended approach is use shorter wires as possible between the boards and debugger to warranty a good connection and signal integrity.
As you can see in this post, the issue was solved with shorter cables soldered to the board.
2. This information is in probe manual since each manufacturer uses their process and scripts to connect with the processor. There is no documentation in our side regarding these probes connection.
3. Unfortunately we do not have this information, I suggest you check our official web site for further updates.
Best regards. Re: JTAG on FRDM iMX95 @Zk47T Hi, I was wondering if you managed to succeed in debugging the cortex cores on the board, and if you have any advice that you're able to share with me. I'm currently facing the same issues trying to debug the M7 core, and any help would be appreciated. Thanks Re: JTAG on FRDM iMX95 Dear @bbggl I still can't make it work on FRDM iMX95 board. And as i upgrade to FRDM iMX95 Pro which even have more mess up pin layout. I don't pursue the JTAG on these board any more As suggest by @JorgeCas , you should ask the author on this thread as they say they successfully make it work. Re: JTAG on FRDM iMX95 Thanks you for the reply, I have reached out to the other author. What did you decide on for your debugging setup? Is there another device like the MCU link or EVK board that works better, or have you used alternate methods? Re: JTAG on FRDM iMX95 Hi, After all, seem like it really the wire issue. I solder directly jumper with copper wire to the JTAG test point, then connect from CH347F module and it did work. I can even able to get some ETM trace here
View full article