NXP MIMXRT1062DVL6B
regarding toy design.
In regards to your unit number: NXP MIMXRT1062DVL6B
a powerful 600MHz CortexM7 and it may be more then I need.
I am using it to only to recognize a two word phrase. IS there a least expensive NXP processor that can reliably run VIT + two microphones + a custom wake phrase?
Would appreciate an email to discuss: [email protected]
Hi @toy_maker ,
Thanks for your questions!
Please refer to the list of supported part numbers provided by VIT.
Gavin_Jia_0-1785724846969.png
Also, the discussion in this thread should be helpful: https://community.nxp.com/t5/MCX-Microcontrollers/Wake-Word-and-Voice-command-engines/m-p/2054222
For more information about MCXN, we recommend that you post your question in the relevant community forum. Thank you!
Best regards,
Gavin