Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Recover bricked imxrt1024 board I have one board that is bricked and i also tried to recover the board by performing below steps. 1. Change Boot Mode to Serial Downloader mode. 2. Via UART, Erase the chip and then flash a good bootable image (led_blinky). 3. Change the boot mode again, But the device is not recovered. Using j-link commander i am getting this issue 'loadbin': Performing implicit reset & halt of MCU. ResetTarget() start Core did not halt on flash image verification. Assuming faulty flash settings. Halting target manually. ResetTarget() end - Took 329ms Device specific reset executed. AfterResetTarget() start MPU was enabled and is now disabled. AfterResetTarget() end - Took 2.92ms Downloading file [C:\M7Binaties Prep\Secure Boot extebded implementation\M7SafetBoot+Combined_SignedPackage.bin]... Error while programming flash: Programming failed. Also there is one additional observation ;- 1. Device put on serial downloader mode. 2. Flash the led blinky image. 3. Read back the image in serial mode only  4. I can able to see that the binary is successfully flashed  After that i put in Internal Boot Mode  5. Read back using J_Flash but now whole flash region is 0 What to do now , why i am not able to recover it Re: Recover bricked imxrt1024 board Hello @Abhay2080, In order to support you better, could you please provide the following details? Are you currently using a custom board or our EVK? Was the LED blinky example modified before flashing? Have any fuses been burned on this device previously? Looking at the J-Link log, it appears you are trying to flash a signed image. Has Secure Boot been enabled on this board before? Are you currently using the Secure Provisioning Tool to write the image and perform a mass erase? Could you please test the debugger connection using the Connection With Target Processor feature and let me know your results? BR Habib Re: Recover bricked imxrt1024 board Hello @Abhay2080, Since HAB is enabled, the image must be signed with the private key and must contain the corresponding public keys within the program image, as mentioned in chapter 9.2 "Overview" of the Reference Manual. If the comparison between the reference hash value and the current hash value calculated from the software in flash does not match, or if the image is not signed at all, authentication will fail and the device will not boot, as mentioned in the chapter 7.3.1 "HAB process flow" of the RM. Could you please confirm whether you are flashing the LED blinky signed with the correct keys, and let me know the steps you followed to sign this image and how you enabled the HAB? Also, could you clarify if the error started occurring right when you enabled HAB? BR Habib Re: Recover bricked imxrt1024 board 1. Custom Board. 2. No led blinky is not modified, even i tried with my working project also. 3. Yes device have HAB enabled . SEC_CONFIG and SRK_HASH are fused 4. Yes HAB is enabled. 5. Yes SPT is used. 6. Yes i am able to connect with target Re: Recover bricked imxrt1024 board Hi @Habib_MS  I do understand that since HAB is enabled only signed image can boot but the issue here is i am not able to flash any image.  Also i have one observation that when i am ersing the flash using SPT even i am selection whole flash region 4MB but in the logs i am getting Detected erasable block size : 0x1000 . Please find the screenshot attached. And moreover i tried flashing signed led blink image also but still board is not recovered Re: Recover bricked imxrt1024 board Hello @Abhay2080, This Erasable block size Defines the minimal erasable block size. This value is read from FCB if available or from the boot memory configuration for memories that do not use FCB. As mentioned on the Flash Programmer section. SPT erases all sectors across the full memory range, so the entire 4 MB of flash is erased. To help determine whether the issue is related to the J-Flash programming algorithm, could you please follow the steps mentioned in the Booting authenticated (HAB) image section using the pre-built .s19 file called "mimxrt1024evk_iled_blinky_flash.s19" signed with the correct keys and let me know your results ? BR Habib Re: Recover bricked imxrt1024 board Hi @Habib_MS , As mentioned by you i tried the iled_blink.s19 signed image and write the image. Below are the steps i did  i write the image but still i am not able to flash the binary using J-flash
View full article
关于 FS2643D 空白 OTP 变体 OTP 编程的查询 您好, 我计划在我的 24 V 应用中使用 FS2643D 型号,特别是 MFS2643HMDA0AD 空白 OTP 型号。 我了解到 KITFS26SKTEVM 插座板可用于 OTP 配置和编程。但是,使用插座板可能会使工作流程复杂化,因为需要将 IC 放入插座中进行编程,然后再将其焊接到目标 PCB 上。 是否有其他方法可以使用外部编程器或目标板直接在目标 PCB 上配置和编程 OTP,而无需 KITFS26SKTEVM 插座板? 请问这种方法是否可行,并能否推荐一个合适的解决方案? https://www.nxp.com/part/MFS2643HMDA0AD 谢谢。 Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant 你好,萨克希, 对于原型设计,建议使用插座板、我们的其他硬件和 NXP Ringo GUI 进行基准测试。设计原型板时,请参考 FS26 数据手册和我们的其他文档。尤其是AN12995。 要下载这些机密文件,您需要与 NXP 签订有效的保密协议。如果您还没有保密协议,并且想要签署一份,请在此处创建一个新工单,恩智浦代表将协助您完成该流程。 如果没有 FS26 数据表和其他机密文件,就无法使用 FS26。 一旦您有了原型原理图,我们就可以帮您检查了。请注意,我们不检查布局。或者您可以联系我们的授权代理商,他们有工程师可以帮您检查原理图。 最诚挚的问候, 约瑟夫 Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant 嗨,约瑟夫, 感谢您的反馈。由于我们目前处于原型制作阶段,因此我们的初始产量较低,我们主要专注于台式评估和系统验证。 鉴于目前处于小批量原型阶段,您能否与我们联系,告知我们您建议我们如何进行首批电路板的开发?您建议我们与授权代理商(例如 Arrow 或 Avnet)合作进行小批量编程,还是您建议采用其他途径进行早期基准测试? 我们希望在开发定制目标原型时,确保符合 NXP 的功能安全和验证准则。 此致, Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant 你好,萨克希, 请注意,我们的评估板和插座板仅设计用于评估我们的元器件,并且推荐用于此用途。只有 NXP 或我们授权的代理商才能对我们的元器件进行 OTP 编程。根据特定元器件的年产量而定。请告知您使用 FS2643D 空白 OTP 变体的项目的年度产量。 我们不允许客户对我们的元器件进行OTP编程。如果客户自行编程,我们不保证这些元器件的安全性和正确性。 最诚挚的问候, 约瑟夫
View full article
i.MX95 LPDDR4x READ simulation pass/fail criteria specifically Hi Team for the Processor i.MX95 can i have LPDDR4x Read Timing margins & simulation pass/fail criteria Automotive Industrial
View full article
KinetisとLPC用のデバッグインターフェースのおすすめはありますか? 私は主にKinetisシリーズで開発をしており、近い将来LPCのパーツもいくつか手がけるかもしれません。P&E Microのデバッグインターフェースが引き出しいっぱいにあり、よく使っているCyclone ACPも含まれています。 時々、600ドルのCycloneから20ドルのLPC-Link2に切り替えることがあります。なぜなら、CycloneはMCUXpressoに多くの奇妙な問題があるからです。正直なところ、LPC-Link2は私の必要な機能のほとんどを満たしてくれるのですが、少し動作が遅いのが難点です。 Seggerインターフェースを検討しるべきでしょうか?MCUXpresso(そしてできればCodeWarrior 11でも)で十分にサポートされ、クラッシュや走行中のターゲットを止められない信頼性が高く、そこそこ高速なインターフェースを誰かおすすめできませんか?トレースサポートがあれば助かります。 よろしくお願いします! Re: Debug interface recommendations for Kinetis and LPC? こんにちは、@swetie42 さん。 NXP製品にご関心いただきありがとうございます。 あなたの用途には、MCU-Link Pro Debug Probeを検討してみてください。 標準のCMSIS-DAPファームウェアを使用したMCUXpresso IDEと良好に動作し、ベースのMCU-Linkとは異なり、MCU-Link ProはJ-Link LITEのファームウェアオプションも提供しています。CodeWarriorはJ-Linkをサポートしているため、Kinetisデバイス上でMCUXpresso IDEとCodeWarriorの両方を扱う必要がある場合に役立ちます。 MCU-Link ProはSWOプロファイリングもサポートし、エネルギー測定やアナログ信号監視などの追加機能も提供しています。   もちろん、SEGGERのエコシステムを好む場合や、より高度なデバッグ/トレース機能が必要な場合は、SEGGER J-Linkも良い選択肢です。正確なトレース能力はプローブモデルとターゲットデバイスによって異なります。詳細については、直接Seggerサポートにお問い合わせください:チケット |SEGER - The Embedded Experts(組み込みエキスパート)   つまり、一言で言えば、まずMCU-Link Proを検討する価値があると思います。   お役に立てば幸いです。   BR セレステ
View full article
S32K358 MC33FS6523CAE(FS6500 SBC)を用いた電源設計 Hello 私はS32K358を使用して設計しており、MC33FS6523CAEシングルボードコンピュータを使用する予定です。これはサポートされている組み合わせですか?また、S32K3の内蔵SMPSを考慮すると、VDD_HV_A/B、VREFH、V15にはどのSBC出力(VCORE、VCCA)を推奨しますか? よろしくお願いします。 https://www.nxp.com/products/FS6500?page=9&nrnd=false Re: S32K358 power supply design with MC33FS6523CAE (FS6500 SBC) こんにちは、サクシさん。 MC33FS6523CAEは、S32K358と互換性のあるシングルボードコンピュータです。しかしながら、以下に述べる理由から、S32K358に推奨するコンパニオンSBCはFS26であることを強調しておきたいと思います。 FS26は、S32K3シリーズ(S32K358を含む)向けに設計された専用のセーフティSBC取り付けソリューションです。S32K358デザインに特に関連するいくつかの利点を提供します。 - 専用のドキュメント:AN13850(FS26実装および動作)にはFS26とS32K358の接続に関する明示的なセクションが含まれています。 - ASIL D機能安全保障:FS26ファミリはS32K3搭載のASIL Dアプリケーション向けに特別に開発・検証されており、専用のRTDソフトウェアドライバとセーフティアプリケーションノートの組み合わせが本番環境で利用可能です。 - より高い電流LDO出力:FS26のLDO1とLDO2は、VDD_HV_AとVDD_HV_BをS32K358に直接供給します。当社のFRDM-A-S32K358評価ボードはFS26を伴うSBCとして使用しており、LDO1はVDD_HV_A(+3.3 V)、LDO2はVDD_HV_B(+3.3 V)を供給しています。 - 既製品ソフトウェア:S32K3 + FS26向けの本番対応RTDパッケージが利用可能で、ソフトウェア開発の労力を大幅に削減します。 MC33FS6523CAEは、単一のSBCパッケージに統合されたCAN FD + LINトランシーバが必要な場合、S32K358としてサポートされ機能的なSBCの選択肢として依然として存在します。 BRs、トーマス
View full article
采用 MC33FS6523CAE (FS6500 SBC) 的 S32K358 电源设计 Hello 我正在使用 S32K358 进行设计,并计划使用 MC33FS6523CAE SBC。这种搭配是否受支持?考虑到S32K3内部采用开关电源,您推荐将VDD_HV_A/B、VREFH和V15分别连接到哪些SBC输出(VCORE、VCCA)? 谢谢! https://www.nxp.com/products/FS6500?page=9&nrnd=false Re: S32K358 power supply design with MC33FS6523CAE (FS6500 SBC) 你好,萨克希, MC33FS6523CAE 是与 S32K358 兼容的 SBC。不过,我想强调的是,我们推荐与 S32K358 搭配使用的 SBC 是 FS26,原因如下所述。 FS26 是专为 S32K3 系列(包括 S32K358)设计的功能安全 SBC 连接解决方案。它为S32K358设计提供了一些特别相关的优势: - 专用的参考文档:AN13850(FS26 实现和行为)包含一个专门介绍 FS26 与 S32K358 连接的章节。 -ASIL D 功能安全覆盖范围:FS26 系列专用的 ASIL D 应用而开发和验证,采用 S32K3,并配备专用的 RTD 软件驱动程序和安全应用笔记组合,可随时用于生产。 - 更高电流的 低压差线性稳压器\(LDO\) 输出:FS26 低压差线性稳压器\(LDO\)1 和 LDO2 直接向 S32K358 提供 VDD_HV_A 和 VDD_HV_B。我们的 FRDM-A-S32K358 评估板使用 FS26 作为配套 SBC,其中 LDO1 提供 VDD_HV_A (+3.3 V),LDO2 提供 VDD_HV_B (+3.3 V)。 - 现成的软件:适用于 S32K3 + FS26 的生产就绪 RTD 软件包已可用,大大减少了软件开发工作量。 如果您需要在单个 SBC 封装中集成 CAN FD + LIN 收发器,MC33FS6523CAE 仍然是 S32K358 的一个受支持且功能齐全的 SBC 选择。 BRs,托马斯
View full article
i.MX95 LPDDR4x 读取模拟通过/失败标准 大家好 对于 i.MX95 处理器,能否提供 LPDDR4x读取时序裕量和仿真通过/失败标准? 汽车电子 工业控制
View full article
MIMXRT700-EVK 刷写错误 你好, 我无法使用 NXP LinkServer 将我的应用程序刷写到MIMXRT700-EVK上。 硬件/软件: 电路板:MIMXRT700-EVK MCU:MIMXRT798S 调试器:板载 MCU-Link MCU-Link固件版本:V3.172 链接服务器:26.6.137 操作系统:Ubuntu Linux 电源通过 J54 提供 刷写过程中,LinkServer 报告: Error: Wire Ack Fault - target connected? Error: Wire not connected Failed on connect: Ee(42). Could not connect to core. No connection to chip's debug port Flash operation exited with code 1 PC 可以正确检测到 MCU-Link,LinkServer 可以检测到探针。 重要的硬件观察结果是D4红色LED指示灯不亮。根据MIMXRT700-EVK文档,D4指示MCU/RESET状态,其中ON表示处理器正常活动,OFF表示处理器处于RESET状态。 我还执行了RT700预连接脚本,但SWD连接仍然失败,并显示以下错误: Error: Wire Ack Fault - target connected? Error: Wire not connected 支持请求 请问您能否提供以下建议: 为什么 当电路板通过 J54 供电时, D4 LED 灯不亮 ? 如何使RT700处理器退出RESET状态? 是否需要检查任何RESET、启动或硬件配置? 我应该使用哪种恢复程序来恢复LinkServer 的连接,以便我可以刷写应用程序? 评估板 Re: MIMXRT700-EVK Flashing Error 嗨@Aparna1 , 电源很可能没有正确分配给 MCU/电路板的其他部分,而是只分配给了板载调试器。 绿色的D10 LED指示灯也熄灭了吗? 请确保 J2 的跳线位置将引脚 7 和 8 短接。 BR, 埃德温。 Re: MIMXRT700-EVK Flashing Error 您好, 是的,我已经核实了以下内容: 绿色D10 LED指示灯亮起。 J2 将引脚 7 和 8 短接。 如果还需要我进行任何额外的检查,请告知。 问候, 阿帕娜 Re: MIMXRT700-EVK Flashing Error 这是连接 USB 后的状态 Re: MIMXRT700-EVK Flashing Error 您好, 请问我的工单有什么最新进展吗?我仍在等待回复。   谢谢!     Re: MIMXRT700-EVK Flashing Error 您好, 请问我的工单有什么最新进展吗?我仍在等待回复。   谢谢!   Re: MIMXRT700-EVK Flashing Error 您好, 请问我的工单有什么最新进展吗?我仍在等待回复。   谢谢!
View full article
iMX95 - EMMC 部件确认 大家好, 我们为 128GB EMMC 部件提供了两种替代方案。请问以下部件是否可以与IMX95一起使用? BIWIN零件 - BWEFMA128GN9KC SANDISK 零件 - SDINBDA6-128G-ZA 此致, 因德拉吉特·S Re: iMX95 - EMMC Part confirmation 你好@indrajith_shanmugam , 对于 eMMC i.MX95,支持 eMMC 5.1,没有特殊需求。 在这里,您可以根据 i.MX95 usdhc1 的接口需求来修改 emmc 数据表,这样就可以了。 希望这对您有所帮助。 如有任何疑问,请随时与我联系。 祝你今天过得愉快 顺祝商祺! Rita
View full article
MIMXRT700-EVK フラッシュエラー こんにちは、 NXP LinkServerを使って MIMXRT700-EVK にアプリケーションをフラッシュできません。 ハードウェア/ソフトウェア: ボード: MIMXRT700-EVK MCU:MIMXRT798S デバッガ:搭載MCU-Link MCU-Linkファームウェア:V3.172 リンクサーバー: 26.6.137 OS:Ubuntu Linux 電源はJ54から供給されます。 フラッシュ処理中、LinkServerは以下を報告します。 Error: Wire Ack Fault - target connected? Error: Wire not connected Failed on connect: Ee(42). Could not connect to core. No connection to chip's debug port Flash operation exited with code 1 MCU-LinkはPCによって正しく検出され、LinkServerはプローブを検出できます。 重要なハードウェアの観察点は、D4の赤いLEDが点灯していないことです。MIMXRT700-EVKのドキュメントによると、D4はMCU/リセットの状態を示し、ONは通常のプロセッサ活動、OFFはプロセッサがリセット中であることを示します。 RT700のプリコネクトスクリプトも実行しましたが、SWD接続は依然として以下のエラーで失敗します。 Error: Wire Ack Fault - target connected? Error: Wire not connected サポートリクエスト 何かアドバイスをいただけますか: 基板がJ54から電源供給されているのに、 D4 LEDが消灯しているのはなぜですか? RT700プロセッサをリセット状態からどうやって解除 できますか? リセット、起動、またはハードウェア構成の確認が必要な項目はありますか? アプリケーションをフラッシュするためにLinkServerのコネクティビティを復元するには、どのような復旧手順を使えばよいでしょうか? 評価ボード Re: MIMXRT700-EVK Flashing Error こんにちは、@Aparna1 さん。 おそらく、電力がMCUや基板全体に適切に分配されておらず、搭載デバッガにだけ送られている可能性が高いです。 緑色のD10 LEDも消灯していますか? J2のジャンパー位置がピン7と8をショートさせていることを確認してください。 BR、 エドウィン。 Re: MIMXRT700-EVK Flashing Error これはUSB接続後の状態です Re: MIMXRT700-EVK Flashing Error こんにちは、 はい、以下の点を確認しました。 緑色のD10 LEDが点灯しています。 J2はピン7と8を短絡させている。 私の方で追加の確認が必要な場合はお知らせください。 よろしくお願いいたします。 アパルナ Re: MIMXRT700-EVK Flashing Error こんにちは、 チケットの状況を教えていただけますか?まだ返答を待っています。   よろしくお願いします。     Re: MIMXRT700-EVK Flashing Error こんにちは、 チケットの状況を教えていただけますか?まだ返答を待っています。   よろしくお願いします。   Re: MIMXRT700-EVK Flashing Error こんにちは、 チケットの状況を教えていただけますか?まだ返答を待っています。   よろしくお願いします。
View full article
iMX95 - EMMC Part confirmation Hi team, We have two alternate part suggestion for 128GB EMMC part. Can you please confirm we can use below parts with IMX95? BIWIN part - BWEFMA128GN9KC SANDISK part - SDINBDA6-128G-ZA Regards, Indrajith S Re: iMX95 - EMMC Part confirmation Hi @indrajith_shanmugam , For the emmc i.MX95 support the emmc 5.1, and do not have special need. Here you make the emmc datasheet fit for the need for the interface of the i.MX95 usdhc1  will be OK. Hope this can do help for you Any questions please contact me freely Wish you have a nice day Best Regards Rita
View full article
i.MX95 LPDDR4x READシミュレーションの合否判定基準 こんにちは、チームの皆さん。 プロセッサi.MX95の場合、LPDDR4x の読み取り タイミングマージンとシミュレーションの合格/失敗基準を設定できますか? オートモーティブ インダストリアル
View full article
Debug interface recommendations for Kinetis and LPC? I do most of my development on the Kinetis series, and potentially some LPC parts in the near future. I've got a drawer full of debug interfaces from P&E Micro, including a Cyclone ACP that I use most. I sometimes find myself switching from the $600 Cyclone to the $20 LPC-Link2 because the Cyclone has so many weird problems with MCUXpresso. Honestly the LPC-Link2 does most of what I need, it's just a bit slow. Should I be looking at Segger interfaces? Can someone recommend a reliable, reasonably fast interface that's well-supported in MCUXpresso (and hopefully CodeWarrior 11 as well) that doesn't cause crashes all of the time, or fail to halt a running target? Trace support would be nice. Thanks! Re: Debug interface recommendations for Kinetis and LPC? Hello @swetie42 , Thanks for your interest in NXP products.  For your use case, I would suggest taking a look at MCU-Link Pro Debug Probe. It works well with MCUXpresso IDE using the standard CMSIS-DAP firmware, and unlike the base MCU-Link, MCU-Link Pro also provides a J-Link LITE firmware option. Since CodeWarrior supports J-Link, this can be useful if you need to work with both MCUXpresso IDE and CodeWarrior on Kinetis devices. MCU-Link Pro also supports SWO profiling and provides additional features such as energy measurement and analog signal monitoring.   Of course, a SEGGER J-Link is also a good option if you prefer the SEGGER ecosystem or need more advanced debug/trace capabilities. The exact trace capability will depend on the probe model and the target device. For more details, I suggest you directly contact Segger support: Ticket | SEGGER - The Embedded Experts   So, in a word, I think MCU-Link Pro would be worth considering first.   Hope it helps.   BR Celeste
View full article
MIMXRT700-EVK Flashing Error Hi, I am unable to flash my application to the MIMXRT700-EVK using NXP LinkServer. Hardware/Software: Board: MIMXRT700-EVK MCU: MIMXRT798S Debugger: On-board MCU-Link MCU-Link firmware: V3.172 LinkServer: 26.6.137 OS: Ubuntu Linux Power is supplied through J54 During flashing, LinkServer reports: Error: Wire Ack Fault - target connected? Error: Wire not connected Failed on connect: Ee(42). Could not connect to core. No connection to chip's debug port Flash operation exited with code 1 The MCU-Link is detected correctly by the PC, and LinkServer can detect the probe. The important hardware observation is that the D4 red LED is not glowing. According to the MIMXRT700-EVK documentation, D4 indicates the MCU/reset status, where ON indicates normal processor activity and OFF indicates that the processor is in reset. I also executed the RT700 preconnect script, but the SWD connection still fails with: Error: Wire Ack Fault - target connected? Error: Wire not connected Support Request Could you please advise: Why is the D4 LED OFF when the board is powered through J54? How can I bring the RT700 processor out of the reset state? Is there any required reset, boot, or hardware configuration that needs to be checked? What recovery procedure should I use to restore LinkServer connectivity so that I can flash the application? Evaluation Board Re: MIMXRT700-EVK Flashing Error Hi @Aparna1, It's likely that the power is not being properly distributed to the MCU/rest of the board, but rather just to the on-board debugger. Is the green D10 LED also OFF? Please make sure that the jumper position of J2 is shorting pins 7 and 8. BR, Edwin. Re: MIMXRT700-EVK Flashing Error Hi, Yes, I have verified the following: The green D10 LED is ON. J2 is shorting pins 7 and 8 . Please let me know if any additional checks are required from my side. Regards, Aparna Re: MIMXRT700-EVK Flashing Error    This is the Status after connecting USB  Re: MIMXRT700-EVK Flashing Error Hi, could you please provide an update on my ticket? I am still waiting for a response.   Thank you.     Re: MIMXRT700-EVK Flashing Error Hi, could you please provide an update on my ticket? I am still waiting for a response.   Thank you.   Re: MIMXRT700-EVK Flashing Error Hi, could you please provide an update on my ticket? I am still waiting for a response.   Thank you.
View full article
S32K358 power supply design with MC33FS6523CAE (FS6500 SBC) Hello I’m designing with the S32K358 and plan to use the MC33FS6523CAE SBC. Is this a supported pairing, and which SBC outputs (VCORE, VCCA) do you recommend for VDD_HV_A/B, VREFH and V15, given the S32K3 internal SMPS?  Thanks https://www.nxp.com/products/FS6500?page=9&nrnd=false Re: S32K358 power supply design with MC33FS6523CAE (FS6500 SBC) Hello Sakshi, The MC33FS6523CAE is a compatible SBC for the S32K358. However, I would like to highlight that our recommended companion SBC for the S32K358 is the FS26, for the reasons outlined below. The FS26 is the purpose-designed safety SBC attach solution for the S32K3 series, including the S32K358. It offers a number of advantages specifically relevant to S32K358 designs: - Dedicated reference documentation: AN13850 (FS26 Implementation and Behaviors) includes an explicit section on FS26 connection to the S32K358.  -ASIL D functional safety coverage: The FS26 family is specifically developed and validated for ASIL D applications with S32K3, with a dedicated RTD software driver and safety application note combination ready for production use. - Higher current LDO outputs: FS26 LDO1 and LDO2 directly supply VDD_HV_A and VDD_HV_B to the S32K358. Our FRDM-A-S32K358 evaluation board uses the FS26 as the companion SBC, with LDO1 supplying VDD_HV_A (+3.3 V) and LDO2 supplying VDD_HV_B (+3.3 V). - Ready-made software: A production-ready RTD package for S32K3 + FS26 is available, significantly reducing software development effort. The MC33FS6523CAE is still a supported and functional SBC choice for S32K358 if you require integrated CAN FD + LIN transceivers in a single SBC package. BRs, Tomas
View full article
iMX95 - EMMC部品確認 チームの皆さん、こんにちは。 128GBのeMMC部品については、代替部品を2つご提案できます。以下の部品をIMX95で使えるか確認していただけますか? BIWIN部品番号 - BWEFMA128GN9KC サンディスク部品 - SDINBDA6-128G-ZA よろしくお願いいたします。 インドラジットS Re: iMX95 - EMMC Part confirmation こんにちは、 @indrajith_shanmugam さん。 emmc i.MX95はemmc 5.1をサポートしており、特別な必要性はありません。 ここでは、iのインターフェースのニーズに合ったemmcのデータシートを作ってください。MX95のusdhc1は問題ありません。 これがあなたの役に立てば幸いです ご質問があれば、どうぞお気軽にお問い合わせください 素敵な一日をお過ごしください よろしくお願いいたします。 リタ
View full article
Query Regarding OTP Programming of FS2643D Blank OTP Variant Hi, I am planning to use the FS2643D variant, specifically the MFS2643HMDA0AD blank OTP variant, for my 24 V application. I understand that the KITFS26SKTEVM socket board can be used for OTP configuration and programming. However, using the socket board may complicate the workflow, as the IC needs to be placed in the socket for programming and then soldered onto the target PCB. Is there an alternative method to configure and program the OTP directly on the target PCB using an external programmer or target board, without requiring the KITFS26SKTEVM socket board? Could you please advise whether this approach is supported and recommend a suitable solution? https://www.nxp.com/part/MFS2643HMDA0AD Thanks. Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant Hi Sakshi, for prototyping, using the socket board, our other hardware and the NXP Ringo GUI is recommended for benchmarking. For designing your prototype board, please follow the FS26 datasheet and our other documents. Especially the AN12995.  To be able to download these confidential documents, you need to have a valid NDA with NXP. If you have not an NDA yet and you would like to sign one, please create a new ticket here and an NXP representative for NDA matters will help you with the process.  Without the FS26 datasheet and other confidential documents would not be possible to work with the FS26. Once you will have your prototype schematic, we can check it for you. Please note, we do not check layouts. Alternatively you can contact our authorized distributors, they have engineers who can also check the schematic for you. With Best Regards, Jozef Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant Hi Jozef, Thank you for the feedback. Since we are currently in the prototyping phase, our initial volume count is low, and we are focused strictly on bench evaluation and system validation. Given that this is a low-volume prototype phase, could you let us know how you recommend we proceed for our initial boards? Do you recommend we work with an authorized distributor (such as Arrow or Avnet) to get a small batch programmed, or is there an alternative path you suggest for early benchmarking? We want to ensure we align with NXP’s safety and validation guidelines while we bring up our custom target prototype. Best regards, Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant Hi Sakshi, please note, that our evaluation boards and socket boards are designed and recommended to be used for evaluation of our components only. OTP programming of our components are allowed only by NXP or by our authorized distributors. Depending on annual volume of the specific component. Please let me know your annual volume for your project using the FS2643D Blank OTP Variant. We do not allow to program the OTP of our components by our customers. If customers will program themselves, then we do not guarantee safe and correct function of such components.  With Best Regards, Jozef
View full article
Kinetis 和 LPC 的调试接口有什么建议? 我目前主要从事 Kinetis 系列芯片的开发工作,未来可能还会开发一些 LPC 芯片。我抽屉里装满了 P&E Micro 的调试接口,其中最常用的是 Cyclone ACP。 我有时会发现自己从 600 美元的 Cyclone 换成了 20 美元的 LPC-Link2,因为 Cyclone 与 MCUXpresso 存在很多奇怪的问题。说实话,LPC-Link2 基本能满足我的需求,只是速度有点慢。 我应该考虑使用Segger接口吗?请问有人可以推荐一款可靠、速度适中、在 MCUXpresso(最好也能在 CodeWarrior 11)中支持良好的接口吗?这款接口不会经常导致程序崩溃,也不会无法停止正在运行的目标。如果能支持追踪功能就更好了。 谢谢您! Re: Debug interface recommendations for Kinetis and LPC? 你好@swetie42 , 感谢您对恩智浦产品的关注。 针对您的使用场景,我建议您了解一下MCU-Link Pro Debug Probe。 它与使用标准 CMSIS-DAP 固件的 MCUXpresso IDE 配合良好,而且与基础版 MCU-Link 不同的是,MCU-Link Pro 还提供J-Link LITE 固件选项。由于 CodeWarrior 支持 J-Link,因此如果您需要在 Kinetis 设备上同时使用 MCUXpresso IDE 和 CodeWarrior,这将非常有用。 MCU-Link Pro 还支持 SWO 我的,并提供能量测量和模拟信号监控等附加功能。   当然,如果您更喜欢 SEGGER 生态系统或需要更高级的调试/跟踪功能,SEGGER J-Link 也是一个不错的选择。具体的追踪能力取决于探头型号和目标设备。如需了解更多详情,建议您直接联系 Segger 支持:提交工单 | SEGGER - 嵌入式专家   总之,我认为MCU-Link Pro值得优先考虑。   希望对您有所帮助。   BR 塞莱斯特
View full article
FS2643DブランクOTPバリアントのOTPプログラミングに関する問い合わせ こんにちは、 私は24V用途にFS2643Dバリアント、特にMFS2643HMDA0ADブランクOTPバリアントを使う予定です。 KITFS26SKTEVMソケットボードはOTPの設定やプログラミングに使えると理解しています。しかし、ソケットボードを使用すると、ICをプログラミングのためにソケットに挿入し、その後ターゲットのPCBにはんだ付けする必要があるため、ワークフローが複雑になる可能性があります。 外部プログラマーやターゲットボードを使って、KITFS26SKTEVMソケットボードを必要とせずに、OTPを直接ターゲットPCB上で設定・プログラムする代替方法はありますか? この方法が支持されているか、また適切な解決策を提案していただけますか? https://www.nxp.com/part/MFS2643HMDA0AD ありがとうございます。 Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant こんにちは、サクシさん。 プロトタイプ作成には、ソケットボード、その他のハードウェア、およびNXP Ringo GUIを使用したベンチマークテストをお勧めします。試作基板の設計にあたっては、FS26のデータシートおよびその他の関連資料をご参照ください。特にAN12995。 これらの機密文書をダウンロードするには、NXPとの有効な秘密保持契約(NDA)が必要です。まだNDAを持っていなければ、署名を希望される場合は 、こちらから 新しいチケットを作成してください。NDAマターに関するNXP担当者が手続きをサポートします。 FS26のデータシートやその他の機密文書がなければ、FS26を扱うことは不可能です。 試作設計図が手に入ったら、私たちが確認します。レイアウトの確認は行っておりませんので、ご了承ください。あるいは、当社の正規代理店にご連絡いただければ、エンジニアが回路図のチェックも可能です。 敬具、 ヨゼフ Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant こんにちは、ヨゼフさん。 ご意見ありがとうございます。現在プロトタイプ開発段階にあるため、初期の生産量は少なく、ベンチテストとシステム検証に重点的に取り組んでいます。 これは低生産量のプロトタイプ段階であることを踏まえ、初期のボード制作をどのように進めるべきか教えていただけますか?ArrowやAvnetなどの正規販売代理店と協力して小規模なバッチをプログラムすることを勧めますか?それとも早期ベンチマークの代替ルートを提案しますか? カスタムターゲットプロトタイプを提出する際には、NXPのセーフティおよび検証ガイドラインに準拠していることを確認したいと考えています。 よろしくお願いします、 Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant こんにちは、サクシさん。 当社の評価ボードおよびソケットボードは、当社の部品評価のみを目的として設計・推奨されていますのでご注意ください。当社のコンポーネントのOTPプログラミングは、NXPまたは 当社の認可代理店のみが許可しています。特定の部品の年間生産量によって異なります。FS2643DブランクOTPバリアントを使用したプロジェクトの年間生産量をお知らせください。 当社はお客様がコンポーネントのOTPをプログラムすることを許可していません。お客様が自分でプログラムする場合、そのような部品の安全かつ正しい動作を保証するものではありません。 敬具、 ヨゼフ
View full article
SPI NAND boot on i.MX8ULP SPI NAND boot on i.MX8ULP This article is about the SPI NAND boot on the i.MX8ULP, some customers using the i.MX8ULP want to use the SPI NAND on it. We just have verified the NOR NAND on the i.MX8ULP EVK board, for the SPI NAND use customers do not clear and do not know how to realized, here will give details steps and modifications for customers to refer to. 1\The boot mode support on the i.MX8ULP For the i.MX8ULP support many kinds of external memory devices SD, eMMC, SPI NOR and Flash SPI NAND Flash. Compared to traditional parallel NAND (which requires GPMI/NFC controllers), SPI NAND can be accessed through a serial FlexSPI interface. For the i.MX8ULP for the SPI NAND use need to connect to the FlexSPI2 interface. 2\ Hardware SPI NAND boot configuration On the i.MX8ULP the SPI NAND is mounted on the FlexSPI2 interface, the configuration need to follow the section in the RM. Boot configuration needs to follow the Table 84. Boot configuration. In our reference design use the NOR SPI flash, for the SPI NAND connection can refer to it. 3\Software realized for the SPI NAND boot on the i.MX8ULP Make sure the hardware connections are proper. Next step is to boot up. On our 8ULP EVK board I have confirmed that do not have the SPI NAND on it. The default u-boot and the imx-mkimage flash_singleboot_m33_flexspi is for the SPI NOR, not for the SPI NAND, for the SPI NAND is using the different mechanism with SPI NOR, so if customer use ROM code read it fail, in our default released BSP do not include the build images for the 8ULP SPI NAND https://github.com/nxp-imx/imx-mkimage/blob/lf-6.18.20_2.0.0/iMX8ULP/soc.mak. So it need the special build images, and realized by customer themselves. For the i.MX8ULP ROM code already confirm that support the SPI NAND boot, so in customer’s side they need to porting in their side to support it. The SPI NAND boot mechanism for the i.MX8ULP is the same as that of the i.MX91, so we can refer to the i.MX91 design. For support the SPI NAND boot, the actual project needs to supplement U-Boot, imx mkimage, FCDBBT, download, and Linux support for related NAND part numbers. The core of SPI NAND boot is not a single binary image, but a set of data structures for ROM to identify media, bad blocks, and boot image locations. The key structures as FCB, DBBT, and Image Container. 3.1 U-boot modify Add the NAND related information and parameters in the driver: Take the Winbond NAND as an example, https://github.com/nxp-imx/uboot-imx/blob/lf-6.18.20-2.0.0/drivers/mtd/nand/spi/winbond.c Add customized header support for SPI NAND boot in the cmd_fspinand.c (Added customized FlexSPI NAND header support: allowing different configurations to be generated for different NAND models.) https://github.com/nxp-imx/uboot-imx/blob/lf_v2026.04/arch/arm/mach-imx/cmd_fspinand.c 3.2 Add the SPI NAND support in the imx-mkimage imx-mkimage is a boot image generation tool provided by NXP, used to package multiple boot components such as U-Boot, ATF, OP-TEE, DDR firmware, ELE,SECO firmware into the final boot image (flash.bin). imx-mkimage generates the Container Images that meet Boot ROM requirements. The default code: https://github.com/nxp-imx/imx-mkimage/tree/lf-6.18.20_2.0.0/iMX8ULP Need to add the related information for the SPI NAND support refer to the i.MX91:https://github.com/nxp-imx/imx-mkimage/tree/lf-6.18.20_2.0.0/iMX91 Generate the flash_fw.bin and flash.bin . flash_fw.bin is a temporary boot image used by the UUU tool during SPI NAND programming. flash.bin is the Boot image programmed into the SPI NAND flash. The write the boot images to UUU command is: uuu -b spinand flash_fw.bin flash.bin 3.3 Kernel modify For the kernel need to add the driver and spi-nand node in the board device tree. Add the NAND related information and parameters in the driver like u-boot. Configure FLEXSPI2 and add the SPI NAND Flash node in the board Device Tree (DTS): Build the source code, test on the customer’s board. 4\ Trouble shooting a.Need to check the hardware design is proper, check the connection and pins mux. b.Confirm the i.MX8ULP if validation the 4KB SPI NAND Page size. For the page_data_size and page_total_size 2K      config->pageDataSize = 2048;     config->pageTotalSize = 4096; 4K     config->pageDataSize = 4096; config->pageTotalSize = 8192; Confirm if configuration the FCB to 4KB page size or still 2K. At firstly in the 91 RM we can see that there is BOOT_CFG0[7] FlexSPI_NAND_4K_Page_Selection, no describe for the i.MX8ULP. We thought need special configuration for the i.MX8ULP. But for the i.MX8ULP do not use this BOOT_CFG0[7] FlexSPI_NAND_4K_Page_Selection. And in the default ROM Code support 2K and 4K, details can see in the ROM document . c. The FCB, DBBT, flash.bin, and all contained boot images are 4 KB aligned to match the SPI NAND page size requirement.  Make sure already confirm the FCB configure to 4KB page size. If not 4KB aligned will all met fail boot. d. uboot/arch/arm/mach-imx/cmd_fspinand.c The original code use the fspinand_prep_micron_mem_config() configure NAND's in-die ECC using a semi-hardcoded approach, then write to the SR2 register, this method will cover other key configuration bits in the Winbond W25N04L series SR2. Firstly ask customer to commit out the function of the “fspinand_prep_micron_mem_config()” to see if can pass the fail. (Commenting out the fspinand_prep_micron_mem_config() function in uboot: arch/arm/mach-imx/cmd_fspinand.c will be quick way(not a solution) to verify if this causes the boot failure.) After annotation, the spi nand can start normally, but this is only a verification method and not the final solution. Then customer try to modify the value configuration for the SR2 from 0x10 to 0x19: - config->mem_config.configCmdArgs[1] = 0x10; + config->mem_config.configCmdArgs[1] = 0x19; This works well in customer’s side. But fixed the SR2 value not suit for all customer’s situation using other vendors’ chip. NXP do not use the hard code, because this may affect other NAND customers and instead increase the customized flexspi_nand_config header support. Using the attached U-Boot and mkimage tool patches to generate the required custom header for the target SPI NAND device. Note: Please use our official patches (Already merged in NXP 2026 Q3 release) to address this issue. We have introduced support for customized flexspi_nand_config headers. Please use the attached U-Boot and mkimage tool patches to generate the required custom header for the target SPI NAND device. Please note that the changes in our mkimage patch are based on the SPI NAND implementation for the NXP release of the i.MX91 platform. Please make the corresponding modifications according to the platform you are using. If you are using the Linux 6.18.37_2.1.0 our newest released BSP, we already apply this patch.  Just make porting SPI Nand boot according the i.MX91 section code to finish. If you are using the before released version, the following two patches are needed. 0001-iMX91-soc.mak-add-flash_singleboot_spinand_customhdr.patch.txt 0001-LFU-1037-cmd_fspinand-add-customized-header-support-.patch.txt
View full article