Hi,
I am unable to flash my application to the MIMXRT700-EVK using NXP LinkServer.
Hardware/Software:
During flashing, LinkServer reports:
Error: Wire Ack Fault - target connected?
Error: Wire not connected
Failed on connect: Ee(42). Could not connect to core.
No connection to chip's debug port
Flash operation exited with code 1The MCU-Link is detected correctly by the PC, and LinkServer can detect the probe.
The important hardware observation is that the D4 red LED is not glowing. According to the MIMXRT700-EVK documentation, D4 indicates the MCU/reset status, where ON indicates normal processor activity and OFF indicates that the processor is in reset.
I also executed the RT700 preconnect script, but the SWD connection still fails with:
Error: Wire Ack Fault - target connected?
Error: Wire not connectedCould you please advise:
Hi @Aparna1,
It's likely that the power is not being properly distributed to the MCU/rest of the board, but rather just to the on-board debugger.
Is the green D10 LED also OFF?
Please make sure that the jumper position of J2 is shorting pins 7 and 8.
BR,
Edwin.
Hi,
Yes, I have verified the following:
Please let me know if any additional checks are required from my side.
Regards,
Aparna
This is the Status after connecting USB
Hi,
could you please provide an update on my ticket? I am still waiting for a response.
Thank you.