Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
过温 hi 我想知道S32K32是否有内置温度传感器来监测芯片自身温度? 假设S32K32带有内部温度传感器,软件该如何设置和处理? 坦克。 Re: overtemperature 嗨@qiaoqin_wang 是的。 请参考示例 S32K344 温度传感器 S32DS36 RTD600/500/400_p24 此致敬礼, Robin
View full article
Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar Hello, My name is Eunjin Kwon, and I am a researcher in the Eco-Friendly Building Research Team at GS Engineering & Construction in South Korea. We are currently exploring the application of mmWave radar technology for non-contact fall detection and activity monitoring in residential environments. One of our key technical requirements is to distinguish humans from pets (such as dogs and cats) to prevent false alarms caused by pet movements while ensuring reliable fall detection for human occupants. We are particularly interested in NXP's 77–81 GHz FMCW radar solutions and would appreciate your technical guidance on the following questions: 1. Does NXP have any existing technologies, research results, or application examples related to human versus pet (Human / Non-human) classification using mmWave radar? 2. Is it technically feasible to distinguish humans from pets using radar data, such as point clouds and Doppler information, through AI-based classification algorithms? 3. Are there any relevant reference designs, technical documents, or development resources available for this application? We would also appreciate the opportunity to discuss this topic with an NXP radar technical specialist or Field Application Engineer (FAE) in South Korea. Thank you for your time and assistance. I look forward to your response. Best regards, Eunjin Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar Hello, Let me look closer if we have done something similar as our RADARs are automotive. Best regards, Peter Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar Hello, 1. Does NXP have any existing technologies, research results, or application examples related to human versus pet (Human / Non-human) classification using mmWave radar? NXP does not currently offer a ready-to-use 77–81 GHz reference solution specifically for residential fall detection and human-versus-pet classification. NXP’s 77–81 GHz radar portfolio is primarily intended for automotive radar applications. 2. Is it technically feasible to distinguish humans from pets using radar data, such as point clouds and Doppler information, through AI-based classification algorithms? Human/pet classification using radar is technically feasible in principle. Machine-learning models can use features such as range, velocity, Doppler or micro-Doppler characteristics, spatial distribution and movement over time. Nevertheless, this would require customer-specific data collection, model training and validation under representative residential conditions. Robust performance cannot be guaranteed based on point-cloud data alone; lower-level range-Doppler or range-angle data may be beneficial. 3. Are there any relevant reference designs, technical documents, or development resources available for this application? NXP can provide radar evaluation hardware and signal-processing resources based on the SAF85xx platform to support feasibility evaluation and custom development. These resources do not include a finished fall-detection or pet-classification algorithm. We would also appreciate the opportunity to discuss this topic with an NXP radar technical specialist or Field Application Engineer (FAE) in South Korea. Please get in touch with NXP representative Sales/FAE assigned to your company or with your distributor so the separate support channel can be established. Best regards, Peter
View full article
BCC MC33771Cの測定タイミング こんにちは、チームの皆さん、   私たちはMC33771Cバッテリー・セルコントローラ(BCC)を使って作業しており、異なる読み取り間隔を使うと電圧/温度測定の読み取りタイミングに違いがあることが観察されました。   テスト結果:   構成:スレーブ4台を備えた、BCCと同じ構成。 読み取り間隔:10 ms:4 つのスレーブすべてから温度データを読み取るのに約 40 ms かかります。 読み取り間隔: 100 ms: 4 つのスレーブすべてから同じ温度データを読み取るのに約 7.7 ms かかります。 設定は変更されていないにもかかわらず、読み取り間隔を10msに設定すると、測定全体の読み取り時間が著しく長くなることが観察された。   以下の点についてご理解いただけますか?   10ミリ秒と100ミリ秒の読み取り間隔で、測定値の読み取り時間が大きく異なるのはなぜですか? 読み取り間隔とADC変換、測定値更新、またはBCC通信タイミングの間には、何らかの依存関係がありますか? 4台のBCCスレーブを使用する場合、電圧/温度の読み取りタイミングを安定かつ最適化するための推奨構成や手順はありますか? 複数のMC33771Cデバイスから測定データを読み取る際に考慮すべき、特定のタイミング制約や同期要件はありますか? さらなる分析のために、追加の設定情報や測定ログが必要な場合はお知らせください。 Re: BCC MC33771C measurement timing こんにちは、ニルマルさん。 ADCの設定をご確認いただきありがとうございます。これは重要な補足事項です。ADC_CFG[AVG] = 0、16ビット分解能の場合、ハードウェアtEOCはわずか約520µsです。10ms間隔で40msの読み出し時間が見られるのはADC変換自体によるものではなく、ほぼ間違いなくファームウェアの測定シーケンスによるものです。 tEOCが約520µsの場合、データはどちらの間隔が満了するよりもかなり前に準備完了となる。したがって、観測される読み出し時間の差は、ファームウェアがSOCをトリガーし、間隔に対して結果を読み取る方法とタイミングに起因する。この特定の症状の最も一般的な原因は以下のとおりです。 1. SYS_CFG1[CYCLIC_TIMER]は10msでアクティブになります 周期タイマーが10msに設定されている場合、デバイスは10msごとに自動的に周期変換をトリガーします。ただし、周期的な変換ではMEAS_xxxx測定レジスタは更新されず、OV/UV/OT/UT障害フラグのみが更新されます。MCUファームウェアがオンデマンドSOCを発行する前にサイクリックトリガーを待つと、実効測定サイクルはサイクル周期と連動し、各読み取りまでに最大10msのレイテンシが加算されます。100msの周期周期でこのレイテンシは消えます。なぜならMCUは独立してオンデマンドSOCを発行するためです。SYS_CFG1[CYCLIC_TIMER]の値を確認し、もし有効であれば無効化するか、MCUのリードシーケンスを完全に切り離すことを検討してください。 2. 読み取り前に固定間隔の遅延を挿入(EOCを待たない) ファームウェアがSOCを発行し、EOCフラグをポーリングするのではなく、読み取り間隔全体(10msまたは100ms)待ってから読み取る場合、動作は次のようになります。 100 ms: SOC → 100 ms待機 → 読み取り (7.7 ms 通信) → 測定値 ≈ 7.7 ms ✓ 10 ms: SOC → 10 ms 待機 → 読み取り (7.7 ms 通信) → しかし、サイクルが繰り返され、タイミングが複合すると、実効測定期間が長くなります。 3. SOCはブロードキャストではなく、スレーブごとに発行される ファームウェアが各スレーブに対して個別にSOCをトリガーし、各スレーブ間の読み取り間隔を強制する場合、4つのスレーブの合計は間隔の倍数になります。 4体の奴隷の正しい順序は次のとおりです。 - 4つのスレーブすべてに同時に単一のブロードキャストSOCを発行します。 - EOCフラグをポーリングする(または16ビットで最低520µs待機する、AVG=0)—読み取り間隔と同じ固定遅延は使用しない。 - EOCが確認された後、4つのスレーブすべてを順番に読み込む。 BRs、トーマス お好みの間隔で繰り返してください。 Re: BCC MC33771C measurement timing こんにちは、 @TomasVaverka さん。 詳しい説明をありがとうございました。 私たちの構成では、以下の設定を使用しています。 ADC_CFG[AVG] = 0 ADC分解能 = 16ビット BCCスレーブの数 = 4 両方のテストCASE(10msと100msの読み取り間隔)で同じ構成を使用しています。 しかしながら、以下のようなタイミングのずれが観察された。 10 ms 読み取り間隔: 4 つのスレーブすべてから温度データを読み取るのに約 40 ms かかります。 100 ms 読み取り間隔: 4 つのスレーブすべてから温度データを読み取るのに約 7.7 ms かかります。 ADCの平均化と解像度の設定は両者で同じですが、なぜ変換と測定表示のタイミングが大きく異なるのか、説明していただけますか? この動作を説明するために、SOCトリガー間隔、ADC変換状況、EOCフラグ処理に何か依存関係があるのでしょうか? また、10msの測定間隔で一貫した測定表示タイミングを実現する方法についても提案していただけますか? Re: BCC MC33771C measurement timing こんにちは、ニルマルさん。 タイミングのずれは、おそらくADC_CFG[AVG]の平均化設定が原因です。 平均化が有効になっている場合、tEOC(SOCからデータ準備完了までの時間)はサンプル数に比例して変化します。例えば、16ビット解像度でAVG=64の場合、tEOCは約32.5msとなり、10msの読み取り間隔をはるかに超えます。これは、観察された挙動を説明するものです。 100 ms間隔で:MCUが読み取り→通信時間のみ(~7.7 ms)を測定した時点で変換は完了しています。 10 ms間隔で:MCUは変換完了を待つ必要があります →測定時間=残りのtEOC待ち時間+通信≈40ms。 ご質問に関連する追加事項をいくつかご紹介します。 1. サイクルモード (SYS_CFG1[CYCLIC_TIMER]) は MEAS_xxxx レジスタを更新しません。障害フラグ (OV/UV/OT/UT) のみを更新します。実際の電圧/温度測定値を取得するには、オンデマンドSOCが必要です。平均化機能は、周期モードでは利用できません。 2. 結果を読む前に、必ずEOCフラグが表示されるまで待ってください。読み取り間隔と同じ固定遅延時間は、tEOCを超えることが保証されている場合を除き、使用しないでください。 3. 4台のスレーブの場合:1つのSOCをすべてのスレーブに同時にブロードキャストし(すべてが並列で変換し、tEOCで完了)、その後、順次読み取ります。16ビット、AVG=0の場合、最小合計時間は約0.52ms(tEOC)+ 4×0.7ms(TPL通信)≈3.3msです。 4. フルタイム最適化フレームワークについては、AN12637 MC33771CおよびMC33772Cベースのシステムタイミング最適化(nxp.com で利用可能、ログインが必要)を参照してください。 BRs、トーマス Re: BCC MC33771C measurement timing こんにちは、 @TomasVaverka さん、 SOCにブロードキャストメッセージを使用していますが、それでもタイミングのずれが発生しています。
View full article
PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value As part of the code migration task, we are facing an issue where the BSF flag is being set. Due to the BSF flag being set, the EMON bit in the Minutes register is also getting set. As a result, the Minutes value displayed on the screen is showing an arbitrary value. Additionally, the Year value is not being saved correctly and continuously shows 2000 even after setting the RTC date and time. I tried to test the condition mentioned below, but the problem still persists.  I set the flag register (0x43) to 0x00 and read it immediately; it showed 0x00. However, when I read the register again after 3 seconds, the value was set again to 0x08 (or 0x00).   Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value Hello Ris_eek Good day! The BSF flag is not simply failing to clear. Instead, the RTC is detecting a new battery switch-over event and setting BSF again. According to the datasheet, BSF is set whenever the battery switch-over logic detects a power transition event The fact that it re-asserts after ~3 seconds means the VDD supply is repeatedly dropping below the battery switch-over threshold causing repeated VDD>VBAT>VDD transitions. Each transition re-sets the BSF. RafaR_0-1788887610951.pngRafaR_0-1788887610951.pngRafaR_0-1788887610951.pngRafaR_0-1788887610951.png This constant voltage fluctuation causes the RTC to constantly reset, which is why it only shows the year 2000. I recommend checking if there's a problem with the power supply signal. I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck. Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value Dear Rafar; Thanks for your mail.    In the hardware, the VDD (4.93 VDC) and VBAT (3.02 VDC) voltages are constant. As a precaution against voltage fluctuations, a 100 nF capacitor is connected across the battery supply. The Battery Switch Register (26h) is set to 0x00. Therefore, the BSM (Battery Switch Mode) is configured to switch at the Vth level. The Vth level is 1.5 V because the BSTH (Battery Switch Threshold Voltage) bit is set to 0. As per Figure 25, referenced in previous email: When VDD < Vth, the BSF is set to 1. When VDD > VBAT, the BSF should be cleared. However, under the power-ON condition, the measured voltage is VDD = 4.93 VDC, which is greater than VBAT = 3.02 V. Even then, the BSF is not cleared. Could you please clarify why the BSF remains set even though VDD is greater than VBAT? Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value Hello Ris_eek Good day! The datasheet says the following: The assertion of the flag BSF (register Flags, address 2Bh) can be used to generate an interrupt at pins INTA and INTB. The interrupt can be generated as a pulsed signal or alternatively as a permanently active signal, which follows the condition of bit BSF. BSF remains set until cleared by command. The reference image I sent also indicates the following: "cleared via interface." It’s not automatically, you have to cleared I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck. Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value Okay RafaR Thank you for this. But the BSF flag is cleared in software, but after some time, it is set again, as described in my previous post. Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value Thanks, Now my code migration for the PCF85263AT/AJ is done. We now want to use the offset register in the RTC to improve clock accuracy and we are using it in OFFM=1 (fast mode). While testing the firmware built for offset correction, we observed that the frequency of the INTA(CLK) pin's signal on a DSO varies between 32.68kHz and 32.80kHz. Please check the attached photo. And the same is being read by our microcontroller as well. Offset Value Calculations for 32.68kHz as per fig 20 under section 7.8.3 of the datasheet: A) Consider: CLKOUT fmeas = 32680 Hz so Tmeas = 30.599755 usec B) Dmeas = 30.517578 usec - 30.599755 usec = -0.082176 usec C) Eppm = 10^6 x (-0.082176/30.599755) = -2685.51169 ppm D) Offset Value (when OFFM=1, i.e. Fast Mode) = -2685.51169/2.0345 = -1319.98 ~ -1320 As per the table no. 24 under section 7.8 of the datasheet, the demonstration shows offset values in decimal from -127 to +128 only. But in our case, we are now not able to understand what is to be written to the OFFSET[7:0] register, when our caluclated value is -1320. Hence, we're unsure how or what to write in the application code, so as to test the offset calibration. Kindly guide us on the next steps.
View full article
77〜81GHz FMCWレーダーを用いた人間およびペットの分類に関する技術的調査 こんにちは、 私の名前はクォン・ウンジンで、韓国のGSエンジニアリング&建設の環境に優しいビルディング研究チームの研究者です。 現在、住宅環境における非接触落下検知および活動モニタリングにmmWaveレーダー技術の応用を模索しています。 当社の重要な技術要件の一つは、ペット(犬や猫など)の動きによる誤報を防ぎつつ、人間の転倒を確実に検知するために、人間とペットを区別することです。 特にNXPの77–81 GHz FMCWレーダーソリューションに関心があり、以下の質問について技術的なご指導をいただけるとありがたいです。 1. NXPには、mmWaveレーダーを用いた人間とペット(人間/非人間)の分類に関する既存のテクノロジ、研究成果、またはアプリケーション例はありますか? 2. 点群やドップラー情報などのレーダーデータを使って、AIベースの分類アルゴリズムを使って人間とペットを技術的に区別することは可能でしょうか? 3. このアプリケーションに関連するリファレンスデザイン、技術文書、または開発リソースはありますか? また、韓国のNXPレーダー技術専門家やフィールドアプリケーションエンジニア(FAE)とこのテーマについて議論する機会があればありがたいです。 お時間とご協力に感謝いたします。ご回答をお待ちしております。 よろしくお願いいたします。 ウンジン Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar こんにちは、 もし私たちも同じようなことをしたことがあるなら、もっと詳しく見てみます。私たちのレーダーはオートモーティブです。 よろしくお願いいたします。 ピーター Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar こんにちは、 1. NXPには、mmWaveレーダーを用いた人間とペット(人間/非人間)の分類に関する既存のテクノロジ、研究成果、またはアプリケーション例はありますか? NXPは現在、住宅における転倒検知および人間とペットの識別を目的とした、すぐに使用できる77~81GHz帯のリファレンスソリューションを提供していません。NXPの77〜81 GHzレーダーポートフォリオは主に自動車用レーダー用途を想定しています。 2. 点群やドップラー情報などのレーダーデータを使って、AIベースの分類アルゴリズムを使って人間とペットを技術的に区別することは可能でしょうか? レーダーを使った人間とペットの分類は理論的には可能です。機械学習モデルは、距離、速度、ドップラーやマイクロドップラーの特性、空間分布、時間経過の動きなどの特徴を利用できます。しかしながら、これにはお客様専用のデータ収集、モデルのトレーニング、代表的な居住条件下での検証が必要です。点雲データだけでは堅牢な性能を保証できません。低レベルの距離ドップラーや距離角データが有益である場合があります。 3. このアプリケーションに関連するリファレンスデザイン、技術文書、または開発リソースはありますか? NXPはSAF85xxプラットフォームに基づくレーダー評価ハードウェアおよび信号プロセッシングリソースを提供し、実現可能性評価やカスタム開発をサポートします。これらのリソースには、完成した転倒検知アルゴリズムやペット分類アルゴリズムは含まれていません。 また、韓国のNXPレーダー技術専門家やフィールドアプリケーションエンジニア(FAE)とこのテーマについて議論する機会があればありがたいです。 ご自社に配属されているNXPの営業担当者/FAE、または代理店にご連絡いただき、別のサポートチャネルを確立してください。 よろしくお願いします、 ピーター
View full article
s32 design studio license expired Hello. My S32 Design studio license will be expired soon.  Could you renew the license? License code is 085B-C474-AA78-FC99. Thank you! Re: s32 design studio license expired Hi,  your S32DS license has been extended.  Re: s32 design studio license expired Hi,  I checked your account right now and the license is valid till 2030. You can wait till license is not really expired or return existing one and activate it again with your old code.  Re: s32 design studio license expired Hello. ssong_0-1789444671642.png It looks not extended yet. Could you check this again? thanks. Re: s32 design studio license expired Hello NXP Support, I hope this message finds you well. My S32DS license has expired, and it’s blocking my current development work. Could you kindly help extend it? My Activation ID : 406C-B408-57DB-0C62.  Product : S32 Design Studio for ARM v2.2. Thank you very much.
View full article
关于使用77–81 GHz FMCW雷达进行人和宠物分类的技术咨询 你好, 我的名字是权恩珍,我是韩国GS工程建设公司环保建筑研究团队的研究员。 我们目前正在探索毫米波雷达技术在住宅环境中的非接触式跌倒检测和活动监测方面的应用。 我们的关键技术要求之一是区分人和宠物(如狗和猫),以防止宠物移动引起的误报,同时确保对居住者进行可靠的跌倒检测。 我们对恩智浦半导体的77–81 GHz FMCW雷达解决方案特别感兴趣,希望您能就以下问题提供技术指导: 1. NXP 是否有利用毫米波雷达进行人与宠物(人/非人)分类的现有技术、研究成果或应用实例? 2. 通过基于人工智能的分类算法,利用雷达数据(如点云和多普勒信息)区分人类和宠物在技术上是否可行? 3. 是否有与此应用相关的参考设计、技术文档或开发资源? 我们也希望有机会与恩智浦半导体(NXP)韩国的雷达技术专家或现场应用工程师(FAE)讨论这个话题。 感谢您抽出时间提供帮助。期待您的回复。 顺祝商祺! 恩真 Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar 你好, 让我仔细看看我们是否做过类似的事情,因为我们的雷达是汽车雷达。 顺祝商祺! Peter Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar 你好, 1. NXP 是否有利用毫米波雷达进行人与宠物(人/非人)分类的现有技术、研究成果或应用实例? NXP 目前没有提供专门用于住宅跌倒检测和人与宠物分类的即用型 77–81 GHz 参考解决方案。NXP 的 77–81 GHz 雷达产品组合主要面向汽车雷达应用。 2. 通过基于人工智能的分类算法,利用雷达数据(如点云和多普勒信息)区分人类和宠物在技术上是否可行? 利用雷达进行人/宠物分类在技术上是可行的。机器学习模型可以使用距离、速度、多普勒或微多普勒特性、空间分布和随时间变化的运动等特征。然而,这需要针对特定客户收集数据,并在具有代表性的居住条件下进行模型训练和验证。仅凭点云数据无法保证稳健的性能;较低级别的距离多普勒或距离角度数据可能有所帮助。 3. 是否有与此应用相关的参考设计、技术文档或开发资源? NXP 可提供基于 SAF85xx 平台的雷达评估硬件和信号处理资源,以支持可行性评估和定制开发。这些资源不包含完整的跌倒检测或宠物分类算法。 我们也希望有机会与恩智浦半导体(NXP)韩国的雷达技术专家或现场应用工程师(FAE)讨论这个话题。 请联系分配给贵公司的恩智浦代表销售/现场应用工程师或贵公司的分销商,以便建立单独的支持渠道。 此致, 彼得
View full article
Coupon not valid for FRDM-MCXN236 NXP website advertises this free board to get started. But the coupon code returns invalid when applying at checkout. I feel NXP should honor current advertisements, or, take them offline. Development Board FRDM-Training Re: Coupon not valid for FRDM-MCXN236 Glad to hear that! You can submit the request as a hobbyist. A Does the button appear greyed out? If yes, could you please try logging in using an Incognito window in Chrome, a Private window in Firefox, or a different browser? Sometimes browser cookies can prevent the login process from working correctly. Please also try clearing your browser cache and cookies, then attempt to log in again. Let me know if the issue persists, and I'll be happy to help further. Best regards,  Alondra Re: Coupon not valid for FRDM-MCXN236 Thank you for the quick fix! Coupon works now. However, the checkout stage has several form entries like company name, url etc. Since I am a inidividual and intend to use the board for self learning, I have marked NA for these fields. Unfortunately the next button at end of the form does not respond. Re: Coupon not valid for FRDM-MCXN236 Thank you for contacting us. Could you please try again? We have updated the coupon, and you should now be able to use it successfully. Please let me know if the issue persists, and I will be happy to assist further. Best regards, Alondra Olvera Re: Coupon not valid for FRDM-MCXN236   It's not working for me either, may I know if it's still available or is their any other coupon code for the same ? Regards, Anukul Anand Re: Coupon not valid for FRDM-MCXN236 Hi, I ran into a similar promo error on checkout when applying regional codes. Usually, promo vouchers like ADCWFBXT are restricted by geographical region or distributor inventory allocations. If you are ordering from certain regions—such as developers connected through fiwfans - asia (fiwfan. app) or other local tech hubs—the NXP direct cart often flags the voucher as invalid due to regional shipping rules. The best solution is to open a direct support ticket with NXP Customer Care or contact your local regional distributor. They can either manually issue a regional promo code or release the order allocation for your account. Re: Coupon not valid for FRDM-MCXN236 Now it's back to invalid coupon. Re: Coupon not valid for FRDM-MCXN236 Greetings,  I tried all the steps you mentioned above, cleared the cookies and logged in through an incognito window on Chrome, yet it shows invalid coupon.  Would be glad to use this for my upcoming project so need some help with this coupon thing Thanks Re: Coupon not valid for FRDM-MCXN236 still facing the same probleme with the code "ATWQBE0T" Re: Coupon not valid for FRDM-MCXN236 Unfortunately, this coupon has already reached its usage limit. We will be removing the coupon in the next couple of days. We appreciate your understanding regarding this matter Best regards,  Alondra Re: Coupon not valid for FRDM-MCXN236 Hi NXP Support / Community Team, I am currently trying to purchase the FRDM-MCXN236 development board ($20.00 USD) through the NXP e-commerce store, but I am encountering an issue at checkout.   When attempting to apply the promo code ADCWFBXT, the cart displays an error stating: "Coupon is not valid." Could you please verify if this coupon code is currently active or if there are specific terms/conditions required to apply it to this development board? Any help to resolve this would be greatly appreciated. Thank you!
View full article
RW612用32.768kHz水晶発振子 こんにちは、 現在、u-bloxのIRIS-W10モジュールにRW612を内蔵したPCB設計プロジェクトに取り組んでいます。これはNXP MCUを使った初めてのデザインです。 RTC外部クリスタルの回路設計方法が迷っています。STM32などの他のMCUでは、水晶発振器のピン両方に外部負荷コンデンサが必要であることがわかっています。しかし、NXPのMCUの中には、内部で設定可能な負荷容量を備えているものもあるようだ。RW612レジスタリストで、RTC CTRLレジスタ、特にRTC_OSC_LOADCAPフィールドを見つけました。これはこのMCUに内部負荷上限があることを示していますが、この分野に関するドキュメントは見つかりませんでした。 SO 質問ですが、このレジスタで特定のコンデンサ値を設定するためのビットフォーマットは何でしょうか? 製品: WiFi RW6XX Re: 32.768kHz Crystal for RW612 以下は、32k XTALに関連するレジスタです。RTC_OSC_LOADCAPのレジスターはこの製品に当てはまらない可能性があるため謎のようです Re: 32.768kHz Crystal for RW612 ご返信よろしくお願いします。 RTC水晶発振器の構成は2つのセクションに分かれているようだ。あなたが見せてくれたのはPMUからのものです。私にとって頭痛の種はRTCセクションです。 下のスクリーンショットでは外部コンデンサは見当たりませんが、内部のコンデンサは見当たりません このスクリーンショットでは、私が質問で話していた特定のレジスターが見えます。 このMCUには内部コンデンサが全くないというあなたの言う通りかもしれませんが、もしそうならRTC_OSC_LOADCAPフィールドはレジスタのドキュメントに表示されないはずです。 一方、FRDM-RW612のこの水晶回路には、工場出荷時には負荷コンデンサが取り付けられていません。 Re: 32.768kHz Crystal for RW612 こんにちは、 @Niwo さん。お元気でお過ごしでしょうか。 すでに32kHzのクリスタルを選んでいるか確認していただけますか?これは重要な点で、各結晶はデータシートで定義された一定の負荷静電容量を必要とします。 また、水晶発振回路周辺の適切な特性を決定するためには、水晶発振器メーカーと連携して作業を進めることを強くお勧めします。 Re: 32.768kHz Crystal for RW612 こんにちは、 @RomanVR さん、 ご返信ありがとうございます。 まだ部品は注文していませんが、これを使おうと思っています。 https://eu.mouser.com/de/ProductDetail/ECS/ECS-.327-6-16-TR3?qs=A6eO %2BMLsxmSq6P7XbVvfvw% 3D%3D よろしくお願いいたします。 Re: 32.768kHz Crystal for RW612 こんにちは、 @Niwo さん。返信が遅れて申し訳ありません。 共有された結晶データシートによると、必要な負荷静電容量は12pFであるため、外部回路の構成時の指針とし、結晶メーカーと連携して最適な性能提案を検討するべきです。 前述のレジスタについては、外部結晶負荷静電容量の設定に使用すべきではありません。この点は適切なチームに提出され、さらなる対応が求められました。XTAL32Kの機能および水晶発振器関連の要件については、UM11865の第10章を参照してください。 お役に立てば幸いです! Re: 32.768kHz Crystal for RW612 こんにちは、 @RomanVR さん、 32.768kHzのクリスタルデザインに他の人が取り組みやすくなると思うドキュメントのいくつか変更点を提案したいと思います。 RM00278およびMCUXpressoSDKドライバからRTC CTRLレジスタのRTC_OSC_LOADCAPフィールドの削除 UM11865の図71に外部負荷コンデンサを追加するか、さらに良いのは10章に結晶と負荷コンデンサがGPIO[22]およびGPIO[23]にコネクテッドされていることを示す回路図を追加することです。 UM11865の第10章第2節にある「外部コンデンサ:18 pF」が読者に何を伝えようとしているのか理解できません。これについてもっと詳しく説明してください。 私のフィードバックがお役に立てば幸いです。 よろしくお願いいたします。
View full article
S32DS 2018 ライセンス期限 こんにちは: S32 Design Studio for ARM v2018 R1 ライセンス过期,麻烦帮繁忙处理一下,谢谢! Re: S32DS 2018 license 过期 こんにちは、 S32DS ライセンスが延長されました。 回复: S32DS 2018 license 过期 こんにちは: S32 Design Studio for ARM v2018 R1 license 过期,麻烦帮忙处理一下,谢谢! @jiri_kral
View full article
過熱 hi S32K32には内蔵温度センサが付いていて、自己チップの温度を監視できるのか知りたいです。 S32K32には内部温度センサが搭載されていて、ソフトウェアの設定や処理方法ができると仮定します。 戦車。 Re: overtemperature こんにちは@qiaoqin_wang はい。 例S32K344温度センサーS32DS36 RTD600/500/400_p24を参照してください。 よろしくお願いいたします ロビン
View full article
BCC MC33771C measurement timing Hello Team,   We are working with the MC33771C Battery Cell Controller (BCC) and have observed a difference in voltage/temperature measurement readout timing when using different read intervals.   Test observations:   Configuration: Same BCC configuration with 4 slaves. Read interval: 10 ms: Reading temperature data from all 4 slaves takes approximately 40 ms. Read interval: 100 ms: Reading the same temperature data from all 4 slaves takes approximately 7.7 ms. We observe that the total measurement readout time is significantly higher when the read interval is set to 10 ms, even though the configuration remains unchanged.   Could you please help us understand the following?   Why does the measurement readout time differ significantly between the 10 ms and 100 ms read intervals? Is there any dependency between the read interval and the ADC conversion, measurement update, or BCC communication timing? Is there any recommended configuration or procedure to achieve consistent and optimized voltage/temperature readout timing when using 4 BCC slaves? Are there any specific timing constraints or synchronization requirements that we should consider when reading measurement data from multiple MC33771C devices? Please let us know if any additional configuration details or measurement logs are required for further analysis. Re: BCC MC33771C measurement timing Hello Nirmal, Thank you for confirming the ADC configuration. This is a critical clarification: with ADC_CFG[AVG] = 0 and 16-bit resolution, the hardware tEOC is only ~520 µs. The 40 ms readout time you observe at 10 ms intervals cannot be caused by the ADC conversion itself, it is almost certainly caused by the firmware measurement sequence. With tEOC ≈ 520 µs, data is ready well before either interval expires. The difference in observed readout time therefore comes from how and when the firmware triggers SOC and reads results relative to the interval. The most common causes of this specific symptom are: 1. SYS_CFG1[CYCLIC_TIMER] is active at 10 ms If the cyclic timer is set to 10 ms, the device autonomously triggers a cyclic conversion every 10 ms. However, cyclic conversions do not update the MEAS_xxxx measurement registers — they only update OV/UV/OT/UT fault flags. If the MCU firmware waits for a cyclic trigger before issuing an on-demand SOC, the effective measurement cycle gets coupled to the cyclic period, adding up to 10 ms of latency before each read. At 100 ms cyclic period, this latency disappears because the MCU issues on-demand SOC independently. Please verify the value of SYS_CFG1[CYCLIC_TIMER] and, if active, consider disabling it or decoupling your MCU read sequence from it entirely. 2. Fixed interval delay inserted before reading (not waiting for EOC) If the firmware issues SOC, then waits the full read interval (10 ms or 100 ms) before reading — rather than polling the EOC flag — the behavior would be: 100 ms: SOC → wait 100 ms → read (7.7 ms comm) → measured ≈ 7.7 ms ✓ 10 ms: SOC → wait 10 ms → read (7.7 ms comm) → but then if the cycle repeats and timings compound, the effective measured duration grows. 3. SOC issued per slave rather than as a broadcast If the firmware triggers SOC individually to each slave and enforces the read interval between each, the total for 4 slaves compounds to a multiple of the interval. The correct sequence for 4 slaves is: - Issue a single broadcast SOC to all 4 slaves simultaneously. - Poll the EOC flag (or wait a minimum of 520 µs at 16-bit, AVG=0) — do not use a fixed delay equal to the read interval. - Read all 4 slaves sequentially after EOC is confirmed. BRs, Tomas Repeat at your desired interval. Re: BCC MC33771C measurement timing Hello @TomasVaverka  Thank you for the detailed explanation. In our configuration, we are using the following settings: ADC_CFG[AVG] = 0 ADC Resolution = 16-bit Number of BCC slaves = 4 We are using the same configuration for both test cases (10 ms and 100 ms read intervals). However, we observe the following timing difference: 10 ms read interval: Approximately 40 ms to read temperature data from all 4 slaves. 100 ms read interval: Approximately 7.7 ms to read temperature data from all 4 slaves. Since the ADC averaging and resolution settings are identical in both cases, could you please clarify why the conversion and measurement readout timing differs significantly? Is there any dependency on the SOC trigger interval, ADC conversion status, or EOC flag handling that could explain this behavior? Could you also suggest how we can achieve consistent measurement readout timing with a 10 ms measurement interval? Re: BCC MC33771C measurement timing Hello Nirmal, The timing difference is most likely caused by your ADC_CFG[AVG] averaging setting. When averaging is enabled, tEOC (time from SOC to data ready) scales proportionally with the sample count. For example, at 16-bit resolution with AVG=64, tEOC ≈ 32.5 ms — far exceeding your 10 ms read interval. This explains the observed behavior: At 100 ms interval: Conversion is already complete when the MCU reads → only communication time is measured (~7.7 ms). At 10 ms interval: The MCU must wait for conversion to finish → measured time = remaining tEOC wait + communication ≈ 40 ms. A few additional points relevant to your questions: 1. Cyclic mode (SYS_CFG1[CYCLIC_TIMER]) does NOT update MEAS_xxxx registers — it only updates fault flags (OV/UV/OT/UT). For actual voltage/temperature readings, on-demand SOC is required. Averaging is also not available in cyclic mode. 2. Always wait for the EOC flag before reading results. Do not use a fixed delay equal to the read interval unless it is guaranteed to exceed tEOC. 3. For 4 slaves: broadcast a single SOC to all slaves simultaneously (all convert in parallel, completing at tEOC), then read sequentially. At 16-bit, AVG=0, the minimum total time is approximately 0.52 ms (tEOC) + 4 × 0.7 ms (TPL comm) ≈ 3.3 ms. 4. For a full timing optimization framework, refer to AN12637: MC33771C and MC33772C Based System Timing Optimization (available on nxp.com, login required). BRs, Tomas Re: BCC MC33771C measurement timing Hello @TomasVaverka , I am using broadcast message for SOC, still i am facing timing difference.
View full article
PCF85263AT/AJ -- 画面に表示される分数が任意の値を示しています コード移行作業の一環として、BSFフラグが設定されてしまうという問題に直面しています。BSFフラグが設定されていることにより、分レジスタのEMONビットも設定されます。 その結果、画面に表示される「分」の値は任意の値を示しています。さらに、年の値が正しく保存されず、RTCの日付と時刻を設定した後でも、2000年と表示され続けます。 下記の条件でテストを試みましたが、問題は依然として解決していません。 フラグレジスタ(0x43)を0x00に設定し、すぐに読み取ったところ、0x00が表示されました。しかし、3秒後にレジスタを再度読み取ったところ、値は再び0x08(または0x00)に設定されていた。 Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value こんにちは、Ris_eekさん 良い一日! BSFフラグが単にクリアできないというだけではない。代わりにRTCは新しいバッテリー切り替えイベントを検出し、再びBSFを設定しています。データシートによると、バッテリー切り替えロジックが電源遷移イベントを検出したときにBSFが設定されます 約3秒後に再アサートされるという事実は、VDDの電源が繰り返しバッテリー切り替え閾値を下回り、繰り返しVDD>VBAT>VDDの切り替えを引き起こしていることを意味します。各遷移はBSFをリセットします。 RafaR_0-1788887610951.pngRafaR_0-1788887610951.pngRafaR_0-1788887610951.pngRafaR_0-1788887610951.png この絶え間ない電圧変動により、RTC(リアルタイムクロック)が常にリセットされるため、常に2000年と表示されるのです。電源信号に問題がないか確認することをお勧めします。 この情報がお役に立てば幸いです。他に何かご不明な点がありましたら、お気軽にお問い合わせください。 良い一日をお過ごしください。幸運を祈ります。 Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value こんにちは、Ris_eekさん 良い一日! データシートには次のように記載されています。 フラグBSF(レジスタフラグ、アドレス2Bh)の主張は、ピンINTAおよびINTBで割り込みを生成するために使用できます。割り込みはパルス信号として生成されるか、あるいはビットBSF条件に従う恒常アクティブ信号として生成されることがあります。BSFはコマンドによって解除されるまで設定されたままになります。 私が送った参照画像には「インターフェース経由でクリア済み」と記載されています。 自動的にクリアされるわけではなく、クリアする必要があります。 この情報がお役に立てば幸いです。他に何かご不明な点がありましたら、お気軽にお問い合わせください。 良い一日をお過ごしください。幸運を祈ります。 Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value 親愛なるラファールへ メールありがとうございます。   ハードウェアにおいては、VDD(4.93VDC)とVBAT(3.02VDC)の電圧は一定である。電圧変動を防ぐため、バッテリー供給には100 nFのコンデンサが接続されています。 バッテリースイッチレジスタ(26h)は0x00に設定されています。したがって、BSM(バッテリースイッチモード)はVレベルでスイッチングするように設定されています。Vレベルが1.5Vなのは、BSTH(バッテリースイッチ閾値電圧)ビットが0に設定されているためです。 前回のメールで参照した図25に示すように: VDD < Vth の場合、BSF は 1 に設定されます。 VDD > VBAT の場合、BSF をクリアする必要があります。 しかし、電源投入状態では、測定された電圧はVDD = 4.93 VDCであり、これはVBAT = 3.02 Vよりも大きい。それでも、BSFは許可されない。 なぜBDDがVBATより大きいのにBSFが固定されているのか、説明していただけますか? Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value 了解、ラファール ありがとうございます。 しかし、BSFフラグはソフトウェア上でクリアされますが、しばらくするとまた設定されます。これは私の前回の投稿で説明した通りです。 Re: PCF85263AT/AJ -- Minutes value displayed on the screen is showing an arbitrary value ありがとう、 これでPCF85263AT/AJのコード移行が完了しました。クロック精度を向上させるために、RTCのオフセットレジスタを使用することにします。OFFM=1(高速モード)で使用します。オフセット補正用に構築されたファームウェアをテスト中に、DSO上のINTA(CLK)ピンの信号周波数が32.68kHzから32.80kHzの間で変動することを確認しました。添付の写真をご確認ください。そして同じことが私たちのマイクロコントローラでも読み取られています。 データシートの7.8.3節の図20に基づく32.68kHzのオフセット値計算: A) CLKOUT fmeas = 32680 Hz を考えると、Tmeas = 30.599755 usec B) Dmeas = 30.517578 usec - 30.599755 usec = -0.082176ユースク C) Eppm = 10^6 × (-0.082176/30.599755)= -2685.51169 ppm D) オフセット値(OFFM=1 の場合、つまり高速モード) = -2685.51169/2.0345= -1319.98 ~ -1320 表番号に従って。データシートのセクション7.8にあるように、このデモではオフセット値を-127から+128までの10進数でのみ示しています。しかし私たちの場合、計算値が-1320である場合、OFFSET[7:0]レジスタに何を書くべきか理解できません。そのため、オフセットのキャリブレーションをテストするためにアプリケーションコードにどのように、または何を書けばよいのか分かりません。今後の手順についてご教示ください。
View full article
32.768kHz Crystal for RW612 Hello, I'm currently working on a PCB design project that includes an IRIS-W10 module from u-blox with an RW612 inside. This is my first design with an NXP MCU. I'm unsure, how I should design the circuit for the RTC external crystal. From other MCUs like STM32 I know they need an external load capacitor on both of the crystal pins. But for NXP MCUs it seems that some have internal configurable load caps. In the RW612 register list I stumbled upon the RTC CTRL register and in particular the field RTC_OSC_LOADCAP. To me this indicates that this MCU has in fact internal load caps, but I couldn't find any documentation on this field. So my question is: What is the bit-format to set a specific capacitor value in this register? Product: WiFi RW6XX Re: 32.768kHz Crystal for RW612 Here is the related register for 32k XTAL. The register for RTC_OSC_LOADCAP looks as a mystery since may not applicable to this product Re: 32.768kHz Crystal for RW612 Thank you for your reply. It seems that the configuration of the RTC crystal is split up into two section. The one you showed me is from the PMU. What causes me a headache is the RTC section. In the screen shot below you can see there are no external capacitors, but I don't see any internal caps eighter And in this screen shot you can see the particular register I was talking about in my question. You might be right that this MCU has no internal capacitors at all, but if so the RTC_OSC_LOADCAP field should not be visible in the register documentation. On the other hand this crystal circuit from the FRDM-RW612 has no load caps from factory. Re: 32.768kHz Crystal for RW612 Hi @Niwo, hope you are doing well. Could you please confirm if you have already selected a 32kHz crystal? This is important as each crystal requires a certain load capacitance defined in their datasheet. Also, it is strongly recommended to work along the crystal manufacturer to determine the proper characteristics around the crystal circuitry. Re: 32.768kHz Crystal for RW612 Hello @RomanVR, Thank you for your response. I haven't ordered any parts yet, but I intend to use this one: https://eu.mouser.com/de/ProductDetail/ECS/ECS-.327-6-16-TR3?qs=A6eO%2BMLsxmSq6P7XbVvfvw%3D%3D Best regards Re: 32.768kHz Crystal for RW612 Hi @Niwo, I apologize for the delay. As per the shared crystal datasheet, the required load capacitance is 12pF, hence this should be taken as guide to configure any external circuitry and further analyzed with the crystal manufacturer for optimal performance suggestions. Regarding the mentioned register, it should not be used to configure the external crystal load capacitance, this observation has been raised with the appropriate teams to take further action. For XTAL32K functionality and crystal-related requirements, Chapter 10 of UM11865 is the proper reference. Hope this helps! Re: 32.768kHz Crystal for RW612 Hello @RomanVR, I would like to suggest a few changes for the documentation that I think will make it easier for others to approach the design for the 32.768kHz crystal: Removal of the RTC_OSC_LOADCAP field in the RTC CTRL register from RM00278 and also from the MCUXpressoSDK drivers Add external load capacitors to figure 71 of UM11865 or even better add a schematic to chapter 10 that shows the crystal and load caps beeing connected to GPIO[22] and GPIO[23] In chapter 10 section 2 of UM11865 I don't understand what "External capacitor: 18 pF" should tell the reader. Please go into more detail about this I hope my feedback is helpful to you. Best regards
View full article
s32设计工作室许可证已过期 您好。 我的S32设计工作室许可证即将到期。 能否续签许可证? 许可证代码为 085B-C474-AA78-FC99。 谢谢! Re: s32 design studio license expired 你好, 您的S32DS许可证已延期。 Re: s32 design studio license expired 你好, 我刚刚查看了您的账户,许可证有效期至 2030 年。您可以等到许可证真正过期后再操作,或者退回现有许可证并使用旧代码重新激活。 Re: s32 design studio license expired 您好。 ssong_0-1789444671642.png 看起来还没有扩展。您能再检查一遍吗?谢谢。 Re: s32 design studio license expired 您好,NXP技术支持,希望您一切安好。我的 S32DS 许可证已过期,这阻碍了我目前的开发工作。您能否帮忙延长一下? 我的激活 ID: 406C-B408-57DB-0C62 。 产品:S32 Design Studio for ARM v2.2。 非常感谢。
View full article
S32DS 2018 许可证 过期 你好:适用于 ARM v2018 的 S32 Design Studio R1 许可证已过期,麻烦帮忙处理一下,谢谢! Re: S32DS 2018 license 过期 你好、 您的 S32DS 许可证已延期。 回复: S32DS 2018 license 过期 你好: S32 Design Studio for ARM v2018 R1许可证已过期,麻烦帮忙处理一下,谢谢! @jiri_kral
View full article
FRDM-MCXN236にはクーポンは適用されません NXPのウェブサイトでは、この無料ボードを入門用として宣伝している。しかし、チェックアウト時にクーポンコードを適用すると、無効と表示されます。 NXPは現在の広告を尊重するか、あるいは広告をオフラインにするべきだと思う。 開発ボード FRDMトレーニング Re: Coupon not valid for FRDM-MCXN236 それは嬉しいですね! 趣味としてリクエストを提出できます。A ボタンがグレー表示されていますか?もしそうなら、Chromeのシークレットウィンドウ、Firefoxのプライベートウィンドウ、または別のブラウザでログインしてみていただけますか? 時にはブラウザクッキーがログインプロセスの正常な動作を妨げることがあります。ブラウザのキャッシュとCookieを削除してから、再度ログインをお試しください。 問題が解決しない場合はお知らせください。喜んでさらにサポートさせていただきます。 よろしくお願いします、 アロンドラ Re: Coupon not valid for FRDM-MCXN236 迅速な対応ありがとうございました! クーポンは現在有効です。ただし、チェックアウト段階では会社名やURLなど複数のフォームエントリーがあります。私は個人であり、この掲示板を自己学習のために利用する予定なので、これらの項目には「該当なし」と記入しました。 残念ながら、フォームの最後にある「次へ」ボタンが反応しません。 Re: Coupon not valid for FRDM-MCXN236 お問い合わせいただきありがとうございます。 もう一度お試しいただけますか?クーポンを更新しましたので、問題なくご利用いただけるはずです。 問題が解決しない場合はお知らせください。喜んでさらにサポートさせていただきます。 よろしくお願いします、 アロンドラ・オルベラ Re: Coupon not valid for FRDM-MCXN236 私も同じように使えないのですが、まだ利用できるのでしょうか?それとも、同じクーポンコードが他にありますか? よろしくお願いいたします。 アヌクル・アナンド Re: Coupon not valid for FRDM-MCXN236 こんにちは、 地域コードを適用しようとした際、チェックアウト時に同様のプロモーションエラーが発生しました。通常、ADCWFBXTのようなプロモーションバウチャーは地理的地域や代理店の在庫割りに制限されます。もし特定の地域、例えばfiffanを通じてコネクテッド開発者からご注文する場合、アジア(fiwfan)でもあります。アプリ)やその他のローカルのテクノロジーハブなどでは、NXP の直接カートは、地域の配送規則により、バウチャーを無効と判断することがよくあります。 最善の方法は、NXPカスタマーケアに直接サポートチケットを発行するか、地域の代理店に連絡することです。彼らは手動で地域プロモコードを発行するか、あなたのアカウントの注文割り当てを解放してくれます。 Re: Coupon not valid for FRDM-MCXN236 今度はクーポンが無効です。 Re: Coupon not valid for FRDM-MCXN236 ご挨拶申し上げます。 上記の手順をすべて試しました。Cookieを削除し、Chromeのシークレットウィンドウからログインしましたが、それでもクーポンが無効と表示されます。 これからのプロジェクトで使えたら嬉しいので、このクーポンの件で助けが必要です ありがとうございます Re: Coupon not valid for FRDM-MCXN236 残念ながら、このクーポンは既に利用限度に達しています。クーポンは数日中に削除いたします。このマターについてご理解いただき感謝いたします よろしくお願いします、 アロンドラ Re: Coupon not valid for FRDM-MCXN236 コード「 ATWQBE0T」で依然として同じ問題が発生しています Re: Coupon not valid for FRDM-MCXN236 こんにちは、NXPサポート/コミュニティチームの皆さん、 私は現在、NXPのeコマースストアを通じてFRDM-MCXN236開発ボード(20ドル)を購入しようとしています。00USDです。 しかし、レジで問題が発生しています。   プロモーションコード 「ADCWFBXT」 を適用しようとすると 、 カートに 「クーポンが無効です」 というエラーが表示されます 。 このクーポンコードが現在有効かどうか、またはこの開発ボードに適用されるための特定の条件があるか確認いただけますか? この問題を解決するためのご協力をいただけると大変ありがたいです。 ご回答をお待ちしています。
View full article
此优惠券不适用于 FRDM-MCXN236 NXP 网站宣传这款免费板可供入门。但是结账时应用该优惠券代码时,显示无效。 我认为恩智浦应该尊重目前的广告,或者将其撤下。 开发板 FRDM 培训 Re: Coupon not valid for FRDM-MCXN236 很高兴听到这个消息! 您可以以业余爱好者的身份提交申请。一个 按钮是否显示为灰色?如果可以,请尝试使用 Chrome 的隐身窗口、Firefox 的隐私窗口或其他浏览器登录? 有时浏览器 cookie 会阻止登录过程正常进行。请尝试清除浏览器缓存和cookie,然后再次尝试登录。 如果问题仍然存在,请告诉我,我很乐意提供进一步的帮助。 此致, 阿隆德拉 Re: Coupon not valid for FRDM-MCXN236 谢谢你们迅速解决问题! 优惠券现在可以使用了。但是,结账阶段有多个表单条目,例如公司名称、网址等。由于我是个人用户,打算使用板进行自学,因此我在这些字段中标记为“不适用”。 很遗憾,表单末尾的“下一步”按钮没有反应。 Re: Coupon not valid for FRDM-MCXN236 感谢您与我们联系。 请您再试一次好吗?我们已更新优惠券,您现在应该可以成功使用了。 如果问题仍然存在,请告知我,我将很乐意提供进一步的帮助。 此致, 阿隆德拉·奥尔维拉 Re: Coupon not valid for FRDM-MCXN236 我这边也用不了,请问这个优惠码还能用吗?或者还有其他优惠码可以兑换吗? 问候, 阿努库尔·阿南德 Re: Coupon not valid for FRDM-MCXN236 您好, 我在结账时使用地区代码时也遇到了类似的促销错误。通常情况下,像 ADCWFBXT 这样的促销券会受到地理区域或代理商存货分配的限制。如果您从某些地区订购——例如通过 fiwfans 连接的开发者——亚洲(fiwfan。应用程序)或其他本地技术中心——由于区域运输规则,NXP 直接购物车经常将优惠券标记为无效。 最佳解决方案是直接向 NXP 客户服务中心提交支持请求,或联系您当地的区域代理商。他们可以手动发放区域促销代码,或者释放您账户的订单配额。 Re: Coupon not valid for FRDM-MCXN236 现在又显示优惠券无效了。 Re: Coupon not valid for FRDM-MCXN236 问候, 我尝试了您上面提到的所有步骤,清除了 cookie,并通过 Chrome 的隐身窗口登录,但仍然显示优惠券无效。 我打算在即将开展的项目中使用这个优惠券,所以需要一些帮助。 谢谢 Re: Coupon not valid for FRDM-MCXN236 代码“ ATWQBE0T”仍然存在同样的问题。 Re: Coupon not valid for FRDM-MCXN236 很遗憾,这张优惠券已经达到使用次数上限。我们将在未来几天内移除该优惠券。感谢您对此事的理解。 此致, 阿隆德拉 Re: Coupon not valid for FRDM-MCXN236 您好,NXP支持/社区团队, 我目前正在尝试 通过 NXP 电子商务商店 购买 FRDM-MCXN236 开发板(20.00 美元), 但在结账时遇到了问题。   尝试使用促销代码ADCWFBXT时,购物车显示错误信息: “优惠券无效”。 请问这个优惠码目前是否有效?或者使用这个优惠码是否需要满足某些特定条件?非常感谢您的帮助。 谢谢!
View full article
Secure DFU on RT600 Board: RT685 EVK Zephyr toolchain: zephyr-sdk-1.0.1, zsdk nxp-v4.4.1.1 Hi Team! I am working on a Zephyr-based RT600 application, which should include three images in total ( MCUBoot, ARM core image, and DSP core image). Since the RT600 is a flash-less MCU, those images have to live in the external flash, and I am looking for a proper way to protect them against read-back and other potential risks that could leak the image. On top of that, I would like to have the DFU feature to update both the ARM core and the DSP core images via SMP protocol (RT600 running as SMP server, or through MCUBoot serial recovery, or both) in an encrypted manner. I failed to find an example shipped with nxp-zsdk, could you please help me find a practical path to follow? Best regards, Yue Re: Secure DFU on RT600 Hi @YueZ , For the RT685 EVK, I recommend treating this as two related design tasks : securing what is stored in external flash, and securely updating the Arm and DSP firmware. An encrypted update alone does not establish that the active image is protected against external-flash read-back. A practical starting point is to package the DSP firmware with the Arm application and update them as one signed image . That lets you bring up a single MCUboot primary/secondary-slot update path before taking on independent DSP image management. Zephyr’s SMP image-management flow uploads an update to a secondary slot for MCUboot to process at boot.(zephyr/doc/services/device_mgmt/smp_groups/smp_group_1.rst at main · zephyrproject-rtos/zephyr · GitHub) On RT600, the boot images reside outside internal flash, either for loading into SRAM or for execution from external memory, so the flash layout and boot chain need to be designed together. - https://www.nxp.com/docs/en/application-note/AN12985.pdf  I would proceed in this order: Establish a trusted boot chain : authenticate the bootloader at startup, then have it verify signed application updates. Include production key provisioning and debug-access policy in the design. Demonstrate a signed Arm-plus-DSP update through an application-side SMP server, with a defined primary and secondary flash slot. Confirm that the newly built DSP firmware is actually included in the image being uploaded. Address confidentiality of the installed image separately . NXP’s RT600 secure-provisioning workflow describes writing an encrypted application and OTFAD key blobs,(mcuxpresso.nxp.com/secure/latest/_sources/06_processor_specific_workflow.md) and its RT600 FOTA note describes a signed-and-encrypted OTA approach. Those are useful RT600 references, but their procedures are not a ready-made Zephyr SMP integration. - https://www.nxp.com/docs/en/application-note/AN13478.pdf  If independent Arm and DSP updates are required, design separate image storage and verification, plus a way to prevent incompatible Arm/DSP versions from being activated together. I would treat that as a second integration milestone, not as a capability already demonstrated by the combined-image example. Application-side SMP and bootloader-side serial recovery can both be considered, but they are distinct update paths; you do not need to implement both to validate the first DFU milestone.  Could you confirm whether the DSP must be updated independently, or whether updating Arm and DSP together is acceptable? That decision determines whether the simpler combined-image path meets your requirements or whether a multi-image boot and rollback design is necessary.   Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: Secure DFU on RT600 Hi Kan, Thank you very much for the information, it is really clear and helpful! To answer your question, I am fine with packing the two images into one; they don't need to be separate. Additionally, I am eager to know your suggestions on a few more questions, and please correct me if I am wrong since I am new to the NXP secure-provisioning workflow: The two milestones are, if I understood it correctly: 1) verify FOTA image signing and boot chain; 2) verify OTFAD on the off-chip flash. It looks like the west build process only signs the image without encryption; the output hex(bin) image file remains in plaintext, which is supposed to be encrypted in the second step for OTFAD. On an OTA update, a signed image is received and then written into flash as OTFAD-encrypted. Does that mean the image in transit is exposed to attack? XIP or loading in RAM, which would you recommend for less workload in Zephyr if combined with signing and encryption?  Is there an example available in Zephyr demonstrating the OTFAD feature on RT600 (and whether OTFAD is supported by MCUBoot serial recovery)? I found modules/hal/nxp/mcux/mcux-sdk-ng/drivers/otfad/fsl_otfad.h, but nothing has referred to it yet. A starting point would be very much appreciated! Best regards, Yue Re: Secure DFU on RT600 Hi @YueZ , Thank you for confirming that the Arm and DSP firmware can be packaged together. That is the path I would start with: one signed application update containing both firmwares , rather than two independently managed application images. Your proposed milestones are sensible, but I would separate them slightly differently: Prove the boot and update chain: boot the combined image through MCUboot, upload a signed replacement through application-side SMP, and verify the upgrade and recovery behavior. Prove encrypted boot on the RT685 EVK: use Secure Provisioning Tool (SPT) to build and boot an OTFAD-encrypted image from external flash, initially using the documented shadow-register development workflow. - Processor-specific workflows — Secure Provisioning Tool 26.09  Integrate the two: determine how a field update will be staged and installed in the encrypted flash layout without breaking image verification or recovery. This last step is not provided automatically by enabling OTFAD. - Generic workflows — Secure Provisioning Tool 26.09  On the plaintext build output and transmission: your understanding is substantially correct. The documented Zephyr/MCUboot workflow produces a signed application file, zephyr.signed.bin ; signing does not conceal its contents. If that file is distributed and uploaded as-is, someone able to obtain the file or observe an unprotected transfer can read the firmware. You can protect the transfer with an appropriately authenticated, encrypted transport, or distribute an encrypted update artifact. These are separate from protecting the installed image in external flash. - Generic workflows — Secure Provisioning Tool 26.09 Encrypted XIP and MCUboot — MCUXpresso SDK Documentation I would make one correction to the proposed OTA diagram: do not assume that receiving a signed plaintext image and writing it with Zephyr’s flash driver automatically produces OTFAD-encrypted flash contents. SPT’s RT5xx/6xx workflow explicitly writes an encrypted application and OTFAD key blobs . A field updater must reproduce a compatible result—or use another validated installation scheme—while accounting for the protected address ranges and keys. The RT600 OTFAD reference describes decryption of encrypted flash during reads; the SPT provisioning procedure should not be taken as an implementation of Zephyr’s runtime update writer. -https://www.nxp.com/docs/en/training-reference-material/RT600_Security_Architecture_sb.pdf  XIP versus load-to-RAM: since your goal is specifically to protect an application stored in external flash with OTFAD, I would use encrypted XIP as the first security proof of concept . SPT documents that boot workflow for RT5xx/6xx. This is a recommendation for the boot experiment , not a claim that encrypted XIP makes the Zephyr DFU integration easy. Load-to-RAM is also a documented RT5xx/6xx image arrangement, but it does not remove the need to protect the stored image and design a secure update path. I cannot substantiate that either option is a turnkey, lower-workload Zephyr solution for your SDK version. Regarding examples and serial recovery: I have not found a validated RT685 Zephyr example combining OTFAD, MCUboot and SMP/serial-recovery encrypted updates for nxp-v4.4.1.1 . The fsl_otfad.h header establishes that a driver interface exists; it does not establish that the RT685 MCUboot recovery or flash-installation path integrates it. NXP’s Encrypted XIP and MCUboot documentation describes an encrypted-XIP extension, but its listed OTFAD example boards are RT1152/RT1160/RT1170, not RT685 . I would not assume that its serial-recovery or installation behavior carries over to this board. That is something I still need to check with the team. For a concrete starting reference, use SPT 26.09, “RT5xx/6xx device workflow → Booting OTFAD encrypted image using shadow registers” to establish the encrypted-boot baseline. In parallel, use AN13478, Implementing FOTA on i.MX RT600 to study NXP’s RT600 signed-and-encrypted update approach. That application note is not a Zephyr SMP example, so the remaining work is to reconcile its encrypted-image installation approach with your Zephyr/M​​CUboot slot layout and chosen update path.    For this board, I would validate signed combined-image DFU and SPT-generated OTFAD XIP separately, then treat encrypted field installation—including any serial-recovery support—as an integration task requiring its own test.   Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: Secure DFU on RT600 Hi Kan, This is enough information for me to digest at this point, I will mark it as a solution. Please notify me if the team has any updates on the capability of RT685 MCUboot recovery with OTFAD. Thank you very much for the details! You have a great day too! Yue
View full article
RW612 出力クロックをピンへ こんにちは、 オシロスコープで測定できるように、ピンにクロック信号を出力する方法のソフトウェア例を探しています。 CLKOUT信号(下の画像参照)で実現できると思いますが、正しく設定できませんでした。 ユーザーマニュアルのこのセクションには、CLKOUTはIOMUX経由でピンにルーティングしなければならないと書かれていますが、MCI_IO_MUX->FSELレジスタでその関数のフィールドを見つけることができませんでした。 製品: WiFi RW6XX Re: RW612 output clock to pin MCUXpressoはクロック生成に役立つかもしれません Re: RW612 output clock to pin こんにちは、 @Niwo さん。 CLKOUTの設定を追加するには、 MCuxpresso Config Toolsを使用することをお勧めします。このツールはMCUのクロックツリーとピンを設定し、対応するAPIを自動的にclock_config.cで生成することを可能にします。pinmux.c、および pinmux.hファイル。 このツールに慣れていない場合は、まずMCUXpresso設定ツールのクイックスタートガイドを確認することをお勧めします。また、ピンやクロックの設定には、MCUXpresso設定ツール26.09のドキュメントの 「Starting with pin/internal signal select 」ガイドや 「Clocks Tool 」セクションも役立つかもしれません。 他に質問がありましたら、お気軽にお知らせください。 BR ハビブ
View full article