Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
EB tresos Studio 32.1.4许可证密钥 您好,NXP团队: 我想下载并使用 EB tresos Studio 32.1.4。请问这款软件需要单独购买许可证吗?还是可以使用页面上提供的激活码?已附上激活密钥供您参考。本软件的使用不得用于任何商业用途。仅供学习之用。 谢谢! 基兰 kiran5_0-1790066799166.png Re: EB tresos Studio 32.1.4 License keys 嗨@kiran5 NXP 为 EB tresos Studio 提供基本评估许可证,您可以使用下载页面上提供的激活密钥。此许可具有局限性,主要用于评估和配置 NXP 提供的 RTD 软件。 请注意,此许可证不提供 EB tresos Studio 的所有功能,也不允许您配置完整的 AUTOSAR 堆栈。为此,必须直接从 Elektrobit 获取完整许可证。商业/生产用途也需要获得 Elektrobit 的相应许可。 因此,如果您的目的仅仅是学习、评估和使用 NXP RTD 进行基本操作,则可以使用 NXP 提供的激活密钥。 此致, Lukas Re: EB tresos Studio 32.1.4 License keys 嗨@lukaszadrapa 请问该许可证是否可以供公司员工用于公司内部的学习和教育目的? 仅供学习、培训和评估之用,不得用于商业产品开发或生产用途。请确认许可条款是否允许此类用途,或者该许可是否仅供个人使用。 谢谢! 基兰 Re: EB tresos Studio 32.1.4 License keys 嗨@kiran5 根据许可条款(2.1.4.教育许可证),教育许可证旨在用于大学和技术学校的教育、非商业用途。如果您需要确认贵公司内部的特定培训或学习用途是否在您的许可范围内,我建议您直接与 Elektrobit 讨论此事,因为他们是许可方,可以对许可条款提供权威的解释。 此致, Lukas
View full article
EB tresos Studio 32.1.4 License keys Hi NXP Team, I wanted to download an use the EB tresos Studio 32.1.4. Can you please tell me if the software needs a seperate license to be purchased or can i use the activation key given in the page. Have attached the activation key for reference. The use of this software is not for any commercial purpose. It is only for learning purpose. Thanks Kiran kiran5_0-1790066799166.png Re: EB tresos Studio 32.1.4 License keys Hi @kiran5  NXP provides a basic evaluation license for EB tresos Studio, and you can use the activation key provided on the download page. This license is limited and is primarily intended for evaluation and configuration of the RTD software provided by NXP. Please note that this license does not provide all EB tresos Studio features and does not allow you to configure the complete AUTOSAR stack. For that purpose, a full license must be obtained directly from Elektrobit. A commercial/production use also requires an appropriate license from Elektrobit. Therefore, if your intention is only learning, evaluation, and basic work with NXP RTD, you can use the activation key provided by NXP. Regards, Lukas Re: EB tresos Studio 32.1.4 License keys Hi @lukaszadrapa  Could you please clarify whether this license can be used by an employee for learning and educational purposes within a company? The intended use is only for learning, training, and evaluation purposes, and not for commercial product development or production use. Please confirm whether such usage is permitted under the license terms, or whether the license is intended strictly for individual/personal use. Thanks Kiran Re: EB tresos Studio 32.1.4 License keys Hi @kiran5  Based on the license terms (2.1.4. EDUCATIONAL LICENSE), the Educational License is intended for educational, non-commercial use at universities and technical schools. If you need confirmation whether your specific internal company training or learning use is permitted under your license, I recommend discussing this directly with Elektrobit, as they are the licensor and can provide an authoritative interpretation of the license terms. Regards, Lukas
View full article
How to extend S32 Design Studio license? 回复: How to extend S32 Design Studio license? Hi, My lisence is missing. Activation code: 3730-E558-FBD6-7835 Please help me extend. Thansk you! Re: How to extend S32 Design Studio license? Hi, My lisence will be expired 10.01.2026 Activation code: E328-2768-778F-27B5 br: Jarmo Re: How to extend S32 Design Studio license? @jiri_kral  Please help me to extend the S32 Design Studio license, thank you! Activation Code: 52A6-DAFA-222F-03DF Re: How to extend S32 Design Studio license? Your S32DS license has been extended.  Re: How to extend S32 Design Studio license? Help me, tks. Activation Code: 067C-DFBC-9C46-C280 Re: How to extend S32 Design Studio license? Hi,  your S32DS license has been extended. Please activate S32DS again with your old code. Re: How to extend S32 Design Studio license? Please help me to extend the S32 Design Studio license, thank you! Activation Code: 0D99-A811-65CE-5DB9 回复: How to extend S32 Design Studio license? Hello! When installing S32DS 3.5 and entering the activation code, it says the code is already in use by 3.6. Please help me resolve this, thank you!
View full article
EB tresos Studio 32.1.4ライセンスキー こんにちは、NXP チームの皆様、 EB Tresos Studio 32.1.4をダウンロードして使いたかったのです。ソフトウェアが別途ライセンスを購入する必要があるのか、それともページに記載されているアクティベーションキーを使ってもよいのか教えていただけますか?参考までに、アクティベーションキーを添付しました。このソフトウェアの使用は商業目的ではありません。これは学習目的のみに使用されます。 よろしくお願いします。 キラン kiran5_0-1790066799166.png Re: EB tresos Studio 32.1.4 License keys こんにちは、 @kiran5さん NXPはEB Tresos Studioの基本的な評価ライセンスを提供しており、ダウンロードページに記載されているアクティベーションキーを使用できます。このライセンスは限定的であり、主にNXPが提供するRTDソフトウェアの評価および設定を目的としています。 このライセンスはEB Tresos Studioのすべての機能を提供するわけではなく、AUTOSARの完全なスタックを設定することはできませんのでご注意ください。そのためには、Elektrobitから直接正式なライセンスを取得する必要があります。商用利用または制作利用の場合は、Elektrobit社からの適切なライセンスも必要となります。 したがって、学習、評価、基本的な作業だけを目的としている場合は、NXPが提供するアクティベーションキーを利用できます。 よろしくお願いいたします。 ルーカス Re: EB tresos Studio 32.1.4 License keys こんにちは、 @lukaszadrapa このライセンスは従業員が社内で学習や教育目的で使用できるのか、もう少し詳しく教えていただけますか? 意図された使用は学習、トレーニング、評価の目的のみであり、商業的な製品開発や生産目的ではありません。このような使用がライセンス条項で許可されているか、あるいはライセンスが個人使用のみを目的としているかをご確認ください。 よろしくお願いします。 キラン Re: EB tresos Studio 32.1.4 License keys こんにちは、 @kiran5さん ライセンス条項(2.1.4)に基づきます。教育ライセンス)は、大学や専門学校での教育目的の非営利利用を目的としています。もしあなたの社内のトレーニングや学習利用がライセンスの下で許可されているかどうか確認が必要な場合は、Elektrobitに直接相談することをお勧めします。彼らはライセンス提供者であり、ライセンス条項の権威ある解釈を提供してくれます。 よろしくお願いいたします。 ルーカス
View full article
i.MX8に推奨されるCVBS(PAL/NTSC)ビデオエンコーダー i.MX8ベースのボード上でPAL/NTSCコンポジット出力を生成するための、適切な外部ビデオエンコーダー/CVBS DACを探しています。 要件: - CVBS出力×1(PAL/NTSC) 質問: i.MX8と組み合わせるビデオエンコーダーとして、現在おすすめするものは何ですか? ADV7391/ADV7393は今でも定番の部品ですか?それとも、より新しく、サポート体制の整った代替品がありますか? よろしくお願いいたします! グラフィックスとディスプレイ Re: Recommended CVBS (PAL/NTSC) video encoder for i.MX8 こんにちは、 @kbchさん あなたの調子が良いといいのですが。 i.MX8ファミリは、専用のBT656/BT1120出力ポートを持つIPUを持つi.MX6とは異なり、ネイティブのBT656並列出力インターフェースを持たない。 i.MX8ファミリーのディスプレイ出力は、MIPI-DSI、HDMI、LVDS(正確な部品番号によって異なります)です。 Q1. 現時点では、i.MX8向けにNXPが公式に推奨またはカーネルでサポートされている外部CVBSエンコーダーはありません。i.MX8は、BT656出力バスをネイティブに提供していません。 Q2. adv739x Linuxカーネルドライバーは存在し、i.MX6で使われていましたが、i.MX8ファミリには使われていません。 よろしくお願いいたします。 サラス。
View full article
如何扩展 S32 Design Studio 许可证? 回复: How to extend S32 Design Studio license? 您好, 我的许可证不见了。 激活代码3730-E558-FBD6-7835 请帮我延长。 谢谢! Re: How to extend S32 Design Studio license? 你好,我的许可证将于 2026 年 1 月 10 日到期。 激活代码E328-2768-778F-27B5 br:Jarmo Re: How to extend S32 Design Studio license? @jiri_kral 请帮我扩展S32 Design Studio 许可证,谢谢! 激活代码:52a6-dafa-222f-03df Re: How to extend S32 Design Studio license? 您的 S32DS 许可证已延期。 Re: How to extend S32 Design Studio license? help me ,tks. Activation Code: 067C-DFBC-9C46-C280 Re: How to extend S32 Design Studio license? 你好、 您的 S32DS 许可证已延期。请使用旧代码重新激活 S32DS。 Re: How to extend S32 Design Studio license? 请帮我延长S32设计工作室的许可证,谢谢! 激活码:0D99-A811-65CE-5DB9 回复: How to extend S32 Design Studio license? 您好!安装S32DS 3.5输入激活码时提示已经被3.6占用了,请帮忙处理,谢谢!
View full article
how to enable a second camera on mx95 evk board Spoiler (Highlight to read) Hello, we would like to know how to use a camera in the DSI/CSI slot of the MX95 EVK evk board. Our camera has reset and standby pins, but we cannot find any GPIO pins to control them in the MX95 EVK schematic. Hello, we would like to know how to use a camera in the DSI/CSI slot of the MX95 EVK evk board. Our camera has reset and standby pins, but we cannot find any GPIO pins to control them in the MX95 EVK schematic. Re: how to enable a second camera on mx95 evk board Hi @yipingwang  Thank you. The camera we are using is the TechNexion AR0235, and we would like to use it with the CSI and CSI/DSI slots. Re: how to enable a second camera on mx95 evk board Let me confirm with the AE team. Re: how to enable a second camera on mx95 evk board Hi @yipingwang  Thank you for your help, but the camera still isn't working. Do you have any suggestions? Re: how to enable a second camera on mx95 evk board J14 A10 DSICSI_RST_SYNC → ADP5585 C0 → gpiochip9 line 6 → reset is typically active-low J14 A11 DSICSI_EN_PWDN → ADP5585 R4 → gpiochip9 line 4 → power-down is typically active-high Normal operation: line 6 = high , line 4 = low . Re: how to enable a second camera on mx95 evk board hi @yipingwang  @yipingwang  @I applied the following settings, but the camera initialization still failed hankwang_0-1790059212233.png Re: how to enable a second camera on mx95 evk board Hi @yipingwang  Thank you for confirming that J14 A10 (DSICSI_RST_SYNC) and A11 (DSICSI_EN_PWDN) are controlled via U81 (ADP5585). We've confirmed the ADP5585 on our board (i2c address 0x34, reporting as adp5585-00) probes successfully and is exposed to Linux as gpiochip9 with 11 GPIO lines (0-10; line 5 is reserved for PWM per our device tree). Could you help us map these two signals to the exact ADP5585 GPIO pins (e.g. R0-R4/C0-C4 per the datasheet), and the corresponding Linux gpiochip line number (0-10)? Also, what is the correct polarity (active-high/active-low) for each signal? We've already brute-force tested all pairwise combinations of the 10 available lines (90 combinations, both pulled low simultaneously) without success — the camera's boot-state register (0x3004) remains 0x0000 in every case. A precise pin mapping from the schematic or UM12022 would let us verify directly rather than continuing to guess. Re: how to enable a second camera on mx95 evk board On the 19 mm × 19 mm i.MX 95 EVK , The reset and standby pins on the i.MX95 EVK DSI/CSI connector (J14) are controlled through the ADP5585 GPIO expander U81 , not directly by i.MX95 GPIOs: J14 A10 – DSICSI_RST_SYNC : camera reset J14 A11 – DSICSI_EN_PWDN : camera standby/power-down Control voltage: 1.8 V In the device tree, reference U81 for reset-gpios and pwdn-gpios . Use NXP’s imx95-19x19-evk-os08a20-combo.dtb overlay as the example for enabling the second camera on the shared DSI/CSI port. Re: how to enable a second camera on mx95 evk board Please confirm that you are using 19x19 or 15x15 evk? Re: how to enable a second camera on mx95 evk board 95 and sensor must be configured in pair, take ov5640 for example,     PWDN (EN), B11 RESET (RST_B), A9 So on 95 side, A11 should be for pwdn, and B9 for reset. Looking into the 95 19x19 BB board schematic,  A11 is controlled by ADP5585 R4 pin B9 is controlled by soc gpio3 27       So in the dts, user should configure as follows, pinctrl_mipi_dsi_csi: mipidsigrp {         fsl,pins = <                 IMX95_PAD_CCM_CLKO2__GPIO3_IO_BIT27                     0x31e         >; }; pinctrl-0 = <&pinctrl_mipi_dsi_csi>; powerdown-gpios = <&adp5585gpio 4 GPIO_ACTIVE_HIGH>; reset-gpios = <&gpio3 27 GPIO_ACTIVE_LOW>; If user needs to connect to 15x15 evk board, then   pinctrl_mipi_dsi_csi_rst: mipidsirstgrp {         fsl,pins = <                IMX95_PAD_XSPI1_DATA7__GPIO5_IO_BIT7                    0x31e         >; }; pinctrl_mipi_dsi_csi: mipidsigrp {         fsl,pins = <                IMX95_PAD_XSPI1_DATA6__GPIO5_IO_BIT6                    0x31e         >; }; pinctrl-0 = <&pinctrl_mipi_dsi_csi_rst>, <&pinctrl_mipi_dsi_csi>; powerdown-gpios = <&gpio5 6 GPIO_ACTIVE_HIGH>; reset-gpios = <&gpio5 7 GPIO_ACTIVE_LOW>; Re: how to enable a second camera on mx95 evk board @yipingwang I am using the 19x19 EVK board, and I have resolved the issue. Thank you. The reset pin configuration needs to be changed; J14 A10 DSICSI_RST_SYNC cannot be used.
View full article
GPIO218エミュレータモード出力エラー GPIO218の出力レベルは、フルスピードで動作しているときは正しく切り替わります。しかし、LauterbachのAttach接続を使用すると、ポートレベルが低くなり、切り替わらなくなります。この問題をどのように分析すればよいでしょうか? Re: GPIO218仿真器模式下输出异常 こんにちは@liyongfengさん 「もう転売できない」とはどういう意味ですか?Siul2_Dio_Ip_WritePin() 関数を実行した際に、GPDO218 の値が「1」に変化しないのでしょうか?どのようにテストしていますか? 「Go」を選択するか、デバッガーを切断すると、GPIOは切り替わりますか? 簡単なテストを行ったところ、デバッガを接続するとGPDOが切り替わるのが見えました。 よろしくお願いします、 ジュリアン
View full article
i.MX95 19x19 EVK: SMMUコヒーレントテーブルウォーク(IDR0.COHACC)およびSMMUが有効なDPDK用のvfio-pci こんにちは、NXP チームの皆様、 私たちは、i.MX95 19x19 LPDDR5 EVKと公式のNXP Linux BSP LF 6.6.52_2.2.2を組み合わせた高スループット・低レイテンシのネットワーク製品を開発しています。 ユーザー空間PMDと共に、 netc関数(例: 0002:00:00.0 やSR-IOV VF)で vfio-pci を 用いてDPDKを実行する必要があります 。しかし、 SMMUが有効になると vfio-pciへのバインド が失敗します。 64バイトフレームのベンチマークでは: Linuxカーネルドライバー(fsl_enetc4😞 約17万ページ SMMUが無効になっているVFでのネイティブPMD:約456,000pps パフォーマンスの違いにより、ユーザー空間のDPDKドライバが私たちのアプリケーションに必要です。 本番システムではハードウェアによるDMA隔離が必要なため、SMMUを無効化したりenable_unsafe_noiommu_mode=1を使うことはできません。 SMMUが有効になっている場合、NETC機能をfsl_enetc4からバインド解除してvfio-pciにバインドすると、 -EINVALエラーで失敗します。 root@imx95-19x19-lpddr5-evk:~# lspci -k -s 0002:00:00.0 0002:00:00.0 Ethernet controller: Philips Semiconductors Device e101 (rev 04) Subsystem: Philips Semiconductors Device e101 Kernel driver in use: fsl_enetc4 root@imx95-19x19-lpddr5-evk:~# echo 0002:00:00.0 > /sys/bus/pci/drivers/fsl_enetc4/unbind root@imx95-19x19-lpddr5-evk:~# echo "1131 e101" > /sys/bus/pci/drivers/vfio-pci/new_id [ 143.562552] vfio-pci: probe of 0002:00:00.0 failed with error -22 Linux VFIOおよびArm SMMUコードの追跡から、この障害はSMMUのコヒーレンシー能力に関連しているようです。VFIOはIOMMU_CAP_CACHE_COHERENCYを必要とし、Arm SMMUドライバーは IDR0 に基づいてARM_SMMU_FEAT_COHERENCYを有効にします。COHACCです。 i.MX95 EVKでは、IDR0。COHACCは0を読み取り、SMMUは一貫した翻訳テーブルウォークをサポートしていないと報告されます。これにより、device_iommu_capable(..., IOMMU_CAP_CACHE_COHERENCY)がfalseを返し、vfio-pciが-EINVALで失敗します。 We understand that adding dma-coherent; to the SMMU device-tree node can force the Linux SMMUドライバー to enable ARM_SMMU_FEAT_COHERENCY. However, this also causes io-pgtable-arm to configure pgtbl_cfg.coherent_walk = true, which disables the CPU cache maintenance normally performed for page-table updates. したがって、DMAコヒーレントを有効にしたくありません。i.MX95ハードウェアがコヒーレントなSMMU変換テーブルウォークをサポートすることが確認されていない限りです。インターコネクトがSMMUテーブルウォークのためにCPUキャッシュをスヌープしない場合、動的IOMMUマッピング中にページテーブルエントリの古びやメモリ破損を引き起こす可能性があります。 NXPの皆さん、以下の点を明確にしていただけますか? i.MX95シリコン/インターコネクトは 、 CPUキャッシュの必要なキャッシュスヌーピングを含む ハードウェアコヒーレントなSMMU変換テーブルウォーク をサポートしていますか? もしコヒーレントテーブルウォークがサポートされている場合、 SMMUがコヒーレントウォークを報告する前に、インターコネクト、システムマネージャー、ATF/ファームウェア、またはその他のプラットフォーム初期化で有効化しなければならない設定はありますか? もしコヒーレントテーブルウォークがサポートされている場合、NXP推奨のデバイスツリー/ファームウェア構成は安全に有効化されるためのもので、EVK上でどのように検証できますか? も しコヒーレントテーブルウォーク が サポートされていない 場合、 SMMU/DMAのアイソレーションを有効にしたまま vfio-pciでDPDK を使用する際、NXPが推奨する本番環境で安全な方法は何ですか? i.MX95でSMMUを有効にした状態でDPDK + vfio-pciをサポートする構成について、何かご助言いただければ大変ありがたいです。 Re: i.MX95 19x19 EVK: SMMU coherent table walks (IDR0.COHACC) and vfio-pci for DPDK with SMMU enable 顧客が他の用途でSMMUを使いたいが、DPDKのバイパスは許容される場合(bootargsでiommu.passthrough=1を使ったり、dtsでSMMUノードを無効にしたくない場合)。 その後、uio-pci-genericフレームワークをバインドし、VSI-PSIメッセージングを無効にしようと試みることができます(エクスポートENETC4_VSI_MSG_DISABLE=1)。しかしVSI-PSIメッセージを無効にすると、ユーザーはpromisc、VLAN MACフィルタリング、リンク情報などのENETC機能が使えなくなります。 Re: i.MX95 19x19 EVK: SMMU coherent table walks (IDR0.COHACC) and vfio-pci for DPDK with SMMU enable DPDKチームからフィードバックがあり、以下の質問をされました。 これは既知の制約事項です。i.MX95-evkはIOキャッシュでないコヒーレントプラットフォームであり、SMMU対応のドライバ VFIO_PCI「IOMMU_CAP_CACHE_COHERENCY」に依存しており、これは公表できません。 詳細はすべてREADMEに記載されています: dpdk/nxp/README_imx95_enetc_vf_vfio at 25.11-qoriq · NXP/dpdk · GitHub dpdkのデータパスでも確認できますが、ドライバは非キャッシュ可能なメモリを使用しているか、SWキャッシュの保守命令を使っています: dpdk/drivers/net/enetc/enetc_rxtx.c at 25.11-qoriq ·NXP/dpdk ·GitHub Re: i.MX95 19x19 EVK: SMMU coherent table walks (IDR0.COHACC) and vfio-pci for DPDK with SMMU enable DPDKチームと話し合っています。 Re: i.MX95 19x19 EVK: SMMU coherent table walks (IDR0.COHACC) and vfio-pci for DPDK with SMMU enable こんにちは、イーピンワンさん 迅速なご返信と貴重なご意見をありがとうございます。今後、さらにご不明な点が生じた場合は、改めてご連絡させていただきます。
View full article
MPC561/562/563/564の評価ボード例 こんにちは、みんな、 MPC561/562/563/564のサンプルの評価ボードを取得するにはどうすればよいですか?MXPのウェブサイトでは見つかりません。 どんなアドバイスでもありがたいです。ありがとう! MPC561/2/3/4汎用評価ボード |NXPセミコンダクターズ Re: Evaluation Board for MPC561/562/563/564 Examples こんにちは@tangyuan2013 これは時代遅れの製品で、もう販売されなくなります。すべてのMPC5xxデバイスは新設計推奨不可のステータスで、徐々に寿命切れに近づいています。これらのデバイスで**お客様**が**製品**を設計することは今後**サポート**しません。より新しい機種を選択することをお勧めします。 よろしくお願いいたします。 ルーカス
View full article
GPIO218仿真器模式下输出异常 GPIO218在全速运行时端口输出电平能够正常翻转。当使用lauterbach的Attach连接后端口电平变成低电平并且不会再进行翻转。请问我该如何分析这个问题? Re: GPIO218仿真器模式下输出异常 你好@liyongfeng , 你说的“无法再翻转”是什么意思?当您执行Siul2_Dio_Ip_WritePin() 函数时,GPDO218 的值是否没有变为 '1'?您是如何测试的? 如果选择“开始”或断开调试器,GPIO 会切换吗? 我做了一个简单的测试,当连接调试器时,可以看到 GPDO 开关。 此致, 朱利安
View full article
Evaluation Board for MPC561/562/563/564 Examples Hello everyone,       How can I get the Evaluation Board for MPC561/562/563/564 Examples?  I can not find in the MXP website.    Any advice is appreciated. Thank you! MPC561/2/3/4 General Purpose Evaluation Board | NXP Semiconductors Re: Evaluation Board for MPC561/562/563/564 Examples Hi @tangyuan2013  this is outdated product which won't be available anymore. All MPC5xx devices are in Not Recommended For New Design status and they are slowly reaching end of life status. We won't support customers designing a product with these devices anymore. We recommend to select newer device. Regards, Lukas
View full article
如何在 MX95 EVK 板上启用第二个摄像头 剧透 (高亮部分可供阅读) 您好,我们想知道如何在 MX95 EVK evk 板的 DSI/CSI 插槽中使用摄像头。我们的相机有RESET和待机引脚,但在 MX95 EVK 原理图中找不到任何 GPIO 引脚来控制它们。 您好,我们想知道如何在 MX95 EVK evk 板的 DSI/CSI 插槽中使用摄像头。我们的相机有RESET和待机引脚,但在 MX95 EVK 原理图中找不到任何 GPIO 引脚来控制它们。 Re: how to enable a second camera on mx95 evk board 嗨@yipingwang谢谢。我们使用的是 TechNexion AR0235 相机,我们希望将其与 CSI 和 CSI/DSI 插槽一起使用。 Re: how to enable a second camera on mx95 evk board 我需要和AE团队确认一下。 Re: how to enable a second camera on mx95 evk board 您好@yipingwang,谢谢您的帮助,但是摄像头仍然无法工作。您有什么建议吗? Re: how to enable a second camera on mx95 evk board J14 A10 DSICSI_RST_SYNC → ADP5585 C0 → gpiochip9 第 6 行 → RESET 通常为低电平有效 J14 A11 DSICSI_EN_PWDN → ADP5585 R4 → gpiochip9 第 4 行 → 掉电通常为高电平有效 正常操作:第 6 行 = 高电平,第 4 行 = 低电平。 Re: how to enable a second camera on mx95 evk board 嗨@yipingwang @yipingwang我应用了以下设置,但相机初始化仍然失败。 hankwang_0-1790059212233.png Re: how to enable a second camera on mx95 evk board 嗨@yipingwang 感谢您确认 J14 A10 (DSICSI_RST_SYNC) 和 A11 (DSICSI_EN_PWDN) 是通过 U81 (ADP5585) 控制的。我们已经确认,我们板上的 ADP5585(i2c 地址 0x34,报告为 adp5585-00)探测成功,并且在 Linux 中作为 gpiochip9 暴露出来,具有 11 条 GPIO 线(0-10;根据我们的设备树,第 5 线保留用于 PWM)。 您能否帮助我们将这两个信号映射到 ADP5585 的确切 GPIO 引脚(例如,根据数据手册,R0-R4/C0-C4 对应的 Linux GPIO 芯片行号(0-10)是多少?另外,每个信号的正确极性(高电平有效/低电平有效)是什么? 我们已经对 10 条可用线路的所有两两组合(90 种组合,两条线路同时拉低)进行了暴力测试,但没有成功——相机的启动状态寄存器 (0x3004) 在所有情况下都保持为 0x0000。如果能从原理图或 UM12022 中获得精确的引脚映射,我们就可以直接验证,而无需继续猜测。 Re: how to enable a second camera on mx95 evk board 在 19 毫米 × 19 毫米的 i.MX 95 EVK 上,i.MX95 EVK DSI/CSI 连接器 (J14) 上的复位和待机引脚是通过 ADP5585 GPIO 扩展器 U81 控制的,而不是直接由 i.MX95 GPIO 控制的: J14 A10 – DSICSI_RST_SYNC:摄像头RESET J14 A11 – DSICSI_EN_PWDN:摄像机待机/掉电 控制电压:1.8V 在设备树中,引用 U81 以进行 reset-gpios 和 pwdn-gpios 的配置。以 NXP 的 imx95-19x19-evk-os08a20-combo.dtb 覆盖层为例,启用共享 DSI/CSI 端口上的第二个摄像头。 Re: how to enable a second camera on mx95 evk board 请确认您使用的是19x19 还是 15x15 evk? Re: how to enable a second camera on mx95 evk board 95 和传感器必须成对配置,以 ov5640 为例。     PWDN(英文),B11 RESET (RST_B), A9 所以在 95 侧,A11 应该是 pwdn,B9 应该是 reset。查看95款19x19 BB板的原理图, A11 由 ADP5585 R4 引脚控制 B9 由 SoC GPIO3 27 控制       因此,在 dts 文件中,用户应按如下方式配置: pinctrl_mipi_dsi_csi: mipidsigrp { fsl,pins = ; }; pinctrl-0 = <&pinctrl_mipi_dsi_csi>; powerdown-gpios = <&adp5585gpio 4 GPIO_ACTIVE_HIGH>; reset-gpios = <&gpio3 27 GPIO_ACTIVE_LOW>; 如果用户需要连接到 15x15 evk 板,那么   pinctrl_mipi_dsi_csi_rst: mipidsirstgrp { fsl,pins = ; }; pinctrl_mipi_dsi_csi: mipidsigrp { fsl,pins = ; }; pinctrl-0 = <&pinctrl_mipi_dsi_csi_rst>, <&pinctrl_mipi_dsi_csi>; powerdown-gpios = <&gpio5 6 GPIO_ACTIVE_HIGH>; reset-gpios = <&gpio5 7 GPIO_ACTIVE_LOW>; Re: how to enable a second camera on mx95 evk board @yipingwang我使用的是 19x19 EVK 主板,我已经解决了这个问题。谢谢。 RESET 引脚配置需要更改;不能使用 J14 A10 DSICSI_RST_SYNC。
View full article
i.MX 95:M7とA55間の動的TRDC/システムマネージャーリソース割り当ておよびGPIO共有 こんにちは、チームのみなさん。 私たちは i.MX 95プラットフォームを開発しており、まずM7コアからMIPI DSIペリフェラルを使用し、その後実行時にリソースをA55コアに引き渡したいと考えています。 私たちの理解では、周辺リソースとその所有権は 、 System Managerツール を通じて生成・設定 された mx95evk.cfg ファイル内の各論理マシン/プロセッサごとに最初に定義されています。 以下の点について明確にしておきたいと思います。 動的リソースハンドオーバー: 実行時にM7からA55へMIPI DSIペリフェラルリソースを動的に移すことは可能でしょうか?例えば、M7は最初にMIPI DSIを所有・使用し、その後リリースし、その後A55が所有権を取得し同じペリフェラルを使用します。 動的リソース配分: ランタイムハンドオーバーがサポートされている場合、リソースの所有権やアクセス権限を動的に変更するための推奨されるメカニズムやAPIは何ですか?これはSystem Manager、TRDC、または他の仕組みで処理されるのでしょうか? GPIO共有: 同じGPIOポート/リソースをM7とA55の両方が同時にアクセスすることは可能でしょうか?もし可能なら、GPIOリソースを安全に共有するためにTRDCの設定要件やソフトウェア同期メカニズムを実装する必要がありますか? i.MX 95におけるM7とA55間の動的ペリフェラルハンドオーバーやリソース共有の実装方法について、推奨される方法についてのご指針をいただけるとありがたいです。 Re: i.MX 95: Dynamic TRDC/System Manager Resource Allocation and GPIO Sharing Between M7 and A55 こんにちは、 i.MX 95では、MIPI DSIリソースは当初M7で使用され、後にA55に引き継がれます。リソースアクセスと所有権はSystem Manager/TRDCの設定で設定し、実際のランタイムハンドオーバーはソフトウェアで処理すべきです。TRDCはどの論理マシン/ドメインが周辺機器にアクセスできるかを制御しますが、M7とA55間の同期は管理しません。したがって、M7はまずすべてのDSI操作を完了し、ペリフェラルの使用を停止し、A55が制御を取る前にMU/IPCなどのコア間機構を通じてA55に通知すべきです。同様に、GPIOリソースは適切なTRDC構成を通じてM7とA55の両方にアクセス可能ですが、同時アクセスはソフトウェアによる同期が必要です。DSIのユースケースでは、同時に1つのコアだけがペリフェラルをアクティブに使い、ハンドオーバーはMU/IPCで行うのが推奨されます。 Re: i.MX 95: Dynamic TRDC/System Manager Resource Allocation and GPIO Sharing Between M7 and A55 AEチームと話し合った結果、以下のアップデート内容をご参照ください。 i.MX 95では、リソース所有権とTRDC権限は、SM構成ファイル(mx95evk.cfg)でビルド時に静的に定義されます。→はconfig_.h)を生成し、MIXが起動するとシステムマネージャー(SM)によって適用されます。*実行時に周辺機器の所有権を論理マシン(LM)から別の論理マシンへ移すSCMI/SMメッセージはありません。 しかし、SMのドキュメントでは「ディスプレイを別のLMへ引き継ぐこと」がSM_SCMI_PERM_EXCLUSIVEモデルの正確な動機として挙げられています。したがって、引き継ぎは可能ですが、所有権を「移動」するだけでは不可能です。 Q1 & Q2 — MIPI DSI M7 → A55 ハンドオーバー:やり方 LMM(論理マシン管理)SCMIプロトコルは、LMの起動・リセット・シャットダウン・サスペンド・ウェイクのみを行い、RESOURCE_ASSIGNやメッセージOWNERSHIP_TRANSFERはありません。代わりに、時間分割ハンドオフを使用してください。 mx95evk.cfgで両方のLMに最初にアクセス権を付与してください。デフォルトでは、EVK の設定により、MIPI_DSI、MIPI_PHY、DC_DISPENG、BLK_CTRL_DISPLAYMIX、ディスプレイのクロック/電源 (PD_DISPLAY、CLK_DISP*)が AP (LM2) の所有者としてのみ割り当てられます。M7 を優先的に使用するには、これらを M7 LM (LM1) にも追加する必要があります。 SM管理リソース(クロック、電源、リセット)をSM_SCMI_PERM_EXCLUSIVE(api=all)としてマークし、2つのLMからのリクエストが静かに集約・上書きされないようにします。 ハンドオーバー時にM7はDSI/DCIFを静止し、アプリケーションレベルのIPC(MUメールボックスまたはSCMI通知)を通じてA55に信号を送ります。A55(Linux/DRM DSI+DPUスタック)は同じIPを表示します。 ハンドオフシーケンスはお客様のソフトウェア責任(時間的区分)です。SMは、両方のLMが事前にアクセス許可されているため、HWがどちら側からも運転可能であることを保証しています。TRDCの所有権は実行時に書き換えられず、SMプログラムのみがTRDCを実行し、MIX電源投入時の静的設定からのみ可能です。 これを制御するTRDC設定(.cfgファイルに記載): MDAC_am=... — マスタードメイン割り当て(バス・マスタをドメインIDにマッピング) MBC_am=s.b— メモリブロックチェック — ここでペリフェラルアクセスがゲートされます MRC_am=… — メモリ領域チェック(DDRなどの大規模メモリ領域) 各LMはDIDにバインドされます。例:SMは2、AP(LM2)は3、M7(LM1)は4でした。 Q3 — M7とA55の間でGPIOを共有 はい、TRDCはM7ドメインとA55ドメインの両方に同じGPIOインスタンスへの同時アクセスを許可できます(両方のDIDでMBCブロックを有効にすること)。しかし、重要な注意点と、支持される2つのパターンがあります。 注意点:i.MX 95 GPIOにはハードウェア仲裁機能がなく、PDR/DR/GDIRレジスタは物理的に共有されるため、両コアレースから非調整の読み書き・修正・書き込みが可能です。 パターンA(分離ピン+ソフトウェア同期):慣例に従って各コアに特定のピンを割り当てます(設定では既にLMごとにピンが分割されています)。データ/方向レジスタバンクは依然として共有されているため、ハードウェアセマフォ/MUを使用して同時RMWを保護するか、コアが同じレジスタバンクに同時にアクセスしないようにしてください。 パターンB(SM仲裁、真に共有されたインスタンスに推奨): SMが所有し、文書化された役割は 「共有アクセスの仲裁 」とされる常時接続 GPIO1 を経由します。IOMUXC/IOMUX_GPRも同様にSMによって調停されます。Pinmux/daisyは、エージェントごとの権限を持つSCMIピン制御プロトコルを介して設定されます。GPIOデータ操作は直接MMIOで行われます。 Re: i.MX 95: Dynamic TRDC/System Manager Resource Allocation and GPIO Sharing Between M7 and A55 チームの皆さん、こんにちは。 私たちは i.MX 95の19x19 EVK を使っており M7とA55/Linux 間のLVDSディスプレイハンドオーバーを以下のアーキテクチャで実装しようとしています。 M7: 当初はLVDSディスプレイを所有し、制御する。 A55/Linux: その後、Linux起動後にディスプレイの制御を奪います。 現在の実装 開発の初期段階として、LVDSディスプレイをM7によって初期化および制御するように設定しました。M7はディスプレイの初期化に成功し、フレームバッファを青色で埋め尽くし、それがLVDSパネルに正しく表示されます。 以下のリソースをデフォルトのA55所有権から M7に変更しつつ、A55へのアクセスは提供しました。 DC DC0 DC1 DC_CMDSEQ DC_DISPENG DC_DISPENG_INT DC_FL0 DC_FL1 DC_INT_CTL DC_PIXENGINE DC_XPC DC_YUV0 DC_YUV1 DC_YUV2 DC_YUV3 BLK_CTRL_DISPLAYMIX LVDS MIPI_PHY LDB_PLL CLOCK_DISP1PIX ビデオPLL1 PIN_I2C2_SCL PIN_I2C2_SDA LPI2C2 観察された行動 現在の動作は以下のとおりです。 M7は起動し、ディスプレイの初期化に成功した。 青色で塗りつぶされたフレームバッファは、LVDSパネル上に正しく表示されます。 M7の動作中は、ディスプレイは表示されたままになります。 その後、A55/Linuxの起動プロセスが始まります。 Linuxカーネルが起動すると、ディスプレイが真っ白になります。 次のデバイスツリーを使用する場合:fdtファイル imx95-19x19-evk-it6263-lvds1.dtbLinuxはカーネル起動時に常に進行が止まります。 カーネルパニックやコンソール上の明確なエラーメッセージは確認されませんでした。起動プロセスが進行しなくなる。 資源所有権調査 私たちの理解によれば、リソース所有権は System Managerの設定 を通じて静的に設定されており、SCMIメッセージを通じて論理マシン間で所有権を動的に移譲することはできません。 そこで、表示資源をM7とA55の両方に割り当てられるかどうかを調査しました。 しかし、重要なDCリソースの中には、二重所有を支持していないものもあります。特に以下の通りです: DC DC_XPC DC_YUV0 DC_YUV1 DC_YUV2 DC_YUV3 DC_FL0 DC_FL1 DC_2DBLIT これにより、LinuxがDRM/DPUやIT6263/LVDSの初期化時にM7専用の表示リソースにアクセスしようとしている可能性が示唆されます。 質問 以下の点を明確にしていただけますか? 1. DC 、 DC_XPC 、 DC_YUV *、 DC_FL* 、または DC_2DBLIT などのリソース がM7独占的に所有されている場合 、Linuxがハングすることは予想されます か?   2. Linuxの起動時およびDRM/DPU、IT6263/LVDSの初期化時にA55/Linuxがアクセスするディスプレイリソースは? 特に、以下の人々が正確にどのようなリソースにアクセスしているのかを理解したいと思います: LinuxのDRM/DPU ディスプレイコントローラ(DC) IT6263ドライバ LVDS/LDBドライバ ディスプレイクロック/PLL構成 3. 以下のシーケンスを可能にするサポートされたSystem マネージャのリソース所有設定はありますか? M7はLVDSディスプレイを初期化し、駆動します。 A55/Linuxは正常に起動します。 その後、A55/Linuxがディスプレイの制御を引き継ぎます。 両方の論理マシンはハンドオーバーに必要なリソースにアクセスできます。 4. DアドレスリソースがM7とA55間で共有できない場合、M7のディスプレイとA55/Linuxの共存またはディスプレイハンドオーバーの推奨アーキテクチャは何でしょうか?   5. A55/Linuxは、起動初期段階でディスプレイを積極的に駆動することを意図していなくても、DCリソース階層全体の所有権を必要とするのでしょうか?   6. このユースケースで、以下の部分で追加の構成変更が必要か? System マネージャリソース構成 TRDCの権限 SCMI構成 Linuxデバイスツリー ディスプレイ/LVDS構成 7. Linuxのブートハングは、特にIT6263/LVDSディスプレイパスの初期化時に、A55/LinuxがM7が所有するディスプレイリソースにアクセスしようとした際に起こる可能性はありますか?     現段階の主な目的は、 早期起動時やDRM/DPU、IT6263/LVDS初期化時にLinuxがアクセスする正確な表示リソース を特定し、それらのリソースがM7の所有権と共存できるかどうかを判断することです。 参照のために System Managerの設定ファイル(.cfg)とLinuxのブートログを添付しています 。 サポートされているリソース所有権構成、表示リソースの依存関係、または実装のための推奨アーキテクチャに関するガイダンス M7/A55 LVDSディスプレイの引き継ぎ 大変ありがたく思います。   よろしくお願いします。   Re: i.MX 95: Dynamic TRDC/System Manager Resource Allocation and GPIO Sharing Between M7 and A55 この問題を解決するためのAN15131があり、このANにはソースコードも添付されています。 ただし、このANのステータスは「ウェブ出版保留中」で、nxp.com ではリリースされていません。 数日お待ちください。
View full article
'examples/freemaster_examples/fmstr_example_pdbdm' 中的应用程序命令问题 各位 已下载 sdk.sdk_2.x_lpcxpresso54114仅提供 FreeMASTER 示例。除了应用程序命令部分之外,其他方面都运行正常,而我在应用程序命令部分发现了一些奇怪的行为。 更多详情已发布在 GitHub 上,链接如下: https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10 祝好 Paolo Re: Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm 您好,如果我理解正确的话,您不明白为什么示例应用程序中的命令 0x10 返回代码 16。 命令 0x10 已注册为回调函数: 因此,当FreeMASTER探测到命令执行时,函数“my_appcmd_handler”会自动被调用。这个回调函数的示例代码非常简单: 这就是为什么你会得到返回代码 16 (=0x10) 作为答案的原因。 我也确认 FreeMASTER 存在一个问题,即对于未知响应,无法显示消息,正如您报告的 app.command(ID 为 0x02)的问题一样。响应 0xcd 应该报告为“未知响应”,但实际上并未生成任何消息。 谢谢, 米哈尔
View full article
imx95 jailhouse iommu configuration Hi, Is it possible to configure the IOMMU for i.MX95 on Jailhouse? I'm comparing https://github.com/nxp-imx/imx-jailhouse/blob/lf-6.18.20_2.0.0/configs/arm64/imx8qm.c with https://github.com/nxp-imx/imx-jailhouse/blob/lf-6.18.20_2.0.0/configs/arm64/imx95.c and latter does not have any .iommu_units defined. Is this an oversight or is this not possible with i.MX95? From my understanding i.MX95 supports the newer SMMUv3, I would expect something like this in the root cell file: .iommu_units= {   {     .type = JAILHOUSE_IOMMU_SMMUV3,     .base = 0x36600000,     .size = 0x100000,   }, } Thanks. Re: imx95 jailhouse iommu configuration Discussed with the AE team. IOMMU is default enabled on i.MX95. Re: imx95 jailhouse iommu configuration IOMMU setting is default enabled in System Manager config file and kernel dts
View full article
MCSPTE1AK144 – 霍尔FOC在转速超过约600 rpm时停止,且Simulink自动部署功能失效 你好, 我正在使用 NXP MCSPTE1AK144芯片和 Sunrise 永磁同步电机,并参考霍尔传感器永磁同步电机 FOC 示例。 软件安装: MATLAB R2025b NXP S32K1xx 2.2.0 支持包 NXP S32K1xx 4.3.0 基于模型的设计工具箱 模型构建成功并生成了 .mot 文件。文件。当我手动复制 .mot 文件时将文件传输到 EVB-S32K144 驱动器后,电机运行正常。通过主机模型,我可以启动和停止电机并更改速度参考值。 我目前面临两个问题。 电机转速超过约 600 转/分钟时停止运转。 电机在低速运转时运行正常。我测试了从每分钟 10 转左右开始的运行情况,也逐渐提高了速度。 当转速超过大约 600 rpm 时,电机停止运转,D11 开始闪烁红色。 我该如何确定导致此次停机的确切故障原因?我应该监测哪个故障变量或寄存器? Simulink 自动部署 Simulink 模型构建成功并生成 .mot 文件。文件已存在,但固件不会自动刷写到主板上。手动复制相同的 .mot 文件将文件写入 EVB-S32K144 驱动器可以正常工作。 如何正确配置才能通过 OpenSDA 将生成的代码自动部署到 S32K144? 我还找到了 NXP 针对此示例的较早建议,该建议使用 MATLAB R2021a 和 NXP 支持包 S32K1xx 2.3.0。您会推荐使用此配置而不是 R2025b 和 MBDT 4.3.0 吗? 谢谢!
View full article
LPSPI3 registers inaccessible from Linux (Bus error on devmem read) — external SPI device on P11 EXP Summary I'm trying to bring up two external MCP2515 CAN controllers (Waveshare 2‑CH CAN HAT, confirmed working on a genuine Raspberry Pi) on the FRDM‑IMX93 board's P11 EXPI header, using LPSPI3 on GPIO_IO08‑11 (the pins that match the Raspberry‑Pi‑compatible header positions per UM12181 Table 21). After fixing every device‑tree‑level issue I could find (power, pinmux, chip‑select, pinctrl‑assert‑gpios), the SPI clock (SCK) never toggles on the physical header pin, and a direct register read of the LPSPI3 block causes a Bus error. A different, known‑working peripheral (LPUART1) reads back fine from the same address space. This points to a resource/bus access restriction (RDC or similar) rather than anything fixable from the Linux device tree. Board / software Board: FRDM‑IMX93 (NXP), SoC: MIMX9352CVVXMAB BSP: NXP i.MX Release Distro, kernel 6.18.2-1.0.0-gf49f45233f7b Target peripheral: lpspi3 (spi@42550000, aliased spi2 in /aliases, real dts label confirmed via /proc/device-tree/__symbols__ to be lpspi3) External device under test: 2× MCP2515 (Waveshare 2‑CH CAN HAT) on CS0/CS1 What's already confirmed working (ruled out) Power to the header. reg_vexp_3v3 / reg_vexp_5v are regulator-fixed nodes that default to disabled (regulator_summary showed use=0). Added regulator-always-on + regulator-boot-on via overlay fragments targeting &reg_vexp_3v3 / &reg_vexp_5v (confirmed real labels via __symbols__). Verified 3.3 V / 5 V physically present on P11 afterwards. Pinmux. GPIO_IO08‑11 correctly muxed to LPSPI3_PCS0/SIN/SOUT/SCK using the official macros from imx93-pinfunc.h. input_reg/input_val are 0x0000/0x0 for these three functions, so no DAISY‑chain select is required (ruled out via macro inspection, no separate register needed). Chip‑select. cs-gpios = <&gpio2 8 GPIO_ACTIVE_LOW>, <&gpio2 7 GPIO_ACTIVE_LOW>; (bit‑banged GPIO CS, matching NXP's own upstream board‑support pattern for this node). Confirmed via cat /sys/kernel/debug/gpio and multimeter/logic‑analyzer: CS0 toggles correctly and physically reaches the header pin. pinctrl-assert-gpios. NXP's own upstream &lpspi3 reference for this board includes pinctrl-assert-gpios = <&pcal6408 0 GPIO_ACTIVE_HIGH>; (this line does not appear in most public guides, only in the board's own dts patch). Added it; confirmed via /proc/device-tree/__symbols__ that pcal6408 resolves, and via cat /sys/kernel/debug/gpio that the GPIO is asserted (out hi) once lpspi3's default pinctrl state is requested. Overlay applies cleanly. No FDT_ERR_NOTFOUND from U‑Boot's fdt apply; /sys/bus/spi/devices/ shows spi2.0 and spi2.1 registered by the SPI core. ERR051608 (LPSPI TCR[PRESCALE] errata). Checked spi-fsl-lpspi.c history — the fix (prescale_max = 1 for fsl,imx93-spi) landed in mainline Aug 2024 / stable 6.6.51 & 6.10.10 Sept 2024, well before this kernel version (6.18.2), and the compatible string (fsl,imx93-spi) is already present in the base board dts, so the driver should auto‑apply this limit. Not ruled out with certainty (no direct register confirmation of the actual PRESCALE field written), but timeline strongly suggests it's already handled. The actual symptom With CS0/CS1, MISO, MOSI, SCK probed on the physical P11 pins (multimeter, then a logic analyzer at 10–20 MSa/s triggered on CS0 falling edge) while continuously retrying a transfer (spidev_test in a loop, and separately by repeatedly forcing mcp251x re‑probe via echo spi2.0 > /sys/bus/spi/drivers/mcp251x/bind): CS0 toggles. Confirmed on both multimeter and logic analyzer. SCK never toggles. Flat, no activity, regardless of continuous transfer attempts. MOSI never toggles. Both MCP2515s fail identically: mcp251x spi2.0/spi2.1: MCP251x didn't enter in conf mode after reset / Probe failed, err=110 (ETIMEDOUT) — i.e. the driver's own SPI‑level reset+read‑CANSTAT sequence gets no response, consistent with SCK never leaving the SoC. Root cause narrowed to clock / bus access, not device tree   # clk_enable_count AND clk_prepare_count are both 0, despite the controller # actively being used in a continuous retry loop $ cat /sys/kernel/debug/clk/clk_summary | grep -i lpspi3 lpspi3_root 0 0 0 50000000 0 0 50000 N deviceless no_connection_id lpspi3 0 0 0 50000000 0 0 50000 N 42550000.spi per $ cat /sys/kernel/debug/clk/lpspi3/clk_prepare_count 0 lpspi3's functional (per) clock shows clk_enable_count=0 and clk_prepare_count=0 even while 42550000.spi (the real, bound consumer) is actively attempting transfers in a loop (spidev_test loop, and separately by repeatedly forcing mcp251x re‑probe via echo spi2.0 > /sys/bus/spi/drivers/mcp251x/bind). clk_prepare() is the step before clk_enable() — the fact that it's never even called suggests the driver's transfer path (or a pm_runtime_get() in front of it) never reaches its own clock‑management code for this device, rather than the clock being requested and then failing to gate on. I don't have kernel build tooling to add tracepoints, so I can't yet tell whether this is a pm_runtime resume that silently no‑ops, a missing dependency (e.g. a power-domains reference this board's lpspi3 node needs but doesn't have), or something else in spi-fsl-lpspi.c for this specific kernel build. The decisive register‑level test — direct devmem read:   $ devmem 0x44380000 32 # LPUART1 base — known-good peripheral 0x04040007 $ devmem 0x42550000 32 # LPSPI3 base (VERID register) Bus error (core dumped) A completely unrelated, working peripheral (LPUART1, used for the debug console) reads back fine from the same CPU/bus context; LPSPI3's base address faults on a plain 32‑bit read. I initially suspected a Resource Domain Controller (RDC) style access restriction specific to this board, but several NXP Community threads (i.MX25/i.MX6ULL "devmem return bus error", i.MX8MP I2C‑from‑DSP thread) point to the same symptom being the normal, expected result of touching an AIPS‑bus peripheral whose clock is gated off — not necessarily a security/domain restriction. That's consistent with clk_enable_count=0 above and makes me now think this is a clock‑enablement bug in the driver/PM path for this device, not (necessarily) an RDC block — though I can't fully rule out RDC without lower‑level tooling. This isn't a general i.MX93 LPSPI3 limitation For context: a separate NXP Community thread ([iMX93AUTO EVK] SPI Configuration for QCA7006AQ, community.nxp.com/t5/i-MX-Processors/iMX93AUTO-EVK-SPI-Configuration-for-QCA7006AQ-with-imx93AUTO-EVK/m-p/1839847) shows someone successfully driving an external SPI device over LPSPI3 on the same GPIO_IO08‑11 pins on the i.MX93‑11x11‑EVK (same SoC), using:   c &lpspi3 { compatible = "fsl,imx93-spi", "fsl,lpspi"; cs-gpios = <&gpio2 8 GPIO_ACTIVE_LOW>; status = "okay"; ... }; &iomuxc { pinctrl_lpspi3_qca: lpspi3grp { fsl,pins = < MX93_PAD_GPIO_IO11__LPSPI3_SCK 0x3fe MX93_PAD_GPIO_IO10__LPSPI3_SOUT 0x3fe MX93_PAD_GPIO_IO09__LPSPI3_SIN 0x3fe MX93_PAD_GPIO_IO08__LPSPI3_PCS0 0x3fe /* native PCS0, not plain GPIO */ >; }; }; I tried this exact variant (native LPSPI3_PCS0/LPSPI3_PCS1 instead of plain GPIO2_IO08/GPIO2_IO07, plus the explicit compatible override) on the FRDM board — no change, devmem 0x42550000 32 still faults, clk_enable_count/clk_prepare_count still 0. This rules out pinmux/compatible‑string choice as the cause on this board, and — combined with the EVK success — makes me suspect something FRDM‑board‑specific (either in imx93-11x11-frdm.dts's handling of lpspi3, or in this board's U‑Boot/ATF‑level RDC/power‑domain setup) rather than a general i.MX93 SoC or mainline‑driver limitation. Questions for NXP Given clk_prepare_count/clk_enable_count stay at 0 for lpspi3 even while the SPI core is actively driving transfers to a bound spi2.0/spi2.1 device, and a plain register read of 0x42550000 bus‑faults — what's missing from the FRDM‑IMX93's lpspi3 device‑tree node (or from board‑level RDC/power‑domain setup) that the working EVK config doesn't need? Is LPSPI3 on the FRDM‑IMX93 intentionally reserved for another domain (e.g. Cortex‑M33 / secure world, or the on‑board MAYA‑W2 tri‑radio module path) at the board's default RDC/ATF configuration, unlike the EVK? Is there a reference imx93-11x11-frdm-lpspi.dts (analogous to imx93-11x11-evk-lpspi.dts) for using LPSPI3 externally via P11 on this specific board? How to reproduce Base board dtb: stock imx93-11x11-frdm.dtb shipped with the i.MX Release Distro image (unmodified NXP lpspi3 + pcal6408 + reg_vexp_3v3/reg_vexp_5v nodes — all confirmed present via __symbols__). Apply the overlay described above (regulator always‑on, pinctrl + cs‑gpios + pinctrl‑assert‑gpios on &lpspi3; tried both plain‑GPIO and native‑PCS0/PCS1 pinmux variants, same result both times). Bind spidev (built‑in, CONFIG_SPI_SPIDEV=y) manually to spi2.0:   echo spidev > /sys/bus/spi/devices/spi2.0/driver_override echo spi2.0 > /sys/bus/spi/drivers/spidev/bind spidev_test -D /dev/spidev2.0 -s 1000000 -v — "succeeds" (no I/O error) but RX data is not a loopback of TX even with MOSI/MISO physically shorted; SCK never toggles on a logic analyzer regardless. cat /sys/kernel/debug/clk/clk_summary | grep lpspi3 → clk_enable_count=0. cat /sys/kernel/debug/clk/lpspi3/clk_prepare_count → 0. devmem 0x42550000 32 → Bus error. devmem 0x44380000 32 (LPUART1) → succeeds normally. Happy to provide the full overlay source, dmesg, and clk_summary/gpio dumps if useful. Re: LPSPI3 registers inaccessible from Linux (Bus error on devmem read) — external SPI device on P11 Hello @irfanktm  Please take a look to the below community post: https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX93-LPSPI3-EXPI-P11-SPI-pins-produce-no-valid-SPI/td-p/2413472 Best regards, Salas.
View full article
FRDM-IMX93:Linux 无法访问 LPSPI3 寄存器(读取设备内存时出现总线错误)——外部 SPI 设备 摘要 我正在尝试在 FRDM-IMX93 板的P11 EXPI 接头上使用LPSPI3在 GPIO_IO08-11 上启动两个外部 MCP2515 CAN 控制器(Waveshare 2-CH CAN HAT,已确认在真正的 Raspberry Pi 上工作)(引脚与 UM12181 表 21 中 Raspberry Pi 兼容接头的位置相匹配)。 在修复了我能找到的所有设备树级问题(电源、引脚复用、片选、引脚控制断言-GPIO)之后,SPI 时钟 (SCK)始终无法在物理接头引脚上切换,并且直接读取 LPSPI3 块的寄存器会导致总线错误。另一个已知工作正常的外部设备(LPUART1)可以从相同的地址空间正常读取数据。这表明存在资源/总线访问限制(RDC 或类似限制),而不是 Linux 设备树中可以修复的问题。 板/软件 开发板:FRDM-IMX93(恩智浦),SoC:MIMX9352CVVXMAB BSP:NXP i.MX 发布发行版,内核版本 6.18.2-1.0.0-gf49f45233f7b 目标外设:lpspi3(spi@42550000,别名在 /aliases 中为 spi2,通过 /proc/device-tree/__symbols__ 确认实际 dts 标签为 lpspi3) 被测外部设备:CS0/CS1 上的 2 个 MCP2515(Waveshare 2 通道 CAN HAT) 已确认有效(已排除) 给排气歧管供电。reg_vexp_3v3 / reg_vexp_5v 是默认禁用的调节器固定节点(regulator_summary 显示 use=0)。通过覆盖片段添加了 regulator-always-on + regulator-boot-on,目标为 &reg_vexp_3v3 / &reg_vexp_5v(通过 __symbols__ 确认了真实标签)。事后验证 P11 上实际存在 3.3 V / 5 V 电压。 Pinmux。使用 imx93-pinfunc.h 中的官方宏,GPIO_IO08‑11 已正确复用到 LPSPI3_PCS0/SIN/SOUT/SCK。对于这三个函数,input_reg/input_val 均为 0x0000/0x0,因此不需要 DAISY 链选择(通过宏检查排除,不需要单独的寄存器)。 芯片选择。cs-gpios = , (位操作 GPIO CS,与 NXP 针对此节点的上游板级支持模式相匹配)。通过 cat /sys/kernel/debug/gpio 和万用表/逻辑分析仪确认: CS0 切换正常,并且物理上连接到了接头引脚。 pinctrl-assert-gpios。NXP自己的上游 &lpspi3 参考中包含 pinctrl-assert-gpios = <&pcal6408 0 GPIO_ACTIVE_HIGH>;(此行并未出现在大多数公开指南中,仅出现在板自己的 dts 补丁中)。已添加;通过 /proc/device-tree/__symbols__ 确认 pcal6408 已解析,并通过 cat /sys/kernel/debug/gpio 确认,一旦请求 lpspi3 的默认 pinctrl 状态,GPIO 就会被钳位(输出 hi)。 覆盖层涂抹顺畅。U-Boot 的 fdt apply 没有出现 FDT_ERR_NOTFOUND;/sys/bus/spi/devices/ 显示 SPI 内核已注册 spi2.0 和 spi2.1。 ERR051608(LPSPI TCR[PRESCALE] 勘误)。已检查 spi-fsl-lpspi.c历史记录——该修复(fsl、imx93-spi 的 prescale_max = 1)已于 2024 年 8 月合并到主线版本 / 稳定版 6.6.51。& 6.10.10 2024 年 9 月,远早于此内核版本 (6.18.2),并且兼容字符串 (fsl,imx93-spi) 已存在于主板 dts 中,因此驱动程序应该自动应用此限制。虽然不能完全排除这种可能性(没有直接的注册确认实际写入了 PRESCALE 字段),但时间线强烈表明此事已经处理完毕。 实际症状 使用万用表探测物理 P11 引脚上的 CS0/CS1、MISO、MOSI、SCK,然后使用逻辑分析仪以 10–20 MSa/s 的采样率在 CS0 下降沿触发,同时不断重试传输(在循环中使用 spidev_test,以及通过 echo spi2.0 > /sys/bus/spi/drivers/mcp251x/bind 反复强制 mcp251x 重新探测): CS0切换。经万用表和逻辑分析仪验证。 SCK 从不切换。平坦,无任何活动,无论持续尝试转移。 MOSI 从不切换。 两个 MCP2515 的故障情况完全相同:mcp251x spi2.0/spi2.1:MCP251x 在复位后未进入配置模式 / 探测失败,错误代码为 110 (ETIMEDOUT) — 即驱动程序自身的 SPI 级复位 + 读取 CANSTAT 序列未得到响应,这与 SCK 从未离开 SoC 的情况一致。 根本原因已缩小到时钟/总线访问,而非设备树。   # clk_enable_count is 0 despite the controller actively being used $ cat /sys/kernel/debug/clk/clk_summary | grep -i lpspi3 lpspi3_root 0 0 0 50000000 0 0 50000 N deviceless no_connection_id lpspi3 0 0 0 50000000 0 0 50000 N 42550000.spi per 即使 42550000.spi(真正的、绑定的消费者)正在循环中积极尝试传输,lpspi3 的功能(每个)时钟也显示 enable_count=0——它并非只是“未使用”(与 lpspi1/2/4 相比,它们是无设备的,也显示 0,因此仅凭这一点并不能得出结论)。 决定性的测试——通过 devmem 直接读取寄存器:   $ devmem 0x44380000 32 # LPUART1 base — known-good peripheral 0x04040007 $ devmem 0x42550000 32 # LPSPI3 base (VERID register) Bus error (core dumped) 一个完全无关的、工作正常的外部设备(LPUART1,用于调试控制台)可以从相同的 CPU/总线上下文中正常读取数据。LPSPI3 的基地址在普通的 32 位读取中就会出现故障,甚至在任何时钟门控或引脚复用考虑之前就会发生这种情况。这看起来像是资源域控制器 (RDC) 或类似的访问控制机制,在硬件级别阻止 Cortex-A55 (Linux) 域访问此外围设备的地址范围,而与 Linux 设备树中的任何可配置项无关。 向恩智浦提出的问题 FRDM-IMX93 上的 LPSPI3 是否故意保留给另一个功能域(例如,该板默认的 RDC 配置中包含 Cortex-M33 / secure world 内核,导致在 Linux 系统下,如果不进行额外的 SPL/ATF/TF-A 级重新配置,则无法使用该内核? 如果是这样,是否有记录在案的方法将 LPSPI3 总线访问权限重新分配给 Cortex-A55 非安全域(U-Boot SPL 中的 RDC 配置,或 OP-TEE/TF-A 更改),或者尽管 GPIO_IO08-11 已引出,但此板的 P11 接头上根本不支持外部 SPI? 这是我的板/内核版本特有的问题,还是默认 FRDM-IMX93 电路板支持包的已知特性?如果存在参考文件 imx93-11x11-frdm-lpspi.dts(类似于 EVK 的 imx93-11x11-evk-lpspi.dts),将会非常有帮助。 如何重现 底板 dtb:随 i.MX 版本 发行版镜像一起提供的标准 imx93-11x11-frdm.dtb(未修改的 NXP lpspi3 + pcal6408 + reg_vexp_3v3/reg_vexp_5v 节点 — 全部通过 __symbols__ 确认存在)。 应用上述覆盖层(regulator always‑on, pinctrl + cs‑gpios + pinctrl‑assert‑gpios on &lpspi3)。 手动将 spidev(内置,CONFIG_SPI_SPIDEV=y)绑定到 spi2.0:   echo spidev > /sys/bus/spi/devices/spi2.0/driver_override echo spi2.0 > /sys/bus/spi/drivers/spidev/bind spidev_test -D /dev/spidev2.0-s 1000000 -v — 传输“成功”(无 I/O 错误),但即使 MOSI/MISO 物理短路,RX 数据也不是 TX 的环回。 devmem 0x42550000 32 → 总线错误。 如果需要,我很乐意提供完整的 overlay 源代码、dmesg 和 clk_summary/gpio 转储。 Re: FRDM-IMX93: LPSPI3 registers inaccessible from Linux (Bus error on devmem read) — external SPI d 你好@irfanktm 希望你一切都好。 请查看以下社区帖子: https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX93-LPSPI3-EXPI-P11-SPI-pins-produce-no-valid-SPI/td-p/2413472 顺祝商祺! 萨拉斯。
View full article
利用智能家居设备节约能源? 有没有人尝试过通过使用智能家居设备来降低能源费用?我即将搬进一套新的出租公寓,希望能想办法减少开支。与伴侣同住。
View full article