Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
KW45B41Z-EVK BLE examples fail with NBU/rpmsg assertion while other examples work normally Hi,   I am using the KW45B41Z-EVK with MCUXpresso IDE.   The following examples run successfully: - lpuart_polling - freertos_hello - flexcan_loopback_transfer - connectivity_test_bm   However, BLE examples such as: - wireless_uart_bm - beacon_bm   fail during startup and stop at an NBU/rpmsg-related assertion before BLE advertising starts.   I also tried using SDK 26.09, but I am having difficulties importing some example projects into MCUXpresso IDE.   My questions are: 1. Are there any required NBU firmware images that must be programmed before running BLE examples? 2. Is there any additional setup required for BLE examples on the KW45B41Z-EVK? 3. Are there any known issues with SDK 26.09 example import in MCUXpresso IDE?   Any guidance would be greatly appreciated.   Thank you. Re: KW45B41Z-EVK BLE examples fail with NBU/rpmsg assertion while other examples work normally Hello, hope you are doing well.   MCUXpresso IDE support has been removed from wireless board examples starting from SDK version 25.06. I would recommend continuing your development using MCUXpresso for VS Code. Here is additional documentation and guides that might be helpful: MCUXpresso for VS Code 26.09 documentation Before running any BLE examples, the NBU firmware must be programmed. For the KW45B41Z-EVK board, use a prepared SB file with NBU firmware. The NBU is programmed with a signed image with provisioned NXP keys. NXP provides the default keys in the fuse (SB3KDK and RoTKTH). The *.sb3 file related to these keys is included in each SDK under the path \main\mcuxsdk\mcuxsdk\middleware\wireless\ble_controller\bin. The steps to load the NBU firmware for KW45 are included in section 6.1 of AN14796.   Best regards, Sofia.
View full article
S32K118 Erase Flash Sector command address format 您好 在手册中 Erase Flash Sector command要求写入的擦除地址为24位,但是DFLASH的起始地址为0x1000_0000 ,我在手册中没有找到写入的24位地址相关说明,请问这方面是有什么特殊映射吗,如果我想擦除0x1000_0000处扇区,我要写入地址为什么 Re: S32K118 Erase Flash Sector command address format 你好@TakanashiLika , FTFC->FCCOB[2] = 0x80; // Flash address [23:16] 0x1000_0000 FTFC->FCCOB[1] = 0x00; // Flash address [15:8] FTFC->FCCOB[1] = 0x00; // Flash address [7:0] 此致, 丹尼尔 Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
View full article
驾照缺失 您好:我的 S32 Design Studio for S32 DS for ARM v.2.2 许可证即将到期。您能帮我检查并延长一下吗?激活码: 7FC9-0FD2-6345-A5F8 谢谢。 Re: Lisence missing 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。
View full article
No organization or sector address map in flash programmer Good day, I am attempting to program a custom board with a MPC8347 and a S29JL064.  I have a fresh install of CodeWarrior 8.8 with the 8.8.5 and 8.8.6 patches on Windows 11.  We are using a CodeWarrior TAP hooked up to ethernet. I need to build a custom config for this in the FPDDeviceConfig.xml.  I was going to use the existing device as a template as suggested but that does not appear to be correct as no organization or sectors show up. I have tried deleting the FlashProgramer folder and using the installer repair option, but it just places the same file back. Is there an error with the config file or is there something else wrong? Thanks Re: No organization or sector address map in flash programmer Hello, There are two distinct problems commonly causing "no organization or sectors" in CW 8.8 Flash Programmer when adding a custom device: 1. Missing Algorithm ELF File (Most Common) When you copy an existing Spansion/Cypress S29GL-series entry as a template, its tag references S29GL-P_16x1.elf , which does not ship with CodeWarrior PA V8.8. When the Flash Programmer cannot resolve the algorithm file, it silently renders the device with no sectors/organization. Fix: Replace the algorithm with amd16x1.elf , which is present in CW 8.8 and is fully compatible with the S29JL064 (AMD command set). 2. Incorrect or Incomplete XML Entry Structure The CW 8.8 XML parser is strict — if the or elements are malformed or copied from an incompatible template, the UI suppresses them silently. File Location The file you need to edit is: C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml     Reference documentation (already on your install): ...\PowerPC_EABI_Tools\FlashProgrammer\Documentation\AddFlashDevs.pdf ...\PowerPC_EABI_Tools\FlashProgrammer\Documentation\AN3630.CreatingFlashAlgorithm.pdf Correct XML Entry for S29JL064 Add this block inside the root element. The S29JL064 is 64 Mbit (8 MB), AMD/CFI command set, 16-bit bus. Sector layout differs by boot variant — use the one matching your part suffix: S29JL064H — Bottom Boot (8×8KB parameter sectors at bottom, 127×64KB main) <Device> <Name>S29JL064HName> <Algorithm>amd16x1.elfAlgorithm> <BusWidth>16BusWidth> <Organizations> <Org> <Name>16x1Name> <Width>16Width> <Interleave>1Interleave> <Sectors> <Sector size="0x2000" number="8"/> <Sector size="0x10000" number="127"/> Sectors> Org> Organizations> Device>   S29JL064J — Top Boot (127×64KB main, 8×8KB parameter sectors at top) <Device> <Name>S29JL064JName> <Algorithm>amd16x1.elfAlgorithm> <BusWidth>16BusWidth> <Organizations> <Org> <Name>16x1Name> <Width>16Width> <Interleave>1Interleave> <Sectors> <Sector size="0x10000" number="127"/> <Sector size="0x2000" number="8"/> Sectors> Org> Organizations> Device>     Regards
View full article
i.MX95 NPUのReLU6出力が6を超えてもエラーや警告なしに問題ないのは予想されますか? こんにちは、 私たちは、i.MX95 Neutron NPU上でReLU6がどのように挙動するかを理解しようとしています。 私たちが理解している限りでは、ReLU6は常に0から6の間の出力値を維持するはずです。私たちは気づきました SSD MobileNet V1モデルではCPUに比べてNPUの検出精度が低いため、 中間層の出力をチェックし始めました。ReLU6を使うレイヤーの場合、基板上の値は 6を超え(最大で約25まで)、同じCPUの同じレイヤー(同じモデル、同じ入力)が常に使われていました 予想通り0-6の差を保ちました。 実行時にボード上でこれに関するエラーや警告は一切表示されませんでした。モデル変換中、 Neutron-compilerは量子化に関する一般的な警告をいくつか表示しますが、どれも表示していません この点に関係しているようです。 以下の点について教えていただけますか: 1.このNPUでReLU6の出力が6を超えることは期待できますか? 2. もしそうでなければ、その場合にコンパイラやランタイムがエラーや警告を表示するべきではないでしょうか? 環境: - ボード:i.MX95 EVK - BSP:LF_6.18.20_2.0.0 - eIQ Neutron SDK: 3.2.3 - モデル:SSD MobileNet V1(uint8、Arm ML-Zoo) ご回答をお待ちしています。 Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 ReLU6はNeutron Supported Operatorsのマークダウンでサポートされているオペレーターとしてリストされていますが、もしそのレイヤーがReLUに変更されていないか確認したいのですが、再現の手順と入手するバイナリを教えていただけますか? eIQ Model Zoo mobilenetv1を試して、Neutronに変換するのも良いでしょう。 よろしくお願いします。 Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? こんにちは、 迅速なご返信ありがとうございます。 1) ReLUではなくReLU6であることを確認する いいえ、この層はReLUに変更されていません。ニュートロンコンパイラ自身のニュートロンIR(--dump-neutron-ir-final-file) それでもFusedActivation = "Relu6"と表示されており、私たちのファイルの解釈ではありません。参照 正確なモデル、コマンド、出力のためのevidence/01_confirm_still_relu6/。 2) 再現手順と取得したバイナリ 正確なコマンド、コンパイルされたモデル、入力についてはevidence/02_reproduction_npu_exceeds_bound/を参照してください。 スクリプト、コンソールログ、そして生の出力テンソルです。i.MX95 EVKボードについて: 最小値=-15 最大値=96 ReLU6の上限値(生データ):上限値を超える要素数:720000個中4650個(0.65%) CPU 上の同じレイヤーは予想通り 0~6 の範囲内に収まります (実際の最大値=5.999、NPU の実際の最大値=24.664)。 3) eIQ Model Zoo mobilenetv1 を試すについて 試してみました(あなたのrecipe.shにあるmobilenet_v1_0.25_128_quant.tflite)。28人のうち、誰もいない CONV_2D/DEPTHWISE_CONV_2Dオペレーターは実際にはReLU6を融合した作動として使っているので、このモデルには含まれていません 報告している問題を再現(または除外)してください。 参考までに、これらはすべてeIQ Neutron SDK 3.2.3を使用していますコンパイラおよび搭載ランタイム全体で。私たちは 問題はNeutronコンパイラ自体にあると推測されます。ReLU6でこのレイヤーをコンパイルするとプレーンに変更されました ReLUはバイトごとに同一のマイクロコードを生成したため、上限は 生成コード自体が問題ありません。 ご自身で確認していただけますか?他に何か必要なことがあれば教えてください。 ご回答をお待ちしています。 Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? こんにちは。 専門家からはまだ最新情報が届いておらず、彼らはまだ調査中です。できるだけ早く最新情報をお伝えします。 その間に、この Thread を参照してサポートチケットを作成してもらえますか?https://support.nxp.com/s/?language=en_US よろしくお願いいたします。 Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? こんにちは。この件に関して何か進展があったかどうか確認したくご連絡いたしました。ありがとう! Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? こんにちは。 内部チームはi.MX95 FRDMボード上でNeutron delegate v1.0.0-d98743a7に、あなたの証拠パッケージを改変せずに再現しました。 これにより、問題はNeutron-compilerのIR生成(正しくFusedActivation = "Relu6"を報告する)ではなく、Neutron NPUのヒューズ済みReLU6クランプの扱いに起因していることが確認されます。 新しいeIQリリースでこの問題は解決するのでしょうか?いいえ 、eIQ Neutron SDK 3.2.3が現在最新リリース版です。Neutron NPUに対して内部チケットを提出しました。 その間、回避策として、下流のロジックがハード [0,6] の範囲を想定するレイヤーでは、NPU 融合 ReLU6 クランプに頼らないようにしてください。NPUサブグラフの後に明示的な非融合クランプ演算を挿入するか、影響を受けるレイヤーをCPUで実行してください。 よろしくお願いします。 Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? こんにちは、 @JosephAtNXP さん。 最新情報のご提供と、そちら側で問題を再現していただき、ありがとうございます。明確な説明とご提案いただいた回避策に感謝いたします。これらは、現在開発中のプロジェクトにおいて検討させていただきます。 前回のメッセージでご要望通り、このThreadを参照したプライベートサポートチケット(CASE番号:01010058)を作成しました。FUTUREアップデートやパッチを追跡CAN SO、内部チケットにリンクしていただけるとありがたいです。 引き続き応援してくださりありがとうございます! よろしくお願いいたします。
View full article
ライセンスがありません こんにちは:私のS32 Design Studioのライセンス(S32 Design Studio for S32 DS for ARM v.2.2)がもうすぐ期限切れになります。確認して延長してもらえますか?アクティベーションコード: 7FC9-0FD2-6345-A5F8 ありがとうございます。 Re: Lisence missing こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。
View full article
KW45B41Z-EVK BLEのサンプルはNBU/rpmsgアサーションで失敗するが、他のサンプルは正常に動作する こんにちは、   私はKW45B41Z-EVKとMCUXpresso IDEを使っています。   以下の例は正常に実行されます。 - lpuart_polling - freertos_hello - フレックスカンループバック転送 - connectivity_test_bm   しかし、BLEの例としては次のようなものがあります。 - ワイヤレスUART_BM - beacon_bm   起動中に失敗し、BLEアドバタイジングが開始される前にNBU/rpmsg関連のアサーションで停止します。   SDK 26.09も試しましたが、いくつかのサンプルプロジェクトをMCUXpresso IDEにインポートするのに苦労しています。   私の質問は以下のとおりです。 1. BLEのサンプルを実行する前に、必ずプログラムしておくべきNBUファームウェアイメージはありますか? 2. KW45B41Z-EVKでBLEのサンプルを使用するには、他に何か設定が必要ですか? 3. MCUXpresso IDEでのSDK 26.09例インポートに既知の問題はありますか?   何かご助言いただければ大変ありがたいです。   よろしくお願いします。 Re: KW45B41Z-EVK BLE examples fail with NBU/rpmsg assertion while other examples work normally こんにちは、お元気でお過ごしでしょうか。   MCUXpresso IDEのサポートは、SDKバージョン25.06以降、ワイヤレスボードの例から削除されました。MCUXpresso for VS Codeを使って開発を続けることをお勧めします。役立つかもしれない追加のドキュメントとガイドはこちらです: MCUXpresso for VS Code 26.09のドキュメント BLEのサンプルを実行する前に、NBUファームウェアをプログラムする必要があります。KW45B41Z-EVKボードの場合は、NBUファームウェアが組み込まれた準備済みのSBファイルを使用してください。NBUには、NXPのプロビジョニング済みキーを含む署名済みイメージがプログラムされています。NXPは、ヒューズにデフォルトのキー(SB3KDKとRoTKTH)を提供しています。これらのキーに関連する*.sb3ファイルは、各SDKsのパス \main\mcuxsdk\mcuxsdk\middleware\wireless\ble_controller\bin の下に含まれています。 KW45用のNBUファームウェアをロードする手順は、 AN14796のセクション6.1に記載されています。   よろしくお願いします、 ソフィア。
View full article
S32K118 フラッシュセクター消去コマンドのアドレス形式 こんにちは。マニュアルには、フラッシュセクタ消去コマンドには24ビットの消去アドレスの書き込みが必要だと記載されています。しかし、DFLASHの開始アドレスは0x1000_0000で、マニュアルには24ビットアドレスの書き込みに関する説明が見当たりません。特別なマッピングが必要なのでしょうか?0x1000_0000のセクタを消去したい場合、どのアドレスを書き込めば良いのでしょうか? Re: S32K118 Erase Flash Sector command address format こんにちは、 @TakanashiLika さん、 FTFC->FCCOB[2] = 0x80; // Flash address [23:16] 0x1000_0000 FTFC->FCCOB[1] = 0x00; // Flash address [15:8] FTFC->FCCOB[1] = 0x00; // Flash address [7:0] よろしくお願いいたします。 ダニエル Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
View full article
Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? Hello, We're trying to understand how ReLU6 behaves on the i.MX95 Neutron NPU. As far as we understand, ReLU6 should always keep its output between 0 and 6. We noticed lower detection accuracy on the NPU compared to the CPU for an SSD MobileNet V1 model, so we started checking intermediate layer outputs. For a layer using ReLU6, the value on the board went above 6 (up to about 25), while the same layer on the CPU (same model, same input) always stayed within 0-6, as expected. We didn't see any error or warning about this at runtime on the board. During model conversion, neutron-compiler does show a couple of general warnings about quantization, but none of them seem related to this specific point. Could you help us understand: 1. Is it expected that a ReLU6 output can go above 6 on this NPU? 2. If not, shouldn't the compiler or the runtime show an error or a warning in that case? Environment: - Board: i.MX95 EVK - BSP: LF_6.18.20_2.0.0 - eIQ Neutron SDK: 3.2.3 - Model: SSD MobileNet V1 (uint8, Arm ML-Zoo) Thank you! Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? Hi, Thank you for your interest in NXP Semiconductor products, ReLU6 is listed as a supported operator in Neutron Supported Operators markdown, I would like to confirm if such layer wasn't changed to ReLU, could you please share the steps to reproduce and the binaries you get? You could try eIQ Model Zoo mobilenetv1 and convert it to Neutron. Regards Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? Hi, Thanks for the quick reply. 1) Confirming it's still ReLU6, not ReLU No, this layer was not changed to ReLU. neutron-compiler's own NeutronIR (--dump-neutron-ir-final-file) still shows FusedActivation = "Relu6" for it - not our interpretation of the file. See evidence/01_confirm_still_relu6/ for the exact model, command, and output. 2) Steps to reproduce, and the binaries we get See evidence/02_reproduction_npu_exceeds_bound/ for the exact commands, the compiled model, input, script, console log, and raw output tensor. On the i.MX95 EVK board: min=-15 max=96 ReLU6 upper bound (raw): 12 elements above the bound: 4650 of 720000 (0.65%) The same layer on the CPU stays within 0-6 as expected (real max=5.999, vs. NPU's real max=24.664). 3) Re: trying eIQ Model Zoo mobilenetv1 We tried it (mobilenet_v1_0.25_128_quant.tflite, from your recipe.sh). None of its 28 CONV_2D/DEPTHWISE_CONV_2D operators actually have ReLU6 as a fused activation, so this model doesn't reproduce (or rule out) the issue we're reporting. For reference, this all uses eIQ Neutron SDK 3.2.3 throughout (compiler and on-board runtime). We suspect the problem is in neutron-compiler itself: compiling this layer with ReLU6 changed to plain ReLU produced byte-for-byte identical microcode, so the upper bound doesn't seem to make it into the generated code at all. Could you confirm this on your end, and let us know if there's anything else you need from us? Thank you! Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? Hi, I’m following up to see if there are any updates on this issue. Thanks! Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? Hi @YoshihiroFurudera, No update has been received from the experts, they are still looking into this. I will share an update as soon as possible. Could you please create a support ticket referencing this thread in the meantime? https://support.nxp.com/s/?language=en_US Regards, Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? Hi @YoshihiroFurudera, Internal team reproduced on i.MX95 FRDM board Neutron delegate v1.0.0-d98743a7, using your evidence package unmodified. This confirms the issue is in the Neutron NPU runtime's handling of the fused ReLU6 clamp, not in neutron-compiler's IR generation (which correctly reports FusedActivation = "Relu6") Would a newer eIQ release fix this? No - eIQ Neutron SDK 3.2.3 is currently the latest released version; I've filed an internal ticket against the Neutron NPU. In the meantime, as a workaround, avoid relying on the NPU-fused ReLU6 clamp for layers where downstream logic assumes a hard [0,6] range - e.g. insert an explicit unfused clamp op after the NPU subgraph, or run the affected layer(s) on CPU. Regards Re: Is it expected that a ReLU6 output can exceed 6 on the i.MX95 NPU, with no error or warning? Hi @JosephAtNXP, Thank you for the update and for reproducing the issue on your end. We appreciate the clear explanation and the suggested workarounds, which we will consider for our current development. As requested in your previous message, I have created a private support ticket (Case Number: 01010058) referencing this thread. We would appreciate it if you could link it to the internal ticket so we can track future updates or patches. Thank you for your continued support! Regards,
View full article
フラッシュプログラマーに組織またはセクターのアドレスマップはありません 良い一日、 MPC8347とS29JL064を搭載したカスタム基板のプログラミングを試みています。Windows 11にCodeWarrior 8.8を新規インストールし、8.8.5と8.8.6のパッチを適用しました。私たちはイーサネットに接続したCodeWarrior TAPを使っています。 FPDDeviceConfig.xmlに、このためのカスタム設定を作成する必要があります。提案されたように既存のデバイスをテンプレートとして使用しようとしたのですが、組織やセクターが表示されないため、それは正しくないようです。 FlashProgramerフォルダを削除してインストーラーの修復オプションを使ってみましたが、同じファイルが元に戻ってしまうだけです。 設定ファイルにエラーがあるのでしょうか、それとも他に何か問題があるのでしょうか? よろしくお願いします。 Re: No organization or sector address map in flash programmer こんにちは、 CW 8.8 Flash Programmerでカスタムデバイスを追加する際に、「組織化やセクター化が行われない」という問題が発生する一般的な原因は、主に2つあります。 1. アルゴリズムELFファイルが見つからない(最もよくあるケース) 既存の Spansion/Cypress S29GL シリーズのエントリをテンプレートとしてコピーすると、その タグは S29GL-P_16x1.elf を参照します。これはCodeWarrior PA V8.8には同梱されていません。フラッシュプログラマーがアルゴリズムファイルを解決できない場合、セクタや組織を一切持たずにデバイスを静かにレンダリングします。 修正:アルゴリズムを amd16x1.elf に置き換えます。これはCW 8.8に搭載されており、S29JL064(AMDコマンドセット)と完全に互換性があります。 2. XMLエントリ構造が不正確または不完全 CW 8.8のXMLパーサーは厳格です。 または 要素の形式が不正であったり、互換性のないテンプレートからコピーされた場合、UIはそれらを黙って非表示にします。 ファイルの場所 編集する必要のあるファイルは次のとおりです。 C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml     リファレンスドキュメント(すでにインストール時にあります): ...\PowerPC_EABI_Tools\FlashProgrammer\Documentation\AddFlashDevs.pdf ...\PowerPC_EABI_Tools\FlashProgrammer\Documentation\AN3630.CreatingFlashAlgorithm.pdf S29JL064の正しいXMLエントリ このブロックを ルート要素内に追加してください。S29JL064は、64Mbit(8MB)、AMD/CFIコマンドセット、16ビットバスです。セクターレイアウトはブートの種類によって異なります。ご使用のパーツのサフィックスに一致するものを使用してください。 S29JL064H — ボトムブート(下部に8×8KBのパラメータセクタ、メイン領域に127×64KB) <Device> <Name>S29JL064HName> <Algorithm>amd16x1.elfAlgorithm> <BusWidth>16BusWidth> <Organizations> <Org> <Name>16x1Name> <Width>16Width> <Interleave>1Interleave> <Sectors> <Sector size="0x2000" number="8"/> <Sector size="0x10000" number="127"/> Sectors> Org> Organizations> Device>   S29JL064J — トップブート(メイン127×64KB、最上位パラメータセクター8×8KB) <Device> <Name>S29JL064JName> <Algorithm>amd16x1.elfAlgorithm> <BusWidth>16BusWidth> <Organizations> <Org> <Name>16x1Name> <Width>16Width> <Interleave>1Interleave> <Sectors> <Sector size="0x10000" number="127"/> <Sector size="0x2000" number="8"/> Sectors> Org> Organizations> Device>     よろしくお願いします。
View full article
iMX8MPとデシリアライザ こんにちは、みんな! 当社では、デジタルビデオレコーダーにi.MX 8M Plusを使用しています。現在、SerDesチップを使って少なくとも2台(より良い4台)のカメラを接続する設計を修正する任務を負っています。調べてみると、DS90UB960やDS90UB954を接続すると問題があるかもしれません。なぜなら、プロセッサは仮想チャネルをサポートしていないからです。 他のデシリアライザー(TI、アナログ Devices、THine Electronicsなど)との接続について、何か情報や良い経験はありますか? 敬具 セルジュ Re: iMX8MP and Deserializers こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 ご指摘の通り、8M Plus i.MX では仮想チャネルがないためシリアライザーは利用できません。i.MX8QMやi.MX8QXP i.MX 8シリーズプロセッサの参照があり、95 i.MX VCをサポートし、シリアライザーの参照もあります。 よろしくお願いします。 Re: iMX8MP and Deserializers デシリアライザーを使って2台のカメラを単一のMIPIインターフェースにコネクテッドすることはできないと理解しています。 しかし、シングルまたはツーカメラをシングルまたは2台のCSI/MIPIインターフェースに接続する実証済みのデシリアライザーソリューションはありますか? 例えば、MAX96714を使用することは可能ですか? Re: iMX8MP and Deserializers こんにちは、 いいえ、説明されているような解決策は証明されていません。 よろしくお願いいたします。 Re: iMX8MP and Deserializers それはとても奇妙だ。私は個人的にTHCV242A+iMXMPを基にしたソリューションを見て手に取ったことがありますが、それが1台のカメラを接続したのか2台のカメラだったかは覚えていません。 Re: iMX8MP and Deserializers こんにち@sfatyushkin、プラットフォームはバーチャルチャネルをサポートしていないため、CSI/MIPIポートごとに一度に1台のカメラからしかストリーミングできません。例えば、2つのデシリアライザがそれぞれ1つのCSI/MIPIポートに接続されている場合です。GMSLに関する資料はこちらです。よろしければご覧ください。 連続したストリーミングが不要で、4つのセンサすべてで低いキャプチャレートを許容できるなら、カメラのストリームを切り替えて各センサを起動・停止するカスタムドライバを実装するのも考えられます。理想的には、ユーザースペースアプリケーションと同期して、フレームが正しく撮影され、正しいカメラに関連付けられていることを確実にする方法も必要です。 よろしくお願いします、 ダニエル・ゴンザレス RidgeRunの組み込みソフトウェアエンジニア 開発者向けWiki: https://developer.ridgerun.com ウェブサイト: www.ridgerun.com
View full article
S32DS_ARM_Win32_v2.2 激活码获取问题 S32DS_ARM_Win32_v2.2现在官网没有提供激活码了,也找不到链接,但是客户的软件过期,想继续使用2.2版本,能帮忙提供一个激活码吗 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 对不起,它是 S32DS_Power_Win32_v2.1 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 我的 S32DS_ARM_Win32_v2.2 许可证也过期了。 您能帮我延长许可证的有效期吗? 59DD-0D10-2BAA-6F30 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 你好、 您的 S32DS 许可证已延期。 回复: S32DS_ARM_Win32_v2.2 激活码获取问题 我的 S32DS_ARM_Win32_v2.2 许可证也过期了。 您能帮我延长许可证的有效期吗? 95F3-8275-56B8-B07D Software Activation Code is already used on this station for 3 Activated 2.2.   AI 润色 130/5000   这是我的激活码。B029-D748-6F13-04AD 软件激活码已在该台用于 3 激活 2.2. 您能帮帮我吗?谢谢 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 能帮我延期一下这个吗 0D8B-07F9-C5B6-3AD8 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 这个问题如何解决呀,帮我解决一下呢,我在安装S32 Design Studio for ARM 2.2,输入官网提供的激活码,每次都会提示for another feature,然后提示三次机会用尽,请帮助我把激活码与旧设备完全解绑,并取消当前设备的次数限制,使我能在新设备上正确安装S32DS V2.2. Re: S32DS_ARM_Win32_v2.2 激活码获取问题 您好,我的也无法激活,显示"您的软件激活码用于其他功能。您想把它退回去吗?"能帮我解决一下吗? Re: S32DS_ARM_Win32_v2.2 激活码获取问题 产品:适用于 ARM 的 S32 设计工作室 激活 ID:9123-5215-159A-B8D0 您能帮忙延长许可证的有效期吗?谢谢。 回复: S32DS_ARM_Win32_v2.2 激活码获取问题 我目前的执照已经过期,您能帮我申请新执照吗? 4249-2545-9811-9321 谢谢 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 我目前的执照即将到期,您能帮我申请新执照吗? 0513-AA9F-08E2-FFE7 谢谢 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 嘿,哥们,你能帮我延长一下 S32DS_ARM_Win32_v2.2 的激活期限吗? C22F-C69B-A049-B9D3 无论如何,谢谢。
View full article
PIC CLB 上的 Eureka 某些 PIC MCU(例如 pic16f13145 系列)具有类似 FPGA 的可编程逻辑,称为可配置逻辑块。 我使用的 pic16f13115 有 32 个单元,每个单元都有一个 4 输入查找表和一个 D 触发器。 为了学习如何使用这些工具,今天我实现了对 6 个 LED 的 Charlieplexing 的 PWM 亮度控制支持,并进行了模拟。我使用 Verilog 来定义电路,而不是使用逻辑 CAD 画布。 我差不多有一半的时间都在用头撞墙。我慢慢地把 Verilog 代码写对了,让它能够综合(版本),然后让它能够仿真。 CLB 编程逻辑即使在 CPU 休眠状态下也能正常工作,这很棒。它非常适合功能安全至关重要的应用。例如,可用于实现复杂的中断触发逻辑。CLB 逻辑与外围输入输出的连接方式非常灵活。它比PIC单片机中一直使用的笨重的CLC可编程逻辑电路灵活得多。 只是想和大家分享一下我的 Eureka 经历。
View full article
IMX95でUSB3.0デバイス接続後にカーネルがクラッシュする こんにちは、 i.MX95 15x15 SoCをベースにしたカスタムデザインでUSB 3.0インターフェースを起動します。私たちのデザインでは、USBハブをネイティブのUSB 3.0ポートに接続しています。 ハブは正常に列挙されますが、USB 3.0 デバイス(例えば、USB ペン ドライブ)をハブに接続すると、カーネル クラッシュが発生します(ログは以下を参照)。これは奇妙だ。なぜなら、同じポートに接続されたUSB 2.0デバイスは問題なく動作するからだ。 デバイスツリーでmaximum-speed = "high-speed";を設定してポートを高速のみに制限すると、同じ USB 3.0 ペン ドライブが USB 2.0 デバイスとして列挙され、正常に動作します。 SMMUの問題ではないことを確認するために、カーネルコマンドラインにiommu.passthrough=1を追加してみましたが、動作は変わりませんでした。 根本原因を特定する手助けをしていただけますか? 私たちはLinuxカーネルバージョン6.18のNXP BSPを使っています。 クラッシュログは以下のとおりです。 root@imx95-15x15-lpddr4x-evk:~# lsusb Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub Bus 001 Device 002: ID 05e3:0610 Genesys Logic, Inc. Hub Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub Bus 002 Device 002: ID 05e3:0620 Genesys Logic, Inc. GL3523 Hub Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub root@imx95-15x15-lpddr4x-evk:~# [ 527.354709] usb 2-1.1: new SuperSpeed USB device number 3 using xhci-hcd [ 527.379284] usb-storage 2-1.1:1.0: USB Mass Storage device detected [ 527.387024] scsi host0: usb-storage 2-1.1:1.0 [ 528.405103] scsi 0:0:0:0: Direct-Access USB SanDisk 3.2Gen1 1.00 PQ: 0 ANSI: 6 [ 528.423345] sd 0:0:0:0: [sda] 60125184 512-byte logical blocks: (30.8 GB/28.7 GiB) [ 528.431953] sd 0:0:0:0: [sda] Write Protect is off [ 528.437387] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA [ 528.492698] sda: sda1 [ 528.495895] sd 0:0:0:0: [sda] Attached SCSI removable disk [ 529.708851] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008 [ 529.717662] Mem abort info: [ 529.720448] ESR = 0x0000000096000004 [ 529.724184] EC = 0x25: DABT (current EL), IL = 32 bits [ 529.729478] SET = 0, FnV = 0 [ 529.732521] EA = 0, S1PTW = 0 [ 529.735649] FSC = 0x04: level 0 translation fault [ 529.740511] Data abort info: [ 529.743380] ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000 [ 529.748848] CM = 0, WnR = 0, TnD = 0, TagAccess = 0 [ 529.753884] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0 [ 529.759179] user pgtable: 4k pages, 48-bit VAs, pgdp=00000001049be000 [ 529.765601] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000 [ 529.772381] Internal error: Oops: 0000000096000004 [#1] SMP [ 529.778031] Modules linked in: polyval_ce mxc_jpeg_encdec v4l2_jpeg snd_soc_imx_card snd_soc_fsl_sai snd_soc_fsl_xcvr snd_soc_fsl_micfil imx_pcm_dma overlay snd_soc_fsl_utils pwm_fan fuse [ 529.794728] CPU: 1 UID: 0 PID: 217 Comm: kworker/1:2H Not tainted 6.18.2-g81bb96fa4952-dirty #15 PREEMPT [ 529.804281] Hardware name: NXP i.MX95 15X15 Mecha Comet (DT) [ 529.809929] Workqueue: blk_mq_run_work_fn (kblockd) [ 529.814899] pstate: 604000c9 (nZCv daIF +PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 529.821847] pc : process_one_work+0xc8/0x284 [ 529.826112] lr : worker_thread+0x2c4/0x3e0 [ 529.830205] sp : ffff800081ff3db0 [ 529.833504] x29: ffff800081ff3dc0 x28: 0000000000000000 x27: 0000000000000000 [ 529.840628] x26: 0000000000000000 x25: ffff00008459e4c0 x24: ffff0000fbb90480 [ 529.847752] x23: ffff000081f1f248 x22: ffff0000fbb90458 x21: 0000000000000000 [ 529.854876] x20: ffff000081f1f240 x19: ffff00008459e480 x18: 0000000000000001 [ 529.862000] x17: 000000040044ffff x16: 005000f2b5503510 x15: 00000027f3567fb3 [ 529.869124] x14: 00000000000000d2 x13: ffff00008495d800 x12: 0000000000000000 [ 529.876248] x11: 00000000000000c0 x10: 0000000000000ab0 x9 : ffff800081ff3d30 [ 529.883372] x8 : ffff00008495e290 x7 : 0000000000000001 x6 : 0000000000000000 [ 529.890496] x5 : 000000050a0a3e6a x4 : ffff000081f1f240 x3 : ffff0000fbb90478 [ 529.897620] x2 : 0000000000000020 x1 : 0000000000000008 x0 : ffff00008459e500 [ 529.904746] Call trace: [ 529.907181] process_one_work+0xc8/0x284 (P) [ 529.911444] worker_thread+0x2c4/0x3e0 [ 529.915188] kthread+0x12c/0x204 [ 529.918412] ret_from_fork+0x10/0x20 [ 529.921987] Code: d2800402 f84086f8 53041f01 b9003261 (f94006a1) [ 529.928068] ---[ end trace 0000000000000000 ]--- [ 529.932679] note: kworker/1:2H[217] exited with irqs disabled [ 529.938512] note: kworker/1:2H[217] exited with preempt_count 1 [ 529.938795] Internal error: Oops - Undefined instruction: 0000000002000000 [#2] SMP [ 529.952155] Modules linked in: polyval_ce mxc_jpeg_encdec v4l2_jpeg snd_soc_imx_card snd_soc_fsl_sai snd_soc_fsl_xcvr snd_soc_fsl_micfil imx_pcm_dma overlay snd_soc_fsl_utils pwm_fan fuse [ 529.968852] CPU: 3 UID: 0 PID: 648 Comm: syslogd Tainted: G D 6.18.2-g81bb96fa4952-dirty #15 PREEMPT [ 529.979530] Tainted: [D]=DIE [ 529.982398] Hardware name: NXP i.MX95 15X15 Mecha Comet (DT) [ 529.988041] pstate: 80400009 (Nzcv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 529.994990] pc : copy_folio_from_iter_atomic+0x260/0x89c [ 530.000303] lr : copy_folio_from_iter_atomic+0x250/0x89c [ 530.005607] sp : ffff800088073ac0 [ 530.008909] x29: ffff800088073b30 x28: 000000000000000f x27: 0001000000000000 [ 530.016033] x26: ffff00008e3236c0 x25: 0000000000000000 x24: 0000000000000462 [ 530.023157] x23: 0000000000000000 x22: ffff000081ba9180 x21: ffff800088073cd0 [ 530.030281] x20: 000000000000000f x19: 0000000000000085 x18: 0000000000000000 [ 530.037405] x17: 0000000000000000 x16: 0000000000000000 x15: 0000ffffcef03a40 [ 530.044529] x14: 0000000000000000 x13: 0000000000000000 x12: ffff000081ba9180 [ 530.051653] x11: ffff00008e3236c0 x10: 0000fffffffffff1 x9 : ffff000081ba9180 [ 530.058777] x8 : 000000000000000f x7 : ffff000091bff462 x6 : ffff000091bff471 [ 530.065901] x5 : 0000000000000085 x4 : ffff000081ba9180 x3 : ffff000091bff000 [ 530.073025] x2 : 000000000000000f x1 : 000000000000000f x0 : 0000000000000000 [ 530.080153] Call trace: [ 530.082595] copy_folio_from_iter_atomic+0x260/0x89c (P) [ 530.087898] generic_perform_write+0x14c/0x25c [ 530.092335] shmem_file_write_iter+0xa0/0xa8 [ 530.096598] do_iter_readv_writev+0xfc/0x1e0 [ 530.100863] vfs_writev+0x134/0x2c0 [ 530.104346] do_writev+0x7c/0x148 [ 530.107657] __arm64_sys_writev+0x20/0x34 [ 530.111661] invoke_syscall+0x48/0x104 [ 530.115405] el0_svc_common.constprop.0+0x40/0xe0 [ 530.120103] do_el0_svc+0x1c/0x28 [ 530.123413] el0_svc+0x34/0xec [ 530.126464] el0t_64_sync_handler+0xa0/0xf0 [ 530.130641] el0t_64_sync+0x198/0x19c [ 530.134302] Code: cb000281 a9408fe7 8b01039c a941a7e5 (8f010339) [ 530.140385] ---[ end trace 0000000000000000 ]--- Same way when we connect USB 2.0 Device on same port. root@imx95-15x15-lpddr4x-evk:~# lsusb Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub Bus 001 Device 002: ID 05e3:0610 Genesys Logic, Inc. Hub Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub Bus 002 Device 002: ID 05e3:0620 Genesys Logic, Inc. GL3523 Hub Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub root@imx95-15x15-lpddr4x-evk:~# [ 106.150901] extcon-tusb320 2-0047: TUSB Device Detected [ 111.942409] usb 1-1.1: new full-speed USB device number 3 using xhci-hcd [ 112.166092] hid-generic 0003:3151:1020.0001: device has no listeners, quitting [ 112.191037] input: YICHIP 2.4G Receiver Mouse as /devices/platform/soc/4c010010.usb/4c100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1.1/1-1.1:1.1/0003:3151:1020.0002/input/input1 [ 112.207047] input: YICHIP 2.4G Receiver System Control as /devices/platform/soc/4c010010.usb/4c100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1.1/1-1.1:1.1/0003:3151:1020.0002/input/input2 [ 112.279679] input: YICHIP 2.4G Receiver Consumer Control as /devices/platform/soc/4c010010.usb/4c100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1.1/1-1.1:1.1/0003:3151:1020.0002/input/input3 [ 112.296313] hid-generic 0003:3151:1020.0002: input: USB HID v2.00 Mouse [YICHIP 2.4G Receiver] on usb-xhci-hcd.2.auto-1.1/input1 root@imx95-15x15-lpddr4x-evk:~# lsusb Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub Bus 001 Device 002: ID 05e3:0610 Genesys Logic, Inc. Hub Bus 001 Device 003: ID 3151:1020 YICHIP 2.4G Receiver Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub Bus 002 Device 002: ID 05e3:0620 Genesys Logic, Inc. GL3523 Hub Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub Linux マルチメディア ソフトウェア不具合の疑い Re: IMX95 Kernel crash after connecting USB3.0 device こんにちは、 デバイスツリーの設定を教えていただけますか? よろしくお願いいたします。 Re: IMX95 Kernel crash after connecting USB3.0 device こんにちは、 @JorgeCas さん。ご返信ありがとうございます。下記のdt設定をご確認ください。 /{ usb1_ss_mux: ptn36043 { compatible = "nxp,ptn36043"; pinctrl-names = "default"; switch-gpios = <&pca9535 00 GPIO_ACTIVE_LOW>; orientation-switch; port { usb1_sw_ep: endpoint { remote-endpoint = <&usb1_sw_ss>; }; }; }; &usb2 { dr_mode = "host"; disable-over-current; status = "okay"; }; &lpi2c3 { clock-frequency = <400000>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_lpi2c3>; status = "okay"; tcpc_1: tusb320@47 { compatible = "ti,tusb320"; reg = <0x47>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_tusb>; interrupt-parent = <&gpio4>; interrupts =<23 IRQ_TYPE_LEVEL_LOW>; vbus-gpios = <&pca9535 8 GPIO_ACTIVE_HIGH>; status = "okay"; connector { compatible = "usb-c-connector"; label = "USB-C-Port1"; data-role = "dual"; power-role = "source"; typec-power-opmode = "default"; ports { #address-cells = <1>; #size-cells = <0>; port@1 { reg = <1>; usb1_sw_ss: endpoint { remote-endpoint = <&usb1_sw_ep>; }; }; }; }; }; &usb3 { status = "okay"; disable-over-current; }; &usb3_dwc3 { dr_mode = "host"; snps,dis-u1-entry-quirk; snps,dis-u2-entry-quirk; status = "okay"; };
View full article
S32DS EcuM ドキュメント 現在、S32K116でLINを実装しようとしています。 Lin_43_LPUAR_FLEXIOモジュールを追加した後、プロジェクトがコンパイルされなくなりました。 どうやら EcuM モジュールも追加しないと動かないようです(この情報はLINドキュメントに追加することをおすすめします)。 EcuMモジュールを追加した後、ドキュメントが付いていないことに気づきました。 私の質問: EcuMモジュールは何のためにあるのですか? これで何ができて、どう使えばいいのでしょうか? なぜLINに必須なのですか? そのドキュメントはどこで見つけられますか? Re: S32DS EcuM documentation こんにちは、 @daniel_meier さん。 EcuM(ECUステートマネージャー)は、ECU状態の共通の側面を管理するAUTOSAR基本ソフトウェア(BSW)モジュールです。 RTDリリースノートに記載されているように 、「Dem、Det、EcuC、EcuM、Rteおよびインターフェースプラグインに含まれる機能はサンプルスタブ関数です」 つまり、RTDにはこれらのモジュールのサンプル実装が含まれており、対応するAUTOSAR基本ソフトウェアモジュールが利用できない場合でもアプリケーションがコンパイルして実行できるようにします。 完全なAUTOSAR環境では、EcuM、Dem、Det、Rteなどのモジュールは通常、Vector、ElektrobitなどのAUTOSARベンダー、またはその他のサードパーティサプライヤーから提供されます。RTDに含まれる実装はあくまでプレースホルダーとして意図されており、インターフェース依存性を満たすために必要な最小限の機能を提供します。 EcuMに関する詳細情報については、モジュールの詳細な説明が記載されているECUステートマネージャーのAUTOSAR仕様をご参照ください。 このモジュールをLINと組み合わせて使う場合、ドライバーユーザーマニュアルと統合マニュアルの確認もお勧めします。これらの文書は、ハードウェアおよびソフトウェアの要件、対応構成、使用ガイドライン、統合手順、既知の制限事項に関する詳細な情報を提供します。これらの文書は、例えば以下で見つけることができます: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K1_S32M24\RTD\Lin_43_LPUART_FLEXIO_TS_T40D2M30I0R0\doc BR、VaneB
View full article
S32DS_ARM_Win32_v2.2 アクティベーションコード取得問題 S32DS_ARM_Win32_v2.2 公式サイトでは現在アクティベーションコードが提供されておらず、リンクも見つかりません。しかし、お客様のソフトウェアの有効期限が切れているため、バージョン2.2を引き続き使用したいのですが、アクティベーションコードの提供をお手伝いいただけますか? Re: S32DS_ARM_Win32_v2.2 激活码获取问题 申し訳ありませんが、S32DS_Power_Win32_v2.1です Re: S32DS_ARM_Win32_v2.2 激活码获取问题 こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 私のS32DS_ARM_Win32_v2.2ライセンスも期限切れです。ライセンスを延長していただけますか? 59DD-0D10-2BAA-6F30 Software Activation Code is already used on this station for 3 Activated 2.2.   愛润色 130 / 5000   これが私の認証コードです。B029-D748-6F13-04AD ソフトウェアのアクティベーションコードは、このステーションで既に3つのアクティベート済み2.2に使用されています。 手伝っていただけませんか?ありがとう!! Re: S32DS_ARM_Win32_v2.2 激活码获取问题 您好,我的也無法激活,显表示「あなたのソフトウェア アクティベーション コードは別の機能用です。返却しますか?」能帮我解决一下吗? Re: S32DS_ARM_Win32_v2.2 激活码获取问题 製品:S32 Design Studio for ARM アクティベーションID: 9123-5215-159A-B8D0 ライセンスの延長にご協力いただけますでしょうか?ありがとう。 回复: S32DS_ARM_Win32_v2.2 激活码获取问题 現在の免許証の有効期限が切れたので、新しい免許証の申請手続きを手伝っていただけますか? 4249-2545-9811-9321 よろしくお願い申し上げます。 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 私の現在の免許証の有効期限が間もなく切れるので、新しい免許証の申請手続きを手伝っていただけませんか? 0513-AA9F-08E2-FFE7 ありがとう Re: S32DS_ARM_Win32_v2.2 激活码获取问题 ねえ、S32DS_ARM_Win32_v2.2の有効化延長を手伝ってもらえますか? C22F-C69B-A049-B9D3 ともかく、ありがとう。
View full article
S32DS EcuM 文档 我目前正在尝试在 S32K116 上实现 LIN。 添加Lin_43_LPUAR_FLEXIO模块后,项目无法编译了。 显然我还需要添加EcuM模块才能使其正常工作(我建议将此信息添加到 LIN 文档中)。 添加EcuM模块后,我发现它没有附带文档。 我的问题: EcuM模块是做什么用的? 我可以用它做什么?我该如何使用它? 为什么LIN需要它? 哪里可以找到相关文档? Re: S32DS EcuM documentation 嗨@daniel_meier EcuM(ECU 状态管理器)是一个 AUTOSAR 基础软件 (BSW) 模块,负责管理 ECU 状态的通用方面。 正如RTD版本说明中所述: "Dem、Det、EcuC、EcuM、Rte和接口插件中包含的函数是示例短截线函数" 这意味着 RTD 包含了这些模块的示例实现,即使相应的 AUTOSAR 基本软件模块不可用,应用程序也能编译和运行。 在完整的 AUTOSAR 环境中,EcuM、Dem、Det 和 Rte 等模块通常由 Vector、Elektrobit 等 AUTOSAR 供应商或其他第三方供应商提供。RTD 中包含的实现仅用作占位符,并提供满足接口依赖关系所需的最低功能。 有关 EcuM 的更多信息,请参阅 ECU 状态管理器的 AUTOSAR 规范,其中提供了该模块的详细描述。 关于将此模块与 LIN 配合使用,我还建议您查阅驱动程序用户手册和集成手册。这些文档提供了有关硬件和软件要求、支持的配置、使用指南、集成程序和已知限制的详细信息。例如,您可以在以下位置找到这些文件: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K1_S32M24\RTD\Lin_43_LPUART_FLEXIO_TS_T40D2M30I0R0\doc BR,VaneB
View full article
S32DS EcuM documentation I am currently trying to implement LIN on an S32K116. After adding the Lin_43_LPUAR_FLEXIO module, the project did not compile anymore. Apparently I need to add the EcuM module as well for it to work (I recommend adding this information to the LIN documentation). After adding the EcuM module, I noticed that it does not come with documentation. My questions: What is the EcuM module for? What can I do with it and how do I use it? Why is it required for LIN? Where can I find the documentation for it? Re: S32DS EcuM documentation Hi @daniel_meier  EcuM (ECU State Manager) is an AUTOSAR Basic Software (BSW) module responsible for managing common aspects of ECU states. As stated in the RTD release notes: "The functions contained in the Dem, Det, EcuC, EcuM, Rte and interface plugins are sample stub functions" This means that RTD includes sample implementations of these modules to allow the applications to compile and run even when the corresponding AUTOSAR Basic Software Modules are not available. In a full AUTOSAR environment, modules such as EcuM, Dem, Det, and Rte are typically provided by AUTOSAR vendors such as Vector, Elektrobit, or other third-party suppliers. The implementations included with RTD are intended only as placeholders and provide the minimum functionality required to satisfy the interface dependencies. For additional information about EcuM, please refer to the AUTOSAR Specification of ECU State Manager, which provides a detailed description of the module. Regarding the use of this module with LIN, I would also recommend reviewing the Driver User Manual and the Integration Manual. These documents provide detailed information on hardware and software requirements, supported configurations, usage guidelines, integration procedures, and known limitations. These documents can be found, for example, at: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K1_S32M24\RTD\Lin_43_LPUART_FLEXIO_TS_T40D2M30I0R0\doc BR, VaneB
View full article
S32DS_ARM_Win32_v2.2 activation code acquisition problem S32DS_ARM_Win32_v2.2 The official website does not provide an activation code now, and I can't find a link. However, the customer's software has expired and I want to continue using version 2.2. Can you help me provide an activation code? Re: S32DS_ARM_Win32_v2.2 激活码获取问题 Hi,  I checked the account related to the activation key and it looks, that the S32DS license is already extended.  Re: S32DS_ARM_Win32_v2.2 激活码获取问题 Hi,  your S32DS license has been extended.  Re: S32DS_ARM_Win32_v2.2 激活码获取问题 My S32DS_ARM_Win32_v2.2 license has expired too.  Could you please extend the license for me?  59DD-0D10-2BAA-6F30 Re: S32DS_ARM_Win32_v2.2 激活码获取问题 Sorry , it's S32DS_Power_Win32_v2.1 Software Activation Code is already used on this station for 3 Activated 2.2.   AI润色 130/5000   This is my activation code. B029-D748-6F13-04AD Software Activation Code is already used on this station for 3 Activated 2.2. Could you please help me? Thank you!! Re: S32DS_ARM_Win32_v2.2 激活码获取问题 您好,我的也无法激活,显示“Your  Software Activation Code is for another feature. Do you want to return it?”能帮我解决一下吗? Re: S32DS_ARM_Win32_v2.2 激活码获取问题 Product: S32 Design Studio for ARM Activation ID: 9123-5215-159A-B8D0 Could you please help to extend the license? Thank you. 回复: S32DS_ARM_Win32_v2.2 激活码获取问题 Could you help me apply for a new license since my current license has expired? 4249-2545-9811-9321 thank you Re: S32DS_ARM_Win32_v2.2 激活码获取问题 Could you help me apply for a new license since my current license is about to expire? 0513-AA9F-08E2-FFE7 thank you Re: S32DS_ARM_Win32_v2.2 激活码获取问题 Hey buddy, could you help me extend the activation for S32DS_ARM_Win32_v2.2? C22F-C69B-A049-B9D3 Thanks anyway.
View full article
iMX8MP 和解串器 大家好! 我们的数字视频注册器中使用的是 i.MX 8M Plus。我们目前的任务是修改设计,使用 SerDes 芯片连接至少两个(最好是 4 个)摄像头。在研究过程中,我发现连接 DS90UB960 或 DS90UB954 可能会有问题,因为该处理器不支持虚拟通道。 是否有关于连接其他解串器(例如 TI、模拟设备、THine Electronics 等)的信息或积极经验? 此致, 哔叽 Re: iMX8MP and Deserializers 您好, 感谢您对恩智浦半导体产品的关注, 正如您所提到的,由于缺少虚拟通道,i.MX 8M Plus 没有可用的串行器,但有适用于 i.MX 8 系列处理器(使用 i.MX8QM 和 i.MX8QXP)的参考,i.MX 95 支持虚拟通道,并且也有串行器参考。 此致 Re: iMX8MP and Deserializers 我知道不能使用解串器将两台摄像机连接到单个 MIPI 接口。 但是,是否有成熟的解串器解决方案可以将单个/两个摄像头连接到单个/两个 CSI/MIPI 接口? 例如,是否可以使用 MAX96714? Re: iMX8MP and Deserializers 您好, 不,目前还没有像文中描述的那样被证实有效的解决方案。 此致, Re: iMX8MP and Deserializers 这很奇怪。我亲眼见过并亲手体验过基于 THCV242A + iMXMP 的解决方案——虽然我不记得它连接的是一台摄像头还是两台摄像头了…… Re: iMX8MP and Deserializers 嗨@sfatyushkin,由于该平台不支持虚拟通道,因此每个 CSI/MIPI 端口一次只能从一个摄像头进行流传输。例如,两个解串器分别连接到一个 CSI/MIPI 端口。这里有一份关于GMSL的资源,如果你想了解一下的话。 如果您不需要连续流传输,或者可以容忍所有四个传感器较低的捕获速率,那么另一种可能的方法是实现一个自定义驱动程序,该驱动程序可以在摄像头流之间切换,并根据需要启动和停止每个传感器。理想情况下,还需要一种方法将其与用户空间应用程序同步,以确保捕获帧并将其与正确的摄像头关联起来。 此致, 丹尼尔·冈萨雷斯 RidgeRun公司的嵌入式软件工程师 开发者维基: https://developer.ridgerun.com 网站: www.ridgerun.com
View full article