こんにちは、
i.MX95 15x15 SoCをベースにしたカスタムデザインでUSB 3.0インターフェースを起動します。私たちのデザインでは、USBハブをネイティブのUSB 3.0ポートに接続しています。
ハブは正常に列挙されますが、USB 3.0 デバイス(例えば、USB ペン ドライブ)をハブに接続すると、カーネル クラッシュが発生します(ログは以下を参照)。これは奇妙だ。なぜなら、同じポートに接続されたUSB 2.0デバイスは問題なく動作するからだ。
デバイスツリーでmaximum-speed = "high-speed";を設定してポートを高速のみに制限すると、同じ USB 3.0 ペン ドライブが USB 2.0 デバイスとして列挙され、正常に動作します。
SMMUの問題ではないことを確認するために、カーネルコマンドラインにiommu.passthrough=1を追加してみましたが、動作は変わりませんでした。
根本原因を特定する手助けをしていただけますか?
私たちはLinuxカーネルバージョン6.18のNXP BSPを使っています。
クラッシュログは以下のとおりです。
root@imx95-15x15-lpddr4x-evk:~# lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 05e3:0610 Genesys Logic, Inc. Hub
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 002 Device 002: ID 05e3:0620 Genesys Logic, Inc. GL3523 Hub
Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
root@imx95-15x15-lpddr4x-evk:~# [ 527.354709] usb 2-1.1: new SuperSpeed USB device number 3 using xhci-hcd
[ 527.379284] usb-storage 2-1.1:1.0: USB Mass Storage device detected
[ 527.387024] scsi host0: usb-storage 2-1.1:1.0
[ 528.405103] scsi 0:0:0:0: Direct-Access USB SanDisk 3.2Gen1 1.00 PQ: 0 ANSI: 6
[ 528.423345] sd 0:0:0:0: [sda] 60125184 512-byte logical blocks: (30.8 GB/28.7 GiB)
[ 528.431953] sd 0:0:0:0: [sda] Write Protect is off
[ 528.437387] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA
[ 528.492698] sda: sda1
[ 528.495895] sd 0:0:0:0: [sda] Attached SCSI removable disk
[ 529.708851] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000008
[ 529.717662] Mem abort info:
[ 529.720448] ESR = 0x0000000096000004
[ 529.724184] EC = 0x25: DABT (current EL), IL = 32 bits
[ 529.729478] SET = 0, FnV = 0
[ 529.732521] EA = 0, S1PTW = 0
[ 529.735649] FSC = 0x04: level 0 translation fault
[ 529.740511] Data abort info:
[ 529.743380] ISV = 0, ISS = 0x00000004, ISS2 = 0x00000000
[ 529.748848] CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[ 529.753884] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[ 529.759179] user pgtable: 4k pages, 48-bit VAs, pgdp=00000001049be000
[ 529.765601] [0000000000000008] pgd=0000000000000000, p4d=0000000000000000
[ 529.772381] Internal error: Oops: 0000000096000004 [#1] SMP
[ 529.778031] Modules linked in: polyval_ce mxc_jpeg_encdec v4l2_jpeg snd_soc_imx_card snd_soc_fsl_sai snd_soc_fsl_xcvr snd_soc_fsl_micfil imx_pcm_dma overlay snd_soc_fsl_utils pwm_fan fuse
[ 529.794728] CPU: 1 UID: 0 PID: 217 Comm: kworker/1:2H Not tainted 6.18.2-g81bb96fa4952-dirty #15 PREEMPT
[ 529.804281] Hardware name: NXP i.MX95 15X15 Mecha Comet (DT)
[ 529.809929] Workqueue: blk_mq_run_work_fn (kblockd)
[ 529.814899] pstate: 604000c9 (nZCv daIF +PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 529.821847] pc : process_one_work+0xc8/0x284
[ 529.826112] lr : worker_thread+0x2c4/0x3e0
[ 529.830205] sp : ffff800081ff3db0
[ 529.833504] x29: ffff800081ff3dc0 x28: 0000000000000000 x27: 0000000000000000
[ 529.840628] x26: 0000000000000000 x25: ffff00008459e4c0 x24: ffff0000fbb90480
[ 529.847752] x23: ffff000081f1f248 x22: ffff0000fbb90458 x21: 0000000000000000
[ 529.854876] x20: ffff000081f1f240 x19: ffff00008459e480 x18: 0000000000000001
[ 529.862000] x17: 000000040044ffff x16: 005000f2b5503510 x15: 00000027f3567fb3
[ 529.869124] x14: 00000000000000d2 x13: ffff00008495d800 x12: 0000000000000000
[ 529.876248] x11: 00000000000000c0 x10: 0000000000000ab0 x9 : ffff800081ff3d30
[ 529.883372] x8 : ffff00008495e290 x7 : 0000000000000001 x6 : 0000000000000000
[ 529.890496] x5 : 000000050a0a3e6a x4 : ffff000081f1f240 x3 : ffff0000fbb90478
[ 529.897620] x2 : 0000000000000020 x1 : 0000000000000008 x0 : ffff00008459e500
[ 529.904746] Call trace:
[ 529.907181] process_one_work+0xc8/0x284 (P)
[ 529.911444] worker_thread+0x2c4/0x3e0
[ 529.915188] kthread+0x12c/0x204
[ 529.918412] ret_from_fork+0x10/0x20
[ 529.921987] Code: d2800402 f84086f8 53041f01 b9003261 (f94006a1)
[ 529.928068] ---[ end trace 0000000000000000 ]---
[ 529.932679] note: kworker/1:2H[217] exited with irqs disabled
[ 529.938512] note: kworker/1:2H[217] exited with preempt_count 1
[ 529.938795] Internal error: Oops - Undefined instruction: 0000000002000000 [#2] SMP
[ 529.952155] Modules linked in: polyval_ce mxc_jpeg_encdec v4l2_jpeg snd_soc_imx_card snd_soc_fsl_sai snd_soc_fsl_xcvr snd_soc_fsl_micfil imx_pcm_dma overlay snd_soc_fsl_utils pwm_fan fuse
[ 529.968852] CPU: 3 UID: 0 PID: 648 Comm: syslogd Tainted: G D 6.18.2-g81bb96fa4952-dirty #15 PREEMPT
[ 529.979530] Tainted: [D]=DIE
[ 529.982398] Hardware name: NXP i.MX95 15X15 Mecha Comet (DT)
[ 529.988041] pstate: 80400009 (Nzcv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 529.994990] pc : copy_folio_from_iter_atomic+0x260/0x89c
[ 530.000303] lr : copy_folio_from_iter_atomic+0x250/0x89c
[ 530.005607] sp : ffff800088073ac0
[ 530.008909] x29: ffff800088073b30 x28: 000000000000000f x27: 0001000000000000
[ 530.016033] x26: ffff00008e3236c0 x25: 0000000000000000 x24: 0000000000000462
[ 530.023157] x23: 0000000000000000 x22: ffff000081ba9180 x21: ffff800088073cd0
[ 530.030281] x20: 000000000000000f x19: 0000000000000085 x18: 0000000000000000
[ 530.037405] x17: 0000000000000000 x16: 0000000000000000 x15: 0000ffffcef03a40
[ 530.044529] x14: 0000000000000000 x13: 0000000000000000 x12: ffff000081ba9180
[ 530.051653] x11: ffff00008e3236c0 x10: 0000fffffffffff1 x9 : ffff000081ba9180
[ 530.058777] x8 : 000000000000000f x7 : ffff000091bff462 x6 : ffff000091bff471
[ 530.065901] x5 : 0000000000000085 x4 : ffff000081ba9180 x3 : ffff000091bff000
[ 530.073025] x2 : 000000000000000f x1 : 000000000000000f x0 : 0000000000000000
[ 530.080153] Call trace:
[ 530.082595] copy_folio_from_iter_atomic+0x260/0x89c (P)
[ 530.087898] generic_perform_write+0x14c/0x25c
[ 530.092335] shmem_file_write_iter+0xa0/0xa8
[ 530.096598] do_iter_readv_writev+0xfc/0x1e0
[ 530.100863] vfs_writev+0x134/0x2c0
[ 530.104346] do_writev+0x7c/0x148
[ 530.107657] __arm64_sys_writev+0x20/0x34
[ 530.111661] invoke_syscall+0x48/0x104
[ 530.115405] el0_svc_common.constprop.0+0x40/0xe0
[ 530.120103] do_el0_svc+0x1c/0x28
[ 530.123413] el0_svc+0x34/0xec
[ 530.126464] el0t_64_sync_handler+0xa0/0xf0
[ 530.130641] el0t_64_sync+0x198/0x19c
[ 530.134302] Code: cb000281 a9408fe7 8b01039c a941a7e5 (8f010339)
[ 530.140385] ---[ end trace 0000000000000000 ]---
Same way when we connect USB 2.0 Device on same port.
root@imx95-15x15-lpddr4x-evk:~# lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 05e3:0610 Genesys Logic, Inc. Hub
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 002 Device 002: ID 05e3:0620 Genesys Logic, Inc. GL3523 Hub
Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
root@imx95-15x15-lpddr4x-evk:~# [ 106.150901] extcon-tusb320 2-0047: TUSB Device Detected
[ 111.942409] usb 1-1.1: new full-speed USB device number 3 using xhci-hcd
[ 112.166092] hid-generic 0003:3151:1020.0001: device has no listeners, quitting
[ 112.191037] input: YICHIP 2.4G Receiver Mouse as /devices/platform/soc/4c010010.usb/4c100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1.1/1-1.1:1.1/0003:3151:1020.0002/input/input1
[ 112.207047] input: YICHIP 2.4G Receiver System Control as /devices/platform/soc/4c010010.usb/4c100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1.1/1-1.1:1.1/0003:3151:1020.0002/input/input2
[ 112.279679] input: YICHIP 2.4G Receiver Consumer Control as /devices/platform/soc/4c010010.usb/4c100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1.1/1-1.1:1.1/0003:3151:1020.0002/input/input3
[ 112.296313] hid-generic 0003:3151:1020.0002: input: USB HID v2.00 Mouse [YICHIP 2.4G Receiver] on usb-xhci-hcd.2.auto-1.1/input1
root@imx95-15x15-lpddr4x-evk:~# lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 05e3:0610 Genesys Logic, Inc. Hub
Bus 001 Device 003: ID 3151:1020 YICHIP 2.4G Receiver
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 002 Device 002: ID 05e3:0620 Genesys Logic, Inc. GL3523 Hub
Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
こんにちは、
デバイスツリーの設定を教えていただけますか?
よろしくお願いいたします。