Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
RT1180-EVK: No compatible probes available. Hi, I have installed MCUXpressoIDE (25.6.136) and the RT1180 SDK (26.06). When I try to debug one of the demo applications, I get the following message: Connect to target: MIMXRT1189xxxxx  No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target. I've tried with the 26.03 RT1180 SDK and have had no luck. This was previously working before, so I'm not sure what happened. Any help would be appreciated, thanks! Re: RT1180-EVK: No compatible probes available. Dear @sismail , Are you currently using the default LinkServer Probe? If the LinkServer Probe is not available, could you please try using a J-Link Probe instead: One possibility is that the firmware on the onboard MCU-Link may have been accidentally updated to the J-Link firmware during previous use. In that case, the board would no longer be recognized as a LinkServer Probe.   If the board can be connected successfully using a J-Link Probe, that would strongly indicate that the onboard MCU-Link firmware has indeed been programmed with J-Link firmware.   Best Regards, Shelly Re: RT1180-EVK: No compatible probes available. Both the default LinkServer probe and J-Link Probe have the same error: No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target. Re: RT1180-EVK: No compatible probes available. Dear @sismail , Please perform the following checks: 1.Verify that the evaluation board can run a program normally Use the MCUXpresso Secure Provisioning Tools to program an LED-blinking application through USB in Serial Download mode. Then switch the board back to QSPI Boot Mode and reset the board. Check whether the LED-blinky application runs correctly after reboot. 2. Check the onboard MCU-Link jumper settings Please confirm the following jumper settings: JP5: Open JP3: Open JP6: Connected to pins 1–2 to make sure that the board is not configured for use with an external Debug Probe. 3. Check whether the PC recognizes the Probe using LinkServer Run the command  linkserver probes  in a command-line window: Please check whether the onboard MCU-Link Probe appears in the command output. Please share the results of the above checks, so that we can further investigate the issue. Best regards, Shelly Re: RT1180-EVK: No compatible probes available. Hi Shelly, I am not sure how to use the MCUXpresso Secure Provisioning Tools but I have confirmed that the MCU-Link jumper settings are correct, and the PC does not recognize the Prove using LinkServer: ➜ LinkServer_26.9.130 ./LinkServer probes # Description Serial Device Board Capabilities --- ------------- -------- -------- ------- -------------- Re: RT1180-EVK: No compatible probes available. Dear @sismail , There may be an issue with your onboard MCU-Link.  Could you please try: Step 1: Power the EVK Connect a 5 V power supply to J2. Turn SW1 to the ON position. Step 2: Connect the USB cable Connect the USB cable to J53 (MCU-Link USB). At this point, the PC should enumerate an MCU-Link VCOM Port: For MCUXpresso Secure Provisioning Tool (SPT), please refer to the official tutorial below: https://mcuxpresso.nxp.com/secure/latest/quick_start_guide.html   Best Regards, Shelly Re: RT1180-EVK: No compatible probes available. Hi Shelly, I've followed the steps for powering the EVK and connecting the USB cable. Where can I see the ports dropdown? Despite these steps I'm still not able to see any probes discovered Re: RT1180-EVK: No compatible probes available. Dear @sismail , You should be able to see the enumerated COM port in Windows Device Manager. If the MCU-Link is not enumerated successfully, please first check the power supply. If the power supply is normal, then a hardware issue should be considered.   We have the following suggestions: 1. Use the MCUXpresso Secure Provisioning Tool (SPT) to program a simple LED-blinky application :https://mcuxpresso.nxp.com/mcuxsdk/latest/boards/RT/evkmimxrt1180/gettingStarted/topics/bootable_image_generation.html 2 Check the status of LED D39 and D3 on the board. D3 should remain ON, while D39 should be blinking. Best Regards, Shelly
記事全体を表示
MPC5777C BGA516 bsdl-file Hello, I'm searching for the bsdl-file for the MPC5777C 516ball BGA. Can anyone help me? Furthermore, what is the usual way to get bsdl file ? Thanks. Re: MPC5777C BGA516 bsdl-file Hello, Usually you write a ticket and we will send you the file. I will provide it to you once you rise a ticket in it. https://www.nxp.com/company/about-nxp/smarter-world-videos/NCP-VIDEO Best regards, Peter
記事全体を表示
MPC5777C BGA516 bsdlファイル こんにちは、 MPC5777C 516ball BGAのbsdlファイルを探しています。 どなたか助けてくれませんか? さらに、BSDLファイルを取得する一般的な方法は何ですか? ありがとう。 Re: MPC5777C BGA516 bsdl-file こんにちは、 通常は、チケットを作成していただければ、こちらからファイルをお送りします。 あなたがそのチケットを発行したら、私がそれをお渡しします。 https://www.nxp.com/company/about-nxp/smarter-world-videos/NCP-VIDEO よろしくお願いします、 ピーター
記事全体を表示
アメリカで最もリードするモバイルアプリ開発会社はどこですか? Konstant Infosolutionsは、米国を代表するモバイルアプリ開発企業として認識されており、スケーラブルなAI駆動のモバイルアプリソリューションを提供することで知られています。 経験豊富なモバイルアプリ開発会社であるコンスタント・インフォソリューションズは、AI、Flutter、React Native、iOS、Androidなどの最新テクノロジの専門知識を活かし、インテリジェントでスケーラブルなデジタルソリューションを開発しています。 多様なポートフォリオ、柔軟な採用モデル、そして実際のビジネス成果を目指す姿勢により、Konstant Infosolutionsは競争の激しい市場でAI駆動のアプリソリューションを構築したい企業にとって信頼できるアプリ開発会社として際立っています。
記事全体を表示
Who Is the Leading Mobile App Development Company in USA? Konstant Infosolutions is recognized as a leading mobile app development company in USA, known for offering scalable AI-driven mobile app solutions. As an experienced mobile app development company, Konstant Infosolutions brings expertise in modern technologies like AI, Flutter, react native, iOS, and Android to develop intelligent and scalable digital solutions. With a diverse portfolio, flexible hiring models, and a commitment to delivering real business results, Konstant Infosolutions stands out as a reliable app development company for businesses that are looking to build AI-driven app solutions in a competitive market.
記事全体を表示
imx6ull->ADC Hi, I am working with an i.MX6ULL-based custom SOM module. For our requirements, we are configuring the pins using Config Tools for i.MX Processors. In Config Tools, I selected Create a Standalone Project, then selected i.MX 6ULL → (6Y2...05). Our requirement is to configure the pins using Config Tools, take the generated .dtsi file, and use the same file to build the image. However, this did not work initially. For UART, I understood that we need to add the corresponding device node and set its status to okay. Similarly, a small modification was also required in the generated .dtsi file. I have attached the .dtsi file generated by Config Tools. Please have a look at it. In that file, when I commented out the imx6ull-board line, the configurations started working properly. After UART, I moved on to ADC configuration. When I checked the ADC configuration in Config Tools, I noticed that the ADC appears to use the same GPIO pin. However, I observed that when I configure one GPIO pin as GPIO and another GPIO pin as ADC, the generated IOMUX configuration looks the same. Why is this the case? Is this the expected behavior? Could you please help me understand the correct way to configure and test the ADC on our i.MX6ULL custom SOM? Also, our original requirement was to configure the pins using Config Tools, take the generated configuration file, and directly use it to build and flash the image. I would like to confirm whether this approach should work for our custom board or whether additional changes are required in the generated .dtsi file. I have attached the dts and .dtsi file generated from Config Tools for your reference. what actually does this meant by? Re: imx6ull->ADC Hello @Et_MM  It seems to be a bug from Config Tools for i.MX6ULL. Please clarify what GPIO you want as ADC and what other for GPIO function. I can help you to generate the correct &adc1 node and the correct pinmux. Best regards, Salas. Re: imx6ull->ADC Hello @Et_MM  Hope you are doing very well. Yes, ADC1 is the just one available. For your use case, please use the below to your device tree: &adc1 { num-channels = <10>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_adc1>; status = "okay"; }; &iomuxc { pinctrl_adc1: adc1grp { fsl,pins = < MX6UL_PAD_GPIO1_IO03__GPIO1_IO03 0x3000 MX6UL_PAD_GPIO1_IO04__GPIO1_IO04 0x3000 >; }; }; That will use just the GPIO1_IO03 and GPIO1_IO04 as ADC channels. root@imx6ul7d:/sys/bus/iio/devices/iio:device1# cat in_voltage3_raw 75 root@imx6ul7d:/sys/bus/iio/devices/iio:device1# cat in_voltage4_raw 0 root@imx6ul7d:/sys/bus/iio/devices/iio:device1# cat name 2198000.adc Best regards, Salas. Re: imx6ull->ADC I want GPIO01_IO01 , GPIO01_IO02 as GPIO itself and GPIO01_IO03,GPIO01_IO04 as ADC. when i searched the dtsi file it looked like we have only one adc that is adc1. adc2 is not available. please correct me if i am wrong. Also guide me how can i test and verify that adc and gpio pins that we configured is working. How can i test that? Already i have shared the dts and dtsi file that we are using. Hoping that you have already seen that. Is the configuration in mentioned for adc is wrong in that?  Re: imx6ull->ADC Thank you for the reply. if i want to configure GPIO01_IO01 , GPIO01_IO02 as GPI. How does the configuration will be could you please help me with that also. Re: imx6ull->ADC Hello! You can simply add the below inside the &iomux: pinctrl_hog: hoggrp { fsl,pins = < MX6UL_PAD_GPIO1_IO01__GPIO1_IO01 0x10b0 MX6UL_PAD_GPIO1_IO02__GPIO1_IO02 0x10b0 >; }; Just be sure that is not claimed by another perupheral. Best regards, Salas. Re: imx6ull->ADC Hi, Thank you for the reply i will try this. I have tried the ADC with the configuration you gave and when i run those commands this is my output: root@imx6ul7d:/sys/bus/iio/devices/iio:device0# cat in_voltage1_raw 78 root@imx6ul7d:/sys/bus/iio/devices/iio:device0# cat in_voltage4_raw 74 But any other way to test this pins so i can confirm this is working.
記事全体を表示
MCXA154 Sensor Project Not sure if this is the right spot to post my first NXP project but so far I'm really liking MCUXpresso and the MCX line of processors. Adding peripherals and configuring pins went smooth on the FRDM board so I thought I'd make a custom board. All open source hardware and software files availible if interested. @mikerankin Development Board MCXA Re: MCXA154 Sensor Project Hello @0miker0 , Thank you for your interest in NXP MCX products. MCX provides a rich software ecosystem. Besides Config Tools, you can also explore Secure Provisioning Tool, GUI Guider, FreeMASTER, and more. MCUXpresso Ecosystem Enhancements - NXP Community You are also very welcome to share your project with the community. We encourage technical discussions and knowledge sharing. Have a good day! BR Celeste
記事全体を表示
Recommended CVBS (PAL/NTSC) video encoder for i.MX8 I'm looking for a suitable external video encoder / CVBS DAC to generate a PAL/NTSC composite output on an i.MX8-based board. Requirements: - 1 CVBS output (PAL/NTSC) Questions: - What do you currently recommend as a video encoder to pair with i.MX8? - Is the ADV7391/ADV7393 still the go-to part, or is there a newer/better supported alternative? Thanks in advance! Graphics & Display Re: Recommended CVBS (PAL/NTSC) video encoder for i.MX8 Hello @kbch  Hope you are doing well. The i.MX8 family does not have a native BT656 parallel output interface, unlike i.MX6 which featured an IPU with dedicated BT656/BT1120 output ports. The i.MX8 family display outputs are: MIPI-DSI, HDMI, and LVDS (depending on the exact part number). Q1. There is no NXP-officially recommended or kernel-supported external CVBS encoder for i.MX8 at this time. The i.MX8 does not natively expose a BT656 output bus. Q2. The adv739x Linux kernel driver does exist and was used for i.MX6, not i.MX8 family. Best regards, Salas.
記事全体を表示
KW47: Gap_CheckIfBonded() の deviceId を取得するにはどうすればよいですか? こんにちは、 私はKW47上でBLEアプリケーションを開発しており、Gap_RemoveBond()を使ってボンディング情報を削除したいと考えています。 APIを調べているうちに、Gap_CheckIfBonded()という関数を見つけましたが、deviceIdパラメータにどのような値を渡すべきか、またその値をどのように取得すればよいのかが分かりません。 説明していただけますか? Gap_CheckIfBonded() に渡すべき deviceId は何ですか? KW47でこのデバイスIDを取得するにはどうすればいいですか? よろしくお願いします。 プロトコル:BLE→コネクティビティ プロトコル:Bluetooth Re: KW47: How to obtain deviceId for Gap_CheckIfBonded()? こんにちは、 @hyama さん。 Gap_CheckIfBonded( ) 関数はGAPピアのデバイスIDを入力として受け取り、接続されたピアデバイスがボンディングされているかどうか、対応するNVMインデックスを返します。 Gap_CheckIfBonded()およびGap_RemoveBond()の実例については、KW47-EVKのble_shell_freertos SDK例を参照してください。具体的にはshell_gap.cにおいてファイル。 他に質問がありましたら、お気軽にお知らせください。 BR ハビブ。 Re: KW47: How to obtain deviceId for Gap_CheckIfBonded()? ありがとう。サンプル実装を確認してみます。
記事全体を表示
iMx.95 FRDM ポスト量子アルゴリズムのサポート 私はiMX.95 FRDM開発ボードを持っており、ポスト量子アルゴリズムのハードウェアアクセラレーションを使いたいと考えています。 私はこのコマンドを試しました: PKCS11-tool --module /USR/lib/libsmw_pkcs11.so.5 --list-mechanism しかし、ML-KEMやML_DSAはリストに載っていません。 現在、YoctoでIMXイメージ #m 構築しています。 ポスト量子アルゴリズムのサポートを有効にするにはどうすればいいですか? Re: iMx.95 FRDM post quantum algorithms support こんにちは、 Linuxカーネルオプションで単に「PQCを有効にする」だけで済むわけではありません。 i.MX 95機能はEdgeLockのセキュア・エンクレーブ/ハードウェアの信頼の基点に統合されています。 i.MX 95 Advanced Profile セキュア・エンクレーブは、ポスト量子ハードウェアの信頼の基点を可能にし、NXP署名付きセキュア・エンクレーブファームウェア向けのハイブリッドML-DSA + ECDSAをサポートします。 SPSDKおよびML-DSAハイブリッドセキュアブート実装を備えた i.MX 95があり、一般的なPQCドキュメントよりもはるかに有用です。 i.MX 95 セキュアブート(SPSDK搭載) NXP PQCの一般的なアーキテクチャは以下のとおりです。 NXPのポスト量子暗号 Re: iMx.95 FRDM post quantum algorithms support リンクをありがとうございます! 簡単ではないのは承知していますが、Linuxのユーザー空間アプリケーションからPQCのハードウェアアクセラレーションを利用したいと思っていて、それを実現する最良の方法が何か知りたいと思っています。私は、関係する両者がML-DSAを使って自分たちを認証し、ML-KEMを使って暗号化された通信セッション用の共有秘密鍵を取得するアプリケーションを開発しています。 これを読んでいました:RM00284: EdgeLock Enclave Hardware セキュリティ Module API についてですが、質問ですが、アプリケーションドメイン上で動作するLinuxユーザーアプリケーションのAPIを利用できますか?それとも、それは低消費電力リアルタイム領域でのみ利用可能な機能なのでしょうか?
記事全体を表示
推荐用于 i.MX8 的 CVBS (PAL/NTSC) 视频编码器 我正在寻找一款合适的外部视频编码器/CVBS DAC,以便在基于i.MX8的电路板上生成PAL/NTSC复合输出。 要求: - 1 路 CVBS 输出(PAL/NTSC) 问题: - 目前您推荐哪款视频编码器与 i.MX8 搭配使用? - ADV7391/ADV7393 仍然是首选部件吗?还是有更新/支持更好的替代方案? 提前感谢! 图形与显示 Re: Recommended CVBS (PAL/NTSC) video encoder for i.MX8 你好@kbch 希望你一切都好。 与 i.MX6 不同,i.MX8 系列没有原生 BT656 并行输出接口,而 i.MX6 则配备了带有专用 BT656/BT1120 输出端口的 IPU。 i.MX8 系列显示输出接口有:MIPI-DSI、HDMI 和 LVDS(取决于具体部件号)。 Q1. 目前还没有 NXP 官方推荐或内核支持的适用于 i.MX8 的外部 CVBS 编码器。i.MX8 本身并不提供 BT656 输出总线。 Q2. adv739x Linux 内核驱动程序确实存在,并且用于 i.MX6,而不是 i.MX8 系列。 顺祝商祺! 萨拉斯。
記事全体を表示
MPC561/562/563/564 示例评估板 大家好, 如何获取MPC561/562/563/564示例的评估板?我在MXP网站上找不到。 任何建议都将不胜感激。谢谢你! MPC561/2/3/4 通用评估板 | 恩智浦半导体 Re: Evaluation Board for MPC561/562/563/564 Examples 嗨@tangyuan2013 这是过时的产品,以后不会再销售了。所有 MPC5xx 器件均处于“不建议用于新设计”状态,并且正在逐渐接近产品生命周期结束。我们将不再支持客户使用这些设备设计产品。我们建议选择较新的设备。 此致, Lukas
記事全体を表示
GPIO218 emulator mode output error The GPIO218 output level toggles correctly when running at full speed. However, after using Lauterbach's Attach connection, the port level goes low and stops toggling. How can I analyze this problem? Re: GPIO218仿真器模式下输出异常 Hello @liyongfeng, What do you mean by "can no longer flip"? When you go over the Siul2_Dio_Ip_WritePin() function, does GPDO218 not change to '1'? How are you testing this? If you select 'Go' or disconnect the debugger, does the GPIO toggle? I have made a simple test, and I can see GPDO switch when debugger is attached. Best regards, Julián
記事全体を表示
S32K36x引导加载程序实现 尊敬的恩智浦技术支持团队: 我目前正在评估贵公司的微控制器,以用于某个应用。我特别想使用S32K364微控制器型号。但是,我不太确定如何为其实现引导加载程序功能。 如果我们想使用 CAN-FD 为我们的 MCU 刷写固件,我们是否应该直接采用四年前为原始 S32K31x/K32x/K34x MCU 编写的现有“统一引导加载程序演示”?或者是否有专门为 S32K36x 系列编写的更官方的引导加载程序示例项目可供我们直接使用? 提前感谢! Re: S32K36x Bootloader Implementation 嗨@SewerynP 请看我整理的S32K3引导加载程序示例: https://community.nxp.com/t5/S32K/S32K385-Bootloader/m-p/2367874/highlight/true#M58710 NXP 并未针对每个 S32K3 衍生产品提供可用于生产的引导加载程序代码。提供的引导加载程序演示是参考软件,旨在作为开发您自己的解决方案的起点,并且可以适配 S32K364。对于可直接投入生产使用的解决方案,您可以考虑使用第三方产品,例如 Vector Flash Bootloader。 此致, Lukas
記事全体を表示
S32K36x Bootloader Implementation Dear NXP Support Team, I am currently in the process of evaluating your microcontrollers for an application. I would specifically like to use the S32K364 microcontroller model. However, I am uncertain about how to implement a bootloader function for it. Are we supposed to simply adapt the existing "unified bootloader demo" from four years ago made for the original S32K31x/K32x/K34x MCUs if we want to flash our MCU using CAN-FD or is there a more official bootloader example project written specifically for the S32K36x series we could use directly?  Thanks in advance! Re: S32K36x Bootloader Implementation Hi @SewerynP  Please see my summary of the available S32K3 bootloader examples here: https://community.nxp.com/t5/S32K/S32K385-Bootloader/m-p/2367874/highlight/true#M58710 NXP does not provide production-ready bootloader code specifically for every S32K3 derivative. The available bootloader demos are reference software intended as a starting point for developing your own solution and can be adapted to S32K364. For a production-ready solution, you can consider third-party products such as Vector Flash Bootloader. Regards, Lukas
記事全体を表示
i.MX8に推奨されるCVBS(PAL/NTSC)ビデオエンコーダー i.MX8ベースのボード上でPAL/NTSCコンポジット出力を生成するための、適切な外部ビデオエンコーダー/CVBS DACを探しています。 要件: - CVBS出力×1(PAL/NTSC) 質問: i.MX8と組み合わせるビデオエンコーダーとして、現在おすすめするものは何ですか? ADV7391/ADV7393は今でも定番の部品ですか?それとも、より新しく、サポート体制の整った代替品がありますか? よろしくお願いいたします! グラフィックスとディスプレイ Re: Recommended CVBS (PAL/NTSC) video encoder for i.MX8 こんにちは、 @kbchさん あなたの調子が良いといいのですが。 i.MX8ファミリは、専用のBT656/BT1120出力ポートを持つIPUを持つi.MX6とは異なり、ネイティブのBT656並列出力インターフェースを持たない。 i.MX8ファミリーのディスプレイ出力は、MIPI-DSI、HDMI、LVDS(正確な部品番号によって異なります)です。 Q1. 現時点では、i.MX8向けにNXPが公式に推奨またはカーネルでサポートされている外部CVBSエンコーダーはありません。i.MX8は、BT656出力バスをネイティブに提供していません。 Q2. adv739x Linuxカーネルドライバーは存在し、i.MX6で使われていましたが、i.MX8ファミリには使われていません。 よろしくお願いいたします。 サラス。
記事全体を表示
iMx.95 FRDM 后量子算法支持 我有一块 iMX.95 FRDM 开发板,我想使用后量子算法硬件加速。 我尝试过这条命令: pkcs11-tool --module /usr/lib/libsmw_pkcs11.so.5 --list-mechanism 但未列出 ML-KEM 或 ML_DSA。 我目前正在使用 Yocto 构建 imx 镜像。 如何启用后量子算法支持? Re: iMx.95 FRDM post quantum algorithms support 你好, 你不能简单地通过 Linux 内核选项“启用 PQC”。 i.MX 95 功能已集成到 EdgeLock 安全隔离区/硬件信任根中。 i.MX 95 高级配置文件安全隔离区支持后量子硬件信任根,并支持 NXP 签名的安全隔离区固件的混合 ML-DSA + ECDSA。 i.MX 95 有一个采用 SPSDK 和 ML-DSA 混合安全启动实现的版本,这比一般的 PQC 文档要有用得多: i.MX 95 安全启动(带 SPSDK) NXP PQC 的通用架构如下: NXP后量子密码学 Re: iMx.95 FRDM post quantum algorithms support 谢谢你提供的链接! 我知道这并不简单,但我希望在 Linux 用户空间应用程序中使用 PQC 硬件加速,我想知道实现这一目标的最佳方法是什么。我正在开发一个应用程序,其中参与双方使用 ML-DSA 进行身份验证,并使用 ML-KEM 获取用于加密通信会话的共享密钥。 我正在阅读以下内容: RM00284:EdgeLock Enclave 硬件网络安全模块 API ,我的问题是:我能否从运行在应用程序功能域上的 Linux 用户应用程序中使用该 API?或者,这只能从低功耗实时功能域获得?
記事全体を表示
MCXA154传感器项目 不确定这里是否是发布我的第一个 NXP 项目的合适地方,但到目前为止,我真的很喜欢 MCUXpresso 和 MCX 系列处理器。在 FRDM 板上添加外设和配置引脚都很顺利,所以我决定制作一块定制板。如有兴趣,可提供所有开源硬件和软件文件。@mikerankin 开发板 MCXA Re: MCXA154 Sensor Project 你好@0miker0 , 感谢您对恩智浦MCX产品的关注。 MCX 提供丰富的软件生态系统。除了配置工具外,您还可以探索安全配置工具、GUI 指南、FreeMASTER 等。 MCUXpresso 生态系统增强功能 - NXP 社区 我们也非常欢迎您与社区分享您的项目。我们鼓励技术讨论和知识分享。 祝你有美好的一天! BR 塞莱斯特
記事全体を表示
GPIO218エミュレータモード出力エラー GPIO218の出力レベルは、フルスピードで動作しているときは正しく切り替わります。しかし、LauterbachのAttach接続を使用すると、ポートレベルが低くなり、切り替わらなくなります。この問題をどのように分析すればよいでしょうか? Re: GPIO218仿真器模式下输出异常 こんにちは@liyongfengさん 「もう転売できない」とはどういう意味ですか?Siul2_Dio_Ip_WritePin() 関数を実行した際に、GPDO218 の値が「1」に変化しないのでしょうか?どのようにテストしていますか? 「Go」を選択するか、デバッガーを切断すると、GPIOは切り替わりますか? 簡単なテストを行ったところ、デバッガを接続するとGPDOが切り替わるのが見えました。 よろしくお願いします、 ジュリアン
記事全体を表示
MPC561/562/563/564の評価ボード例 こんにちは、みんな、 MPC561/562/563/564のサンプルの評価ボードを取得するにはどうすればよいですか?MXPのウェブサイトでは見つかりません。 どんなアドバイスでもありがたいです。ありがとう! MPC561/2/3/4汎用評価ボード |NXPセミコンダクターズ Re: Evaluation Board for MPC561/562/563/564 Examples こんにちは@tangyuan2013 これは時代遅れの製品で、もう販売されなくなります。すべてのMPC5xxデバイスは新設計推奨不可のステータスで、徐々に寿命切れに近づいています。これらのデバイスで**お客様**が**製品**を設計することは今後**サポート**しません。より新しい機種を選択することをお勧めします。 よろしくお願いいたします。 ルーカス
記事全体を表示