Hi, I have installed MCUXpressoIDE (25.6.136) and the RT1180 SDK (26.06). When I try to debug one of the demo applications, I get the following message:
Connect to target: MIMXRT1189xxxxx
No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target.
I've tried with the 26.03 RT1180 SDK and have had no luck. This was previously working before, so I'm not sure what happened. Any help would be appreciated, thanks!
Dear @sismail ,
Are you currently using the default LinkServer Probe?
If the LinkServer Probe is not available, could you please try using a J-Link Probe instead: