Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
.exe 是常用的代码包,软件包格式吗? 您好, 我是某些微控制器系列的 CAN/UART 引导加载程序的开发者。我想弄清楚扩展支持的微控制器范围并增加对一些 NXP 设备的支持是否有意义。到目前为止,我还没有接触过恩智浦(NXP)的微控制器。 令我有点惊讶的是,当我在论坛和 NXP 网站上搜索“引导加载程序”一词时,我发现有很多 Windows 可执行文件可供下载。当我在主网站的搜索栏中输入“bootloader”一词时,第二个搜索结果竟然是指向加密货币网站的直接链接。 如果我想查看“统一引导加载程序演示”,真的必须拥有一台 Windows 电脑,并且下载并运行一个 .exe 文件吗?文件? 顺祝商祺! 托斯滕
View full article
Fault flag clearing behavior of FS6500 Hi team, I have a question regarding the fault flag clearing behavior of FS6500.   According to the datasheet, the LPOOF (bit0) and DFS (bit1) flags inside the MODE register (address 0x15) shall be cleared only by Power-on reset or register read operation. However, from my hardware test:   Writing to the MODE register also clears LPOOF and DFS fault bits unexpectedly.   There is no description in the datasheet mentioning that write access can clear these status flags. Could you help explain the root cause for this phenomenon?   Is this intended silicon behavior or undocumented side effect?   Thanks & Best regards   DEVKIT-MPC5744P FS6500  Re: Fault flag clearing behavior of FS6500 Hello, Check you write instruction. In most software drivers, a register write is implemented as a read-modify-write (RMW) sequence. If the datasheet specifies that reading MODE clears LPOOF/DFS, then the flags may already be cleared during the read phase. The subsequent write merely creates the impression that the write operation caused the clearing. Best regards, Peter
View full article
KW45B41Z-EVK:BLE 时钟源和内部时钟路径,用于 BLE 无线电模块获取 2.4GHz 频段。 您好,NXP团队, 我正在使用 KW45B41Z-EVK,想了解BLE 子系统使用的时钟架构。 我已查阅了KW45B41 参考手册、 KW45B41Z-EVK 用户手册和 SDK 时钟初始化代码,但仍然找不到有关 BLE 时钟源及其内部时钟路径的详细说明。 请您澄清以下问题: BLE 使用的主要时钟源是什么(例如,SOSC、FRO、PLL 或其他时钟源)? 要获得 2.4GHz 的频率,从振荡器到 BLE 无线电的完整时钟路径是什么?具体来说,在时钟信号到达 BLE 子系统之前,涉及哪些时钟模块、多路复用器、分频器或锁相环? BLE 子系统在广播模式、扫描模式、连接模式或睡眠模式下是否使用不同的时钟源? 是否有时钟树图或应用笔记说明 KW45B41 设备的 BLE 时钟架构? 参考手册或其他恩智浦文档的哪些章节对此进行了详细描述? 如果可以,请提供 BLE 时钟路径的框图或相关文档的参考,引用,我们将不胜感激。 感谢您的支持。 顺祝商祺! Re: KW45B41Z-EVK: BLE clock source and internal clock path for the BLE radio to get 2.4GHz 你好, 希望你一切都好! BLE 子系统的主要时钟源是 OSC-RF(射频振荡器),它与外部晶体或谐振器结合使用,为 KW45 无线电生成参考时钟。它支持 26 MHz 或 32 MHz,并且在与主 CPU 时钟域完全独立的功率域中运行,专门用作无线电子系统的参考时钟。 KW45 参考手册中包含两张图,可能对理解 BLE 时钟架构特别有帮助: 图 68。设备时钟源和树 图 222。无线电时钟 如 RM 第 55.4.4 节所述,该无线电使用三个时钟源:无线电 XO (OSC-RF)、FRO-192M 和来自 CCM32K 模块的 SOC 32.768 kHz。在活动运行模式(包括广播、扫描和连接)期间,所有三个时钟域同时处于活动状态。OSC-RF 及其 XCVR PLL 正在运行以支持无线电 TX 和 RX(这由 NBU 固件在内部管理),FRO-192M 正在为 NBU CM3 内核提供时钟以执行链路层,而 32K_CLK 正在后台运行以跟踪连接和广播间隔。 对于低功耗模式行为,表 209 描述了每个时钟模块在不同功率状态下的行为。 使用MCUXpresso 配置工具中的“时钟”选项卡也可能有所帮助。在那里,您可以可视化每个功能域的时钟源路由,查看交互式时钟树,并根据需要更改时钟源。它还会生成时钟初始化源代码,这对于了解启动时如何配置每个时钟域来说是一个有用的参考。 此致, 索菲亚。
View full article
FRDM-MX95 PRO software packages? I was wondering what OS software packages will be available for the MX95 PRO?  Will Android AAOS be available for it as a demo image?  Is there anyone we can communicate with about what will specifically be available? Re: FRDM-MX95 PRO software packages? currently, only linux 6.18.20_2.0.0 demo images for imx95 frdm pro Embedded Linux for i.MX Applications Processors | NXP Semiconductors you can download demo images from the link above, for android, I checked the board file, the latest android 16.0.0_2.0.0 is based on kernel 6.18.20_2.0.0, so should support frdm pro, but this version android hasn't verified on this board yet, only 19x19 evk and 15x15 frdm Re: FRDM-MX95 PRO software packages? Any news if we will get android automotive on the frdm-mx95 or would we have to upgrade to frdm-mx95 pro version? Re: FRDM-MX95 PRO software packages? let me confirm auto android team again, the owner is on vacation, and come back office in next week, any update I will let you know it Re: FRDM-MX95 PRO software packages? refer to the link as below https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/android-automotive-os-for-i-mx-applications-processors:ANDROID-AUTO auto android demo images are only for imx95 19x19 evk Re: FRDM-MX95 PRO software packages? Are there any plans for android or AAOS?  Seems weird that the FRDM MX95 Pro wouldn't have an AAOS version especially since the Evaluation board 19x19 has been discontinued and benched.  Is there a reason the pro being a 19x19 processor wouldn't work as the evaluation board. Re: FRDM-MX95 PRO software packages? Thanks. There seems to be a genuine lack of Android automotive support. The frdm has a lot of potential but without additional support from nxp we are left on our own. From my understanding the evk has been dropped from support from toradex and discontinued. With the frdm pro having the same hardware there should be some support. We need the BSP which would make building the images a lot easier. Re: FRDM-MX95 PRO software packages? Is there any way i can contact them to ask a question? Or could they give us some instructions on how to compile the new frdm pro board, maybe they can provide the board package file to make it easier for us to compile? Re: FRDM-MX95 PRO software packages? unfortunately, got information from auto android team that they haven't any plan to support any imx95 frdm board Re: FRDM-MX95 PRO software packages? since they don't have plan to support this yet, I don't think they can offer any packages to build Re: FRDM-MX95 PRO software packages? Even though it isn't listed yet, I just wanted to let the community know that I was able to flash Android 16.0.0_2.0.0 (L6.18.20_2.0.0 BSP) to eMMC, and it ran fine on my FRDM-IMX95-PRO board.  AOSP Android 16 worked well enough that I could deploy my own custom Trusty applet and have a corresponding Android app communicate with it afterward. I just saw Android 17.0.0_1.0.0 (L6.18.37_2.1.0 BSP) posted on the NXP website today (if Android 16 worked, I'm guessing Android 17 should work as well too)
View full article
KW45B41Z-EVK: BLEクロックソースおよびBLE無線用の2.4GHz内部クロックパス NXPチームの皆様、こんにちは。 私はKW45B41Z-EVKを使用しており、 BLEサブシステムで使用されているクロックアーキテクチャについて理解したいと考えています。 KW45B41のリファレンス・マニュアル、KW45B41Z-EVKユーザーマニュアル、SDKsのクロック初期化コードを調べましたが、BLEクロックソースとその内部クロック経路の詳細な説明は見つかりませんでした。 以下の点を明確にしていただけますか? BLEで使用される主要なクロックソースは何ですか(例えば、SOSC、FRO、PLL、または別のクロックソースなど)? 発振器からBLE無線機まで、2.4GHzを実現するための完全なクロックパスはどのようなものですか?具体的には、クロックがBLEサブシステムに到達する前に、どのクロックモジュール、マルチプレクサ、分周器、またはPLLが関与しているのでしょうか? BLEサブシステムは広告、スキャン、コネクテッドモード、またはスリープモードで異なるクロックソースを使っていますか? KW45B41デバイスのBLEクロックアーキテクチャを示すクロックツリー図やアプリケーションノートはありますか? リファレンス・マニュアルや他のNXPドキュメントのどのセクションでこの点が詳しく説明されていますか? 可能であれば、BLEクロックパスのブロック図や関連ドキュメントの参照をぜひ提供していただけると助かります。 再開まで今しばらくお待ちください。 よろしくお願いいたします。 Re: KW45B41Z-EVK: BLE clock source and internal clock path for the BLE radio to get 2.4GHz こんにちは、 あなたの調子が良いといいのですが! BLEサブシステムの主要なクロック源はOSC-RF(RF オシレーター)であり、外部クリスタルや共振器と連携してKW45無線機の基準クロックを生成します。26 MHzまたは32 MHzのいずれかに対応し、CPUのメインクロックドメインとは完全に別の電力領域で動作し、無線サブシステムのリファレンスクロックとして専ら機能します。 KW45リファレンスマニュアルには、BLEクロックアーキテクチャを視覚化するのに特に役立つ2つの図が含まれています。 図68。デバイスのクロックソースとツリー 図222。ラジオ時計 RMの55.4.4節に記載されているように、無線機は3つのクロックソースを使用しています:Radio XO(OSC-RF)、FRO-192M、そしてCCM32KモジュールからのSOC 32.768 kHzです。アクティブ動作モード(広告、スキャン、コネクテッドを含む)では、3つのクロックドメインすべてが同時にアクティブです。OSC-RFとそのXCVR PLLは無線TXおよびRXをサポートするために動作しており(これはNBUファームウェアによって内部的に管理)、FRO-192Mはリンク層実行のためにNBU CM3コアをクロックし、32K_CLKはバックグラウンドで接続および広告間隔を追跡しています。 低電力モードの動作については、表209に各クロックモジュールが異なる電力状態においてどのように動作するかを示します。 MCUXpresso Config Toolsの Clocks タブを使用すると役立つ場合もあります。そこでは、各ドメインごとにルーティングされたクロックソースを可視化し、インタラクティブなクロックツリーを確認し、必要に応じてクロックソースを変更できます。また、クロックの初期化ソースコードを生成し、各クロックドメインが起動時にどのように設定されているかを理解するのに役立つ参考資料となります。 よろしくお願いします、 ソフィア。
View full article
SENTプロトコル こんにちは、コミュニティの皆さん。 位置センサが付いているアクチュエータの位置検出のためにS32K311基板上でSENTプロトコルを実装する方法を模索しています。NXPはSENTプロトコルに関連するブロックセットを持っていません。どなたか情報を共有していただけると大変助かります。 Re: SENT Protocol こんにちは、@ Ganesh808 S32 DS + RTD を使用している場合は、弊社の S32 DS サンプルコードに flexio を使用して SENT プロトコルを実装するデモが含まれています。 MBDTを使用している場合、以下のような同様の回答を見たことがあります。 https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SENT-Protocol-Support-in-S32K3-MBDT/td-p/1775025 MBDTを使用してプロジェクトを開発していて問題が発生した場合は、次回からはMBDTフォーラムで質問してください。ここはMBDTに関する質問に答えるための専用フォーラムです。
View full article
Kinetis (KW3x/4x, MCX W7x & MCX W23) Power Profile Tools for Automotive, IIoT, CGM & Localization This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47) and MCX Wx (MCX W71/72) One Connectivity Power Profiling Tool (experimental). It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery life time of your solution. This page content a dedicated power profile tool for 'One Connectivity Power Profiling Tool' which includes: New: KW43 (Automotive) and MCX W70 (IIoT) products in standalone based on simulation. KW3x/KW4x (Automotive) and MCX W7x (IIoT) products in standalone. MCX W23 (IIoT) product in standalone. MCX W71 & W72 product in standalone (IIoT). New: MCX W70 product in standalone (IIoT) based on simulation. Bluetooth LE 802.15.4 Matter & ZED id:NXP-Knowledge-Base [start:July 31 2026]
View full article
.exe通常のパッケージ形式ですか? こんにちは、 私は一部のマイクロコントローラファミリ向けのCAN/UARTブートローダーの開発者です。サポートするマイクロコントローラのラインナップを拡大し、一部のNXPデバイスのサポートを追加することが理にかなっているのかを考えたいです。これまでNXPのマイクロコントローラを使ったことはありません。 フォーラムやNXPのウェブサイトで「bootloader」という用語を検索すると、多くのWindows実行ファイルがダウンロードされているのが見つかり、少し驚きました。メインサイトの検索バーに「bootloader」という言葉を追加すると、2つ目のヒットは暗号通貨のウェブ側への直接リンクまで出てきます。 「Unified bootloader Demo」を見たい場合、本当にWindows PCが必要で、.exeファイルをダウンロードして実行する必要があるのでしょうか?ファイル? よろしくお願いいたします トルステン
View full article
i.MX8MQ:启动 ROM 是否支持从 FlexSPI/QSPI NOR 闪存启动? 你好, 硬件: - i.MX8MQ(REV A0),基于 EVK 设计的定制板 - QSPI 或非:Micron MT25QL256A(32MB,3.3V,四路连接) - 电路板支持包。Yocto Scarthgap、NXP 电路板支持包。、U-启动 2024.04 (u-启动-imx) 目标:从 FlexSPI 或非闪存启动启动加载程序(SPL + ATF + U-Boot)。 内核和根文件系统仍然保留在 eMMC 上。 有效的方法: - U-启动(通过 uuu SDP/SDPV 加载到 RAM 中)运行正常 - “sf probe”正确检测到闪存:mt25ql256a,32 MiB - U-启动 可以可靠地读取和写入闪存(已通过 “sf protect unlock”之后的回读测试验证) - 镜像版本使用了 IMXBOOT_TARGETS = "flash_evk_flexspi" 闪存布局(已通过读取芯片数据验证): 0x000000:FCFB 标头 - “qspihdr 检查”报告 “在 Q(F)SPI 中找到启动配置头” 标签 = 42464346,版本 = 56010000 0x001000: IVT - d1 00 20 41,入口 = 0x007E1000, boot_data = 0x007E0FE0,self = 0x007E0FC0 0x060000:U-Boot 正确的 FIT(d00dfeed),匹配 CONFIG_SYS_SPI_U_BOOT_OFFS=0x60000 问题: 启动开关设置为 QSPI/FlexSPI 启动,并使用 USB 电缆 物理断开连接后,板无法启动。什么都没有 打印在串口控制台上(SPL 横幅从未出现),并且 ROM 回退到串行下载模式: uuu -lsusb 2:1 MX8MQ SDP:0x1FC9 0x012B NXP 闪存 BT_FUSE_SEL 未熔断;启动配置通过 GPIO 完成。 启动引脚。 我已经尝试过: - 两种标头格式:scripts/qspi_header(c0ffee01 标签)和 scripts/fspi_header(FCFB 标签)。修复了 soc.mak,使其 flash_evk_flexspi 使用偏移量为 0 的 fspi_header。 - 改变 FCFB 参数:sflashA1Size、serialClkFreq(50MHz -> 20MHz), dataSetupTime/dataHoldTime,sflashPadType - "uuu -b qspi"(官方内置脚本) - "qspihdr update safe" 和 "qspihdr init safe" - 完全擦除闪存与写入完整图像: 启动行为基本相同(SDP 出现于之后)。 (约 1.6 秒 vs 约 1.8 秒),这表明 ROM 可能没有被读取。 完全不开闪光灯。 问题: 1.i.MX8MQ 启动 ROM 是否支持从串行 或非 卡启动 是否支持通过 FlexSPI 进行闪存刷新?我拥有的参考手册部分 列出了与非闪存和 SD/MMC 作为引导设备,但我无法 找到列出的 FlexSPI/QSPI 或非。i.MX8MM/8MN 文档似乎 可以描述一下,但我不太确定 8MQ。 2. 如果支持,预期的闪存布局具体是什么? 当 FCFB 为真时,IVT 应该位于偏移量 0x400 还是 0x1000? 位于 0x0 处? 3. 应选择正确的 BOOT_MODE / BOOT_CFG 组合。 i.MX8MQ 上采用 FlexSPI 或非 启动? 4. 关于 REV A0 硅片,是否存在任何已知的勘误? FlexSPI 启动? 谢谢!
View full article
How to Watch CCTV Overseas When You See "Unavailable in Your Region" Trying to watch CCTV or CCTV-5 from overseas but getting a message that says "This content is unavailable in your region"? You're not alone. Many overseas Chinese, international students, and travelers encounter regional restrictions when using CCTV apps or China Media Group (CMG) streaming platforms. The good news is that there are several ways to improve your access and continue watching your favorite programs. Why Does CCTV Show "Unavailable in Your Region"? CCTV broadcasts many TV channels, live events, sports competitions, news programs, documentaries, and variety shows. However, due to copyright agreements and broadcasting licenses, some content is available only to viewers connecting from mainland China. If you're accessing CCTV from another country, you may experience: "This content is unavailable in your region." Live channels that fail to load. Black screens or playback errors. Sports events that cannot be streamed. Buffering or unstable video quality. These issues are especially common when watching CCTV-5, major sporting events, and exclusive live broadcasts. How to Watch CCTV from Abroad If you're overseas, the following methods can help improve your viewing experience. 1. Use a China-Optimized Network A connection that routes your traffic through mainland China can help the platform recognize your network as a domestic connection, allowing access to more region-restricted content. Many overseas users choose SpeedX China accelerator because it provides optimized China routes with stable speeds for streaming live TV, sports, and on-demand programs. 2. Sign In to Your CCTV or CMG Account Logging into your account can synchronize your viewing history and preferences across different devices. 3. Update the App Regularly Keeping the CCTV or related streaming app up to date helps ensure better compatibility and reduces playback issues caused by outdated software. What Content Is Commonly Restricted? Depending on licensing policies, overseas viewers may have limited access to: CCTV-5 live sports Major football and basketball events TV dramas Variety shows Documentaries Special live broadcasts News content is often available globally, while entertainment and sports programming are more likely to be region-locked. Final Thoughts Regional restrictions can make it difficult to watch CCTV while living or traveling abroad. Fortunately, using a reliable China-optimized connection can greatly improve your ability to access live channels and on-demand content. Whether you're following breaking news, watching CCTV-5 sports, or enjoying Chinese TV programs, SpeedX(回国VPN工具) offers a stable solution for many overseas users looking for a smoother viewing experience. Student Project
View full article
如何在海外观看监控录像,即使看到“您所在地区无法观看”的提示? 想在海外观看中央电视台或中央电视台五台,却收到“您所在地区无法观看此内容” 的提示 ?您并非个例。许多海外华人、留学生和旅行者在使用中央电视台应用程序或中华媒体集团(CMG)流媒体平台时都会遇到地区限制。 好消息是,有几种方法可以改善您的访问体验,让您继续观看您喜爱的节目。 为什么监控录像显示“您所在地区无法观看”? 中央电视台播出众多电视频道、现场直播活动、体育赛事、新闻节目、纪录片和综艺节目。但是,由于版权协议和广播许可证的限制,部分内容仅供中国大陆观众观看。 如果您从其他国家/地区访问闭路电视监控系统,可能会遇到以下情况: “您所在的地区无法访问此内容。” 直播频道加载失败。 黑屏或播放错误。 无法进行直播的体育赛事。 视频缓冲或视频质量不稳定。 观看中央电视台5台、重大体育赛事和独家直播节目时,这些问题尤其常见。 如何从国外观看监控录像 如果您身在海外,以下方法可以帮助改善您的观看体验。 1. 使用针对中国市场优化的网络 通过中国大陆路由流量的连接可以帮助平台将您的网络识别为国内连接,从而允许您访问更多受地区限制的内容。 许多海外用户选择SpeedX 中国加速器,因为它提供优化的中国线路,速度稳定,可用于流畅观看直播电视、体育赛事和在线点播节目。 2. 登录您的闭路电视或 CMG 帐户 登录您的帐户即可在不同设备上同步您的观看历史记录和偏好设置。 3. 定期更新应用程序 保持监控录像或相关流媒体应用程序的更新有助于确保更好的兼容性,并减少因软件过时而导致的播放问题。 哪些内容通常会受到限制? 根据许可政策,海外观众可能无法观看以下内容: 中央电视台5台体育直播 重大足球和篮球赛事 电视剧 综艺节目 纪录片 特别现场直播 新闻内容通常面向全球,而娱乐和体育节目则更有可能受到地区限制。 总结与展望 地区限制可能会使在国外居住或旅行时难以观看监控录像。幸运的是,使用可靠的、针对中国网络优化的连接可以大大提高您访问直播频道和在线点播内容的能力。 无论您是关注突发新闻、观看中央电视台5台体育频道,还是欣赏中国电视节目, SpeedX(回国VPN工具)都能为众多寻求更流畅观看体验的海外用户提供稳定的解决方案。 学生项目
View full article
RW612 FLEXCOMM3/I2S3 支持驱动程序 我们使用 RW612 FLEXCOMM3/I2S3,并采用以下固定硬件布线: - GPIO24 = 来自 PCM6120 SDOUT 的 I2S 数据输入 - GPIO25 = I2S SCK 输出至 PCM6120 BCLK - GPIO26 = I2S WS 输出至 PCM6120 FSYNC 编解码器为 PCM6120,处于从属模式。 RW612 旨在作为 I2S 主设备,生成 BCLK/WS 并接收音频数据。 我们已核实的内容: - GPIO25/GPIO26 可以在普通 GPIO 模式下正确驱动 - FLEXCOMM3 时钟源为 12.288 MHz 的音频 PLL - 与 PCM6120 的 I2C 通信正常 PCM6120寄存器配置已接受 观察到的行为: 1. 配置为 I2S RX 且 kI2S_MasterSlaveNormalMaster 的 FLEXCOMM3 不会在 GPIO25/GPIO26 上生成任何 SCK/WS 边沿。 2. 将 FLEXCOMM3 配置为 I2S TX,并使用 kI2S_MasterSlaveNormalMaster 也无法工作:FIFOSTAT.TXNOTFULL=1,但在写入 FIFOWR 后 TXLVL 仍为 0,并且引脚上没有出现 SCK/WS 边沿。 3. PCM6120 报告缺少时钟(ASI_STS=0xFF,DEV_STS1=0x80)。 问题: 1.RW612 FLEXCOMM I2S RX 在正常主模式下是否会将 SCK/WS 驱动到外部引脚? 2. 对于“主时钟生成 + 从外部编解码器接收数据”的使用场景,是否支持单个 FLEXCOMM 实例,还是需要双 FLEXCOMM 架构(TX 主设备 + RX 从设备,带 I2S 桥接器)? 3.对于 FLEXCOMM3 I2S TX 主站,除了 I2S_TxInit()、FIFOWR 写入和 MAINENABLE 之外,接受 FIFO 写入是否还有其他先决条件? 4. 对于 I2S 时钟输出,FLEXCOMM3 在 GPIO24/25/26(AON 功能域)上是否存在任何已知的限制? 请帮忙解答这个话题 Re: RW612 FLEXCOMM3/I2S3 Supporting driver 嗨@duyhung ,希望你一切都好。 请问您进行测试时使用的是 FreeRTOS 还是 Zephyr?你使用的是FRDM-RW612板吗? 请同时提供您使用的版本(SDK 或 Zephyr),以及您是否以示例为基础进行开发。 此外,RW612(UM11865)参考手册第28.2节包含I2S外设的基本配置指南,请问您是否已按照这些一般步骤操作? Re: RW612 FLEXCOMM3/I2S3 Supporting driver 嗨@RomanVR , 感谢您的回复。详情如下。 1. 实时操作系统 我们正在使用 裸机和 FreeRTOS 均用于测试。这些测试中没有 Zephyr 参与。所有初始化和 I2S 配置均直接使用 NXP SDK 驱动程序完成。 2. 板 我们是 不是 使用 FRDM-RW612。我们正在使用一个 定制开发板 基于 RW612ETA2I。MCU相同,但板布局不同。 音频编解码器(PCM6120)通过线路连接到 FLEXCOMM3 / I2S3 在以下固定引脚上: GPIO 信号方向 I2S 数据(来自 PCM6120 的 SDOUT) GPIO24 输入 I2S SCK(BCLK 至 PCM6120) GPIO25 输出 I2S WS(FSYNC 到 PCM6120) GPIO26 输出 I2C SDA(PCM6120 配置) GPIO56 (FC14) 双向 I2C SCL(PCM6120 配置) GPIO57 (FC14) 双向 AUX_EN(PCM6120 电源) GPIO54 输出 3. SDK 版本 我们正在使用 SDK_2.x_RD-RW612-BGA,版本 25.03.00 。 4. 基本示例 我们使用了 rdrw612bga_i2s_dma_record_playback 作为参考示例。该示例使用 FLEXCOMM1(TX 主设备)+ FLEXCOMM0(RX 从设备)+ I2S 桥接器,我们已确认其工作正常。 然而,由于硬件限制,我们不得不使用一种 单路 FLEXCOMM(仅限 FC3) 整个 I2S 链路到 PCM6120。PCM6120 必须以从机模式工作,因为我们没有外部时钟源作为 BCLK。我们尝试将 FC3 配置为 kI2S_主从正常主 使其在接收数据时生成 SCK/WS。 5. UM11865 第 28.2 节 – I2S 配置步骤 我们已审阅 UM11865 第 28.2 节,并确认所有 6 种配置均正确无误。 步骤如下: 步骤 1:启用 Flexcomm,使用 CLOCK_EnableClock + RESET + CLOCK_AttachClk 步骤 2:FIFO 配置(FIFOCFG=0x35,ENABLETX=1,SIZE=8) 步骤 3:通过 IO_MUX_SetPinMux(IO_MUX_FC3_I2S) 设置 I2S 引脚,启用 AON MCI_IOMUX 步骤 4:速率配置(CFG1 MSTSLVCFG=0b11=NormalMaster,DIV=3 → BCLK=3.072MHz) 步骤 6:在 FIFOCFG 中启用 DMA 尽管我们已遵循所有步骤,但仍观察到以下情况: - GPIO25/GPIO26 上没有 SCK/WS 边沿 - TX FIFO 不接受数据:TXNOTFULL=1,但 FIFOWR 写入后 TXLVL 仍为 0 第 28.2 节步骤 4 指出:“对于控制器操作,时钟决定 I2S 速率”,但没有具体说明 PERSEL=I2S_RECEIVE 是否与 NormalMaster 预计会将 SCK/WS 驱动到焊盘上。 请您澄清一下: 1.PERSEL=I2S_RECEIVE (0b101) 是否能够驱动 SCK/WS 作为输出 当 MSTSLVCFG=NormalMaster 时? 2. 为什么在使用 PERSEL=I2S_TRANSMIT 向 FIFOWR 写入数据后,TXLVL 仍然为 0? FIFOWR 写入操作是否需要先启用 MAINENABLE 权限? 6. 观察到的问题——我们的具体问题 完成以上所有配置后, GPIO25 和 GPIO26 产生零边沿。PCM6120 报告缺少时钟信号(ASI_STS = 0xFF, DEV_STS1 = 0x80)。 我们进一步运行了诊断程序:我们将 FC3 配置为 I2S TX 主控端 (而不是 RX 主控端)并发现 写入 FIFOWR 不会递增 TXLVL — FIFOSTAT 保持不变 0x30 无论我们写多少个字,(TXNOTFULL=1,TXLVL=0)。 TX 主探测后的相关寄存器状态:   CFG1 = 0x17003C(MSTSLVCFG=3 = NormalMaster,DATALEN=24,MAINENABLE=0) 分频比 = 3(分频器=4,BCLK = 12.288MHz / 4 = 3.072MHz) FIFOCFG = 0x35 (ENABLETX=1, TXI2SE0=1) FIFOSTAT = 0x30(写入后 TXNOTFULL=1,TXLVL=0) MAINENABLE=1 之后: STAT = 0x5(BUSY=1,LR=1 — 内部时钟逻辑运行) GPIO25/GPIO26 上的 SCK/WS 边沿:0 我们向恩智浦提出的具体问题: 当 FLEXCOMM3 I2S 配置为 kI2S_主从正常主 (无论是 TX 还是 RX),RW612 上的 SCK/WS 是否是预期行为? 不是 即使 STAT 显示外设内部正在运行,驱动信号仍然会输出到 GPIO25/GPIO26(AON 功能域)? 或者:采用单FLEXCOMM拓扑结构(一个飞控同时作为时钟主控和RX数据接收器)。 有 对于这种使用场景,RW612 I2S 硬件是否必须支持两个独立的 FlexComm 实例(一个 TX 主站 + 一个 RX 从站,通过 I2S 桥接器)? 谢谢! Re: RW612 FLEXCOMM3/I2S3 Supporting driver 嗨@duyhung ,感谢您提供更多关于您设置的详细信息。 根据参考手册(RM00278),当 I2S 实例配置为正常主模式时,SCK 和 WS 信号配置为生成,但不发送或接收数据,如RM00278的CFG1[MSTSLVCFG]寄存器中的31.1.2 节所述。在 I2S 驱动程序中,此配置应用于“ I2S_TxInit(); ”函数中,该函数还将正在使用的 Flexcomm 实例和 FIFO 配置为发射器实例。 根据前面的信息,建议采用共享信号的双 Flexcomm 拓扑结构(就像您已经测试过的示例一样),正如UM11865的3.6.2.1.1 节中的图 9所示的类似示例所演示的那样。 此外,如果您以 I2S with DMA 回放示例为基础,能否请您分享一下您对该示例所做的修改?
View full article
S32K3 spi clk 异常低 我使用 S32K344 EVB 进行 SPI 测试。我使用 LPSPI1 单元作为主控端,引脚从 PTB14 到 PTB17,以及 RTD 4.0.0。P19.SPI 模式为 3:CPOL=1,CPHA=1 调用 Spi_SyncTransmit 后,我按照如下方式测量示波器,时钟引脚在帧真正传输之前变为低电平,这是什么原因造成的?如何解决这个问题? Re: S32K3 spi clk abnormal low 嗨@zyt 这种行为通常是由 ERR050456 的第一个解决方法引起的,该解决方法会对 LPSPI 模块执行 RESET。这种情况已经在其他帖子中讨论过了,例如[MCU S32K312] 上 CS 线变低之前出现额外的 SPI 时钟脉冲。 正如该帖子中所解释的,可以采用另一种变通方法,预计可以消除低脉冲。要启用此变通方法,请在项目中定义以下宏: ERR_IPV_LPSPIV2_E050456_2ND_SOLUTION BR,VaneB
View full article
S32K3 DMA logic link channel Hello, How should I use the DMA logic link channel function (major loop or minor loop)? I use channel 0 to link to channel 1. Why does channel 0 complete the transport and cause an interruption, but channel 1 does not transport any data. Attached is my test project BR Jason 回复: S32K3 DMA logic link channel This configuration needs to be checked
View full article
i.MX8MP Heat Spreader Solution We are considering the following passive thermal solution for our i.MX 8M Plus–based infotainment application: Aluminum heat spreader: 20 × 20 × 1.5 mm (up to 30 × 30 × 2 mm) TIM: Henkel Bergquist Gap Filler TGF 2000 The aluminum plate will be used as a heat spreader on top of the i.MX 8M Plus. Would this solution be sufficient for a typical infotainment workload? If not, could you recommend the appropriate heat-spreader size or any additional thermal requirements? Re: i.MX8MP Heat Spreader Solution Hi @Wobaffet, Thank you for contacting NXP Support! For this purpose, I recommend reviewing the i.MX8MP Hardware Design Guide, specifically Chapter 7.8, "Heat Sink Considerations", which provides detailed information and design recommendations for thermal management and heat sink implementation on the i.MX8MP. This chapter covers the key requirements and considerations needed to ensure proper thermal performance and reliable operation of the device. Best regards, Chavira
View full article
BLEと従来のBluetoothを統合してデュアルモード動作を実現する方法 チームの皆さん、こんにちは。 私は以下を使用しています: MCU:i.MX RT1176 EVKB WiFi/Bluetoothモジュール:村田IW416 BLEのwireless_uart_cm7サービスを アプリケーションhandsfree_ag_cm7、アプリケーションが両方をサポートするようにします: - Bluetooth Classic (HFP AG) - BLE GATT(ワイヤレスUART) BT_features.h では、私は以下の点に気づきました。 #ifndef CFG_CLASSIC #define BT_LE #endif CFG_CLASSICはプロジェクトプリプロセッサで定義されているため、BT_LEは決して 定義済み。 デュアルモード(クラシック+BLE)を作るのに推奨される方法は何ですか? EdgeFast Bluetoothスタックを使っているアプリケーションについて? CFG_CLASSICを削除すべきでしょうか、それとも別のプロジェクト構成があるのでしょうか それともデュアルモードアプリケーション向けのビルドオプションですか? マージの方法を示す例やアプリケーションノートはありますか? wireless_uart_cm7 handsfree_ag_cm7? MCXA Re: How to integrate the BLE and Classic Bluetooth for dual-mode operation @Karthick_KL様、 統合の方向性は正しいです。HFP AGが主なアプリケーションであるため、「handsfree_ag_cm7」はベースプロジェクトとして残され、BLEワイヤレスUART GATTサービスもこのプロジェクトに追加されるべきです。 `CFG_CLASSIC`はBluetooth Classic HFP AGプロファイルで必要とされるため、削除しないでください。この問題は、おそらくサンプルプロジェクトの機能選択ロジック(`BT_features.h`内)に起因していると考えられます。 #ifndef CFG_CLASSIC #define BT_LE #endif このロジックにより、`BT_LE`は非クラシックのサンプルプロジェクトでのみ有効になります。単一機能SDKの例には適していますが、カスタムデュアルモードアプリケーションには十分ではありません。 デュアルモードアプリケーションの場合、プロジェクトはClassic/HFP AG構成を有効にし、BLEホスト/GATT構成も明示的に有効化すべきです。つまり、デュアルモードプロジェクトでは、クラシックパスとLEパスの両方を構築する必要があります。 一つの方向性としては、プロジェクトレベルのデュアルモードやBLEマクロ(例えば「CFG_BLE」や「CFG_DUAL_MODE」)を導入し、機能選択を更新して「CFG_CLASSIC」が定義されていても「BT_LE」を有効化できるようにすることです。例えば: #if defined(CFG_BLE) || defined(CFG_DUAL_MODE) || !defined(CFG_CLASSIC) #define BT_LE #endif その後、ワイヤレスUART BLEサービス、広告データ、GATTコールバック、BLE接続処理のみを「handsfree_ag_cm7」アプリケーションに統合します。Bluetoothスタックの初期化は単一インスタンスのままにしておく必要があり、HFP AG Classicパスも変更してはならない。 「handsfree_ag_cm7」と「wireless_uart_cm7」を直接統合した、すぐに使える公開SDKの例やアプリケーションノートは知られていません。公開されている例では「handsfree_ag」と「wireless_uart」を別々に示しているため、これはカスタムデュアルモードアプリケーション統合として扱うべきです。 よろしくお願いします! よろしくお願いいたします。 維東 Hi , Thank you for your reply to my previous post. Follow... こんにちは@weidong_sunさん 前回の投稿へのご返信ありがとうございました。 ご提案いただいた通り、BT_features.h のマクロを修正して、BLE と Bluetooth Classic の両方を統合しました。 #if defined(CFG_BLE) || defined(CFG_DUAL_MODE) || !defined(CFG_CLASSIC) #define BT_LE #endif そして、クラシック版とBLE版の両方のスタックを追加しました。今は正常に動作しています。 evkbmimxrt1170_wifi_wpa_supplicant_cm7例を使って、BT/BLEアプリケーションにWi-Fiを統合しました。 Wi-FiはWi-Fi Direct(P2P)接続を確立するために使われ、オーディオはHFPインターフェースを通じてストリーミングされます。 しかし、オーディオストリーミング中にWi-Fi直接続の問題に直面しています。 事前にWi-Fi Direct接続を確立した場合 HFPオーディオストリーミングを開始し、接続は成功しました。 しかし、HFPのオーディオがストリーミングされている間にWi-Fi Direct接続を確立しようとすると、Wi-Fi Direct接続が失敗します。 端末出力は以下のとおりです。 p2p_connectまずは大丈夫です! P2P-GO-NEG-SUCCESS role=client freq=5240 ht40=0 peer_dev=72:1a:2e:a3:f8:17 peer_iface=72:1a:2e:a3:f8:17 wps_method=PBC WF3:WPS-PBC-アクティブ wf3: SME: 72:1a:2e:a3:f8:17で認証しようとしています (SSID='DIRECT-69-Realme Narzo N55' 周波数=5240 MHz) wf3:72:1a:2e:a3:f8:17(SSID='DIRECT-69-Realme Narzo N55' 周波数=5240 MHz)と関連付けようとしています。 wf3:72:1a:2e:a3:f8:17に関連する wf3: CTRL-EVENT-SUBNET-STATUS-UPDATE STATUS=0 wf3: CTRL-EVENT-EAP-STARTED EAP認証開始 wf3: CTRL-EVENT-EAP-PROPOSED-METHOD vendor=14122 method=1 wf3: CTRL-EVENT-EAP-METHOD EAP VENDOR 14122 方法 1 (WSC) SELECTED P2P-グループ形成-失敗 wf3: CTRL-EVENT-DISCONNECTED bssid=72:1a:2e:a3:f8:17 reason=3 locally_generated=1 WF3: CTRL-EVENT-DSCP-POLICY clear_all P2P-GROUP-REMOVED wf3 client reason=FORMATION_FAILED この 共存問題 を完全に解決せずに解決する方法があるのか知りたいです Bluetoothの無効化 それとも、この問題に対処するために他に設定が必要なことはありますか? ご回答をお待ちしています。   Re: Hi , Thank you for your reply to my previous post. Follow... @Karthick_KL様、 詳細な情報を提供していただきありがとうございます。 あなたが説明した挙動からすると、これはBluetooth ClassicとBLEの統合問題というより、Wi-FiとBluetoothの共存ポリシーに関連しているようです。 共存アルゴリズムでは、HFPオーディオ(SCO/eSCO)トラフィックに音声品質を維持するために非常に高い優先度が割り当てられています。その結果、HFP音声ストリーミングがすでにアクティブな状態でWi-Fi Direct(P2P)接続の試みが開始されると、認証/WPSフェーズ中にP2Pグループ形成手順が失敗する可能性があります。 この観察結果は、あなたのテスト結果と一致しています。 P2P接続 --> HFPオーディオストリーミング:OK HFP音声ストリーミング --> P2P接続:失敗する可能性   したがって、推奨される手順はまずWi-Fi Direct(P2P)接続を確立し、その後HFPのオーディオ接続/ストリーミングを開始することです。 現在のログに基づき、アクティブHFP音声ストリーミング中の認証やグループ形成の失敗は、Bluetoothスタックの問題ではなく、予想される共存挙動です。 よろしくお願いします! よろしくお願いいたします。 維東 Re: Hi , Thank you for your reply to my previous post. Follow... こんにちは @weidong_sun 詳しい説明とサポートをありがとうございます。とても助かりました。
View full article
S32K3 DMAロジックリンクチャネル こんにちは、 DMAのロジックリンクチャネル機能(メジャーループかマイナーループか)はどのように使えばよいでしょうか?チャネル0を使ってチャネル1に接続しています。なぜチャネル0はトランスポートを完了して中断を引き起こすのに、チャネル1はデータを一切転送しないのでしょうか。 テストプロジェクトを添付します。 BR ジェイソン 回复: S32K3 DMA logic link channel この設定を確認する必要があります
View full article
i.MX8MP ヒートスプレッダーソリューション 私たちは i.MX 8M Plusベースのインフォテインメント用途に、以下のパッシブサーマルソリューションを検討しています。 アルミ製ヒートスプレッダー:20×20×1.5mm(最大30×30×2mm) TIM:ヘンケル・ベルクヴィスト ギャップフィラー TGF 2000 アルミ板は、i.MX 8M Plusの上部に設置する放熱板として使用されます。 このソリューションは、一般的なインフォテインメントシステムのワークロードに対して十分でしょうか?もしなければ、適切なヒートスプレッダーのサイズや追加の熱要件を教えてもらえますか? Re: i.MX8MP Heat Spreader Solution こんにちは、@Wobaffet。 NXPサポートにご連絡いただきありがとうございます! この目的のために、 i.MX8MPハードウェアデザインガイド、 特に第7.8章「ヒートシンクの考慮事項」をよく確認することをお勧めします。そこにはi.MX8MPの熱マネジメントやヒートシンク実装に関する詳細な情報とデザイン推奨が載っています。 本章では、デバイスの適切な熱性能と信頼性の高い動作を確保するために必要な主要な要件と考慮事項について説明します。 よろしくお願いします、 チャビラ
View full article
Kinetis(KW3x/4x、MCX W7x 和 MCX W23)汽车、工业物联网、CGM 和定位电源我的工具 本页面是 Kinetis (KW35/KW38/KW45/KW47) 和 MCX Wx (MCX W71/72) One 连接电源分析工具的专用页面(实验性)。 它将帮助您估算应用(汽车或工业物联网)中的功耗,并评估解决方案的电池寿命。 本页面包含一个专用的电源配置文件工具,名为“One 连接 Power 我的 Tool”,其中包括: 新增:基于仿真的独立组网 \(SA\)产品 KW43(汽车)和 MCX W70(工业物联网)。 KW3x/KW4x(汽车)和 MCX W7x(工业物联网)产品均为独立组网 (SA)。 MCX W23(工业物联网)产品独立组网 (SA)。 MCX W71 & W72 产品独立组网 (SA)(工业物联网)。 新增:基于仿真的独立组网 (SA)(工业物联网)MCX W70 产品。 BLE 802.15.4 物质与ZED id:NXP知识库 [开始日期:2026年7月31日]
View full article
How to integrate the BLE and Classic Bluetooth for dual-mode operation Hi Team, I am using: MCU: i.MX RT1176 EVKB WiFi/Bluetooth module: Murata IW416 I want to add the BLE wireless_uart_cm7 service into the handsfree_ag_cm7 application so that the application supports both: - Bluetooth Classic (HFP AG) - BLE GATT (Wireless UART) In BT_features.h, I noticed that: #ifndef CFG_CLASSIC #define BT_LE #endif Since CFG_CLASSIC is defined in the project preprocessor, BT_LE is never defined. What is the recommended method to build a dual-mode (Classic + BLE) application using the EdgeFast Bluetooth stack? Should CFG_CLASSIC be removed, or is there another project configuration or build option intended for dual-mode applications? Is there any examples or application notes demonstrating how to merge handsfree_ag_cm7 with wireless_uart_cm7? MCXA Re: How to integrate the BLE and Classic Bluetooth for dual-mode operation Dear @Karthick_KL , Your integration direction is correct. Since HFP AG is the main application, `handsfree_ag_cm7` should remain the base project, and the BLE Wireless UART GATT service should be added into this project. `CFG_CLASSIC` should not be removed, because it is required by the Bluetooth Classic HFP AG profile. The issue is more likely caused by the sample project feature selection logic in `BT_features.h`: #ifndef CFG_CLASSIC #define BT_LE #endif This logic makes `BT_LE` enabled only for non-Classic example projects. It is suitable for single-feature SDK examples, but it is not sufficient for a custom dual-mode application. For a dual-mode application, the project should keep the Classic/HFP AG configuration enabled and explicitly enable the BLE host/GATT configuration as well. In other words, the dual-mode project should build both the Classic path and the LE path. A possible direction is to introduce a project-level dual-mode or BLE macro, for example `CFG_BLE` or `CFG_DUAL_MODE`, and update the feature selection so that `BT_LE` can be enabled even when `CFG_CLASSIC` is also defined. For example: #if defined(CFG_BLE) || defined(CFG_DUAL_MODE) || !defined(CFG_CLASSIC) #define BT_LE #endif Then merge only the Wireless UART BLE service, advertising data, GATT callbacks, and BLE connection handling into the `handsfree_ag_cm7` application. The Bluetooth stack initialization should remain single-instance, and the HFP AG Classic path should remain unchanged. We are not aware of a ready-to-use public SDK example or application note that directly merges `handsfree_ag_cm7` with `wireless_uart_cm7`. The available public examples demonstrate `handsfree_ag` and `wireless_uart` separately, so this should be treated as a custom dual-mode application integration. Thanks! Regards, Weidong Hi , Thank you for your reply to my previous post. Follow... Hi @weidong_sun, Thank you for your reply to my previous post. Following your suggestion, I integrated both BLE and Bluetooth Classic by modifying the macro in BT_features.h #if defined(CFG_BLE) || defined(CFG_DUAL_MODE) || !defined(CFG_CLASSIC) #define BT_LE #endif And I have added the stack for both classic and ble. Now it is working correctly. I have now integrated Wi-Fi with the BT/BLE application using the evkbmimxrt1170_wifi_wpa_supplicant_cm7 example. The Wi-Fi is used to establish a Wi-Fi Direct (P2P) connection, while audio is streamed over the HFP interface. However, I am facing an issue with Wi-Fi Direct connection during audio streaming. If I establish the Wi-Fi Direct connection before starting HFP audio streaming, the connection is successful. But if I attempt to establish the Wi-Fi Direct connection while HFP audio is streaming, the Wi-Fi Direct connection fails. The terminal output is shown below: p2p_connect start ok! P2P-GO-NEG-SUCCESS role=client freq=5240 ht40=0 peer_dev=72:1a:2e:a3:f8:17 peer_iface=72:1a:2e:a3:f8:17 wps_method=PBC wf3: WPS-PBC-ACTIVE wf3: SME: Trying to authenticate with 72:1a:2e:a3:f8:17 (SSID='DIRECT-69-Realme Narzo N55' freq=5240 MHz) wf3: Trying to associate with 72:1a:2e:a3:f8:17 (SSID='DIRECT-69-Realme Narzo N55' freq=5240 MHz) wf3: Associated with 72:1a:2e:a3:f8:17 wf3: CTRL-EVENT-SUBNET-STATUS-UPDATE status=0 wf3: CTRL-EVENT-EAP-STARTED EAP authentication started wf3: CTRL-EVENT-EAP-PROPOSED-METHOD vendor=14122 method=1 wf3: CTRL-EVENT-EAP-METHOD EAP vendor 14122 method 1 (WSC) selected P2P-GROUP-FORMATION-FAILURE wf3: CTRL-EVENT-DISCONNECTED bssid=72:1a:2e:a3:f8:17 reason=3 locally_generated=1 wf3: CTRL-EVENT-DSCP-POLICY clear_all P2P-GROUP-REMOVED wf3 client reason=FORMATION_FAILED I would like to know if there is a way to resolve this coexistence issue without completely disabling Bluetooth or is there any other configuration I need to do to handle this issue? Thank you!   Re: Hi , Thank you for your reply to my previous post. Follow... Dear @Karthick_KL , Thank you for the detailed information. Based on the behavior you described, this appears to be related to the Wi-Fi/Bluetooth coexistence policy rather than a Bluetooth Classic/BLE integration issue. In the coexistence algorithm, HFP audio (SCO/eSCO) traffic is assigned a very high priority to maintain voice quality. As a result, if a Wi-Fi Direct (P2P) connection attempt is initiated while HFP audio streaming is already active, the P2P group formation procedure may fail during the authentication/WPS phase. This observation is consistent with your test results: P2P Connection --> HFP Audio Streaming : OK HFP Audio Streaming --> P2P Connection : May Fail   Therefore, the recommended sequence is to establish the Wi-Fi Direct (P2P) connection first and then start the HFP audio connection/streaming. Based on the current logs, the observed authentication/group formation failure during active HFP audio streaming is an expected coexistence behavior rather than a Bluetooth stack issue. Thanks! Regards, Weidong Re: Hi , Thank you for your reply to my previous post. Follow... Hello @weidong_sun Thank you for your detailed explanation and support. It was very helpful.
View full article