2401024_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2401024_en-US

2401024_en-US

FRDM-MX95 PRO software packages?

I was wondering what OS software packages will be available for the MX95 PRO?  Will Android AAOS be available for it as a demo image?  Is there anyone we can communicate with about what will specifically be available?

Re: FRDM-MX95 PRO software packages?

currently, only linux 6.18.20_2.0.0 demo images for imx95 frdm pro

Embedded Linux for i.MX Applications Processors | NXP Semiconductors

you can download demo images from the link above, for android, I checked the board file, the latest android 16.0.0_2.0.0 is based on kernel 6.18.20_2.0.0, so should support frdm pro, but this version android hasn't verified on this board yet, only 19x19 evk and 15x15 frdm

joanxie_0-1785570929815.pngjoanxie_0-1785570929815.png


Re: FRDM-MX95 PRO software packages?

Any news if we will get android automotive on the frdm-mx95 or would we have to upgrade to frdm-mx95 pro version?

Re: FRDM-MX95 PRO software packages?

let me confirm auto android team again, the owner is on vacation, and come back office in next week, any update I will let you know it

Re: FRDM-MX95 PRO software packages?

refer to the link as below

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/android-automotive...

auto android demo images are only for imx95 19x19 evk

Re: FRDM-MX95 PRO software packages?

Are there any plans for android or AAOS?  Seems weird that the FRDM MX95 Pro wouldn't have an AAOS version especially since the Evaluation board 19x19 has been discontinued and benched.  Is there a reason the pro being a 19x19 processor wouldn't work as the evaluation board.

Re: FRDM-MX95 PRO software packages?Thanks. There seems to be a genuine lack of Android automotive support. The frdm has a lot of potential but without additional support from nxp we are left on our own. From my understanding the evk has been dropped from support from toradex and discontinued. With the frdm pro having the same hardware there should be some support. We need the BSP which would make building the images a lot easier.Re: FRDM-MX95 PRO software packages?

Is there any way i can contact them to ask a question?

Or could they give us some instructions on how to compile the new frdm pro board, maybe they can provide the board package file to make it easier for us to compile?

Re: FRDM-MX95 PRO software packages?

unfortunately, got information from auto android team that they haven't any plan to support any imx95 frdm board

Re: FRDM-MX95 PRO software packages?

since they don't have plan to support this yet, I don't think they can offer any packages to build

Tags (1)
No ratings
Version history
Last update:
‎08-11-2026 02:40 AM
Updated by: