Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
S32 Design Studio: Add UART to the Imported Project using AI Introduction In Tutorial 1, the AI agent imported the GPIO Blinking LED Demo and ran it on the FRDM-A-S32K312 board. This second article extends that project with two new features: a multi-color LED sequence, and a UART output that reports what the board is doing.   Using S32 Configuration Tools, you will map LPUART6 pins (PTA15 / PTA16), configure the peripheral at 115200 baud, regenerate code, and flash the firmware so the board echoes the current LED color over UART to a serial terminal.  Estimated time: ~20 minutes. System Architecture   Add UART to the Imported Project – system architecture overview   The components involved are:   FRDM-A-S32K312 – Target evaluation board. Runs GPIO Blinking LED firmware with LPUART6 enabled on PTA15 (RX) / PTA16 (TX). Transmits the current LED color over UART at 115200 baud. Host PC – Runs S32 Design Studio and the S32 Design Studio AI Support. A serial terminal (e.g. VS Code Serial Monitor) receives and displays the LED colour echo at 115200 / 8N1. Prerequisites   What you need before starting   Tutorial 1 completed — the GPIO Blinking LED Demo for FRDM-A-S32K312 must already be imported and building in S32 Design Studio One FRDM-A-S32K312 evaluation board + USB cable A serial terminal application (e.g. PuTTY, Tera Term, or VS Code Serial Monitor) S32 Design Studio AI Support configured (download, install and configure it following the steps from Installation & Usage Guide)   Note: This tutorial uses these paths: Installation: C:\NXP\2026\K3_kit\S32DS_3.6.8 Workspace: C:\NXP\2026\K3_kit\workspace_S32DS_3.6.8_K3_kit You can use any location. If you do, update the paths in the prompt to match. Connect the FRDM-A-S32K312 board to the PC via USB. Open Device Manager → Ports and note the virtual COM port number – you will need it for the serial terminal. Steps   Send the following prompts to your AI assistant in order. Each prompt is a complete, self-contained instruction.   Step 1 – Add RGB LED cycling (red → green → blue) In S32DS, use the dm-gpio-blinky-s32k312 project on a S32K312 FRDM board. Add pins PTA30 and PTA31 in the Pins tool (green and blue of the on-board RGB LED; red is the existing PTA29). In the existing blink cycle where the red LED is toggled, replace it with a switch-case that lights one color at a time, cycling red -> green -> blue, ~500 ms each. Important: these RGB LEDs are active-low. Confirm the polarity from the board schematic/user guide before writing GPIO values. Map: red=PTA29, green=PTA30, blue=PTA31. Then generate code and build (report any errors) and flash/run it. Use the s32ds-agentic-ai MCP server for all IDE/config/flash actions; if the MCP server disconnects at any point, stop immediately and notify me. AI will:   Open Pins Tool and add PTA30 (green) and PTA31 (blue) alongside existing PTA29 (red) Replace the existing blink loop with a switch-case cycling red → green → blue, ~500 ms each Respect active-low polarity, confirmed from board schematic/user guide Click Generate Code, build and report any errors Flash and run the firmware on the FRDM-A-S32K312 board Stop and notify the user immediately if the s32ds-agentic-ai server disconnects   Step 2 – Add UART functionality to echo the LED colour Add UART functionality to echo the color of the LED (RED, GREEN, BLUE) but keep it lightweight by using the LPUART IP-layer: - In Pins tool: map the PTA15 as LPUART6_RX and PTA16 as LPUART6_TX pins - In Peripherals tool: set LPUART_6 channel configured for baudrate 115200 / 8 data bits / no parity / 1 stop bit Then generate code and build (report any errors) and flash/run it. Use the s32ds-agentic-ai MCP server; if the MCP server disconnects at any point, stop immediately and notify me. AI will:   Open Pins Tool and map PTA15 → LPUART6_RX and PTA16 → LPUART6_TX Open Peripherals Tool and configure LPUART6: 115200 baud / 8 data bits / no parity / 1 stop bit Click Generate Code, build and report any errors Flash and run the firmware on the FRDM-A-S32K312 board Stop and notify the user immediately if the s32ds-agentic-ai server disconnects Verifying the Result   Work through this final check to confirm that both prompts completed successfully.   Final check Build completes with zero errors. Firmware is flashed and running on the FRDM-A-S32K312 board (RGB LED is blinking). Open a serial terminal at 115200 baud / 8N1 on the board's COM port. Confirm messages such as LED: RED, LED: GREEN, LED: BLUE appear in sync with the physical LED colour changes. Troubleshooting   Symptom Fix No UART output in serial terminal Open Pins Tool. Confirm PTA15 → LPUART6_RX and PTA16 → LPUART6_TX are routed. Regenerate code after any change. LPUART6 not found or not initialised Open Peripherals Tool. Verify LPUART6 is enabled and configured: 115200 baud / 8 data bits / no parity / 1 stop bit. Regenerate code if you make changes. LPUART6 absent at runtime Open Peripherals Tool › McuPartition. Enable LPUART6 in the partition configuration, then regenerate and rebuild. Garbled characters in serial terminal Baud rate mismatch. Confirm the terminal is set to 115200 and the peripheral configuration matches. Regenerate code after any baud rate change. Build errors after Generate Code Check that the generated LPUART6_init() call is present in main.c and that the correct header is included. Re-run Generate Code if source files are missing. LED colour not echoed over UART Confirm the UART transmit call is placed after each LED colour change in the main loop. Verify LPUART6_init() is called before the loop starts. Wrong COM port in serial terminal Open Device Manager → Ports and identify the virtual COM port assigned to the FRDM-A-S32K312 board. Use that port number in your terminal application. s32ds-agentic-ai server disconnects during operation Stop immediately and restart the MCP server following the setup instructions. Do not continue until the server is confirmed connected. File Reference   File Step Description src/main.c 2 Main firmware file — contains LED loop and LPUART6 transmit calls generate/src/Lpuart_Uart_Ip_PBcfg.c 1 Generated LPUART6 peripheral configuration generate/include/Lpuart_Uart_Ip_Cfg.h 1 Generated LPUART6 configuration header *.mex 1 S32 Configuration Tools project file (Pins, Clocks, Peripherals)   Map the pins, configure LPUART6 and regenerate – your board now reports every LED colour change over UART in about 20 minutes. Examples
View full article
S32 Design Studio: Add FreeMASTER Lite Configuration to Existing UART Project using AI Introduction In Tutorial 2, the application was extended to cycle the FRDM-A-S32K312 board's RGB LED through red, green, and blue, while sending corresponding status messages to a serial terminal. This third article shows how to add a FreeMASTER Lite server configuration using S32 Design Studio AI Support to an existing UART project on the FRDM-A-S32K312 board and create a browser dashboard that displays the current LED color – replacing the plain UART color echo.   Estimated time: ~20 minutes. System Architecture Add FreeMASTER to existing UART project – system architecture overview   The components involved are:   FRDM-A-S32K312 – Target evaluation board. Runs the existing UART project extended with FreeMASTER TSA, streaming the LED colour variable to the host over USB at 115200 baud. Host PC – Runs FreeMASTER Lite (fmlite.exe) on the board's COM port, 115200 baud, port 8090. Serves the LED colour dashboard to the browser. Prerequisites   What you need before starting   Tutorial 2 completed — the GPIO Blinking LED Demo with UART must already be imported and building in S32 Design Studio One FRDM-A-S32K312 evaluation board + USB cable Download and install FreeMASTER Lite (fmlite.exe) from LINK  Any modern browser (Chrome / Edge / Firefox) S32 Design Studio AI Support configured in your agent (download, install and configure it following the instruction from Installation & Usage Guide)    Note: This tutorial uses these paths: S32 Design Studio Installation: C:\NXP\2026\K3_kit\S32DS_3.6.8 Workspace: C:\NXP\2026\K3_kit\workspace_S32DS_3.6.8_K3_kit FreeMASTER Installation: C:\NXP\2026\K3_kit\FM_32 You can use any location. If you do, update the paths in the prompt to match. Connect the FRDM-A-S32K312 board to the PC via USB, open Device Manager → Ports (COM & LPT) and note the virtual COM port number. You must know this port before sending the prompt below — replace every COM# in the prompt with your own port (for example COM7), otherwise FreeMASTER Lite cannot open the serial connection to the board. Steps   Send the following prompt to your AI assistant. It is a complete, self-contained instruction. Replace COM# with the COM port of your board before sending.   Step 1 – Create FreeMaster Lite dashboard and server configuration Using FreeMaster Lite create a self contained web dashboard and the server configuration file in the project folder called dashboard. FreeMaster Lite is installed at c:\NXP\2026\K3_kit\FM_32\FreeMASTER Lite\fmlite.exe The dashboard should have a volatile variable that will be used to reflect the color of the RGB LED At the top should have the controls for the board serial connection, default: connection name "S32K312 RGB Board", COM#, 115200 baud, 8 data bits, no parity, 1 stop bit The board is connected on COM# - use this serial port for the FreeMaster Lite connection The project is a plain GPIO demo with no FreeMASTER driver - add whatever is needed on the target side so it can talk to FreeMaster Lite, then build and flash it in S32DS and confirm the color actually changes from the dashboard. Start FreeMaster server and run the dashboard at the end Use the s32ds-agentic-ai MCP server; if the MCP server disconnects at any point, stop immediately and notify user. AI will:   Create a self-contained web dashboard in the dashboard project folder Create a FreeMASTER Lite server configuration file in the same folder Add a volatile variable to reflect the RGB LED colour in the dashboard Add serial connection controls at the top (name: S32K312 RGB Board, COM#, 115200 baud, 8N1) Start the FreeMASTER Lite server and open the dashboard in the browser Stop and notify the user immediately if the s32ds-agentic-ai server disconnects Verifying the Result   Work through this final check to confirm that the prompt completed successfully.   Final check FreeMASTER Lite server is running with no errors. Open http://localhost:8090 in your browser. The LED colour dashboard loads and shows the current LED colour within ~5 seconds. The displayed colour changes in sync with the physical LED on the board. Troubleshooting   Symptom Fix ReadTSA returns count=0 TSA not enabled (FMSTR_USE_TSA 1) or FMSTR_Poll() missing. StartComm times out Wrong COM port in .fmcfg, baud mismatch, or board not powered. fmlite.exe exits immediately Activation code not entered, or path has spaces — wrap in quotes. LPUART0 baud rate wrong or peripheral not running Open Peripherals Tool. Verify LPUART0 is enabled and its clock source is set to AIPS_PLAT_CLK. Regenerate code if you change anything. LPUART0 absent at runtime Open Peripherals Tool › McuPartition. Enable LPUART0 in the partition configuration, then regenerate. FreeMASTER host times out or drops connection FMSTR_Poll() must be called frequently — place it in the main loop or a fast periodic task. The host requires low-latency responses. LPUART6 interrupts conflict with FreeMASTER Open Peripherals Tool (Platform). Disable LPUART6 interrupts — FreeMASTER operates in polling mode and does not use interrupt-driven UART. File Reference     File Step Description dashboard/led_color.html 1 LED colour dashboard dashboard/board_115200.fmcfg 1 FreeMASTER Lite server configuration src/main.c 1 Firmware with FreeMASTER TSA and LED colour variable   Add the FreeMASTER Lite configuration and dashboard – watch your board's LED colour live in the browser in about 20 minutes. Examples
View full article
S32 Design Studio: Import, Build, and Monitor a Motor Control Project using AI Introduction This tutorial demonstrates an end-to-end, AI-assisted motor control workflow using S32 Design Studio AI Support. You'll find a motor control application for the FRDM-A-S32K312 on the NXP Application Code Hub, import it into S32 Design Studio, generate code, build and flash the project, and then create a FreeMASTER dashboard with motor controls, speed selection, and live parameter monitoring. The tutorial uses the NXP PMSM Low Voltage Motor Control Accessory Kit as the motor hardware.   Everything is done through two prompts – jump straight to the steps if you already have the tools installed.   Estimated time: ~35 minutes. System Architecture S32K312 Motor Control + FreeMASTER – system architecture overview   The components involved are:   Motor – NXP PMSM Low Voltage Motor Control Accessory Kit is connected to the FRDM-A-S32K312 board. The Motor is driven by PWM output from the MCU. FRDM-A-S32K312 – Runs motor control firmware with FreeMASTER TSA enabled. Streams live data to the host PC over USB (UART). Host PC – Runs FreeMASTER Lite (fmlite.exe) on COM#, 115200 baud, port 51234. Serves the HTML5 dashboard to the browser. Prerequisites   What you need before starting   Download and install the FRDM Automotive S32K3 + S32M27 Board Installation Package from the Automotive Package Manager – LINK Update S32 Design Studio to v3.6.11 or later using the S32 Design Studio Platform package available in the Extensions and Updates panel Install the S32 Design Studio MCP REST Server (bundled with S32 Design Studio 3.6.11+ or available for installation via Extensions and Updates in older versions starting with 3.6.5) Install the AMMCLIB for S32K3xx/S32M27x (Automotive Math and Motor Control Library) using S32DS Extensions and Updates required by the motor control demo Install the NXP GCC for Arm Embedded Processors v10.2 toolchain using S32DS Extensions and Updates — this is the toolchain used to build the motor control example Install FreeMASTER Lite into your working directory – download from LINK One FRDM-A-S32K312 evaluation board + USB cable One NXP PMSM Low Voltage Motor Control Accessory Kit (motor and driver hardware for the FRDM-A-S32K312) Connect the board to the PC via USB and find out which COM port it was assigned — open Device Manager → Ports (COM & LPT) and note the port of the board's USB-serial interface (it can be any COMx ). You will hand this value to the AI agent, which uses it for the FreeMASTER Lite serial connection Any modern browser (Chrome / Edge / Firefox) Download, install and configure your agent to use the S32 Design Studio AI Support following the Installation & Usage Guide   Note: This tutorial uses these paths: S32 Design Studio Installation: C:\NXP\2026\K3_kit\S32DS_3.6.8 Workspace: C:\NXP\2026\K3_kit\workspace_S32DS_3.6.8_K3_kit FreeMASTER Installation: C:\NXP\2026\K3_kit\FM_32 You can use any location. If you do, update the paths in the prompt to match. Connect the FRDM-A-S32K312 board to the PC via USB before starting, then tell the agent the COM port of the board — for example: "the board is connected on COM7, use it for FreeMASTER Lite". Everywhere this tutorial shows COMx , replace it with your own port number. The AI will search the Application Code Hub and select the most suitable motor control demo automatically. Steps   Send the following prompts to your AI assistant in order. Each is a complete, self-contained instruction.   Step 1 – Import motor control demo, build and run You are a software developer that needs to use S32K312 FRDM board to control a motor. I have the NXP PMSM Low Voltage Motor Control Accessory Kit available for my application. Check NXP Application Code Hub for an application that can be used and import the selected application into S32 Design Studio IDE. S32DS is installed at C:\NXP\2026\K3_kit\S32DS_3.6.8. Run S32 Configuration Tools to generate code, build it, load into the flash memory and run the project. Use the s32ds-agentic-ai MCP server; if the MCP server disconnects at any point, stop immediately and notify user. AI will:   Search NXP Application Code Hub for a motor control application suitable for the FRDM-A-S32K312 and compatible with the NXP PMSM Low Voltage Motor Control Accessory Kit Import the selected project into S32 Design Studio at C:\NXP\2026\K3_kit\S32DS_3.6.8 Open S32 Configuration Tools and click Generate Code (Pins, Clocks, Peripherals) Build the project and confirm zero errors Flash the .elf binary into the board's flash memory and run the project Stop and notify the user immediately if the s32ds-agentic-ai MCP server disconnects   Step 2 – Create FreeMASTER dashboard and run it Using FreeMaster Lite create a self contained web dashboard and the server configuration file in the project folder called dashboard. FreeMaster Lite is installed at c:\NXP\2026\K3_kit\FM_32\FreeMASTER Lite\fmlite.exe The dashboard should define and connect all the variables for the 4 panels and contained components: - top panel: contains the controls for the board serial connection, default: connection name "S32K312 Board", COM#, 115200 baud, 8 data bits, no parity, 1 stop bit - left panel: contains the motor control panel: motor state (on/off), actual RPM and desired RPM, slider for selecting the RPMs in both directions, a 0 RPM button, and +- 10/100 RPMs buttons - middle panel: contains a graphical representation of the motor, spinning the NXP logo in sync with the motor actual speed - right panel: contains all the board\motor parameters that you can find relevant Start FreeMaster server and run the dashboard at the end Once the JS client confirms that the board is connected it should start reading desired and actual RPMs Use the s32ds-agentic-ai MCP server; if the MCP server disconnects at any point, stop immediately and notify user. AI will:   Create a FreeMASTER configuration file in the project subfolder dashboard/: COM#, 115200 baud, 8 data bits, no parity, 1 stop bit, connection name "S32K312 Board" Generate a self-contained HTML5 dashboard saved to the project subfolder dashboard/ with all FreeMASTER variables defined, organised in four panels Once the JS client confirms the board is connected, automatically start reading desired and actual RPMs Start the FreeMASTER server and open the dashboard in the browser Stop and notify the user immediately if the s32ds-agentic-ai MCP server disconnects   Verifying the Result   Work through this final check to confirm that both prompts completed successfully.   Final check Motor control project imported and visible in S32DS Project Explorer. S32 Configuration Tools ran – code generated with no errors. Build completes with zero errors. Firmware flashed and running – motor responds as expected. PMSM kit connected and motor responds to commands from the dashboard. FreeMASTER configuration file created in dashboard/: COM#, 115200 baud, 8 data bits, no parity, 1 stop bit, connection name "S32K312 Board". FreeMASTER server is running. Dashboard opens in browser – all four panels visible. Once connected, the dashboard automatically starts reading desired and actual RPMs. Left panel shows motor on/off state, actual and desired RPM, slider for both directions, 0 RPM button, and ±10/100 RPM buttons. Middle panel shows the NXP logo spinning in sync with the actual motor speed. Right panel shows all relevant board/motor parameters updating in real time. Troubleshooting   Symptom Fix No motor control demo found on ACH Try broader search terms such as "motor", "PWM", or "BLDC". Confirm the s32ds-agentic-ai server is connected. Import fails or project missing from Project Explorer Try File › Import › Existing Projects into Workspace manually. Confirm S32DS path is C:\NXP\2026\K3_kit\S32DS_3.6.8. S32 Configuration Tools does not open Double-click the .mex file. Ensure the S32K3 SDK is installed and the project SDK is correctly configured. Generate Code produces errors Check Pins, Clocks, and Peripherals tabs for red validation markers. Resolve conflicts before regenerating. Build errors after Generate Code Ensure the generated src/ folder is in the build path. Try Project › Clean then rebuild. Motor does not respond after flashing Check hardware connections between board and motor driver. Verify correct PWM output pins per the demo schematic. FreeMASTER dashboard does not connect Confirm the FreeMASTER server is running and COM# / 115200 baud / port 51234 match the configuration file. Check that the board is powered and running. Dashboard does not auto-read RPMs after connect Check the JS connect callback in the dashboard HTML. Ensure the ReadVariable calls for desired and actual RPM are triggered after the WebSocket StartComm response confirms success. Actual/desired RPM shows 0 or stale Verify the variable names match those in the FreeMASTER project. Check that FMSTR_Poll() is called in the main loop and TSA is enabled. Right panel parameters not updating Verify FreeMASTER TSA is enabled (FMSTR_USE_TSA 1) and FMSTR_Poll() is called in the main loop. s32ds-agentic-ai MCP server disconnects Stop immediately and restart the MCP server following the Installation & Usage Guide. File Reference   File Step Description src/main.c 1 Main firmware – motor control loop with FreeMASTER TSA *.mex 1 S32 Configuration Tools project file (Pins, Clocks, Peripherals) generate/src/ 1 Auto-generated peripheral initialisation source files generate/include/ 1 Auto-generated peripheral configuration headers dashboard/board_115200.fmcfg 2 FreeMASTER server configuration: COM#, 115200 baud, 8 data bits, no parity, 1 stop bit, "S32K312 Board" dashboard/motor_dashboard.html 2 Self-contained HTML5 dashboard with all FreeMASTER variables, 4 panels (top: serial connection; left: motor control with slider, 0 RPM button, ±10/100 RPM buttons; middle: NXP logo spinning in sync with actual speed; right: board/motor parameters), auto-read on connect   Import the demo, build it and let your AI assistant generate the FreeMASTER dashboard – a complete motor control setup in about 35 minutes. Examples
View full article
S32 Design Studio: Import and Build an Application Code Hub Project using AI Introduction This tutorial shows how an AI agent, together with S32 Design Studio AI Support, can run a complete S32 Design Studio workflow from one natural-language prompt. The workflow covers importing an NXP Application Code Hub example, generating configuration code, building the project, and running it on hardware. Instead of clicking through wizards, configuration views, and debug settings, you describe the result you want in plain language. The agent then uses S32 Design Studio AI Support's MCP tools to carry out each step. In this scenario, you ask the agent to complete an end-to-end task: Start S32 Design Studio with a dedicated workspace. Import the GPIO Blinking LED Demo from the NXP Application Code Hub. Target the FRDM-A-S32K312 board. Generate code for Pins, Clocks, and Peripherals using S32 Configuration Tools. Build the project with zero errors. Flash and run the firmware on the connected board. The agent breaks this request into a sequence of tool calls. It starts the IDE, searches the Application Code Hub, imports the demo, runs code generation, builds the project, and flashes the board.  Estimated time: ~20 minutes. System Architecture GPIO Blinking LED Demo — FRDM-A-S32K312 – system architecture overview   The components involved are:   FRDM-A-S32K312 – Target evaluation board. Runs the GPIO Blinking LED Demo firmware. Host PC – Runs S32 Design Studio and the S32 Design Studio AI Support. Imports the project, generates code, builds, and flashes the firmware over USB. Prerequisites   What you need before starting Download and install the FRDM Automotive S32K3 + S32M27 Board Installation Package from the Automotive Package Manager – LINK Update S32 Design Studio to v3.6.11 or later using the S32 Design Studio Platform package available in the Extensions and Updates panel Install the S32 Design Studio MCP REST Server (bundled with S32 Design Studio 3.6.11+ or available for installation via Extensions and Updates in older versions starting with 3.6.5) One FRDM-A-S32K312 evaluation board + USB cable Download, install and configure your agent to use the S32 Design Studio AI Support from Installation & Usage Guide  Note: This tutorial uses these paths: Installation: C:\NXP\2026\K3_kit\S32DS_3.6.8 Workspace: C:\NXP\2026\K3_kit\workspace_S32DS_3.6.8_K3_kit You can use any location. If you do, update the paths in the prompt to match. Connect the FRDM-A-S32K312 board to the PC via USB before starting. The AI will detect the board automatically through the MCP server. Steps   Send the following prompt to your AI assistant. It is a complete, self-contained instruction that drives the demo.   Step 1 – Import GPIO Blinking LED Demo & build You are a software developer that needs to use S32K312 FRDM board, start S32DS that is installed at C:\NXP\2026\K3_kit\S32DS_3.6.8, import the GPIO Blinking LED Demo for FRDM-A-S32K312 from the NXP Application Code Hub into S32 Design Studio IDE. After importing, run S32 Configuration Tools to generate code (Pins, Clocks, Peripherals), build and run the project. Use s32ds-agentic-ai MCP server and if the server disconnects, stop and notify the user. AI will:   Start S32 Design Studio from C:\NXP\2026\K3_kit\S32DS_3.6.8 Search NXP Application Code Hub for GPIO Blinking LED Demo for FRDM-A-S32K312 and import it into S32DS Open S32 Configuration Tools and click Generate Code (Pins, Clocks, Peripherals) Trigger a full build and confirm zero errors Flash and run the project on the board Stop and notify the user if the s32ds-agentic-ai server disconnects Verifying the Result   Work through this final check to confirm that the prompt completed successfully.   Final check The project is imported and visible in the S32DS Project Explorer. S32 Configuration Tools ran successfully – Pins, Clocks, and Peripherals code was generated with no errors. Build completes with zero errors. Firmware is flashed and running on the FRDM-A-S32K312 board. The onboard LED should toggle with a 500ms cadence (500ms on, 500ms off). Troubleshooting   Symptom Fix Project not found in Application Code Hub Confirm the search term is GPIO Blinking LED Demo for FRDM-A-S32K312. Check that the s32ds-agentic-ai is connected and the ACH tool is available. Import fails or project does not appear in Project Explorer Try File › Import › Existing Projects into Workspace manually. Confirm the workspace path is C:\NXP\2026\K3_kit\workspace_S32DS_3.6.8_K3_kit. S32 Configuration Tools does not open Double-click the .mex file in the project root. Ensure the S32K3 SDK is installed and the project SDK is correctly configured. Generate Code produces errors Check the Pins, Clocks, and Peripherals tabs for validation errors (red markers). Resolve conflicts before regenerating. Build errors after Generate Code Ensure the generated src/ folder is included in the build path. Try Project › Clean then rebuild. Flash / debug fails Ensure the board is powered via USB and the J-Link / OpenSDA debugger is recognised. Try Run › Debug Configurations and re-select the correct debug probe. LED does not blink after flashing Confirm the correct binary was flashed. Check that the debug session started and the program counter advanced past main(). s32ds-agentic-ai server disconnects Stop immediately and restart the MCP server following the setup instructions. Do not continue until the server is confirmed connected. File Reference   File Step Description src/main.c 1 Main firmware entry point — GPIO LED blinking loop *.mex 1 S32 Configuration Tools project file (Pins, Clocks, Peripherals) generate/src/ 1 Auto-generated peripheral initialization source files generate/include/ 1 Auto-generated peripheral configuration headers   Import the demo, generate the configuration code and flash it – your first Application Code Hub project running on the FRDM-A-S32K312 in about 20 minutes. Examples
View full article
MCXN547 SC Timer0 SDK 驱动程序问题 我使用的是MCXN547VKL单片机和SDK版本26.06.00。 背景:我使用 SCT timer0 通过分割模式下的 COUNTER 生成两个不同的 PWM 波形,CONFIG[UNIFY] = 0;即 COUNT_L 用于一个 PWM 生成器,COUNT_H 用于另一个 PWM 生成器。 问题:当我使用驱动程序 API " SCTIMER_SetCOUNTValue(SCT0,kSCTIMER_Counter_H,0U);" 加载 COUNTER_H 时,发生总线故障。 我发现问题出在 SDK 驱动程序代码上。驱动程序代码使用 32 位写入同时写入 COUNT_H 和 COUNT_L,而不是仅使用 16 位写入 COUNT_H。在写入 COUNT_H 时,COUNT_L 正在运行,这导致了总线故障。我修改了 SDK 驱动程序代码,使其使用 16 位写入,总线故障就没有发生。我已附上驱动程序代码,并用颜色标记出导致问题的代码行和解决方法。如果这确实是问题所在,可以更新 SDK 驱动程序。- 谢谢 /*! * @brief 设置计数器的值。 * 该功能用于设置计数寄存器的值,写入 COUNT_L、COUNT_H 或统一寄存器。 只有当相应的计数器停止时(CTRL 寄存器中的 HALT 位设置为 1),才允许使用 *。 * * @Param base SCTimer 外设基地址 * @Param whichCounter 要使用的 SCTimer 计数器。在 16 位模式下,我们可以选择 Counter_L 和 Counter_H。 * 在 32 位模式下,我们可以选择 Counter_U。 * @Param value 计数器值更新到 COUNT 寄存器。 */ static inline void SCTIMER_SetCOUNTValue ( SCT_Type *base, sctimer_counter_t whichCounter, uint32_t value) { SCTIMER_StopTimer(base, ( uint32_t )whichCounter); 切换(whichCounter) { case kSCTIMER_Counter_L : assert(value <= 0xFFFFU); assert(0U == (base-> CONFIG & SCT_CONFIG_UNIFY_MASK)); /* 当用户想要设置低计数器时,请使用 Counter_L 位 */ base-> COUNT_ACCESS16BIT.COUNTL = ( uint16_t ) value; 休息; case kSCTIMER_Counter_H : assert(value <= 0xFFFFU); assert(0U == (base-> CONFIG & SCT_CONFIG_UNIFY_MASK)); /* 当用户想要设置高位计数器时,请使用 Counter_H 位 */ // base->COUNT = (uint32_t)base->COUNT_ACCESS16BIT.COUNTL | SCT_COUNT_CTR_H(value); base-> COUNT_ACCESS16BIT.COUNTH = ( uint16_t ) value; //修复 休息; case kSCTIMER_Counter_U : assert(1U == (base-> CONFIG & SCT_CONFIG_UNIFY_MASK)); /* 当计数器在 32 位模式下运行时,同时使用 Counter_L/Counter_H 位(统一计数器)。*/ 基本->计数= 值; 休息; 默认: /* 修复 MISRA C-2012 问题规则 16.4。*/ 休息; } SCTIMER_StartTimer(base, ( uint32_t )whichCounter); } 时钟|计时器 Re: MCXN547 SC Timer0 SDK driver Issue 你好@JawaharA 感谢您的反馈。您对总线故障原因的分析是正确的:更新 COUNT_H 需要对 COUNT 寄存器进行 32 位写入,但当前函数只会停止 H 计数器。如果 L 计数器仍在运行,则此写入访问会触发 SCT 总线错误。 然而,将对 COUNTH 的访问更改为 16 位写入不符合 SCT 硬件访问要求,因为 COUNT_H 必须与 COUNT_L 一起作为一个字写入。正确的软件解决方案是在对 COUNT 执行 32 位写入之前停止 L 计数器和 H 计数器,然后在之后恢复它们之前的运行状态。我们建议相应地审查和更新 SDK,而不是使用单独的 16 位写入 COUNT_H。 BR 哈里 Re: MCXN547 SC Timer0 SDK driver Issue 嗨,哈里, 感谢您的快速回复。 根据您在回复中引用的手册页,如果 CONFIG[UNIFY] = 0,则在相应的计数器未运行时,可以单独读取或写入 COUNT_L 和 COUNT_H 寄存器。SDK 对 COUNT_L 寄存器使用 16 位写入。无论 CONFIG[UNIFY] 设置如何,COUNT_H 寄存器都应该使用 32 位写入进行写入 - 这是未记录的条件吗? 谢谢 - 贾瓦哈尔
View full article
PXP screen rotation issue based on i.MXRT1052 I'm using rt1052PXP to rotate a landscape view to a portrait view, but the overall display shifts downwards when I refresh the page. Why is this happening?   static void DEMO_FlushDisplay(lv_disp_drv_t *disp_drv, const lv_area_t *area, lv_color_t *color_p) { lv_area_t dest_area = { .x1 = 0, .x2 = 480 - 1, .y1 = 0, .y2 = 800 - 1, }; lv_gpu_nxp_pxp_blit(((lv_color_t *)s_inactiveFrameBuffer), area, 800, color_p, area,480, LV_OPA_COVER, LV_DISP_ROT_270); DCACHE_CleanInvalidateByRange((uint32_t)color_p, DEMO_FB_SIZE); ELCDIF_SetNextBufferAddr(LCDIF, (uint32_t)s_inactiveFrameBuffer); s_framePending = true;if (xSemaphoreTake(s_frameSema, portMAX_DELAY) == pdTRUE) { /* IMPORTANT!!! * Inform the graphics library that you are ready with the flushing*/ lv_disp_flush_ready(disp_drv); } else { PRINTF("Display flush failed\r\n"); assert(0); } }   i.MXRT 105x 回复: 基于i.MXRT1052的pxp屏幕旋转问题 I've noticed an offset issue when drawing with PXP. Is it because the default initialization `#define LV_USE_GPU_NXP_PXP_AUTO_INIT 1` generated by guiguider can't be used directly? void lv_disp_drv_init(lv_disp_drv_t * driver) { lv_memset_00(driver, sizeof(lv_disp_drv_t)); driver->hor_res = 320; driver->ver_res = 240; driver->physical_hor_res = -1; driver->physical_ver_res = -1; driver->offset_x = 0; driver->offset_y = 0; driver->antialiasing = LV_COLOR_DEPTH > 8 ? 1 : 0; driver->screen_transp = 0; driver->dpi = LV_DPI_DEF; driver->color_chroma_key = LV_COLOR_CHROMA_KEY; #if LV_USE_GPU_NXP_PXP // driver->draw_ctx_init = lv_draw_pxp_ctx_init; // driver->draw_ctx_deinit = lv_draw_pxp_ctx_deinit; // driver->draw_ctx_size = sizeof(lv_draw_pxp_ctx_t); driver->draw_ctx_init = lv_draw_sw_init_ctx; driver->draw_ctx_deinit = lv_draw_sw_init_ctx; driver->draw_ctx_size = sizeof(lv_draw_sw_ctx_t); #else driver->draw_ctx_init = lv_draw_sw_init_ctx; driver->draw_ctx_deinit = lv_draw_sw_init_ctx; driver->draw_ctx_size = sizeof(lv_draw_sw_ctx_t); #endif } 回复: 基于i.MXRT1052的pxp屏幕旋转问题 Hi  @dsd, The LV_USE_GPU_NXP_PXP_AUTO_INIT allows LVGL to leverage the user of PXP for internal widget rendering, which could definitely cause issues when the application also uses this PXP in parallel for whole screen rotation. However, it is likely not the source of the issue. From the initial code, it seems like you are not using dest_area, or rather you are using area as both source and destination for the PXP blit, which means that only the partial dirty region might be getting placed on different absolute positions rather than the intended. 回复: 基于i.MXRT1052的pxp屏幕旋转问题 I used the code generated by guiguider to test it, even without using pxp rotation. static void DEMO_FlushDisplay(lv_disp_drv_t *disp_drv, const lv_area_t *area, lv_color_t *color_p) { DCACHE_CleanInvalidateByRange((uint32_t)color_p, DEMO_FB_SIZE); ELCDIF_SetNextBufferAddr(LCDIF, (uint32_t)color_p); s_framePending = true; if (xSemaphoreTake(s_frameSema, portMAX_DELAY) == pdTRUE) { /* IMPORTANT!!! * Inform the graphics library that you are ready with the flushing*/ lv_disp_flush_ready(disp_drv); } else { PRINTF("Display flush failed\r\n"); assert(0); } } Simply modify the macro /*Use NXP's PXP GPU iMX RTxxx platforms*/ #define LV_USE_GPU_NXP_PXP 1 #if LV_USE_GPU_NXP_PXP /*1: Add default bare metal and FreeRTOS interrupt handling routines for PXP (lv_gpu_nxp_pxp_osa.c) * and call lv_gpu_nxp_pxp_init() automatically during lv_init(). Note that symbol SDK_OS_FREE_RTOS * has to be defined in order to use FreeRTOS OSA, otherwise bare-metal implementation is selected. *0: lv_gpu_nxp_pxp_init() has to be called manually before lv_init() / #define LV_USE_GPU_NXP_PXP_AUTO_INIT 1 #endif /* LV_USE_GPU_NXP_PXP */ The same problem will occur, and the direction of the offset will be the same as after rotation. 回复: 基于i.MXRT1052的pxp屏幕旋转问题 What's even stranger is that there are two different results within the same project, even though I thought the configuration should be the same. No display offset occurred Display offset occurs    
View full article
基于i.MXRT1052的pxp屏幕旋转问题 我正在使用rt1052的pxp将横屏旋转成竖屏显示,但是在不断刷新的情况下,整体显示会向下偏移,这是为什么?   static void DEMO_FlushDisplay(lv_disp_drv_t *disp_drv, const lv_area_t *area, lv_color_t *color_p) { lv_area_t dest_area = { .x1 = 0, .x2 = 480 - 1, .y1 = 0, .y2 = 800 - 1, }; lv_gpu_nxp_pxp_blit(((lv_color_t *)s_inactiveFrameBuffer), area, 800, color_p, area,480, LV_OPA_COVER, LV_DISP_ROT_270); DCACHE_CleanInvalidateByRange((uint32_t)color_p, DEMO_FB_SIZE); ELCDIF_SetNextBufferAddr(LCDIF, (uint32_t)s_inactiveFrameBuffer); s_framePending = true;if (xSemaphoreTake(s_frameSema, portMAX_DELAY) == pdTRUE) { /* IMPORTANT!!! * Inform the graphics library that you are ready with the flushing*/ lv_disp_flush_ready(disp_drv); } else { PRINTF("Display flush failed\r\n"); assert(0); } }   i.MXRT 105x 回复: 基于i.MXRT1052的pxp屏幕旋转问题 我发现当我使用pxp绘制的时候就会出现偏移问题,是因为guiguider生成的默认初始化#define LV_USE_GPU_NXP_PXP_AUTO_INIT 1不能直接使用吗? void lv_disp_drv_init(lv_disp_drv_t * driver) { lv_memset_00(driver, sizeof(lv_disp_drv_t)); driver->hor_res = 320; driver->ver_res = 240; driver->physical_hor_res = -1; driver->physical_ver_res = -1; driver->offset_x = 0; driver->offset_y = 0; driver->antialiasing = LV_COLOR_DEPTH > 8 ? 1 : 0; driver->screen_transp = 0; driver->dpi = LV_DPI_DEF; driver->color_chroma_key = LV_COLOR_CHROMA_KEY; #if LV_USE_GPU_NXP_PXP // driver->draw_ctx_init = lv_draw_pxp_ctx_init; // driver->draw_ctx_deinit = lv_draw_pxp_ctx_deinit; // driver->draw_ctx_size = sizeof(lv_draw_pxp_ctx_t); driver->draw_ctx_init = lv_draw_sw_init_ctx; driver->draw_ctx_deinit = lv_draw_sw_init_ctx; driver->draw_ctx_size = sizeof(lv_draw_sw_ctx_t); #else driver->draw_ctx_init = lv_draw_sw_init_ctx; driver->draw_ctx_deinit = lv_draw_sw_init_ctx; driver->draw_ctx_size = sizeof(lv_draw_sw_ctx_t); #endif } 回复: 基于i.MXRT1052的pxp屏幕旋转问题 嗨@dsd , LV_USE_GPU_NXP_PXP_AUTO_INIT 允许 LVGL 利用 PXP 进行内部控件渲染,当应用程序还并行使用此 PXP 进行全屏旋转时,这肯定会导致问题。然而,这可能并非问题的根源。 从初始代码来看,你似乎没有使用 dest_area,或者说你将 area 同时用作 PXP blit 的源和目标,这意味着只有部分脏区域可能会被放置在不同的绝对位置,而不是预期的位置。 回复: 基于i.MXRT1052的pxp屏幕旋转问题 我用guiguider生成的代码去测试,即便我不使用pxp旋转 static void DEMO_FlushDisplay(lv_disp_drv_t *disp_drv, const lv_area_t *area, lv_color_t *color_p) { DCACHE_CleanInvalidateByRange((uint32_t)color_p, DEMO_FB_SIZE); ELCDIF_SetNextBufferAddr(LCDIF, (uint32_t)color_p); s_framePending = true; if (xSemaphoreTake(s_frameSema, portMAX_DELAY) == pdTRUE) { /* IMPORTANT!!! * Inform the graphics library that you are ready with the flushing*/ lv_disp_flush_ready(disp_drv); } else { PRINTF("Display flush failed\r\n"); assert(0); } } 仅仅去修改宏/*Use NXP's PXP GPU iMX RTxxx platforms*/ #define LV_USE_GPU_NXP_PXP 1 #if LV_USE_GPU_NXP_PXP /*1: Add default bare metal and FreeRTOS interrupt handling routines for PXP (lv_gpu_nxp_pxp_osa.c) * and call lv_gpu_nxp_pxp_init() automatically during lv_init(). Note that symbol SDK_OS_FREE_RTOS * has to be defined in order to use FreeRTOS OSA, otherwise bare-metal implementation is selected. *0: lv_gpu_nxp_pxp_init() has to be called manually before lv_init() */ #define LV_USE_GPU_NXP_PXP_AUTO_INIT 1 #endif /* LV_USE_GPU_NXP_PXP */ 也会有同样的问题,并且偏移的方向与旋转后的一致 回复: 基于i.MXRT1052的pxp屏幕旋转问题 更奇怪的是在同一个工程下会有两种不同的结果,我认为配置应该是相同的 没有发生显示偏移 发生显示偏移    
View full article
MPXV7002DPはLPGおよびプロパンに対応しています。 こんにちは、 私は大学4年生です。現在、家庭用LPG配管の圧力差を測定するプロジェクトに取り組んでいます。配管内の通常の圧力は約2.30kPaから3.60kPaです。データシートを確認しましたが、LPGとの互換性については明確な記載がありませんでした。もし過去にこれを試した方や技術関係者がいれば教えていただけると助かります。 ありがとう 。 Re: MPXV7002DP compatibility with LPG and Propane こんにちは、 2026年2月2日現在、NXP MEMSセンサ製品はSTMicroelectronicsに移管されました。詳細についてはSTMicroelectronicsまでサポートまでお問い合わせください。
View full article
wifi驱动程序崩溃- 88w8997 我使用FN-Link L297B-SR模块(Wi-Fi 和蓝牙共用一个天线)时,遇到了间歇性 Wi-Fi 驱动程序崩溃的问题。该问题随机发生,有时在 1 天后,有时在 2 天后,偶尔在连续运行 4 到 5 天后才会发生。 请检查日志 [64622.321614]mwifiex_sdio mmc2:0001:1: 信息:已成功断开与 ca:c6:5c:cb:ad:7e 的连接:原因代码 3 [64624.050010]mwifiex_sdio mmc2:0001:1: 信息:尝试关联到 BSSID ca:c6:5c:cb:ad:7e [64624.072596]mwifiex_sdio mmc2:0001:1: 事件:未知事件 ID:0x95 [64624.085770]mwifiex_sdio mmc2:0001:1: 信息:已成功关联到 bssid ca:c6:5c:cb:ad:7e [64987.640381]蓝牙:hci0:帧重组失败(-84) [65060.466817]蓝牙:hci0:帧重组失败(-84) [65184.303423]mwifiex_sdio mmc2:0001:1: 信息:已成功断开与 ca:c6:5c:cb:ad:7e 的连接:原因代码 0 [65204.712100]ieee80211 phy0:sched_scan 开始:n_ssids=4 n_match_sets=4 [65204.725038]ieee80211 phy0:通道数=41,间隔=10,IE长度=13 [65259.046894]ieee80211 phy0:计划扫描停止! [65259.067983]mwifiex_sdio mmc2:0001:1: 信息:尝试关联到 BSSID ca:c6:5c:cb:ad:7e [65260.594440]mwifiex_sdio mmc2:0001:1: ASSOC_RESP: 失败,状态码=2 错误=0xfffa a_id=0x3fff [65260.611662]mwifiex_sdio mmc2:0001:1: 关联失败:原因未知连接失败 [65260.624191]mwifiex_sdio mmc2:0001:1: 信息:与 bssid ca:c6:5c:cb:ad:7e 的关联失败 [65260.636278]ieee80211 phy0:sched_scan 开始:n_ssids=4 n_match_sets=4 [65260.645499]ieee80211 phy0:通道数=41,间隔=10,IE长度=13 [65271.191030]mwifiex_sdio mmc2:0001:1: mwifiex_cmd_timeout_func: 超时命令 ID = 0x6b,操作 = 0x1 [65271.199985]mwifiex_sdio mmc2:0001:1: num_data_h2c_failure = 0 [65271.205896]mwifiex_sdio mmc2:0001:1: num_cmd_h2c_failure = 0 [65271.211654]mwifiex_sdio mmc2:0001:1: is_cmd_timedout = 1 [65271.217064]mwifiex_sdio mmc2:0001:1: num_tx_timeout = 0 [65271.222454]mwifiex_sdio mmc2:0001:1: last_cmd_index = 0 [65271.227893]mwifiex_sdio mmc2:0001:1: last_cmd_id: 6b 00 28 00 16 00 12 00 6b 00 [65271.235303]mwifiex_sdio mmc2:0001:1: last_cmd_act: 01 00 13 00 01 00 ca c6 01 00 [65271.242862]mwifiex_sdio mmc2:0001:1: last_cmd_resp_index = 4 [65271.248670]mwifiex_sdio mmc2:0001:1: last_cmd_resp_id: 0c 81 28 80 16 80 12 80 6b 80 [65271.256568]mwifiex_sdio mmc2:0001:1: last_event_index = 3 [65271.262131]mwifiex_sdio mmc2:0001:1: last_event: 18 00 0b 00 0a 00 65 00 0a 00 [65271.269514]mwifiex_sdio mmc2:0001:1: 数据已发送=0 指令已发送=1 [65271.275248]mwifiex_sdio mmc2:0001:1: ps_mode=1 ps_state=0 [65271.281497]mwifiex_sdio mmc2:0001:1:忽略扫描。卡已移除或固件状态异常 [65271.290880]mwifiex_sdio mmc2:0001:1: ===mwifiex 驱动程序信息转储开始=== [65271.317907]mwifiex_sdio mmc2:0001:1: 信息: MWIFIEX 版本: mwifiex 1.0 (16.92.21.p76) [65271.326650]mwifiex_sdio mmc2:0001:1: 扫描失败: -14 [65271.350746]mwifiex_sdio mmc2:0001:1:SDIO 寄存器转储开始 [65271.369462]mwifiex_sdio mmc2:0001:1: SDIO Func0 (0x0-0x9): 43 03 02 02 03 02 00 02 03 00 [65271.385505]mwifiex_sdio mmc2:0001:1: SDIO Func1 (0x10-0x17): 00 00 00 00 00 00 e0 ff [65271.396619]mwifiex_sdio mmc2:0001:1: SDIO 功能1: (0x8) c3 (0x58) 00 (0x5c) 48 (0x5d) 00 (0x60) 07 (0x61) 0c (0x62) 00 (0x64) 10 (0x65) 00 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a) 00 [65271.416154]mwifiex_sdio mmc2:0001:1: SDIO Func1 (0xe8-0xf2): dc fe 7e 00 62 00 3f a7 24 14 70 [65271.580586]mwifiex_sdio mmc2:0001:1: SDIO 功能1 (0xe8-0xf2): dc fe 8f 00 73 00 3f a7 24 14 70 [65271.594858]mwifiex_sdio mmc2:0001:1:SDIO 寄存器转储结束 [65271.610712]mwifiex_sdio mmc2:0001:1: ===mwifiex 驱动程序信息转储结束=== [65271.628592]mwifiex_sdio mmc2:0001:1: == mwifiex 固件转储开始 == [65271.666427]mwifiex_sdio mmc2:0001:1: 无法拉取 ctrl_data [65271.676062]mwifiex_sdio mmc2:0001:1:固件转储失败 [65271.693018]mwifiex_sdio mmc2:0001:1: == mwifiex 转储信息到 /sys/class/devcoredump 开始 [65271.710201]mwifiex_sdio mmc2:0001:1: == mwifiex 转储信息到 /sys/class/devcoredump 结束 [65271.723737]mwifiex_sdio mmc2:0001:1: PREP_CMD: 固件状态异常 [65271.735173]mwifiex_sdio mmc2:0001:1: 信息:mwifiex 已关闭... [65271.769056]mwifiex_sdio mmc2:0001:1: PREP_CMD: 卡已移除 [65271.812192]mwifiex_sdio mmc2:0001:1: PREP_CMD: 卡已移除 [65271.855652]蓝牙:hci0:帧重组失败(-84) [65271.870925]蓝牙:hci0:帧重组失败(-84) [65271.967852]蓝牙:hci0:帧重组失败(-84) [65272.068050]蓝牙:hci0:帧重组失败(-84) [65272.168010]蓝牙:hci0:帧重组失败(-84) [65272.268029]蓝牙:hci0:帧重组失败(-84) [65272.368215]蓝牙:hci0:帧重组失败(-84) [65272.468007]蓝牙:hci0:帧重组失败(-84) [65272.567994]蓝牙:hci0:帧重组失败(-84) [65272.668015]蓝牙:hci0:帧重组失败(-84) [65272.768055]蓝牙:hci0:帧重组失败(-84) [65272.839448]mwifiex_sdio mmc2:0001:1: 信息:固件下载完成,大小为 622240 字节 [65273.607175]mwifiex_sdio mmc2:0001:1: WLAN 固件已激活 [65273.641454]mwifiex_sdio mmc2:0001:1: 未知 api_id: 5 [65273.687228]mwifiex_sdio mmc2:0001:1: 信息: MWIFIEX 版本: mwifiex 1.0 (16.92.21.p76) [65273.713221]mwifiex_sdio mmc2:0001:1: driver_version = mwifiex 1.0 (16.92.21.p76) [65277.145122]mwifiex_sdio mmc2:0001:1: 信息:尝试关联到 BSSID ca:39:a3:cb:ad:7e [65278.668157]mwifiex_sdio mmc2:0001:1: ASSOC_RESP: 失败,状态码=2 错误=0xfffc a_id=0x3fff [65278.677711]mwifiex_sdio mmc2:0001:1: 关联失败:原因 CONNECT_ERR_ASSOC_ERR_TIMEOUT [65278.691251]mwifiex_sdio mmc2:0001:1: ASSOC_RESP: AUTH 超时 [65278.710528]mwifiex_sdio mmc2:0001:1: 信息:与 bssid ca:39:a3:cb:ad:7e 的关联失败 [65279.781236]mwifiex_sdio mmc2:0001:1: 信息:尝试关联到 BSSID ca:c6:5c:cb:ad:7e [65281.310722]mwifiex_sdio mmc2:0001:1: ASSOC_RESP: 失败,状态码=2 错误=0xfffa a_id=0x3fff [65281.320307]mwifiex_sdio mmc2:0001:1: 关联失败:原因未知连接失败 我在下面的 GitHub 链接中找到了同样的问题,但它显示该问题仍处于开放状态。 https://www.bing.com/ck/a?!&&p=6f8995a9ee8bc78d51549c45a34f5deee2c26e49fb129fa9306c277b1df3c48cJmltdHM9MTc5MDQ2NzIwMA&ptn=3&ver=2&hsh=4&fclid=28fe8c6f-37d9-6a8e-3ad5-9b0736ee6b90&psq=wifi+driver+crashes+while+trying+to+reconnect+-+88w8997&u=a1aHR0cHM6Ly9naXRodWIuY29tL254cC1pbXgvaW14LWZpcm13YXJlL2lzc3Vlcy81 提前致谢 Re: wifi driver crashes- 88w8997 您好, 感谢您提供的详细日志。根据崩溃信息,我们可以看到您正在运行固件版本 16.92.21.p76。 请注意,88W8997 已不再包含在标准的 imx 固件版本中。不过,我们有一个专门的热修复分支,其中包含最新的固件,可在此处获取: https://github.com/nxp-imx/mwifiex/tree/hotfix/lf-6.12.49_2.2.0_hotfix_w8997 https://github.com/nxp-imx/imx-firmware/tree/hotfix/lf-6.12.49_2.2.0_hotfix_w8997 我们建议您升级到该分支中提供的固件,该固件比您当前的版本新得多,并且包含稳定性修复程序,可以解决您遇到的命令超时和固件状态错误问题。 问候, 丹尼尔。 Re: wifi driver crashes- 88w8997 DanielRuvalcaba,谢谢你的支持。 我们将热修复固件加载到组合芯片上,并连续运行了大约一周。在此期间,我们遇到了另一个问题。与之前 Wi-Fi 固件崩溃的问题不同,这次 Wi-Fi 功能仍然可用,但 BLE 在连续运行 3-4 天后停止工作。 仅通过 RESET HCI 接口无法恢复 BLE 故障。为了恢复 BLE 功能,我们必须重新加载组合芯片上的固件。我们已附上 BLE 故障期间捕获的最新日志,以供进一步分析。 [308423.524163] Bluetooth: hci0: 命令 0x0406 发送超时 [308454.723609]蓝牙:hci0:命令 0x2011 发送超时 [308454.728959]蓝牙:hci0:操作码 0x2011 失败:-110 [308454.734354]蓝牙:hci0:无法添加到允许列表:-110 [308456.771606]蓝牙:hci0:操作码 0x200b 失败:-110 [308456.776986]蓝牙:hci0:命令 0x200b 发送超时 [308456.782265]蓝牙:hci0:启动后台扫描失败:-110 [308458.819547]蓝牙:hci0:操作码 0x2011 失败:-110 [308458.824925]蓝牙:hci0:命令 0x2011 发送超时 [308458.830210]蓝牙:hci0:无法添加到允许列表:-110 [308460.867534]蓝牙:hci0:操作码 0x200b 失败:-110 [308460.872908]蓝牙:hci0:命令 0x200b 发送超时 [308460.878263]蓝牙:hci0:启动后台扫描失败:-110 [308462.915455]蓝牙:hci0:操作码 0x2011 失败:-110 [308462.920957]蓝牙:hci0:命令 0x2011 发送超时 [308462.926341]蓝牙:hci0:无法添加到允许列表:-110 [308464.963435]蓝牙:hci0:操作码 0x200b 失败:-110 [308464.968817]蓝牙:hci0:命令 0x200b 发送超时 [308464.974104]蓝牙:hci0:启动后台扫描失败:-110 [308467.747431]蓝牙:hci0:命令 0x200a 发送超时 提前致谢。
View full article
MCXN547 SC Timer0 SDKドライバーの問題 私はMCUとSDK MCXN547VKLバージョン26.06.00を使っています。 コンテキスト: 私は SCT タイマー 0 を使用して、スプリット モードの COUNTER を使用して 2 つの異なる PWM 波形を生成しています。CONFIG[UNIFY] = 0、つまり COUNT_L を 1 つの PWM ジェネレーターに、COUNT_H を別の PWM ジェネレーターに使用しています。 問題はこうです:ドライバーAPI「SCTIMER_SetCOUNTValue(SCT0,kSCTIMER_Counter_H,0U)」でCOUNTER_Hを読み込むと、バスフォールトが発生します。 問題の原因をSDKのドライバーコードに突き止めました。ドライバコードはCOUNT_H単独で16ビットの書き込みではなく、COUNT_HとCOUNT_Lの両方を32ビット書き込みで行います。COUNT_H が書き込まれている間に COUNT_L が実行されていたため、バス障害が発生しました。SDKのドライバーコードを16ビット書き込みに変更したところ、バスの故障は発生しませんでした。ドライバーコードを添付し、問題の原因となったコードラインと修正方法を色で示しました。もし本当にこれが問題なら、SDKドライバーを更新できます。- ありがとう /*! * @brief カウンターの値を設定します。 * * この機能は、カウントレジスタの値を設定することであり、COUNT_L、COUNT_H、または統合レジスタに書き込みます。 * は、対応するカウンタが停止しているとき(CTRL レジスタの HALT ビットが 1 に設定されているとき)にのみ許可されます。 * * @param base SCTimer ペリフェラル ベースアドレス * @param whichCounter SCTimer カウンターを使います。16ビットモードでは、Counter_LとCounter_Hを選択できます。 * 32ビットモードではCounter_Uを選択できます。 * @Param value COUNTレジスタへのカウンタ値の更新。 */ static inline void SCTIMER_SetCOUNTValue ( SCT_Type *base, sctimer_counter_t whichCounter, uint32_t value) { SCTIMER_StopTimer(base, ( uint32_t )whichCounter); スイッチ (whichCounter) { case kSCTIMER_Counter_L: assert(value <= 0xFFFFU); assert(0U == (base-> CONFIG & SCT_CONFIG_UNIFY_MASK)); /* ユーザーがLowカウンターを設定したいときにビットCounter_Lを使います */ base-> COUNT_ACCESS16BIT.COUNTL = ( uint16_t ) value; 壊す; case kSCTIMER_Counter_H: assert(value <= 0xFFFFU); assert(0U == (base-> CONFIG & SCT_CONFIG_UNIFY_MASK)); /* ユーザーがHighカウンターを設定したいときにCounter_Hビットを使う */ // base->COUNT = (uint32_t)base->COUNT_ACCESS16BIT.COUNTL | SCT_COUNT_CTR_H(value); base- > COUNT_ACCESS16BIT.COUNTH = ( uint16_t )value; //修正 壊す; CASE kSCTIMER_Counter_U: assert(1U == (base-> CONFIG & SCT_CONFIG_UNIFY_MASK)); /* カウンタが 32 ビットモードで動作している場合 (カウンタを統合する場合) は、Counter_L ビットと Counter_H ビットの両方を使用します。*/ base-> COUNT = value; 壊す; デフォルト: /* MISRA C-2012 問題ルール 16.4 を修正します。*/ 壊す; } SCTIMER_StartTimer(base, ( uint32_t )whichCounter); } クロック|タイマー Re: MCXN547 SC Timer0 SDK driver Issue こんにちは、 @JawaharA さん。 ご意見ありがとうございます。バス障害の原因に関するあなたの分析は正しいです。COUNT_H の更新には COUNT レジスタへの 32 ビット書き込みが使用されますが、現在の関数は H カウンタのみを停止します。Lカウンタがまだ動作している場合、この書き込みアクセスはSCTバスエラーを引き起こします。 しかし、COUNTHへの16ビット書き込みへのアクセス変更はSCTハードウェアアクセス要件に適合しません。なぜなら、COUNT_HはCOUNT_L と一緒にワードとして書かなければならないからです。正しいソフトウェアの解決策は、32ビットのCOUNTへの書き込みを行う前にLとHの両方のカウンターを停止し、その後に以前の実行状態を復元することです。別途16ビットの書き込みを使わずにSDKをレビューし、適切に更新することを推奨COUNT_H。 BR ハリー Re: MCXN547 SC Timer0 SDK driver Issue こんにちは、ハリーさん。 迅速なご対応ありがとうございます。 ご回答で参照されたマニュアルページによると、CONFIG[UNIFY] = 0の場合、COUNT_LレジスタとCOUNT_Hレジスタの両方をそれぞれカウンタが動作していない間に個別に読み書きできます。SDKはレジスタに16ビット書き込みCOUNT_L使っています。COUNT_HレジスタはCONFIG[UNIFY]の設定に関係なく32ビット書き込みで書き込む必要がありますが、これは非公式な条件でしょうか? ありがとう - ジャワハル
View full article
FRDM-MCXN236にはクーポンは適用されません NXPのウェブサイトでは、この無料ボードを使って始められると宣伝していた。しかし、在庫があるにもかかわらず、クーポンコードがチェックアウト時にまだ使えません。 評価ボード Re: Coupon not valid for FRDM-MCXN236 こんにちは、 PLACEHOLDER7 その場合は、 [email protected] までにショッピングカートチームまでメールをお送りください。 そのチームはオンライン注文を担当しています。 ご理解いただきありがとうございます。 ベッキー
View full article
「examples/freemaster_examples/fmstr_example_pdbdmにおけるアプリケーションコマンドの問題 親愛なるみんな sdk.sdk_2.x_lpcxpresso54114をダウンロードしましたFreeMASTERの例のみを使用します。アプリケーションコマンドセクションで奇妙な挙動が見つかる以外は、すべての面で正常に動作しています 詳細はGitHubに掲載されています。こちらをご覧ください。 https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10 敬具 パオロ Re: Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm こんにちは、問題の理解が正しければ、例のアプリケーションでコマンド0x10がコード16を返す理由が見当たりません。 コマンド0x10はコールバック関数に登録されています。 したがって、FreeMASTERがコマンド実行をプロブリングすると、「my_appcmd_handler」関数は自動的に呼び出されます。このコールバックのサンプルコードは非常に単純です。 そのため、戻りコード16(=0x10)が回答として返されます。 また、ご報告いただいたように、ID 0x02 の app.command で、FreeMASTER に不明な応答に対するメッセージ表示に関する問題があることも確認しました。応答0xcdは「不明な応答」として報告されるべきだが、実際には何もメッセージが生成されない。 ありがとう、 ミハル
View full article
LS1046A カスタムデザインHRESET_Bリリースされていません <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 LS1046Aプロセッサーを活用したカスタムデザインを作ろうとしています。(基板設計ではRDBを基準にしていました。)すべての電源レール電圧が正しいことを確認し、電源シーケンスのタイミングを測定したところ、すべてデータシートに記載されている許容範囲内であることが確認されました。私が経験している問題は、プロセッサーをリセットから解除できないことです。測定したところ、プロセッサーがHRESET_B信号を放っていません。リファレンスマニュアルによると、初期化中はプロセッサがこのラインを低く保ち、RCWの読み込みやPLLのロック後はリリースするそうです。RCWにエラーがあるのかと思い、代わりに内蔵のRCW値を使いました。(プロセッサに0x9Eと0x9F RCWの両方を固定しましたが、結果は同じでした。) 今のところ、私は少し途方に暮れています。クロックは納期通りに納品され、スルーレートはすべて仕様範囲内であり、ストラップ値を解放する前に適切な時間保持しています。リファレンスマニュアルには、PBLがエラーに遭遇した場合にRESET_REQ信号を切り替えると書かれていますが、私はそのような現象は見ていません。私の現時点での結論は、PBLが実行されていないということです。これはプロセッサがまだリセット状態にあるサインです。 何か見落としている点があるのでしょうか?次にどこを探せばいいでしょうか?私のタイミングは仕様の範囲内ですが、RDBとは完全に一致しません(ボード上の関連信号をプローブしました)。LS1046の電源シーケンス制御はどの程度敏感ですか? よろしくお願いいたします。 Re: LS1046A Custom Design HRESET_B not released こんにちは、ブライス 正しい方向にするためにどのシーケンスを変更したのか説明してもらえますか?現在、私もカスタムLS1046Aボードで同様の問題に直面しています。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 上記のご回答、ありがとうございました。 最後に、CPLDコードのパワーシーケンスの問題を解決しました。元のコードがこの問題を引き起こしていたため、コードを書き直したところ、問題は解消されました。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> プロセッサ接続の回路図を確認できるように、技術CASEを作成してください。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ハードウェアには、フラッシュメモリから取得したRCWではなく、ハードコードされたRCWを使用するように設定しました。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> RCWが外部フラッシュメモリから読み取られているかどうかを、デジタルオシロスコープを使用して確認してください。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 ご回答ありがとうございます。上記すべてが良好な状態であることを確認しました。ただし、最後の点について一つ質問があります。これは電源投入リセットシーケンスを完了するために必要な手順なのでしょうか?先ほど述べたように、RESET_REQ信号を観測できないため、PBLの実行はできないと考えています。SerDesリファレンスクロックは、PBLを実行するために必須ですか、それともPBLがシステムをセットアップしている段階で必要になりますか? よろしくお願いします。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 最初の確認段階として、以下を点検してください。 1) QorIQ LS1046A、LS1026Aデータシートの表1の注記に明示的に記載されているすべての信号のPORレベル。バスごとのピン配置リスト。 2) HRESET_Bは外部からアサートされない 3) SerDesリファレンスクロックはデータシートの要件に準拠しています。 問題が解決しない場合は、次のブリングアップステージを技術ケースとして行う方が便利です。 https://community.nxp.com/thread/381898
View full article
LS1046A Custom Design HRESET_B not released Hello, I am working to bringup a custom design making use of the LS1046A processor. (Board design used the RDB as a reference).  I have verified that all power rail voltages are correct and have have measured the power sequencing timing which all appear to be withing the tolerances found in the datasheet. The issue I am experiencing is that I am not able to bring the processor out of reset. When measuring, I found that the processor is not releasing the HRESET_B signal. The reference manual indicates that the processor will hold this line low while it is performing initialization and will release it after loading the RCW and locking PLL's, etc. Thinking perhaps I had an error in my RCW, I used the built-in RCW values instead. (I strapped the processor with both the 0x9E and 0x9F RCW values with the same result). At this point, I'm at a bit of a loss. My clocks are provided on time, my slew rates are all within spec, and I am holding the strapping values for the correct amount of time before releasing them. The reference manual also indicates that the PBL will toggle the RESET_REQ signal if it has encountered an error, but I am not seeing this happen. So my conclusion currently is that the PBL is not even being executed which, to me, is a sign that the processor is still in a reset state. Is there something here that I am missing? Anywhere I should look next? My timings are within spec, but do not match the RDB exactly (I probed the relevant signals on the board). How sensitive is the power sequencing on the LS1046? Thanks in advance. Re: LS1046A Custom Design HRESET_B not released Hi bryce  Can you explain what sequence did you chnage to get it right? Currently I am also facing similar issue with cutsom ls1046a board Re: LS1046A Custom Design HRESET_B not released Thank you for your above answers. To tie off the thread, I have solved the issue with the power sequencing in my CPLD code. Because the original code I had was causing this issue, I re-wrote it and I no longer see the issue.  Re: LS1046A Custom Design HRESET_B not released Please create a Technical Case so I will be able to check the processor connection schematics. Re: LS1046A Custom Design HRESET_B not released We have strapped the hardware to use the hard-coded RCW, not the RCW from flash. Re: LS1046A Custom Design HRESET_B not released Please use a digital scope to check whether RCW is read from an external flash. Re: LS1046A Custom Design HRESET_B not released Hello, Thanks for your response.  I have verified that all of the above are in a good state. One question I did have about your last point, however: Is this required in order for the power-on reset sequence to complete? As I stated earlier, we are not able to observe the RESET_REQ signal, so I believe we are unable to execute the PBL. Are SerDes reference clocks required in order execute the PBL, or are they required later on while PBL is already setting up the system? Thanks Re: LS1046A Custom Design HRESET_B not released As first checking stage please inspect: 1) POR levels of all signals explicitly mentioned in the notes to the QorIQ LS1046A, LS1026A Data Sheet, Table 1. Pinout list by bus. 2) HRESET_B is not asserted externally 3) SerDes reference clocks conform to the Data Sheet requirements. If the issue will not be resolved, it is more convenient to perform next bring-up stage as Technical Case: https://community.nxp.com/thread/381898 
View full article
此优惠券不适用于 FRDM-MCXN236 NXP 网站宣传了这款免费板。但是即使商品有库存,结账时优惠券代码仍然无法使用。 评估板 Re: Coupon not valid for FRDM-MCXN236 你好PLACEHOLDER7 在这种情况下,请您发送电子邮件至[email protected]联系我们的购物车团队。 该团队负责处理线上订单。 谢谢您的理解 贝基
View full article
LS1046A 定制设计 HRESET_B 未发布 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好, 我正在努力开发一个使用 LS1046A 处理器的定制设计。(电路板设计参考了RDB。)我已经确认所有电源轨电压均正确,并且测量了电源时序时序,所有参数似乎都在数据手册规定的容差范围内。我遇到的问题是无法将处理器从重置状态中恢复。测量时,我发现处理器没有释放 HRESET_B 信号。参考手册指出,处理器在执行初始化时会将此线路保持低电平,并在加载 RCW 和锁定 PLL 等操作后将其释放。考虑到我的 RCW 设置可能有误,我改用了内置的 RCW 值。(我分别用 0x9E 和 0x9F RCW 值给处理器加装了 RCW 参数,结果相同)。 此时此刻,我有点不知所措。我的时钟按时交付,我的转换速率均在规格范围内,并且在释放之前,我会将捆扎值保持正确的时间。参考手册还指出,如果 PBL 遇到错误,它会切换 RESET_REQ 信号,但我没有看到这种情况发生。因此,我目前的结论是 PBL 根本没有执行,在我看来,这表明处理器仍处于 RESET 状态。 我是不是漏掉了什么?接下来我应该从哪里入手?我的时序符合规格,但与 RDB 不完全匹配(我探测了板上的相关信号)。LS1046的电源时序控制有多敏感? 先行致谢。 Re: LS1046A Custom Design HRESET_B not released 嗨,布莱斯 你能解释一下你修改了哪些步骤才做对了吗?目前我也遇到了类似的问题,使用的是定制的LS1046A主板。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 感谢您之前的解答。 最后,我已经解决了 CPLD 代码中的电源时序问题。由于我之前的代码导致了这个问题,所以我重写了代码,现在问题已经解决了。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 请创建一份技术案例,以便我能够查看处理器连接原理图。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我们已经将硬件绑定到使用硬编码的 RCW,而不是来自闪存的 RCW。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 请使用数字示波器检查是否能从外部闪存读取 RCW。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好, 谢谢你的回复。我已经确认以上所有物品都处于良好状态。关于您最后一点,我还有一个问题:这是上电复位序列完成的必要条件吗?正如我之前所说,我们无法观察到 RESET_REQ 信号,所以我认为我们无法执行 PBL。SerDes 参考时钟是执行 PBL 所必需的,还是在 PBL 设置系统时才需要的? 谢谢! Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 第一阶段检查请检查: 1) QorIQ LS1046A、LS1026A 数据表表 1 中明确提及的所有信号的 POR 水平。按总线列出引脚图。 2) HRESET_B 未被外部钳位 3) SerDes 参考时钟符合数据手册的要求。 如果问题无法解决,则更方便地将下一阶段的启动工作作为技术案例来执行: https://community.nxp.com/thread/381898
View full article
Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm Dear All Downloaded sdk.sdk_2.x_lpcxpresso54114 with only FreeMASTER examples. It works correctly in any aspect apart the Application Command section where I find strange behavior More details has been posted in github here: https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10 Regards Paolo Re: Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm Hello, if I understand the issue correctly, you do not see a reason why command 0x10 returns code 16 in the example application. The command 0x10 is registered for a callback function: So the function "my_appcmd_handler" gets called automatically when FreeMASTER probes the command execution.  The example code of this callback is quite trivial: Which is the reason you get the return code 16 (=0x10) as answer. I also confirm there is an issue in FreeMASTER with displaying a message for unknown responses as you reported for app.command with Id 0x02. The response 0xcd should be reported as "unknown response" but generates no message at all. Thanks, Michal
View full article
wifi driver crashes- 88w8997 I am facing an intermittent Wi-Fi driver crash issue with the FN-Link L297B-SR module (Wi-Fi and Bluetooth sharing a single antenna). The issue occurs randomly, sometimes after 1 day, sometimes after 2 days, and occasionally only after 4 to 5 days of continuous operation. please check the logs  [64622.321614] mwifiex_sdio mmc2:0001:1: info: successfully disconnected from ca:c6:5c:cb:ad:7e: reason code 3 [64624.050010] mwifiex_sdio mmc2:0001:1: info: trying to associate to bssid ca:c6:5c:cb:ad:7e [64624.072596] mwifiex_sdio mmc2:0001:1: event: unknown event id: 0x95 [64624.085770] mwifiex_sdio mmc2:0001:1: info: associated to bssid ca:c6:5c:cb:ad:7e successfully [64987.640381] Bluetooth: hci0: Frame reassembly failed (-84) [65060.466817] Bluetooth: hci0: Frame reassembly failed (-84) [65184.303423] mwifiex_sdio mmc2:0001:1: info: successfully disconnected from ca:c6:5c:cb:ad:7e: reason code 0 [65204.712100] ieee80211 phy0: sched_scan start : n_ssids=4 n_match_sets=4 [65204.725038] ieee80211 phy0: n_channels=41 interval=10 ie_len=13 [65259.046894] ieee80211 phy0: sched scan stop! [65259.067983] mwifiex_sdio mmc2:0001:1: info: trying to associate to bssid ca:c6:5c:cb:ad:7e [65260.594440] mwifiex_sdio mmc2:0001:1: ASSOC_RESP: failed, status code=2 err=0xfffa a_id=0x3fff [65260.611662] mwifiex_sdio mmc2:0001:1: assoc failure: reason Unknown connect failure [65260.624191] mwifiex_sdio mmc2:0001:1: info: association to bssid ca:c6:5c:cb:ad:7e failed [65260.636278] ieee80211 phy0: sched_scan start : n_ssids=4 n_match_sets=4 [65260.645499] ieee80211 phy0: n_channels=41 interval=10 ie_len=13 [65271.191030] mwifiex_sdio mmc2:0001:1: mwifiex_cmd_timeout_func: Timeout cmd id = 0x6b, act = 0x1 [65271.199985] mwifiex_sdio mmc2:0001:1: num_data_h2c_failure = 0 [65271.205896] mwifiex_sdio mmc2:0001:1: num_cmd_h2c_failure = 0 [65271.211654] mwifiex_sdio mmc2:0001:1: is_cmd_timedout = 1 [65271.217064] mwifiex_sdio mmc2:0001:1: num_tx_timeout = 0 [65271.222454] mwifiex_sdio mmc2:0001:1: last_cmd_index = 0 [65271.227893] mwifiex_sdio mmc2:0001:1: last_cmd_id: 6b 00 28 00 16 00 12 00 6b 00 [65271.235303] mwifiex_sdio mmc2:0001:1: last_cmd_act: 01 00 13 00 01 00 ca c6 01 00 [65271.242862] mwifiex_sdio mmc2:0001:1: last_cmd_resp_index = 4 [65271.248670] mwifiex_sdio mmc2:0001:1: last_cmd_resp_id: 0c 81 28 80 16 80 12 80 6b 80 [65271.256568] mwifiex_sdio mmc2:0001:1: last_event_index = 3 [65271.262131] mwifiex_sdio mmc2:0001:1: last_event: 18 00 0b 00 0a 00 65 00 0a 00 [65271.269514] mwifiex_sdio mmc2:0001:1: data_sent=0 cmd_sent=1 [65271.275248] mwifiex_sdio mmc2:0001:1: ps_mode=1 ps_state=0 [65271.281497] mwifiex_sdio mmc2:0001:1: Ignore scan. Card removed or firmware in bad state [65271.290880] mwifiex_sdio mmc2:0001:1: ===mwifiex driverinfo dump start=== [65271.317907] mwifiex_sdio mmc2:0001:1: info: MWIFIEX VERSION: mwifiex 1.0 (16.92.21.p76) [65271.326650] mwifiex_sdio mmc2:0001:1: scan failed: -14 [65271.350746] mwifiex_sdio mmc2:0001:1: SDIO register dump start [65271.369462] mwifiex_sdio mmc2:0001:1: SDIO Func0 (0x0-0x9): 43 03 02 02 03 02 00 02 03 00 [65271.385505] mwifiex_sdio mmc2:0001:1: SDIO Func1 (0x10-0x17): 00 00 00 00 00 00 e0 ff [65271.396619] mwifiex_sdio mmc2:0001:1: SDIO Func1: (0x8) c3 (0x58) 00 (0x5c) 48 (0x5d) 00 (0x60) 07 (0x61) 0c (0x62) 00 (0x64) 10 (0x65) 00 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a) 00 [65271.416154] mwifiex_sdio mmc2:0001:1: SDIO Func1 (0xe8-0xf2): dc fe 7e 00 62 00 3f a7 24 14 70 [65271.580586] mwifiex_sdio mmc2:0001:1: SDIO Func1 (0xe8-0xf2): dc fe 8f 00 73 00 3f a7 24 14 70 [65271.594858] mwifiex_sdio mmc2:0001:1: SDIO register dump end [65271.610712] mwifiex_sdio mmc2:0001:1: ===mwifiex driverinfo dump end=== [65271.628592] mwifiex_sdio mmc2:0001:1: == mwifiex firmware dump start == [65271.666427] mwifiex_sdio mmc2:0001:1: Fail to pull ctrl_data [65271.676062] mwifiex_sdio mmc2:0001:1: firmware dump failed [65271.693018] mwifiex_sdio mmc2:0001:1: == mwifiex dump information to /sys/class/devcoredump start [65271.710201] mwifiex_sdio mmc2:0001:1: == mwifiex dump information to /sys/class/devcoredump end [65271.723737] mwifiex_sdio mmc2:0001:1: PREP_CMD: FW is in bad state [65271.735173] mwifiex_sdio mmc2:0001:1: info: shutdown mwifiex... [65271.769056] mwifiex_sdio mmc2:0001:1: PREP_CMD: card is removed [65271.812192] mwifiex_sdio mmc2:0001:1: PREP_CMD: card is removed [65271.855652] Bluetooth: hci0: Frame reassembly failed (-84) [65271.870925] Bluetooth: hci0: Frame reassembly failed (-84) [65271.967852] Bluetooth: hci0: Frame reassembly failed (-84) [65272.068050] Bluetooth: hci0: Frame reassembly failed (-84) [65272.168010] Bluetooth: hci0: Frame reassembly failed (-84) [65272.268029] Bluetooth: hci0: Frame reassembly failed (-84) [65272.368215] Bluetooth: hci0: Frame reassembly failed (-84) [65272.468007] Bluetooth: hci0: Frame reassembly failed (-84) [65272.567994] Bluetooth: hci0: Frame reassembly failed (-84) [65272.668015] Bluetooth: hci0: Frame reassembly failed (-84) [65272.768055] Bluetooth: hci0: Frame reassembly failed (-84) [65272.839448] mwifiex_sdio mmc2:0001:1: info: FW download over, size 622240 bytes [65273.607175] mwifiex_sdio mmc2:0001:1: WLAN FW is active [65273.641454] mwifiex_sdio mmc2:0001:1: Unknown api_id: 5 [65273.687228] mwifiex_sdio mmc2:0001:1: info: MWIFIEX VERSION: mwifiex 1.0 (16.92.21.p76) [65273.713221] mwifiex_sdio mmc2:0001:1: driver_version = mwifiex 1.0 (16.92.21.p76) [65277.145122] mwifiex_sdio mmc2:0001:1: info: trying to associate to bssid ca:39:a3:cb:ad:7e [65278.668157] mwifiex_sdio mmc2:0001:1: ASSOC_RESP: failed, status code=2 err=0xfffc a_id=0x3fff [65278.677711] mwifiex_sdio mmc2:0001:1: assoc failure: reason CONNECT_ERR_ASSOC_ERR_TIMEOUT [65278.691251] mwifiex_sdio mmc2:0001:1: ASSOC_RESP: AUTH timeout [65278.710528] mwifiex_sdio mmc2:0001:1: info: association to bssid ca:39:a3:cb:ad:7e failed [65279.781236] mwifiex_sdio mmc2:0001:1: info: trying to associate to bssid ca:c6:5c:cb:ad:7e [65281.310722] mwifiex_sdio mmc2:0001:1: ASSOC_RESP: failed, status code=2 err=0xfffa a_id=0x3fff [65281.320307] mwifiex_sdio mmc2:0001:1: assoc failure: reason Unknown connect failure I found same issue on below github link but it show it is still open https://www.bing.com/ck/a?!&&p=6f8995a9ee8bc78d51549c45a34f5deee2c26e49fb129fa9306c277b1df3c48cJmltdHM9MTc5MDQ2NzIwMA&ptn=3&ver=2&hsh=4&fclid=28fe8c6f-37d9-6a8e-3ad5-9b0736ee6b90&psq=wifi+driver+crashes+while+trying+to+reconnect+-+88w8997&u=a1aHR0cHM6Ly9naXRodWIuY29tL254cC1pbXgvaW14LWZpcm13YXJlL2lzc3Vlcy81 thanks in advance Re: wifi driver crashes- 88w8997 Hi, Thank you for the detailed logs. Based on the crash information, we can see you are running firmware version 16.92.21.p76. Please note that the 88W8997 is no longer included in the standard imx-firmware releases. However, we have a dedicated hotfix branch with the latest firmware available here: https://github.com/nxp-imx/mwifiex/tree/hotfix/lf-6.12.49_2.2.0_hotfix_w8997 https://github.com/nxp-imx/imx-firmware/tree/hotfix/lf-6.12.49_2.2.0_hotfix_w8997 We recommend upgrading to the firmware available in that branch, which is significantly newer than your current version and includes stability fixes that may address the command timeout and firmware bad state issue you are experiencing. Regards, Daniel. Re: wifi driver crashes- 88w8997 DanielRuvalcaba thanks for the support. We loaded the hotfix firmware on the combo chip and ran it continuously for approximately one week. During this period, we encountered a different issue. Unlike the previous problem where the Wi-Fi firmware crashed, this time the Wi-Fi functionality remained operational, but BLE stopped working after 3-4 days of continuous operation. The BLE failure was not recoverable by simply resetting the HCI interface. To restore BLE functionality, we had to reload the firmware on the combo chip. We have attached the latest logs captured during the BLE failure for further analysis. [308423.524163] Bluetooth: hci0: command 0x0406 tx timeout [308454.723609] Bluetooth: hci0: command 0x2011 tx timeout [308454.728959] Bluetooth: hci0: Opcode 0x2011 failed: -110 [308454.734354] Bluetooth: hci0: Unable to add to allow list: -110 [308456.771606] Bluetooth: hci0: Opcode 0x200b failed: -110 [308456.776986] Bluetooth: hci0: command 0x200b tx timeout [308456.782265] Bluetooth: hci0: start background scanning failed: -110 [308458.819547] Bluetooth: hci0: Opcode 0x2011 failed: -110 [308458.824925] Bluetooth: hci0: command 0x2011 tx timeout [308458.830210] Bluetooth: hci0: Unable to add to allow list: -110 [308460.867534] Bluetooth: hci0: Opcode 0x200b failed: -110 [308460.872908] Bluetooth: hci0: command 0x200b tx timeout [308460.878263] Bluetooth: hci0: start background scanning failed: -110 [308462.915455] Bluetooth: hci0: Opcode 0x2011 failed: -110 [308462.920957] Bluetooth: hci0: command 0x2011 tx timeout [308462.926341] Bluetooth: hci0: Unable to add to allow list: -110 [308464.963435] Bluetooth: hci0: Opcode 0x200b failed: -110 [308464.968817] Bluetooth: hci0: command 0x200b tx timeout [308464.974104] Bluetooth: hci0: start background scanning failed: -110 [308467.747431] Bluetooth: hci0: command 0x200a tx timeout Thanks in advance.
View full article
'examples/freemaster_examples/fmstr_example_pdbdm' 中的应用程序命令问题 各位 已下载 sdk.sdk_2.x_lpcxpresso54114仅提供 FreeMASTER 示例。除了应用程序命令部分之外,其他方面都运行正常,而我在应用程序命令部分发现了一些奇怪的行为。 更多详情已发布在 GitHub 上,链接如下: https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10 祝好 Paolo Re: Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm 您好,如果我理解正确的话,您不明白为什么示例应用程序中的命令 0x10 返回代码 16。 命令 0x10 已注册为回调函数: 因此,当FreeMASTER探测到命令执行时,函数“my_appcmd_handler”会自动被调用。这个回调函数的示例代码非常简单: 这就是为什么你会得到返回代码 16 (=0x10) 作为答案的原因。 我也确认 FreeMASTER 存在一个问题,即对于未知响应,无法显示消息,正如您报告的 app.command(ID 为 0x02)的问题一样。响应 0xcd 应该报告为“未知响应”,但实际上并未生成任何消息。 谢谢, 米哈尔
View full article
Coupon not valid for FRDM-MCXN236 NXP Website advertised this free board to get started . But the coupon code is still not working during checkout even though the product is in stock.  Evaluation Board Re: Coupon not valid for FRDM-MCXN236 Hello PLACEHOLDER7 In this case, please kindly send an email to our shopping cart team by [email protected]. The team is in charge of online orders. Thanks for understanding Becky
View full article