In
Tutorial 1, the AI agent imported the GPIO Blinking LED Demo and ran it on the
FRDM-A-S32K312 board. This second article extends that project with two new features: a multi-color LED sequence, and a UART output that reports what the board is doing.
Using S32 Configuration Tools, you will map LPUART6 pins (PTA15 / PTA16), configure the peripheral at 115200 baud, regenerate code, and flash the firmware so the board echoes the current LED color over UART to a serial terminal.
Estimated time: ~20 minutes.
System Architecture
Add UART to the Imported Project – system architecture overview
The components involved are:
FRDM-A-S32K312 – Target evaluation board. Runs GPIO Blinking LED firmware with LPUART6 enabled on PTA15 (RX) / PTA16 (TX). Transmits the current LED color over UART at 115200 baud.
Host PC – Runs S32 Design Studio and the S32 Design Studio AI Support. A serial terminal (e.g. VS Code Serial Monitor) receives and displays the LED colour echo at 115200 / 8N1.
Prerequisites
What you need before starting
- Tutorial 1 completed — the GPIO Blinking LED Demo for FRDM-A-S32K312 must already be imported and building in S32 Design Studio
- One FRDM-A-S32K312 evaluation board + USB cable
- A serial terminal application (e.g. PuTTY, Tera Term, or VS Code Serial Monitor)
- S32 Design Studio AI Support configured (download, install and configure it following the steps from Installation & Usage Guide)
Note: This tutorial uses these paths:
- Installation: C:\NXP\2026\K3_kit\S32DS_3.6.8
- Workspace: C:\NXP\2026\K3_kit\workspace_S32DS_3.6.8_K3_kit
You can use any location. If you do, update the paths in the prompt to match.
Connect the FRDM-A-S32K312 board to the PC via USB. Open Device Manager → Ports and note the virtual COM port number – you will need it for the serial terminal.
Steps
Send the following prompts to your AI assistant in order. Each prompt is a complete, self-contained instruction.
Step 1 – Add RGB LED cycling (red → green → blue)
In S32DS, use the dm-gpio-blinky-s32k312 project on a S32K312 FRDM board.
Add pins PTA30 and PTA31 in the Pins tool (green and blue of the on-board RGB LED; red is the existing PTA29).
In the existing blink cycle where the red LED is toggled, replace it with a switch-case that lights one color at a time, cycling red -> green -> blue, ~500 ms each.
Important: these RGB LEDs are active-low. Confirm the polarity from the board schematic/user guide before writing GPIO values. Map: red=PTA29, green=PTA30, blue=PTA31.
Then generate code and build (report any errors) and flash/run it.
Use the s32ds-agentic-ai MCP server for all IDE/config/flash actions; if the MCP server disconnects at any point, stop immediately and notify me.
AI will:
- Open Pins Tool and add PTA30 (green) and PTA31 (blue) alongside existing PTA29 (red)
- Replace the existing blink loop with a switch-case cycling red → green → blue, ~500 ms each
- Respect active-low polarity, confirmed from board schematic/user guide
- Click Generate Code, build and report any errors
- Flash and run the firmware on the FRDM-A-S32K312 board
- Stop and notify the user immediately if the s32ds-agentic-ai server disconnects
Step 2 – Add UART functionality to echo the LED colour
Add UART functionality to echo the color of the LED (RED, GREEN, BLUE) but keep it lightweight by using the LPUART IP-layer:
- In Pins tool: map the PTA15 as LPUART6_RX and PTA16 as LPUART6_TX pins
- In Peripherals tool: set LPUART_6 channel configured for baudrate 115200 / 8 data bits / no parity / 1 stop bit
Then generate code and build (report any errors) and flash/run it.
Use the s32ds-agentic-ai MCP server; if the MCP server disconnects at any point, stop immediately and notify me.
AI will:
- Open Pins Tool and map PTA15 → LPUART6_RX and PTA16 → LPUART6_TX
- Open Peripherals Tool and configure LPUART6: 115200 baud / 8 data bits / no parity / 1 stop bit
- Click Generate Code, build and report any errors
- Flash and run the firmware on the FRDM-A-S32K312 board
- Stop and notify the user immediately if the s32ds-agentic-ai server disconnects
Verifying the Result
Work through this final check to confirm that both prompts completed successfully.
Final check
- Build completes with zero errors.
- Firmware is flashed and running on the FRDM-A-S32K312 board (RGB LED is blinking).
- Open a serial terminal at 115200 baud / 8N1 on the board's COM port.
- Confirm messages such as LED: RED, LED: GREEN, LED: BLUE appear in sync with the physical LED colour changes.
Troubleshooting
| Symptom |
Fix |
| No UART output in serial terminal |
Open Pins Tool. Confirm PTA15 → LPUART6_RX and PTA16 → LPUART6_TX are routed. Regenerate code after any change. |
| LPUART6 not found or not initialised |
Open Peripherals Tool. Verify LPUART6 is enabled and configured: 115200 baud / 8 data bits / no parity / 1 stop bit. Regenerate code if you make changes. |
| LPUART6 absent at runtime |
Open Peripherals Tool › McuPartition. Enable LPUART6 in the partition configuration, then regenerate and rebuild. |
| Garbled characters in serial terminal |
Baud rate mismatch. Confirm the terminal is set to 115200 and the peripheral configuration matches. Regenerate code after any baud rate change. |
| Build errors after Generate Code |
Check that the generated LPUART6_init() call is present in main.c and that the correct header is included. Re-run Generate Code if source files are missing. |
| LED colour not echoed over UART |
Confirm the UART transmit call is placed after each LED colour change in the main loop. Verify LPUART6_init() is called before the loop starts. |
| Wrong COM port in serial terminal |
Open Device Manager → Ports and identify the virtual COM port assigned to the FRDM-A-S32K312 board. Use that port number in your terminal application. |
| s32ds-agentic-ai server disconnects during operation |
Stop immediately and restart the MCP server following the setup instructions. Do not continue until the server is confirmed connected. |
File Reference
| File |
Step |
Description |
| src/main.c |
2 |
Main firmware file — contains LED loop and LPUART6 transmit calls |
| generate/src/Lpuart_Uart_Ip_PBcfg.c |
1 |
Generated LPUART6 peripheral configuration |
| generate/include/Lpuart_Uart_Ip_Cfg.h |
1 |
Generated LPUART6 configuration header |
| *.mex |
1 |
S32 Configuration Tools project file (Pins, Clocks, Peripherals) |
Map the pins, configure LPUART6 and regenerate – your board now reports every LED colour change over UART in about 20 minutes.