Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on specific Device: S32K312 Toolchain: Green Hills ELXR (compiler) HSE Firmware: s32k312_hse_fw_0.13.0_2.55.0_pb250129.bin Debugger: Lauterbach TRACE32 Software: AUTOSAR RTD-based Bootloader (FBL) + Application (APP), two-image structure ISSUE SUMMARY On a subset of production units, the CPU hangs immediately after a Functional (software) reset. The same units always boot correctly after a Destructive (power-on) reset. The hang does not reproduce on our reference/known-good units. EVIDENCE THAT AN NMI OCCURS BEFORE ANY APPLICATION CODE EXECUTES 1) CPU context captured at the hang point (auto-stacked exception frame): - R0-R3 = 0x00000000, R12 = 0x00000000 - LR = 0xFFFFFFFF (reset default -> no BL has executed yet) - PC = 0x00416904 (the very first instruction address of our Reset_Handler) - xPSR = 0x01000000 2) SCB->ICSR = 0x00000802 Chibeom_3-1785136456875.pngChibeom_3-1785136456875.pngChibeom_3-1785136456875.png - VECTACTIVE[8:0] = 2 -> NMI is the currently active exception - RETTOBASE = 1 This confirms the CPU is currently executing inside the NMI handler. 3) Our vector table entry for the NMI offset correctly points to our own default exception handler, so this is a genuine NMI event, not vector table corruption. REGISTERS CHECKED AT THE SAME HANG STATE (all read as clean / inactive) - MC_RGM_DES = 0x00000000 (not a destructive reset) - MC_RGM_FES = 0x20000000 (bit 29 only) (only "software functional reset" flag set, no other functional reset source flagged) - FCCU: STAT, N2AF_STATUS, A2FF_STATUS, N2FF_STATUS, NCF_S0, IRQ_STAT all = 0x00000000 - CMU_FC instances 0, 3, 4: SR = 0x00000000 (no frequency high/low fault) - PMC LVSC = 0x00000000 (no LVD/HVD flag, latched or live) - ERM (0x4025C000): could not be read on either good or failing units (likely clock-gated in our configuration), so ERM status is unverified. QUESTIONS 1. Are there any NMI sources -- other than FCCU / CMU_FC / PMC / MC_RGM -- that could fire before the application's Reset_Handler executes its first instruction? 2. Since the HSE subsystem runs independently of the application core, is it possible for an application-core Functional reset (which does not reset HSE) to create a state mismatch that triggers an NMI on the application core? 3. Is there a known errata for S32K312 matching this symptom (NMI only on functional/software reset, never on power-on reset)? Any guidance on additional registers to check, or documentation covering NMI sources outside FCCU / ERM / CMU_FC / PMC, would be greatly appreciated. Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi @Chibeom, Could you please read registers MU_0.MUB CSSR0 and MU_1.MUB CSSR0 at the hang state, and confirm whether bit 0 (NMIC) is set in either of them? Thank you Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi @danielmartynek , Thank you for pointing us to MU_0.MUB / MU_1.MUB CSSR0. CSSR0 (bit 0, NMIC) on both MU_0.MUB and MU_1.MUB reads 0x00000000 on the failing unit at the hang state, so the MU->NMI request path (CCR0[NMI] / CSSR0[NMIC]) does not appear to be pending. However, while comparing MU registers between a known-good unit and a failing unit (both captured at the identical hang-state address range), we found a consistent difference:                                Good unit Failing unit MU_0.MUB VER 0x0300000F 0x0300000F (identical) MU_0.MUB PAR 0x20200404 0x20200404 (identical) MU_0.MUB CR 0x00000000 0x00000000 (identical) MU_0.MUB SR 0x00000000 0x00000002 <- MURIP set MU_1.MUB VER/PAR/CR: identical between good and failing units MU_1.MUB SR 0x00000000 0x00000002 <- MURIP set So on BOTH MU instances, SR bit 1 (MURIP) is set only on the failing unit, consistently. Per the reference manual, MURIP indicates that "processor A" has issued an MU reset, and can only be cleared by a system reset (not by an MU reset). Since the CPU is frozen inside the NMI handler before executing any application code, it could not have cleared this flag itself, so it must have been set prior to (or as part of) this boot sequence. We'd appreciate your input on the following: 1. For MU_0.MUB and MU_1.MUB, which processor is "processor A" (i.e. who sets MURIP)? Our header only exposes the "MUB" register block at the application-core-accessible address -- does this imply the application core is always "processor B" and HSE is "processor A" for these instances? 2. Does "system reset" (required to clear MURIP) include a Functional/SW reset of the application core, or only a Destructive/POR reset? If MURIP is not cleared by our functional reset, that would explain why it stays set across SW reset while it is clear after power-on. 3. Independent of the NMI question: is a set/stuck MURIP flag itself expected or considered anomalous during normal operation? 4. Since CSSR0[NMIC] currently reads 0, is it possible for hardware to auto-clear NMIC upon NMI exception entry, or does it only clear via an explicit software write (in which case NMIC=0 would mean the MU->NMI channel was never asserted in the first place)? Thanks again for your help so far. Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi @Chibeom, I'm sorry for the delay. I was out of office for two days. 1. Yes, the HSE_B core controls the MUA interfaces of MU_0 and MU_1. 2. Any system reset should reset MURIP. 3. I would consider this an anomaly, as I do not have much information about it. 4. It requires an explicit write, as it is a W1C register. Can you make sure that HSE_B is inactive at the time the functional reset is triggered? Also, what is the state of HSE_B while the application is stuck in the NMI handler? Can you read the standard HSE GPR (0x4039_C028), FSR, and GSR registers on the MU_0 B side? Do you use the NMI pin in the application? Regards, Daniel Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi Daniel, Please find three combined register-dump screenshots attached, followed by our findings organized by your questions. -------------------------------------------------------- ATTACHMENTS -------------------------------------------------------- Attachment 1: GOOD unit (Secure Debug enabled, running normally) Chibeom_3-1785730814252.pngChibeom_3-1785730814252.pngChibeom_3-1785730814252.png Attachment 2: FAILING unit, immediately BEFORE the functional reset is triggered (normal operation) Chibeom_4-1785730831377.pngChibeom_4-1785730831377.pngChibeom_4-1785730831377.png Attachment 3: FAILING unit, AFTER the functional reset, stuck in the NMI handler (hang state) Chibeom_5-1785730838688.pngChibeom_5-1785730838688.pngChibeom_5-1785730838688.png -------------------------------------------------------- FINDINGS 1) HSE_B activity at the time the functional reset is triggered, and 2) state of HSE_B while stuck in the NMI handler: Comparing Attachment 2 (before reset) and Attachment 3 (after reset, hang state) on the failing unit, every register we checked reads IDENTICALLY before and after the reset: - MU_0.MUB / MU_1.MUB TSR = 0x0000000F, RSR = 0x00000000 (no pending messages on transmit/receive channels, unchanged by the reset) - MU_0.MUB GSR = 0x00000000 (unchanged) - MU_0.MUB FSR = 0x03600000 (unchanged) - HSE GPR (0x4039C028) = 0x000001C1 (unchanged) - MU_0.MUB / MU_1.MUB SR bit 1 (MURIP) = 0x00000002 -- already set BEFORE the reset is triggered, and remains set, unchanged, after the reset So MURIP was already set prior to this reset cycle, and the functional reset itself does not change any of these HSE-related registers. For reference, on a good unit with the same Secure Debug configuration (Attachment 1), MURIP reads 0x00000000 on both MU_0.MUB and MU_1.MUB, while HSE GPR and WKPU NCR read the same values as the failing unit. 3) Regarding whether a set/stuck MURIP is anomalous: Understood, thank you for confirming. 4) NMI pin usage: We do not use the WKPU-routed NMI path (WKPU_IP_USED is not enabled; no WKPU driver code is compiled into either our bootloader or application image). WKPU NCR (0x402B4008) = 0x60000000 identically across all three attachments. NSR = 0x00000000 in all cases. Since this is unchanged across all units and conditions, we don't believe an external/WKPU-routed NMI source is involved. SUMMARY OF FINDINGS SO FAR MURIP (MU_0.MUB and MU_1.MUB SR bit 1) is already set on the failing unit BEFORE the functional reset is even triggered, and remains unchanged throughout the hang. It reads 0 on a good unit with the same Secure Debug configuration. This is the only consistent, reproducible difference we have found across every register we've compared (FCCU, CMU_FC, PMC, WKPU, and MU CSSR0/GSR/TSR/RSR/GPR/FSR). Since MURIP is set by "processor A" (HSE_B) and should be cleared by "any system reset" per your answer, and since it is already set before our functional reset is triggered (and the reset itself does not appear to change it), this suggests HSE_B issued an MU reset at some earlier point that was never cleared by a "system reset" recognized by HSE_B. QUESTIONS 1. Is there a way to determine, from the HSE side, what would cause HSE_B (processor A) to issue an MU reset in the first place? We'd like to understand why MURIP gets set at all. 2. Is there a recommended way for us to trigger a reset that HSE_B recognizes as a "system reset" (to clear MURIP) from application software, short of a full power cycle? 3. Could a stuck MURIP flag on the application-core side be related to the NMI we are observing, or are these more likely two independent symptoms of the same earlier event? Thanks again for your continued help with this. Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hello @Chibeom, Thank you for the detailed register dumps. I have escalated the questions around MURIP behavior and the potential NMI path between HSE_B and CM7_0 to our internal HSE team, as this seems to be not documented. I will get back to you once I have their input. Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hello @danielmartynek,  Thank you for the update, and for escalating the MURIP / NMI path question to your internal HSE team. We appreciate it, and we'll wait for their input. In the meantime, we found an additional data point that may be relevant, so we wanted to share it now rather than wait. While comparing OTP fields in the UTEST Flash area between a good unit and a failing unit, we found a difference in the Lifecycle slots. CUST_DEL (0x1B000220-22F) and OEM_PROD (0x1B000230-23F) are identically programmed (0x55AA50AF across all words) on both the good unit and the failing unit. The difference is in the IN_FIELD slot (0x1B000240-24F): - Good unit: begins being programmed Chibeom_2-1786069927793.pngChibeom_2-1786069927793.pngChibeom_2-1786069927793.png - Failing unit: reads as unprogrammed (0xFFFFFFFF) Chibeom_1-1786069910918.pngChibeom_1-1786069910918.pngChibeom_1-1786069910918.png We are still double-checking the exact byte pattern within the IN_FIELD slot on our side, but the good/failing difference at this slot appears consistent. Could you clarify: 1. Does this suggest that the failing unit's configuration became corrupted or incomplete partway through the transition into IN_FIELD? 2. Could an incomplete or missing lifecycle advancement to IN_FIELD explain the NMI/hang behavior we have been investigating in this thread? 3. Is there a safe way to check or complete this lifecycle advancement on the failing units, without a full production re-flow? Thanks again for your help. Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi @Chibeom, Based on the memory view, OEM_PROD = Inactive, IN_FIELD = Erased. Can you please first read the DCM registers: RM, rev.12, Section 39.3.1 DCM memory map. And Section 38.2.3 Read-Only GPR On Destructive Reset 3 (DCMROD3)? You can also use the HSE_FW APIs to get the LC attribute? Thank you Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi @danielmartynek , Thank you for pointing us to the DCM memory map and DCMROD3. We captured DCMSTAT (0h), DCMLCS (8h), DCMLCS_2 (80h), and DCMROD3 (208h) on both units, and decoded them against RM rev.9. ---------------------------------------------------- CAPTURED VALUES ---------------------------------------------------- Good unit: Chibeom_0-1786500129171.pngChibeom_0-1786500129171.pngChibeom_0-1786500129171.png - DCMSTAT (0h) = 0x00000E11 - DCMLCS (8h) = 0x00000000 - DCMLCS_2 (80h) = 0x00000000 - DCMROD3 (208h) = 0x00000000 Failing unit: Chibeom_1-1786500144600.pngChibeom_1-1786500144600.pngChibeom_1-1786500144600.png - DCMSTAT (0h) = 0x00000E03 - DCMLCS (8h) = 0x06184104 - DCMLCS_2 (80h) = 0x00000006 - DCMROD3 (208h) = 0x00400000 ---------------------------------------------------- DECODED FIELDS (FAILING UNIT ONLY, since good unit reads all-zero) ---------------------------------------------------- DCMSTAT: - bit1 DCMERR = 1 (DCM completed with error) -- good unit has this bit = 0 - bit4 DCMLCST = 0 (LC scanning status not "completed successfully") -- good unit has this bit = 1 DCMLCS: - bits 21-19 DCMLCC4 (IN_FIELD Marking) = 011b = "Region is erased/virgin" - bits 15-13 DCMLCC3 (OEM_PROD Marking) = 010b = "Marked as inactive" - bits 27-25 DCMLCC5 (Pre-FA Marking) = 011b = "erased/virgin" - All associated *_ECE/*_CFE/*_CSS bits = 0. DCMLCS_2: - bits 3-1 DCMLCC6 (FA Marking) = 011b = "erased/virgin" DCMROD3: - bit22 LC_ERR = 1 ("Error In Life Cycle Scanning") This is consistent with the UTEST OTP dump we shared earlier: the IN_FIELD slot on the failing unit reads as erased/virgin. ---------------------------------------------------- HSE_FW API RESULT (HseReadLifecycle) ON THE FAILING UNIT ---------------------------------------------------- HseReadLifecycle() returns 0x10 = HSE_LC_IN_FIELD. So from the HSE firmware's point of view, the current lifecycle is already IN_FIELD. This appears to conflict with the DCM/OTP data above: DCM's DCMLCC4 field reads IN_FIELD marking as "erased/virgin," and the UTEST OTP IN_FIELD slot (0x1B000240h onward) reads as unprogrammed (0xFFFFFFFF), yet the HSE API reports the lifecycle as confirmed IN_FIELD. We wanted to share this as-is rather than draw a conclusion, since we don't know whether HSE tracks lifecycle through a separate/secure store independent of the DCM flash marking, or whether this indicates the marking itself is the problem. Regards, Chibeom Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hello @Chibeom, Thanks for the data. Since the IN_FIELD slot is still in the erased state, could you try setting the attribute again to advance it? As I mentioned, the case is currently under internal discussion. I will update this thread as soon as I have any new information. Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi @Chibeom, Probably the HSE service responsible for advancing the Life Cycle (LC) was interrupted, leaving the LC in this state. The LC and LC Control (DCMLCC) register reports 0x77 (IN_FIELD) as the HSE_FW does, but the UTEST area is not programmed correctly. In theory, you could program the UTEST IN_FIELD slot using a debugger, which should clear the DCM error.  Regards, Daniel Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hello @danielmartynek  We tried setting the IN_FIELD attribute again on the failing unit, as suggested. Result: HSE_SRV_RSP_NOT_ALLOWED (0xAA55A21C) Regards, Chibeom Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi @danielmartynek  Thank you for the suggestion to program the UTEST IN_FIELD slot using a debugger. We checked our internal OTP field reference table, and the IN_FIELD lifecycle slot (1B00_0240-024F) is listed as write-protected for any master except HSE once LC > MCU_PROD (OEM_PROD). Since HseReadLifecycle() on this unit already reports IN_FIELD, this LC condition appears to already be met. Could you clarify how a debugger write to this slot would be expected to succeed under this protection rule? Is there a specific procedure, mode, or authentication step required for the debugger to be treated as an allowed master in this case? Separately, do you have any findings yet on why the LC advancement to IN_FIELD was left in this partial state in the first place? We'd like to understand the root cause, not just the recovery step, if that analysis is available. Thank you, Chibeom Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci Hi @Chibeom, Thank you for the information. It seems there is no option to recover the MCU at this point. One possibility is that the HSE set attribute service request to advance the LC was interrupted by a system reset (I understand the LC was not advanced using the LCW within the IVT).: Do you read the HSE response of the service request? Do you log whether there was an error? Before triggering the service, do you verify that HSE_STATUS_INIT_OK is set? How many boards/MCUs are affected by this issue? Is it limited to a few units, or have you observed it across a larger number of devices? Thank you, Daniel
記事全体を表示
How to transfer/re-register an S32 Design Studio license to my own NXP account Hello, Dear Support Team, That is Second Message  ( First : https://community.nxp.com/t5/MPC5xxx/Request-for-Software-License-Extension-Due-to-Expiration/m-p/2396968#M28490 ) I inherited my work PC from my former manager, and S32 Design Studio is still activated under his NXP account, not mine. Because of this, the installed license appears to have expired on my machine. I have confirmed that my own license is valid until 2028, so I would like to switch S32DS on this PC over to my NXP account and license instead of the previous owner's. Could you let me know the correct procedure for this? Specifically: 1. Is there a way to deactivate or release the existing activation tied to the previous account? 2. Can I simply re-activate S32DS with my own account credentials, or is a full uninstall and clean reinstall required? Thank you for your help. Best regards, Re: How to transfer/re-register an S32 Design Studio license to my own NXP account Hi,  you can use the old activation code from previous user. The activation code is not connected to specific account.  You can re-activate existing installation with the old code. 
記事全体を表示
DPAA2 DPDK RTE フロー こんにちは、 DPAA2 SolidRun LX2160A Clearfog CX上でDPDK RTE FLOWを作成しようとしていますが、うまくいきません。 動作しないのは普通のことですか? うまくいくには何ができるでしょうか? 私はNXP DPAA2やNXP全般についてかなり初心者なので、技術的な言葉を教えてもらえますか? ありがとうございます。 testpmd> flow create 0 ingress pattern eth / ipv4 / end actions rss queues 0 1 end types ip ipv4 end / end DPAA2_NET: Add entry(0) to table(0) failed DPAA2_NET: Create flow failed (-22) port_flow_complain(): Caught PMD error type 1 (cause unspecified): cause: 0xfffff340a300, unknown: Operation not permitted Re: DPAA2 DPDK RTE FLOW DPDKポートの背後にあるDPNIがどのように作成されたかを確認してください。基板上のLinuxシェルから: restool dprc show dprc.1 --resources # DPDKポートが使用するdpni.Xを見つけます restool dpni info dpni.X # "options" 行と "num_queues" を確認してください オプションに DPNI_OPT_NO_FS が表示される場合、または DPNI_OPT_HAS_KEY_MASKING が表示されない場合は、それが問題の原因です。 適切なオプションを使用してDPNIを再作成します。dynamic_dpl.sh を編集するか、(または読み取る環境 — NXP LSDK では通常 DPNI_OPTIONS 変数です)なので、Create コールは次のようになります: restool dpni create \ --options=DPNI_OPT_HAS_KEY_MASKING \ --num-queues=2 \ --num-tcs=1 \ --container=dprc.2 要点: DPNI_OPT_NO_FSを含めないでください。 DPNI_OPT_HAS_KEY_MASKINGを含めてください。 --num-queuesをRSSアクションが参照するキューの数に設定してください(キュー0と1を指定したので、2≥です)。 次に、その DPNI を DPDK コンテナにアタッチし (restool dprc assign …)、testpmd を再実行します。 静的DPLファイルを使用する場合は、同じファイルをdpni@Xノードに追加してください。 dpni@1 { オプション = "DPNI_OPT_HAS_KEY_MASKING"; num_queues = <2>; ... }; そして、U-Bootでfsl_mc apply dpl …を使用してDPLを再フラッシュします。 まずはもっと簡単なルールで妥当性を確認してみましょう。RSSの前に、プレーンステアリングが正常に動作することを確認してください。 testpmd> flow create 0 ingress pattern eth / ipv4 src is 10.0.0.1 / end \ アクションキューインデックス 1 / 終了 これが成功してもRSSバリアントが失敗する場合は、残りの問題はDPNIオプションではなく、キュー数/配信構成です。 Re: DPAA2 DPDK RTE FLOW https://www.nxp.com/webapp/Download?colCode=DPAA2UM&location=null DPAA2ユーザーマニュアルが役立つかもしれません ちなみに。どのようなBSPやSDKが使われていますか?公式ウェブサイトからの情報源はありますか?
記事全体を表示
PN7642のRFデバッグ信号の設定方法 PN7642のデータシートを確認したところ、このチップにはAPIを介してデジタルおよびアナログのデバッグ信号を観測するための設定機能があることが分かりました。そこで、評価ボードを使って設定を試みたところ、SDK(PN76_Testbus.h)に該当するAPIが見つかりました。しかし、その.hファイルの説明だけでは、これらのAPIの使い方が分かりません。例えば、観測したい信号を確認するには、どのようなパラメータを渡せば良いのでしょうか?このシナリオに関する関連資料はありますか? 回复: PN7642 RF Debug Signals如何设置 image.jpg   こんにちは。ご指摘いただいたファイルの中に画像(CTS_TESTBUS_Signals.png)を見つけましたが、この画像のデジタル信号がPN7642のデータシートのデジタル信号と完全に一致していないことに気づきました。完全な対応表を入手するにはどうすればよいでしょうか? 回复: PN7642 RF Debug Signals如何设置 image.jpg   image.jpg   image.jpg   こんにちは。このドキュメントは以前にも読んだことがありますが、明確な説明がありません。例えば、ドキュメントを読み返しても、ADC IQ信号やその他のデジタル/アナログ信号を出力するために、これらのAPIにどのようなパラメータを渡せばよいのかがまだよく分かりません。 回复: PN7642 RF Debug Signals如何设置 SDKの「doc」フォルダの下に「PN76-FW-apiguide」があります。 回复: PN7642 RF Debug Signals如何设置 受け取りました、ありがとうございます。 回复: PN7642 RF Debug Signals如何设置 残念ながら、これについて詳しく説明した公開ドキュメントは存在しません。 NXPはUM11566で追加情報を提供しており、これにはTestBusの選択レジスタと値レジスタに関するレジスタ情報が含まれています。この文書はNDAの下で行われているため、アクセスは制限されています。 この情報が必要な場合は、NXPとの間でNDA(秘密保持契約)の手続きを完了してください。NDA承認後、文書はNXPウェブサイトの PN7642製品ページの 「ドキュメント」セクションの「Secure」セクションからダウンロードできます。
記事全体を表示
CGM-RD (UM12423) — NHS2634 が割り込みピンをアサートせず、NHS2x34_Init() が永久にハングアップする NHS2x34_Init() は、NHS2634 の割り込みピンがハイになるのを無期限に待機してハングアップします。これがハードウェアの問題なのか、電源供給シーケンスの問題なのか、それともファームウェアの設定の問題なのかを判断するのにご協力をお願いします。 イベント情報の順序: 1. NHS2634_HOSTIF_InitSpiAndInterrupt() が実行され、成功を返します。 2. NHS2x34_PMC_ResetAFE() が呼び出されます。これは、PMC制御レジスタへのSPI書き込み(AFEリセットビットの設定)を実行します。成功(ステータス=0)を返します。 3. その後、コードは次のループで待機し、チップがSPIコマンドを受け入れる準備ができたら割り込みピンをハイにするのを待ちます。このループは決して終了しない。 while (!NHS2634_HOSTIF_GetInterruptPinLevel()) { } 既に実行された診断: 1. SEGGER RTT ログにより、ループが実際に回転していること (ライブ ポーリング カウンターが継続的に数千万まで増加していること) が確認され、フリーズしたりクラッシュしたりしていないことが確認されました。CPUは動作しており、ピンを積極的に再チェックしています。 2. デバッガ(J-Link/GDB)を接続し、ループの途中で2回停止しました。プログラムカウンタはNHS2634_HOSTIF_GetInterruptPinLevel()の中にあり、GPIO_PinRead()を2回呼び出しており、アクティブポーリングと一致している。 3. PMC制御レジスタに書き込みを行った直後に、その内容を読み戻してください。リセットビットと書き込み保護バイトを反映したゼロでないパターンを期待していましたが、返0x00000000されました。 4. 生のSPIループバックテストを実行しました(MOSIからMISOへのショートをセンサーコネクタに直接接続し、NHS2634モジュールを完全に切り離しました)。送信したバイトのエコーではなく、特徴的なテストパターンに対して0x00000000が返ってきた。 5. 上記の手順をNHS2634モジュールを完全に取り外した状態で繰り返した。結果はコネクテッド時と全く同じでした。 私が明らかにしようとしていること: 私はNXPが提供する公式SDKを使っており、ドライバーコードは変更していません。これがハードウェアの問題なのか、電源供給シーケンスの問題なのか、それとも私の側のファームウェア設定の問題なのか、また、これが私のユニット固有のハードウェア障害のように見えるのかどうかを判断する必要があります。 次にどこを調べれば良いか、何かアドバイスをいただけるとありがたいです。 MCU-リンク-PRO、 MCUXPRESSO-VSC、 血液グルコースモニター  @nxp 、 @nxp5 通信・制御(I3C |I2C |SPI |FlexCAN |イーサネット |FlexIO) MCXA MCX C MCX N パッケージとIO|GPIO パワー Re: CGM-RD (UM12423) — NHS2634 never asserts INTERRUPT pin, NHS2x34_Init() hangs forever SPIループバックが0x00を読み取れなかったため、ホストマイクロコントローラのSPIペリフェラル/ GPIO ルーティング は 実際には データを 転送していません ホストピン の 多重接続 、クロック、GPIO初期化 を修正してください
記事全体を表示
How to configure PN7642 RF Debug Signals While reviewing the PN7642 datasheet, I discovered that the chip provides configuration for observing digital and analog debug signals via APIs. I then tried to configure it using an evaluation board and found the corresponding API in the SDK (located in PN76_Testbus.h). However, based solely on the description in that .h file, I don't know how to use these APIs. For example, what parameters should I pass in to observe the signals I want to see? Are there any relevant documents for this scenario? 回复: PN7642 RF Debug Signals如何设置 image.jpg   Hello, I found an image (CTS_TESTBUS_Signals.png) in the file you mentioned, but I noticed that the digital signals in this image do not correspond one-to-one with the digital signals in the PN7642 datasheet. How can I obtain the complete mapping table? 回复: PN7642 RF Debug Signals如何设置 image.jpg   image.jpg   image.jpg   Hello, I have read this document before, but it does not provide clear instructions. For example, after reviewing the documentation, I am still unclear about what parameters should be passed to these APIs to output the ADC IQ signals or other digital/analog signals. 回复: PN7642 RF Debug Signals如何设置 Under the "doc" folder in the SDK, there is "PN76-FW-apiguide". 回复: PN7642 RF Debug Signals如何设置 Received, thank you 回复: PN7642 RF Debug Signals如何设置 Unfortunately, we do not have any publicly available documentation that describes this in more detail. NXP provides additional information in UM11566, which includes the register information about the TestBus Select and Value registers. Since this document is under NDA, access is restricted. If you require this information, please complete the NDA process with NXP. After NDA approval, the document can be downloaded from the "Secure" under Documentation section of the PN7642 product page on the NXP website.
記事全体を表示
如何将 S32 Design Studio 许可证转移/重新注册到我自己的 NXP 帐户 你好, 尊敬的技术支持团队: 这是第二条信息 (第一页: https ://community.nxp.com/t5/MPC5xxx/Request-for-Software-License-Extension-Due-to-Expiration/mp/2396968#M28490) 我的办公电脑是我从前任经理那里继承来的,S32 Design Studio 仍然是在他的 NXP 账户下激活的,而不是我的。因此,我电脑上安装的许可证似乎已经过期了。 我已经确认我的许可证有效期至 2028 年,因此我想将这台电脑上的 S32DS 切换到我的 NXP 帐户和许可证,而不是前任所有者的帐户和许可证。 请问正确的操作步骤是什么?具体来说: 1. 是否有办法停用或解除与先前帐户关联的现有激活状态? 2. 我能否使用我自己的帐户凭据重新激活 S32DS,还是需要完全卸载并重新安装? 感谢您的帮助。 顺祝商祺! Re: How to transfer/re-register an S32 Design Studio license to my own NXP account 你好, 您可以使用之前用户的旧激活码。激活码与特定账户无关。 您可以使用旧代码重新激活现有安装。
記事全体を表示
自分のNXPアカウントにS32 Design Studioライセンスを移管/再登録する方法 こんにちは、 サポートチームの皆様、 これは2番目のメッセージです (まずはこちら: https ://community.nxp.com/t5/MPC5xxx/Request-for-Software-License-Extension-Due-to-Expiration/mp/2396968#M28490) 私は元マネージャーから仕事用PCを引き継ぎましたが、S32 Design Studioは私のではなく彼のNXPアカウントでまだ有効化されています。そのため、私のマシンにインストールされているライセンスの有効期限が切れてしまったようです。 自分のライセンスが2028年まで有効であることを確認したので、このPCのS32DSを前の所有者ではなくNXPのアカウントとライセンスに切り替えたいと考えています。 正しい手順を教えてもらえますか?具体的には: 1. 前のアカウントに紐づいた既存のアクティベーションを無効化または解除する方法はありますか? 2. 自分のアカウント認証情報でS32DSを再アクティベートできますか?それとも完全なアンインストールとクリーンインストールが必要ですか? ご協力ありがとうございます。 よろしくお願いいたします。 Re: How to transfer/re-register an S32 Design Studio license to my own NXP account こんにちは、 前のユーザーの古いアクティベーションコードを使うことができます。アクティベーションコードは特定のアカウントにコネクテッドしていません。 古いコードで既存のインストールを再開できます。
記事全体を表示
How does the on-board emulator of the FRDM-A-S32K344 board support comsis-dap or jlink? NXP has launched the FRDM-A-S32K344 universal development board. However, the on-board emulator does not support comsis-dap and jlink, which significantly hinders its use in general applications for Zephyr firmware burning, debugging, and VSCode development. Are there any plans for future support in this regard?
記事全体を表示
旧版软件许可 Codewarrior 10.4.1 你好, 截至 2026 年,是否有办法使用免费许可证在 Power Quicc III 等旧设备上使用 CodeWarrior 10.4.1? Re: Legacy Software License Codewarrior 10.4.1 你好, CodeWarrior for Power Architecture(支持 PowerQUICC III 的工具,例如 MPC85xx 系列)没有免费/特别版。 PowerQUICC III 器件(MPC8540、MPC8548、MPC8560、MPC8572 等)受CodeWarrior Development Studio for Power Architecture v10.x支持,但需要付费许可证(基本版、标准版或专业版套件)。 NXP提供的付费选项包括: CW 开发套件 – 基本版– 最低级别,包括 Power Architecture(Eclipse、Windows 和 Linux 主机),但可能存在代码/数据大小限制。 CW 开发套件 – 专业版– 功能齐全,无大小限制,包含经典和 Eclipse IDE,支持 Linux 和 Windows。 面向网络应用的 CW 开发套件– 专门针对 PowerQUICC I/II/II Pro/III、QorIQ P/T 系列和 Layerscape。   此致
記事全体を表示
SE050 vulnerability reporting   I have a technical support question regarding the SE050. We are bringing a product to market that uses the SE050, and this product will not receive software updates in the field. Under the EU Cyber Resilience Act (CRA), we have an obligation to monitor for vulnerabilities in the components we use and to report actively exploited vulnerabilities and severe incidents within the required timelines.   Could you tell us: - Does NXP operate a vulnerability disclosure or security notification process for the SE050 (e.g. a mailing list, security advisories page, or PSIRT feed) that we could subscribe to or monitor? - How are known vulnerabilities and their status (fixed, mitigated, not applicable) communicated to customers using the SE050, given that this specific product line does not support field updates? - Is there a way to get proactive notifications rather than having to check manually? SE050 Re: SE050 vulnerability reporting Hi @djdirkj , [Product Security Vulnerability | NXP Semiconductors|https://www.nxp.com/support/support/product-security-vulnerability:PSIRT] PSIRT team can be reported of vulnerabilities, they evaluate, find apt solution and communicate to affected buyers of the product - direct customers and distis which then inform their buyers. Errors and mitigiations are documented in errata sheet and user guidance. Anyone can receive updates of these documents by clicking the "receiving alerts" option on the website of the product page to get informed on document updates. Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示
RDK358BMU压力传感器启动时的压力传感器建议。 RD-K358BMU 我正在研究 RDK358BMU 评估板,并计划启动压力传感器。 请您提供以下信息: 1.RDK358BMU推荐使用的压力传感器零件号是多少? 2. NXP 参考设计中是否使用了或验证了特定的压力传感器? 3. 您能否也分享一下传感器接口、连接详情以及启动所需的任何软件配置? 任何与压力传感器与 BMU 集成相关的参考文档或应用笔记都将不胜感激。 Re: Pressure sensor recommendation for RDK358BMU pressure sensor bring-up. 你好@shweta_jagadale , 1. 和 2. RDK358BMU 使用高度集成的电池压力监测传感器 NBP8-9x 。 3. 有关压力传感器的连接和编程的更多信息,请参阅压力传感器数据表。 RD-K358BMU 用户指南还介绍了压力传感器软管接口。 最后,您可以通过我们的汽车软件包管理器找到 RD-K358 (S32K358) 所需的所有相关软件。此外,还有连接到 NBP8 – KE15Z FreeMASTER 演示的主机 MCU 的应用软件。 此致, 朱利安
記事全体を表示
GCC 10.2ツールチェーンのインストールに失敗しました。 屏幕截图 2026-07-27 091847.png Re: GCC10.2工具链安装失败 コンピューターを再起動して、もう一度試してみましたか?
記事全体を表示
「セキュアボックス版」とは何ですか? AN12413仕様のGetVersion-APDUでは、「VersionInfo」に2バイトの「セキュアボックスバージョン」が定義されています。それが一体何なのか、明確な定義はない。 なぜこの情報が必要なのですか? 私は現在、通知機関との製品の認証手続きの最中です。この製品は特定のセキュリティ機能のためにSE050を使用しており、SE050にはファームウェアも含まれているため、これは認証の一部です。 SE050 Re: What is "Secure Box version"? こんにちは@Kan_Liさん 迅速なご返信ありがとうございます。感謝いたします。 すべての SE050A2 が同じかどうか確認できますか? OEF ID、プラットフォームビルドID、OSパッチレベル、アプレットのバージョン、機能設定。 そして、新たなロットを注文した場合でも、この点は変わりません。 この話題について知っておくべきことはこれだけです。 敬具 ダーク・ヤン Re: What is "Secure Box version"? こんにちは、 @djdirkj さん。 SE050A2すべてのチップが文字通り同一であることを証明しようとしないでください。OEF ID、プラットフォームビルドID、OSパッチレベル、アプレットバージョン、機能構成が同じであることを証明しつつ、トレーサビリティのために独自のシリアル/バッチデータを記録してください。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 ------------------------------------------------------------------------------- Re: What is "Secure Box version"? こんにちは@Kan_Liさん ご回答ありがとうございます! 質問を言い換えてみましょう。 弊社のEMS(電子機器受託製造業者)には、SE050A2部品が約500個入ったリールがあります。これらのSE050で500個の製品を生産した場合、すべてのSE050がまったく同じかどうかどうやって確信できますか? SE050に違いがある場合、証明書に適合しておらず、証明書の修正が必要です。これが望ましい状況ではないことをご理解いただければ幸いです。 Re: What is "Secure Box version"? こんにちは、 @djdirkj さん。 Secure Box版はSE050ソフトウェア/構成証拠の一部として記録してください。ただし、NXPが管理された定義を提供しない限り、独立して解釈しようとしないでください。認証の場合は完全なものが必要です  GetVersion  /  se05x_GetInfo  出力はより強力なトレーサビリティのアーティファクトです。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 ------------------------------------------------------------------------------- Re: What is "Secure Box version"? こんにちは、 @djdirkj さん。 はい、SE050Aではこれらのパラメータはすべて静的です。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 -------------------------------------------------------------------------------
記事全体を表示
如何从 MCUXpresso 安全配置工具构建 FCB 数据 您好。 我目前正在RT1010 EVK板上测试OTFAD配置。 我想使用 MCUXpresso Secure Provisioning Tool 26.03 配置 OTFAD 并构建项目以生成二进制文件。 版本结果如下: MIMXRT1011_Project.bin MIMXRT1011_Project_hab.bin otfad_keyblobs.bin unsigned_MIMXRT1010_flashloader.bin 这是四个文件。 当我使用 MCUXpresso Secure Provisioning Tool 26.03 执行写入操作并读取闪存时,程序在 0x0400 区域包含被认为是 FCB 的数据。 然而,在版本文件中,似乎没有与 FCB 对应的文件。 是否可以在版本过程中生成包含 FCB 信息的文件? i.MX RT101x Re: how i can build FCB data from MCUXpresso Secure Provisioning Tool 感谢您的回复。 我参考您提供的链接创建了 FCB。 我还有一个问题。 我可以在哪个文档中找到有关 OTFAD 设置中 Region 0 信息关键数据的说明? 我感兴趣的部分是用户密钥数据和计数器数据部分。 你能给我解释一下吗? 谢谢! TnseoRnr_0-1785208042935.png Re: how i can build FCB data from MCUXpresso Secure Provisioning Tool 嗨@TnseoRnr , 请参阅 SPT 文档中的以下链接,其中详细说明了如何从简化配置创建完整的 FCB: https://mcuxpresso.nxp.com/secure/26.03/05_user_interface.html#spi-nor 它还提到,如果您愿意,也可以通过 MCUXpresso 的外设工具生成 FCB。 最后提醒一下,SPT 有更新的版本(v26.06),所以我建议您继续使用最新版本进行开发。 BR, 埃德温。 Re: how i can build FCB data from MCUXpresso Secure Provisioning Tool 嗨@TnseoRnr , 如果您指的是这些字段将如何在您创建的 OTFAD 配置中使用,或许以下链接会有所帮助: https://mcuxpresso.nxp.com/secure/latest/06_processor_specific_workflow.html#booting-otfad-encrypted-image-unsigned-with-user-keys 也就是说,如果您正在寻找有关这些密钥的内部运作或更深入的解释,您需要请求访问 RT1010 安全文件,并查看网络安全参考手册,其中详细解释了 RT1010 的网络安全功能。 系统会提示您下载此文件,或者在需要时请求访问权限,方法是单击 RT1010 产品页面文档部分的“安全”复选框: https://www.nxp.com/products/i.MX-RT1010#documentation BR, 埃德温。
記事全体を表示
S32ds许可证已过期 2107-4B0B-EBCA-A774 S32 ARM 设计工作室 v2.2 申请延长激活时间 申请延长激活 Re: S32ds license expired 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。
記事全体を表示
什么是“安全盒版本”? AN12413 规范中的 GetVersion-APDU 定义了“VersionInfo”,其中包含 2 字节的“Secure Box 版本”。对于“它”究竟是什么,并没有一个明确的定义。 我为什么需要这些信息? 我正在协助一家认证机构对一款产品进行认证。本产品使用 SE050 来实现某些安全功能,由于 SE050 也包含某种形式的固件,因此这也是认证的一部分。 SE050 Re: What is "Secure Box version"? 嗨@Kan_Li , 感谢您的及时回复,非常感谢。 能否确认所有 SE050A2 都具有相同的以下特性: OEF ID、平台构建 ID、操作系统补丁级别、小程序版本和功能配置。 如果我们订购新一批,情况也不会改变。 关于这个话题,我只需要知道这些就够了。 此致敬礼, 德克·扬 Re: What is "Secure Box version"? 嗨@djdirkj , 请不要试图证明所有 SE050A2 芯片完全相同;请证明它们具有相同的 OEF ID、平台构建 ID、操作系统补丁级别、小程序版本和功能配置,同时记录唯一的序列号/批次数据以进行追溯。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 ------------------------------------------------------------------------------- Re: What is "Secure Box version"? 嗨@Kan_Li , 谢谢你的回复! 让我换个方式问: 我们EMS有一卷大约500个SE050A2元件。如果我用这些 SE050 生产 500 件产品,如何才能确保每个 SE050 都完全相同? 如果 SE050 存在差异,则不符合证书要求,需要对证书进行修改。我希望您明白,这样做并不可取。 Re: What is "Secure Box version"? 嗨@djdirkj , 请将 Secure Box 版本记录为 SE050 软件/配置证据的一部分,但除非 NXP 提供受控定义,否则请勿尝试自行解读;对于认证,请使用完整的版本信息。  GetVersion  /  se05x_GetInfo  输出是更强的可追溯性凭证。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 ------------------------------------------------------------------------------- Re: What is "Secure Box version"? 嗨@djdirkj , 是的,SE050A上的所有这些参数都是静态的。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 -------------------------------------------------------------------------------
記事全体を表示
S32ds license expired 2107-4B0B-EBCA-A774  S32 Design Studio for ARM v2.2 申请延长激活时间 申请延长激活 Re: S32ds license expired Hi,  your S32DS license has been extended. Please activate S32DS again with your old code. 
記事全体を表示
What is "Secure Box version"? The GetVersion-APDU in AN12413 specification defines "VersionInfo" with a 2-byte "Secure Box version". There is no definition as to what is exactly is. Why do I need this information? I'm in the middle of a certification of a product with a notified body. This product uses a SE050 for certain security features and this is part of the certification since the SE050 also contains a form of firmware.  SE050 Re: What is "Secure Box version"? Hi @Kan_Li , thank you for your timely reply, I appreciate it. Can you confirm that every SE050A2 has the same: OEF ID, platform build ID, OS patch level, applet version, and feature configuration. And if we order a new batch, this does not change. This is all I need to know regarding this topic. Kind regards, Dirk Jan Re: What is "Secure Box version"? Hi @djdirkj , Please do not try to prove that all SE050A2 chips are literally identical; prove that they have the same OEF ID, platform build ID, OS patch level, applet version, and feature configuration, while recording unique serial/batch data for traceability. Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: What is "Secure Box version"? Hi @Kan_Li , thank you for your response! Let me rephrase the question: I have a reel of about 500 SE050A2 components at our EMS. If I produce 500 products with these SE050, how can I be sure that every SE050 is exactly the same? If there is a difference in the SE050 it does not adhere to the certificate and it needs amendments to the certificate. I hope you understand that this is not desirable. Re: What is "Secure Box version"? Hi @djdirkj , Please record the Secure Box version as part of the SE050 software/configuration evidence, but do not try to interpret it independently unless NXP provides a controlled definition; for certification, the full  GetVersion  /  se05x_GetInfo  output is the stronger traceability artifact. Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: What is "Secure Box version"? Hi @djdirkj , Yes, all these parameters are static on SE050A. Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示
GCC 10.2 toolchain installation failed. 屏幕截图 2026-07-27 091847.png Re: GCC10.2工具链安装失败 Have you tried to restart your computer and test it again?
記事全体を表示