asoc-simple-card: parse error after upgrading to kernel 6.18.x Hi, here is my working DT for Kernel 6.6.52: / {
codec: max98357a@0{
compatible = "maxim,max98357a";
#sound-dai-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&sdmode_en>;
sdmode-gpios = <&gpio4 28 GPIO_ACTIVE_HIGH>;
status = "okay";
};
sound {
compatible = "simple-audio-card";
simple-audio-card,name = "SAI3 MAX98357A";
simple-audio-card,format = "i2s";
simple-audio-card,widgets = "Speaker","Speakers";
simple-audio-card,routing = "Speakers","Speaker";
simple-audio-card,bitclock-master = <&cpu_dai>;
simple-audio-card,frame-master = <&cpu_dai>;
cpu_dai: simple-audio-card,cpu {
sound-dai = <&sai3>;
clocks = <&clk IMX8MP_CLK_SAI3>;
clock-names = "mclk";
//system-clock-frequency = <&clk IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
codec_dai: simple-audio-card,codec {
sound-dai = <&codec>;
//clocks = <&clk IMX8MP_CLK_SAI3>;
};
};
};
&sai3{
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai3>;
#sound-dai-cells = <0>;
clocks = <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_IPG>,
<&clk IMX8MP_CLK_DUMMY>,
<&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>,
<&clk IMX8MP_CLK_DUMMY>,
<&clk IMX8MP_CLK_DUMMY>,
<&clk IMX8MP_AUDIO_PLL1_OUT>,
<&clk IMX8MP_AUDIO_PLL2_OUT>;
clock-names = "bus", "mclk0", "mclk1", "mclk2", "mclk3", "pll8k", "pll11k";
assigned-clocks = <&clk IMX8MP_CLK_SAI3>,
<&clk IMX8MP_AUDIO_PLL1>,
<&clk IMX8MP_AUDIO_PLL2>;
assigned-clock-parents = <&clk IMX8MP_AUDIO_PLL2_OUT>,
<&clk IMX8MP_AUDIO_PLL1_OUT>;
// Try common MCLK rates that divide well to 48 kHz multiples
// Option A: 24.576 MHz (very common for MAX98357A + 48 kHz)
assigned-clock-rates = <24576000>, // PLL2 for 48 kHz
<22579200>; // PLL1 for 44.1 kHz
// Option B (if 44.1 kHz needed later): use PLL1 + 22579200
//assigned-clock-rates = <22579200>;
fsl,sai-asynchronous;
fsl,sai-mclk-direction-output;
status = "okay";
}; After moving to kernel 6.18.20 SAI3 is not probing and I got no sound-card. The boot log shows: platform sound: deferred probe pending: asoc-simple-card: parse error What changes in the DT syntax from kernel 6.6.52 to 6.18.x? I didn't find anything relevant. How can I investigate the parse error? i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Linux Yocto Project Re: asoc-simple-card: parse error after upgrading to kernel 6.18.x Hello,
Could you please share your dmesg log?
Best regards. Re: asoc-simple-card: parse error after upgrading to kernel 6.18.x Hi Jorge, dmesg log and running device tree (./dtc -I fs -O dts /proc/device-tree > /tmp/running.dts) attached. Re: asoc-simple-card: parse error after upgrading to kernel 6.18.x Hi, I have moved one step forward. After enabling the kernel configuration option CONFIG_IMX_AIPSTZ=y, the sound card device is now available. Because sai3 node is a sub node of aips5 I also had to enable aips5 in my devicetree: &aips5 {
status = "okay";
}; Now I got the following error messages: [ 13.081746] fsl-sai 30c30000.sai: ASoC error (-110): at snd_soc_dai_hw_params() on sai-tx-rx
[ 13.090223] sai-tx-rx-HiFi: ASoC error (-110): at __soc_pcm_hw_params() on sai-tx-rx-HiFi speaker-test -c 2 -r 48000 -t sine 2>&1 | head -20
[ 31.368187] fsl-sai 30c30000.sai: ASoC error (-110): at snd_soc_dai_hw_params() on sai-tx-rx
[ 31.376682] sai-tx-rx-HiFi: ASoC error (-110): at __soc_pcm_hw_params() on sai-tx-rx-HiFi
Unable to set hw params for playback: Connection timed out
speaker-test 1.2.11
Playback device is default
Stream parameters are 48000Hz, S16_LE, 2 channels
Sine wave rate is 440.0000Hz
Rate set to 48000Hz (requested 48000Hz)
Buffer size range from 24 to 131072
Period size range from 12 to 16383
Periods = 4
Setting of hwparams failed: Connection timed out Re: asoc-simple-card: parse error after upgrading to kernel 6.18.x I got it, sound is working. My kernel configs: CONFIG_SND_IMX_SOC=m
CONFIG_SND_IMX_SOC=m
CONFIG_SND_SOC_FSL_SAI=m
CONFIG_SND_SOC_FSL_UTILS=m
CONFIG_IMX_AIPSTZ=y The devicetree part: /{
codec: max98357a@0{
compatible = "maxim,max98357a";
#sound-dai-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&sdmode_en>;
sdmode-gpios = <&gpio4 28 GPIO_ACTIVE_HIGH>;
status = "okay";
};
sound {
compatible = "simple-audio-card";
status = "okay";
simple-audio-card,name = "SAI3 MAX98357A";
simple-audio-card,format = "i2s";
simple-audio-card,widgets = "Speaker", "Speaker Ext";
simple-audio-card,routing = "Speaker Ext", "Speaker";
simple-audio-card,bitclock-master = <&cpu_dai>;
simple-audio-card,frame-master = <&cpu_dai>;
cpu_dai: simple-audio-card,cpu {
sound-dai = <&sai3>;
clocks = <&clk IMX8MP_CLK_SAI3>;
clock-names = "mclk";
//system-clock-frequency = <&clk IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
codec_dai: simple-audio-card,codec {
sound-dai = <&codec>;
};
};
};
&sdma2 {
status = "okay";
fsl,sdma-ram-script-name = "imx/sdma/sdma-imx7d.bin";
};
&aips5 {
status = "okay";
};
&audio_blk_ctrl {
status = "okay";
assigned-clocks = <&clk IMX8MP_AUDIO_PLL1>,
<&clk IMX8MP_AUDIO_PLL2>;
assigned-clock-rates = <393216000>, <361267200>;
};
&sai3{
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai3>;
#sound-dai-cells = <0>;
assigned-clocks = <&clk IMX8MP_CLK_SAI3>;
assigned-clock-parents = <&clk IMX8MP_AUDIO_PLL1_OUT>;
assigned-clock-rates = <12288000>;
clocks = <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_IPG>,
<&clk IMX8MP_CLK_DUMMY>,
<&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>,
<&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK2>,
<&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK3>;
clock-names = "bus", "mclk0", "mclk1", "mclk2", "mclk3";
dmas = <&sdma2 4 2 0>, <&sdma2 5 2 0>;
dma-names = "rx", "tx";
fsl,sai-asynchronous;
fsl,sai-mclk-direction-output;
status = "okay";
}; The devicetree base is imx8mp.dtsi
記事全体を表示