Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
使用主机上的 SPIGen 无法驱动 FRDMPT2001EVM 上的 DRVEN 和 RESETB 引脚。 你好, 我按照 KTFRDMPT2001EVMUG.pdf 配置了 FRDM-KL25Z 板,并用电缆将其连接到我的 PC。FRDM-KL25Z 板上的蓝色 LED 灯亮起。在主机上的 SPIGen 中加载 *.spi 文件后,我可以正常下载并读取/写入寄存器。然而,DRVEN 和 RESETB 引脚仍然保持默认状态。我无法使用 SPIGen 面板/GUI 中的按钮将板上的相应引脚拉高或拉低。 我应该如何解决这个问题?感谢你的回复! PT2001 FRDM-KL25Z Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC 嗨 Lex( @LexLiu ), 请问您能否帮忙解决一下使用 SPIGen SW 驱动 FRDMPT2001EVM 上的 DRVEN 和 RESETB 引脚时遇到的问题? 谢谢您! BRs,托马斯 Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC 这个问题我还没解决。你能帮助我吗? 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC 无论在 SPIGen 中选择“高”还是“低”,RESETB 引脚始终保持在 3.203 V。DRVEN 引脚也无法正确切换。输出结果似乎始终保持默认状态。 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC 喂?有人能帮帮我吗? 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC 嗨@TomasVaverka 请您帮忙看一下我无法驱动 DRVEN 和 RESETB 引脚的问题?非常感谢您的帮助。非常感谢! 此致敬礼, zaoluo Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC 嗨@LexLiu , 问题已解决。非常感谢您的帮助! Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC 你好, 请您在SPIGen上查看一下您的KL25Z主板的固件版本。请您尝试一下 5.2.6 版本?
記事全体を表示
Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC Hello, I configured the FRDM-KL25Z board according to KTFRDMPT2001EVMUG.pdf and connected it to my PC with a cable. The blue LED on the FRDM-KL25Z board turns on. After loading the *.spi file in SPIGen on the host PC, I can download normally and read/write registers. However, the DRVEN and RESETB pins remain in their default state. I cannot use the buttons in the SPIGen panel/GUI to drive the corresponding pins on the board high or low. How should I solve this issue? Thank you for your reply! PT2001  FRDM-KL25Z  Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC Hi Lex (@LexLiu), Could you please help with this question regarding the problem with driving both the DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen SW? Thanks! BRs, Tomas Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC I haven't solved this problem yet. Can you help me? 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC The RESETB pin stays at 3.203 V regardless of whether "High" or "Low" is selected in SPIGen. The DRVEN pin likewise does not toggle correctly. The outputs appear to remain in their default state at all times. 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC Hello? Can anyone help me? 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC Hi @TomasVaverka  Could you please take a look at my issue regarding the inability to drive the DRVEN and RESETB pins? I would really appreciate your help. Thank you very much! Best regards, zaoluo Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC HI, Can you please check the Firmware version of your KL25Z board on SPIGen? Can you please try Version 5.2.6? Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC Hi @LexLiu , The issue has been resolved. Thank you very much for your help!
記事全体を表示
Ibis Lx2160a 型号 嗨,大家好 我想知道如何才能获得适用于 lx2160a 的 ibis 型号,有人可以帮帮我吗? 非常感谢您 元 Re: Ibis model for Lx2160a IBIS模型不公开,请在此处创建案例: https://support.nxp.com/s/?language=en_US  并分享你的保密协议。 谢谢!
記事全体を表示
ホストPC上のSPIGenを使用してFRDMPT2001EVMのDRVENピンとRESETBピンを駆動できません こんにちは、 KTFRDMPT2001EVMUG.pdfに従ってFRDM-KL25Zボードを設定し、ケーブルでPCに接続しました。FRDM-KL25Z基板上の青色LEDが点灯します。ホストPCのSPIGenで*.spiファイルを読み込んだ後、通常通りレジスタをダウンロードし読み書きできるようになりました。しかし、DRVENとRESETBのピンはデフォルトのままです。 SPIGenパネルやGUIのボタンを使って、基板上の対応するピンを高くまたは低く動かすことはできません。 この問題をどう解決すればいいでしょうか?お返事ありがとうございます! PT2001 FRDM-KL25Z Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC こんにちは、Lex( @LexLiu ) SPIGen SWでFRDMPT2001EVMのDRVENピンとRESETBピンの両方を駆動する際の問題について、この質問についてご協力いただけますか? よろしくお願いします! BRs、トーマス Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC 私はまだこの問題を解決していません。助けてくれないか? 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC SPIGenで「High」または「Low」のどちらが選択されていても、RESETBピンは3.203Vのままです。DRVENピンも同様に正しく切り替わりません。出力は常にデフォルトの状態のままであるように見える。 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC もしもし?どなたか助けてくれませんか? 回复: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC こんにちは、 @TomasVaverka さん。 DRVENとRESETBピンが動けないという私の問題について、見ていただけませんか?ご協力いただけると大変ありがたいです。どうもありがとうございます! よろしくお願いいたします、 zaoluo Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC こんにちは、 @LexLiu さん。 問題は解決しました。ご協力いただき、本当にありがとうございました! Re: Unable to drive DRVEN and RESETB pins on FRDMPT2001EVM using SPIGen on the host PC こんにちは、 SPIGenでKL25Zボードのファームウェアバージョンを確認してもらえますか?バージョン5.2.6を試してみてもらえますか?
記事全体を表示
mcxn947 加密区指定可范围么,程序内部フラッシュ加密区 暗号化や署名は特定のフラッシュ空間の範囲に適用できますか? 暗号化されたフラッシュ領域内におけるプログラム自身の読み書き動作は、以前とどのように異なりますか(読み戻されるデータは暗号文ですか?書き込まれるデータは平文ですか?)? OTAアップグレードの際、チップの暗号化/復号に適合するアーキテクチャを競合なくするにはどうすればよいのでしょうか? Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 こんにちは、 まず明確にしておきたいのは、暗号化が有効になると、チップ上で実行されているプログラムがフラッシュメモリに書き込む際、書き込まれるデータは平文ですが、最終的にフラッシュメモリに保存されるのは暗号文です。そして、チップ上で実行されているプログラムがフラッシュメモリ内の暗号文を読み取ると、平文として出力されます。 正しい 上記の観点に基づくと: そして、Secure Provisioningソフトウェアが読み取るSBファイルは暗号文であり、シリアルISP経由でチップの純正ISP ROMブートローダーに送られるものも暗号文でなければなりません(そうでなければ論理的な欠陥が生じます)。工場出荷時のISP ROMブートローダーは、シリアル通信で受信した暗号文を平文に復号化し、その平文データをフラッシュメモリに書き込みますが、最終的にフラッシュメモリに保存されたデータは再び暗号化され、暗号文になります。 つまり、ISPプログラミング中、工場出荷時のISP ROMブートローダーはまず復号化を行い、次に暗号化を行うため、復号化と暗号化の往復処理が行われる。 もう少し詳しく説明させてください。 はい、SBファイルは暗号化されているため、フラッシュメモリに書き込む前にROMで復号化する必要があります。しかし、SBファイルはOEMと製造工場間のファームウェアを保護するために、完全に独立して暗号化されています。 フラッシュメモリのプログラミング(内蔵型か外付け型かを問わず)はまた別の話で、全く使用されないか、あるいは異なるアルゴリズム、初期ベクトルなどを用いて使用されます。 よろしくお願いいたします。 リボル Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 まず明確にしておきたいのは、暗号化が有効になると、チップ上で実行されているプログラムがフラッシュメモリに書き込む際、書き込まれるデータは平文ですが、最終的にフラッシュメモリに保存されるのは暗号文です。そして、チップ上で実行されているプログラムがフラッシュメモリ内の暗号文を読み取ると、平文として出力されます。   上記の観点に基づくと: そして、Secure Provisioningソフトウェアが読み取るSBファイルは暗号文であり、シリアルISP経由でチップの純正ISP ROMブートローダーに送られるものも暗号文でなければなりません(そうでなければ論理的な欠陥が生じます)。工場出荷時のISP ROMブートローダーは、シリアル通信で受信した暗号文を平文に復号化し、その平文データをフラッシュメモリに書き込みますが、最終的にフラッシュメモリに保存されたデータは再び暗号化され、暗号文になります。 つまり、ISPプログラミング中、工場出荷時のISP ROMブートローダーはまず復号化を行い、次に暗号化を行うため、復号化と暗号化の往復処理が行われる。                           Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 こんにちは、 MCXNデバイスの場合: 暗号化や署名は特定のフラッシュ空間の範囲に適用できますか? SECツール: - アプリケーション全体に署名 - 暗号化領域は製品のライフ期間中に一度設定され、FUTUREのアップデート(アプリの拡張)のために予約を取る必要があります。 暗号化されたフラッシュ領域内におけるプログラム自身の読み書き動作は、以前とどのように異なりますか(読み戻されるデータは暗号文ですか?書き込まれるデータは平文ですか?)? 暗号化/復号化はリアルタイムで行われます。アプリがフラッシュメモリから読み込む場合、そのことを気にする必要はありません。透過的に処理されます。アプリケーション自体から暗号化されたフラッシュ領域に書き込むことについては、調査が必要です。注意点があるかはわかりません。 OTAアップグレードの際、チップの暗号化/復号に適合するアーキテクチャを競合なくするにはどうすればよいのでしょうか? 前述のとおり、暗号化には適切なサイズのメモリ領域を指定する必要があります。もしアプリケーションが暗号化領域を超えた場合、OTAは動作しますが、暗号化圏外のアプリ部分だけが動作し、IPアドレスは暗号化で保護されません。 よろしくお願いいたします。 リボル
記事全体を表示
启用 Falcon 模式下的安全启动(内核版本 6.12.49)|| iMX8MP_EVK 大家好, 请问您能帮我启用Falcon模式下的安全启动吗? 我已成功借助 meta-imx-fastboot GitHub 代码库实现了 Falcon 模式。但是,我发现 meta-imx-fastboot 的实现会 在 Falcon 模式启动过程中 有意移除 OP-TEE 。 由于我的用例也需要用到 OP-TEE,我在 NXP 论坛上提出了一个问题, @elena_popa提供了一个保留并启用 OP-TEE 的解决方案。我附上了论坛链接供您参考。 目前,我在启用 安全启动 时遇到了问题 ,因为我找不到任何关于我的当前内核版本在 Falcon 模式下启用安全启动的文档。 环境详情: 主板: i.MX8M Plus EVK(i.MX8MP EVK) 内核版本: 6.12.49 Yocto 环境:基于 Yocto 的 NXP 电路板支持包。 启动模式:猎鹰模式 要求:猎鹰模式 + OP-TEE + 安全启动 Yocto Project Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK 你好, 请问您遇到了什么错误? 顺祝商祺! Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK 嗨@JorgeCas 我所做的:扩展了 imx-boot-signature 配方,使其也能对我们的 Falcon FIT 包(kernel-atf-dtb.itb)进行签名。u-boot-atf.itb)使用 imx_signer + 与主 imx-boot 容器相同的 sign.cfg。 问题: HAB 处于打开状态(未烧断熔丝),hab_status 显示: u-boot=> hab_status 安全启动已禁用 HAB配置:0xf0,HAB状态:0x66 --------- HAB 事件 1 ----------------- 事件数据: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x00 0x40 0x1f 0xdd 0xc0 0x00 0x00 0x00 0x20 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 2 ----------------- 事件数据: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x00 0x40 0x1f 0xad 0xc0 0x00 0x00 0x00 0x04 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 3 ----------------- 事件数据: 0xdb 0x00 0x3c 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x34 0x00 0x02 0xc5 0x00 0x00 0x00 0x00 0x0b 0x50 0x40 0x1f 0xad 0xc0 0x00 0x00 0x30 0x20 0x40 0x20 0x00 0x00 0x00 0x12 0x12 0xb8 0x40 0x32 0x12 0xb8 0x00 0x01 0x44 0x68 0x00 0x97 0x00 0x00 0x00 0x00 0xbd 0x00 0x56 0x00 0x00 0x00 0x00 0x09 0x57 0x50 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 4 ----------------- 事件数据: 0xdb 0x00 0x3c 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x34 0x00 0x02 0xc5 0x00 0x00 0x00 0x00 0x0b 0x50 0x40 0x1f 0xad 0xc0 0x00 0x00 0x30 0x20 0x40 0x20 0x00 0x00 0x00 0x12 0x12 0xb8 0x40 0x32 0x12 0xb8 0x00 0x01 0x44 0x68 0x00 0x97 0x00 0x00 0x00 0x00 0xbd 0x00 0x56 0x00 0x00 0x00 0x00 0x09 0x57 0x50 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) 失败的块地址/大小与 u-boot-atf.itb 的完全匹配。可加载程序(U-Boot、ATF、OP-TEE)。这是在全新重建过程中确定性的。同时,已签名的 imx-boot SPL+ATF+U-Boot 容器(通过相同的配方/工具签名)验证正常。 问题:对 Falcon 模式的 u-boot-atf.itb(多加载 FIT:U-Boot + ATF + OP-TEE)进行签名时,是否需要与 imx_signer 为标准 imx-boot SD 容器生成的默认 csf_hab4.cfg 不同的 CSF 结构?是否有专门针对 Falcon u-boot-atf.itb/kernel-atf-dtb.itb 签名的参考资料? Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK 你好, 很抱歉耽搁了这么久。 如仓库中所述,lf-6.6.36-2.1.0-secure 已启用安全启动支持。分支可以作为参考,但遗憾的是,lf-6.12.20-2.0.0-secure 版本存在问题。Falcon 分支明确指出,该 电路板支持包 及更新版本不支持安全启动。 目前没有关于如何将 6.6 安全分支上的安全 Falcon 实现移植到新版本系统的文档。imx-boot 容器的身份验证表明 FIT CSF 块映射或 CSF 插入偏移量不匹配。 顺祝商祺! Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK 请帮帮忙!
記事全体を表示
Re: S32G274A LLCE CAN 現在、自社開発のボードはマルチコアモードで動作しています。1つのA53コアは他のデバイスとのネットワーク通信タスクに使用され、他の複数のA53コアはバス通信ドライバを実行します。各バスタイプはそれぞれ別のA53コアを使用します。問題が発生しました。現在のLLCE CANリカバリ操作は、LLCE CANモードを停止してから再開するように構成されています。実際のほとんどのシナリオでは通信は復旧できますが、バスリカバリが頻繁に実行される場合があり、他のA53コアの正常な動作に影響を与えます(ネットワーク通信タスクが中断されます)。質問は、LLCE CANバスリカバリにはどのような方法があるか、また、LLCE CANを別のコアで実行しても他のコアに影響を与えるのはなぜか、ということです。バージョン情報は、S32G_LLCE_1_0_9、SW32G_RTD_4.4_4.0.2_P04_D2312です。 Re: S32G274A LLCE CAN こんにちは、 @JACK_Q こんにちは ソフトウェアおよびハードウェアのテスト環境について、詳細な説明をいただけますでしょうか? 1. あなたのシステムでは、MコアとAコアは同時に使用されていますか?M7コアはどのようなタスクを実行しますか?どのソフトウェアパッケージに依存していますか? 2. あなたの説明によると、A53側の各コアはそれぞれ独自のタスクを実行しているようですが、どのようなソフトウェアが動作していますか?Linux BSPでしょうか? BR チェイン
記事全体を表示
Difference between S32K1_S32M24X and S32K1 RTD packages? I am developing for the S32K116. I noticed while going through the S32DS Extensions an dUpdates that I have two S32K1 packages installed: "S32K1_S32M24X Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 QLP06" and "S32K1 Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 QLP06" What is the difference between the two? If they do the same for my case, which one should I keep/uninstall? I tried removing one of them (the S32K1 one) but then my projects couldn't load their .mex files anymore. Re: Difference between S32K1_S32M24X and S32K1 RTD packages? Hi @daniel_meier  Although the packages may appear similar, they have dependencies between themselves and with S32DS, and are not intended to be treated as standalone components that can be used independently of one another. Therefore, we recommend reinstalling the package and keeping both packages installed to ensure proper project functionality. BR, VaneB
記事全体を表示
Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK Hi Team, Could you please help me enable Secure Boot in Falcon Mode? I have successfully achieved Falcon Mode with the help of the meta-imx-fastboot GitHub repository. However, I observed that the meta-imx-fastboot implementation intentionally removes OP-TEE during the Falcon Mode boot flow. Since OP-TEE is also required for my use case, I raised a query on the NXP forum, where @elena_popa provided a solution to retain and enable OP-TEE. I have attached the forum link for reference. Currently, I am facing an issue with enabling Secure Boot, as I could not find any document for Secure Boot with falcon mode for my current kernel version. Environment details: Board: i.MX8M Plus EVK (i.MX8MP EVK) Kernel Version: 6.12.49 Yocto Environment: Yocto-based NXP BSP Boot Mode: Falcon Mode Requirement: Falcon Mode + OP-TEE + Secure Boot Yocto Project Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK Hello, Could you please share which error are you getting? Best regards. Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK Hi @JorgeCas What I did: Extended the imx-boot-signature recipe to also sign our Falcon FIT bundles (kernel-atf-dtb.itb, u-boot-atf.itb) using imx_signer + the same sign.cfg used for the main imx-boot container. Issue: With HAB open (no fuses burned), hab_status shows: u-boot=> hab_status Secure boot disabled HAB Configuration: 0xf0, HAB State: 0x66 --------- HAB Event 1 ----------------- event data: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x00 0x40 0x1f 0xdd 0xc0 0x00 0x00 0x00 0x20 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HAB Event 2 ----------------- event data: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x00 0x40 0x1f 0xad 0xc0 0x00 0x00 0x00 0x04 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HAB Event 3 ----------------- event data: 0xdb 0x00 0x3c 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x34 0x00 0x02 0xc5 0x00 0x00 0x00 0x00 0x0b 0x50 0x40 0x1f 0xad 0xc0 0x00 0x00 0x30 0x20 0x40 0x20 0x00 0x00 0x00 0x12 0x12 0xb8 0x40 0x32 0x12 0xb8 0x00 0x01 0x44 0x68 0x00 0x97 0x00 0x00 0x00 0x00 0xbd 0x00 0x56 0x00 0x00 0x00 0x00 0x09 0x57 0x50 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) --------- HAB Event 4 ----------------- event data: 0xdb 0x00 0x3c 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x34 0x00 0x02 0xc5 0x00 0x00 0x00 0x00 0x0b 0x50 0x40 0x1f 0xad 0xc0 0x00 0x00 0x30 0x20 0x40 0x20 0x00 0x00 0x00 0x12 0x12 0xb8 0x40 0x32 0x12 0xb8 0x00 0x01 0x44 0x68 0x00 0x97 0x00 0x00 0x00 0x00 0xbd 0x00 0x56 0x00 0x00 0x00 0x00 0x09 0x57 0x50 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) The failing block addresses/sizes match exactly u-boot-atf.itb's loadables (U-Boot, ATF, OP-TEE). This is deterministic across clean rebuilds. Meanwhile the signed imx-boot SPL+ATF+U-Boot container (signed via the same recipe/tool) authenticates fine. Question: Does signing a Falcon-mode u-boot-atf.itb (multi-loadable FIT: U-Boot + ATF + OP-TEE) need a different CSF structure than what imx_signer's default csf_hab4.cfg produces for the standard imx-boot SD container? Is there a reference for signing Falcon u-boot-atf.itb/kernel-atf-dtb.itb specifically? Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK Hello, I apologize for the delay. As mentioned in repository, the secure Boot support is enabled in lf-6.6.36-2.1.0-secure branch and can be used as reference but, unfortunately, unfortunately, lf-6.12.20-2.0.0-secure Falcon branch explicitly states that Secure Boot is not supported for that BSP and newer. There is no documentation available for porting the secure Falcon implementation from the 6.6 secure branch. The authentication of the imx-boot container suggests a mismatched FIT CSF block map or CSF insertion offset. Best regards. Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK Please help here..!
記事全体を表示
mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 Can encryption and signing be applied to a specified range of flash space? How does the program's own read/write behavior within the encrypted flash region differ from before (is the data read back ciphertext? is the data written plaintext?)? During OTA upgrades, how can the architecture be made to match the chip's encryption/decryption without conflicts? Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 Hello, To be clear first: once encryption is enabled, when a program running on the chip writes to flash, the data it writes is plaintext, but what is ultimately stored in flash is ciphertext; when the ciphertext in flash is read by a program running on the chip, it comes out as plaintext. Correct Based on above viewpoint : Then, the SB file read by your Secure Provisioning software is ciphertext, and what is sent over serial ISP to the chip’s factory ISP ROM bootloader must also be ciphertext (otherwise there would be a logical flaw). The factory ISP ROM bootloader decrypts the ciphertext received over serial into plaintext, and then writes the plaintext data into flash, but ultimately the data stored in flash is encrypted again, becoming ciphertext. In other words, during ISP programming, the factory ISP ROM bootloader first decrypts and then encrypts, going through a decrypt-then-encrypt round trip. Let me put more light into this: yes SB file is encrypted and must be decrypted by ROM before writing to Flash. But SB file is encrypted completely independently, to protect the firmware between the OEM and manufacturing facility. Programming flash, either internal or external, is different story and either is not used at all or is used with different algorithm, initial vector, etc. Regards, Libor Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 To be clear first: once encryption is enabled, when a program running on the chip writes to flash, the data it writes is plaintext, but what is ultimately stored in flash is ciphertext; when the ciphertext in flash is read by a program running on the chip, it comes out as plaintext.   Based on above  viewpoint : Then, the SB file read by your Secure Provisioning software is ciphertext, and what is sent over serial ISP to the chip’s factory ISP ROM bootloader must also be ciphertext (otherwise there would be a logical flaw). The factory ISP ROM bootloader decrypts the ciphertext received over serial into plaintext, and then writes the plaintext data into flash, but ultimately the data stored in flash is encrypted again, becoming ciphertext. In other words, during ISP programming, the factory ISP ROM bootloader first decrypts and then encrypts, going through a decrypt-then-encrypt round trip.                           Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 Hi, For MCXN devices: Can encryption and signing be applied to a specified range of flash space? SEC tool: - signs whole application - encryption region is configured once in the product lifetime, you need to make a reserve for future updates (increased size of app) How does the program's own read/write behavior within the encrypted flash region differ from before (is the data read back ciphertext? is the data written plaintext?)? Encryption/decryption is on-the-fly. App reading from flash does not need to care, it is transparent. About writing to encrypted flash region from the application itself, you need to investigate, I'm not sure if there are any caveats. During OTA upgrades, how can the architecture be made to match the chip's encryption/decryption without conflicts? As mentioned above, you need to specify reasonable size of memory region for encryption. If you application exceeds the encrypted region, OTA will work, only the part of the app that will be outside of encrypted area will still work, only your IP won't be protected by the encryption. Regards, Libor
記事全体を表示
Re: S32G274A LLCE CAN 当前自研板运行在多核模式下,1个A53核是用来和其他设备网络通信任务的,还有几个A53跑的是一些总线通信的驱动,每个类型的总线单独使用一个A53核。现在出现了一个问题是当前给LLCE CAN配置的恢复操作是设置LLCE CAN的模式先stop再start,在实际运行的场景大部分可以恢复通信的,但是有的时候会频繁的执行总线恢复以至于到影响其他的A53正常运行(网络通信任务中断)。想问的是LLCE CAN有那些方法可以总线恢复,还有是为什么LLCE CAN已经单独放置一个核运行还会影响到其他的核。以下是版本信息:S32G_LLCE_1_0_9;SW32G_RTD_4.4_4.0.2_P04_D2312 Re: S32G274A LLCE CAN Hello, @JACK_Q  您好 麻烦您详细介绍一下您的软硬件测试环境: 1. 在您的系统中,是M核和A核端同时使用吗?M7核运行什么任务?基于哪些软件包? 2. A53端从您的描述来看,每个核都有自己的任务,请问是运行的什么软件?是否是Linux BSP? BR Chenyin
記事全体を表示
Falconモードでセキュアブートを有効にする(カーネルバージョン6.12.49)|| iMX8MP_EVK チームの皆さん、こんにちは。 Falcon ModeでSecure Boot を有効にするのを手伝ってもらえます か? meta-imx-fastboot GitHubリポジトリ の助けを借りて、Falcon Modeの実現に成功しました 。しかし、meta-imx-fastbootの実装では 、Falcon Modeのブートフロー中に 意図的に OP-TEE が削除されていることがわかりました。 OP-TEEも私のユースケースに必要なので、NXPフォーラムで質問をしました。@elena_popa OP-TEEを保持・有効化するソリューションを提供してくれました。参考のためにフォーラム のリンク を添付しました。 現在、Secure Bootを有効にする際に問題に直面しています 現在のカーネルバージョンでファルコンモード付きのセキュアブートに関するドキュメントが見つからなかったためです。 環境詳細: ボード: i.MX8M Plus EVK(i.MX8MP EVK) カーネルバージョン: 6.12.49 Yocto Environment: Yocto拠点のNXP BSP ブートモード:ファルコンモード 要件:ファルコンモード + OP-TEE + セキュアブート Yocto Project Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK こんにちは、 どのエラーが出ているのか教えていただけますか? よろしくお願いいたします。 Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK こんにちは、@JorgeCasさん 私がやったこと: imx-boot-signature レシピを拡張して、Falcon FIT バンドル (kernel-atf-dtb.itb、u-boot-atf.itb)imx_signerと、メインのimx-bootコンテナで使用されているものと同じsign.cfgを使用します。 問題: HABが開いている状態(ヒューズが焼損していない状態)で、hab_statusには以下が表示されます。 u-boot=> hab_status セキュアブートが無効になっています HAB 構成:0xf0、HAB 状態:0x66 --------- HABイベント1 ----------------- イベントデータ: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x00 0x40 0x1f 0xdd 0xc0 0x00 0x00 0x00 0x20 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HABイベント2 ----------------- イベントデータ: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x00 0x40 0x1f 0xad 0xc0 0x00 0x00 0x00 0x04 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HABイベント3 ----------------- イベントデータ: 0xdb 0x00 0x3c 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x34 0x00 0x02 0xc5 0x00 0x00 0x00 0x00 0x0b 0x50 0x40 0x1f 0xad 0xc0 0x00 0x00 0x30 0x20 0x40 0x20 0x00 0x00 0x00 0x12 0x12 0xb8 0x40 0x32 0x12 0xb8 0x00 0x01 0x44 0x68 0x00 0x97 0x00 0x00 0x00 0x00 0xbd 0x00 0x56 0x00 0x00 0x00 0x00 0x09 0x57 0x50 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) --------- HABイベント4----------------- イベントデータ: 0xdb 0x00 0x3c 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x34 0x00 0x02 0xc5 0x00 0x00 0x00 0x00 0x0b 0x50 0x40 0x1f 0xad 0xc0 0x00 0x00 0x30 0x20 0x40 0x20 0x00 0x00 0x00 0x12 0x12 0xb8 0x40 0x32 0x12 0xb8 0x00 0x01 0x44 0x68 0x00 0x97 0x00 0x00 0x00 0x00 0xbd 0x00 0x56 0x00 0x00 0x00 0x00 0x09 0x57 0x50 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) 障害が発生したブロックのアドレス/サイズは、u-boot-atf.itb のものと完全に一致します。ロード可能なファイル(U-Boot、ATF、OP-TEE)。これはクリーンな再建でもデターミニスティックです。一方、署名済みのimx-boot SPL+ATF+U-Bootコンテナ(同じレシピ/ツールで署名済み)は正常に認証される。 質問: Falconモードのu-boot-atf.itb(マルチロード可能なFIT:U-Boot + ATF + OP-TEE)に署名する場合、imx_signerのデフォルトのcsf_hab4.cfgが標準のimx-boot SDコンテナ用に生成するものとは異なるCSF構造が必要ですか?Falconのu-boot-atf.itb/kernel-atf-dtb.itbに署名するための具体的なリファレンスはありますか? Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK どうか助けてください! Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK こんにちは、 遅れて申し訳ありません。 リポジトリで述べられているように、安全なブートサポートはlf-6.6.36-2.1.0-secureで有効化されていますBranch と は参照として使用できますが、残念ながら lf-6.12.20-2.0.0-secure(安全)は使えますFalconブランチでは、そのBSPおよびそれ以降のバージョンではセキュアブートがサポートされていないことが明記されています。 6.6のセキュアブランチから安全なFalcon実装を移植するためのドキュメントは存在しません。imx-bootコンテナの認証は、FIT CSFブロックマップまたはCSF挿入オフセットの不一致を示唆しています。 よろしくお願いいたします。
記事全体を表示
mcxn947加密区域可以指定范围,程序内部如何访问flash加密区域 能否对指定范围的闪存空间进行加密和签名? 程序在加密闪存区域内的读/写行为与之前有何不同(读取回的数据是密文吗?写入的数据是明文吗?)? 在 OTA 升级过程中,如何使架构与芯片的加密/解密相匹配而不发生冲突? Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 你好, 首先要明确一点:一旦启用加密,当芯片上运行的程序向闪存写入数据时,写入的数据是明文,但最终存储在闪存中的是密文;当芯片上运行的程序读取闪存中的密文时,读取出来的却是明文。 正常 基于以上观点: 然后,您的安全配置软件读取的 SB 文件是密文,通过串行 ISP 发送到芯片的工厂 ISP ROM 引导加载程序的内容也必须是密文(否则就会出现逻辑缺陷)。工厂 ISP ROM 引导加载程序将通过串口接收的密文解密为明文,然后将明文数据写入闪存,但最终存储在闪存中的数据又会被加密,变成密文。 换句话说,在 ISP 编程期间,工厂 ISP ROM 引导加载程序首先进行解密,然后再进行加密,经历一个解密再加密的往返过程。 让我再详细解释一下: 是的,SB 文件已加密,必须先由 ROM 解密才能写入 Flash。但SB文件是完全独立加密的,以保护OEM厂商和制造工厂之间的固件安全。 对闪存(无论是内部闪存还是外部闪存)进行编程是另一回事,要么根本不使用闪存,要么使用不同的算法、初始向量等。 此致, 伦敦银行间同业拆借利率 (Libor) Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 首先要明确一点:一旦启用加密,当芯片上运行的程序向闪存写入数据时,写入的数据是明文,但最终存储在闪存中的是密文;当芯片上运行的程序读取闪存中的密文时,读取出来的却是明文。   基于以上观点: 然后,您的安全配置软件读取的 SB 文件是密文,通过串行 ISP 发送到芯片的工厂 ISP ROM 引导加载程序的内容也必须是密文(否则就会出现逻辑缺陷)。工厂 ISP ROM 引导加载程序将通过串口接收的密文解密为明文,然后将明文数据写入闪存,但最终存储在闪存中的数据又会被加密,变成密文。 换句话说,在 ISP 编程期间,工厂 ISP ROM 引导加载程序首先进行解密,然后再进行加密,经历一个解密再加密的往返过程。                           Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 您好, 对于 MCXN 设备: 能否对指定范围的闪存空间进行加密和签名? 高效密码学标准\(SEC\)工具: - 签署整个申请 - 加密区域在产品生命周期内只需配置一次,您需要预留空间以备将来更新(应用程序体积增大)之需。 程序在加密闪存区域内的读/写行为与之前有何不同(读取回的数据是密文吗?写入的数据是明文吗?)? 加密/解密是即时进行的。应用程序从闪存读取数据无需关心,它是透明的。关于从应用程序本身写入加密闪存区域的问题,你需要进行调查,我不确定是否存在任何注意事项。 在 OTA 升级过程中,如何使架构与芯片的加密/解密相匹配而不发生冲突? 如上所述,您需要指定合理大小的加密内存区域。如果您的应用程序超出加密区域,OTA 更新仍可运行,但只有应用程序超出加密区域的部分仍可运行,您的 IP 地址将不再受加密保护。 此致, 伦敦银行间同业拆借利率 (Libor)
記事全体を表示
S32K1_S32M24X 和 S32K1 RTD 封装有什么区别? 我正在为S32K116进行开发。 我在检查 S32DS 扩展和更新时注意到,我安装了两个 S32K1 软件包: “S32K1_S32M24X 实时驱动程序 AUTOSAR R21-11 版本 3.0.0”QLP06” 和 S32K1 实时驱动程序 AUTOSAR R21-11 版本 3.0.0QLP06“ 两者之间有什么区别? 如果他们也对我的情况这样做,我应该保留哪个/卸载哪个? 我尝试移除其中一个(S32K1),但之后我的项目就无法加载它们的 .mex 文件了。文件不再存在。 Re: Difference between S32K1_S32M24X and S32K1 RTD packages? 嗨@daniel_meier 虽然这些软件包看起来可能很相似,但它们彼此之间以及与 S32DS 之间存在依赖关系,因此不应被视为可以彼此独立使用的独立组件。 因此,我们建议重新安装该软件包,并保持两个软件包都已安装,以确保项目功能正常。 BR,VaneB
記事全体を表示
Re: S32G274A LLCE CAN The current self-developed board runs in multi-core mode. One A53 core is used for network communication tasks with other devices, and several other A53 cores run bus communication drivers, with each type of bus using a separate A53 core. A problem has arisen: the current LLCE CAN recovery operation is configured to stop and then start the LLCE CAN mode. In most actual scenarios, communication can be restored, but sometimes bus recovery is executed frequently, affecting the normal operation of other A53 cores (network communication tasks are interrupted). The questions are: what methods are available for LLCE CAN bus recovery, and why does having LLCE CAN running on a separate core still affect other cores? The version information is: S32G_LLCE_1_0_9; SW32G_RTD_4.4_4.0.2_P04_D2312 Re: S32G274A LLCE CAN Hello, @JACK_Q Hello Could you please provide a detailed description of your software and hardware testing environment? 1. In your system, are the M-core and A-core used simultaneously? What tasks does the M7 core run? Which software packages does it rely on? 2. From your description, each core on the A53 side has its own task. What software is it running? Is it a Linux BSP? BR Chenyin
記事全体を表示
S32K1_S32M24XとS32K1のRTDパッケージの違いは何ですか? 私はS32K116向けに開発を行っています。 S32DS拡張機能とdUpdatesを使っているときに、2つのS32K1パッケージがインストールされていることに気づきました: 「S32K1_S32M24X リアルタイム・ドライバ AUTOSAR R21-11 バージョン 3.0.0QLP06" および 「S32K1 リアルタイム・ドライバ AUTOSAR R21-11 バージョン 3.0.0」QLP06" この2つの違いは何ですか? もし私のケースでも同じように対応するなら、どちらを残しておくべきか、アンインストールすべきでしょうか? そのうちの1つ(S32K1)を削除してみましたが、そうするとプロジェクトが.mexファイルを読み込めなくなってしまいました。もうファイルはありません。 Re: Difference between S32K1_S32M24X and S32K1 RTD packages? こんにちは、 @daniel_meier さん。 パッケージは似ているように見えますが、互いに依存関係があり、互いに独立して使用できる独立したコンポーネントとして扱うことを意図していません。 したがって、プロジェクトの適切な機能を確保するために、パッケージを再インストールし、両方のパッケージを同時にインストールしておくことをお勧めします。 BR、VaneB
記事全体を表示
Config Tools for i.MX 26.09 Now Available We are pleased to announce that Config Tools for i.MX 26.09 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) Version 26.09 Framework Added support for downloading all boards associated with a processor when downloading the processor. DDR tool Added support for i.MX 937 Added DDR3 support for i.MX 8MP FRDM board Added support for i.MX93W FRDM and EVK boards at 3600 MT/s Enabled PMIC PF9453 support for i.MX 91 Minor improvements, enhancements, and bug fixes SerDes tool Added support for i.MX 952 System Manager Multiple validation ID issues are resolved. DDR tool – NXP-validated memory configurations for multiple vendors is available System Manager – extended CLI support for a headless setting      
記事全体を表示
MCUXpresso Config Tools 26.09 Now Available We are pleased to announce that MCUXpresso Config Tools 26.09 are now available. Downloads Also via installer in MCUXpresso for VS Code https://marketplace.visualstudio.com/items?itemName=NXPSemiconductors.mcuxpresso In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to https://docs.mcuxpresso.nxp.com/config/latest/ for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details at https://docs.mcuxpresso.nxp.com/config/latest/ Version 26.09 Framework Support public releases of “preliminary” EAR/PRC processor data. Added support for downloading all boards associated with a processor when downloading the processor.
記事全体を表示
Transformed and Quantized your model with NPU of the MX8Mplus     Introduction In this article, we will explain in this article which steps you have to take to transform and quantize your model with different TensorFlow versions. We are only looking into post training quantization. We are using the MX8MPlus EVK run our model that have a dedicated neural network accelerator IP from VeriSilicon (Vivante VIP8000). Press enter or click to view image in full size i.mx8MPlus block diagram from NXP Is the neural processing unit (NPU) from NXP need a fully int8 quantized model we have to look into full int8 quantization of a TensorFlow lite or PyTorch model. Both libraries are supported with the eIQ library from NXP. Here we will only look into the TensorFlow variant. The general overview on how to do post training quantization can be found on the TensorFlow website.  The operations for floating point are more complex than for integer (arithmetic’s, avoiding overflow). This results in the ability to use only the much simpler and smaller arithmetic units instead of the larger floating-point units. ​ ​The physical space needed for float32 operation much larger than for int8. This results in:​ Lower power consumption, ​ Less heat development, ​ The ability to join more calculation units decreasing inference time. Prerequisite To create the code on your PC first, we recommend using Anaconda with a virtual environment running Python 3.6, TensorFlow 2.x, numpy, opencv-python and pandas. Post training quantization with TensorFlow Version 2.x If you created and trained a model via tf.keras there are three similar ways of quantizing the model. First Method — Quantizing a Trained Model Directly The trained TensorFlow model has to be converted into a TFlite model and can be directly quantize as described in the following code block. For the trained model we exemplary use the updated tf,keras_vggface model based on the work of rcmalli . The transformation starts at line 28. from keras_vggface_TF.utils import preprocess_input from keras_vggface_TF.vggfaceTF import VGGFace converter.inference_output_type = tf.int8 import tensorflow as tf import numpy as np tfVersion=tf.version.VERSION.replace(".", "") # can be used as savename print(tf.version.VERSION) # TRAIN A MODEL pretrained_model = VGGFace(model='resnet50', include_top=False, input_shape=(224, 224, 3), pooling='avg') # pooling: None, avg or max #Create a generator for representative Dataset folderpath='./All_croped_images/' def prepare(img):          img = np.expand_dims(img,0).astype(np.float32)          img = preprocess_input(img, version=2) return img repDatagen=tf.keras.preprocessing.image.ImageDataGenerator(preprocessing_function=prepare) datagen=repDatagen.flow_from_directory(folderpath,target_size=(224,224),batch_size=1) def representative_dataset_gen():       for _ in range(10):       Img = datagen.next()       yield [img[0]] #CONVERT YOUR MODEL TO TFLITE AND QUANTIZE TO INT8 converter = tf.lite.TFLiteConverter.from_keras_model(pretrained_model) converter.optimizations = [tf.lite.Optimize.DEFAULT] converter.representative_dataset = representative_dataset_gen converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8] converter.experimental_new_converter = True converter.target_spec.supported_types = [tf.int8] converter.inference_input_type = tf.int8 quantized_tflite_model = converter.convert() #SAVE THE QUANTIZED MODEL AS TFLITE FILE open('quant_model.tflite' , "wb").write(quantized_tflite_model) After loading/training your model you first have to create a representative data set. The representative data set is used by the converter to get the max and min values to be able to estimate the scaling factor. This limits the error introduced by the quantization from float32 to intX. The error comes from the different number-space of float and int. Converting from float to int8 limits the number-space to integer values between -128 to 127. Calibrating the model on the dynamic range of the input limits this error. Here you can just loop through your images or create a generator as in our example. We used the tf.keras.preprocessing.image.ImageDataGenerator() to yield images and do the necessary prepossessing on the images. As a generator you can of course also use the tf.data.Dataset.from_tensors() or … from.tensor_slices(). Just keep in mind to do the same pre-processing on your data here as you did on the data you trained your network with (normalization, resizing, de-noising, …). This can all be packed into the preprocessing_function call of the generator (line 19). The conversion starts at line 28. A simple TensorFlow lite conversion would look like this: converter = tf.lite.TFLiteConverter.from_keras_model(pretrained_model) tflite_model = converter.convert() open('model.tflite' , "wb").write(tflite_model) The quantization part is in-between: converter = tf.lite.TFLiteConverter.from_keras_model(pretrained_model) converter.optimizations = [tf.lite.Optimize.DEFAULT] converter.representative_dataset = representative_dataset_gen converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8] converter.experimental_new_converter = True converter.target_spec.supported_types = [tf.int8] converter.inference_input_type = tf.int8 converter.inteference_output_type=tf.int8 quantized_tflite_model = converter.convert() open('quant_model.tflite' , "wb").write(quantized_tflite_model) Line 3 : optimizations other than default are deprecated. No other options are available at the moment (Year 2020). Line 4 : Here we set the representative data set. Line 5 : Here we make sure that we have a full conversion to int8. Without this option, only the weights and biases would be converted but not the activations. This is used when we only want to reduce the model size. However, our NPU needs full int8 quantization. Having the activations still in floating point would result in overall floating-point and could not run on the NPU. Line 6: Enables MLIR-based conversion instead of TOCO conversion, which enables RNN support, easier error tracking. Line 7: Sets the internal constant value to int8. The target_spec corresponds with the TFLITE_BUILTINS from line 5. Line 9 and 10: Set also the input to int8. This is fully available from TF 2.3 Now if we convert the model using TF2.3 with experimental_new_converter=True inference_input_type=tf.int8 inference_output_type=tf.int8 we receive the following model: However if we do not set the inference_input_type and inference_output_type we receive following model: So the effect is that you can determine which input data type the model accepts and returns. This can be important if you work with an embedded camera, as included with the MX8MPEVK. The mipi camera returns 8bit values, so if you want to spare a conversion to float32 int8 input can be handy. But be aware, if you use a model without prediction layers to gain e.g., embeddings, an int8 output will result in very poor performance. Here an output of float32 is recommended. This shows that each problem needs a specific solution. Second and Third Method — Quantize a Saved Model from *.h5 or *.pb Files If you already have your model, you most likely have it saved somewhere either as an Keras h5 file or a TensorFlow protocol buffer pb. We will quickly save our model using TF2.3: import tensorflow as tf f rom keras_vggface_TF.vggfaceTF import VGGFace pretrained_model = VGGFace(model='resnet50', include_top=False, input_shape=(224, 224, 3), pooling='avg') # pooling: None, avg or max # Saving as a protocol buffer !mkdir -p saved_model pretrained_model.save('saved_model/my_model') #saving as a h5 file (if your Tensorflow Version is < 2.0 use this) !mkdir -p keras_model pretrained_model.save('keras_model/my_model.h5') Following the conversion and quantization is very similar as in Method One. The only difference is how we load the model in with the converter. Either load the model and continue as in Method One. #Load the h5 model pretrained_model = tf.keras.models.load_model('my_model.h5') #Then use the converter as before converter = tf.lite.TFLiteConverter.from_keras_model(pretrained_model) Or load the h5 model directly. When using TensorFlow version 2 and above you have to use a compatible converter: # Or load the h5 model from file # TensorFlow version >2.x converter = tf.compat.v1.lite.TFLiteConverter.from_keras_model_file(saved_model_dir + h5_modelname) #works now also with TF2.x # TensorFlowversion < 2.0 converter = tf.lite.TFLiteConverter.from_keras_model_file(saved_model_dir + h5_modelname) If you load from a TensorFlow pb file use: # Or load the pb file from the modelfolder # TensorFlow version >2.x converter = tf.lite.TFLiteConverter.from_saved_model(saved_model_dir) # the folder contains the pb file and a assets and variables folder Converting with TensorFlow Versions below 2.0 If you want to convert a model written in TensorFlow version < 1.15.3 using Keras, not all options are available for TFlite conversion and quantization. The best way is to save the model with the TensorFlow version it was created in (e.g., rcmalli keras-vggface was trained in TF 1.13.2). I would suggest not using the “saving and freeze graph” method to create a pb file as the pb files differ between TF1 and TF2. The TFLiteConverter.from_saved_model does not work, creating quite a hassle to achieve quantization. I would suggest using the above mentioned method using Keras: import keras …. pretrained_model.save('my_model.h5') Then convert and quantize your model with a TensorFlow version from 1.15.3 onward. From this version on a lot of functions where added in preparation for TF2. I suggest using the latest version. This will result in the same models presented here.          
記事全体を表示
LPC54608 内部温度センサー ユーザーマニュアルに記載されているように内部温度センサ用にADCを設定しようLPC54608が、正しい値を読み取ることができませんでした。データシートに記載されている傾きとオフセットの値も使用しました。 Re: LPC54608 Internal temperature sensor Hello ADCの例をベースに使ったことがあるか確認していただけますか?もしそうなら、どの作品かを示してください。 入力ADCチャネル0と入力選択レジスタを3に設定して温度センサーを選択できるようにしましたか? 詳細については、LPC546xxユーザーマニュアルの第44.6.2章[UM10912]をご参照ください。 もしADC温度センサーをどのように設定したのか、もう少し詳しく教えていただければ教えてください。 LPC546xx製品データシート第7.22章によると、 「電源アップ後、温度センサの出力は安定した値に落ち着くまで待たなければ、正確なADC入力として使用できません。ADCによる温度センサの正確な測定のためには、ADCをシングルチャネルバーストモードに設定する必要があります。9回以上の変換バーストの最後の値が正確な結果を提供します。」したがって、温度センサがまだ安定していないか、単一チャネルバーストモードでさらに変換が必要な可能性があります。 また、外部環境に関連するADC誤差を最小限に抑えるために、ADC外部回路の最適化も検討すべきです。 この応用ノートは、アプリケーションにおけるアナログ-デジタル変換器の精度を高める方法に役立ちます 敬具、ルイス Re: LPC54608 Internal temperature sensor 私は以下のように設定しました。 1. ADC、VREFP、VDDA、TS、ANAをクリアし、20μs待機します。 2. ADCクロック有効化、AHBCLKCTRL0。 3. PRESETCTRL0レジスタを使ってADC0ペリフェラルリセットをクリアする 4. INSELで温度チャネルを設定する 5. ADCを有効にし、制御レジスタのCLKDIVを使用してクロックを15MHzに設定します。 5. 同期モード、12ビット分解能、BYPASS = 0、TSAMP = 0 に設定します。 6. 次にシーケンスAをSEQA_CTRLで構成します。チャネル = 1、TRIGGER = 0、TRIGPOL = 0、SYNCBYPASS = 0、BURST = 0、SINGLESTEP = 0、LOWPRIO = 0、MODE = 0、SEQA_ENA = 1 7. CALIB = 1 に設定し、CALIB = 0 になるまで待機する 8. 次にSTARTビットで変換を開始し、結果を読み取る しかし、結果は毎回同じで、DATA VALID は設定されていません。
記事全体を表示