IMX93 - Poky - Error on U-Boot configuration fspi Hello NXP experts, I am following "UG10164, i.MX Yocto Project User's Guide, Rev. LF6.12.3_1.0.0 — 31 March 2025". I have to configure u-boot with uboot_config_imx93evk="sd fspi" as showed in chapter "5.5 U-Boot configuration". As suggested i runned the command: echo "UBOOT_CONFIG = \"sd fspi\"" >> conf/local.conf and after i runned bitbake core-image-minimal. An error is raised during the bitbake: ERROR: Nothing PROVIDES 'virtual/bootloader' (but /home/imx-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb DEPENDS on or otherwise requires it) u-boot-qoriq PROVIDES virtual/bootloader but was skipped: incompatible with machine imx93-11x11-lpddr4x-evk (not in COMPATIBLE_MACHINE) u-boot PROVIDES virtual/bootloader but was skipped: The selected UBOOT_CONFIG key ['sd', 'fspi'] has no match in dict_keys(['sd', 'ecc', 'ld']). u-boot-fslc PROVIDES virtual/bootloader but was skipped: The selected UBOOT_CONFIG key ['sd', 'fspi'] has no match in dict_keys(['sd', 'ecc', 'ld']). u-boot-imx PROVIDES virtual/bootloader but was skipped: The selected UBOOT_CONFIG key ['sd', 'fspi'] has no match in dict_keys(['sd', 'ecc', 'ld']). edk2-firmware PROVIDES virtual/bootloader but was skipped: incompatible with machine imx93-11x11-lpddr4x-evk (not in COMPATIBLE_MACHINE) u-boot-variscite PROVIDES virtual/bootloader but was skipped: incompatible with machine imx93-11x11-lpddr4x-evk (not in COMPATIBLE_MACHINE) u-boot-toradex PROVIDES virtual/bootloader but was skipped: incompatible with machine imx93-11x11-lpddr4x-evk (not in COMPATIBLE_MACHINE) u-boot-imx PROVIDES virtual/bootloader but was skipped: The selected UBOOT_CONFIG key ['sd', 'fspi'] has no match in dict_keys(['sd', 'ecc', 'ld']). u-boot-kontron PROVIDES virtual/bootloader but was skipped: incompatible with machine imx93-11x11-lpddr4x-evk (not in COMPATIBLE_MACHINE) u-boot-qoriq PROVIDES virtual/bootloader but was skipped: incompatible with machine imx93-11x11-lpddr4x-evk (not in COMPATIBLE_MACHINE) u-boot-boundary PROVIDES virtual/bootloader but was skipped: incompatible with machine imx93-11x11-lpddr4x-evk (not in COMPATIBLE_MACHINE) edk2-firmware PROVIDES virtual/bootloader but was skipped: incompatible with machine imx93-11x11-lpddr4x-evk (not in COMPATIBLE_MACHINE) ERROR: Required build target 'core-image-minimal' has no buildable providers. Missing or unbuildable dependency chain was: ['core-image-minimal', 'virtual/bootloader']. This is my local.conf file: MACHINE ??= 'imx93-11x11-lpddr4x-evk' DISTRO ?= 'fsl-imx-wayland' EXTRA_IMAGE_FEATURES ?= "debug-tweaks" USER_CLASSES ?= "buildstats" PATCHRESOLVE = "noop" BB_DISKMON_DIRS ??= "\ STOPTASKS,${TMPDIR},1G,100K \ STOPTASKS,${DL_DIR},1G,100K \ STOPTASKS,${SSTATE_DIR},1G,100K \ STOPTASKS,/tmp,100M,100K \ HALT,${TMPDIR},100M,1K \ HALT,${DL_DIR},100M,1K \ HALT,${SSTATE_DIR},100M,1K \ HALT,/tmp,10M,1K" PACKAGECONFIG:append:pn-qemu-system-native = " sdl" CONF_VERSION = "2" DL_DIR ?= "${BSPDIR}/downloads/" ACCEPT_FSL_EULA = "1" # Switch to Debian packaging and include package-management in the image PACKAGE_CLASSES = "package_deb" EXTRA_IMAGE_FEATURES += "package-management" UBOOT_CONFIG = "sd fspi" What am I missing? Regards, Alessandro Yocto Project Re: IMX93 - Poky - Error on U-Boot configuration fspi thanks for the support! Re: IMX93 - Poky - Error on U-Boot configuration fspi HI @il_ciancio!
By default is not possible you should do some modifications and we can't validate the image due to the evk board doesn't have fspi installed.
Best Regards!
Chavira Re: IMX93 - Poky - Error on U-Boot configuration fspi Ciao @Chavira. I have a question, maybe I am misunderstanding something. I am working with a custom board without eMMC or SD card and It has only a SPI NOR FLASH, the goal is to boot starting from data inside the SPI memory on target IMX93. There is also this ticket: all(bootloader, device tree, Linux kernel, rootfs) all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek - NXP Community It is made a custom UUU script in order to flash data in SPI memory: uboot; dtb; kernel; rootfs; the flash goes well because it is checked raw data read from spi memory. After the boot, It is read data from SPI and putted in ram (like a bridge), some env vars are setted and after with the command booti: booti ${loadaddr} ${initrd_addr} ${fdt_addr} the kernel should boot. Why did you write "then use the rootfs flashed in eMMC or SD card."? Is it mandatory that rootfs must be in sd/emmc? I hope that I am clear. Thanks a lot! Re: IMX93 - Poky - Error on U-Boot configuration fspi Hi @il_ciancio!
You can't flash the rootfs in the flash memory.
You can boot from fspi and then use the rootfs flashed in eMMC or SD card.
Best Regards!
Chavira Re: IMX93 - Poky - Error on U-Boot configuration fspi Hi @Chavira , congratulation, great job! Now the bitabake is finished and i have u-boot*fspi files in my deploy directory. Just for clarification, which are the kernel/rootfs image "compatible" with fspi? It is always the *.wic file? thanks a lot and again great work! Re: IMX93 - Poky - Error on U-Boot configuration fspi Hi @il_ciancio!
I found the problem!
For some reason the fspi configuration is not included.
You have to add the next lines in the imx93-11x11-lpddr4x-evk.conf file.
UBOOT_CONFIG[fspi] = "${UBOOT_CONFIG_BASENAME}_defconfig"
IMXBOOT_TARGETS_FSPI = "flash_singleboot_flexspi"
IMXBOOT_TARGETS = "${@bb.utils.contains('UBOOT_CONFIG', 'fspi', '${IMXBOOT_TARGETS_FSPI}', 'flash_singleboot', d)}"
after that you can maintain the line UBOOT_CONFIG = "sd fspi" in local.conf file to deploy both images.
Best Regards!
Chavira Re: IMX93 - Poky - Error on U-Boot configuration fspi Hi @Chavira, with UBOOT_CONFIG ??= "sd fspi" the bitbake is finished, but in the output folder there is *.wic file but there isn't a Flex-SPI u-boot binary image. Is there something else? How is the result of your build? Re: IMX93 - Poky - Error on U-Boot configuration fspi Hi @il_ciancio!
Thank you for contacting NXP Support!
I am compiling now.
Try changing UBOOT_CONFIG = "sd fspi" to UBOOT_CONFIG ??= "sd fspi" in the local.conf file.
Best Regards!
Chavira
記事全体を表示