2075299_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2075299_en-US

2075299_en-US

P2020: PCIe PME Link Down Detection (LDD) Interrupt

Hello,

I'm using the P2020 PCIe controller as a host. I try to get an interrupt if a connected device resets itself so that I can re-initialize it. As far as I understand theLDD flag in the PEX_PME_MES_DR, that should be more or less exactly what I search: It detects if the link goes down. In my test case, I can also see that the LDD flag is set in that register. But I don't seem to get an interrupt.

The PEX_PME_MES_DISR[LDDD] is set to 0. I don't really need a message but I don't really care if one is sent either. The PEX_PME_MES_IER[LDDIE] is set to 1. I would have expected that with this some interrupt is generated.

I would have expected that the PCI Express interrupt is triggered (PIC Internal Interrupt number 8 to 10 for PEX3 to 1). But I don't receive that. So I checked all of the other interrupt configuration registers and there doesn't seem to be any active flag set (A bit in the *IVPR*).

What is necessary that the interrupt is generated? Is this kind of interrupt signaled as a MSI so that I need MSI support for it? Is there some other mask or gate for that interrupt that I might have missed?

With kind regards

Christian Mauderer

QorIQ P2 DevicesRe: P2020: PCIe PME Link Down Detection (LDD) Interrupt

I found a problem with the interrupt configuration. So the problem is solved now.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:37 PM
更新者: