2076269_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2076269_en-US

2076269_en-US

IMX.93 LVDS single channel, four lanes

Greetings,

Does the IMX93 support a configuration which has less than four LVDS lanes?

I have an LVDS to RGB  device which we would like to use, but it only supports three lane configurations, single lane (D0), two lanes (D0 and D1), or three lanes (D0, D1 and D2), but no four lane configuration.

Thanks in advance,

Ken




Re: IMX.93 LVDS single channel, four lanesThank you
Ken
Re: IMX.93 LVDS single channel, four lanes

Hello @ken_carlson 


I hope you are doing very well.


Unfortunately there is not way to configure the Data-Lanes on the LVDS or LDB control registers of i.MX93.

Best regards,

Salas.

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 09:36 PM
更新人: