Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
デバイス統合(ソフトウェア)MFRC531 01T用 NXP Mifareリーダー(crypto1)MFRC531 01Tと統合する必要があり、SIDのポーリング、認証、ブロック/セクターの読み取りを行うためのRS232経由の関連プロトコルコマンドについてサポートが必要です。 Re: Device Integration (Software) for MFRC531 01T こんにちは@Menspa 残念ながら、NXPはMFRC531に基づくデモ例を提供していません。したがって、MFRC531データシート(標準ISO/IEC 14443 A/BリーダーソリューションMFRC531を参照し、NXPのライブラリNxpNfcRdLibを使用してカード読み書きアプリケーションを開発する必要があります。
View full article
secure_provisioning 工具烧写 sb格式 加密签名文件后无法用mcu link debug After flashing an SB-format encrypted and signed file with the Secure Provisioning tool, debugging via MCU-Link is no longer possible. justdomyself_0-1790073326861.png justdomyself_1-1790073357176.png when  I  use    mcuexpress  debug my code , error happended: justdomyself_2-1790073419631.png Can my this  board  recover to it's old state to  use zhe  debug function? Re: secure_provisioning 工具烧写 sb格式 加密签名文件后无法用mcu link debug Hi @justdomyself  > So, can I use the Secure Provising tool to make a new lisence, to cmobine a new signed and encrypted sb format file to write to the chip? Yes, Secure Provisioning tool is designed to provision chip, i.e. install secure assets (keys), build signed or encrypted application bootable image and install into the flash. Re: secure_provisioning 工具烧写 sb格式 加密签名文件后无法用mcu link debug @liborukropec   Thanks a lot.  I have resolve my question。 justdomyself_0-1790128360736.png I  have another question : As above picture,  This  erase operation has  erased  ful of the memory chip . So,   can  I  use  the Secure Provising tool to make a new  lisence, to cmobine a new  signed  and encrypted  sb format file  to write to the chip? Re: secure_provisioning 工具烧写 sb格式 加密签名文件后无法用mcu link debug Hi, if you configure ROM to execute only signed images and then you write application from VSCode (or other IDE) unsigned image, ROM refuses from running. Also, if you advance the Life Cycle, then the debugger can be opened only via Debug Authentication (see documentation). In case you did not advance life cycle (on the tool bar), you should be able to erase CMPA. Simplest should be using debug probe and on the Write tab use the "Erase whole chip..." button. liborukropec_0-1790086908628.png After power cycle you should be able to debug again. Regards, Libor
View full article
Step-by-Step Process to Buy a Ready 4 Bed Apartment in Emaar Beachfront Emaar Beachfront has quickly become one of Dubai's most sought-after waterfront destinations, and demand for a 4 bed apartment for sale ready to move Emaar Beachfront continues to grow among families and investors alike. If you are considering purchasing a spacious, move-in-ready home in this island community, understanding the buying process from start to finish will help you avoid delays and make confident decisions. This guide walks you through every stage of buying a ready 4 bedroom apartment in Emaar Beachfront, with practical insights from Takween AlDar, a trusted real estate company in Dubai. Why Emaar Beachfront Appeals to Buyers of Ready 4 Bed Apartments Emaar Beachfront sits between Dubai Marina and Palm Jumeirah, offering private beach access, resort-style facilities, and skyline views. A ready 4 bed apartment here suits larger families who want more living space without waiting years for construction to finish. Since the unit is already built and handed over, buyers can inspect the actual property, move in quickly, and start generating rental income sooner if they choose to lease it out. Step 1: Define Your Budget and Financing Options Before browsing listings, work out how much you can realistically spend. A 4 bedroom apartment in Emaar Beachfront is a premium purchase, so factor in the full cost picture, not just the listing price. Consider the following: Down payment requirements, typically 20 to 25 percent for expats Mortgage pre-approval from a UAE bank if financing is needed Dubai Land Department transfer fee, generally 4 percent of the purchase price Agency commission, usually 2 percent Ongoing service charges tied to the building and community Getting mortgage pre-approval early gives you a clear budget ceiling and strengthens your position when negotiating with sellers. Step 2: Shortlist Ready Units in Emaar Beachfront Once your budget is set, start identifying ready 4 bed apartments that match your needs. Since Emaar Beachfront includes several towers such as Beach Vista, Sunrise Bay, and Beach Isle, availability and layouts can vary significantly between buildings. Working with a knowledgeable agency like Takween AlDar helps narrow down options based on floor level, view, layout efficiency, and proximity to amenities, rather than relying only on online listings that may not reflect current inventory. Step 3: Schedule Property Viewings Unlike off plan purchases, a ready apartment allows you to physically walk through the unit before committing. Use viewings to check: Actual room sizes and layout flow Quality of finishes and fittings Natural light and view orientation Condition of common areas, elevators, and parking If the unit was previously occupied, ask about maintenance history and any recent repairs. Step 4: Verify Ownership and Property Documents Before making an offer, confirm the seller's ownership through the Dubai Land Department and request the title deed. Your agent should also check for any outstanding mortgages, service charge arrears, or legal disputes tied to the property. This verification step protects you from complications later in the transaction. Step 5: Negotiate and Sign the Memorandum of Understanding Once you are satisfied with the property and its documentation, submit an offer. If accepted, both parties sign a Memorandum of Understanding, commonly known as Form F, through the Dubai Land Department's Trakheesi system. At this stage, you typically pay a deposit, often around 10 percent of the purchase price, which is held until the transfer is finalized. Step 6: Obtain the No Objection Certificate The seller must request a No Objection Certificate from the developer, in this case Emaar. This certificate confirms there are no outstanding payments or restrictions on the property and clears the way for ownership transfer. Processing usually takes a few working days and involves a fee paid to the developer. Step 7: Complete the Transfer at the Dubai Land Department With the No Objection Certificate in hand, both buyer and seller attend the Dubai Land Department office, or a registered trustee center, to finalize the transfer. At this appointment, you pay the remaining balance, the transfer fee, and any applicable charges. Once complete, the title deed is issued in your name, officially making you the owner of the apartment. Step 8: Set Up Utilities and Move In After the transfer, register with DEWA for electricity and water, and activate any community services tied to the building. Since the apartment is ready and move-in ready, you can begin the handover process, collect keys, and plan your move without waiting for construction completion. How Takween AlDar Supports Your Purchase Buying a 4 bed apartment for sale ready to move Emaar Beachfront involves multiple steps, and having an experienced partner reduces stress and risk. Takween AlDar guides buyers through property selection, document verification, negotiation, and transfer, ensuring a transparent and well-managed process from first viewing to final handover.  FAQ Q: How long does it take to buy a ready apartment in Emaar Beachfront? A: The process typically takes two to four weeks from signing the Memorandum of Understanding to completing the title deed transfer, assuming financing and documentation are in order. Q: Can foreigners buy a 4 bedroom apartment in Emaar Beachfront? A: Yes, Emaar Beachfront is located in a freehold area, allowing full foreign ownership for buyers from any nationality. Q: Do I need a mortgage pre-approval before viewing properties? A: It is not mandatory, but having pre-approval helps you understand your budget and makes your offer more credible to sellers. Q: What fees should I budget for beyond the purchase price? A: Expect to pay a 4 percent Dubai Land Department transfer fee, a 2 percent agency commission, and possible NOC processing fees from the developer. Q: Is a ready apartment a better option than an off plan unit in Emaar Beachfront? A: A ready apartment allows immediate move-in and physical inspection before purchase, while off plan units may offer lower entry prices but require waiting for handover. Conclusion Purchasing a ready 4 bed apartment in Emaar Beachfront is a structured process that rewards careful planning, from setting a realistic budget to verifying documents and completing the transfer at the Dubai Land Department. With the right guidance, buyers can move through each step confidently and settle into their new waterfront home without unnecessary delays. Takween AlDar is available to support you at every stage of this journey, from your first property search to the final handover.
View full article
在 Emaar Beachfront 购买一套现房四卧公寓的详细步骤 Emaar Beachfront 已迅速成为迪拜最受欢迎的海滨目的地之一,无论是家庭还是投资者,对 Emaar Beachfront 现房出售的 4 居室公寓的需求都在持续增长。如果您正在考虑在这个岛屿社区购买一套宽敞、拎包入住的房屋,了解从头到尾的购买流程将有助于您避免延误并做出自信的决定。 本指南将带您了解在 Emaar Beachfront 购买一套现房四居室公寓的每一个步骤,并提供来自迪拜值得信赖的房地产公司 Takween AlDar 的实用见解。 伊玛尔海滨公寓为何吸引四卧现房买家 Emaar Beachfront 位于迪拜码头和棕榈岛之间,提供私人海滩通道、度假村式设施和天际线景观。这里一套现成的四居室公寓适合想要更多居住空间的大家庭,无需等待数年才能完成建设。由于该单元房已经建成并交付,买家可以实地考察房产,快速入住,如果选择出租,还可以更快地开始产生租金收入。 第一步:确定预算和融资方案 在浏览房源之前,先确定自己实际能负担得起的金额。Emaar Beachfront 的四居室公寓是一笔高端投资,因此要考虑全部成本,而不仅仅是挂牌价格。 考虑以下内容: 首付要求,外籍人士通常为20%至25%。 如果需要融资,需获得阿联酋银行的抵押贷款预批函。 迪拜土地局过户费,通常为购买价格的4%。 代理佣金,通常为2%。 与建筑物和社区相关的持续服务费 尽早获得抵押贷款预批可以让你明确预算上限,并在与卖家谈判时增强你的地位。 第二步:筛选伊玛尔海滨公寓的现成单元 确定预算后,就可以开始寻找符合您需求的现成四居室公寓了。由于 Emaar Beachfront 包括 Beach Vista、Sunrise Bay 和 Beach Isle 等多个塔楼,因此不同建筑物的可用性和布局可能存在很大差异。 与像 Takween AlDar 这样知识渊博的代理机构合作,可以根据楼层、景观、布局效率和便利设施的距离来缩小选择范围,而不是仅仅依赖于可能无法反映当前存货的在线列表。 步骤三:安排房产看房 与期房购买不同,现房公寓允许您在做出决定前亲自参观房屋。利用实地考察来确认: 实际房间尺寸和布局流程 饰面和配件的质量 自然光线和视野方向 公共区域、电梯和停车场的状况 如果该单元之前有人居住,请询问维修记录和最近的维修情况。 第四步:核实所有权和房产文件 在出价之前,请通过迪拜土地局确认卖方的所有权,并索取产权证。您的经纪人还应检查该房产是否存在未偿还的抵押贷款、服务费欠款或法律纠纷。此验证步骤可保护您免受后续交易中可能出现的问题的影响。 第五步:协商并签署谅解备忘录 如果您对房产及其相关文件感到满意,即可提交报价。如果接受,双方将通过迪拜土地局的 Trakheesi 系统签署谅解备忘录(通常称为 F 表格)。在这个阶段,您通常需要支付一笔定金,通常约为购买价格的 10%,这笔定金将被保留到过户完成为止。 第六步:取得无异议证明 卖方必须向开发商(在本例中为 Emaar)索取无异议证明。该证明确认该房产没有任何未付清的款项或限制,并为所有权转移扫清了障碍。处理通常需要几个工作日,并且需要向开发商支付费用。 第七步:在迪拜土地局完成过户手续 买方和卖方在拿到无异议证明后,前往迪拜土地局办公室或注册信托中心完成产权过户手续。在本次预约中,您需要支付剩余款项、转账费以及任何适用的费用。一旦完成,产权证将以您的名义颁发,您正式成为该公寓的所有者。 第 8 步:开通水电煤气等公用设施并搬入 过户后,向迪拜水电局 (DEWA) 登记开通水电,并激活与该建筑物相关的任何社区服务。由于公寓已经准备就绪,可以立即入住,您可以开始办理交房手续、领取钥匙并计划搬家,无需等待施工完成。 Takween AlDar 如何支持您的购买 购买一套可拎包入住的 Emaar Beachfront 四居室公寓涉及多个步骤,而拥有经验丰富的合作伙伴可以减少压力和风险。Takween AlDar 为买家提供房产选择、文件核实、谈判和过户方面的指导,确保从首次看房到最终交房的整个过程透明且管理有序。 常见问题解答 问:在Emaar Beachfront购买一套现房公寓需要多长时间? 答:从签署谅解备忘录到完成产权过户,通常需要两到四周时间,前提是融资和文件齐全。 问:外国人可以在Emaar Beachfront购买四居室公寓吗? 答:是的,Emaar Beachfront 位于永久产权区域,允许任何国籍的买家拥有完全的外国所有权。 问:看房前我需要获得贷款预批吗? 答:虽然不是强制性的,但事先获得批准可以帮助您了解自己的预算,并使您的报价对卖家更具可信度。 问:除了购买价格之外,我还应该预留哪些费用预算? 答:预计需支付 4% 的迪拜土地局过户费、2% 的代理佣金,以及开发商可能收取的无异议证明 (NOC) 处理费。 问:在 Emaar Beachfront,现房公寓是否比期房公寓更好? 答:现房公寓允许立即入住,并在购买前进行实地考察,而期房单元可能提供较低的入门价格,但需要等待交房。 结束语 在 Emaar Beachfront 购买一套现成的 4 居室公寓是一个结构化的过程,需要周密的计划,从制定合理的预算到核实文件,再到在迪拜土地局完成过户。在正确的指导下,买家可以自信地完成每一步,顺利入住他们的新海滨住宅,避免不必要的延误。从您开始寻找房产到最终交房,Takween AlDar 将全程为您提供支持。
View full article
S32 Design Studio for Power Architecture、バージョン2.1ライセンス S32 Design Studio for Power Architecture バージョン2.1のライセンスが切れています。更新や新しい申請を手伝ってもらえますか? F379-CD5D-DAD1-7708 Re: S32 Design Studio for Power Architecture, version 2.1 license こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。 Re: S32 Design Studio for Power Architecture, version 2.1 license こんにちは、 更新を申請しました。 よろしくお願いいたします。 ピーター
View full article
S32 Power Architecture 设计工作室,版本 2.1 许可 我的 S32 Design Studio for Power Architecture 2.1 版许可证已过期。请问您能帮我续期或者申请新卡吗? F379-CD5D-DAD1-7708 Re: S32 Design Studio for Power Architecture, version 2.1 license 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。 Re: S32 Design Studio for Power Architecture, version 2.1 license 你好, 我已经申请续约。 顺祝商祺! Peter
View full article
S32 Design Studio for Power Architecture, version 2.1 license My license for S32 Design Studio for Power Architecture version 2.1 has expired. Could you help me renew it or apply for a new one. F379-CD5D-DAD1-7708 Re: S32 Design Studio for Power Architecture, version 2.1 license Hi,  your S32DS license has been extended. Please activate S32DS again with your old code.  Re: S32 Design Studio for Power Architecture, version 2.1 license Hello, I have asked for renewal. Best regards, Peter
View full article
我可以在哪里获取AN12064文件? 我可以在哪里获取AN12064文件? 评估板
View full article
MCSPTR2AK396——旋转变压器的激励极限? 你好!我正在使用 MCSPTR2AK396 开发套件(S32K396,带旋转变压器的三相 PMSM,3 并联 FOC)。我使用的是标准的解析器到数字信号链:SGEN → SDADC → DSPSS → eTPU 解析器函数。 据我了解,标准激励频率为 10 kHz(SGEN 正弦波驱动旋转变压器激励绕组),eTPU 旋转变压器每 50 µs 处理一次角度更新,使用来自 SDADC 的 16+16 采样缓冲器,并通过慢速 PI 调节器调整激励相移。但我还有一些疑问。 MCSPTR2AK396 套件中使用的具体解析器型号是什么?提供数据手册参考资料将非常有帮助。 该旋转变压器的最大激励频率是多少?例如,能否在不修改 SGEN 寄存器以外的任何内容的情况下,将 SGEN 提高到 100 kHz?或者 SDADC/DSPSS/eTPU 链或模拟正弦/余弦滤波器是否施加了远低于此的硬性限制? 旋转变压器本身允许的最小激励频率是多少?推荐的频率范围是多少? 如果可以提高激励强度,还需要重新配置哪些参数——SDADC 采样率、DMA 缓冲区传输、eTPU HSR 速率、激励相移调节器增益、模拟滤波器? 谢谢! Re: MCSPTR2AK396 — resolver excitation limits? 你好, MCSPTR2AK396 套件中使用的具体解析器型号是什么? 在 TG Drives 电机制造商的网站上,有一个配置器列出了三种可能的旋转变压器选项:ER5Kd411、TS2620N21E11 和 RE-15-1-A15。 如果我没记错的话,当时要求的是成本最低的解析器方案,也就是 ATAS Náchod 公司的 ER5Kd411。 https://www.atas.cz/files/ER5Kd.pdf 打开后盖即可确定具体型号。 MCSPTR2AK396 旋转变压器解决方案是在 10 kHz 激励下设计和验证的。根据应用说明,虽然 SGEN 支持高达 50 kHz 的频率,但高于 10 kHz 的操作需要重新配置和验证 SDADC、DSPSS、DMA、eTPU 解析器处理和模拟信号调理链。此外,对于 TS2620N21E11 等旋转变压器,我们只找到了已公布的标称激励规格为 10 kHz 时 7 Vrms;在可用的旋转变压器数据表中没有指定支持的激励频率范围。因此,根据现有资料,不建议在 100 kHz 频率下运行。 顺祝商祺! Peter Re: MCSPTR2AK396 — resolver excitation limits? 明白了,谢谢。将基频 PWM 生成频率提高到 20–30 kHz 是否具有实际可行性,还是该系统严格受限于该套件的硬件物理特性?
View full article
ls1043a - Linux BSP 中是否应该启用 thermal_zone5? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我正在使用 ls1043 处理器的参考板 ls1043ardb,遇到了散热子系统的问题。我看到的错误是: [ 116.704475] thermal thermal_zone5:已达到临界温度 (104°C),正在关闭 虽然看起来有点零星,但一旦出现,通常会在启动后不久发生。它并非总是发生。当系统稳定时,thermal_zone5 的温度始终为 0。 dts 文件 fsl-ls1043a.dtsi 中已激活 thermal_zone0 - thermo_zone5。( fsl-ls1043a.dtsi\freescale\dts\boot\arm64\arch - qoriq-components/linux - 用于 QorIQ 支持的 Linux 树) 问题是 ls1043 是否应该启用 thermal_zone5?查阅“QorIQ LS1043A 参考手册,修订版 5,04/2019”第 35.1.1 章“本地温度传感器位置”,我可以看到一个表格,其中指出 ls1043 的温度传感器 ID 为 0-4,而 ID 5-15 被标记为保留。hte dtsi 文件是否启用 thermal_zone5,并且在 ls1043 中是否可用? 谢谢, 彼得 Re: ls1043a - should thermal_zone5 be active in the Linux BSP? 你好, 我们在运行 Linux 4.19.68 的 LS1043A 平台上也遇到了类似的问题。 系统偶尔会报告: Thermal_zone5:温度已达临界值(104℃),正在关闭   观察发现,热区 0-4 通常彼此密切相关,而热区 5 经常报告明显不同的值,并且与其他区域的行为不同。   停机前,各热区报告的值与以下值类似: thermal_zone0: 75000 thermal_zone1:76000 thermal_zone2:76000 thermal_zone3:75000 thermal_zone4:74000 thermal_zone5:0 NXP 在之前的回复中提到 thermal_zone5 的值不确定,并将在未来的 LSDK 版本中提供修复程序。 请问这个问题是否已经修复?如果已修复,请问是哪个 LSDK/内核版本包含了该修复? 谢谢。 Re: ls1043a - should thermal_zone5 be active in the Linux BSP? 我在最新的LSDK 20.12(内核版本5.4.47)上也遇到了类似的问题。 [ 2115.927267] thermal thermal_zone1:已达到临界温度(85°C),正在关闭 [ 2116.951246] thermal thermal_zone1:已达到临界温度(85°C),正在关闭 [ 2117.975285] thermal thermal_zone1:已达到临界温度(85°C),正在关闭 请问是否有任何变通方法可以解决这个问题? 这个问题的根本原因是什么? Re: ls1043a - should thermal_zone5 be active in the Linux BSP? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我们已确认该问题,目前热区 5 报告的值不确定,可能会在任何随机时间点导致此类问题。我们将在即将发布的 LSDK 版本中提供正式修复程序。 目前你可以从 dtsi 中移除热区 5,看看是否有帮助。
View full article
燃える導火線 IMXRT1024には、ボードをシリアルダウンローダーモードにすることなく(JTAGやUARTなどを介して)ヒューズを焼却する機能はありますか? Re: Burning fuse こんにちは、 @Abhay2080。 OCOTPモジュールを使えば、 リファレンスマニュアルの23.6.1.2.2章「機能」に記載されているように、ソフトウェアを通じてヒューズを焼くことができます。動作については、SDK(バージョン26.06)の例「ocotp_example」を参照してください。SDK Builderを通じて見つけることができます。 23.3.1.2も参照してください。ヒューズとシャドウレジスタの読み取りと23.3.1.3フューズレジスタとシャドウレジスタは、追加情報を提供するセクションをRMに書き込みます。 BR ハビブ Re: Burning fuse 私の調査によると、ヒューズを焼く方法について 1. SPT(最もシンプル) - ただし、起動モードをISPに変更し、UARTかUSBインターフェースが必要です。 2. CST(製造ツール) - ここでも起動モードをISPに変更し、USBインターフェースが必要です。 3. あなたが言及したOCOTPモジュールを経由します - ISPを入れる必要はなく、署名のないイメージ(OCOTPドライバとヒューズを焼き捨てる)をフラッシュしてヒューズを焼き、基板をロックします 私の理解は正しいでしょうか?それともJTAGやSWDのようなプログラム方法が他に見落としているのでしょうか Re: Burning fuse こんにちは、 @Abhay2080 さん。 OCOTPモジュールはシリアルダウンローダーモードに入らずに使用できます。例えば、この コミュニティ投稿 ではケリーがこの別のヒューズプログラミング方法について説明しています。 ヒューズの焼きは一度きりなので、慎重に燃やしてください。 Secure Provisioning Toolは、選択した構成に基づいて必要な値を決定し、正しいヒューズがプログラムされているかを確認するためのガイドとして利用できます。ヒューズとその目的の詳細な説明については、RMの9.4.1章「ブートeFuseの説明」もご参照ください。 BR ハビブ
View full article
Where can I obtain the AN12064 document? Where can I obtain the AN12064 document? Evaluation Board
View full article
Burning fuse In IMXRT1024 is there any provision to burn fuses without putting the board into serial downloader mode through(may be through JTAG or UART) Re: Burning fuse Hello @Abhay2080, You can burn fuses through software using the OCOTP module, as mentioned in the chapter 23.6.1.2.2 "Function" of the Reference Manual.  Please refer to the SDK (version 26.06) example called ocotp_example in order to know how it works. You can find through SDK Builder. Please also refer to 23.3.1.2 Fuse and Shadow Register Read and 23.3.1.3 Fuse and Shadow Register Writes sections in the RM which provides additional information. BR Habib Re: Burning fuse As per my research to burn fuses 1. SPT(simplest) - But we need to change boot mode to ISP and need either UART or USB interface. 2. CST(Mfg tool) - Here also we need to change boot mode to ISP and need USB interface. 3. Through OCOTP module as you mentioned - No need to put in ISP just flash unsigned image (OCOTP drivers and fuses to burn) and burn fuses and then board is locked Is my understanding correct or i am missing some more ways like through JTAG/SWD we can program Re: Burning fuse Hello @Abhay2080, You can use the OCOTP module without entering Serial Downloader Mode. For example, in this community post Kerry describes this alternative method for programming fuses. Please keep in mind that burning fuses can only be done once, so please burn with caution. The Secure Provisioning Tool can help determine the required value based on the configuration you select, which you can use as guide for ensuring that the correct fuses are programmed. Please also refer to chapter 9.4.1 "Boot eFuse Descriptions" in the RM, which provides a detailed description of fuse and its purpose. BR Habib
View full article
烧断的熔丝 IMXRT1024是否有办法在不将电路板置于串行下载器模式的情况下(例如通过JTAG或UART)烧毁熔丝? Re: Burning fuse 你好@Abhay2080 , 您可以使用 OCOTP 模块通过软件烧断熔丝,如参考手册第 23.6.1.2.2 章“功能”中所述。请参考名为 ocotp_example 的 SDK(版本 26.06)示例,以了解其工作原理。您可以通过SDK Builder找到它。 另请参阅 23.3.1.2熔丝和影子寄存器读取和 23.3.1.3熔丝和阴影寄存器写入 RM 中的部分,以提供附加信息。 BR 哈比卜 Re: Burning fuse 根据我的研究,烧断熔丝是可行的。 1. SPT(最简单)- 但我们需要将启动模式更改为 ISP,并且需要 UART 或 USB 接口。 2. CST(制造工具) - 这里我们也需要将启动模式更改为 ISP,并且需要 USB 接口。 3. 如您所说,通过 OCOTP 模块——无需插入 ISP,只需刷入未签名镜像(包含 OCOTP 驱动程序和待烧录的熔丝),烧录熔丝后,电路板即可锁定。 我的理解是否正确?或者我是否遗漏了其他编程方式,例如通过 JTAG/SWD 等方式? Re: Burning fuse 你好@Abhay2080 , 您无需进入串口下载器模式即可使用 OCOTP 模块。例如,在这篇社区帖子中,Kerry 描述了这种用于对熔丝进行编程的替代方法。 请记住,熔丝只能烧一次,所以请小心操作。 安全配置工具可以根据您选择的配置帮助确定所需的值,您可以将其用作指导,以确保对正确的熔丝进行编程。另请参阅 RM 中的第 9.4.1 章“启动 eFuse 说明”,其中提供了熔丝及其用途的详细说明。 BR 哈比卜
View full article
MCSPTR2AK396 — resolver excitation limits? Hello! I'm working with the MCSPTR2AK396 development kit (S32K396, 3-phase PMSM with resolver, 3-shunt FOC). I'm using the stock resolver-to-digital chain: SGEN → SDADC → DSPSS → eTPU RESOLVER function. As far as I understand, the stock excitation frequency is 10 kHz (SGEN sine wave driving the resolver excitation winding), and the eTPU RESOLVER processes angle updates every 50 µs with a 16+16 sample buffer from SDADC, with a slow PI regulator adjusting the excitation phase shift. But I have a questions. What is the exact resolver model used in the MCSPTR2AK396 kit? A datasheet reference would be very helpful. What is the maximum excitation frequency this resolver ? Can SGEN be raised, for example, to 100 kHz without modifying anything except SGEN registers? Or does the SDADC/DSPSS/eTPU chain, or the analog sin/cos filters, impose a hard limit well below that? What is the minimum excitation frequency allowed by the resolver itself, and what is the recommended range? If higher excitation is possible, what else must be reconfigured — SDADC sampling rate, DMA buffer transfer, eTPU HSR rate, excitation phase-shift regulator gains, analog filters? Thank you. Re: MCSPTR2AK396 — resolver excitation limits? Hello, What is the exact resolver model used in the MCSPTR2AK396 kit? On the TG Drives motor manufacturer's website, there is a configurator that lists three possible resolver options: ER5Kd411, TS2620N21E11, and RE-15-1-A15. If I remember correctly requested was lowest-cost resolver option, which was the ER5Kd411 from ATAS Náchod. https://www.atas.cz/files/ER5Kd.pdf The exact type could be determined by opening the rear cover. The MCSPTR2AK396 resolver solution is designed and validated at 10 kHz excitation. While SGEN supports frequencies up to 50 kHz according to the application note, operation above 10 kHz requires reconfiguration and validation of the SDADC, DSPSS, DMA, eTPU resolver processing and analog signal-conditioning chain. In addition, for resolvers such as TS2620N21E11 we only found a published nominal excitation specification of 7 Vrms at 10 kHz; no supported excitation-frequency range is specified in the available resolver datasheet. Therefore, operation at 100 kHz cannot be recommended based on available documentation. Best regards, Peter Re: MCSPTR2AK396 — resolver excitation limits? Understood, thank you. Is there a practical possibility of increasing the base PWM generation frequency to 20–30 kHz, or is the system strictly limited by the hardware physics of this KIT?
View full article
AN12064書類はどこで入手できますか? AN12064書類はどこで入手できますか? 評価ボード
View full article
MCSPTR2AK396 — レゾルバの励起限界? こんにちは!MCSPTR2AK396開発キット(S32K396、リゾルバ付き3相PMSM、3シャントFOC)を使っています。私は標準のリゾルバからデジタルへのチェーン、つまりSGEN → SDADC → DSPSS → eTPU RESOLVER関数を使用しています。 私の理解では、標準の励起周波数は10kHz(SGEN正弦波がレゾルバ励起巻線を駆動)であり、eTPUレゾルバはSDADCからの16+16サンプルバッファを使用して50µsごとに角度更新を処理し、低速PIレギュレータで励起位相シフトを調整します。しかし、私には疑問があります。 MCSPTR2AK396キットで使われている正確なリゾルバーモデルは何ですか?データシートの参照情報があると大変助かります。 このレゾルバの最大励起周波数はどれくらいですか?例えば、SGENをSGENレジスタ以外に変更せずに100 kHzに上げることは可能でしょうか?それともSDADC/DSPSS/eTPUチェーンやアナログのsin/cosフィルターが、それよりはるかに低い厳しい制限を課しているのでしょうか? レゾルバ自体が許容する最小励起周波数はどれくらいですか?また、推奨される範囲はどれくらいですか? より高い励起が可能なら、他に何を再構成する必要がありますか — SDADCサンプリングレート、DMAバッファ転送、eTPU HSRレート、励起位相シフトレギュレータゲイン、アナログフィルターなど? よろしくお願いします。 Re: MCSPTR2AK396 — resolver excitation limits? こんにちは、 MCSPTR2AK396キットで使われている正確なリゾルバーモデルは何ですか? TG Drivesモーターメーカーのウェブサイトには、ER5Kd411、TS2620N21E11、RE-15-1-A15という3つのレゾルバオプションを表示するコンフィギュレーターがあります。 私の記憶が正しければ、最も低価格なリゾルバの選択肢が求められており、それはATAS Náchod社のER5Kd411でした。 https://www.atas.cz/files/ER5Kd.pdf 正確なタイプはリアカバーを開けて確認できました。 MCSPTR2AK396レゾルバソリューションは、10kHzの励起周波数で設計および検証されています。SGENはアプリケーションノートによると最大50kHzまでの周波数をサポートしていますが、10kHz以上の動作にはSDADC、DSPSS、DMA、eTPUリゾルバプロセッシングおよびアナログ信号調整チェーンの再構成と検証が必要です。さらに、TS2620N21E11などのレゾルバについては、10kHzで7Vrmsという公称励起仕様しか公表されておらず、利用可能なレゾルバのデータシートには、サポートされる励起周波数範囲は記載されていません。したがって、利用可能なドキュメントに基づき100 kHzでの運用は推奨できません。 よろしくお願いいたします。 ピーター Re: MCSPTR2AK396 — resolver excitation limits? 承知いたしました。ありがとうございます。基本PWM生成周波数を20~30kHzまで上げることは現実的に可能でしょうか?それとも、このキットのハードウェアの物理的な制約によってシステムは厳密に制限されているのでしょうか?
View full article
ls1043a - should thermal_zone5 be active in the Linux BSP? I work on with the reference board for ls1043 processor ls1043ardb and having an issue with the thermal subsystem. The error I see is:  [ 116.704475] thermal thermal_zone5: critical temperature reached (104 C), shutting down It seems a bit sporadic but when it comes it comes quite soon after boot. It does not come all the time. When the system is stable the temperature from thermal_zone5 is always 0. The dts file fsl-ls1043a.dtsi have thermal_zone0 - thernal_zone5 active. (fsl-ls1043a.dtsi\freescale\dts\boot\arm64\arch - qoriq-components/linux - Linux Tree for QorIQ support ) The question is if ls1043 should have thermal_zone5 active? Looking in to the "QorIQ LS1043A Reference Manual, Rev. 5, 04/2019" chapter 35.1.1 "Local temperature sensor placement" I can read a table saying that the ls1043 have Temperature sensor ID 0-4 while ID 5-15 is marked as reserved. Is it correct that hte dtsi file enables thermal_zone5 and is it available in ls1043? Thanks, /Peter Re: ls1043a - should thermal_zone5 be active in the Linux BSP? Hello, We are seeing a similar issue on an LS1043A platform running Linux 4.19.68. The system occasionally reports: thermal thermal_zone5: critical temperature reached (104 C), shutting down   One observation is that thermal zones 0-4 generally track each other closely, while thermal_zone5 often reports significantly different values and behaves differently from the other zones.   Prior to shutdown, the thermal zones report values similar to: thermal_zone0: 75000 thermal_zone1: 76000 thermal_zone2: 76000 thermal_zone3: 75000 thermal_zone4: 74000 thermal_zone5: 0 In a previous reply, NXP mentioned that thermal_zone5 values were indeterminate and that a fix would be provided in a future LSDK release. Could you please confirm whether this issue was ever fixed, and if so, which LSDK/kernel release contains the fix? Thanks. Re: ls1043a - should thermal_zone5 be active in the Linux BSP? I am also facing the similar issue on the latest LSDK 20.12, Kernel 5.4.47.  [ 2115.927267] thermal thermal_zone1: critical temperature reached (85 C), shutting down [ 2116.951246] thermal thermal_zone1: critical temperature reached (85 C), shutting down [ 2117.975285] thermal thermal_zone1: critical temperature reached (85 C), shutting down Could you please let me know if any workaround is available to fix this? What is the root cause of this issue? Re: ls1043a - should thermal_zone5 be active in the Linux BSP? We acknowledge the issue, currently the values reported by thermal zone 5 are indeterminate and can cause such issue at any random point We will be providing an official fix in our upcoming LSDK releases. For now you can remove thermal zone 5 from your dtsi  and see if it helps
View full article
ls1043a - Linux BSPでthermal_zone5アクティブであるべきですか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 私はLS1043プロセッサのリファレンスボード、LS1043ardbで作業していますが、サーマルサブシステムに問題が発生しています。表示されるエラーは以下のとおりです。 [ 116.704475] thermal thermal_zone5: 臨界温度に達しました (104 ℃)、シャットダウンします 発生頻度はやや不規則ですが、発生する場合は起動後すぐに起こります。いつも起こるわけではない。システムが安定している場合、thermal_zone5 の温度は常に 0 になります。 dtsファイルfsl-ls1043a.dtsiでは、thermal_zone0~thernal_zone5が有効になっています。(fsl-ls1043a.dtsi\freescale\dts\boot\arm64\arch - qoriq-components/linux - QorIQサポート用のLinuxツリー) 問題は、ls1043でthermal_zone5を有効にするべきかどうかです。「QorIQ LS1043A Reference Manual, Rev. 5, 04/2019」の第35.1.1章「ローカル温度センサの配置」を調べてみると、LS1043の温度センサID 0-4で、ID 5-15は予約済みと記されている表が読めます。dtsiファイルによってthermal_zone5が有効になり、ls1043で利用可能になるというのは正しいでしょうか? ありがとう、 ピーター Re: ls1043a - should thermal_zone5 be active in the Linux BSP? こんにちは、 Linux 4.19.68を搭載したLS1043Aプラットフォームでも同様の問題が発生しています。 システムは時折、以下のことを報告します。 thermal thermal_zone5: 臨界温度(104℃)に達したため、シャットダウンします   観察されたことの一つは、熱ゾーン0~4は概ね互いに近い値を示すのに対し、熱ゾーン5はしばしば著しく異なる値を報告し、他のゾーンとは異なる挙動を示すということである。   シャットダウン前に、熱ゾーンは次のような値を報告します。 thermal_zone0: 75000 熱ゾーン1: 76000 熱ゾーン2: 76000 熱ゾーン3: 75000 熱ゾーン4: 74000 熱ゾーン5: 0 以前の返信でNXPはthermal_zone5値は不確定であり、将来のLSDKリリースで修正を提供すると述べていました。 この問題が修正されたかどうか、もし修正されたならどのLSDK/カーネルリリースに修正が含まれているのか確認していただけますか? ありがとうございます。 Re: ls1043a - should thermal_zone5 be active in the Linux BSP? 私も最新のLSDK 20.12、カーネル5.4.47で同様の問題に直面しています。 [ 2115.927267] thermal thermal_zone1: 臨界温度に達したため、シャットダウンします (85℃) [ 2116.951246] thermal thermal_zone1: 臨界温度に達したため、シャットダウンします (85℃) [ 2117.975285] thermal thermal_zone1: 臨界温度に達したため、シャットダウンします (85℃) この問題を解決する回避策があれば教えていただけませんか? この問題の根本原因は何ですか? Re: ls1043a - should thermal_zone5 be active in the Linux BSP? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 問題を認識しています。現在、サーマルゾーン5で報告される値は不確定で、任意のランダムなタイミングで問題を引き起こす可能性があります。今後のLSDKリリースで公式な修正を提供する予定です。 今のところ、DTSIからサーマルゾーン5を外してみて、改善するか試してみてはどうでしょうか
View full article
how to enable a second camera on mx95 evk board Spoiler (Highlight to read) Hello, we would like to know how to use a camera in the DSI/CSI slot of the MX95 EVK evk board. Our camera has reset and standby pins, but we cannot find any GPIO pins to control them in the MX95 EVK schematic. Hello, we would like to know how to use a camera in the DSI/CSI slot of the MX95 EVK evk board. Our camera has reset and standby pins, but we cannot find any GPIO pins to control them in the MX95 EVK schematic. Re: how to enable a second camera on mx95 evk board Hi @yipingwang  Thank you. The camera we are using is the TechNexion AR0235, and we would like to use it with the CSI and CSI/DSI slots. Re: how to enable a second camera on mx95 evk board Let me confirm with the AE team. Re: how to enable a second camera on mx95 evk board Hi @yipingwang  Thank you for your help, but the camera still isn't working. Do you have any suggestions? Re: how to enable a second camera on mx95 evk board J14 A10 DSICSI_RST_SYNC → ADP5585 C0 → gpiochip9 line 6 → reset is typically active-low J14 A11 DSICSI_EN_PWDN → ADP5585 R4 → gpiochip9 line 4 → power-down is typically active-high Normal operation: line 6 = high , line 4 = low . Re: how to enable a second camera on mx95 evk board hi @yipingwang  @yipingwang  @I applied the following settings, but the camera initialization still failed hankwang_0-1790059212233.png Re: how to enable a second camera on mx95 evk board Hi @yipingwang  Thank you for confirming that J14 A10 (DSICSI_RST_SYNC) and A11 (DSICSI_EN_PWDN) are controlled via U81 (ADP5585). We've confirmed the ADP5585 on our board (i2c address 0x34, reporting as adp5585-00) probes successfully and is exposed to Linux as gpiochip9 with 11 GPIO lines (0-10; line 5 is reserved for PWM per our device tree). Could you help us map these two signals to the exact ADP5585 GPIO pins (e.g. R0-R4/C0-C4 per the datasheet), and the corresponding Linux gpiochip line number (0-10)? Also, what is the correct polarity (active-high/active-low) for each signal? We've already brute-force tested all pairwise combinations of the 10 available lines (90 combinations, both pulled low simultaneously) without success — the camera's boot-state register (0x3004) remains 0x0000 in every case. A precise pin mapping from the schematic or UM12022 would let us verify directly rather than continuing to guess. Re: how to enable a second camera on mx95 evk board On the 19 mm × 19 mm i.MX 95 EVK , The reset and standby pins on the i.MX95 EVK DSI/CSI connector (J14) are controlled through the ADP5585 GPIO expander U81 , not directly by i.MX95 GPIOs: J14 A10 – DSICSI_RST_SYNC : camera reset J14 A11 – DSICSI_EN_PWDN : camera standby/power-down Control voltage: 1.8 V In the device tree, reference U81 for reset-gpios and pwdn-gpios . Use NXP’s imx95-19x19-evk-os08a20-combo.dtb overlay as the example for enabling the second camera on the shared DSI/CSI port. Re: how to enable a second camera on mx95 evk board Please confirm that you are using 19x19 or 15x15 evk? Re: how to enable a second camera on mx95 evk board 95 and sensor must be configured in pair, take ov5640 for example,     PWDN (EN), B11 RESET (RST_B), A9 So on 95 side, A11 should be for pwdn, and B9 for reset. Looking into the 95 19x19 BB board schematic,  A11 is controlled by ADP5585 R4 pin B9 is controlled by soc gpio3 27       So in the dts, user should configure as follows, pinctrl_mipi_dsi_csi: mipidsigrp {         fsl,pins = <                 IMX95_PAD_CCM_CLKO2__GPIO3_IO_BIT27                     0x31e         >; }; pinctrl-0 = <&pinctrl_mipi_dsi_csi>; powerdown-gpios = <&adp5585gpio 4 GPIO_ACTIVE_HIGH>; reset-gpios = <&gpio3 27 GPIO_ACTIVE_LOW>; If user needs to connect to 15x15 evk board, then   pinctrl_mipi_dsi_csi_rst: mipidsirstgrp {         fsl,pins = <                IMX95_PAD_XSPI1_DATA7__GPIO5_IO_BIT7                    0x31e         >; }; pinctrl_mipi_dsi_csi: mipidsigrp {         fsl,pins = <                IMX95_PAD_XSPI1_DATA6__GPIO5_IO_BIT6                    0x31e         >; }; pinctrl-0 = <&pinctrl_mipi_dsi_csi_rst>, <&pinctrl_mipi_dsi_csi>; powerdown-gpios = <&gpio5 6 GPIO_ACTIVE_HIGH>; reset-gpios = <&gpio5 7 GPIO_ACTIVE_LOW>; Re: how to enable a second camera on mx95 evk board @yipingwang I am using the 19x19 EVK board, and I have resolved the issue. Thank you. The reset pin configuration needs to be changed; J14 A10 DSICSI_RST_SYNC cannot be used.
View full article