Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
RDDRONE-BMS772 Development Board I'd like to know more about the RDDRONE-BMS772 board. It includes pins for an external temperature sensor, and a thermistor is also included in the accessories. Can this board be used to measure battery temperature? However, the accessories only list a thermistor, not a temperature sensor. If the board can be used to measure temperature, do I need to buy the temperature sensor separately? And where should the temperature sensor be installed? Re: RDDRONE-BMS772开发板 Hello fan007 Good day! I'd like to know more about the RDDRONE-BMS772 board. It includes pins for an external temperature sensor, and a thermistor is also included in the accessories. Can this board be used to measure battery temperature? However, the accessories only list a thermistor, not a temperature sensor. If the board can be used to measure temperature, do I need to buy the temperature sensor separately? And where should the temperature sensor be installed? In Getting Started with the RDDRONE-BMS772 Reference Design, you can find a chapter that describes everything included in the purchase of this board. Yes, it includes an external thermistor with a cable, which can function as a temperature sensor. However, you can use another sensor that you consider more reliable. The board does have a dedicated port for connecting this sensor. More detailed information about its connection and use can be found in the documentation available on our website. Please review: UM11421, RDDRONE-BMS772 reference design - User guide (you need an account with us to access this document) An optional external temperature sensor can be added onto the RDDRONE-BMS772 board using connector J1. An example of application for this external sensor is used to monitor the cells temperature inside the battery pack. I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck.
記事全体を表示
I tried using EBtresos in AUTOSAR, but it failed to activate. Hello, I tried to use EBtresos in AUTOSAR, but failed to activate it. Activation code: 7416-E905-5CC2-F20A ERROR: flxActAppActivationSend (50040,41147,10248) The specified quantity exceeds the maximum allowed quantity (0). Connection to FlexNet Operations Server failed. Therefore, I need another activation code to use EBtresos. Thanks! Re: 在 AUTOSAR 中使用 EBtresos,但未能激活。 Hi Sorry for the inconvenience we bring you! I have already reported this issue to the internal team, and I will let you know as soon as I receive their reply.   Best Regards, Robin Re: 在 AUTOSAR 中使用 EBtresos,但未能激活。 Thank you for your patience. The internal team has updated the activation code on the webpage. Please click the link below to find the latest activation code: S32K3 Standard Software -> Automotive SW - EB tresos Studio / AUTOSAR Configuration Tool -> EB tresos Studio 29.0.0 
記事全体を表示
8MPLUSLPD4-EVK - 自動電源オン こんにちは、チームのみなさん。 8MPLUSLPD4-EVKは電源供給時に起動(起動)します。 私たちの理解と仮定によれば、搭載をオンにするにはONOFFボタン(SW1)を押す必要があります。 しかし実際には、EVKはONOFFボタン*SW1を押さずにONがオンになります。 この自動電源オンの動作とONOFFボタンの使い方について説明してもらえますか? 私の理解が間違っていたら訂正してください。 🙂 Re: 8MPLUSLPD4-EVK - Autopower ON こんにちは、 @ramkrishさん お元気でお過ごしのことと思います。 実際、その行動は正しい。 SW3の電源を入れると、ボードの電源が入るはずです。 ソフトウェアで基板の電源を切ったら、SW1で再度オン(ONオフ)できます。 よろしくお願いいたします。 サラス。
記事全体を表示
EBライセンスのアクティベーションに失敗しました: エラー「数量が0です」& 50019 シングルユーザーのEBトレソオフラインライセンスを有効化できません。古いライセンスをローカルに返却した後、私の認証コードに関連付けられたすべてのライセンスシートがFlexNetクラウドサーバー上でロックされました。 私はオンライン認証とオフライン認証の両方のワークフローを試しました。各方法の対応する結果は、添付された2枚のスクリーンショットに示されています。
記事全体を表示
TagWriter can not read the PN7160 tag I am running the RWandCE example (LPC55S69+PN7160). When I use the TagWriter app on an Android phone to read the tag, it fails with no response. The log shows that it activated the poll mode. However, TagInfo can read it, but it shows a "communication interrupt" popup, and the result on the phone may be incorrect. Is this because both poll and listen are enabled in the discovery loop? But my requirement is that both poll and listen must be enabled simultaneously. And I have also closed all emulation cards on my android phone. Please help me, thank you. LPC55xx Re: TagWriter can not read the PN7160 tag Hello @BillyHu Hope you are doing well. Please try updating PN7160 FW to the latest version available .You can refer to PN7160 - FW Update via MCUXpresso for more information on this. Regards, Eduardo. Re: TagWriter can not read the PN7160 tag Hi Eduardo, My firmware version is already 12.50.11. Poll and listen work perfectly fine when used individually, but when both are enabled in discoveryTechnologies, I cannot read the card emulation of the PN7160 using the tagwriter. Have you encountered this issue on your side? Thanks, Re: TagWriter can not read the PN7160 tag Dear Eduardo, Do you have any suggestions? Is this phenomenon normal for the PN7160? Thanks,
記事全体を表示
ARC Raiders U4N 试炼第五赛季带来全新挑战 ARC Raiders 第 5 赛季试炼即将改变玩家体验游戏终局内容的方式,带来一系列全新的目标、战斗挑战和外观奖励。随着玩家重返锈带,许多玩家都在寻找更好的方法来准备装备、完成赛季目标和收集宝贵的资源。了解ARC Raiders BluePrints等系统可以帮助玩家规划他们的游戏进程,并在进入艰难的战斗之前做出更好的决定。 新的试炼赛季将于 2026 年 7 月 7 日第四赛季结束后到来,带来以技巧、适应性和实验性为重点的全新内容。新的目标和排名奖励将使那些精心管理装备并了解战场情况的玩家有更多成功的机会。许多玩家也在密切关注季节性经济,包括 ARC 突袭者蓝图和其他有用资源的供应情况。 第五季引入更多样化的审判目标 试炼赛季 5 将于 2026 年 7 月 7 日 12:00 UTC 正式开始,持续至 2026 年 9 月 30 日 07:00 UTC。在此期间,玩家可以完成挑战,提升排名,并根据表现解锁专属奖励。 更新后的目标系统旨在为比赛创造更多变化。玩家不再需要每轮都重复相同的策略,而是需要根据每个试炼的要求调整自己的游戏风格。有些目标要求玩家使用特定武器对特定的 ARC 单位造成伤害,而另一些目标则考验玩家在危险情况下的生存技能。 其中一项重点挑战是直接承受爆炸“砰”的伤害。这种类型的目标鼓励玩家承担风险,并谨慎管理他们的健康状况、位置和时机。它造成了这样一种局面:明智的决策与战斗能力同等重要。 原有目标仍将继续保留,为经验丰富的玩家提供熟悉的任务,同时也为想要提升技能的玩家带来新的挑战。这种组合既能保持《Trials》的独特风格,又能让每一季都感觉不一样。 战斗挑战鼓励玩家尝试不同的装备搭配 第五赛季的一个重点是鼓励玩家探索不同的装备选择。在许多游戏中,玩家最终都会选择用起来顺手的武器和策略。试验的运作方式不同,它会奖励那些愿意尝试的人。 玩家可能需要更换武器、调整移动习惯或改变应对敌人的方法。在正常游戏过程中很少使用的武器,在完成特定挑战时可能会变得非常有用。这使得准备与成功之间建立了更紧密的联系。 开发人员提到的 ARC 活动增加也给每项任务带来了更大的压力。玩家必须考虑何时战斗,何时躲避危险,以及如何有效地利用他们的资源。这些决定可能决定试验能否顺利完成,还是会失去宝贵的进展。 斯考塔套装奖励显示赛季进度 第五赛季最大的奖励是 Scorta 套装,该套装会根据玩家的最终排名而变化。该系统为竞技选手提供了一种在赛季结束后展示自己成绩的直观方式。 达到更高等级的玩家,包括“神枪手”和“酒馆传奇”,可以解锁该服装的特殊红色和蓝色版本。这些外观奖励代表着本赛季的出色表现,可以让经验丰富的玩家在未来的战斗中脱颖而出。 其他奖励包括绿色斗士背包、压力表背包挂饰、液压泵背包附件和“来啊,放马过来”表情。这些物品注重自定义功能,为玩家提供更多个性化角色的方式。 奖励机制表明,试炼正在成为 ARC Raiders 长期发展的重要组成部分。玩家完成挑战不仅是为了获得暂时的奖励,更是为了建立一个能够反映他们成就的收藏品。 第五赛季拓展了ARC突袭者的未来 凭借全新的目标、改进的进度系统和专属外观,Trials 第 5 赛季为玩家提供了更多重返锈带的理由。战斗挑战与排名奖励相结合,打造了一个既能支持竞技玩家,又能支持那些只想提升技能的玩家的系统。 对于想要在整个赛季保持最佳状态的玩家来说,管理资源和升级收藏仍然非常重要。可靠地获取有用的装备可以使困难的任务变得更容易,尤其是在面对更强大的敌人和不可预测的情况时。 对季节性资源日益增长的需求也使得ARC Raiders 物品的出售成为许多玩家在准备下一次冒险时关注的话题。拥有合适的装备和材料可以帮助玩家更专注于完成试炼,而不是为准备工作而烦恼。 随着第五赛季的进行,挑战系统很可能成为 ARC Raiders 体验的另一个重要组成部分。在新赛季中,能够快速适应、尝试不同策略并建立强大阵容的玩家将有最大的机会脱颖而出。
記事全体を表示
Don't support S32K344's PlatformSDK_S32K3_2022_03 version Hi,     Previous I develop S32K344 code based on S32K344 WB board. The platform is S32DS.3.4 and RTD AUTOSAR 4.4.2, the project work well.      Now I want to develop S32G3 code, which requires S32DS.3.5. So I uninstalled the S32DS.3.4 and RTD 4.4.2 ,  install S32DS.3.5. After installation complete, I begin to install Extension and Updates. I can't find S32K3's RTD 4.4.2 version, so I have to install S32K3's RTD 3.0.0 version. After K3's RTD installing done, I import the old S32K344 project and try to open *.mex file, but the project prompt that "current tool doesn't support S32K344‘s PlatformSDK_S32K3_2022_03 version." How to resolve this issue? Re: Don't support S32K344's PlatformSDK_S32K3_2022_03 version Hi Julián,       Thank you for your reply. I create a new application project in S32DS.3.5 and K3 RTD3.0.0, but I can't find *.mex file in new project. Step1: Select S32K344 and M7(Gcc 10.2 for arm 32-bit) Step2. Select core and parameter Step3. Get new project s32k3_can_uart_rtd3, but I can't find the following file previous exist in S32DS.3.4 instance. .ClockConfigurationMappings.txt .ClockYaml.txt .s32k3_wb_can_rtd3.mex .S32K344_flash.cmm file .RTD folder. So, what's the problem for my new RTD3.0.0 project? Re: Don't support S32K344's PlatformSDK_S32K3_2022_03 version Hi @Jimmybai, This is simply an incompatibility error between RTD 2.0.0 & RTD 3.0.0. Unfortunately, there is no simple way of importing it directly from 2.0.0 to 3.0.0. Instead, I recommend to manually port over your application: 1. In your new S32DS instance with RTD 3.0.0, create a new project through "File > New > S32DS Application Project" 2. Select processor, NXP GCC 10.2 toolchain, and attach the new RTD 3.0.0 in the next window. 3. Once the project is created, copy and paste over all of the source files from your pre-existing project. 4. Lastly, open .mex file and copy over the configuration manually.  You can try to use the "Import > S32 Configuration Tools > Import Configuration (*.mex)" option to import the .mex file, however, I've found that RTD 2.0.0 and below mostly creates errors in S32CT, and manually porting the application is a better solution. Best regards, Julián Re: Don't support S32K344's PlatformSDK_S32K3_2022_03 version Hello @Jimmybai, Have you attached the RTD to the project?  Best regards, Julián
記事全体を表示
EB许可证激活失败:错误“允许的数量 (0)”和 50019 我无法激活我的单用户 EB Tresos 离线许可证。在本地退回旧许可证后,我的激活码的所有许可证席位在 FlexNet 云服务器上都被锁定。 我尝试过在线激活和离线激活两种方式。每种方法的相应结果分别显示在附图中的两张截图中。
記事全体を表示
8MPLUSLPD4-EVK - 自动开机 大家好, 当接通电源并打开 SW3 时,8MPLUSLPD4-EVK 启动。 根据我们的理解和假设,需要按下 ONOFF 按钮 (SW1) 才能打开板。 但实际上,EVK 无需按下 ONOFF 按钮 *SW1 即可开启。 能否解释一下自动开机功能的工作原理以及开关按钮的使用场景? 如果我的理解有误,请指正。 🙂 Re: 8MPLUSLPD4-EVK - Autopower ON 你好@ramkrish 希望你一切都好。 实际上,这种行为是正确的。 打开SW3开关后,电路板应该会通电。 当您通过软件关闭电路板电源时,您可以使用 SW1(ONOFF)再次打开板。 顺祝商祺! 萨拉斯。
記事全体を表示
Zephyr:RW61X用の圧縮FWサポート CONFIG_NXP_COMPRESS_WIFI_NB_FW は、 https://github.com/nxp-zephyr/nxp-zephyr/commit/e64f39fa2a05edec7bd8a2b24d9f1236c43d6c35でデフォルトで有効になっています。 rw61x_sb_wifi_a2_compressed.bin ファイルがないと、CMake が失敗します。圧縮処理が抜けているのでしょうか?どの圧迫方法がサポートされていますか? ローダーに変化は見られませんでした。圧縮ファームウェアは自動的に処理されますか? Re: zephyr: support compressed FW for RW61X NXPのZephyrフォーラムがあることを今見かけました。これをあちらに移動すべきでしょうか? Re: zephyr: support compressed FW for RW61X 私はnxp-v4.4-branchを使用しています。Zephyr/Samples/Net/WiFi/Shellはfrdm_rw612で使っています。 何が起こったのか分かりました。私はこの西側アップデートエラーを見落としていました。 === 更新中 wifi_nb_fw (modules/hal/nxp/zephyr/blobs): 致命的な:宛先パス「modules/hal/nxp/zephyr/blobs」はすでに存在しており、空のディレクトリではありません。 次にファームウェアを取得するために、 https://docs.zephyrproject.org/latest/boards/nxp/frdm_rw612/doc/index.html#wireless-connectivity-supportに従って「west blobs fetch hal_nxp」を使用しました。 これにより圧縮イメージがダウンロードされず、CONFIG_NXP_COMPRESSED_WIFI_NB_FW が設定されている場合に表示されるエラーが発生しました。 blobs ディレクトリには既に次の場所からのファイルが含まれていました: https://github.com/nxp-zephyr/hal_nxp/tree/nxp-v4.4-branch/zephyr/blobs/license/ 私は.mcuxpressotools/.mcux-venv-3.12/bin/westからwestを使用していました。これはバージョン1.5.0です。 古いバージョン(v1.3.0)を試してみたところ、westはエラーを起こすことなく、既存の空でないディレクトリにリポジトリを追加するだけでした。 Re: zephyr: support compressed FW for RW61X こんにちは、 あなたの調子が良いといいのですが。何を検査しているのか、詳しく教えていただけますか? 具体的な例を使って作業していますか? 何か変更を加えましたか? よろしくお願いいたします。 リカルド
記事全体を表示
RDDRONE-BMS772開発ボード RDDRONE-BMS772ボードについてもっと詳しく知りたいです。このボードには外部温度センサー用のピンがあり、付属品にはサーミスタも含まれています。このボードはバッテリー温度の測定に使用できますか?ただし、付属品にはサーミスタしか記載されておらず、温度センサーは記載されていません。もしこのボードで温度を測定できる場合、温度センサーは別途購入する必要がありますか?また、温度センサーはどこに取り付ければ良いのでしょうか? Re: RDDRONE-BMS772开发板 こんにちは fan007 良い一日! RDDRONE-BMS772ボードについてもっと詳しく知りたいです。 外部温度センサー用のピンや、サーミスタもアクセサリとして含まれています。このボードはバッテリー温度を測るために使えますか?ただし、アクセサリには温度センサではなくサーミスタのみが記載されています。もし基板で温度測定ができるなら、温度センサは別途購入する必要がありますか?温度センサーはどこに設置すべきでしょうか? RDDRONE-BMS772リファレンスデザインの入門には、このボードの購入に含まれるすべての内容を説明した章があります。 はい、外部サーミスタとケーブルが付属しており、温度センサとして機能します。ただし、より信頼性が高いと考える別のセンサを使うこともできます。この基板にはこのセンサを接続するための専用ポートがあります。その関連性や利用に関するより詳細な情報は、当ウェブサイトのドキュメントでご覧いただけます。 ご確認ください: UM11421、RDDRONE-BMS772 リファレンスデザイン - ユーザーガイド (この文書にアクセスするには当事務所のアカウントが必要です) RDDRONE-BMS772にはオプションの外部温度センサーを追加することも可能です コネクタJ1を使用する基板。この外部センサの応用例としては バッテリーパック内部のセル温度を監視する。 この情報がお役に立てば幸いです。他に何かご不明な点がありましたら、お気軽にお問い合わせください。 良い一日をお過ごしください。幸運を祈ります。
記事全体を表示
ARCレイダーズU4Nトライアルシーズン5では新たな挑戦が待ち受けている ARC Raidersシーズン5のトライアルでは、新たな目標、戦闘チャレンジ、そして装飾アイテムの報酬など、プレイヤーがエンドゲームに取り組む方法を変える準備が進められています。プレイヤーがラストベルトに戻ってくるにつれ、多くのプレイヤーは装備の準備、シーズン目標の達成、貴重な資源の収集をより効率的に行う方法を模索している。ARC Raiders BluePrintsのようなシステムを理解することで、プレイヤーは進行を計画し、困難な遭遇に臨む前により良い判断を下すことができます。 新たなトライアルシーズンは、2026年7月7日にシーズン4が終了した後に登場し、スキル、適応力、そして実験に焦点を当てた新しいコンテンツを提供します。新たな目標とランキング報酬が導入されたことで、装備を慎重に管理し、戦場を理解しているプレイヤーは、より多くの成功の機会を得られるようになるでしょう。多くのプレイヤーは、ARCレイダーズの設計図やその他の有用なリソースの入手可能性など、季節ごとの経済動向を注意深く見守っています。 シーズン5では、より多様な裁判目標が導入されます。 トライアルシーズン5は、2026年7月7日12:00(UTC)に正式に開始され、2026年9月30日07:00(UTC)まで開催されます。この期間中、プレイヤーはチャレンジをクリアし、ランキングを上げ、パフォーマンスに基づく限定報酬をアンロックできます。 更新された目標システムは、試合中の多様性を高めることに重点を置いています。プレイヤーは、毎ラウンド同じ戦略を繰り返すのではなく、各トライアルの要件に応じてプレイスタイルを調整する必要がある。目標によっては、特定の武器を使って特定のARCユニットにダメージを与えることが求められるものもあれば、危険な状況下でのサバイバルスキルが試されるものもある。 注目すべき課題の一つは、爆発的な「ポップ」ダメージを直接受けることである。この種の目標は、プレイヤーがリスクを取り、体力、ポジショニング、タイミングを慎重に管理することを促します。それは、賢明な意思決定能力が戦闘能力と同じくらい重要になる状況を生み出す。 過去の目標も引き続き利用可能となり、経験豊富なプレイヤーには馴染みのあるタスクを提供するとともに、スキルアップを目指すプレイヤーには新たな挑戦の機会を提供する。この組み合わせにより、トライアルズの独自性を維持しつつ、各シーズンがそれぞれ異なる印象を与えることができる。 戦闘チャレンジは装備の試行錯誤を促す シーズン5の大きな焦点の一つは、プレイヤーに様々な装備の選択肢を試してもらうことです。多くのゲームでは、プレイヤーは最終的に自分にとって使いやすい武器や戦略に落ち着く。Trialsは、実験を厭わない人に報酬を与えることで、他とは異なる仕組みで機能する。 プレイヤーは武器を切り替えたり、移動習慣を調整したり、敵との遭遇に対するアプローチを変えたりする必要があるかもしれません。通常のゲームプレイではめったに使われない武器が、特定のチャレンジをクリアするのに非常に役立つことがあります。これにより、準備と成功の間の結びつきがより強固になる。 開発者らが言及したARCの活動増加は、あらゆる任務にさらなるプレッシャーを与えることになる。プレイヤーは、いつ戦うべきか、いつ危険を避けるべきか、そして資源をいかに効果的に活用すべきかを考えなければならない。これらの決断がトライアルの完了と貴重な進行を失うかの分かれ目となることがあります。 スコルタ衣装報酬で季節ごとの進捗状況を表示 シーズン5最大の報酬は、プレイヤーの最終ランキングに応じて変化するスコルタの衣装です。このシステムは、競技プレイヤーがシーズン終了後に自分の成果を目に見える形で示す手段を提供します。 ホットショットやカンティーナ・レジェンドなどの上位ランクに到達したプレイヤーは、特別な赤と青の衣装バージョンをアンロックできます。これらのコスメティック報酬は強力なシーズンパフォーマンスを示し、経験豊富なプレイヤーが今後のバトルで際立つことを可能にします。 その他の報酬には、グリーンブルーザーバックパック、圧力計バックパックチャーム、油圧ポンプバックパックアタッチメント、そして「かかってこい」エモートが含まれます。これらのアイテムはカスタマイズに重点を置いており、プレイヤーがキャラクターをより自分好みにカスタマイズできる方法を提供します。 報酬体系を見ると、トライアルはARCレイダーズの長期的な成長において重要な要素になりつつあることがわかる。プレイヤーは一時的な特典を得るためのチャレンジをクリアするだけでなく、自分の実績を反映したコレクションも構築しています。 シーズン5、ARCレイダースの未来を拡大 新たな目標、改善された進行システム、そして限定コスメティックアイテムなど、トライアルシーズン5では、プレイヤーがラストベルトに戻ってくる理由がさらに増えます。戦闘チャレンジとランキング報酬の組み合わせにより、競技プレイヤーと単にスキルの向上を楽しむプレイヤーの両方をサポートするシステムが生まれています。 シーズンを通して万全の準備を整えておきたいプレイヤーにとって、リソースの管理とコレクションのアップグレードは依然として重要です。有用な装備を確実に手に入れることで、特に強力な敵や予測不能な状況に直面した際には難しいミッションが容易になります。 季節資源の需要増加により、 多くの プレイヤーが次の冒険を準備する際に注目する話題となっています。適切な装備や素材を揃えておくことで、準備に苦労するよりも試練のクリアに集中できます。 シーズン5が進むにつれて、チャレンジシステムはARCレイダーズのゲーム体験におけるもう一つの重要な要素となる可能性が高い。素早く適応し、様々な戦略を試し、強力なコレクションを構築できるプレイヤーは、新シーズンで頭角を現す可能性が最も高いでしょう。
記事全体を表示
EB License Activation Failed: Error "quantity allowed (0)" & 50019 I cannot activate my single-user EB tresos offline license. After returning the old license locally, all license seats of my activation code are locked on the FlexNet cloud server. I have tried both online activation and offline activation workflows. The corresponding results for each method are shown in the two attached screenshots respectively.
記事全体を表示
8MPLUSLPD4-EVK - Autopower ON Hi Team, 8MPLUSLPD4-EVK turns ON (boots) when power supply is provided and SW3 is turned ON. Based on our understanding and assumption ONOFF button (SW1) needs to be pressed to turn ON Board. But in actual case EVK turns ON without pressing ONOFF Button *SW1. Could you clarify how this auto power on works and use case of ONOFF button? Correct me if my understanding is wrong 🙂 Re: 8MPLUSLPD4-EVK - Autopower ON Hello @ramkrish  I hope you are doing very well. Actually, that behavior is correct. When you Turn On the SW3, is expected that board will power up. When you power off the board by software, you can Turn on again with the SW1 (ONOFF). Best regards, Salas.
記事全体を表示
TagWriter can not read the PN7160 tag I am running the RWandCE example(LPC55S69+PN7160). When I use the TagWriter app on an Android phone to read the tag, it fails with no response. The log shows that it activated the poll mode. However, TagInfo can read it, but it shows a "communication interrupt" popup, and the result on the phone may be incorrect. Is this because both poll and listen are enabled in the discovery loop? But my requirement is that both poll and listen must be enabled simultaneously. And  I have also closed all emulation cards on my android phone. Please help me, thanks. LPC55xx Re: TagWriter can not read the PN7160 tag 你好@BillyHu 希望你一切都好。 请尝试将PN7160固件更新到最新版本。您可以参考“PN7160 - 通过MCUXpresso进行固件更新”了解更多信息。 问候, 爱德华多。 Re: TagWriter can not read the PN7160 tag 你好,爱德华多, 我的固件版本已经是 12.50.11 了。单独使用轮询和监听功能时,两者都能正常工作,但当在 discoveryTechnologies 中同时启用这两个功能时,我无法使用 tagwriter 读取 PN7160 的卡模拟信息。您那边遇到过这个问题吗? 谢谢! Re: TagWriter can not read the PN7160 tag 亲爱的爱德华多: 您有什么建议吗?PN7160出现这种现象正常吗? 谢谢!
記事全体を表示
zephyr: support compressed FW for RW61X CONFIG_NXP_COMPRESS_WIFI_NB_FW is enabled by default in https://github.com/nxp-zephyr/nxp-zephyr/commit/e64f39fa2a05edec7bd8a2b24d9f1236c43d6c35 Cmake fails without a rw61x_sb_wifi_a2_compressed.bin file. Is there a missing compression step?  What compress method is supported? I didn't see any changes to the loader.  Will it automatically handle a compressed fw? Re: zephyr: support compressed FW for RW61X I now see there is a NXP zephyr forum. Should this be moved there? Re: zephyr: support compressed FW for RW61X I'm using nxp-v4.4-branch zephyr/samples/net/wifi/shell on frdm_rw612. I see what happened.  I had overlooked this west update error:  === updating wifi_nb_fw (modules/hal/nxp/zephyr/blobs): fatal: destination path 'modules/hal/nxp/zephyr/blobs' already exists and is not an empty directory. Then to get the FW, I used "west blobs fetch hal_nxp" per https://docs.zephyrproject.org/latest/boards/nxp/frdm_rw612/doc/index.html#wireless-connectivity-support This didn't download the compressed images leading to the error I saw with CONFIG_NXP_COMPRESSED_WIFI_NB_FW set. The blobs directory already had files from here it: https://github.com/nxp-zephyr/hal_nxp/tree/nxp-v4.4-branch/zephyr/blobs/license/ I was using west from .mcuxpressotools/.mcux-venv-3.12/bin/west which is v1.5.0. I tried an older version (v1.3.0) and west just adds the repo to the existing non-empty directory without failing. Re: zephyr: support compressed FW for RW61X Hello, Hope you are doing well. Could you please clarify what are you testing? Are you working with a specific example? Did you make any modification? Best Regards, Ricardo
記事全体を表示
在 AUTOSAR 中使用 EBtresos,但未能激活。 您好, 我试图在 AUTOSAR 中使用 EBtresos,但未能激活。 激活代码 :7416-E905-5CC2-F20A ERROR: flxActAppActivationSend (50040,41147,10248) 指定的数量超过允许的最大数量 (0)。 与 FlexNet Operations Server 的连接失败。 因此,我需要另一个激活代码才能使用 EBtresos。 谢谢! Re: 在 AUTOSAR 中使用 EBtresos,但未能激活。 HI 给您带来的不便,我们深表歉意!我已经将此问题报告给了内部团队,一旦收到他们的回复,我会立即通知您。 此致敬礼,罗宾 Re: 在 AUTOSAR 中使用 EBtresos,但未能激活。 感谢您的耐心等待。 内部团队已更新网页上的激活码。 请点击下方链接查找最新激活码: S32K3 标准软件 -> 汽车软件 - EB tresos Studio / AUTOSAR 配置工具 -> EB tresos Studio 29.0.0
記事全体を表示
EBエラー こんにちは、みんな: EB Tresosの有効化時にエラーが発生しました。 エラー: flxActAppActivationSend (50040,41147,10248) 指定された数量は、許容最大数量(0)を超えています。 FlexNetオペレーションサーバーへの接続に失敗しました。 私のコードは7416-E905-5CC2-F20Aで、有効期限は2026年9月30日までです。 この問題を解決する方法についてアドバイスをいただけませんか?ご協力いただけると幸いです。 Re: EB ERROR こんにちは、 つまり、EBから提供された無料ライセンスはすべて使い果たされたということだ。 NXPのウェブサイトに新しい情報が掲載されるまでには、通常数日かかります。 よろしくお願いいたします。 ピーター
記事全体を表示
How to enable the external U.FL antenna on FRDM-RW612 EVK Hi NXP Team, I'm using the FRDM-RW612 EVK with the wifi_cli example from the SDK. The Wi-Fi firmware loaded is rw61x_sb_wifi_a2.bin. I have connected a Molex 1461539050 external antenna to the UFL connector (J11) on the EVK. However, I do not observe any improvement in the RSSI compared to the onboard PCB antenna. In some cases, the RSSI is even slightly lower. From the FRDM-RW612 schematics and user guide, I understand that the RF switch (U16 - RTC7608U) selects between the onboard PCB antenna and the external UFL connector and that RF_CNTL_3 is the control signal for this switch: RF_CNTL_3 = 0 -> PCB antenna (default) RF_CNTL_3 = 1 -> External UFL antenna How to control RF_CNTL_3 ? Is RF_CNTL_3 driven automatically by the Wi-Fi firmware ? If yes what is its default value ? How to modify that value ? Is any hardware or firmware configuration required to enable the external antenna on the EVK? Any guidance or example code would be greatly helpful. Thank you. Re: How to enable the external U.FL antenna on FRDM-RW612 EVK Hi, Let me check this. Regards, Daniel. Re: How to enable the external U.FL antenna on FRDM-RW612 EVK Hi @DanielRuvalcaba , were you able to check this, please let me know if you have any updates regarding this. Thanks & Regards, Prathyush Re: How to enable the external U.FL antenna on FRDM-RW612 EVK Hi, I've sent you a private message. Regards, Daniel. Re: How to enable the external U.FL antenna on FRDM-RW612 EVK Hi @DanielRuvalcaba I also would like to switch antenna to UFL connector (J11) on FRDM-RW612. Could you please share information how to do it? Are we switching antenna through Front-end module (FEM) settings? Regards Marcin Re: How to enable the external U.FL antenna on FRDM-RW612 EVK Hi, I reached you via private message. Regards, Daniel.
記事全体を表示
S32K328:CM7_0 CM7_2 DTCMバックドアへのアクセスが不正確なバスフォールトを引き起こす NXPチームの皆様、こんにちは。   当社では、RTD 7.xを搭載したS32K328を使用しています。   ソフトウェアのセットアップ: - CM7_0はブートローダーを実行します。 - CM7_1は第二のアプリケーションで使用されます。 - CM7_2はアプリケーションコードの実行を目的としていません。 - TCMバックドア/AHBS経路を通じてCM7_2 DTCMをシステムメモリとして使用できるかどうかCM7_0評価しています。   リファレンス・マニュアルの文脈: 「メモリマップ」章では、ITCM/DTCMは他のマスター、特にCortex-M7コアやeDMAから32ビットAHBSインターフェースからアクセス可能であると述べられています。 「TCMをシステムメモリとして」のセクションでは、有効化されたコアは無効化または待機中のコアのTCMを以下以下で使用可能とされています: 1. ターゲットコアTCMコントローラクロックの有効化: MC_ME PRTN2_COFB2_CLKEN[REQ64] for Cortex-M7_2 2. ターゲットコアCPUWAITの設定: DCM_GPR DCMRWF4[CM7_2_CPUWAIT] 3. ターゲットコアクロック/アクセスパスの有効化: MC_ME PRTN0_CORE4_PCONF[CCE]   私たちが試したこと: 1. DCM_GPR DCMRWF4[CM7_2_CPUWAIT]を設定します。 2. MC_ME PRTN2_COFB2_CLKEN[REQ64]を設定します。 3. MC_ME PRTN2_PUPD[PCUD]を設定します。 4. MC_ME CTL_KEYシーケンスを適用しました。 5. PRTN2_PUPD[PCUD]がクリアされるまで待機しました。 6. PRTN2_COFB2_STATを読み取り、bit0/BLOCK64がアクティブであることを確認した。 7. MC_ME PRTN0_CORE4_PCONF[CCE]を設定します。 8. MC_ME PRTN0_CORE4_PUPD[CCUPD]を設定します。 9. MC_ME CTL_KEYシーケンスを適用しました。 10. PRTN0_CORE4_STAT[CCS]が1になるまで待機しました。 11. 実験のため、MPUを一時的に無効にした。 12. CM7_2 DTCMバックドアアドレスへの32ビット書き込みを1回試行しました。   観測結果: - PRTN2_COFB2_STATはTCMコントローラのクロック要求がアクティブであることを示します。 - PRTN0_CORE4_STAT[CCS] が 1 になります。 - CM7_2 DTCMバックドア領域への最初の32ビット書き込みにより、不正確なバスフォルトが発生し、ハードフォルトにエスカレートします。   質問: 1.S32K328の場合、CM7_0からアクセス可能な正しいCM7_2 DTCMバックドア/システムアドレス範囲は何ですか? 2. CM7_2 CM7_0 CM7_2がCPU待機中にいる間、DTCMバックドアアクセスはサポートされていますか? 3.MC_MEとDCM_GPRの設定以外に、CM7_0がCM7_2のDTCMバックドアに書き込めるようにするには、XRDCの設定が必要ですか? 4. テストのためにMPUを一時的に無効にした場合でも、MPU領域は必要ですか? 5. TCMバックドアパスを使用する前に、MSCM/MCM/XBIC/ENEDCの設定が必要ですか? 6.PRTN2_COFB2_STAT[BLOCK64]はTCMコントローラークロックが有効であることCM7_2確認するための正しいステータスビットでしょうか? 7. PRTN0_CORE4_STAT[CCS]は、クロック/アクセスパスが有効であることCM7_2確認するための正しいステータスビットでしょうか? 8. バックドアアクセスによるDTCM ECC初期化の場合、CM7_0からの32ビット書き込みで十分でしょうか? 9. 最初のバックドア書き込みによって不正確なバスフォルトが発生した場合、その障害がXRDC、インターコネクト、またはマッピングされていないアドレスのいずれに起因するものかを特定するために、どのフォルト/XRDCレジスタをチェックする必要がありますか?   現在の目標: 私たちは最小限の煙試験のみを検証したいのです。 - CM7_2 DTCMバックドアへの32ビット書き込み1回、 - それから読み返します、 - 生産用途を検討する前に。   よろしくお願いします。 Re: S32K328: CM7_0 access to CM7_2 DTCM backdoor causes imprecise BusFault こんにちは、 @krishna_Bugudi さん、 1. S32K3xx_memory_map.xlsx を参照してください。DTCM_2 バックドア (アドレス 0x21800000) 2. はい 3. なし 4. なし 5. なし 6. はい、RMのセクション3.4「TCMをシステムメモリとして」を参照してください。 7. はい 8. はい、RMの表102を参照してください。メモリECC初期化の概要 9. XRDCが無効になっていると書かれていましたね。したがって、XRDCによって報告されることはない。 住所はどこに書きますか? よろしくお願いいたします。 ダニエル Re: S32K328: CM7_0 access to CM7_2 DTCM backdoor causes imprecise BusFault こんにちは、ダニエルさん。   ご確認いただきありがとうございます。   テストを更新してRM/NXPの手順に完全に準拠するようにしましたが、依然としてストアのハングアップが発生しています。   確認済みの住所: 私たちは以下の宛先に手紙を書いています。   0x21800000   これはS32K3xx_memory_map.xlsxと一致します。   DTCM_2 バックドア: - 開始アドレス: 0x21800000 - 終了アドレス: 0x2181FFFF - S32K328実装サイズ:128KB   メモリマップには、PRAM2_TCM_XBICがS32K328の以下の場所に存在することも示されています。 0x40408000 - 0x4040BFFF   そしてそれを次のように説明しています。 「クロスバー整合性チェッカー(PRAM2およびTCMバックドアAHBスプリッター)」   一方、0x40400000 の TCM_XBIC は S32K328 用に予約済みとしてマークされています。   最新のテストシーケンス:   1. MC_ME PRTN2_COFB2_CLKEN[REQ64]を設定します。 2. MC_ME PRTN2_PUPD[PCUD]を設定します。 3. MC_ME CTL_KEYシーケンスを適用します。 4. PRTN2_PUPD[PCUD]がクリアされるまで待ちます。 5. PRTN2_COFB2_STATを読み込む。   観察結果: PRTN2_COFB2_STAT = 0x00000039   6. DCM_GPR DCMRWF4[CM7_2_CPUWAIT]を設定します。 読み上げ確認: DCMRWF4 = 0x00080000   7. MC_ME PRTN0_CORE4_ADDR を安全なループアドレスに設定します。 読み返し: PRTN0_CORE4_ADDR = 0x00402408   8. MC_ME PRTN0_CORE4_PCONF[CCE]を設定します。 9. MC_ME PRTN0_CORE4_PUPD[CCUPD]を設定します。 10. MC_ME CTL_KEYシーケンスを適用します。 11. PRTN0_CORE4_STAT[CCS]が1になるまで待ちます。   観察結果: PRTN0_CORE4_STAT = 0x00000001   12. MPU CM7_0一時的に無効化して隔離する。 無効化前のMPU_CTRL = 0x00000003   13. 32ビット書き込みを1回試行します。   *(volatile uint32_t *)0x21800000 = 0u;   最新のパンくずリスト:   [CORE2_DTCM_SMOKE] S4B: WORD0 書き込み開始アドレス=0x21800000   店舗の次のパンくずリストに到達していません。   [CORE2_DTCM_SMOKE] S4B1: DSBの前にWORD0ストアが発行されました   そのため、ストア自体が次の指示に到達する前に停止したり完了しないように見えます。今回の最新のテストでは、DSB(深層破壊領域)には到達していません。   質問: あなたが確認した内容: - 0x21800000 は正しい DTCM_2 バックドア アドレスです。 - CM7_2がCPUWAIT中である間はCM7_0アクセスがサポートされます。 - XRDC/MPU/MSCM/MCM/XBIC/ENEDC の追加設定は不要です。 - PRTN2_COFB2_STAT[BLOCK64] は正しいステータスビットです。 - PRTN0_CORE4_STAT[CCS] は正しいステータスビットです。 - 32ビット書き込みはDTCM ECC初期化に有効です。   最初の32ビットストアが完成前に0x21800000止まる原因は何でしょうか?   S32K328のPRAM2_TCM_XBIC(アドレス0x40408000)でTCMバックドアAHBスプリッタエラーを検査すべきでしょうか?   もしそうなら、以下の場所を教えていただけますか: 1.PRAM2_TCM_XBIC ステータス/エラーレジスタを読み取ります。 2. DTCM_2バックドアトランザクションの失敗時に想定されるエラー表示。 3. アクセスを再試行する前にエラークリアシーケンスが必要かどうか。 4. ストアが完了しなかった場合にキャプチャする必要のあるその他の MC_ME/DCM/MSCM/XBIC/fault レジスタ。   よろしくお願いいたします。 クリシュナ Re: S32K328: CM7_0 access to CM7_2 DTCM backdoor causes imprecise BusFault こんにちは、クリシュナさん。 Copilot は次のように述べています。「テストしたところ、プロジェクトでデフォルトの MPU が有効になっている場合 (system.c で設定) にのみこのエラーを再現できました。」S32DS RTDプロジェクトによって生成されました。プロジェクトでMPUが無効化されているかどうかを確認するためにMPUレジスタをダンプすることはできますか? よろしくお願いいたします。 ダニエル
記事全体を表示