2391305_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2391305_en-US

2391305_en-US

zephyr: support compressed FW for RW61X

CONFIG_NXP_COMPRESS_WIFI_NB_FW is enabled by default in https://github.com/nxp-zephyr/nxp-zephyr/commit/e64f39fa2a05edec7bd8a2b24d9f1236c43d6c35

Cmake fails without a rw61x_sb_wifi_a2_compressed.bin file. Is there a missing compression step?  What compress method is supported?

I didn't see any changes to the loader.  Will it automatically handle a compressed fw?

Re: zephyr: support compressed FW for RW61XI now see there is a NXP zephyr forum. Should this be moved there?Re: zephyr: support compressed FW for RW61X

I'm using nxp-v4.4-branch zephyr/samples/net/wifi/shell on frdm_rw612.

I see what happened.  I had overlooked this west update error: 

=== updating wifi_nb_fw (modules/hal/nxp/zephyr/blobs):
fatal: destination path 'modules/hal/nxp/zephyr/blobs' already exists and is not an empty directory.

Then to get the FW, I used "west blobs fetch hal_nxp" per https://docs.zephyrproject.org/latest/boards/nxp/frdm_rw612/doc/index.html#wireless-connectivity-sup...

This didn't download the compressed images leading to the error I saw with CONFIG_NXP_COMPRESSED_WIFI_NB_FW set.

The blobs directory already had files from here it: https://github.com/nxp-zephyr/hal_nxp/tree/nxp-v4.4-branch/zephyr/blobs/license/


I was using west from .mcuxpressotools/.mcux-venv-3.12/bin/west which is v1.5.0.

I tried an older version (v1.3.0) and west just adds the repo to the existing non-empty directory without failing.

Re: zephyr: support compressed FW for RW61X

Hello,


Hope you are doing well. Could you please clarify what are you testing?

Are you working with a specific example?

Did you make any modification?


Best Regards,

Ricardo

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-08-2026 03:29 AM
更新者: