2391431_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2391431_en-US

2391431_en-US

RDDRONE-BMS772 Development Board

I'd like to know more about the RDDRONE-BMS772 board. It includes pins for an external temperature sensor, and a thermistor is also included in the accessories. Can this board be used to measure battery temperature? However, the accessories only list a thermistor, not a temperature sensor. If the board can be used to measure temperature, do I need to buy the temperature sensor separately? And where should the temperature sensor be installed?

Re: RDDRONE-BMS772开发板

Hello fan007

Good day!

I'd like to know more about the RDDRONE-BMS772 board.

It includes pins for an external temperature sensor, and a thermistor is also included in the accessories. Can this board be used to measure battery temperature? However, the accessories only list a thermistor, not a temperature sensor. If the board can be used to measure temperature, do I need to buy the temperature sensor separately? And where should the temperature sensor be installed?

In Getting Started with the RDDRONE-BMS772 Reference Design, you can find a chapter that describes everything included in the purchase of this board.

Yes, it includes an external thermistor with a cable, which can function as a temperature sensor. However, you can use another sensor that you consider more reliable. The board does have a dedicated port for connecting this sensor. More detailed information about its connection and use can be found in the documentation available on our website.

Please review: UM11421, RDDRONE-BMS772 reference design - User guide (you need an account with us to access this document)

An optional external temperature sensor can be added onto the RDDRONE-BMS772

board using connector J1. An example of application for this external sensor is used to

monitor the cells temperature inside the battery pack.

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-08-2026 03:32 AM
更新者: