Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Is it posibble to advance life cycle to OEM_PROD without program ADKP ? Hi, I am using S32K3xx MCU, and the HSE FW(v2.1.0) is installed (enabled), my question is it posibble to advance the life cycle to OEM_PROD without program ADKP ?  why I asking becuase I changed the life cycle to OEM, but I did not call Csm_SetHSEAttribute() to set the HSE_APP_DEBUG_KEY. Re: Is it posibble to advance life cycle to OEM_PROD without program ADKP ? Hi @snaku_lee  Is it posibble to advance the life cycle to OEM_PROD without program ADKP? No, even if your device is in Simulated_OEM_PROD, transitioning to OEM_PROD or IN_FIELD will only be possible if the Application Debugging Key/Password (ADKP) is provided. BR, VaneB Re: Is it posibble to advance life cycle to OEM_PROD without program ADKP ? I forgot to say that, the original life cycle is "Simulated_OEM_PROD", not "CUST_DEL". Is that possible to change the LC to OEM without ADKP in the "Simulated_OEM_PROD" life cycle?
View full article
Can you provide the FS26 datasheet? Hi, Can you provide the FS26 datasheet?
View full article
S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. I have try the S32 SAF V1.0.4 example code with RTD V4.0.0 1. The system enter ISR_SWT0 during sCheck xbic test (which the next test after SWT0 count test )(please refer screentshot1) 2. I have try to add breakpoint on SWT0 test.  all of count passed(screentshot2).  but scheck ISR triggered after SWT0 uninstall (screenshot3) May I ask if there any suggestion ? screenshot 1 screentshot2 screentshot3 Re: S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. Hi RadoslavB My sales support team told me there is a bug of SWT0  since RTM 1.0.2  , and RTM 1.0.4 not fixed it. Thanks for you help. Re: S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. Hi Sifan, I need to see your setup during debug session. Please contact me via NXP Sales Force system, so we can arrange the debug session. Kind Regards, Radoslav Re: S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. Hi RadoslavB 1. Yes, demo example, not modifed on configuration.  startup & ld file has update to IAR format 2. I have try to add break pointer on SWT0_ISR first line,  but it reboot again & again which seems cause by SWT0 timeout because no ISR handler it  ( stop at breakpoint ) 3. The WEN are zero when hang on SWT0_ISR trap. 4. I have try to disable SWT0 check via EB,  and system won't enter SWT0 ISR. Re: S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. Hi Sifan, if I understand correctly, you are executing SAF demo example, did you anyhow modify the code or configuration? On my side with the Demo example for S32K344 the SWT0 handler is triggered only once during the test as expected. I have all the time FRZ=0. Could you set breakpoint inside SWT0 handler, first intentional break stop should be during execution of sCheck_Swt_CounterTestRun() during the for loop. The SWT0 is enabled and disabled within Check_Swt_CounterBitCycle(), so beside that part the SWT IRQ should not be triggered. You can check if WEN bit is really zeroed or if there is still SWT0 interrupt pending bit set even after leaving SWT0 interrupt routine. Kind Regards, Radoslav Re: S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. Hi RadoslavB 1. SWT0 is disabled before the test. also it is disabled when issue occured. 2. AIPS_SLOW_CLK frequency is 40M.  3. Yes, FRZ bit is set to 0 which as same as SAF Demo V1.0.4.  I have to try to run without any debugger or without any breakpoint, The system hang on SWT0 ISR "while trap", too. Re: S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. Hi Sifan, sCheck does lat1ent faults check, as per ISO26262 it is sufficient to perform the test only once per drive cycle so no need to execute in both startup and runtime/shutdown. Before the test could you please check the SWT0 CR register if it is really disabled? Because SBAF bootrom enables SWT0 if it's enabled in Boot Configuration Word, bit APP_SWT_INIT.  SAF Demo should disable the SWT0 in startup, but please double check. Please check if the selected STM instance in sCheck Tresos is really same as it is configured in the RTD MCU driver And please check also AIPS_SLOW_CLK frequency in RTD MCU (CGM0_MUX0). The interrupt should be not triggered when disabling the SWT0 (if it was really disabled before the test). Edit: If you are using SWT0 setting from the SAF Demo startup, there is FZR bit se to 0 which means that the SWT0 is running even during debug break, so it might happen that if you have breakpoint before the sCheck restore function the timer elapses and trigger interrupt as soon as you continue debugging. For test purpose you can change the bit setting to 1 manually in the startup by modifying the value as depicted: Or use RTD WDG configuration with unchecked depicted option: But for production code you need to have FRZ bit se to 0, this is also checked by the sBoot module as this is recommended safety configuration by NXP.  Kind Regards, Radoslav Re: S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. Hi RadoslavB 1. I'm executing the SWT0 test as Starup & Runtime 2.This issure not 100% occured for each time. so Startup may success ,  but for runtime always hang on ISR trap under continue test. 3.I'm not enable SWT0 . not configure it up & running.  Just test it on runtime continue test. I think it may cause by SWT disable ( when sCheck swt count test done) and SWT interrupt coming at same time,  and S32K has few time to uninstall ISR before it handle the interrupt. Re: S32K344 SAF SWT0 ISR triggerd after sCheck unistall ISR. Hello Sifan, please are you executing the SWT0 test as Starup or Runtime/Shutdown? In case of startup test, sCheck does restore SWT.CR register, so if SWT0 was disabled it should be disabled after the test as well and should not trigger the interrupt. In case you are executing the SWT0 test in runtime/shutdown it is expected that you have configured the SWT0 so it's up and running and therefore you should have implemented also your handler for refreshing the SWT0, from the screenshot I can see there is just the while trap instead. In this case, please update the interrupt handler and replace the while trap with routine refreshing the SWT0. Kind Regards, Radoslav
View full article
FS26 のデータシートを提供できますか? こんにちは、 FS26 のデータシートを提供できますか?
View full article
NTAG5: Read UID via I2C ? Hi ! Is there a way to get the UID of the NTAG5 Link Chip via the I2C Interface ?  best regards  Re: NTAG5: Read UID via I2C ? Hello @rfid_profi  It seems not available for I2C interface. Because INVENTORY and SELECT commands are Supported by NFC interface.
View full article
UART3 on i.MX 8M Mini Hi, I try to use UART3 on i.MX 8M Mini LPDDR4 EVKB M4 core but I'm not getting any signals. I'm using the evkmimx8mm_iuart_interrupt_transfer example. I edited pin_mux.c: IOMUXC_SetPinMux(IOMUXC_UART3_RXD_UART3_RX, 0U); IOMUXC_SetPinConfig(IOMUXC_UART3_RXD_UART3_RX, IOMUXC_SW_PAD_CTL_PAD_DSE(6U) | IOMUXC_SW_PAD_CTL_PAD_FSEL(2U)); IOMUXC_SetPinMux(IOMUXC_UART3_TXD_UART3_TX, 0U); IOMUXC_SetPinConfig(IOMUXC_UART3_TXD_UART3_TX, IOMUXC_SW_PAD_CTL_PAD_DSE(6U) | IOMUXC_SW_PAD_CTL_PAD_FSEL(2U)); I also had to edit the function BOARD_BootClockRUN() in clock_config.c: CLOCK_SetRootMux(kCLOCK_RootUart3, kCLOCK_UartRootmuxSysPll1Div10); CLOCK_SetRootDivider(kCLOCK_RootUart3, 1U, 1U); CLOCK_EnableClock(kCLOCK_Uart3); And I of course changed the definitions in main.c: #define DEMO_UART UART3 #define DEMO_UART_CLK_FREQ \ CLOCK_GetPllFreq(kCLOCK_SystemPll1Ctrl) / (CLOCK_GetRootPreDivider(kCLOCK_RootUart3)) / \ (CLOCK_GetRootPostDivider(kCLOCK_RootUart3)) / 10 The Boot Switches are in Download Mode and I'm uploading the code via J-Link. I also configured UART3 in RDC. Therefore should UART3 be accessible with the M4, right? I connected Pin 8, which should be UART3 TX, from the Expansion Connector J1003 on an oscilloscope to detect signals but I can't see anything. What am I missing here? i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: UART3 on i.MX 8M Mini This worked for me as well , But I want to ask why we have done this. Re: UART3 on i.MX 8M Mini I could fix the issue by using the correct PinMux configuration. Instead of IOMUXC_UART3_RXD_UART3_RX  and IOMUXC_UART3_TXD_UART3_TX I'm using IOMUXC_ECSPI1_SCLK_UART3_RX and IOMUXC_ECSPI1_MOSI_UART3_TX now. Thank you for your help! Re: UART3 on i.MX 8M Mini do you dts has this? if yes, you need set to "disabled," pls double check it linux-imx/arch/arm64/boot/dts/freescale/imx8mm-evk.dtsi at lf-6.6.y · nxp-imx/linux-imx · GitHub &uart3 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_uart3>; assigned-clocks = <&clk IMX8MM_CLK_UART3>; assigned-clock-parents = <&clk IMX8MM_SYS_PLL1_80M>; fsl,uart-has-rtscts; status = "okay"; }; Re: UART3 on i.MX 8M Mini There's no dts when the switches are in Download mode. So UART3 should be free to use. Re: UART3 on i.MX 8M Mini could you confirm if your dts doesn't use uart3? if linux side uses this, you need disable this firstly, I don't know how your SW is, you can check it by yourself
View full article
请问 FS26 datasheet 能提供吗 hi, 请问 FS26 datasheet 能提供吗 Re: 请问 FS26 datasheet 能提供吗 HI Bert 您直接可以下载: FS26 | Safety System Basis Chip with Low Power, for ASIL D Systems | NXP Semiconductors
View full article
i.MX 8M Plus Cortex A53 Bare Metal Programming Hi Team, We are planning to do bare metal programming on i.MX 8M Plus Cortex A53 Processor.  1. Do we have bare metal support for cortex A-35 on the i.MX 8M Plus processor? If so, please share me related document links and sample projects.  2. If bare metal programming is not supported, can we run FreeRTOS on cortex A-35 on the i.MX 8M Plus processor. If so, please share me related document links and sample projects.  Regards, Anand Kumar D Re: i.MX 8M Plus Cortex A53 Bare Metal Programming Hello Zhiming, Thank You! for the support.  We have VAR-SOM-MX8M-PLUS System on Module Eval Kit with us and we will do some trials with it following the guidelines provided in the links.  Regards, Anand Kumar D Re: i.MX 8M Plus Cortex A53 Bare Metal Programming Hello, Please refer zephyrproject and it's source code. https://docs.zephyrproject.org/latest/develop/getting_started/index.html https://github.com/zephyrproject-rtos/zephyr Best Regards, Zhiming
View full article
Kernal build is failed for android bsp 12 showing FAILED: load BTF from vmlinux: Invalid argument I have tried to build the bsp of android 12 for imx-8mn evk board with lunch 61 but i got following error TEE_LOAD_ADDR=0x56000000 ATF_LOAD_ADDR=0x00960000 VERSION=v2 ./print_fit_hab.sh 0x60000 evk.dtb 0x40200000 0x5B000 0xEFEA8 0x402EFEA8 0x14AEA8 0xBE38 0x960000 0x156CE0 0xA0D0 make[1]: Leaving directory '/home/[email protected]/android_build/vendor/nxp-opensource/imx-mkimage' ===================Finish building imx8mn-evk-uuu:imx8mn_evk_android_uuu_defconfig =================== MODPOST vmlinux.symvers MODINFO modules.builtin.modinfo GEN modules.builtin LD .tmp_vmlinux.btf BTF .btf.vmlinux.bin.o LD .tmp_vmlinux.kallsyms1 KSYMS .tmp_vmlinux.kallsyms1.S AS .tmp_vmlinux.kallsyms1.S LD .tmp_vmlinux.kallsyms2 KSYMS .tmp_vmlinux.kallsyms2.S AS .tmp_vmlinux.kallsyms2.S LD vmlinux BTFIDS vmlinux FAILED: load BTF from vmlinux: Invalid argument make[2]: *** [/home/[email protected]/android_build/vendor/nxp-opensource/kernel_imx/Makefile:1247: vmlinux] Error 255 make[2]: *** Deleting file 'vmlinux' make[2]: Leaving directory '/home/[email protected]/android_build/out/target/product/evk_8mn/obj/KERNEL_OBJ' make[1]: *** [Makefile:237: __sub-make] Error 2 make[1]: Leaving directory '/home/[email protected]/android_build/vendor/nxp-opensource/kernel_imx' make: *** [/home/[email protected]/android_build/device/nxp/common/build/kernel.mk:197: /home/[email protected]/android_build/out/target/product/evk_8mn/obj/KERNEL_OBJ/arch/arm64/boot/Image.lz4] Error 2 make: Leaving directory '/home/[email protected]/android_build' full log while running the ./imx-make.sh is attached Android Re: Kernal build is failed for android bsp 12 showing FAILED: load BTF from vmlinux: Invalid argumen Hello, Please use Ubuntu18.04 to compile Android12. Best Regards, Zhiming Re: Kernal build is failed for android bsp 12 showing FAILED: load BTF from vmlinux: Invalid argumen => Can you try to delete /home/[email protected]/android_build/out/target/product/evk_8mn/obj/KERNEL_OBJ and rebuild it again? Ans : Already tried the build multiple times after make clean => Are you using Ubuntu18.04? Ans : No , Ubuntu 22.04.5 LTS => Did you install the gcc here : 1. Prepare the build environment for U-Boot and Linux kernel ? Ans : yes Re: Kernal build is failed for android bsp 12 showing FAILED: load BTF from vmlinux: Invalid argumen Hello, Can you try to delete /home/[email protected]/android_build/out/target/product/evk_8mn/obj/KERNEL_OBJ and rebuild it again? Are you using Ubuntu18.04? Did you install the gcc here : 1. Prepare the build environment for U-Boot and Linux kernel ? Best Regards, Zhiming
View full article
NXP LS1043A 配置 LPUART 实现 RS485 半双工串行通信 你好,我正在尝试配置 LS1043A 中的 LPUART3,以使用 2 线模式进行 RS485 半双工操作。我必须涵盖以下场景: 1. RS485半双工回波接收传输的数据 2. RS485 半双工,无回声,因此没有传输数据的接收 操作将在这两种模式之间切换并正确同步。您能提供上述两种场景的LPUART寄存器配置吗? QorIQ LS1设备 回复:NXP LS1043A 配置 LPUART 进行 RS485 半双工串行通信 非常感谢您的回复! 回复:NXP LS1043A 配置 LPUART 进行 RS485 半双工串行通信 请参阅附件的lpuart设备驱动程序。
View full article
ADC ChannelType 我想知道S32K3XX的ADC中,P、S、MA、X这些通道后缀的含义是什么,在手册中哪个地方有详细的描述呢?
View full article
NXP LS1043A RS485半二重シリアル通信用にLPUARTを構成 こんにちは、私は2線式モードを使用してRS485半二重動作のLS1043AでLPUART3を構成しようとしています。私は次のシナリオをカバーする必要があります: 1. 送信されたデータを受信するためのエコーバック付きRS485半二重 2.エコーバックなしのRS485半二重により、送信データの受信がなくなります 操作はこれらのモード間で切り替えられ、適切に同期されます。上記の 2 つのシナリオで LPUART レジスタの構成を提供できますか。 QorIQ LS1デバイス Re:NXP LS1043A RS485半二重シリアル通信用のLPUARTを構成する ご回答いただき、誠にありがとうございます! Re:NXP LS1043A RS485半二重シリアル通信用のLPUARTを構成する 添付のlpuartデバイスドライバを参照してください。
View full article
NXP LS1043A configure LPUART for RS485 half-duplex serial communication Hi, I am trying to configure LPUART3 in LS1043A for RS485 half-duplex operation using 2-wire mode. I have to cover following scenarios: 1. RS485 half duplex with echo back to receive the transmitted data 2. RS485 half duplex without echo back so that there is no receive of transmitted data The operation will be switched between both these modes and is properly synchronized. Can you provide the configuration of LPUART registers for the above two scenarios? QorIQ LS1 Devices Re: NXP LS1043A configure LPUART for RS485 half-duplex serial communication Thank you very much for your response! Re: NXP LS1043A configure LPUART for RS485 half-duplex serial communication Please refer to the attached lpuart device driver.
View full article
i.MX 8M Plus Cortex A53 ベアメタルプログラミング こんにちはチーム、 私たちは、8M Plus Cortex A53プロセッサでベアメタルプログラミングを行う予定です i.MX。 1. i.MX 8M PlusプロセッサのCortex A-35のベアメタルサポートはありますか?もしそうなら、関連ドキュメントのリンクとサンプルプロジェクトを共有してください。 2.ベアメタルプログラミングがサポートされていない場合、i.MX 8M PlusプロセッサのCortex A-35でFreeRTOSを実行できますか。もしそうなら、関連ドキュメントのリンクとサンプルプロジェクトを共有してください。 よろしくお願いします。 アナンド・クマールD Re:i.MX 8M Plus Cortex A53ベアメタルプログラミング こんにちは、Zhiming、 ありがとうございます!サポートのために。 VAR-SOM-MX8M-PLUS System on Module Eval Kitを使用しており、リンクに記載されているガイドラインに従っていくつかの試用を行います。 よろしくお願いします。 アナンド・クマールD
View full article
i.MX 8M Plus Cortex A53 裸机编程 大家好, 我们计划在 i.MX 8M Plus Cortex A53 处理器上进行裸机编程。 1. 我们是否为 i.MX 8M Plus 处理器上的 Cortex A-35 提供裸机支持?如果有,请与我分享相关文档链接和示例项目。 2.如果不支持裸机编程,我们可以在i.MX 8M Plus处理器上的cortex A-35上运行FreeRTOS吗?如果有,请与我分享相关文档链接和示例项目。 此致, 阿南德·库马尔 回复:i.MX 8M Plus Cortex A53 裸机编程 志明你好, 谢谢!的支持。 我们拥有 VAR-SOM-MX8M-PLUS 系统模块评估套件,我们将按照链接中提供的指南对其进行一些试验。 此致, 阿南德·库马尔
View full article
尝试批量擦除后无法连接到S32K118 大家好,NXP 团队和其他人。 我正在使用 S32k118 CSEc 并尝试了 AN5401 提供的示例 1:配置部件和加载密钥。我在 DebugRAM 配置中运行了该项目,可以对 MCU 进行分区并设置密钥。我没有对密钥设置任何保护,但是当我下次尝试擦除整个芯片时,我收到了保护字节已设置的消息。当我继续时,它不断抛出相同的消息并最终失败。 以下是 JLink 的输出: 正在连接... - 通过 USB 连接到探针/编程器设备 0 - 探针/编程器固件:J-Link Ultra V5 编译于 2024 年 2 月 19 日 15:14:38 探头/编程器序列号:505002010 -选择设备“S32K118(允许安全)”。 - 目标接口速度:4000 kHz(固定) - VTarget = 3.305V - InitTarget() 开始 - 已选择 SWD。执行 JTAG -> SWD 切换序列。 - 设备现在将不再安全。 - 停止 CPU 时超时。 - InitTarget() 结束 - 耗时 4.33 秒 - 找到 ID 为 0x0BC11477 的 SW-DP - DPIDR:0x0BC11477 - CoreSight SoC-400 或更早版本 - 扫描 AP 地图以查找所有可用的 AP - AP[2]: 由于已到达 AP 地图末尾,因此停止 AP 扫描 - AP[0]: AHB-AP (IDR: 0x04770031) - AP[1]: JTAG-AP (IDR: 0x001C0020) - 迭代 AP 映射以找到要使用的 AHB-AP - AP[0]: 已跳过。无法读取 CPUID 寄存器 - AP[1]:已跳过。不是 AHB-AP - 连接到 CPU 失败。重置下执行连接。 - DPIDR:0x0BC11477 - CoreSight SoC-400 或更早版本 - 扫描 AP 地图以查找所有可用的 AP - AP[2]: 由于已到达 AP 地图末尾,因此停止 AP 扫描 - AP[0]: AHB-AP (IDR: 0x04770031) - AP[1]: JTAG-AP (IDR: 0x001C0020) - 迭代 AP 映射以找到要使用的 AHB-AP - AP[0]: 已跳过。无法读取 CPUID 寄存器 - AP[1]:已跳过。不是 AHB-AP - 在 Coresight 设置中找不到核心 我也尝试了这里建议的序列https://community.nxp.com/t5/S32K/Unbricking-S32K146/mp/937227: J-Link>r0 J-Link>swdwritedp 2,0x01000000 写入 DP 寄存器 2 = 0x01000000 J-Link>swdreadap 0 读取 AP 寄存器 0 = 0x00000000 J-Link>swdreadap 0 读取 AP 寄存器 0 = 0x00000037 J-Link>swdreadap 1 读取AP寄存器1 = 0x00000037 J-Link>swdreadap 1 读取 AP 寄存器 1 = 0x00000000 J-Link>解锁 Kinetis 找到 ID 为 0x0BC11477 的 SWD-DP 解锁设备...确定 但我仍然无法连接 我尝试过连接 SEGGER Jlink 和 Onboard Pemicro - 结果是一样的。你能解释一下为什么会发生这种情况以及我该如何克服这个问题并避免将来再发生这种情况吗?谢谢。 回复:尝试批量擦除后无法连接到S32K118 谢谢你的回答。 但是 s32k1-RM rev14.1 中的“36.5.12.2.1 使用后门密钥访问取消保护 MCU”部分又如何呢?有帮助嗎?或者 Jlink 命令“解锁 Kinetis”尝试执行该操作?
View full article
Failed to connect to s32k118 after mass erase attempt Hello, NXP team and others. I am working with the S32k118 CSEc and tried the Example-1: Configure Part and Load Keys, provided by AN5401. I ran the project in DebugRAM config and could partition MCU and set the keys. I haven't set any protection to the keys but when next time I tried to Erase the whole chip I got the message that the protection bytes are set. When I proceed it keeps throwing the same message and eventually fails. Here is the output from JLink: Connecting ... - Connecting via USB to probe/ programmer device 0 - Probe/ Programmer firmware: J-Link Ultra V5 compiled Feb 19 2024 15:14:38 - Probe/ Programmer S/N: 505002010 - Device "S32K118 (ALLOW SECURITY)" selected. - Target interface speed: 4000 kHz (Fixed) - VTarget = 3.305V - InitTarget() start - SWD selected. Executing JTAG -> SWD switching sequence. - Device will be unsecured now. - Timeout while halting CPU. - InitTarget() end - Took 4.33s - Found SW-DP with ID 0x0BC11477 - DPIDR: 0x0BC11477 - CoreSight SoC-400 or earlier - Scanning AP map to find all available APs - AP[2]: Stopped AP scan as end of AP map has been reached - AP[0]: AHB-AP (IDR: 0x04770031) - AP[1]: JTAG-AP (IDR: 0x001C0020) - Iterating through AP map to find AHB-AP to use - AP[0]: Skipped. Could not read CPUID register - AP[1]: Skipped. Not an AHB-AP - Attach to CPU failed. Executing connect under reset. - DPIDR: 0x0BC11477 - CoreSight SoC-400 or earlier - Scanning AP map to find all available APs - AP[2]: Stopped AP scan as end of AP map has been reached - AP[0]: AHB-AP (IDR: 0x04770031) - AP[1]: JTAG-AP (IDR: 0x001C0020) - Iterating through AP map to find AHB-AP to use - AP[0]: Skipped. Could not read CPUID register - AP[1]: Skipped. Not an AHB-AP - Could not find core in Coresight setup I also tried the sequence as suggested here https://community.nxp.com/t5/S32K/Unbricking-S32K146/m-p/937227 : J-Link>r0 J-Link>swdwritedp 2,0x01000000 Write DP register 2 = 0x01000000 J-Link>swdreadap 0 Read AP register 0 = 0x00000000 J-Link>swdreadap 0 Read AP register 0 = 0x00000037 J-Link>swdreadap 1 Read AP register 1 = 0x00000037 J-Link>swdreadap 1 Read AP register 1 = 0x00000000 J-Link>unlock Kinetis Found SWD-DP with ID 0x0BC11477 Unlocking device...O.K. But then I still cannot connect I have tried connecting with SEGGER Jlink and Onboard Pemicro - the result is the same. Could you explain why it happened and how can I overcome this and avoid in the future? Thanks. Re: Failed to connect to s32k118 after mass erase attempt Hello @dmitry_buchynski, It would have to be implemented in the application SW first. https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-Verify-Backdoor-Access-Key-S32DS1-3/ta-p/1102820 Also, the partitioning along with the CSEc keys can be removed, and the CSEc example shows how. But again, such a code would have to be in the MCU already. Regards, Daniel Re: Failed to connect to s32k118 after mass erase attempt Thanks for the answer. But what about section '36.5.12.2.1 Un-securing the MCU using backdoor key access' from s32k1-RM rev14.1? Is it of any help? Or Jlink command "unlock Kinetis" tries to perform exactly that? Re: Failed to connect to s32k118 after mass erase attempt Hello @dmitry_buchynski, If the CSEc key space is allocated by the Program Partition command, the debugger cannot use Mass erase anymore. https://www.nxp.com/docs/en/application-note/AN12130.pdf Section 3.2.5.2 Mass erase and CSEc considerations. Then, the debugger can erase the MCU by sectors only. In this case, however, the MDM-AP Status[2] register shows that the MCU is secure (FSEC[SEC] = secure). That means the previous erasing by sectors/programming must have failed, leaving on the flash configuration field in this secure state. I'm afraid there is nothing we can do to recover it at this point. Regards, Daniel
View full article
大量消去を試みた後、s32k118に接続できませんでした こんにちは、NXPチームなど。 私はS32k118 CSEcを使用しており、AN5401が提供するExample-1:パーツキーとロードキーの設定を試しました。DebugRAM構成でプロジェクトを実行し、MCUをパーティション分割してキーを設定することができました。キーに保護を設定していませんが、次にチップ全体を消去しようとすると、保護バイトが設定されているというメッセージが表示されました。続行すると、同じメッセージがスローされ続け、最終的には失敗します。 JLinkからの出力は次のとおりです。 接続。。。 - プローブ/プログラマデバイス0にUSB経由で接続 - プローブ/プログラマーファームウェア:J-Link Ultra V5 コンパイル済み Feb 19, 2024 15:14:38 - プローブ/プログラマS / N:505002010 - デバイス「S32K118 (ALLOW SECURITY)」が選択されました。 - 目標インターフェース速度:4000kHz(固定) - VTarget = 3.305V - InitTarget() の開始 - SWD が選択されました。JTAG -> SWDスイッチングシーケンスを実行しています。 - これでデバイスのセキュリティが解除されます。 - CPU の停止中にタイムアウトします。 - InitTarget() 終了 - 4.33 秒かかりました - ID 0x0BC11477のSW-DPが見つかりました - DPIDR:0x0BC11477 - CoreSight SoC-400以前 - APマップをスキャンして、使用可能なすべてのAPを見つける - AP[2]: AP マップの末尾に達したため、AP スキャンを停止しました - AP[0]:AHB-AP(IDR:0x04770031) - AP[1]:JTAG-AP(IDR:1 0x001C0020) - APマップを反復処理して、使用するAHB-APを見つける - AP[0]:スキップしました。CPUID レジスタを読み取れませんでした - AP[1]: スキップしました。AHB-APではありません - CPU への接続に失敗しました。リセット状態で接続を実行しています。 - DPIDR:0x0BC11477 - CoreSight SoC-400以前 - APマップをスキャンして、使用可能なすべてのAPを見つける - AP[2]: AP マップの末尾に達したため、AP スキャンを停止しました - AP[0]:AHB-AP(IDR:0x04770031) - AP[1]:JTAG-AP(IDR:1 0x001C0020) - APマップを反復処理して、使用するAHB-APを見つける - AP[0]:スキップしました。CPUID レジスタを読み取れませんでした - AP[1]: スキップしました。AHB-APではありません - Coresightセットアップでコアが見つかりませんでした ここで提案されているように、シーケンスも試してみ ました https://community.nxp.com/t5/S32K/Unbricking-S32K146/m-p/937227: Jリンク>R0 J-Link>swdwritedp 2,0x01000000 DPレジスタの書き込み 2 = 0x01000000 J-リンク>swdreadap 0 APレジスタの読出し0 = 0x00000000 J-リンク>swdreadap 0 APレジスタの読出し0 = 0x00000037 J-リンク>swdreadap 1 APレジスタの読出し1 = 0x00000037 J-リンク>swdreadap 1 APレジスタの読出し1 = 0x00000000 J-Link>ロック解除 Kinetis ID が 0x0BC11477 の SWD-DP が見つかりました デバイスのロック解除...わかりました しかし、それでも私は接続できません SEGGER JlinkとOnboard Pemicroで接続してみましたが、結果は同じです。なぜそれが起こったのか、そしてどうすればこれを克服し、将来回避できるのか説明していただけますか?感謝。 Re:大量消去を試みた後、s32k118に接続できませんでした 答えをありがとう。 しかし、s32k1-RM rev14.1のセクション「36.5.12.2.1バックドアキーアクセスを使用したMCUの保護解除」はどうですか?何かお役に立てますか?それとも、Jlinkコマンドの「Kinetisのロックを解除」はまさにそれを実行しようとしますか?
View full article
Where we can find Chip configuration information Where can we find the chip configuration information for NXP S32K1xx Microcontrollers Re: Where we can find Chip configuration information Hi@gkunalupta PDB is an internal module of the chip, and it has no external pins connected to it directly. PDB needs to be connected to external pins through the TRGMUX module. In the previous answer, I have told you the location of S32K1xx_Trigger_Muxing.xlsx Re: Where we can find Chip configuration information And where can i find information for device chip configuration details  to know about PDB Pulse out pin Re: Where we can find Chip configuration information Hi@gkunalupta S32K1xx_Trigger_Muxing.xlsx can be found in S32K-RM's attachments. Re: Where we can find Chip configuration information I want to know where can i finds chip specific details, for trigger inputs details which are mentioned: I want to know about trigger inputs, for that on datasheet it is written that find information on chip configuration details. Where can i find that??? Re: Where we can find Chip configuration information Hi@gkunalupta Could you describe your problem in more detail? Do you want the datasheet for s32k1 or something else? Re: Where we can find Chip configuration information Also from where can i found information on which pin to use for pulse-out?
View full article
PDB Interrupt in S32K144 how to enable How to enable the interrupt in PDB module of S32K144 MCU via Autosar RTD of 2108 Re: PDB Interrupt in S32K144 how to enable Hi, Thank you so much for your interest in our products and for using our community. There is no PDB example with autosar mcal, but you could refer to the following community thread: https://community.nxp.com/t5/S32K/ADC-project-using-MCAL/td-p/1616331 Hope it helps you. Have a nice day! Re: PDB Interrupt in S32K144 how to enable Also, in Channel Configuration. I cant select channel Index value of 0 for anothe channel. So how i am supposed multiple channels via PDB for ADC?
View full article