1931076_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1931076_en-US

1931076_en-US

Is it posibble to advance life cycle to OEM_PROD without program ADKP ?

Hi,

I am using S32K3xx MCU, and the HSE FW(v2.1.0) is installed (enabled), my question is it posibble to advance the life cycle to OEM_PROD without program ADKP ? 

why I asking becuase I changed the life cycle to OEM, but I did not call Csm_SetHSEAttribute() to set the HSE_APP_DEBUG_KEY.

Re: Is it posibble to advance life cycle to OEM_PROD without program ADKP ?

Hi @snaku_lee 

Is it posibble to advance the life cycle to OEM_PROD without program ADKP? No, even if your device is in Simulated_OEM_PROD, transitioning to OEM_PROD or IN_FIELD will only be possible if the Application Debugging Key/Password (ADKP) is provided.


BR, VaneB

Re: Is it posibble to advance life cycle to OEM_PROD without program ADKP ?I forgot to say that, the original life cycle is "Simulated_OEM_PROD", not "CUST_DEL". Is that possible to change the LC to OEM without ADKP in the "Simulated_OEM_PROD" life cycle?
标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 09:10 PM
更新人: