[S32K344] Random Resets of Type "MCU_F_EXR_RESET" I am developing using a custom PCBA with an S32K344 microcontroller, and I occasionally have seen the board randomly reset and after the board resets, the `Power_Ip_GetResetReason()` function returns `MCU_F_EXR_RESET` (value = 15), which appears to be an external reset (i.e., the RESET pin was pulled low). However, when this has occurred, I have had nothing connected to the RESET pin, and the RESET pin is pulled high with a 10 kOhm resistor. Upon reading documentation, I found this section in the user manual for the S32K344 White Board: Is there a comprehensive list of these "some MCU internal failures" which can pull the RESET line low? Also, does this mean the MCU itself can pull the RESET pin low internally upon some other internal failure? If so would I still receive the `MCU_F_EXR_RESET` reset reason? Re: [S32K344] Random Resets of Type "MCU_F_EXR_RESET" @jleveque, I'm curious if you ever discovered the root cause of your unexpected resets? Re: [S32K344] Random Resets of Type "MCU_F_EXR_RESET" I do not know your API so it hard to judge what is : MCU_F_EXR_RESET "MCU_F_EXR_RESET" is a member of the "Power_Ip_ResetType" enum type in the Power_Ip_Specific.h file (part of the RTD, version 3.0.0). This is the type returned by the Power_Ip_GetResetReason() function defined in the Power_Ip.c file. Internal resets will also be propagated to reset_b pin as it is bidirectional. But there wont be set F_EXR flag in RGM [FES], but some other internal source flag. This is the info I was looking for. As long as it is guaranteed that the F_EXR flag will only ever be set if the RESET pin was pulled low externally (and not from an internal reset) then I can narrow down my search as to what is causing this issue. Thanks again, Peter! Re: [S32K344] Random Resets of Type "MCU_F_EXR_RESET" Hello,
I do not know your API so it hard to judge what is : MCU_F_EXR_RESET
But if you have external reset flag set in the RGM FES register then it mean the reset wa triggered from outside of uC.
Internal resets will also be propagated to reset_b pin as it is bidirectional.
But there wont be set F_EXR flag in RGM [FES], but some other internal source flag.
Best regards,
Peter Re: [S32K344] Random Resets of Type "MCU_F_EXR_RESET" This can be cause also by debugger, which is also pulling external reset. So the question is how do you read this function. Thank you for your reply, Peter! As I stated above, this reset is occurring with nothing connected to the RESET pin (the debugger is not physically connected), so this is being triggered by something else. As to how I read this function, I call the function first thing after boot and store the return value. Per your suggestion, I will add additional direct reads of the RGM [FES/DES] registers in hopes that I can get more insight, but ultimately I really want to know what are the "MCU internal failures" which can cause this "MCU_F_EXR_RESET" reset reason. Re: [S32K344] Random Resets of Type "MCU_F_EXR_RESET" Hello,
`Power_Ip_GetResetReason()` function returns `MCU_F_EXR_RESET`
This can be caused also by debugger, which is also pulling external reset.So the question is how do you read this function.
But nevertheless you can read reset reason from RGM [FES/DES] registers:
Clear FES/DES first.After your reset, read the registers to see the reset root cause.
Usually you in SW clear the FES/DES after power on reset and test if the FES/DES value is 0. If not you run diagnostics to see the reset reason.
Best regards,
Peter
Re: [S32K344] Random Resets of Type "MCU_F_EXR_RESET" Unfortunately, no. I left the company I was working for before this was resolved. It was last left in the hands of the electrical engineer who designed the board to review the PCB design with the suspicion that the cause may be EMI. I will note that on a subsequent project I worked on featuring an S32K358 MCU, I experienced spurious wake-ups from Standby mode, and I was able to reliably reproduce it by standing up out of my office chair. Looking into this phenomenon, I discovered that an office chair with a gas shock and metal legs can act as an EMP antenna, radiating a strong electromagnetic field! I found that there was actually a whitepaper written about it back in 1993: https://www.emcesd.com/pdf/eos93.pdf. I could measure this with an oscilloscope probe connected to nothing. Standing up from my chair would trigger the scope with a very brief spike of ~25V. So my original reset issue may have also been caused by EMI, as we had last suspected. I would suggest looking into EMI as a potential cause of your resets. Good Luck!
View full article