Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
s32 design studio for arm V2.2 license expired Hello, my S32 Design Studio for ARM v2.2 license has expired 12 Oct 2026. Registration Code:S32DS-IDE-ARM-V2-X_181798567 Product Version: S32 Design Studio for ARM v2.2] Please extend the license. Thank you. Re: s32 design studio for arm V2.2 license expired Hi,  your S32DS license has been extended. Please activate S32DS again with your old code. 
View full article
iMX8 支持的端点数量 iMX8 使用 DWC3 作为 USB 控制器,DWC3 是一款 xHCI 控制器。从 iMX8 的寄存器中读取数据后,我发现它最多可以支持 64 个设备。但是当我连接几个设备时,之前就出现了 xHCI 资源错误。似乎端点数量存在某种限制,而且似乎还取决于传输类型(批量、控制等)。在我使用的这类设备(包括集线器)中,似乎在连接 80 个终端后就会出现问题。请问能否提供一些确切的数字/公式,说明支持多少个端点? Re: Number of supported endpoints on the iMX8 你好, i.MX8 xHCI MaxSlots = 64 值指定了可启用 USB 设备插槽的最大数量,而不是端点总容量。xHCI 每个设备最多支持 31 个端点上下文,但控制器不保证所有 64 个插槽都能同时使用最大数量的端点。可用总量主要取决于周期带宽、设备速度、端点间隔和数据包大小、集线器拓扑结构、事务转换器分配和 DWC3 实现资源。   详细信息请参考xHCI规范。 Re: Number of supported endpoints on the iMX8 我查阅了xHCI规范,但没有找到任何相关说明。xHCI 唯一明确规定控制器可以返回资源错误(就是我上面提到的那个错误)的地方是…… 例如。英特尔表示,他们的一款 xHCI 控制器支持多达 2048 个批量/控制 EP 或多达 128 个中断/同步 EP。 https://edc.intel.com/content/www/us/en/design/ipla/software-development-platforms/servers/platforms... 我们有一个测试装置(仅限 USB 2.0),它在 Intel 芯片上运行良好(数百个 EP),但在 iMX8MP 上的部分设备(前面提到的 80 个 EP)上失败。 但是,要了解我们可以支持多少种以及哪些类型的设备,我们需要知道 iMX8MP/DWC3 的限制是什么。如果您能像英特尔那样,为我们提供一些公式或限制条件,那将非常有帮助。
View full article
s32 design studio for arm V2.2 许可证已过期 你好, 我的S32 Design Studio for ARM v2.2许可证已于2026 年 10 月 12 日到期。 注册码:S32DS-IDE-ARM-V2-X_181798567 产品版本:S32 Design Studio for ARM v2.2] 请延长许可证期限。 谢谢! Re: s32 design studio for arm V2.2 license expired 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。
View full article
Inquiry regarding ASHA packet loss, Bluetooth stress test disconnection, [Content Removed] Re: Inquiry regarding ASHA packet loss, Bluetooth stress test disconnection, [Content Removed] Re: Inquiry regarding ASHA packet loss, Bluetooth stress test disconnection, [Content Removed]
View full article
iMX8でサポートされるエンドポイントの数 iMX8はUSB用のDWC3を使っており、これはxHCIコントローラです。iMX8のレジスタを読み上げると、最大64台のデバイスをサポートしている可能性があることがわかりました。しかし、いくつかのデバイスを接続すると、かなり早い段階でxHCIリソースエラーが発生します。エンドポイントの数には何らかの制限があるようで、転送タイプ(バルク、コントロールなど)によっても異なるようです。私が使用しているタイプのデバイス(ハブを含む)では、エンドポイントが80個を超えると問題が発生するようです。サポートされているエンドポイントの数について、正確な数字や計算式を教えていただけますか? Re: Number of supported endpoints on the iMX8 こんにちは、 i.MX8 xHCI MaxSlots = 64という値は、有効にできるUSBデバイススロットの最大数を指定するものであり、エンドポイントの総容量を指定するものではありません。xHCIは1デバイスあたり最大31のエンドポイントコンテキストを利用できますが、コントローラは64スロットすべてが同時に最大数のエンドポイントを使用できる保証はありません。使用可能な合計値は、主に周期的な帯域幅、デバイスの速度、エンドポイントの間隔とパケットサイズ、ハブのトポロジー、トランザクショントランスレータの割り当て、およびDWC3の実装リソースに依存します。   詳細については、xHCI仕様書を参照してください。 Re: Number of supported endpoints on the iMX8 xHCI仕様を確認しましたが、特に表示はありませんでした。xHCIがコントローラがリソースエラーを返すと指定しているのは(先に述べたものです) 例えば。Intelは、xHCIコントローラの一つで最大2048のバルク/コントロールEPまたは最大128の割り込み/アイソクロナスEPをサポートすると説明しています。 https://edc.intel.com/content/www/us/en/design/ipla/software-development-platforms/servers/platforms... 当社にはテスト環境(USB 2.0のみ)があり、Intelチップ(数百個のEP)では正常に動作しますが、iMX8MP搭載デバイスの一部(前述の80個のEP)では動作しません。 しかし、どれくらいのデバイス、どのタイプのデバイスがサポートできるかを知るには、iMX8MP/DWC3の制限を知る必要があります。インテルのように、何らかの公式や制限を教えていただけるととても助かります。
View full article
ASHAパケット損失、Bluetoothストレステスト切断に関する問い合わせ、 [コンテンツ削除済み] Re: Inquiry regarding ASHA packet loss, Bluetooth stress test disconnection, [コンテンツ削除済み] Re: Inquiry regarding ASHA packet loss, Bluetooth stress test disconnection, [コンテンツ削除済み]
View full article
One of the Chinese tags keeps suddenly displaying garbled characters (guiguider2.0.1). The first Chinese character after generating the code is garbled. It works fine when the project is first created, but after subsequent editing, a label suddenly appears that displays incorrectly. Deleting and recreating it fixes the issue, but the same problem occurs randomly next time. Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 1. Currently, only this one project is being used. 2. This can happen after the layout has been modified, such as when the view has been moved to another parent view. 3. Win10 Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 Hello @JasonZhang111111111111111 , Good afternoon. To further investigate this issue, I would like to ask you to confirm the following information: 1. Does this problem only occur in the current project, or can it be reproduced in other projects? 2. Could you provide more detailed steps to reproduce this? 3. What operating system and version are you currently using? For example, Windows 10, Windows 11, Linux, or macOS. BR Celeste Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 Hello @JasonZhang111111111111111 , Sorry for the late reply. Thank you for your explanation. I still haven't been able to reproduce it. I'd like to confirm again, what exactly do you mean by "moving to another parent control"? Is it by copying/pasting to the new parent control, or by directly dragging the control to the new parent control in the control tree? Alternatively, if it's convenient, could you please send us the project files directly for us to try? BR Celeste
View full article
USB VID/PIDプログラムはまだアクティブですか? こんにちは、 私たちはLPC5528をベースにしたUSB CDCインターフェース付きのホームコントローラを開発している小さな会社です。予想販売量は1万ユニットを大きく下回る。NXP VIDのPIDを、USB VID/PIDプログラムを通じて申請したいと考えています。 プログラムFAQ(contact.nxp.com/vid-usb-app)にリンクされている申請フォームは利用できず、CASEポータルは当社のドメインに登録されていないためアカウントを拒否します。 プログラムはまだ有効ですか?もしそうなら、現在の申請方法は何でしょうか? ありがとうございます! Re: USB VID/PID program still active ? はい、NXPのUSB VID/PIDプログラムは現在も有効です。以前のウェブフォーム(`contact.nxp.com/vid-usb-app`)は廃止され、現在はご利用いただけません。 現在の公式な申請方法は、NXPコミュニティポータルから直接サポートチケットを作成することです。 無料のPIDを取得するための手順は以下のとおりです。 1. **NXPコミュニティページへ移動**:公式のNXP USB VID/PIDプログラムページへ移動してください:[リンク] NXP USB VID/PID Programへ 2. **サポートチケットを作成**:そのページの下部に「詳細についてはサポートチケットを作成してください」というセクションがあります。それをクリックしてください。 3. **チケット記入**:チケットには以下の情報を記載する必要があります: - あなたの会社名 - 必要なPIDの数(最大3個まで無料で提供) - 製品とその目的の簡単な説明 4. **承認待ち**:NXPがあなたの申請を審査します。提出から割り当てられたPIDを受け取るまで、手続きには最大1か月かかる場合がありますのでご注意ください。 **LPC5528プロジェクトの重要な注意点:** - **適格性**:LPCシリーズ(Cortex-M)はこのプログラムで完全にカバーされます。 - **数量制限**: お客様の予想数量は10,000ユニット未満ですので、このプログラムの対象となります。生産台数が10,000台を超える場合は、USB.orgから独自のVIDを取得する必要があります。 - **USBロゴ**: NXP VIDを使用しても、USB-IFの商標ロゴを使用するライセンスは付与されません。ロゴを使用する場合は、USB-IF認証プロセスを経て、独自のVIDを取得する必要があります。 Re: USB VID/PID program still active ? ご助力ありがとうございます。でも残念ながら、私はぐるぐる回っています メールアドレスをNXPについてにリンクできないため、CASEポータルで新しいCASEを作成する資格はありません。ご自身のメールアドレスを使って NXP.com にログインするか、NXPコミュニティを通じてご質問をお寄せください。 いつも言われることですが、私たちは小規模な専門エンジニアリング事務所ですが、ドメインを所有していません。なぜなら、必要ないからです。私たちのGMXメールアドレスが受け付けられていないのが最大の問題だと思います。 敬具 トーマス Re: USB VID/PID program still active ? こんにちは、 @Thomas_Mundhenkeさん はい、db16122さんが説明した内容は正しいです。後ほど個別にメールをお送りします。関連するすべての情報をお送りください。ありがとう。 BR アリス
View full article
中文的标签,总是有一个突然会乱码 guiguider2.0.1 生成代码后第一个中文会乱码。项目刚建好时是正常的,后续编辑后,就会突然出现一个标签显示不正常。这次删掉新建好了,下次还是会随机一个有问题。 Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 1.目前只用这一个工程。 2.就是在修改过布局后,比如移动到其他的父控件中后,有概率会出现。 3.win10 Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 Hello @JasonZhang11111111111111 , 下午好。 为了进一步定位这个问题,想请您帮忙确认以下信息: 1. 这个问题是只在当前工程中发生,还是其他工程也可以复现? 2. 能否提供一下更详细的复现步骤? 3. 您当前使用的操作系统及版本是什么?例如 Windows 10、Windows 11、Linux 或 macOS。 BR Celeste Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 Hello @JasonZhang11111111111111 , 抱歉回复晚了。 感谢您的说明。我这边还是没能复现。 想再确认一下,您提到的“移动到其他父控件中”,具体是如何操作的?是通过复制/粘贴到新的父控件,还是直接在控件树中拖动控件到新的父控件? 另外,如果方便的话,能否直接把工程文件发给我们试一下? BR Celeste
View full article
中国語タグの1つが突然文字化けして表示されるようになりました(guiguider2.0.1)。 コード生成後の最初の中国語文字が文字化けします。プロジェクトを最初に作成したときは正常に動作しますが、その後編集を行うと、突然ラベルが表示され、正しく表示されません。ラベルを削除して再作成すると問題は解決しますが、次回以降、同じ問題がランダムに発生します。 Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 1. 現在、使用されているプロジェクトはこの1つのみです。 2. これは、レイアウトが変更された後、例えばビューが別の親ビューに移動された場合などに発生する可能性があります。 3. Windows 10 Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 こんにちは、 @JasonZhang111111111111111 こんにちは。この件についてさらに調査するため、以下の情報をご確認いただけますでしょうか。 1. この問題は現在のプロジェクトでのみ発生するのでしょうか、それとも他のプロジェクトでも再現可能でしょうか? 2. この現象を再現するためのより詳細な手順を教えていただけますか? 3. 現在使用しているオペレーティングシステムとそのバージョンは何ですか?例えば、Windows 10、Windows 11、Linux、macOSなどです。 BR セレステ Re: 中文的标签,总是有一个突然会乱码 guiguider2.0.1 こんにちは、 @JasonZhang111111111111111 返信が遅くなり申し訳ありません。 ご説明ありがとうございます。しかし、まだ再現できていません。 もう一度確認させてください。「別の親コントロールに移動する」とは具体的にどういう意味でしょうか?新しい親コントロールにコピー&ペーストするということでしょうか、それともコントロールツリー内でコントロールを新しい親コントロールに直接ドラッグするということでしょうか? もしくは、もしご都合がよろしければ、試用できるようプロジェクトファイルを直接お送りいただけますでしょうか? BR セレステ
View full article
USB VID/PID 程序仍然处于活动状态吗? 你好, 我们是一家小型公司,正在开发基于 LPC5528 的带 USB CDC 接口的家庭控制器。预计销量远低于1万台。我们希望通过 USB VID/PID 程序申请 NXP VID 下的 PID。 程序常见问题解答 (contact.nxp.com/vid-usb-app) 中链接的申请表不可用,案例门户拒绝了我们的帐户,因为它不是在公司域名上注册的。 该项目目前是否仍在进行?如果仍在进行,目前的申请方式是什么? 谢谢你! Re: USB VID/PID program still active ? 是的,NXP USB VID/PID 程序仍然有效。旧版网页表单(`contact.nxp.com/vid-usb-app`)已被弃用,不再可用。 目前官方的申请方式是通过 NXP 社区门户网站直接创建支持工单。 以下是获取免费PID的步骤: 1. **前往 NXP 社区页面**:导航至 NXP 官方 USB VID/PID 程序页面:[链接] NXP USB VID/PID 程序 2. **创建支持工单**:在该页面的底部,您会看到一个标题为“如需更多详细信息,请创建支持工单”的部分。点击它。 3. **填写工单**:您需要在工单中提供以下详细信息: - 您的公司名称 - 您需要的 PID 数量(最多免费提供 3 个) - 简要描述您的产品及其用途 4. **等待批准**:NXP 将审核您的请求。请注意,从提交申请到收到分配的 PID,整个过程可能需要长达一个月的时间。 **LPC5528 项目重要提示:** - **资格**:LPC 系列(Cortex-M)完全包含在该计划的覆盖范围内。 - **销量限制**:由于您的预期销量低于 10,000 件,因此您符合此计划的资格。如果您的生产批量超过 10,000 台,您需要从 USB.org 获取您自己的 VID。 - **USB 标志**:使用 NXP VID 并不授予您使用 USB-IF 商标标志的许可。如果您想使用该标志,您必须通过 USB-IF 认证流程并拥有自己的 VID。 Re: USB VID/PID program still active ? 非常感谢您的帮助,但很遗憾,我还是原地打转。 由于我们无法将您的电子邮件与公司关联,因此您没有资格在案件门户网站上创建新案件。请使用您的公司邮箱地址登录 NXP.com 或通过 NXP 社区提出您的问题。 我总是得到这样的结果:尽管我们是一家专业的小型工程公司,但我们没有功能域,因为我们不需要它。我认为我们的 GMX 电子邮件地址不被接受,这是最大的问题。 亲切的问候 托马斯 Re: USB VID/PID program still active ? 你好@Thomas_Mundhenke 是的,db16122 的描述是正确的。我会给你发一封私人邮件。请把所有相关信息发给我。谢谢。 BR 爱丽丝
View full article
USB VID/PID program still active ? Hello, we are a small company developing a home controller based on the LPC5528 with a USB CDC interface. Expected volume is well below 10,000 units. We would like to apply for a PID under the NXP VID via the USB VID/PID program. The application form linked in the program FAQ (contact.nxp.com/vid-usb-app) is unavailable, and the Case Portal rejects our account because it is not registered on a company domain. Is the program still active, and if so, what is the current way to apply? Thank you! Re: USB VID/PID program still active ? Yes, the NXP USB VID/PID program is still active. The old web form (`contact.nxp.com/vid-usb-app`) has been deprecated and is no longer available. The current official way to apply is by **creating a support ticket** directly through the NXP Community portal. Here are the steps to get your free PID(s): 1. **Go to the NXP Community page**: Navigate to the official NXP USB VID/PID Program page: [链接] NXP USB VID/PID Program 2. **Create a Support Ticket**: At the bottom of that page, you will see a section titled **"For more details, please create a support ticket"**. Click on it. 3. **Fill out the Ticket**: You will need to provide the following details in the ticket: - Your company name - The number of PIDs you need (up to 3 are provided for free) - A brief description of your product and its purpose 4. **Wait for Approval**: NXP will review your request. Please note that the process can take up to a month from submission to receiving your assigned PID(s). **Important Notes for Your LPC5528 Project:** - **Eligibility**: The LPC series (Cortex-M) is fully covered under this program. - **Volume Limit**: Since your expected volume is below 10,000 units, you qualify for this program. If your production run exceeds 10,000 units, you would need to obtain your own VID from USB.org. - **USB Logo**: Using the NXP VID does not grant you the license to use the USB-IF trademarked logo. If you wish to use the logo, you must go through the USB-IF certification process and have your own VID. Re: USB VID/PID program still active ? Thanks a lot for your help, but unfortunately I'm running in circles As we are not able to link your email with a company, you are not eligible to create a new case on the Case Portal. Please use your company email address to log into NXP.com or raise your question via NXP community. Thats what I always get, despite we're a professional small engeneering office we don't own a domain simply because we don't need it. I think our gmx e-mail adress is not accepted, thats the biggets issue. Kind regards Thomas Re: USB VID/PID program still active ? Hello @Thomas_Mundhenke  Yes, what db16122 described is correct. I will send you a private email. Please send me all the relevant information. Thank you. BR Alice
View full article
关于ASHA数据包丢失、蓝牙压力测试断开连接的查询 [内容已移除] Re: Inquiry regarding ASHA packet loss, Bluetooth stress test disconnection, [内容已移除] Re: Inquiry regarding ASHA packet loss, Bluetooth stress test disconnection, [内容已移除]
View full article
S32 Design Studio for Arm V2.2 ライセンスが切れました こんにちは、 私の S32 Design Studio for ARM v2.2ライセンスは 2026年10月12日に期限切れになりました。 登録コード:S32DS-IDE-ARM-V2-X_181798567 製品バージョン:ARM v2.2用S32 Design Studio] ライセンス期間を延長してください。 よろしくお願いします。 Re: s32 design studio for arm V2.2 license expired こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。
View full article
The s32k2018.R1 cannot be postponed. Could you please extend this activation code for the next period? Thank you. Activation Code D870-0066-E5E6-ACC7 Re: s32k2018.R1没办法延期 Hi,  your S322DS license has been extended. Please activate S32DS again with your old code. 
View full article
Number of supported endpoints on the iMX8 The iMX8 uses the DWC3 for USB, which is an xHCI controller. When I read out the register from iMX8 i can figure out, that it may support up to 64 devices. But when I attach a few devices I much earlier on run in xHCI resource error. It seems there is some kind of a limitation on the number of endpoints, and it also seems that it depends on the type of transfer type (Bulk, Control, ...). On the type of devices I use (includsing the hubs) it seem I run after 80 endpoints into the problem. Could you please provide some exact numbers/formula how many endpoints are supported. Re: Number of supported endpoints on the iMX8 Hello,  The i.MX8 xHCI MaxSlots = 64 value specifies the maximum number of enabled USB device slots, not the total endpoint capacity. xHCI is up to 31 endpoint contexts per device, but the controller does not guarantee that all 64 slots can simultaneously use the maximum number of endpoints. The usable total depends mainly on periodic bandwidth, device speed, endpoint interval and packet size, hub topology, Transaction Translator allocation and DWC3 implementation resources.   Please refer xHCI specification for detailed information. Re: Number of supported endpoints on the iMX8 I checked the xHCI specification and could not find any indication. The only thing xHCI specifies that a controller can return resource error (the one I already mentioned above) E.g. Intel describes for one of their xHCI controller that they support up to 2048 Bulk/Control EPs or up to 128 Interrupt/Isochronous EPs. https://edc.intel.com/content/www/us/en/design/ipla/software-development-platforms/servers/platforms... We have test setup (USB 2.0 only) which works well on Intel chips (several hundred EPs), but fails on a fraction on devices on the iMX8MP (the mentioned 80 EPs). But to know how many and what type of devices we can support we need to know what the limitation of the iMX8MP/DWC3 are. It would be very helpful if you can provide us some kind of formula or limitations, the same way Intel does.
View full article
S32 Design Studio for S32 Platform 3.5 License I have one laptop and one desktop computer. Uninstalling and reinstalling on the laptop requires two licenses for S32 Design Studio for S32 Platform 3.5.
View full article
s32k2018.R1没办法延期 麻烦帮我给这个激活码延下期,谢谢。 Activation Code D870-0066-E5E6-ACC7 Re: s32k2018.R1没办法延期 你好, 您的S322DS许可证已延期。请使用您之前的激活码重新激活S32DS。
View full article
S32 Design Studio for S32 Platform 3.5 License 本人一个笔记本,一个台式机,笔记本卸载重装,需要2个S32 Design Studio for S32 Platform 3.5 的License
View full article
AraRT 3.0 x86:Lenovo Ara240 8GB構成とLinux 6.12ドライバの問題 ホスト:Lenovo ThinkCentre neo Ultra、12W2CTO1WW NPU FRU: 5C50W32071、Lenovoによる説明では8GB LPDDR4X PCI ID: 1e58:0002、リビジョン02 ランタイム:AraRT 3.0 Linux x86-64、Qubes/XenのDebian 13 HVM上で動作。 ゲスト:Debian 13、Linux 6.12.113、Qubes/Xen PCIパススルー PCIパススルーはデバイスを検出します。現在、どのNPUドライバもバインドされていません。 ドライバーソース:nxp-imx-support/uiodma-driver ドライバーコミット:962d11df1a9334e851f1f8a5b00f7e8960609e6a、Linux 6.12.113でコンパイルするためにコールバック署名の変更が必要でした コミュニティの皆様に、以下の件についてできるだけ早くご協力をお願いしたいと心からお願い申し上げます。 - カーネルと互換性のあるx86ドライバを管理し、IRQのクリーンアップとeventfd検証に対応しています。 - このFRUの正しいボード名、ランク、DDR構成ファイル、LPDDR4X設定、および周波数。 - AraRT 3.0が既存のファームウェアおよびXenパススルーを通じた動作をサポートしているかどうか。 Re: AraRT 3.0 x86: Lenovo Ara240 8GB configuration and Linux 6.12 driver issues 公式ウェブサイトでAra240 16GB M.2モジュール用のAraRT-x86 BSPリンクを試してみましたか? Re: AraRT 3.0 x86: Lenovo Ara240 8GB configuration and Linux 6.12 driver issues ありがとう。AraRT 3.0 x86-64ユーザー空間ツールを試してみました。私のカードはLenovo FRU 5C50W32071、8 GB LPDDR4X、PCI 1e58:0002 rev 02です。リンク先のBSPはこのFRUをサポートしていますか?もしそうなら、サポートされているリリース、Linux/カーネルバージョン、正確な8GBのボード構成、そして読み取り専用検出テストを共有してください。Qubes/Xenではデバイスが列挙を行いますが、ゲストは互換性のあるブリッジウィンドウがないためBAR0、2、4を請求できません。私は16GB構成を適用しておらず、カードの書き込みも行っていません。
View full article