Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
RW612: SWDIO (GPIO_14) と SWCLK (GPIO_13) のみを使用した SWD デバッグ? こんにちは、NXPチームの皆様、 私のカスタムRW612ボード(FRDM-RW612 V2由来)では、10ピンCortexヘッダーにSEGGER J-Linkを使っています。回路図を添付します。SWDIO(GPIO_14)とSWCLK(GPIO_13)は、VTrefとGNDとともにヘッダーに配線されています。 SWDIOとSWCLKだけでデバッグに十分かどうか知りたいです。 1. SWDIO + SWCLK + GND(+VTref)で通常のデバッグやフラッシュに十分でしょうか? 2. SWDを選択するにはリセット時にRF_CNTL_2が引き出される必要がありますか? 3. nRESET(PDn)がデバッガに接続されていない場合、ファームウェアがGPIO_13/14の多様化を変更しても復旧は可能でしょうか? ありがとうございます。 Re: RW612: SWD debug with only SWDIO (GPIO_14) and SWCLK (GPIO_13)? こんにちは、 @Yash_shinde。 RW61x設計ガイドのレビューを強くお勧めします。このガイドには、デバッグインターフェースの設計考慮など、RW61xデバイスでPCBを設計する際の重要な考慮事項がいくつか記載されています。詳細は第10章を参照してください。 以下に、ご質問にお答えします。 1. 通常のデバッグとフラッシュ書き込みには、SWDIO + SWCLK + GND (+VTref) で十分ですか? SWDIO、CLK、+VTref、GNDに加えて、nRESETも含めることを強くお勧めします。デバッグのために、ツールは特定の状況下でこれを取得しようとする場合があります(デバッグプローブ、デバッグ構成設定、およびツールによって異なります)。 2. SWDを選択するには、リセット時にRF_CNTL_2をローにプルダウンする必要がありますか? はい。RW61x設計ガイドの表14「ピン構成」に記載されているように、DAPはデフォルトでJTAGを使用しています。したがって、SWDを使用する場合はRF_CNTL_2を0に設定すべきです。同じドキュメント内の図33「設定ピン」は、この構成でこのピンをどのようにコネクテッドすべきかの例を示しています。 3. nRESET(PDn)がデバッガにコネクテッドされていない場合、ファームウェアがGPIO_13/14の多様化を変更しても復旧は可能でしょうか? このCASEでは、ISPモードでボードを復元して再プログラムできます。ISPはイメージプログラミング用のUART、I2C、SPI、USB HIDなどのインターフェースをサポートしています。 この機能については、リファレンス・マニュアルの第43章「ISPとIAP」で詳しくご覧いただけます。 さらに、このコミュニティ投稿では、ISPモードを使用してボードを復旧する方法の例が示されています。 他に質問がありましたら、お気軽にお知らせください。 BR ハビブ
View full article
RW612: SWD debug with only SWDIO (GPIO_14) and SWCLK (GPIO_13)? Hi NXP team, On my custom RW612 board (derived from FRDM-RW612 V2) I use a SEGGER J-Link on a 10-pin Cortex header. Schematic attached. SWDIO (GPIO_14) and SWCLK (GPIO_13) are wired to the header, with VTref and GND. I want to know if SWDIO + SWCLK alone are enough for debug. 1. Is SWDIO + SWCLK + GND (+VTref) enough for normal debug and flashing? 2. Is RF_CNTL_2 pulled low at reset required to select SWD? 3. If nRESET (PDn) is not connected to the debugger, is recovery still possible if firmware changes the GPIO_13/14 mux? Thanks. Re: RW612: SWD debug with only SWDIO (GPIO_14) and SWCLK (GPIO_13)? Hello @Yash_shinde, I highly recommend reviewing the RW61x Design Guide, as it provides several important considerations for designing a PCB with the RW61x device, including design considerations for debug interface, please refer to the chapter 10 for more details. Let me address your questions below: 1. Is SWDIO + SWCLK + GND (+VTref) enough for normal debug and flashing? We would strongly recommend also including nRESET in addition to SWDIO, CLK, +VTref and GND. For debugging, the tools may try to pull this in certain circumstances (depending upon debug probe, debug configuration settings and tools). 2. Is RF_CNTL_2 pulled low at reset required to select SWD? Yes. As mentioned in Table 14 "Pin configurations" of the RW61x Design Guide, the DAP uses JTAG by default. Therefore, RF_CNTL_2 should be set to 0 if you intend to use SWD. Figure 33 "Configuration pins" in the same document shows an example of how this pin should be connected for this configuration. 3. If nRESET (PDn) is not connected to the debugger, is recovery still possible if firmware changes the GPIO_13/14 mux? In this case, you can use ISP mode to recover and reprogram the board. ISP supports interfaces such as UART, I2C, SPI, and USB HID for image programming. You can find more information about this functionality in Chapter 43, "ISP and IAP," of the Reference Manual. Additionally, this community post provides an example of how to recover a board using ISP mode. Please let me know if you have any further questions. BR Habib
View full article
Issue in interfacing Barcode scanner using LPC4337 controller with LPCUSBLIB Hello , I’m currently working on barcode scanner interfacing with LPC4337 using lpcusblib (HID keyboard host example).  Issue: The USB1 host receives only the first character from the scanner after receiving few successful barcode readings, and then stalls. After rescanning, no further data transfers occur. I’ve enabled USB1 interrupts and used HID_Host_ReceiveReport(), but suspect I’m missing proper IN packet handling or report clearing. Has anyone implemented HID barcode scanning with lpcusblib on LPC microcontrollers? Any guidance or code snippets on handling continuous data transfer would be greatly helpful for me and appreciated. i wanted to know that which are the conditions cause to clear the  pipe buffer. some times i receive full barcode properly. some times after first character nothing is received also the usb line gets stuck so that after that nothing is received for several times barcode scanning.  Thank you in advance! #EmbeddedSystems #LPC4337 #USBHost #HID #Firmware  Regards, Re: Issue in interfacing Barcode scanner using LPC4337 controller with LPCUSBLIB Hello @RDGC_member  My colleague has modified the LPC4337 USB host keyboard code to work with the NLS-HR11 barcode scanner on the LPCXpresso4337 EVK using MCUXpresso IDE. It works well. Please see the screenshot of the changed code, as I cannot send the source code to you due to company policy. I have taken a screenshot for you to compare the differences. You can refer to it to check. Thank you. BR Alice
View full article
LPC55xx USARTにおけるFIFOINTSTAT.PERINTフラグの目的は何ですか? こんにちは、 私はLPC55xxファミリ(特にLPC5516)のUSART FIFO割り込み機構を扱っており、FIFOINTSTATレジスタにおけるPERINTビットの意図された目的を理解したいと考えています。 USART割り込みハンドラには、割り込みステータスの独立したソースが2つあるようです。 FIFO 関連の割り込みは、 FIFOINTSTATに報告されます(例: TXLVL 、 RXLVL 、 TXERR 、 RXERR )。 INTSTATで報告されるUSARTペリフェラル割り込み (例:TXIDLE、RXRDY、エラー条件)。 両方の割り込みソースは同じIRQハンドラで処理されるため、ハンドラーはFIFOINTSTATにFIFOINTSTATのFIFOINTイベント情報、INTSTATでUSARTペリフェラルイベント情報を単純にチェックできます。 このCASEでは、追加情報や機能をFIFOINTSTAT.PERINT提供するのか分かりません。 例えば、PERINTがUSARTペリフェラルにアクティブな割り込みがあることを示しても、ハンドラーは実際の 割り込み源(例えばTXIDLE)を特定するためにINTSTATを読み込む必要があります。なぜINTSTAT を直接確認しないのでしょうか? 私の質問は以下のとおりです。 FIFOINTSTAT.PERINTは具体的に何を示しているのでしょうか? 割り込みハンドラ内では、どのような状況で使用されることが想定されていますか? INTSTATを直接チェックするよりも、PERINTのチェックが望ましい、あるいは必要な特定のユースケースはありますか? その意図された使い方を示すコード例を教えていただけますか? MCUXpresso SDKs USARTドライバ(fsl_usart.c),を確認しましたが、FIFOINTSTATはFIFOINTSTATをチェックせずに、FIFO割り込みやUSARTペリフェラル割り込みを直接処理しているようですPERINT。 ご説明いただきありがとうございます。 LPC55xx ペリフェラル
View full article
LPC55xx USART 中的 FIFOINTSTAT.PERINT 标志有什么用途? 你好, 我正在使用 LPC55xx 系列(特别是 LPC5516)上的 USART FIFO 中断机制,我想了解FIFOINTSTAT寄存器中的PERINT位的预期用途。 USART中断处理程序似乎有两个独立的中断状态来源: FIFO 相关中断,在FIFOINTSTAT中报告(例如TXLVL 、 RXLVL 、 TXERR 、 RXERR )。 USART 外设中断,在INTSTAT中报告(例如TXIDLE 、 RXRDY和错误状态)。 由于两个中断源都由同一个 IRQ 处理程序处理,因此该处理程序可以简单地检查FIFOINTSTAT以获取 FIFO 事件,检查 INTSTAT以获取 USART 外设事件。 在这种情况下,我看不出FIFOINTSTAT.PERINT提供了什么额外的信息或功能。 例如,如果PERINT指示 USART 外设有活动中断,处理程序仍然需要读取INTSTAT来确定实际的中断源(例如TXIDLE )。为什么不直接检查INTSTAT呢? 我的问题是: FIFOINTSTAT.PERINT究竟表示什么? 在中断处理程序中,预期在什么情况下会使用它? 是否存在某些特定用例,使得检查PERINT比直接检查INTSTAT更可取或更必要? 能否提供一个代码示例来演示其预期用途? 我检查了 MCUXpresso SDK USART 驱动程序 ( fsl_usart.c ),但它似乎直接处理 FIFO 中断和 USART 外设中断,而没有检查FIFOINTSTAT.PERINT 。 谢谢你的澄清。 LPC55xx 外设
View full article
LPCUSBLIBとLPC4337コントローラを組み合わせたバーコードスキャナーのインターフェースでの問題 こんにちは 、 現在、lpcusblib(HIDキーボードホストのサンプル)を使用して、バーコードスキャナとLPC4337のインターフェースを開発中です。 問題:USB1ホストは、バーコードの読み取りに数回成功した後、スキャナーから最初の文字のみを受信し、その後停止します。再スキャン後は、それ以上のデータ転送は発生しません。 USB1割り込みを有効にしてHID_Host_ReceiveReport()を使用しましたが、INパケットの適切な処理またはレポートのクリアが不足しているのではないかと考えています。 誰かLPCマイコンでLPCマイクロコントローラでIPCのバーコードスキャンを実装したことがありますか?継続的なデータ転送の扱い方に関するアドバイスやコードスニペットがあれば、ぜひ教えていただけると助かります。 パイプバッファをクリアする条件を知りたいです。時々、バーコード全体が正しく表示されることがあります。最初の文字の後に何も受信しないこともあり、USB回線も詰まってしまい、その後何度もバーコードスキャンを繰り返しても何も受信されません。 お手数ですが、よろしくお願いいたします。 #組み込みシステム #LPC4337 #USBホスト #HID #ファームウェア よろしくお願いいたします。 Re: Issue in interfacing Barcode scanner using LPC4337 controller with LPCUSBLIB こんにちは@RDGC_member 同僚がMCUXpresso IDEを使ってLPCXpresso4337 EVKのNLS-HR11バーコードスキャナーに対応しられるように、LPC4337 USBホストキーボードコードを改造しました。うまく機能します。 会社の方針によりソースコードを送ることができないため、変更されたコードのスクリーンショットをご覧ください。違いを比較できるようにスクリーンショットを撮りました。確認するために参照できます。ありがとう。 BR アリス
View full article
使用 LPC4337 控制器和 LPCUSBLIB 接口条码扫描器时出现问题 你好 , 我目前正在研究使用lpcusblib(HID键盘主机示例)将条形码扫描器与LPC4337连接。 问题:USB1 主机在成功读取几次条形码后,仅接收到扫描器的第一个字符,然后就停止工作。重新扫描后,不会再进行数据传输。 我已经启用了 USB1 中断并使用了 HID_Host_ReceiveReport(),但我怀疑我缺少正确的 IN 数据包处理或报告清除。 有人在LPC微控制器上使用lpcusblib实现过HID条形码扫描吗?任何关于处理连续数据传输的指导或代码片段都将对我非常有帮助,不胜感激。 我想知道清除管道缓冲器的条件是什么。有时候我能正确收到完整的条形码。有时扫描第一个字符后就收不到任何数据,而且USB线似乎会卡住,导致之后多次扫描条形码都收不到任何数据。 提前谢谢! #嵌入式系统 #LPC4337 #USB主机 #HID #固件 此致, Re: Issue in interfacing Barcode scanner using LPC4337 controller with LPCUSBLIB 您好@RDGC_member 我的同事修改了 LPC4337 USB 主机键盘代码,使其能够与 LPCXpresso4337 EVK 上的 NLS-HR11 条形码扫描器配合使用,并使用了 MCUXpresso IDE。效果很好。 请查看修改后的代码截图,由于公司政策限制,我无法将源代码发送给您。我截取了屏幕截图,方便您比较差异。你可以参考一下。谢谢。 BR 爱丽丝
View full article
MCU 我们是车企做MCU的,我们想验证自己搭建的simulink控制算法以及一些故障诊断能不能烧入到开发板跑通,我们提供控制算法直接买贵公司的开发板可以直接运行看电机运转情况吗 Re: MCU 你好@wpdbl , 感谢您的联系。 可以将基于 Simulink 的控制算法部署到支持的 MCU 开发平台上,并在目标硬件上进行验证。但是,具体的设置和所需的硬件/软件取决于您打算使用的MCU和开发板。 请您提供以下信息? 你们的目标MCU或MCU系列是哪一款? 您计划使用哪款开发板? 您目前使用的是哪个MATLAB/Simulink版本和工具箱? 你们的目标应用领域是哪种类型的电机和电机控制应用? 有了这些细节,我们就能更好地了解您的使用场景,并提供相应的指导。 顺祝商祺! 德拉戈斯
View full article
What is the purpose of FIFOINTSTAT.PERINT flag in LPC55xx USART? Hello, I am working with the USART FIFO interrupt mechanism on the LPC55xx family (specifically LPC5516) and I would like to understand the intended purpose of the PERINT bit in the FIFOINTSTAT register. The USART interrupt handler appears to have two independent sources of interrupt status: FIFO-related interrupts, reported in FIFOINTSTAT (e.g. TXLVL, RXLVL, TXERR, RXERR). USART peripheral interrupts, reported in INTSTAT (e.g. TXIDLE, RXRDY, and error conditions). Since both interrupt sources are handled by the same IRQ handler, the handler can simply check FIFOINTSTAT for FIFO events and INTSTAT for USART peripheral events. In this case, I don't see what additional information or functionality FIFOINTSTAT.PERINT provides. For example, if PERINT indicates that the USART peripheral has an active interrupt, the handler would still need to read INTSTAT to determine the actual interrupt source (such as TXIDLE). Why not simply check INTSTAT directly? My questions are: What exactly does FIFOINTSTAT.PERINT indicate? Under what circumstances is it expected to be used in an interrupt handler? Is there a specific use case where checking PERINT is preferable or necessary compared to checking INTSTAT directly? Could you provide a code example demonstrating its intended use? I have checked the MCUXpresso SDK USART driver (fsl_usart.c), but it appears to handle FIFO interrupts and USART peripheral interrupts directly, without checking FIFOINTSTAT.PERINT. Thank you for clarifying this. LPC55xx Peripherals
View full article
RW612:仅使用 SWDIO (GPIO_14) 和 SWCLK (GPIO_13) 进行 SWD 调试? 您好,NXP团队: 在我的定制 RW612 板(源自 FRDM-RW612 V2)上,我使用了一个 10 针 Cortex 接头上的 SEGGER J-Link。附图为示意图。SWDIO (GPIO_14) 和 SWCLK (GPIO_13) 连接到接头,VTref 和 GND 也连接到接头。 我想知道单独使用 SWDIO + SWCLK 是否足以进行调试。 1. SWDIO + SWCLK + GND (+VTref) 是否足以满足正常的调试和烧录需求? 2. 复位时是否需要将 RF_CNTL_2 拉低才能选择 SWD? 3. 如果 nRESET (PDn) 未连接到调试器,固件更改 GPIO_13/14 多路复用器时是否仍可恢复? 谢谢。 Re: RW612: SWD debug with only SWDIO (GPIO_14) and SWCLK (GPIO_13)? 你好@Yash_shinde , 我强烈建议您查阅RW61x 设计指南,因为它提供了使用 RW61x 设备设计 PCB 的几个重要考虑因素,包括调试接口的设计考虑因素,请参阅第 10 章了解更多详情。 下面我将回答您的问题: 1. SWDIO + SWCLK + GND (+VTref) 是否足以满足正常的调试和烧录需求? 我们强烈建议除了 SWDIO、CLK、+VTref 和 GND 之外,还要加上 nRESET。为了进行调试,在某些情况下,工具可能会尝试拉取此文件(取决于调试探针、调试配置设置和工具)。 2. RESET时是否需要将 RF_CNTL_2 拉低才能选择 SWD? 是的。如 RW61x 设计指南的表 14“引脚配置”中所述,DAP 默认使用 JTAG。因此,如果您打算使用 SWD,则应将 RF_CNTL_2 设置为 0。同一文档中的图 33“配置引脚”显示了此配置下该引脚的连接示例。 3. 如果 nRESET (PDn) 未连接到调试器,固件更改 GPIO_13/14 多路复用器时是否仍可恢复? 在这种情况下,您可以使用 ISP 模式来恢复和重新编程板。ISP 支持 UART、I2C、SPI 和 USB HID 等接口,用于图像编程。 您可以在参考手册第 43 章“ISP 和 IAP”中找到有关此功能的更多信息。 此外,这篇社区帖子还提供了一个如何使用 ISP 模式恢复板的示例。 如果您还有其他问题,请告诉我。 BR 哈比卜
View full article
MCXA145 flash secure Good morning, I would like to set the flash security bit on the MCXA145 via firmware. On the MCXC444, I used to go into the startup file to configure it; is there a similar option here without using MCUXpresso Secure Provisioning? In production, they simply load the .axf file, and I’d like it to already contain the security settings to avoid them having to carry out a second step. Could you advise me on this? Many thanks Regards Re: MCXA145 flash secure Hello The Flash Security equivalent in MCXA is the Read Out Protection [ROP_STATE];  ROP_STATE is a 32-bit field stored in IFR0; ROP function protects the security of the chip, users can set different levels of ROP according to the requirements of their own applications.   During customer production, customers can impose certain restrictions on ISP and debugging based on their needs through ROP. Customers can choose between ROP level 1 or ROP level 2. Important warning: Take in consideration the restrictions for each ROP Level since some levels may enter NO return LifeCycles. You can configure the Life Cycle settings ROP Level on the Secure Provisioning Tool to build the image and then use the image to the production devices, Using MCUXpresso Secure Provisioning simplifies the ROP configuration process and it’s the recommended path to configure CMPA settings; I would strongly recommend this NXP Community post for more information on the topic and the instructions to configure ROP MCXA153 Read Out Protection And the related information from the Reference Manual MCXA145 Reference Manual Chapter 20.3, 20.3.4 [Read Out Protection] Let me know if you need anything else Best Regards
View full article
MCU 当社は自動車メーカー向けのMCUメーカーです。自社開発のSimulink制御アルゴリズムといくつかの故障診断プログラムを開発ボードに書き込んで正常に動作させることができるかどうかを検証したいと考えています。制御アルゴリズムを提供し、開発ボードを購入してモーターの動作を確認することは可能でしょうか? Re: MCU こんにちは@wpdbl さん、 ご連絡いただきありがとうございます。 Simulinkベースの制御アルゴリズムを対応MCU開発プラットフォームに展開し、ターゲットハードウェア上で検証することが可能です。ただし、具体的なセットアップや必要なハードウェア・ソフトウェアは、使用するMCUや開発ボードによって異なります。 以下の情報を教えていただけますか? どのMCUやMCUファミリをターゲットにしていますか? どの開発ボードを使う予定ですか? 現在使用しているMATLAB/Simulinkのバージョンとツールボックスは何ですか? どのようなモーターおよびモータ制御のアプリケーションを対象としていますか? これらの詳細をもとに、お客様のユースケースをよりよく理解し、適切なガイダンスを提供できます。 よろしくお願いいたします。 ドラゴス
View full article
MCXA145 闪存安全 早上好, 我想通过固件设置 MCXA145 的闪存安全位。 在 MCXC444 上,我以前需要进入启动文件进行配置;这里是否有类似的选项,而无需使用 MCUXpresso Secure Provisioning? 在生产环境中,他们只需加载 .axf 文件即可。文件,我希望它已经包含网络安全设置,以避免他们执行第二步操作。 您能就此事给我一些建议吗? 非常感谢 此致 Re: MCXA145 flash secure Hello MCXA 中的 Flash 网络安全等效项是读取保护 [ROP_STATE] ;ROP_STATE 是存储在 IFR0 中的一个 32 位字段;ROP 功能保护芯片的网络安全,用户可以根据自己应用的需求设置不同级别的 ROP。   在客户生产过程中,客户可以通过 ROP 根据自身需求对 ISP 和调试施加一定的限制。客户可以选择 ROP 等级 1 或 ROP 等级 2。重要提示:请注意每个 ROP 等级的限制,因为某些等级可能会进入不可退货的生命周期。 您可以使用安全配置工具配置生命周期设置 ROP 级别来构建映像,然后将映像用于生产设备。使用 MCUXpresso 安全配置简化了 ROP 配置过程,这是配置 CMPA 设置的推荐方法; 我强烈推荐您阅读这篇 NXP 社区帖子,其中包含更多相关信息以及 ROP 配置说明。 MCXA153 读出保护 以及参考手册中的相关信息 MCXA145 参考手册第 20.3、20.3.4 章 [读取保护] 如果您还需要其他帮助,请告诉我。 顺祝商祺!
View full article
MCU We are an MCU manufacturer for an automotive company. We want to verify whether our self-built Simulink control algorithm and some fault diagnosis can be burned into a development board and run successfully. Can we provide the control algorithm and simply purchase your development board to run it and observe the motor's operation? Re: MCU Hello @wpdbl, Thank you for reaching out. It is possible to deploy Simulink-based control algorithms to supported MCU development platforms and validate them on the target hardware. However, the exact setup and required hardware/software depend on the MCU and development board you intend to use. Could you please provide the following information? Which MCU or MCU family are you targeting? Which development board are you planning to use? Which MATLAB/Simulink version and toolboxes are you currently using? What type of motor and motor-control application are you targeting? With these details, we can better understand your use case and provide the appropriate guidance. Best regards, Dragos
View full article
TCL - EB Tresos v29.0.0 的工具置信度文件 亲爱的恩智浦管理员,你 能不能把关于 EB Tresos 的 TCL 文件发给我们,我在 MCAL/RTD 包里找不到这个文件。 如果可能的话,你能否将功能安全手册发给我们,或者告诉我们在哪里可以在 MCAL/RTD 中找到它? 致以最崇高的敬意 莎伦 Re: TCL - Tool confidence level document for EB Tresos v29.0.0 你好,@sharonfmc93、 TCL 有一些关于 EB Tresos 的信息,但还处于保密状态。您可以输入支持票据吗? 如果可能的话,你能否也给我们发功能安全手册,或者告诉我们在哪里可以在 MCAL/RTD 中找到它? 功能安全手册(以及所有与功能安全相关的信息)位于 S32K3 产品页面文档中的 " 安全文件 " 下: 如果您没有申请安全访问权限,可以查看我们的常见问题解答:安全访问权限常见问题解答|恩智浦半导体。 致以最诚挚的问候, Julián Re: TCL - Tool confidence level document for EB Tresos v29.0.0 嗨,朱利安 我没有找到任何关于 EB tresos TCL 级别的信息,你能指出是哪个文件吗? Re: TCL - Tool confidence level document for EB Tresos v29.0.0 嗨@allenlw , 对于 EB Tresos 而言,刀具冲击为 TI2,刀具检测为 TD1。 我们有一份文件描述了 EB tresos Studio 软件工具的 ISO 26262 置信度。但是,如前所述,本文件受保密协议约束。 请提交支持案例并提供有效的保密协议编号,以便我们能够共享您请求的文件。 致以最诚挚的问候, Julián
View full article
AFT26H250W03SR6(--24SR6) テスト回路部品レイアウト DXFファイル AFT26H250W03SR6(--24SR6)テスト回路コンポーネントレイアウトDXFファイルをサポートしられますか? 私たちはそれを非常に必要としています。 よろしくお願いします。
View full article
MRF300AN 27MHz VSWR Protection and Recovery Strategy We are developing a 300W, 27MHz CW RF generator for medical aesthetic applications using the MRF300AN. The load (handpiece) can momentarily open-circuit, and we need a robust protection and recovery strategy. We are not looking for an open-load safe power level (we know the 65:1 VSWR ruggedness is pulsed). We are trying to optimize the system-level protection architecture and recovery timing to prevent CW overstress. What we have implemented so far: A three-toroid directional coupler samples forward and reflected power. The detected DC levels feed a comparator with hysteresis; when reflected power exceeds the threshold, a latch is set and a shunt FET rapidly pulls the MRF300AN gate bias toward zero. The MCU can reset the latch, and the MCU also has control over the small-signal RF input level. In other words, we have the basic detect, compare, latch, and gate-bias pull-down chain in place, and the MCU can reset the latch and adjust drive level. Our concern and the specific gaps we need help with: The current recovery sequence is essentially MCU resets the latch, gate bias returns, and drive is restored. We recognize that this is too symmetric: protection should be fast, but recovery should be deliberate. We are not sure whether our overall architecture is the right one for this application, and we are not sure how to design the recovery timing so that (1) the PA is not re-activated while the open-load condition is still present, and (2) the first re-entry attempt does not itself create a secondary overstress event. Q1: Architecture Is our comparator-latch-gate-pull-down approach the right primary protection for 27 MHz CW, or is there a better topology for this power class and application? We have seen references to several alternatives, and we would appreciate NXP's application-level judgment on which direction is most appropriate for MRF300AN at 27 MHz in a CW medical generator: - PIN-diode-based shunt or switch protection at the PA output, to present a controlled impedance or isolate the PA during fault conditions. - Circulator/isolator with a terminated load, as commonly used in MRI and other medical RF chains, accepting the cost and volume penalty. - Layered protection, where a very fast hardware path handles the sudden open-circuit event and a slower path (MCU or ALC) manages foldback and recovery. - Keeping the comparator + latch + gate-bias pull-down as the primary protection and adding a TVS clamp as a last-line voltage clamp. For MRF300AN specifically at 27 MHz CW, is there a reason to prefer or avoid any of these? We are particularly interested in whether a PIN-diode output switch would meaningfully reduce the stress on the device compared to gate-bias pull-down alone, or whether it introduces its own loss and reliability trade-offs at this frequency and power level. Q2: Recovery timing We understand that blindly resetting the latch after a fault can cause the PA to chatter at the protection threshold and repeatedly inject stress. We would like NXP's guidance on the holdoff and re-entry scheme: - Should the system enforce a fixed holdoff time after a fault before any re-entry attempt is allowed? - During re-entry, is it acceptable to use a short low-power probe (e.g., a brief low-drive burst) to check whether the load has returned to a safe VSWR, and then ramp the drive slowly rather than stepping back to full power? NXP community guidance already recommends gradual power-up rather than abrupt full drive during initial bring-up; we are trying to extend that principle to fault recovery. - Is there an NXP-recommended ramp profile or re-entry power ceiling for MRF300AN in CW operation, or should this be treated purely as a system-level state-machine design independent of the device? Q3: TVS role In the NXP 27 MHz reference design discussion, a 110 V TVS from drain to ground was discussed, with the guidance that the standoff voltage should sit above the maximum normal drain voltage. In our system, we already have active reflected-power protection. Should the TVS be treated as a last-line clamp for the brief interval before the active protection responds, or is it expected to carry more of the protection burden? At 27 MHz CW, do the junction capacitance and response speed of a TVS introduce any concern for normal RF waveform fidelity? What would be most helpful: Any application-level guidance, a recommended architecture, a pointer to an existing NXP application note on VSWR protection and recovery for LDMOS PAs, or even a brief statement of how NXP's own reference designs handle the fault-holdoff-re-entry sequence, would directly inform our design. Thank you. Re: MRF300AN 27MHz VSWR Protection and Recovery Strategy Hello @fengyuqi , Thank you for the detailed description. Your comparator, hardware latch and active gate-bias pull-down form a reasonable primary protection path. For a 300W CW application, we would recommend using this as part of a layered architecture rather than relying on a single mechanism. Where possible, the fast hardware path should inhibit the RF drive and pull down the gate bias simultaneously. The MCU should not be part of the immediate shutdown loop; it should manage the subsequent holdoff, diagnostics, controlled re-entry, and repeated-fault lockout. A PIN-diode switch could reduce stress only if it transfers the PA output to a known and adequately rated impedance. Simply disconnecting the handpiece may present another open-circuit condition. At this power level, insertion loss, diode heating, voltage rating, switching transients and the impedance presented during switching must all be considered. A circulator with a rated termination provides stronger load isolation, but with significant size, cost and loss trade-offs. For recovery, a fixed minimum holdoff followed by a low-power probe and controlled drive ramp is a reasonable system-level approach. Both forward and reflected power should be monitored during the probe because the reflected-to-forward ratio may become inaccurate near the detector noise floor. Any new fault should immediately return the system to the latched state, and repeated unsuccessful attempts should result in a longer backoff or permanent lockout. NXP does not specify a dedicated holdoff time, ramp profile, or re-entry power ceiling for the MRF300AN. These values depend on the protection-chain response, stored energy in the matching network, detector dynamic range, bias settling, thermal conditions and the expected load behavior. They must therefore be determined and validated at the system level, including testing at multiple mismatch phase angles. The drain TVS should be considered a last-line transient clamp for the interval before the active shutdown becomes effective. It should not be expected to absorb continuous reflected RF power. Its standoff voltage, clamping behavior, pulse-energy capability, junction capacitance and package/layout parasitics must all be included in the RF and transient analysis, since the device can affect the 27 MHz output matching. The published MRF300AN 27 MHz reference design does not define a qualified fault-holdoff-re-entry sequence, so the complete protection architecture remains an application-specific design responsibility. Best regards, Pavel
View full article
ノートPC交換後にS32DS v3.5ライセンスアクティベーション失敗(FNPエラー0) こんにちは、NXPサポートチームの皆さん、 以前、古いノートPCでS32 Design Studio v3.5をアクティベートしていました。 最近ノートPCを交換しましたが、古いマシンにアクセスしてライセンスを返却できません。 新しいノートPCでS32DS v3.5を有効化しようとすると、以下のエラーが表示されます: 指定された数量は、許可されている最大数量(0)を超えています。(FNPエラー0) NXPライセンスポータルには、以下の情報も表示されます。 「このライセンスの返却は許可されていません。」 以前のライセンスの有効化をリセットするか、利用可能なアクティベーション数を増やして、新しいノートPCでS32DS v3.5をアクティベートできるようにしてもらえますか? [email protected] にも連絡を試みました が、SMTP エラー 550 5.4.1 でメールが拒否されました。 必要ならライセンス情報を個人的に提供できます。 ご協力ありがとうございました。 Re: S32DS v3.5 License Activation Failed After Laptop Replacement (FNP Error 0) こんにちは、 利用可能なライセンス数が増加しました。
View full article
TCL - Tool confidence level document for EB Tresos v29.0.0 Dear NXP Admins,  Could you please send us the TCL document regarding EB Tresos , i couldn't find this within the MCAL/RTD package.  If possible could you also send us the Safety Manuals, or tell us where to find it in the MCAL/RTD ? Best regards, Sharon Re: TCL - Tool confidence level document for EB Tresos v29.0.0 Hello @sharonfmc93, There is some information for TCL regarding EB Tresos, but it is under NDA. Can you enter a support ticket instead?  If possible, could you also send us the Safety Manuals, or tell us where to find it in the MCAL/RTD? Safety Manuals (and all safety-related information) is located under "Secure Files" from the S32K3 Product Page's documentation: If you have not requested secure access rights, you can go over our FAQs: Secure Access Rights FAQs | NXP Semiconductors. Best regards, Julián Re: TCL - Tool confidence level document for EB Tresos v29.0.0 Hi @allenlw, For EB Tresos Tool Impact is TI2, and Tool Detection is TD1. We have a document describing ISO 26262 confidence in software tools for EB tresos Studio. However, as mentioned previously, this document is covered under NDA. Please open a support case and provide an active NDA number so that the requested document can be shared. Best regards, Julián Re: TCL - Tool confidence level document for EB Tresos v29.0.0 Hi,julian     I didn't see any information regarding the EB tresos TCL level , can you point out which file?
View full article
MRF300AN 27MHz VSWR保護および回復戦略 私たちはこのMRF300ANを用いて、医療美容アプリケーション向けの300W、27MHzのCW RFジェネレーターを開発しています。荷重(ハンドピース)が一時的に開回路になることがあり、堅牢な保護と回復戦略が必要です。我々は、開放負荷時の安全な電力レベルを求めているわけではありません(65:1 VSWRの堅牢性はパルス状であることがわかっています)。CWへの過負荷を防ぐため、システムレベルの保護アーキテクチャと復旧タイミングの最適化に取り組んでいます。 これまでに実施したこと: 3つのトロイド方向カプラーは、前方および電力の反射をサンプリングします。検出された直流レベルはヒステリシスを伴うコンパレータに供給されます。反射電力が閾値を超えるとラッチが設定され、シャントFETがMRF300ANゲートバイアスを急速にゼロに引き寄せます。MCUはラッチをリセットでき、また小信号のRF入力レベルも制御できます。つまり、基本的な検出、比較、ラッチ、ゲートバイアスのプルダウンチェーンが整っており、MCUはラッチをリセットしドライブレベルを調整できます。 私たちの懸念と具体的な支援が必要なギャップ: 電流回復シーケンスは、基本的にMCUがラッチをリセットし、ゲートバイアスが戻り、ドライブが復元されるというものです。これはあまりにも対称的すぎると認識しています。保護は迅速に行われるべきですが、復旧は慎重に行われるべきです。このアプリケーションに全体のアーキテクチャが適しているか確信が持てず、回復タイミングのデザイン方法も不明です。(1) 開積力状態がまだ存在している間にPAが再作動しないこと、(2) 最初の再突入試み自体が二次的な過負荷イベント情報を生じさせないよう。 Q1:建築 コンパレータ-ラッチ-ゲート-プルダウン方式は27 MHz CWに対する適切な一次保護でしょうか?それともこの電力クラスとアプリケーションに適したトポロジーがあるのでしょうか?いくつかの代替案の言及を見ており、CW医療ジェネレーターの27 MHzでのMRF300ANにどの方向が最も適切かについて、NXPのアプリケーションレベルの判断をいただけるとありがたいです。 - PA出力にPINダイオードを用いたシャントまたはスイッチ保護を施し、障害時に制御インピーダンスを提示したりPAを絶縁したりします。 - MRIやその他の医療用RFチェーンで一般的に用いられる終端負荷を持つ循環器/アイソレーター。コストと体積のペナルティを受け入れます。 - レイヤー保護:非常に高速なハードウェアパスが突然のオープンサーキットイベント情報を処理し、より遅いパス(MCUまたはALC)がフォールドバックとリカバリーを管理します。 - コンパレータ+ラッチ+ゲートバイアスプルダウンを主な保護として保持し、最終線電圧クランプとしてTVSクランプを追加すること。 MRF300ANを特に27MHz CWで使用する場合、これらのうちどれかを好む、あるいは避けるべき理由はありますか?特に、PINダイオード出力スイッチがゲートバイアスプルダウン単独と比べてデバイスの負荷を実質的に軽減できるのか、それともこの周波数と電力レベルで自身の損失と信頼性のトレードオフが生じるのかに関心があります。 Q2:回復のタイミング 故障後に無差別にラッチをリセットすると、PAが保護閾値でチャタリングし、繰り返し応力を注入する可能性があることを理解しています。NXP社による保有期間延長および再参入制度に関するガイダンスを希望します。 ・システムは、障害発生後、再突入試行を許可する前に一定の待機時間を強制すべきでしょうか? 再突入時、負荷が安全なVSWRに戻ったかどうかを確認するために、短時間の低電力プローブ(例えば、短時間の低駆動バースト)を使用し、その後、駆動を徐々に増加させてから、全電力に戻すことは許容されますか?NXPコミュニティのガイダンスでは、初期起動時に急激にフルドライブするのではなく、徐々に電源を入れることを推奨しています。私たちはこの原則を故障復旧にも拡張しようとしています。 - CW動作時のMRF300ANにはNXP推奨のランププロファイルや再突入電力上限があるのか、それともこれはデバイスに依存しないシステムレベルの状態機械設計として扱うべきか? Q3:TVSの役割 NXP 27 MHzのリファレンス・デザインの議論では、ドレインからグラウンドまでの110V TVSについて議論され、スタンドオフ電圧は最大通常のドレイン電圧を上回るべきだというガイダンスが示されていました。当社のシステムには、既に能動的な反射電力保護機能が備わっています。TVSは、アクティブ保護が作動するまでの短い期間における最終ラインの遮断装置として扱うべきなのか、それとも保護機能のより大きな役割を担うことが期待されるのか?27 MHz CWでは、TVSの接合静電容量や応答速度が通常のRF波形忠実度に何か懸念をもたらすのでしょうか? 最も役立つものは以下の通りです: アプリケーションレベルのガイダンス、推奨アーキテクチャ、LDMOS PAのVSWR保護と回復に関する既存のNXPアプリケーションノートへの指針、あるいはNXP自身のリファレンス・デザインが故障・ホールドオフ再突入シーケンスをどのように扱っているかの簡単な説明があれば、デザインに直接反映されるでしょう。 よろしくお願いします。 Re: MRF300AN 27MHz VSWR Protection and Recovery Strategy こんにちは@fengyuqiさん 詳細な説明をありがとうございました。コンパレータ、ハードウェアラッチ、アクティブゲートバイアスプルダウンが合理的な一次保護経路を形成します。300WのCWアプリケーションでは、単一のメカニズムに頼るのではなく、レイヤーアーキテクチャの一部として利用することを推奨します。 可能な限り、高速なハードウェア経路はRFドライブを抑制しつつゲートバイアスを引き下げるべきです。MCUは即時のシャットダウンループの一部であってはなりません。その後のホールドオフ、診断、制御された再突入、繰り返しの故障ロックアウトを管理するべきです。 PINダイオードスイッチは、PA出力を既知で適切に定格されたインピーダンスに転送する場合のみ、ストレスを軽減できます。ハンドピースを単に接続解除するだけでも、別の断線状態が発生する可能性があります。この電力レベルでは、挿入損失、ダイオードの発熱、定格電圧、スイッチング過渡現象、およびスイッチング時に生じるインピーダンスをすべて考慮する必要があります。定格終端を持つ循環器は負荷のアイソレータを強化しますが、サイズ、コスト、損失のトレードオフが大きいです。 回復のためには、一定の最小ホールドオフに続いて低電力プローブと制御されたドライブランプを行うというシステムレベルのアプローチが妥当である。プローブ中は、前方電力と反射電力の両方を監視する必要がある。なぜなら、検出器のノイズフロア付近では、反射電力対前方電力比が不正確になる可能性があるからである。新たな障害が発生した場合は、システムは直ちにラッチ状態に戻り、繰り返し失敗した場合は、より長いバックオフ時間、または永久的なロックアウトとなるべきである。 NXPはMRF300ANについて、専用のホールドオフ時間、ランププロファイル、または再突入電力の上限値を規定していません。これらの値は、保護回路の応答、整合回路に蓄積されたエネルギー、検出器のダイナミックレンジ、バイアスの安定化、熱条件、および想定される負荷挙動に依存します。したがって、それらはシステムレベルで決定および検証される必要があり、複数の位相不整合角でのテストも含まれる。 ドレインTVSは、アクティブシャットダウンが有効になるまでの期間における最終ラインの過渡クランプとして考えるべきである。連続反射RF パワーを吸収することは期待できません。スタンドオフ電圧、クランプ挙動、パルスエネルギー能力、接合静電容量、パッケージ/レイアウトの寄生要素はすべてRFおよび過渡分析に含めなければなりません。なぜなら、デバイスは27 MHzの出力マッチングに影響を与える可能性があるためです。 公開されたMRF300AN 27 MHzリファレンスデザインには、適格な故障ホールドオフ再突入シーケンスは定義されていないため、完全な保護アーキテクチャはアプリケーション固有の設計責任に委ねられています。 よろしくお願いいたします。 パベル
View full article