MQX Software Solutions Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX Software Solutions Knowledge Base

Discussions

Sort by:
A new MQX Flash File System (FFS) add-on is available for Freescale MQX™ 4.0.2.   See MQX Downloads.  FFS provides wear-leveling support required for mapping MFS on top of NAND flash. Files available # Name Description 1 FSL_MQX__FFS_RELEASE_NOTES_4_0_2 Freescale   MQX™ FFS package 4.0.2 Release Notes 2 Freescale   MQX RTOS 4.0.2 FFS package NAND   Flash File System solution for MQX™ 4.0.2
View full article
MQX includes a great demo for the web server in \<MQX_Path>\demo\web_hvac.  The web pages in this demo show how MQX can serve up data through the web server, and dynamically update the web page, for example the thermostat hvac properties are updated every second.  Also, the user can use a web page form to submit data to the server and update the application, like changing the temperature set point.  This is done with HTML forms, javascript, and CGI running in the MQX application. However, the web_pages directory in the web_hvac demo is missing the actual source files for the web pages.  Starting with MQX v4.0.2, they disappeared from the MQX release.  And since then, the web server APIs and CGI functionality has changed.  Posted here is the web_page directory for web_hvac, including the source code for the web pages.
View full article
The attached document explains how to create a C++ project using CW10.6 with GCC compiler, MQX 4.1. Regards, Carlos
View full article
This blog shares several issues reported by China customers when they use NAND FFS in MQX4.1.1. NAND FFS open failure issue Customer reported they can use a pressure test code to continuously open file, write file and close file, each time write about 20 bytes with append and they will find after running for a while, file open will fail and it returns error code 0x3067 (MFS_EOF). Each time file open failed, file has been written with 20480 bytes. This is a typical use case at customer side for data logging. The test code is attached named as "nand_pressure_test.cpp". Attached patch file named "mfs_write.patch" can resolve this issue. Memory allocation issue when using MFS & NAND FFS Customer run pressure test for MFS and NAND FFS by creating multiple levels of sub-folders (up to 100 levels) and in each sub-folder they create random number of files (up to 50). For each file, they will write 250 bytes. They found code failed to open new file when create sub-folders to 41 level. Traced the code on K70 tower and found actually this is not problem with MFS to search clusters for the new file, instead when the issue occurs, it's the drive_ptr (MFS_DRIVE_STRUCT) which is corrupted when MFS use memory allocation routine to allocate file path. The pressure test code for this case is attached. File named "MultiLevel_Folder_Test.zip". The memory corruption for MFS drive info is due to there is no protection in MFS_Parse_pathname() on whether the actual path name used passed from fopen will be exceeding 260 bytes which is fixed in mfs.h file to be compatible with Windows. So need to take care of this internal limitation when handling multiple level folders. MFS deadlock issue when using NAND FFS Customer reported random code block issue when running pressure test against NAND FFS. The issue is quite random, sometimes takes 12 hrs to reproduce the issue. Test code attached. Name is "MFS deadlock issue.zip". The resolution and description on this issue is in attached file named "MQX-4919 NandFFS explanation". Hao
View full article
Video Tutorial 3 of 6 for the iDigi Connector for MQX: Writing Your First iDigi Enabled Application (3 of 6) - iDigi Device Cloud More information and free download at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS_IDIGI_M2M
View full article
Hi All, The new Freescale MQX™ 4.1.1 GA release is now available on www.freescale.com/mqxrtos ·         Files available           # Name Description 1 FSL_MQX_RELEASE_NOTES_4_1_1 Freescale   MQX™ RTOS 4.1.1 Release Notes 2 Freescale   MQX RTOS 4.1.1 for Linux This   release has the same basic code as the 4.1.1 version, with just the changes   needed to build and debug on Linux systems. 3 Freescale   MQX RTOS 4.1.1 MQX™    Source code. Includes an RTOS, File System, TCP/IP and USB host/device   software stacks. ·         What is New? ·         New Board Support Package o   FRDM-K64F o   TWR-K64F120M ·         New Features and Updates o   MQX RTOS 4.1.1 enables development on Linux machines o   MQX RTOS 4.1.1 supports the new Freescale IDE, Kinetis Design Studio o   Example ISR and related documentation is updated to give guidance on setting up a Kernel ISR (a.k.a Gorilla ISR) - extremely high priority ISR o   Power PC (PX) family support has been dropped o   Readme files are added to examples without a description o   Register definition header files for Kinetis MCUs are added for convenience when porting to an MCU sub-family device o   Both interrupt driven I2C master and slave mode drivers are changed to support synchronous blocking mode and share the same API with the polling driver variant.  Improves performance by eliminating the need to poll for data availability. ·         Known issues o   For known issues and limitations please consult the release notes
View full article
Hello I want to share this document that describes steps to configure and use the MQXLite Performance Tool to analyze and debug the applications of the Freescale MQXLite operating system. I hope this helps!! Regards Soledad
View full article
Tutorial 6 of 6 for the iDigi Connector for MQX: Adding Remote Configuration Support (6 of 6) - iDigi Device Cloud More information and free download at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS_IDIGI_M2M
View full article
1. Few basic questions and answers about FlexNVM and FlashX. 1.1 What is FlexNVM? FlexNVM is additional separate block of flash memory which could be used as data flash, as non volatile storage for emulated EEPROM or as combination both option. I will focus on first option in this document – FlexNVM will work simply as data flash. FlexNVM you can find in MCU parts which contain “X” at dedicated place in part number. For example: MK64FX512VMD12 contains 1 block (512 KB) of program flash and 1 block (128 KB) of FlexNVM MK64FN1M0VMD12 contains 2 blocks (512 KB each) of program flash only. For more details about FlexNVM and flash blocks, please see your MCU reference manual. For example chapter “Flash Memory Sizes”. 1.2 What is FlashX? MQX FlashX driver provide ability to write to and read from internal flash. Unfortunately FlexNVM memory is supported only partially in default state – Some of BSPs has implemented configuration and functions for emulated EEPROM (flexnvm example code). For more details, please check MQX_IO_User_Guide.pdf in c:\Freescale\Freescale_MQX_4_2\doc\mqx folder. 1.3 Can I use BSP for MCU without FlexNVM for my own board which has MCU with FlexNVM? It is not recommended. However you can use this BSP as base for your own board BSP. Please check MQX_BSP_Cloning_Wizard_Getting_Started.pdf, MQX_BSP_Porting_Guide.pdf  and MQX_BSP_Porting_Example_User_Guide.pdf documents in C:\Freescale\Freescale_MQX_4_2\doc folder. 1.4 Can I use FlashX in my KSDK project? Unfortunately FlashX driver was not implemented into KSDK. KSDK contains its own Standard Software Driver (SSD) for C90TFS/FTFx Flash family, however this is just low level driver without high level abstraction layer like in case of FlashX driver. 2. Procedure for update MQX FlashX driver to support FlexNVM. 2.1 Please backup these files: user_config.h, <your BSP>.h, init_flashx.c, flash_ftfl.c and flash_ftfe.c files. Note: user_config.h, <your BSP>.h and init_flashx.c are part of your BSP code. 2.2 Enable FlashX in user_config.h file by definition: #define BSPCFG_ENABLE_FLASHX                      1 2.3 Updates of <your BSP>.h file: 2.3.1 Please check MCU reference manual and update BSP_INTERNAL_FLASH_BASE, BSP_INTERNAL_FLASH_SIZE, BSP_INTERNAL_FLASH_SECTOR_SIZE if necessary. Typically we have to decrease BSP_INTERNAL_FLASH_SIZE in case when BSP without FlexNVM was used as base for own BSP. 2.3.2 Add new macros which will define FlexNVM in memory map. For example: #define BSP_INTERNAL_FLEXNVM_BASE  0x10000000 #define BSP_FLEXNVM_SECTOR_SIZE         0x400 #define BSP_INTERNAL_FLEXNVM_SIZE  0x00008000 2.4 Update init_flashx.c in your BSP folder: 2.4.1 Add FlexNVM file block into _bsp_flashx_file_blocks[] table. For example:     // data flash file block     { "dflash", BSP_INTERNAL_FLEXNVM_BASE, (uint32_t) (BSP_INTERNAL_FLEXNVM_BASE+ BSP_INTERNAL_FLEXNVM_SIZE - 1) },    Parameters are {name of file block, start address, end address}.    Note: This is pure software interface; range of addresses doesn’t need fit to physical flash block parameters. You can organize file blocks according your needs. 2.4.2 If you used non-FlexNVM BSP as base for your own BSP, you have to change HW block map for KinetisX devices. Please change _flashx_kinetisN_block_map into _flashx_kinetisX_block_map in _bsp_flashx_init structure. 2.5 Update flash_ftfl.c or flash_ftfe.c file: 2.5.1 Look at MCU reference manual whether your MCU has FTFL or FTFE flash memory module and select appropriate file for editing. 2.5.2 Add FlexNVM memory block into _flashx_kinetisX_block_map[] table. For example: { BSP_INTERNAL_FLEXNVM_SIZE / BSP_FLEXNVM_SECTOR_SIZE, (_mem_size) BSP_INTERNAL_FLEXNVM_BASE,  BSP_FLEXNVM_SECTOR_SIZE }, // FlexNVM block Parameters are {number of sectors, start address, sector size}. Note: This is description of physical hardware memory block; range of addresses must fit to physical flash block parameters. 2.5.3 Now we have to fix problem with FlexNVM address. Both Program Flash and FlexNVM Flash are programmed trough FTFL_FCCOBn / FTFE_FCCOBn registers where FCCOB1.. FCCOB3 contains address in 24bit format. Therefore we cannot work directly with FlexNVM addresses – they will not fit into 24bit due to FlexNVM base 0x10000000. FTFL/FTFE modules specifies that most significant bit in 24bit address (bit 23) will be used for distinguish between Program Flash and FlexNVM Flash. We can use for example such code: //Set 23th bit when FlexNVM flash address     if (write_addr & BSP_INTERNAL_FLEXNVM_BASE)     { write_addr = write_addr | (1 << 23);     }   and add this code into necessary functions prior write into command_array[] (content of command_array[] will be used for filling FTFL_FCCOBn / FTFE_FCCOBn registers). For basic work of FlashX example code is necessary update at least ftfl_flash_erase_sector()/ftfe_flash_erase_sector() and ftfl_flash_write_sector()/ftfe_flash_write_sector() functions. 2.6. After these changes, you can try using FlashX example code in flash_demo.c where you simply open FlexNVM file block instead of default program flash file block. For example: //#define FLASH_NAME "flashx:bank0" #define FLASH_NAME "flashx:dflash" In attachment file you can find example of modification for MQX4.2.0 and MK20DX72 MCU. 3. How to rewrite flash - general notes: Flash data must be in the erased state before being programmed. Cumulative programming of bits (adding more zeros) is not allowed. In case of both FTFL and FTFE modules we program flash by aligned phrases (typically 64 bits). If we want program by smaller chunks (e.g by bytes), FTFL module will allow you write into this phrase even if it is not recommended. However FTFE module will cause bus fault in case of second write into the same phrase. So, only save way how to change data in FTFE phrase which was already written is erase whole sector and rewrite data back. Therefore please use ioctl command FLASH_IOCTL_ENABLE_SECTOR_CACHE for FTFE module. The sector cache allocation is not required in case of Full sector write and partial sector overwrite when the destination area (aligned to phrases) is blank.
View full article
The Freescale MQX™ RTOS for Kinetis SDK FRDM-KL43Z Freescale Freedom Platform is now available on the www.freescale.com ·         Release Files             # Name Description 1                                   Freescale_MQX_KSDK_1.0.0-KL43Z.exe Windows installer. Freescale MQX™ RTOS software   components fully pre-integrated with the Kinetis SDK. Includes the MQX   kernel, USB host and device stacks, MFS file system, and example   applications. Does not require prior installation of Kinetis SDK. 2                                   Freescale_MQX_KSDK_1.0.0-KL43Z.bin Linux installer. Freescale MQX™ RTOS software   components fully pre-integrated with the Kinetis SDK. Includes the MQX   kernel, USB host and device stacks, MFS file system, and example   applications. Does not require prior installation of Kinetis SDK. 3 MQXKSDKKL43Z.pdf Freescale MQX™ RTOS for Kinetis   SDK FRDM-KL43Z Freescale Freedom Platform Release Notes ·         Target HW boards: o   Freescale Freedom FRDM-KL43Z platform with a MKL43Z256VLH4 processor ·         Key features:  o   PSP support for the MKL43Z256VLH4 Microcontroller o   BSP for the Freescale Freedom FRDM-KL43Z platform with a MKL43Z256VLH4 processor o   MQX STDLIB o   nShell o   KSDK Support for the MKL43Z256VLH4 Microcontroller o   MFS file system ·         Known issues For known issues and limitations please consult the release
View full article
Hi Community, Based on How To: Create an MQX RTOS for KSDK project with Processor Expert in Kinetis Design Studio IDE from macl​ and dereksnell you can find in the attached document the steps to include RTCS to a KDS3.0 project using KSDK1.2 and Processor Expert as well as the final project. Thank you RBORB​ for providing the first draft of this process. For information about creating a new KSDK project with MQX and without Processor Expert please see the following document. How To: Create a New MQX RTOS for KSDK Project in KDS If you are looking for a simple document to get started with KSDK please see the following document. Writing my first KSDK1.2 Application in KDS3.0 - Hello World and Toggle LED with GPIO Interrupt Regards, Carlos
View full article
The new Freescale MQX™ 4.1 GA release is now available on the www.freescale.com/MQX ·         Files available # Name Description 1 FSL_MQX_RELEASE_NOTES_4_1_0 Freescale   MQX™ RTOS 4.1 Release Notes 2 Freescale   MQX RTOS 4.1 MQX™    Source code. Includes an RTOS, File System, TCP/IP and USB host/device   software stacks. ·         What is New? o   New Board Support Package added §  TWR-K21F120M o   Vybrid-based board support packages for TWR-VF65GS10 and AutoEVB updated §  Support of audio-related drivers extended--SAI, eSAI, and ASRC. Device driver for DSP Codec CS422888 added (AutoEVB only). §  Support the Quadrature Decoder functionality in the FTM peripheral §  Added eDMA driver §  UART driver updated to use the eDMA §  Clock management component ported §  Added DCU driver §  QSPI driver updated to support the FlashX framework §  NAND FFS support added o   DMA support in device drivers has been extended §  Introduced new DMA device driver, supporting eDMA peripheral on Kinetis and Vybrid processor families §  The SPI device driver was updated to support the new DMA driver §  The SAI and eSAI audio drivers support DMA §  eSDHC drivers were reworked to fully leverage the ADMA peripheral module o   Driver updates §  The LWADC driver has been ported to all supported board support packages. The support of the legacy ADC driver was discontinued. §  The RTC driver was updated on all supported platforms. Provided generic, POSIX compatible API for time conversion functionality. §  FlashX driver extended by handling Flash Swap functionality on Kinetis processors. §  LP Timer module was added to the HW Timer framework. Its usage is demonstrated in the Low Power and HW Timer example applications o   Standardization effort §  Legacy MQX custom integer types were replaced by the Standard C99 set (int_32 -> int32_t, boolean -> bool, etc). A header file is provided with the set of backward compatible type definitions to make the transition to the new types easier. For more details, see Section 3.1 “C99 Types” in the Getting Started with Freescale MQX™ RTOS (document MQXGSRTOS). §  The endian conversion macros were consolidated inside MQX. The htons, ntons and similar conversion functions were renamed to mqx_htons, mqx_nton to avoid a conflict with the standard. o   NAND FFS library is no longer provided as a separate add in package but it is directly included as a part of MQX main package o   RTCS new features and enhancements §  The MQX TCP/IP stack is now available with an optional package to enable the IPv6 protocol support. For more information visit freescale.com/mqx. §  The FTP server was redesigned to provide faster and more stable implementation. §  The DNS resolver was updated. o   USB §  Fixed several EHCI related bugs (HUB, pipe close, audio example) o   MQX startup is now split in two parts to avoid a crash risk if an interrupt occurs during the startup. §  _bsp_enable_card() function has been replaced by the _bsp_pre_init() function that handles initialization of the OS vital functions, such as the timer (system tick), interrupt controller, memory management, etc. The _bsp_pre_init() function is called during the MQX initialization time, before any user task is created and the scheduler is not started. §  The second part of the startup is done in a separate _mqx_init_task that executes _bsp_init() function for I/O drivers or stacks initialization and _bsp_post_init() function for possible post-init operations. After the _bsp_post_init() function execution, the _mqx_init_task is destroyed. o   All BSPs are now adjusted to this concept. All I/O drivers are installed in the context of the _mqx_init_task after the MQX scheduler is started. This concept also allows a complex driver installation (handling ISRs during the driver initialization, drivers can use blocking functionality like _time_delay, etc.). ·         Known issues o   For known issues and limitations please consult the release notes.
View full article
MQX 4.1.0 provides a USB Host CDC demo in the folder of "C:\Freescale\Freescale_MQX_4_1\usb\host\examples\cdc\cdc_serial", but to get it work, several steps need to be done: 1. Change CDC_EXAMPLE_USE_HW_FLOW in cdc_serial.h to 1. #define CDC_EXAMPLE_USE_HW_FLOW 1 2. In config\twrk70f120m\user_config.h, interrupt mode for UART should be set.//It depends on the platform, here given TWR-K70F120M is used. #define BSPCFG_ENABLE_TTYC 0 #define BSPCFG_ENABLE_ITTYC 1 In mqx\source\bsp\twrk70f120m\twrk70f120m.h, specify 'ittyc' instead of 'ttyc' #ifndef BSP_DEFAULT_IO_CHANNEL #if BSPCFG_ENABLE_ITTYC #define BSP_DEFAULT_IO_CHANNEL "ittyc:" /* OSJTAG-COM polled mode */ #define BSP_DEFAULT_IO_CHANNEL_DEFINED #else #define BSP_DEFAULT_IO_CHANNEL NULL #endif #else 3. In usb\host\source\classes\cdc\usb_host_cdc.c, pass fd_ptr instead of data_instance as the argument. a. Around line 977 //usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_in_data_callback, (void *) data_instance); usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_in_data_callback, (void *) fd_ptr); b. Around line 1116 //usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_in_data_callback, (void *) data_instance); usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_in_data_callback, (void *) fd_ptr); c. Around line 1226 //usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_out_data_callback, (void *) data_instance); usb_hostdev_tr_init(&#38;tr, (tr_callback) usb_class_cdc_out_data_callback, (void *) fd_ptr); With above modification , the Host CDC demo can work with a Device CDC demo, such as the one in "C:\Freescale\Freescale_MQX_4_1\usb\device\examples\cdc\virtual_com", which is an echo demo, it would send back anything charactor that it receives. But to see the echo more clearly, I made it echo back the charactor that greater than what is received, for example, if you type A, and will see B from the HyperTerminal. To do that , you have to change Virtual_Com_App(void) in the virtual_com.c as below: void Virtual_Com_App(void) {     /* User Code */     if(g_recv_size)     {         _mqx_int i;                 /* Copy Buffer to Send Buff */         for (i = 0; i < g_recv_size; i++)         {             printf("Copied: %c\n", g_curr_recv_buf[i]);             g_curr_send_buf[g_send_size++] = g_curr_recv_buf[i]+1;         }         g_recv_size = 0;     }         if(g_send_size)     {         uint8_t error;         uint8_t size = g_send_size;         g_send_size = 0;         error = USB_Class_CDC_Send_Data(g_app_handle, DIC_BULK_IN_ENDPOINT,             g_curr_send_buf, size);         if (!error && !(size % DIC_BULK_IN_ENDP_PACKET_SIZE)) {             /* If the last packet is the size of endpoint, then send also zero-ended packet,             ** meaning that we want to inform the host that we do not have any additional             ** data, so it can flush the output.             */             error = USB_Class_CDC_Send_Data(g_app_handle, DIC_BULK_IN_ENDPOINT, NULL, 0);         }         if(error != USB_OK)         {             /* Failure to send Data Handling code here */         }     }     return; } After you download code into, for example, TWR-K70F120(Host) and TWR-K60D100M(Device), and assemble them with TWR-SER and TWR-ELEV, you may connect them via USB port as below: Please also pay attention to J10(USB VBUS Select) and J16(USB Mode Select) according to the function of each tower system. With HyperTerminal connected with TWR-K70F120M system, you may type in any charactor ended with ENTER, and you will see the charactor echoed back as the attached video. This issue would be fixed in the next release, and sorry for the inconvenience that has caused.
View full article
Atheros WiFi Tower Module (TWR-WIFI-AR4100P) support patch for Freescale MQX™ 4.0.2  is available at MQX Downloads. Files available # Name Description 1 FSL_MQX_ATHEROS_RELEASE_NOTES_4_0_2  Freescale   MQX™ Atheros Wifi package 4.0.2 Release Notes 2 Freescale   MQX RTOS 4.0.2 Atheros Wifi package Atheros   Wifi solution for MQX™ 4.0.2
View full article
SPI, which stands for Serial Peripheral Interface, is a standard with a very specific hardware interface. A connection is between a master and a slave, with the master typical being a processor, and the slave being a peripheral such as a sensor, flash memory device, or a modem chip.   It can also be used for processor to processor communications, but in this case, an additional handshake signal is often used. There are normally four signals between a master and a slave, the first is a clock signal, and this signal is always driven by the master, regard which device is transmitting.  The second line is a data line for data going from the master to the slave, and this is designated as the master output, slave input line, are MOSI for short. It connects the SPI data out connection on the master and to the SPI data in connection on the slave. The next conductor is for data in the opposite direction and is labelled as the master input slave output line, are MISO for short. The last conductor is slave select with the slave chip selecting input, and is active low. If you have more than one slave, with the first being perhaps a sensor of some kind, the slave will be dedicated to slave 1. If you add a second sensor, the top 3 interface line will be shared, but it dedicates for slave’s line will be required for the second device, and the same is true of course for each of additional slave device. Most processors have a maxim of 4 slave selected lines.  The four lines could be used effectively as a multiplexed address lines to access more than 4 slaves. You cannot have more than one master on the bus,   since the interface is not support coordination between two masters as to which one is controlling the bus. Transmissions are typically sent as a sequence of bytes, but without a formal protocol, there is nothing restricting communication being   byte based. Typical by frame sizes, are in 8 to 32 bits range.  Also note the bytes and packets are not acknowledged as they are in i2c, and you could have a master synching communicating with the slave but, you don’t really know of your communications are being received OK. However, some slave devices will echo bytes sent to it, which provides an acknowledgement to the master.  it is how the data lines are synchronized with a clock signal. Clock Polarity and Phasing There are four different modes available, one mode each combination clocking in a low state and high state, with a data being read in a rising edge or falling edge of the clock signal.  For modes 0 and 1, the clock is low in idle, which is referred to  as clock and 0,  For modes 2 and 3 then the clock is in high state when idle, so it has  polarity  , one , For modes 0 and 2, the data will be sampled by the receiving device  on the leading edge of a clock signal.  Relative to the idle state, which is referred to a clock phase of zero. So for mode 0, this means the rising edge of the clock and for mode 2, means the following edge of the clock, the other two modes, use a clock phase 1 which means that trailing edge of clock as a returns to an  idle state.  And this translates to a following edge for mode 1 and the rising edge for mode 3.  Mode 0 is the most commonly supported setting. If multiple slaves in the same bus, you may have to reconfigure the settings for the master to which modes when you want to communicate with a different slave.
View full article
A new patch, MQX v4.2.0.2, is now available at www.nxp.com/mqxclassic​.This release comes in one download that contains both .zip packages and patch files. See the Release Notes (attached) for a full list of issues that are fixed in this release. The Release Notes also contain instructions for how to install via the .zip or patch files. To Download the patch: 1. go to www.nxp.com/mqxclassic 2. Click the "Download" button (below the Overview paragraph) -- you may be prompted to Sign In 3. Click on "MQX RTOS v4.2 releases and patches" 4. Review and click through the license agreement 5. Click on "MQX 4.2.0.2 Patch.zip"
View full article
MQX RTOS developers can now build and debug MQX RTOS on Linux computers right out-of-the-box without extensive setup steps.  Linux support is provided in a separate version of MQX 4.1.0, repackaged for use on Linux systems.  Kinetis & Vybrid BSPs from MQX 4.1.0 are supported.  The new package is in beta stage.  It includes the same basic code as the previous 4.1.0 version, with just the changes needed to build and debug on Linux systems. Download Freescale MQX RTOS 4.1.0 for Linux Beta Depending on the popularity of this release, Freescale may extend Linux support to future MQX RTOS mainline releases.  Stay tuned. Give us your feedback!  Post to the MQX community.  Let us know what you think. Development tools Supported: DS-5 Vybrid Controller Edition 5.16.0  (Vybrid) GNU Tools for ARM Embedded Processors version 4.7-2013-q3  (Kinetis & Vybrid) Here are some brief instructions I put together when using with Ubuntu 12.04: - Download and install gcc for arm (comes with gdb for debugging)   See other post:  gcc compiling + gdb debugging on Kinetis on a Linux host - Kinetis L Examples available - Download and extract the .tar.gz file to a location of your choice    mac@mac-VirtualBox:/$  tar -zxvf Freescale_MQX_4_1_LINUX_beta.tar.gz - Edit global.mk to tell it where your gcc toolchain is located.    mac@mac-VirtualBox:/$ cd <directory where you extracted mqx>/Freescale_MQX_4_1_LINUX_beta/build/common/make/    mac@mac-VirtualBox:/$ vi global.mak    un-comment the section on gcc_arm and set the TOOLCHAIN_ROOTDIR.  For my toolchain gcc is installed to the path /usr/    ifreq ($(TOOL),gcc_arm)        TOOLCHAIN_ROOTDIR  =  /usr/   endif - See  MQX GNU Getting Started Guide for instructions on how to build and debug.     This document is located at /Freescale_MQX_4_1_LINUX_beta/doc/tools/gnu/ Good luck with your next project.  Happy developing!
View full article
The new Freescale MQX™ 4.1.1 Cloning Wizard patch is now available on the www.freescale.com/mqxrtos ·         Patch Description o   BSP Cloning Wizard is now based on Eclipse 4.4 o   Kinetis Design Studio support for generating projects (libraries, examples) and working sets (.wsd files for Project of Projects plug-in) o   Remembering opened boards (cloned or opened by user) from previous application run o   BSP Cloning Wizard saves users selection of IDEs, Libraries and Examples in project generator section for all currently opened boards o   Fix the issue of the BSP Cloning Wizard not working in MQX 4.1.1 To get the patch follow the next instructions: Go to www.freescale.com/mqxrtos Click on the big Download Button.  - You will have to log in if you aren’t already.  Click on MQX RTOS for Kinetis, Vybrid, Coldfire v4.1.1….. The patch for the cloning wizard is on the list of files.
View full article
The attached document shows how to get the MQX4.1 Virtual Com Port Example. This document is located in the following path: C:\Freescale\Freescale_MQX_4_1\usb\device\examples\cdc\virtual_com Regards, Carlos
View full article
Table of Contents Product Information on Freescale.com MQX Lite RTOS Product Summary Page Frequently Asked Questions (FAQ) General MQX FAQs Technical MQX FAQs Other Resources MQX Training Videos MQX Add-On Software
View full article