The new Freescale MQX™ 4.1.1 Cloning Wizard patch is now available on the www.freescale.com/mqxrtos
· Patch Description
o BSP Cloning Wizard is now based on Eclipse 4.4
o Kinetis Design Studio support for generating projects (libraries, examples) and working sets (.wsd files for Project of Projects plug-in)
o Remembering opened boards (cloned or opened by user) from previous application run
o BSP Cloning Wizard saves users selection of IDEs, Libraries and Examples in project generator section for all currently opened boards
o Fix the issue of the BSP Cloning Wizard not working in MQX 4.1.1
To get the patch follow the next instructions:
Go to www.freescale.com/mqxrtos
Click on the big Download Button.
- You will have to log in if you aren’t already.
Click on MQX RTOS for Kinetis, Vybrid, Coldfire v4.1.1…..
![Step 1.jpg Step 1.jpg](/t5/image/serverpage/image-id/49800i7689F0FEEBFC975D/image-size/large?v=v2&px=999)
The patch for the cloning wizard is on the list of files.
![Step 2.jpg Step 2.jpg](/t5/image/serverpage/image-id/49853i629912AC0F802D91/image-size/large?v=v2&px=999)