MPC5606B DFLASH,CFLASH erase,write sample code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5606B DFLASH,CFLASH erase,write sample code

3,039件の閲覧回数
明伟张
Contributor III

I had to  configure the flash;please offer me the sample code;

thanks a lot;

2 返答(返信)

2,278件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I could recommend to see following example codes, it shows simple non-SSD flash programming codes:

Example MPC5643L Flash_program_simple CW210 

Example MPC5675K Data_flash_program_simple CW210 

Better solution is to use SSD driver, example codes you may then find in installation package:

pastedImage_3.png

2,278件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

all available sample codes are include in MPC5 example list. Please check the link below:

https://community.nxp.com/docs/DOC-329623 

Regards,

Martin