MPC5606B DFLASH,CFLASH erase,write sample code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5606B DFLASH,CFLASH erase,write sample code

3,076 次查看
明伟张
Contributor III

I had to  configure the flash;please offer me the sample code;

thanks a lot;

2 回复数

2,315 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I could recommend to see following example codes, it shows simple non-SSD flash programming codes:

Example MPC5643L Flash_program_simple CW210 

Example MPC5675K Data_flash_program_simple CW210 

Better solution is to use SSD driver, example codes you may then find in installation package:

pastedImage_3.png

2,315 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

all available sample codes are include in MPC5 example list. Please check the link below:

https://community.nxp.com/docs/DOC-329623 

Regards,

Martin