******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * setup clock for peripherals, * * Initializes the MCU including the FlexCAN peripherals. * Configures the FlexCAN to transmit and receive a CAN message. * * Individual RX masking was added to the last version of this example. * Three messages with different ID's are sent via FlexCAN_0 MB0 MB1 and MB2. * These messages are received by FlexCAN_1 MB0, MB1 and MB2 according to masking * register settings. * * For MB0 data receive is used interrupt. * * * ------------------------------------------------------------------------------ * Test HW: S32R274RRUEVB, MPC57xx Motherboard * MCU: S32R274KAMMM 1N58R * Fsys: PLL0 240MHz * Z4 Core 120MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: internal_FLASH (debug mode, debug_ram and release mode) * EVB connection: * * It is necessary to remove both J35 jumpers. * * * Connect J35.2 to PA14 (CAN_1 TX) * Connect J35.4 to PA15 (CAN_1 RX) * * CAN0 is connected internally to J37 (this pin is placed on daughter card) * * Connect CAN P5.2 to J37.2 (CAN_1 and CAN_0 CANL) * Connect CAN P5.1 to J37.1 (CAN_1 and CAN_0 CANH) * * This connection has to be observed, otherwise correct communication between * CAN modules is not guaranteed. * * ********************************************************************************
View full article