MPC5xxx Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5xxx Knowledge Base

Labels
  • General 164
  • test 7

Discussions

Sort by:
******************************************************************************** * Detailed Description: * Initializes eQADC module, converts specified command queue and displays * results into terminal window when EOQ is reached. Used analog inputs ANA_0 and * ANA_1 requires external connection to converted voltage (potentiometer) to * see some valid numbers. For simplicity, ADC module is not calibrated. * ------------------------------------------------------------------------------ * Test HW:         XPC567XKIT516 - MPC5674ADAT516 Rev.C, MPC567XEVBFXMB Rev.B * MCU:             PPC5674FMVYA264 * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys:            264/200/150/60 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          RAM, internal_FLASH * EVB connection:  Potentiometers     --> ADC inputs *                  USER_DEV_RV2(J4-7) --> ANA_0 (J18-3) *                  USER_DEV_RV3(J4-8) --> ANA_1 (J18-4)                * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * Unlock, erase and program of flash mid block 0x00FB_8000 - 0x00FB_FFFF. * ------------------------------------------------------------------------------ * Test HW:        X - PC5748G - MB (rev C) * MCU:             PPC5748GMMN6A * Maskset:       1N81M * Fsys:             160 MHz * Debugger:     Lauterbach Trace32 *             * Target:     Internal_FLASH * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * Example shows MCU's temperature measurement with the help of TSENS. * Calibartion constants for TSENS0 and TSENS1 are read from Test Flash and * ADC0/ADC1 is set to measure Vbg and TSENS outputs. * Calculated internal temperature can be desplayed on the Terminal. * * EVB connection: * *   Route LINFlexD_0 TXD/RXD (PB2/PB3) signals to the main board RS-232 transceiver *   Daughtercard: *   J17.11–12 ON  .. Connect LINFlexD_0 TXD (PB2) to main board. *   J17.8–9 ON .. Connect LINFlexD_0 RXD (PB3) to main board. * *   Motherboard *   J14 - SCI_RX ON *   J13 - SCI_TX ON *   J25 - SCI_PWR ON * * See results on PC terminal (19200, 8N1, None). You should get following text * (with different values for sure) * * TSENS0/TSENS1 temperature measurement * press any key to continue... * * Calibration constants read from Test Flash * * TSENS0                           TSENS1 * * K1 = 429                         K1 = -220 * K2 = -5785                       K2 = -5767 * K3 = -12800                      K3 = -12736 * K4 = 45                          K4 = 45 * *      K1 * Vbg_code * 2^-1 + K2 * TSENS_code * 2^3 * T = ------------------------------------------------------------------------- / 4 - 273.15 [degC] *     [K3 * Vbg_code * 2^2 + K4 * TSENS_code] * 2^-10 * * Vbg0_code      = 1502               Vbg1_code      = 1502 * TSENS0_code = 2002               TSENS1_code = 1988 * * TSENS0 temp = 34.57 degC         TSENS1 temp = 36.78 degC * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  RAM, internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference * Terminal: 19200, 8N1, None ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Inject and handles HVD and LVD faults. Application also configures FCCU_F pins * to see possible faults externally - normally these two pins toggles antiphase, * in case error these pins toggles inphase. If you step the code not allowing * alarm interrupt to be handled on time, device goes to safe mode and FCCU_F * pins toggles in phase. * ------------------------------------------------------------------------------ * Test HW:         xPC564xLKIT, PPC5643L Cut3 silicon * Target :         internal_FLASH, RAM * Fsys:            120 MHz PLL0 * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0 * EVB connection:  FCCU_F0 and FCCU_F1 connected to the scope - pay attention to *                  J16 and J18 jumpers on mini-module (FCCU_F0 and FCCU_F1). * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, second LED by software * loop, initializes and display notice via UART terminal and then terminal ECHO. * The example configures the device for maximum performance (OPTIMIZATIONS_ON). * Its intention is to offer advanced startup code additional to CW stationery. * ------------------------------------------------------------------------------ * Test HW:        MPC5566EVB * MCU:            PPC5566MVR132 * Fsys:           144/132/112/80/12 MHz * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: TPU_PORT_37 -> USER_LED_8 *                 TPU_PORT_38 -> USER_LED_7 (to see blinking LEDs)    * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * Simple LINFlex UART mode transmit and receive without interrupts (polled UART) * TXFIFO and RXFIFO macro is used to select between buffer and FIFO mode * * EVB connection: * *   Route LINFlexD_0 TXD/RXD (PB2/PB3) signals to the main board RS-232 transceiver *   Daughtercard: *   J17.11–12 ON  .. Connect LINFlexD_0 TXD (PB2) to main board. *   J17.8–9 ON .. Connect LINFlexD_0 RXD (PB3) to main board. * *   Motherboard *   J14 - SCI_RX ON *   J13 - SCI_TX ON *   J25 - SCI_PWR ON * * See results on PC terminal (19200, 8N1, None). * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  RAM, internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference * Terminal: 19200, 8N1, None ********************************************************************************
View full article
This document gives a basic insight into bit timings relationship and provide easy step-by-step guide to calculate CAN bit timing parameters for desired baudrate.
View full article
This document summarizes simple I2C driver implementation for MPC5xxx devices. The code follows Reference Manual's Flow-Chart of Typical I2C Interrupt Routine.
View full article
******************************************************************************** Detailed Description:  Example shows MCU's temperature measurement with the help of TSENS.  Calibration constants for TSENS0 are read from Test Flash and  SARADC_B is set to measure Vbg and TSENS outputs.  Calculated internal temperature can be displayed on the Terminal.  EVB connection:    Motherboard    J14 - SCI_RX ON    J13 - SCI_TX ON    J25 - SCI_PWR ON    See results on PC terminal (19200, 8N1, None). You should see following text  (with different values for sure)  TSENS - temperature measurement  press any key to continue...  TSENS's calibration constants read from Test Flash  TSCA = 184  TSCB = 21    T = (232 + TSCA * 2^-6) * TSENS_code / VBG_code - (273 + TSCB * 2^-4) [degC]  ----------------------------------------------------------------------------  VBG_code   =  251  TSENS_code =  339  TSENS temp = 42.91 degC  ------------------------------------------------------------------------------  Test HW:  MPC5777M  Maskset:  0N50N  Target :  RAM, internal_FLASH  Fsys:     600 MHz PLL1 with 40 MHz crystal reference  Terminal: 19200baud, 8N1 ********************************************************************************
View full article
This document shows, how to use CodeWarrior 10.6 to program QSPI flash for Power Architecture microcontrollers.   1) Create new project for appropriate microcontroller. 2) Open Debug configuration and duplicate one of the target.   3) Rename duplicated target (optional) 4) Choose the duplicated (renamed) target and click Edit button in Target settings tab.   5) In new screen, click Advanced Programming Options.   6) Check Use Alternative Algorithm and choose the algorithm you want to use. Algorithms are place in CodeWarrior installation folder. Full path is CodeWarrior_installation_folder\MCU\bin\plugins\support\EPPC\gdi\P&E\   7) On the screen Debug configuration, choose the file you want to program to QSPI flash.   Click Apply and Debug.
View full article
******************************************************************************** * Detailed Description: * * Example gives possible implementation of input signal period/freq measurement. * eTimer channel capture 1 and 2 features are used. CAPT1/CAPT2 capture counter * value on rising/falling edge of input signal. The FIFO is set to 2 entries * and ICF2 is monitored. Free-running mode is used here. * * eTimer channel 0-1 are cascaded to achieve 1sec/1Hz measuring with 32bit counter.   * EVB connection: *   P8.2  - A[1]  .. eTimer0 channel1 input signal *   P8.1  - A[0]  .. GPIO output, used to show measurement period * *   Route LINFlexD_0 TXD/RXD (PB2/PB3) signals to the main board RS-232 transceiver *   Daughtercard: *   J17.11–12 ON  .. Connect LINFlexD_0 TXD (PB2) to main board. *   J17.8–9 ON .. Connect LINFlexD_0 RXD (PB3) to main board. * *   Motherboard *   J14 - SCI_RX ON *   J13 - SCI_TX ON *   J25 - SCI_PWR ON * * connect pulse signal to the P8.2. * See results on PC terminal (19200, 8N1, None). * Change freq/duty of input signal. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference * Terminal: 19200, 8N1, None ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Sensor board OM11057A which includes two PCF8885 circuits is connected * to MPC5748G via I2C. MPC5748G continuously reads the state of touch sensors * and the state is shown on LED diodes which are driven by I2C circuit PCA9535. * * Used I2C driver: https://community.freescale.com/docs/DOC-330972 * * Touch sensor board (page 9 and 10): * http://www.nxp.com/documents/user_manual/UM10505.pdf * * ------------------------------------------------------------------------------ * * Connection: * * Connect I2C bus (I2C_2 on MPC5748G) to sensor board: * I2C_SCL: P24-33 (pin PE9) on MPC574XG-MB to K3-1 on OM11057A * I2C_SDA: P24-35 (pin PE8) on MPC574XG-MB to K3-13 on OM11057A * Note: use two pull-up resistors on I2C signals (pulled to 3.3V). * The value should be 3k3 - 10k * * Connect power supply from MPC574XG-MB to OM11057A: * GND: P24-2 on MPC574XG-MB to K3-7 on OM11057A * 3.3V: P24-1 on MPC574XG-MB to K3-9 on OM11057A * * Connect SLEEP pins of both PCF8885 to GND (this will ensure that sleep mode * is not entered): * SLEEP1: K3-11 to K2-3 (both on OM11057A) * SLEEP2: K1-6 to K1-8 (both on OM11057A) * * ------------------------------------------------------------------------------ * Sensor board:    OM11057A *                  http://www.nxp.com/documents/user_manual/UM10505.pdf * Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * MCU:             PPC5748GMMN6A 1N81M * Fsys:            160 MHz PLL * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
View full article
/* * Queue.h * *  Created on: May 28, 2015 *      Author: ShuLizhong */     #ifndef QUEUE_H_ #define QUEUE_H_ #ifdef _cplusplus extern "C" { #endif /*If you want to change the queue type(QUEUE_TYPE) and queue max size(QUEUE_MAX_SIZE),   you should define it at front of include queue.h file. eg: ******in xxx.h file***** code**** #define QUEUE_TYPE   Other type(unsigned int) #define QUEUE_MAX_SIZE   Other size(100) #include "qeue.h" code**** */ #ifndef QUEUE_TYPE #define QUEUE_TYPE unsigned char #endif #ifndef QUEUE_MAX_SIZE #define QUEUE_MAX_SIZE 100 #endif #define bool unsigned int typedef enum {   OK,   FULL,   EMPTY }QUEUE_STATUS; typedef struct {   unsigned int tail;   unsigned int head;   unsigned int size;   unsigned int length;   QUEUE_TYPE data[QUEUE_MAX_SIZE]; }Queue_tag,*pQueue_tag;     __inline void InitQueue(pQueue_tag q) {   q->tail = q->head = q->size = 0;   q->length = QUEUE_MAX_SIZE; } __inline  QUEUE_STATUS EnQueue(pQueue_tag q,QUEUE_TYPE data) {   if(q->size++ == QUEUE_MAX_SIZE)   return FULL;   q->data[q->tail] = data;   q->tail = (q->tail+1) % QUEUE_MAX_SIZE;   return OK; } __inline QUEUE_STATUS DeQueue(pQueue_tag q, QUEUE_TYPE *data) {   if(q->size-- == 0)   return EMPTY;   *data = q->data[q->head];   q->head = (q->head+1) % QUEUE_MAX_SIZE;   return OK; } __inline bool IsQueueEmpty(pQueue_tag q) {   return q->size == 0; } __inline bool IsQueueFull(pQueue_tag q) {   return q->size == QUEUE_MAX_SIZE; } __inline unsigned int GetQueueSize(pQueue_tag q) {   return q->size; } __inline unsigned int GetQueueLength(pQueue_tag  q) {   return q->length; } /*__inline unsigned int DeMoreBytesFromQueue(pQueue_tag q,QUEUE_TYPE *data,unsigned int len) {   unsigned int i = 0;   len++;   return 0; }*/     #ifdef _cplusplus } #endif #endif /* QUEUE_H_ */
View full article
This excel tool simplifies setting of PLL on MPC55xx/56xx devices. First select device and define input/output frequency. Possible configurations are calculated and basic PLL init code is generated as well. NOTE: macro has to be enabled! BR, Petr
View full article
******************************************************************************** * Detailed Description: * This example content a driver for CGM module configuration. * ------------------------------------------------------------------------------ * Test HW:  MPC57xx Motherboard + MPC5744PE257DC minimodule, MPC5744P, * silicon mask set 1N65H * Target :  internal_FLASH* ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Initializes eQADC module, performs calibration and converts channel 146 * (voltage level of VDD) to check core voltage level and displays it into * terminal window. No external connection required excluding terminal via eSCI. * * ------------------------------------------------------------------------------ * Test HW:        XPC564AKIT208S and XPC564AKIT324S * MCU:            SPC5644AMMG1,0M14X and SPC5644AMVZ1,0M14X * Fsys:           150/132/120/12 MHz * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: default * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Example configures Sigma_Delta ADC and periodically converts ANA0_SDA0 input * (EVB's potentiometer can be connected i.e. J53-1 --> PO15) and displays * results in the terminal window (USBtoUART bridge J21). Terminal settings is * 19200-8-no parity-1 stop bit-no flow control on eSCI_A. * * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 2N45H CTZZS1521A * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A *                  eSCI_A is USBtoUART bridge (connector J21) * EVB connection:  For ADC: J53-1 (EVB pot's wiper) --> PO15 (header P22) * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * This example shows how to reprogram the shadow flash. * * It is highly recommended to read application note "Preventing Device Lockout * via Censorship on MPC55xx and MPC563x Families" * http://www.freescale.com/files/32bit/doc/app_note/AN3787.pdf * * This examples erases the shadow flash, then it restores censorship information * and then NVUSRO nonvolatile register is reprogrammed to disable the watchdog. * The watchdog is disabled by clearing of bit WATCHDOG_EN in NVUSRO. It ensures * that watchdog is disabled automatically during startup of MCU. * Watchdog can be also disabled by software (shown in the code). * * It is important to execute the code from RAM memory because Read-While-Write * is not supported here. * * ------------------------------------------------------------------------------ * Test HW:  XPC56xxMB2 + XPC560B 144LQFP, SPC5604B, silicon mask set 2M27V * Target :  internal_FLASH, RAM * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, * initializes and display notice via UART terminal and then terminal ECHO. * ------------------------------------------------------------------------------ * Test HW:        XPC5607B 176LQFP, XPC56XX EVB MOTHEBOARD Rev.C * MCU:             PPC5607BMLUAM03Y * Fsys:             64/48 MHz * Debugger:      Lauterbach Trace32 *                      PeMicro USB-ML-PPCNEXUS * Target:           RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on LINFLEX_0 * EVB connection: default * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * This example shows how to use CRC module. * - CRC32 is used * - byte stream is written into input register * - one test case uses direct access to CRC registers * - second test case uses DMA to write the data stream * - the results can be compared using this online calculator: *   http://www.zorc.breitbandkatze.de/crc.html * - screenshots from online calculator are attached * ------------------------------------------------------------------------------ * Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * MCU:             PPC5748GMMN6A 1N81M * Fsys:            160 MHz PLL * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH ********************************************************************************
View full article