Layerscape ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Layerscape Knowledge Base

ディスカッション

ソート順:
Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images in QSPI NOR flash. In LS2088ARDB, Boot option switching between parallel NOR boot and QSPI NOR boot cannot be performed using commands. Boot option switching can be done by adjusting DIP switch settings and jumper settings on the Reference Design Board. For details, see Layerscape Software Development Kit User Guide. Obtaining MC firmware Clone the qoriq-mc-binary repository. $ git clone https://github.com/NXP/qoriq-mc-binary.git $ cd qoriq-mc-binary/ls2088a/ $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 The prebuilt MC firmware image, mc_10.18.0_ls2088a.itb, is available at /qoriq-mc-binary/ls2088a/. Note that the name of the MC firmware image may vary depending on the release version used.  Obtaining DPC and DPL images Clone the mc-utils repository and compile the DPC and DPL images. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils $ cd mc-utils $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 If required, make changes to the DPC and DPL files. $ make -C config/ The compiled dpc.0x2A_0x41.dtb and  dpl-eth.0x2A_0x41.dtb images are available at /mc-utils/config/ls2088a/RDB/. Note that the name of the DPC and DPL images may vary depending on the release version used.  Flashing MC firmware, DPC, and DPL images to QSPI NOR flash Boot LS2088ARDB from QSPI. Ensure that the switches and jumpers are set to boot the board from QSPI. For booting from QSPI: SW5[1:8] = 1111 1111 SW3[1:8] = 0011 0001 SW4[1:8] = 0011 1111 SW6[1:8] = 1111 1111 SW7[1:8] = 0100 1010 SW9[1:8] = 0100 0100 SW8[1:8] = 0111 1111 In addition to the above switch settings, make sure the following jumper settings are correct (for RDB Rev E and later).  J8 = 1-2 for QSPI boot, via onboard QSPI flash J8 = 2-3 for QSPI boot, via QSPI emulator J14 = 2-3, for QSPI boot For LS2088ARDB, in boot log, you'll see: Board: LS2088AE Rev1.1-RDB, Board Arch: V0, Board version: A, boot from vBank: 0 Option 1: Load image from the TFTP server Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@xgmii, DPMAC6@xgmii, DPMAC7@xgmii, DPMAC8@xgmii    Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1>    Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS2088ARDB Ethernet port mappingfor the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC1@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC1@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC1@xgmii device host 192.168.1.1 is alive Load images from a TFTP server Flash MC firmware to QSPI NOR flash: => sf probe 0:0 => tftp 0xa0000000 mc_10.18.0_ls2088a.itb => print filesize => sf erase 0x00A00000 +$filesize && sf write 0xa0000000 0x00A00000 $filesize Address 0x00A00000 is the location of MC firmware in QSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image to QSPI NOR flash: => sf probe 0:0 => tftp 0xa0000000 dpl-eth.0x2A_0x41.dtb => print filesize  => sf erase 0x00D00000 +$filesize && sf write 0xa0000000 0x00D00000 $filesize Address 0x00D00000 is the location of DPL image in alternate NOR bank. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPC image to QSPI NOR flash: => sf probe 0:0 => tftp 0xa0000000 dpc.0x2A_0x41.dtb => print filesize  => sf erase 0x00E00000 +$filesize && sf write 0xa0000000 0x00E00000 $filesize Address 0x00E00000 is the location of DPC image in alternate NOR bank. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Reset from QSPI NOR flash: => reset Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored in QSPI NOR flash. Option 2: Load images from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on the storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 If the ls command fails to run, check that U-Boot in QSPI NOR flash supports the command by typing ls at the U-Boot prompt: => ls ls - Lists files in a directory (default) Usage: ls <interface> [<dev[:part]> [directory]] - Lists files in directory [directory] of partition [part] on device type [interface] and instance [dev]. If U-Boot does not support this command, then update the composite firmware image in QSPI NOR flash. For steps to update composite firmware image in QSPI NOR flash, see Layerscape Software Development Kit User Guide . Use the following command if the SD card is formatted/created using LSDK flex-installer command: => load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: =>load mmc 0:2 $load_addrmc_10.18.0_ls2088a.itb Use the following command if the SD card is formatted/created on a Windows PC: => fatload <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: =>fatload mmc 0:2 $load_addrmc_10.18.0_ls2088a.itb Use the following command if the SD card is formatted/created on a Linux PC: => ext2load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: =>ext2load mmc 0:2 $load_addrmc_10.18.0_ls2088a.itb Also note that LSDK flex-installer command puts the images on the IInd partition, so 0:2 is used in the load command. If the SD card is formatted on Windows PC or Linux PC for single partition only, then 0 should be used instead of 0:2 in the fatload/ext2load command. Flash MC firmware: Program QSPI NOR flash: => sf probe 0:0 Load MC firmware image from the storage device => load mmc 0:2 80000000 <mc firmware> For example: => load mmc 0:2 80000000 mc_10.18.0_ls2088a.itb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program MC firmware image to QSPI NOR flash: => sf erase 0x00A00000 +$filesize && sf write 0x80000000 0x00A00000 $filesize Address 0x00A00000 is the location of MC firmware in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Program QSPI NOR flash: => sf probe 0:0 Load DPL image from the storage device => load mmc 0:2 80000000 <dpl image> For example: => load mmc 0:2 80000000 dpl-eth.0x2A_0x41.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program DPL image to QSPI NOR flash: => sf erase 0x00D00000 +$filesize && sf write 0x80000000 0x00D00000 $filesize Address 0x00D00000 is the location of DPL image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image: Flash DPC image: Program QSPI NOR flash: => sf probe 0:0 Load DPC image from the storage device => load mmc 0:2 80000000 <dpc image> For example: => load mmc 0:2 80000000 dpc.0x2A_0x41.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program DPC image to QSPI NOR flash: => sf erase 0x00E00000 +$filesize && sf write 0x80000000 0x00E00000 $filesize Address 0x00E00000 is the location of DPC image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Reset and boot from QSPI NOR flash: => reset Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored in QSPI NOR flash.
記事全体を表示
Follow these steps to update the composite firmware image in QSPI NOR flash. qixis_reset boots the board from QSPI NOR flash0 and qixis_reset altbank boots the board from QSPI NOR flash1. sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from QSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program QSPI NOR flash1. Obtaining composite firmware image  LSDK includes pre-built firmware images for QSPI NOR flash. The LSDK composite firmware includes RCW+PBI, boot loader firmware, DPAA1 FMan ucode, QE/uQE firmware, Ethernet PHY firmware, DPAA2 MC firmware, DPAA2 DPL, DPAA2 DPC, device tree, and lsdk_linux_<arch>.itb images. Refer the Layerscape Software Development Kit <version> Documention for the complete flash memory layout of the images.  On a Linux host machine, download composite firmware image from nxp.com.    $ wget http://www.nxp.com/lgfiles/sdk/lsdk<lsdk_version>/firmware_<RDB_name>_uboot_qspiboot.img  For example: For LS1088ARDB:  $ wget http://www.nxp.com/lgfiles/sdk/lsdk1809/firmware_ls1088ardb_uboot_qspiboot.img  For LS1088ARDB-PB:  $ wget https://www.nxp.com/lgfiles/sdk/lsdk1809/firmware_ls1088ardb_pb_uboot_qspiboot.img Flashing composite firmware images to QSPI NOR flash Boot LS1088ARDB/LS1088ARDB-PB from QSPI. Ensure that the switches are set to boot the board from QSPI. For booting from QSPI , SW1[1:8] + SW2[1] = 0011_0001_X Boot from QSPI NOR flash0: => qixis_reset For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:0 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 Composite firmware image can be loaded to the LS1088ARDB/LS1088ARDB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server   Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@qsgmii, DPMAC4@qsgmii, DPMAC5@qsgmii, DPMAC6@qsgmii, DPMAC7@qsgmii, DPMAC8@qsgmii, DPMAC9@qsgmii, DPMAC10@qsgmii Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LS1088ARDB/LS1088RDB-PB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@qsgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@qsgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@qsgmii device host 192.168.1.1 is alive   Load U-Boot image from the TFTP server Program QSPI NOR flash1: => sf probe 0:1 Flash LS1088ARDB or LS1088ARDB-PB composite firmware image: For LS1088ARDB: => tftp 0xa0000000 firmware_ls1088ardb_uboot_qspiboot.img => print filesize filesize=2351db0 For LS1088ARDB-PB: => tftp 0xa0000000 firmware_ls1088ardb_pb_uboot_qspiboot.img => print filesize filesize=2351db0 Program composite firmware image to QSPI NOR flash: => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:1 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:1 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash. Option 2: Load image from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 Program QSPI NOR flash1: => sf probe 0:1 Load composite firmware image from the storage device => load mmc 0:2 a0000000 <image name> => print filesize For example, for LS1088ARDB: => load mmc 0:2 a0000000 firmware_ls1088ardb_uboot_qspiboot.img => print filesize filesize=235bd40 For example, for LS1088ARDB-PB: => load mmc 0:2 a0000000 firmware_ls1088ardb_pb_uboot_qspiboot.img => print filesize filesize=2351db0 Or => load usb 0:2 a0000000 <image name> => print filesize Or => load scsi 0:2 a0000000 <image name> => print filesize Program image to QSPI NOR flash: => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Boot from QSPI NOR flash1: => qixis_reset altbank In boot log, you’ll see: For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:1 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:1 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.
記事全体を表示
ENETC is a PCI Integrated End Point(IEP). IEP implements peripheral devices in an SoC such that software sees them as PCIe device. ENETC is an evolution of BDR(Buffer Descriptor Ring) based networking IPs. Key goal of the DPDK is to provide a simple, complete framework for fast packet processing in data plane applications. Using the APIs provided as part of the framework, applications can leverage the capabilities of underlying network infrastructure.DPDK been prominent software in user space for networking applications pushes for eNetc driver to be written in user space. This document introduces overview of the NXP ENETC and how its driver is implemented and integrated into the DPDK. DPDK eNetc Driver support features queue start/stop, MTU update, promisc, Unicast and multicast MAC filtering, rss hash, crc offload, vlan offload, Rx checksum offload, basic stats. 1. ENETC Hardware Introduction 2. LS1028 Default ENETC Driver 3. User Space eNetc Driver design 4. DPDK eNetc Driver support features 5. Setup DPDK applications over ENETC platform
記事全体を表示
The table below shows the mapping of the Ethernet port names appearing on the front panel of the LS1046ARDB chassis with the port names in U-Boot, tinyDistro, and NXP LSDK userland.  Port name on chassis Port name in U-Boot Port name in Linux (tinyDistro) Port name in Linux (LSDK userland) RGMII1 FM1@DTSEC3 eth0 fm1-mac3 RGMII2 FM1@DTSEC4 eth1 fm1-mac4 SGMII1 FM1@DTSEC5 eth2 fm1-mac5 SGMII2 FM1@DTSEC6 eth3 fm1-mac6 10G Copper FM1@TGEC1 eth4 fm1-mac9 10G SEP+ FM1@TGEC2 eth5 fm1-mac10
記事全体を表示
Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Please note the steps listed in this topic can only be performed with LSDK 18.12 and newer releases.  Also the TF-A boot flow is applicable only for LS1088ARDB-PB. LS1088ARDB is not supported LSDK 18.12 release onwards. To migrate to the TF-A boot flow from the previous boot flow (with PPA), you need to compile the TF-A binaries, bl2_<boot_mode>.pbl and fip.bin, and flash these binaries on the specific boot medium on the board. For SD boot, you need to compile the following TF-A binaries. TF-A binary name Components bl2_sd.pbl BL2 binary: Platform initialization binary RCW binary for SD boot  fip.bin BL31: Secure runtime firmware BL32: Trusted OS, for example, OPTEE (optional) BL33: U-Boot/UEFI image Follow these steps to compile and deploy TF-A  binaries (bl2_sd.pbl and fip.bin) on the SD card. Compile PBL binary from RCW source file Compile U-Boot binary [Optional] Compile OPTEE binary  Compile TF-A binaries (bl2_sd.pbl and fip.bin) for SD boot Program TF-A binaries to the SD card Step 1: Compile PBL binary from RCW source file You need to compile the rcw_1600_sd.bin binary to build the bl2_sd.pbl binary. Clone the  rcw repository and compile the PBL binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12  $ cd ls1088ardb If required, make changes to the rcw files. $ make   The compiled PBL binary for SD boot on LS1088ARDB-PB, rcw_1600_sd.bin, is available at rcw/ls1088ardb/FCQQQQQQQQ_PPP_H_0x1d_0x0d/.   See the rcw/ls1088ardb/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. Step 2: Compile U-Boot binary You need to compile the u-boot.bin binary to build the fip.bin binary. Clone the u-boot repository and compile the U-Boot binary for TF-A. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12  $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make ls1088ardb_tfa_defconfig $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building the LSDK 18.12 U-Boot binary.  The compiled U-Boot binary, u-boot.bin, is available at u-boot/. Step 3: [Optional] Compile OPTEE binary  You need to compile the tee.bin binary to build fip.bin with OPTEE. However, OPTEE is optional, you can skip the procedure to compile OPTEE if you want to build the FIP binary without OPTEE. Clone the optee_os repository and build the OPTEE binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/optee_os $ cd optee_os $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make CFG_ARM64_core=y PLATFORM=ls-ls1088ardb $ aarch64-linux-gnu-objcopy -v -O binary out/arm-plat-ls/core/tee.elf out/arm-plat-ls/core/tee.bin The compiled OPTEE image, tee.bin, is available at optee_os/out/arm-plat-ls/core/. Step 4: Compile TF-A binaries for SD boot Clone the atf repository and compile the TF-A binaries, bl2_sd.pbl and fip.bin. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf $ cd atf $  git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- Build BL2 binary with OPTEE. $ make PLAT=ls1088ardb bl2 SPD=opteed BOOT_MODE=sd pbl RCW=<path_to_rcw_binary>/rcw_1600_sd.bin The compiled BL2 images, bl2.bin and bl2_sd.pbl are available at atf/build/ls1088ardb/release/. For any update in the BL2 source code or RCW binary, the bl2_sd.pbl binary needs to be recompiled. To compile the BL2 binary without OPTEE: $ make PLAT=ls1088ardb bl2 BOOT_MODE=sd pbl RCW=<path_to_rcw_binary>/rcw_1600_sd.bin Build FIP binary with OPTEE and without trusted board boot. $ make PLAT=ls1088ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed BL32=<path_to_optee_binary>/tee.bin The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/ls1088ardb/release/. For any update in the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled. To compile the FIP binary without OPTEE and without trusted board boot: $ make PLAT=ls1088ardb fip BOOT_MODE=sd BL33=<path_to_u-boot_binary>/u-boot.bin To compile the FIP binary with trusted board boot, refer the read me at <atf repository>/plat/nxp/README.TRUSTED_BOOT Step 5: Program TF-A binaries to SD card Boot LS1088ARDB-PB from QSPI. Ensure that the switches are set to boot the board from QSPI. For booting from QSPI , SW1[1:8] + SW2[1] = 0011_0001_X Boot from QSPI NOR flash0: => qixis_reset For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 Please ensure that you are using LS1088ARDB-PB to flash the TF-A binaries, as LS1088ARDB is not supported LSDK 18.12 release onwards.   Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@qsgmii, DPMAC4@qsgmii, DPMAC5@qsgmii, DPMAC6@qsgmii, DPMAC7@qsgmii, DPMAC8@qsgmii, DPMAC9@qsgmii, DPMAC10@qsgmii Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS1088ARDB/LS1088RDB-PB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@qsgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@qsgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@qsgmii device host 192.168.1.1 is alive   Load TF-A binaries from the TFTP server For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow. Flash bl2_sd.pbl: => tftp 82000000 bl2_sd.pbl => mmc write 82000000 8 <blk_cnt> Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load bl2_sd.pbl from the TFTP server, if the bytes transferred is 82809 (14379 hex), then blk_cnt is calculated as 82809/512 = 161 (A1 hex). For this example, mmc write command will be: => mmc write 82000000 8 A1 Flash fip.bin: => tftp 82000000 fip.bin => mmc write 82000000 800 <blk_cnt> Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load fip.bin from the TFTP server, if the bytes transferred is 1077157 (106fa5 hex), then blk_cnt is calculated as 1077157/512 = 2103 (837 hex). For this example, mmc write command will be: => mmc write 82000000 800 837 Boot from SD card: => qixis_reset sd LS1088ARDB-PB will boot with TF-A. In the boot log, you will see: NOTICE: UDIMM 18ASF1G72AZ-2G6B1 NOTICE: 8 GB DDR4, 64-bit, CL=15, ECC on, CS0+CS1 NOTICE: BL2: v1.5(release):LSDK-18.12 NOTICE: BL2: Built : 11:57:03, Dec 23 2018 NOTICE: BL31: v1.5(release):LSDK-18.12 NOTICE: BL31: Built : 15:21:44, Feb 11 2019 NOTICE: Welcome to LS1088 BL31 Phase For steps to deploy TF-A binaries in QSPI NOR flash, see LS1088ARDB-PB - How to deploy TF-A binaries in QSPI NOR flash
記事全体を表示
boot loader requirements to boot Kernel ARM64 Virtual Memory Layout ARM64 IRQ Vectors Setup FDT Mapping ARM64 Kernel booting process        5.1 Prior to start_kernel              5.1.1__create_page_tables              5.1.2 __cpu_setup              5.1.3 __primary_switch       5.2 Start_kernel             5.2.1 Start_kernel -> setup_arch                     5.2.1.1 Start_kernel -> setup_arch -> setup_machine_fdt                     5.2.1.2 Start_kernel -> setup_arch -> paging_init / bootmem_init                     5.2.1.3 Start_kernel -> setup_arch -> psci_init             5.2.2 Start_kernel -> Rest_init                      5.2.2.1 Start_kernel -> Rest_init -> kernel_init
記事全体を表示
To boot a Layerscape board with an empty DPL file: Create an empty DPL file, content.dts. For example: /dts-v1/; / { dpl-version = <0x0000000a>; containers { dprc@1 { compatible = "fsl,dprc"; parent = "none"; options = "DPRC_CFG_OPT_SPAWN_ALLOWED", "DPRC_CFG_OPT_ALLOC_ALLOWED", "DPRC_CFG_OPT_IRQ_CFG_ALLOWED"; objects { obj_set@dpmcp { type = "dpmcp"; ids = <0x1 0x2 0x3 0x4 0x5 0x6 0x7 0x8 0x9 0xa 0xb 0xc 0xd>; }; }; }; }; objects { dpmcp@1 { compatible = "fsl,dpmcp"; }; dpmcp@2 { compatible = "fsl,dpmcp"; }; dpmcp@3 { compatible = "fsl,dpmcp"; }; dpmcp@4 { compatible = "fsl,dpmcp"; }; dpmcp@5 { compatible = "fsl,dpmcp"; }; dpmcp@6 { compatible = "fsl,dpmcp"; }; dpmcp@7 { compatible = "fsl,dpmcp"; }; dpmcp@8 { compatible = "fsl,dpmcp"; }; dpmcp@9 { compatible = "fsl,dpmcp"; }; dpmcp@10 { compatible = "fsl,dpmcp"; }; dpmcp@11 { compatible = "fsl,dpmcp"; }; dpmcp@12 { compatible = "fsl,dpmcp"; }; dpmcp@13 { compatible = "fsl,dpmcp"; }; dpmcp@14 { compatible = "fsl,dpmcp"; }; dpmcp@15 { compatible = "fsl,dpmcp"; }; dpmcp@16 { compatible = "fsl,dpmcp"; }; dpmcp@17 { compatible = "fsl,dpmcp"; }; dpmcp@18 { compatible = "fsl,dpmcp"; }; dpmcp@19 { compatible = "fsl,dpmcp"; }; }; }; ​ Note: There is no network object capable of receiving Ethernet frames in the DPL file. You can create more dpmcps if the number of objects that will be created dynamically is high. Generate the DPL file using content.dts. dtc -I dts -O dtb -o dpl.dtb content.dts​ Flash the DPL file, dpl.dtb to the alternate bank.  tftp 0x80000000 dpl.dtb; i2c mw 66 50 20;sf probe; sf erase 0x00D00000 +$filesize && sf write 0x80000000 0x00D00000 $filesize​ Boot the board. After the board boots, create a dpmac. (Make sure you create a DPMAC that is valid based on the selected SERDES protocol configured by the RCW). restool dpmac create --mac-id=3​ Probe the dpmac driver. restool dprc assign dprc.1 --object=dpmac.3 --plugged=1​ Create a network interface. ls-addni dpmac.3​ Save contents as content_new.dts. restool dprc generate-dpl dprc.1 > content_new.dts​    
記事全体を表示
The attached patch is to support DDR3L in LS1043A. The SDK version is Linux-LS1043A-SDK-V0.5-SOURCE-20151223-yocto.iso. Not SDK2.0. The DDR3L part number is two Winbond W632GU6KB(16M x 8 banks x 16 bits DDR3L SDRAM).
記事全体を表示
PPS (Pulses Per Second) signal applies to most network controllers of Layerscape, including DPAA1 platforms. PPS signal is output through 1588 timer pulse out pin. The QorIQ PTP driver configured fixed interval period pulse (FIPER) generator as PPS signal in default. This document describes how to create dts file to customize configuration on the 1588 timer such as selecting other reference clock source, and configuring nominal clock period, FIPERs period, and output clock period to generate the required PPS signal.
記事全体を表示
Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Please note the steps listed in this topic can only be performed with LSDK 18.12 and newer releases.  Also the TF-A boot flow is applicable only for LS1088ARDB-PB. LS1088ARDB is not supported LSDK 18.12 release onwards. To migrate to the TF-A boot flow from the previous boot flow (with PPA), you need to compile the TF-A binaries, bl2_<boot_mode>.pbl and fip.bin, and flash these binaries on the specific boot medium on the board. For QSPI NOR flash boot, you need to compile the following TF-A binaries. TF-A binary name Components bl2_qspi.pbl BL2 binary: Platform initialization binary RCW binary for QSPI NOR flash fip.bin BL31: Secure runtime firmware BL32: Trusted OS, for example, OPTEE (optional) BL33: U-Boot/UEFI image Follow these steps to compile and deploy TF-A  binaries (bl2_qspi.pbl and fip.bin) in QSPI NOR flash. Compile PBL binary from RCW source file Compile U-Boot binary [Optional] Compile OPTEE binary  Compile TF-A binaries (bl2_qspi.pbl and fip.bin) for QSPI NOR flash Program TF-A binaries to QSPI NOR flash Step 1: Compile PBL binary from RCW source file  You need to compile the rcw_1600_qspi.bin binary to build the bl2_qspi.pbl binary. Clone the  rcw repository and compile the PBL binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12  $ cd ls1088ardb If required, make changes to the rcw files. $ make   The compiled PBL binary for QSPI NOR flash on LS1088ARDB-PB, rcw_1600_qspi.bin, is available at rcw/ls1088ardb/FCQQQQQQQQ_PPP_H_0x1d_0x0d/.   See the rcw/ls1088ardb/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. Step 2: Compile U-Boot binary You need to compile the u-boot.bin binary to build the fip.bin binary. Clone the u-boot repository and compile the U-Boot binary for TF-A. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12  $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make ls1088ardb_tfa_defconfig $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.12 U-Boot binary.  The compiled U-Boot image, u-boot.bin, is available at u-boot/. Step 3: [Optional] Compile OP-TEE binary You need to compile the tee.bin binary to build fip.bin with OPTEE. However, OPTEE is optional, you can skip the procedure to compile OPTEE if you want to build the FIP binary without OPTEE. Clone the optee_os repository and build the OPTEE binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/optee_os $ cd optee_os $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make CFG_ARM64_core=y PLATFORM=ls-ls1088ardb $ aarch64-linux-gnu-objcopy -v -O binary out/arm-plat-ls/core/tee.elf out/arm-plat-ls/core/tee.bin The compiled OPTEE image, tee.bin, is available at optee_os/out/arm-plat-ls/core/. Step 4: Compile TF-A binaries for QSPI NOR flash Clone the atf repository and compile the TF-A binaries, bl2_qspi.pbl and fip.bin. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf $ cd atf $  git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- Build BL2 binary with OPTEE. $ make PLAT=ls1088ardb bl2 SPD=opteed BOOT_MODE=qspi pbl RCW=<path_to_rcw_binary>/rcw_1600_qspi.bin The compiled BL2 binaries, bl2.bin and bl2_qspi.pbl are available at atf/build/ls1088ardb/release/. For any update in the BL2 source code or RCW binary, the bl2_qspi.pbl binary needs to be recompiled. To compile the BL2 binary without OPTEE: make PLAT=ls1088ardb bl2 BOOT_MODE=qspi pbl RCW=<path_to_rcw_binary>/rcw_1600_qspi.bin Build FIP binary with OPTEE and without trusted board boot. $ make PLAT=ls1088ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed BL32=<path_to_optee_binary>/tee.bin The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/ls1088ardb/release/. For any update in the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled. To compile the FIP binary without OPTEE and without trusted board boot: make PLAT=ls1088ardb fip BOOT_MODE=sd BL33=<path_to_u-boot_binary>/u-boot.bin To compile the FIP binary with trusted board boot, refer the read me at <atf repository>/plat/nxp/README.TRUSTED_BOOT Step 5: Program TF-A binaries to QSPI NOR flash Boot LS1088ARDB-PB from QSPI. Ensure that the switches are set to boot the board from QSPI. For booting from QSPI , SW1[1:8] + SW2[1] = 0011_0001_X Boot from QSPI NOR flash0: => qixis_reset For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 Please ensure that you are using LS1088ARDB-PB to flash the TF-A binaries, as LS1088ARDB is not supported LSDK 18.12 release onwards. Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@qsgmii, DPMAC4@qsgmii, DPMAC5@qsgmii, DPMAC6@qsgmii, DPMAC7@qsgmii, DPMAC8@qsgmii, DPMAC9@qsgmii, DPMAC10@qsgmii Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LS1088ARDB/LS1088RDB-PB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@qsgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@qsgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@qsgmii device host 192.168.1.1 is alive   Load TF-A binaries from the TFTP server For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow. Program QSPI NOR flash1: => sf probe 0:1 Flash bl2_qspi.pbl: => tftp 0xa0000000 bl2_qspi.pbl => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Flash fip.bin: => tftp 0xa0000000 fip.bin => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize Boot from QSPI NOR flash1: => qixis_reset altbank LS1088ARDB-PB will boot with TF-A. In the boot log, you will see: => NOTICE: UDIMM 18ASF1G72AZ-2G6B1 NOTICE: 8 GB DDR4, 64-bit, CL=15, ECC on, CS0+CS1 NOTICE: BL2: v1.5(release):LSDK-18.12 NOTICE: BL2: Built : 16:23:18, Feb 8 2019 NOTICE: BL31: v1.5(release):LSDK-18.12 NOTICE: BL31: Built : 16:25:08, Feb 8 2019 NOTICE: Welcome to LS1088 BL31 Phase For steps to deploy TF-A binaries on SD card, see LS1088ARDB-PB - How to deploy TF-A binaries on SD card
記事全体を表示
How to bring up a card when the flash is blank, or the image is corrupted. How to boot cards from various boot mode when changed the RCW as requirements. This documentation will use LS1046ARDB as new board to realize the functions (all target board in the document is LS1046ARDB). Content Bring up LS1046A with CodeWarrior TAP Boot up from the SD card Compile PBL binary from RCW source file Compile the PBL binary into firmware Program the firmware into the target board (LS1046ARDB) Boot up from the QSPI Compile firmware from RCW source file Program the firmware into the target board (LS1046ARDB) Boot up from the eMMC Enable the on board eMMC Compile firmware from RCW source file Program the firmware into the target board (LS1046ARDB)
記事全体を表示
This topic shows steps to customize LITB by using a different kernel image instead of the existing kernel image. Browse to the FlexBuild installation directory. Modify the kernel image in linux_arm64_LS.its. $ vi configs/linux/linux_arm64_LS.its linux_arm64_LS.png Save the changes done in the file. Generate LITB using flex-builder. $ source setup.env $ flex-builder -i mkitb -r <distro_type>:<distro_scale> -a <arch> For example: $ source setup.env $ flex-builder -i mkitb -r ubuntu:main -a arm64 INSTRUCTION: mkitb DISTRO TYPE: ubuntu DISTRO SCALE: main .... .... /home/flexbuild_lsdk2004/build/images/lsdk2004_ubuntu_main_LS_arm64.itb [Done]   Note: To create .itb file directly from .its file, run this command: mkimage -f <xyz.its> <xyz.itb> Connect to the board console via terminal and run following commands at U-boot to boot the board with customized LITB. => ping $serverip Using e1000#0 device host 192.168.3.1 is alive => Using e1000#0 device host 192.168.3.1 is alive => tftp 0xa0000000 lsdk2004_ubuntu_main_LS_arm64.itb Using e1000#0 device TFTP from server 192.168.3.1; our IP address is 192.168.3.49 Filename 'lsdk2004_ubuntu_main_LS_arm64.itb'. Load address: 0xa0000000 Loading: ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# #################################### 9.8 MiB/s done Bytes transferred = 683506200 (28bd7a18 hex) => bootm 0xa0000000#lx2160ardb ## Loading kernel from FIT Image at a0000000 ... Using 'lx2160ardb' configuration Trying 'kernel' kernel subimage Description: ARM64 Kernel Created: 2021-02-03 6:01:29 UTC Type: Kernel Image Compression: gzip compressed Data Start: 0xa00000d0 Data Size: 14086432 Bytes = 13.4 MiB   Check timestamp in boot log to ensure that the board is booted with the updated kernel image in the customized LITB.   Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd083] [ 0.000000] Linux version 5.4.3 (test@Ubuntu-18) (gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04)) #1 SMP PREEMPT Wed Feb 3 00:04:09 IST 2021 [ 0.000000] Machine model: NXP Layerscape LX2160ARDB [ 0.000000] earlycon: pl11 at MMIO32 0x00000000021c0000 (options '') [ 0.000000] printk: bootconsole [pl11] enabled [ 0.000000] efi: Getting EFI parameters from FDT:  
記事全体を表示
DPDK(Data Plane Development Kit) provides a simple, complete framework for fast packet processing in data plane applications. This IPsec security gateway application demonstrates the implementation of a security gateway using DPDK cryptodev framework with crypto protocol offloading support. This document introduces DPDK IPsec gateway application architecture, DPAA2 SEC driver and ipsec-secgw application implementation for crypto protocol offloading, running ipsec-secgw application on LS2088ARDB.
記事全体を表示
Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images in QSPI NOR flash. qixis_reset boots the board from QSPI NOR flash0 and qixis_reset altbank boots the board from QSPI NOR flash1. sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from QSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program QSPI NOR flash1. Obtaining MC firmware Clone the qoriq-mc-binary repository. $ git clone https://github.com/NXP/qoriq-mc-binary.git $ cd qoriq-mc-binary/ls1088a/ $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09 The prebuilt MC firmware image, mc_10.10.0_ls1088a_20180814.itb, is available at /qoriq-mc-binary/ls1088a/. Note that the name of the MC firmware image may vary depending on the release version used.  Obtaining DPC and DPL images Clone the mc-utils repository and compile the DPC and DPL images. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils $ cd mc-utils $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09 If required, make changes to the DPC and DPL files. $ make -C config/ The compiled dpc.0x1D-0x0D.dtb and dpl-eth.0x1D_0x0D.dtb images are available at /mc-utils/config/ls1088a/RDB/. Note that the name of the DPC and DPL images may vary depending on the release version used.  Flashing MC firmware, DPC, and DPL images to QSPI NOR flash Boot LS1088ARDB/LS1088ARDB-PB from QSPI. Ensure that the switches are set to boot the board from QSPI, SW1[1:8] + SW2[1] = 0011_0001_X Boot from QSPI NOR flash0: => qixis_reset For example: For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:0 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 The images can be loaded to the LS1088ARDB/LS1088ARDB-PB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@qsgmii, DPMAC4@qsgmii, DPMAC5@qsgmii, DPMAC6@qsgmii, DPMAC7@qsgmii, DPMAC8@qsgmii, DPMAC9@qsgmii, DPMAC10@qsgmii Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LS1088ARDB/LS1088RDB-PB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@qsgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@qsgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@qsgmii device host 192.168.1.1 is alive Load images from a TFTP server Program QSPI NOR flash1: sf probe 0:1 Flash MC firmware: => tftp 0x80000000 mc_10.10.0_ls1088a_20180814.itb => print filesize => sf erase 0xa00000 +$filesize && sf write 0x80000000 0xa00000 $filesize Address 0xa00000 is the location of MC firmware in QSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPC image: => tftp 0x80000000 dpc.0x1D-0x0D.dtb => print filesize  => sf erase 0xe00000 +$filesize && sf write 0x80000000 0xe00000 $filesize Address 0xe00000 is the location of DPC image in QSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image: => tftp 0x80000000 dpl-eth.0x1D_0x0D.dtb => print filesize  => sf erase 0xd00000 +$filesize && sf write 0x80000000 0xd00000 $filesize Address 0xd00000 is the location of DPL image in QSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:0 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash. Option 2: Load images from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on the storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 Program QSPI NOR flash1: => sf probe 0:1 Flash MC firmware: Load MC firmware image from the storage device => load mmc 0:2 80000000 <mc firmware> For example: => load mmc 0:2 80000000 mc_10.10.0_ls1088a_20180814.itb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program MC firmware image to QSPI NOR flash: => sf erase 0xa00000 +$filesize && sf write 0x80000000 0xa00000 $filesize  Address 0xa00000 is the location of MC firmware in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image: Load DPL image from the storage device => load mmc 0:2 80000000 <dpl image> For example: => load mmc 0:2 80000000 dpl-eth.0x1D_0x0D.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program DPL image to QSPI NOR flash: => sf erase 0xd00000 +$filesize && sf write 0x80000000 0xd00000 $filesize  Address 0xd00000 is the location of DPL image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPC image: Load DPC image from the storage device => load mmc 0:2 80000000 <dpc image> For example: => load mmc 0:2 80000000 dpc.0x1D-0x0D.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program DPC image to QSPI NOR flash: => sf erase 0xe00000 +$filesize && sf write 0x80000000 0xe00000 $filesize Address 0xe00000 is the location of DPC image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:1 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:1 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.
記事全体を表示
Follow these steps to update the DPAA1 FMan ucode image in NOR flash.  cpld reset boots the board from NOR bank 0 and cpld reset altbank boots the board from the NOR bank  4.  0x64000000 is the location of RCW in the alternate NOR bank, that is NOR bank 4.  0x60000000 is the location of RCW in the NOR bank 0.   Obtaining DPAA1 FMan ucode image Clone the qoriq-fm-ucode repository. $ git clone https://github.com/NXP/qoriq-fm-ucode.git $ cd qoriq-fm-ucode $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-19.06 The prebuilt FMan ucode images, fsl_fman_ucode_ls1043_r1.1_<microcode version>.bin, are at qoriq-fm-ucode/. In the binary file, ls1043_r1.1 refers to the LS1043A silicon revision 1.1. See qoriq-fm-ucode/readme for a description of the ucode version numbers. Programming FMan ucode image to NOR flash FMan ucode image can be loaded to LS1043ARDB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server Boot LS1043ARDB from NOR flash. Ensure that the switches are set to boot the board from NOR bank 0. For booting from NOR bank 0, switch settings are as follows: SW3[1:8] = 10110011 SW4[1:8] = 00010010 SW5[1:8] = 10100010 Boot from NOR bank 0: => cpld reset For LS1043ARDB, in boot log, you'll see: Board: LS1043ARDB, boot from vBank 0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5 Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS1043ARDB Ethernet and FMC port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime FM1@DTSEC4 => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact FM1@DTSEC4 Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using FM1@DTSEC4 device host 192.168.1.1 is alive Load FMan ucode image from the TFTP server Load FMan ucode image in DDR memory: => tftp a0000000 <path to FMan ucode>/fsl_fman_ucode_ls1043_r1.1_<ucode version>.bin Program the FMan ucode image to NOR bank 4: => erase 64900000 +$filesize && cp.b a0000000 64900000 $filesize Address  0x64900000 is the location of the FMan ucode image in NOR bank 4.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from NOR bank 4 and press Enter to stop the autoboot: => cpld reset altbank In boot log, you’ll see: Board: LS1043ARDB, boot from vBank 4 You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image in NOR bank 4 is updated. Fman1: Uploading microcode version 106.4.18 Ensure that SD card, USB flash drive, or SCSI hard disk installed with NXP LSDK userland is plugged into the board to boot the board to the LSDK userland.  => cpld reset altbank NXP LSDK 1906 main localhost login: root [ OK ] Stopped Serial Getty on ttyS0. [ OK ] Started Serial Getty on ttyS0. NXP LSDK 1906 main localhost login: root Password: Last login: Fri Feb 22 04:29:12 UTC 2019 on ttyS0 Welcome to NXP LSDK 1906 main (GNU/Linux 4.19.46 aarch64) * Support: https://www.nxp.com/lsdk * Documentation: https://lsdk.github.io/document * Licensing: https://lsdk.github.io/eula root@localhost:~# Option 2: Load image from partition on mass storage device (SD, USB, or SATA) Boot LS1043ARDB from NOR flash. Ensure that the switches are set to boot the board from NOR bank 0. For booting from NOR bank 0, switch settings are as follows: SW3[1:8] = 10110011 SW4[1:8] = 00010010 SW5[1:8] = 10100010 Boot from NOR bank 0: => cpld reset   For LS1043ARDB, in boot log, you'll see: Board: LS1043ARDB, boot from vBank 0 Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on storage device => ls mmc <device:partition> For example: => ls mmc 0:3 System Volume Information/ 32604 fsl_fman_ucode_ls1043_r1.1_106_4_18.bin 1 file(s), 1 dir(s) Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 If the ls command fails to run, check that U-Boot in NOR bank 0 supports the command by typing ls at the U-Boot prompt: => ls ls - lists files in a directory (default) Usage: ls <interface> [<dev[:part]> [directory]] - Lists files in directory [directory] of partition [part] on device type [interface] and instance [dev]. If U-Boot does not support this command, then update the composite firmware image in NOR bank 0. For steps to update composite firmware image in NOR flash, see Layerscape Software Development Kit User Guide. Load FMan ucode image from the storage device. => load mmc <device:partition> 80000000 <image name> => print filesize For example: => load mmc 0:3 80000000 fsl_fman_ucode_ls1043_r1.1_106_4_18.bin 32604 bytes read in 18 ms (1.8 MiB/s) => print filesize filesize=7f5c Or => load usb <device:partition> 80000000 <image name> => print filesize Or => load scsi <device:partition> 80000000 <image name> => print filesize Program the FMan ucode image to NOR bank 4: => erase 64900000 +$filesize && cp.b 80000000 64900000 $filesize Address  0x64900000 is the location of the FMan ucode image in NOR bank 4.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from NOR bank 4 and press Enter to stop the autoboot: => cpld reset altbank In boot log, you’ll see: Board: LS1043ARDB, boot from vBank 4 You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image in NOR bank 4 is updated. Fman1: Uploading microcode version 106.4.18 Ensure that SD card, USB flash drive, or SCSI hard disk installed with NXP LSDK userland is plugged into the board to boot the board to the LSDK userland.  => cpld reset altbank NXP LSDK 1906 main localhost login: root [ OK ] Stopped Serial Getty on ttyS0. [ OK ] Started Serial Getty on ttyS0. NXP LSDK 1906 main localhost login: root Password: Last login: Fri Feb 22 04:29:12 UTC 2019 on ttyS0 Welcome to NXP LSDK 1906 main (GNU/Linux 4.19.46 aarch64) * Support: https://www.nxp.com/lsdk * Documentation: https://lsdk.github.io/document * Licensing: https://lsdk.github.io/eula root@localhost:~#
記事全体を表示
Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images in NOR flash. qixis_reset boots the board from NOR bank 0 and qixis_reset altbank boots the board from NOR bank 4. Obtaining MC firmware Clone the qoriq-mc-binary repository. $ git clone https://github.com/NXP/qoriq-mc-binary.git $ cd qoriq-mc-binary/ls2088a/ $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 The prebuilt MC firmware image, mc_10.18.0_ls2088a.itb, is available at /qoriq-mc-binary/ls2088a/. Note that the name of the MC firmware image may vary depending on the release version used.  Obtaining DPC and DPL images Clone the mc-utils repository and compile the DPC and DPL images. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils $ cd mc-utils $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 If required, make changes to the DPC and DPL files. $ make -C config/ The compiled dpc.0x2A_0x41.dtb and  dpl-eth.0x2A_0x41.dtb images are available at /mc-utils/config/ls2088a/RDB/. Note that the name of the DPC and DPL images may vary depending on the release version used.  Flashing MC firmware, DPC, and DPL images to NOR flash Boot LS2088ARDB from NOR flash. Ensure that the switches are set to boot the board from NOR bank 0. For booting from NOR bank 0, switch settings are as follows:         SW5[1:8] = 1111 1111      SW3[1:8] = 0001 0010      SW4[1:8] = 1111 1111      SW6[1:8] = 1111 1111      SW7[1:8] = 0100 0010      SW9[1:8] = 0100 0000      SW8[1:8] = 0111 1111     In addition to the above switch settings, make sure the following jumper settings are correct (for RDB Rev E and later) J14 = 1-2, for NOR boot Boot from NOR bank 0: => qixis_reset   For LS2088ARDB, in boot log, you'll see: Board: LS2088AE Rev1.1-RDB, Board Arch: V1, Board version: F, boot from vBank: 0 The images can be loaded to the LS2088ARDB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@xgmii, DPMAC6@xgmii, DPMAC7@xgmii, DPMAC8@xgmii    Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1>    Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS2088ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.                                                                       => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC1@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC1@xgmii    Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp    Save the settings. => saveenv    Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC1@xgmii device host 192.168.1.1 is alive Load images from a TFTP server Flash MC firmware to NOR bank 4 (after booting from NOR bank 0): => tftp 0x80000000 mc_10.18.0_ls2088a.itb => print filesize => erase 0x584A00000 +$filesize;cp.b 80000000 0x584A00000 $filesize Address 0x584A0000 is the location of MC firmware in alternate NOR bank. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image to NOR bank 4 (after booting from NOR bank 0): => tftp 0x80000000 dpl-eth.0x2A_0x41.dtb => print filesize  => erase 0x584D00000 +$filesize;cp.b 80000000 0x584D00000 $filesize Address 0x584D00000 is the location of DPL image in alternate NOR bank. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPC image to NOR bank 4 (after booting from NOR bank 0): => tftp 0x80000000 dpc.0x2A_0x41.dtb => print filesize  => erase 0x584E00000 +$filesize;cp.b 80000000 0x584E00000 $filesize Address 0x584E00000 is the location of DPC image in alternate NOR bank. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from NOR bank 4: => qixis_reset altbank Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored in NOR flash. Option 2: Load images from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on the storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 If the ls command fails to run, check that U-Boot in NOR bank 0 supports the command by typing ls at the U-Boot prompt: => ls ls - Lists files in a directory (default) Usage: ls <interface> [<dev[:part]> [directory]] - Lists files in directory [directory] of partition [part] on device type [interface] and instance [dev]. If U-Boot does not support this command, then update the composite firmware image in NOR bank 0. For steps to update composite firmware image in NOR bank, see Layerscape Software Development Kit User Guide . Use the following command if the SD card is formatted/created using LSDK flex-installer command: => load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: => load mmc 0:2 $load_addr mc_10.18.0_ls2088a.itb Use the following command if the SD card is formatted/created on a Windows PC: => fatload <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: => fatload mmc 0:2 $load_addr mc_10.18.0_ls2088a.itb Use the following command if the SD card is formatted/created on a Linux PC: => ext2load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: =>ext2load mmc 0:2 $load_addr mc_10.18.0_ls2088a.itb Also note that LSDK flex-installer command puts the images on the IInd partition, so 0:2 is used in the load command. If the SD card is formatted on Windows PC or Linux PC for single partition only, then 0 should be used instead of 0:2 in the fatload/ext2load command. Flash MC firmware: Load MC firmware image from the storage device => load mmc 0:2 80000000 <mc firmware> For example: => load mmc 0:2 80000000 mc_10.18.0_ls2088a.itb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program MC firmware image to NOR bank 4 (after booting from NOR bank 0): => erase 0x584A00000 +$filesize;cp.b 80000000 0x584A00000 $filesize  Address 0x584A00000 is the location of MC firmware in alternate NOR bank.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image: Load DPL image from the storage device => load mmc 0:2 80000000 <dpl image> For example: => load mmc 0:2 80000000 dpl-eth.0x2A_0x41.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program DPL image to NOR bank 4 (after booting from NOR bank 0): => erase 0x584D00000 +$filesize;cp.b 80000000 0x584D00000 $filesize Address 0x584D00000 is the location of DPL image in alternate NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPC image: Load DPC image from the storage device => load mmc 0:2 80000000 <dpc image> For example: => load mmc 0:2 80000000 dpc.0x2A_0x41.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program DPC image to NOR bank 4 (after booting from NOR bank 0): => erase 0x584E00000 +$filesize;cp.b 80000000 0x584E00000 $filesize Address 0x584E00000 is the location of DPC image in alternate NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from NOR bank 4: => qixis_reset altbank Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored in NOR flash.
記事全体を表示
CMSIS-DAP is a useful tool and exists in some NXP reference boards, but how to use it. This document describes the steps how to use the CMSIS-DAP in the LS1034ARDB as a reference for user.
記事全体を表示
In the U-Boot log, the names of the Ethernet interfaces are printed in the format <name>@<interface type>, for example, DPMAC2@xgmii. DPMAC is a DPAA2 object that identifies the physical interface.  For Linux, in TinyDistro as well as in Ubuntu distribution, by default, only one MAC is enabled as a standard Kernel Ethernet Interface. This interface is named eth0 by default (or eth1 if PCI Express network interface card is discovered first). For details regarding creation of a DPAA2 network interface (DPNI) in Linux, see "LSDK Quick Start Guide for LS2088ARDB -> Bringing up DPAA2 network interfaces" in Layerscape Software Development Kit User Guide. The table below shows the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux for LS2088ARDB.  In Linux, the mapping of Ethernet port names is not strict. The port names are mapped based on the order in which the Ethernet interfaces are created. As an example, consider a DPL file which defines only one DPMAC object, DPMAC3. When Linux starts, if a net device is created using DPMAC3, it will be labeled eth1 (assuming PCIe interface is eth0). Port name on chassis Port name in U-Boot Port name in Linux (tinyDistro and Ubuntu userland) Description ETH0  DPMAC5@xgmii eth0 by default (or eth1 if PCI Express network interface card is discovered first) XFI copper interface ETH1 DPMAC6@xgmii not enabled by default XFI copper interface ETH2 DPMAC7@xgmii not enabled by default XFI copper interface ETH3 DPMAC8@xgmii not enabled by default XFI copper interface ETH4 DPMAC1@xgmii not enabled by default XFI copper interface ETH5 DPMAC2@xgmii not enabled by default XFI copper interface ETH6 DPMAC3@xgmii not enabled by default XFI copper interface ETH7 DPMAC4@xgmii not enabled by default XFI copper interface
記事全体を表示
Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. In LS2088ARDB, Boot option switching between parallel NOR boot and QSPI NOR boot cannot be performed using commands. Boot option switching can be done by adjusting DIP switch settings and jumper settings on the Reference Design Board. For details, see Layerscape Software Development Kit User Guide.                        To migrate to the TF-A boot flow from the previous boot flow (with PPA), you need to compile the TF-A binaries, bl2_<boot_mode>.pbl and fip.bin, and flash these binaries on the specific boot medium on the board. For QSPI NOR flash boot, you need to compile the following TF-A binaries. TF-A binary name Components bl2_qspi.pbl BL2 binary: Platform initialization binary RCW binary for QSPI NOR flash fip.bin BL31: Secure runtime firmware BL32: Trusted OS, for example, OPTEE (optional) BL33: U-Boot/UEFI image Follow these steps to compile and deploy TF-A  binaries (bl2_qspi.pbl and fip.bin) in QSPI NOR flash. Compile RCW binary  Compile U-Boot binary [Optional] Compile OPTEE binary  Compile TF-A binaries (bl2_qspi.pbl and fip.bin) for QSPI NOR flash Program TF-A binaries to QSPI NOR flash Step 1: Compile RCW binary You need to compile the rcw_2000_qspi.bin binary to build the bl2_qspi.pbl binary. Clone the  rcw repository and compile the PBL binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09  $ cd ls2088ardb If required, make changes to the rcw files. $ make The compiled PBL binary for QSPI NOR flash on LS2088ARDB, rcw_2000_qspi.bin, is available at  rcw/ls2088ardb/FFFFFFFF_PP_HH_0x2a_0x41 See the rcw/ls2088ardb/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. Step 2: Compile U-Boot binary You need to compile the u-boot.bin binary to build the fip.bin binary. Clone the u-boot repository and compile the U-Boot binary for TF-A. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make ls2088ardb_tfa_defconfig $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.12 and onwards U-Boot binary.  The compiled U-Boot image, u-boot.bin, is available at u-boot/. Step 3: [Optional] Compile OP-TEE binary You need to compile the tee.bin binary to build fip.bin with OPTEE. However, OPTEE is optional, you can skip the procedure to compile OPTEE if you want to build the FIP binary without OPTEE. Clone the optee_os repository and build the OPTEE binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/optee_os $ cd optee_os $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make CFG_ARM64_core=y PLATFORM=ls-ls2088ardb $ aarch64-linux-gnu-objcopy -v -O binary out/arm-plat-ls/core/tee.elf out/arm-plat-ls/core/tee.bin The compiled OPTEE image, tee.bin, is available at optee_os/out/arm-plat-ls/core/. Step 4: Compile TF-A binaries for QSPI NOR flash Clone the atf repository and compile the TF-A binaries, bl2_qspi.pbl and fip.bin. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf $ cd atf $  git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- Build BL2 binary with OPTEE. $ make PLAT=ls2088ardb bl2 SPD=opteed BOOT_MODE=qspi BL32=<path_to_optee_binary>/tee.bin pbl RCW=<path_to_rcw_binary>/rcw_2000_qspi.bin The compiled BL2 binaries, bl2.bin and bl2_qspi.pbl are available at atf/build/ls2088ardb/release/. For any update in the BL2 source code or RCW binary, the bl2_qspi.pbl binary needs to be recompiled. To compile the BL2 binary without OPTEE: make PLAT=ls2088ardb bl2 BOOT_MODE=qspi pbl RCW=<path_to_rcw_binary>/rcw_2000_qspi.bin               Build FIP binary with OPTEE and without trusted board boot. $ make PLAT=ls2088ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed BL32=<path_to_optee_binary>/tee.bin The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/ls2088ardb/release/. For any update in the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled. To compile the FIP binary without OPTEE and without trusted board boot: make PLAT=ls2088ardb fip BOOT_MODE=sd BL33=<path_to_u-boot_binary>/u-boot.bin To compile the FIP binary with trusted board boot, refer the read me at <atf repository>/plat/nxp/README.TRUSTED_BOOT Step 5: Program TF-A binaries to QSPI NOR flash Boot LS2088ARDB from QSPI. Ensure that the switches and jumpers are set to boot the board from QSPI. For booting from QSPI: SW5[1:8] = 1111 1111 SW3[1:8] = 0011 0001 SW4[1:8] = 0011 1111 SW6[1:8] = 1111 1111 SW7[1:8] = 0100 1010 SW9[1:8] = 0100 0100 SW8[1:8] = 0111 1111 In addition to the above switch settings, make sure the following jumper settings are correct (for RDB Rev E and later).  J8 = 1-2 for QSPI boot, via onboard QSPI flash J8 = 2-3 for QSPI boot, via QSPI emulator J14 = 2-3, for QSPI boot For LS2088ARDB, in boot log, you'll see: Board: LS2088AE Rev1.1-RDB, Board Arch: V0, Board version: A, boot from vBank: 0 TF-A binaries can be loaded to LS2088ARDB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load TF-A binaries from the TFTP server Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@xgmii, DPMAC6@xgmii, DPMAC7@xgmii, DPMAC8@xgmii Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LS2088ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.                         => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> => setenv gatewayip <gateway addr> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@xgmii device host 192.168.1.1 is alive Load TF-A binaries from the TFTP server For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow. Program QSPI NOR flash: => sf probe 0:0 Flash bl2_qspi.pbl: => tftp 0xa0000000 bl2_qspi.pbl => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Flash fip.bin: => tftp 0xa0000000 fip.bin => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize Boot from QSPI NOR flash: => reset LS2088ARDB will boot with TF-A. In the boot log, you will see: => NOTICE: UDIMM 18ASF1G72AZ-2G3B1 NOTICE: 16 GB DDR4, 64-bit, CL=15, ECC on, 256B, CS0+CS1 NOTICE: UDIMM 18ASF1G72AZ-2G3B1 NOTICE: 4 GB DDR4, 32-bit, CL=11, ECC on, CS0+CS1 NOTICE: BL2: v1.5(release):LSDK-19.09 NOTICE: BL2: Built : 15:19:13, Nov 11 2019 NOTICE: BL31: v1.5(release):LSDK-19.09 NOTICE: BL31: Built : 15:21:14, Nov 11 2019 NOTICE: Welcome to LS2088 BL31 Phase U-Boot 2019.04 (Nov 11 2019 - 15:12:53 +0530) SoC: LS2088AE Rev1.1 (0x87090011) Clock Configuration: CPU0(A72):2000 MHz CPU1(A72):2000 MHz CPU2(A72):2000 MHz CPU3(A72):2000 MHz CPU4(A72):2000 MHz CPU5(A72):2000 MHz CPU6(A72):2000 MHz CPU7(A72):2000 MHz Bus: 800 MHz DDR: 2133.333 MT/s DP-DDR: 1600 MT/s Reset Configuration Word (RCW): 00000000: 503040c0 50500050 00000000 00000000 00000010: 00000000 00000000 00a00000 00000000 00000020: 01e01180 00002581 00000000 00000000 00000030: 00400c0b 00000000 00000000 00000000 00000040: 00000000 00000000 00000000 00000000 00000050: 00000000 00000000 00000000 00000000 00000060: 00000000 00000000 00027000 00000000 00000070: 412a0000 00040000 Model: Freescale Layerscape 2080a RDB Board Board: LS2088AE Rev1.1-RDB, Board Arch: V0, Board version: A, boot from vBank: 0 Option 2: Load image from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 If the ls command fails to run, check that U-Boot in QSPI NOR flash supports the command by typing ls at the U-Boot prompt: => ls ls - Lists files in a directory (default) Usage: ls <interface> [<dev[:part]> [directory]] - Lists files in directory [directory] of partition [part] on device type [interface] and instance [dev]. If U-Boot does not support this command, then update the composite firmware image in QSPI NOR flash. For steps to update composite firmware image in QSPI NOR flash, see Layerscape Software Development Kit User Guide . Use the following command if the SD card is formatted/created using LSDK flex-installer command: => load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: => load mmc 0:2 $load_addr bl2_qspi.pbl Use the following command if the SD card is formatted/created on a Windows PC: => fatload <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: => fatload mmc 0:2 $load_addr bl2_qspi.pbl Use the following command if the SD card is formatted/created on a Linux PC: => ext2load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: => ext2load mmc 0:2 $load_addr bl2_qspi.pbl Also note that LSDK flex-installer command puts the images on the IInd partition, so 0:2 is used in the load command. If the SD card is formatted on Windows PC or Linux PC for single partition only, then 0 should be used instead of 0:2 in the fatload/ext2load command. Load bl2_qspi.pbl image from the storage device => load mmc 0:2 0xa0000000 <image name> => print filesize For example: => load mmc 0:2 0xa0000000 bl2_qspi.pbl => print filesize filesize=14379 Or => load usb 0:2 0xa0000000 <image name> => print filesize Or => load scsi 0:2 0xa0000000 <image name> => print filesize Program bl2_qspi.pbl to QSPI NOR flash: => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Load fip.bin image from the storage device => load mmc 0:2 0xa0000000 <image name> => print filesize For example: => load mmc 0:2 0xa0000000 fip.bin => print filesize filesize=131510 Or => load usb 0:2 0xa0000000 <image name> => print filesize Or => load scsi 0:2 0xa0000000 <image name> => print filesize Program fip.bin to QSPI NOR flash: => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize Boot from QSPI NOR flash: => reset LS2088ARDB will boot with TF-A.
記事全体を表示
1. Debugging Packet Loss Issue 1.1 Frame Manager(FMan) Introduction 1.2 Frame Manager Buffer Manager Interface (BMI) Rx Port Statistics Counters 1.3 Linux Sysfs Support for Fman Rx Port Statistics 2. Queue Manager(Qman) Enqueue Rejections 2.1 Reasons for an Enqueue Rejection 2.2 Frame Queue Descriptor 2.3 Qman Debugfs 2.4 Buffer Manager (BMan) Debugfs
記事全体を表示