Bring up the LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bring up the LS1046A

Bring up the LS1046A

How to bring up a card when the flash is blank, or the image is corrupted. How to boot cards from various boot mode when changed the RCW as requirements. This documentation will use LS1046ARDB as new board to realize the functions (all target board in the document is LS1046ARDB).

Content

Bring up LS1046A with CodeWarrior TAP

Boot up from the SD card

Compile PBL binary from RCW source file

Compile the PBL binary into firmware

Program the firmware into the target board (LS1046ARDB)

Boot up from the QSPI

Compile firmware from RCW source file

Program the firmware into the target board (LS1046ARDB)

Boot up from the eMMC

Enable the on board eMMC

Compile firmware from RCW source file

Program the firmware into the target board (LS1046ARDB)

Labels (1)
Attachments
100% helpful (1/1)
Version history
Last update:
‎12-27-2022 09:40 PM
Updated by: